S12 / MagniVマイクロコントローラ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12 / MagniV Microcontrollers Knowledge Base

ラベル

ディスカッション

ソート順:
The S12Z MCU has linear address space therefore constant, variable, code placement is easier in compare with older S12 or S12X MCUs. But still, there are several ways and potential issues.   The object placement is made by Smart Linker. The linker configuration is defined by settings in project *.prm file and also by linker command line options (menu - Project – Properties – C/C++ Build – Settings – S12Z Linker). The detail information about linker options may be found in MCU_Build_Tools_Utilities.pdf with default path: "c:\Freescale\CW MCU v10.7\MCU\Help\PDF\MCU_Build_Tools_Utilities.pdf"   We may define memory segments in *.prm linker file. The default prm file contains segments for RAM, EEPROM, and ROM (Flash). The sizes of these segments typically reflect our MCU derivative physical memory map, but we may redefine that and use more virtual segments per our needs. The physical/virtual segments definition in prm linker file is located at: SEGMENTS // segments definition END‍‍‍‍‍‍   The general data placement may be divided into two main approaches: Manual – the programmer will specify fix address for some of the data Automatic – the placement will be driven automatically by Smart Linker   Manual placement The first option is an exact specification of specific content at a specific address. This may be managed for a small amount of data by FILL linker command in *.prm linker parameter file. For example: SEGMENTS //… ROM_CONST       = READ_ONLY   0xFE0000 TO 0xFE0000 FILL 0x5A;  //insert 0x5A value at address 0xFE0000 //… END‍‍‍‍‍‍‍‍‍‍ Such placement isn’t very comfortable, but it might be simply used for some configuration data out of project code. Note: you may use more than one bytes (e.g. FILL 0x0A 0x34). If segment size is bigger than a number of specified bytes, the bytes will be used as a pattern for filling whole target segment. Note: The potential linker placement will overlap such defined data.   The next option is using address specification by an @ qualifier directly in C code. For example: unsigned const int rom_const @0xFE0100 = 0x5AA5;‍‍ This may be used also for more complex types than simple byte – typically arrays,...   Since such type of placement is still manual, the linker parameters must be configured for avoiding possible overlapping. Be aware! The default CW project has disabled memory overlapping warnings. So, we must exclude target memory area from linker using. For example, in the *.prm file: SEGMENTS //… ROM_1           = READ_ONLY   0xFE0000 TO 0xFE00FF //ROM_CONST  = READ_ONLY   0xFE0100 TO 0xFE0101;            //we use the 0xFE0100 byte for rom_const ROM_2           = READ_ONLY   0xFE0102 TO 0xFFFDFF //… END‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Note: We use qualifiers for define memory access type. READ_ONLY is used for Flash, READ_WRITE for RAM and NO_INIT for RAM where we do not want to initialize data after reset. Sections placed in an NO_INIT segment should not contain any initialized variables (variable defined as int c = 8).   Note: The manual placement may be also implemented by assembler code. For example: XDEF MyVariable MyVariable: equ $1100‍‍‍‍ However, also in this case, we must exclude target memory area from linker use like in the case of @ qualifier for avoiding memory overlapping.   Automatic placement by linker The PLACEMENT block allows us to physically place each section from the application in a specific memory area (segment). The sections specified in a PLACEMENT block may be linker-predefined sections (like DEFAULT_ROM, DEFAULT_RAM, COPY, SSTACK,…) or user sections specified in one of the source file building the application (like MY_RAM,…). PLACEMENT // section(s) INTO segment(s); MY_CODE INTO ROM_1; END‍‍‍‍‍‍‍‍ Note: Since the linker is case sensitive, the name of the section names specified in the PLACEMENT block must be valid predefined or user-defined section names. Note: There is quite mess in ELF/Freescale section/segment terminology. Please take this information as simplified as possible. Please look at MCU_Build_Tools_Utilities.pdf for more details about predefined segments/sections. Note: We may place a various number of sections into a various number of segments. The “,” is used as section/segment delimiter. Note: In general, the placement order is given by simple list order (first specified section will be allocated from first specified segment, after that next section …). But, there are still few limitations for sections list order. The error is generated in the case of wrong list order – for example: ERROR L1122: only checksum section may be behind .copy in the section list.   The default variable/constant/code placement may be changed by #pragma commands. Note: Most of these pragma commands are not limited to the single file. Therefore, we should keep it in complementary pairs. An example of placing code into specific section: #pragma CODE_SEG MY_CODE void f(void) { //… } #pragma CODE_SEG DEFAULT‍‍‍‍‍‍‍‍‍‍‍‍ The #pragma DATA_SEG modifies variable placement. For example: #pragma DATA_SEG MY_RAM unsigned int counter; //… #pragma DATA_SEG DEFAULT‍‍‍‍‍‍‍‍   The #pragma CONT_SEG modifies variable placement. For example: #pragma CONT_SEG MY_ROM const unsigned int my_parameter; //… #pragma CONT_SEG DEFAULT‍‍‍‍‍‍‍‍   Note: The shorter option for directly allocating variables in a named segment, rather than using a #pragma may be used. For example: unsigned int counter@"MY_RAM";‍‍ However, even in such case, the #pragma command like #pragma DATA_SEG MY_RAM must be used at least once prior that variable declaration.   Note: The S12Z compiler/linker allows to use also already predefined sections like DEFAULT_ROM, DEFAULT_RAM or ROM_VAR as target sections in #pragma commands (not possible in the case of older S12(X) compiler/linker).     More details about #pragma commands may be found in MCU_S12Z_Compiler.pdf with default path: "c:\Freescale\CW MCU v10.7\MCU\Help\PDF\MCU_S12Z_Compiler.pdf" Data alignment Sometimes we need to keep allocated data aligned. This is for example typical requirement for ADC command and result list where DMA is used for transfer data between ADC module and memory. The simplest method is using alignment attribute. For example: volatile unsigned long adc0_cmdlist[NR_A_CH] __attribute__ ((aligned (4))); //max 256 bytes = 64 commands per 4-byte entries volatile unsigned int adc0_results[NR_A_CH] __attribute__ ((aligned (4)));  //max 128 bytes = 64 results per 2-byte entries‍‍‍‍ I hope it helps you. Best regards Radek
記事全体を表示
Since there isn't a CAN based bootloader developed for S12X device family, here are some useful documents that might be of help for creating such bootloader:   - The AN3312 is an application note of a BootLoader that uses CAN but it is targetted for our DSC family of devices. These devices have the FlexCAN module (the silicon that handles CAN Communications is different to the one in the MC9S08DZ60). However this document can be used as a reference on how to build a loader. https://www.nxp.com/docs/en/application-note/AN3312.pdf    - Following document explains how to use the msCAN module for communications. It provides basic examples on how to send and receive data through the port. https://www.nxp.com/docs/en/application-note/AN3034.pdf    - Next document provides the source code and documentation for an assembly-written Bootloader. This software loads the code through the serial port and burns it into flash. This document can help you understand the specific details of the bootloader implementation. This code is available for a lot of S08 families included the MC9S08DZ60 device. https://www.nxp.com/docs/en/application-note/AN2295.pdf  - Serial booloader for S12(X) family: https://www.nxp.com/docs/en/application-note/AN4258.pdf    With the information in these documents you can design your loader and plan how to solve the 5 main challenges of a loader application:   ++Memory Protection++ The Boot Loader handles the non-volatile memory of the microcontroller. The developer must plan how much memory is needed for the loader and protect it. Memory protection provides a guideline of the final system memory organization. A section of memory is used for the loader and another section for the application. Applications that will be executed with a loader are affected by how the loader manages memory and interrupt vectors.   ++Burning Flash++ Programming and Erasing non-volatile memory requires special attention as the procedure must be executed in RAM. The process of handling NVM may vary between devices. We have source code that provides routines to write Flash and that solves the problem of executing in RAM.   ++Vector Redirection+ Interrupt vectors should be shared between the application and the users code. Hardware vector redirection is supported by the microcontrollers but with some limitations. It is necessary to decide how vector redirection will be implemented. Software and hardware methods can be used to redirect vectors.   ++Data Interface++ Different applications required different interfaces to receive s-record information. Serial Ports are used widely for this purpose although the bootloader implementation should allow exchanging interfaces in a simple way. For your case you want CAN interface. CAN frames support up to 8 bytes of data per frame. This requires the developer to fully design a protocol or a data structure mounted over the CAN frames to be able to send the complete frames to the device that will be reprogrammed.   ++Mode Selection++ The Boot Loader is the owner of the reset vector. Upon startup the Boot Loader should select if the User code will be executed or if the Boot Loader mode should execute. The applicaton determines the best way to select between User/Loader mode. It might be a simple GPIO or a CAN frame or any input that can be recognized by the application and Loader to be able to set the loader mode when needed. Developing a loader is not easy, but hopefully this information will be of a great help.
記事全体を表示
Hello, Devkit-S12XE includes a bug on the PORT J2. This document shows the correct connection. The pin designation in the schematic, QSG, and pin markings on the board does not correspond to the connection on the board. Schematic: https://www.nxp.com/downloads/en/schematics/DEVKIT-S12XE-SCH.pdf  QSG: https://www.nxp.com/docs/en/quick-reference-guide/DEVKIT-S12XE-QSG.pdf  Pin markings on the board: In particular, these are the following pin numbers of PORT J2 where the bug was found: 16, 17, 18, 19 The real connection is as follows: I hope it helps, Best regards, Diana
記事全体を表示
How to get device ID and write program once field without programming application to the S12Z device in the CodeWarrior (Eclipse).   Even the datasheet does not present the device ID it can be read at address 0x1FC000. The device ID is size of 8 bytes from 1F_C000 to 1F_C007. The meaning of the field is confidential information. Of course, other "reserved" fields on higher addresses can also be read but their meaning is also confidential. The ID is not presented in the documentation because it has reason for company only. However, some users require unique identification of the device. It is possible to use this number. In order to read the ID, it is enough to create simple project in the CodeWarrior and connect to the device without programming it and run “mem” command in the debug shell window. If you do not want to remember address ranges, then it is better to prepare command file and execute it.   Of course, we can also simply use memory window.   It is a different story if we want also to see program once field. In this case we have to execute a set of commands to get it. As an example of command file which can be executed to get device ID and program the program once field I present two command files. They can be executed in the debugger window – see and test attached project. They are AAA_Read_Device_ID_And_OTPROM.cmd  and AAA_ProgramOnceField.cmd. The project which also presents reading and writing program once field is not relevant but should be created for the device we want to play with. It is not required to be code (simple code, enough to use what is generated by wizard) loaded into the MCU’s memory. However, necessary is the debugger is connected to a memory. Because of this it is enough to set:   …. And press debug   In the debug enable “Debugger Shell”:   Before continuing please modify flash clock setup in both files to value suitable for programming on the basis of the oscclk you use. In the files search for lines    Write into debugger shell command which runs the AAA_Read_Device_ID_And_OTPROM.cmd: source "c:\D\CODING & SW\ECLIPSE\S12ZVMC-FLASH-WRITEONCEFIELD-CW106\AAA_Read_Device_ID_And_OTPROM.cmd" (it is possible you have different path to the file…please change it)   The command will execute and shows: Device ID And Program field phrase 0. If you want to see another phrase you should modify AAA_Read_Device_ID_And_OTPROM.cmd line set PHRASE 1. Change 1 to the phrase you want to see and run the command presented above “source …..” again. It is enough to press arrow up on the keyboard to see and use previous commands.   In order to program selected field use and run command “source” with the file: AAA_ProgramOnceField.cmd source "c:\D\CODING & SW\ECLIPSE\S12ZVMC-FLASH-WRITEONCEFIELD-CW106\AAA_ProgramOnceField.cmd"   The same note as previosly, the path you have could be different so adjust it. The same line as in previous file should be changed to select the phrase you want to program. As a result, you will see programming algorithm and also read back of the field, example of output: %>source "c:\D\CODING & SW\ECLIPSE\S12ZVMC-FLASH-WRITEONC EFIELD-CW106\AAA_ProgramOnceField .cmd" ############################ Programming Field = 2 ############################ cmdwin::mem 0x0386 %x = 0x30 cmdwin::wait 1000 cmdwin::mem 0x0382 %x = 0x05 cmdwin::mem 0x038C %x = 0x07 cmdwin::mem 0x038D %x = 0x00 cmdwin::mem 0x038E %x = 0x00 cmdwin::mem 0x038F %x = 2 cmdwin::mem 0x0390 %x = 0xA2 cmdwin::mem 0x0391 %x = 0xB2 cmdwin::mem 0x0392 %x = 0xC2 cmdwin::mem 0x0393 %x = 0xD2 cmdwin::mem 0x0394 %x = 0xE2 cmdwin::mem 0x0395 %x = 0xF2 cmdwin::mem 0x0396 %x = 0xA3 cmdwin::mem 0x0397 %x = 0xB3 cmdwin::mem 0x0386 %x = 0x80 cmdwin::wait 1000 ############################ Read back Programmed Field = 2 ############################ cmdwin::mem 0x0386 %x = 0x30 cmdwin::wait 1000 cmdwin::mem 0x0382 %x = 0x01 cmdwin::mem 0x038C %x = 0x04 cmdwin::mem 0x038D %x = 0x00 cmdwin::mem 0x038E %x = 0x00 cmdwin::mem 0x038F %x = 2 cmdwin::mem 0x0386 %x = 0x80 cmdwin::wait 1000 cmdwin::mem 0x0390 8      390  $a2 $b2 $c2 $d2 $e2 $f2  $a3 $b3   . . . . . . . .    Now the question, where to find commands to be able to prepare such a command files, can be asked. 1) The first information source is the CodeWarrior help. For example, search for keyword DW and it could find a command list. 2) Tcl Reference Manual  3) http://www.tcl.tk/    Finally, in the attached project can be seen also approach how to write program once field by SW. Of course, mentioned cmd files are also part of the project.
記事全体を表示
This example shows a few possible configurations of the S12PWM8B8CV2 PWM module. Five PWM channels are configured with different clock source, polarity, alignment, period and duty-cycle.   Four clock sources (A, B, SA, SB) are derived from bus clock using dividers.   Selected polarity of PWM channel determines the duty-cycle whereas the alignment determines the period of the PWM signal.   Four 8-bit channels (4-5, 6-7) are concatenated into two 16-bit channels. Channels 4 and 6 become high-order channels while channels 5 and 7 become low-order channels. These low-order channels (5 and 7) are the output channels routed to a port  and they configure the clock, polarity, alignment and enablement of the PWM signal.  Period and duty-cycle of the signal are configured with both the low-order and high-order channels.   The period registers (PWMPERx) and the duty-cycle registers (PWMDTYx) are double buffered. When they are rewritten while the channel is enabled, the change will not take effect until one of the following occurs: 1. The effective period ends 2. Counter resets 3. The channel is disabled
記事全体を表示
Interrupt catcher example code catches all unexpected interrupts. It can be used for debugging or directly in the application software. The Machine Exception routine is used here as example of expected interrupt.   A few notes: 1. For each expected interrupt you must remove a code line for given interrupt     from the part of the code "A Set of unimplemented interrupts" and     create your own service routine as it is, for example, made     for interrupt 5 void Machine_Exception_ISR(void)   2. All interrupt vectors have 32bit size, however, addresses have only 24bit,     therefore the most significant byte in interrupt vector is not used.     Definitions with the keyword "interrupt XX" where XX represents vector     order in the interrupt vector is used to define interrupt service function.      3. Interrupt number 0 is assigned to POR reset vector,                      1 is assigned to Unimplemented page1 op-code trap vector                      2 is assigned to Unimplemented page2 op-code trap vector                      3  ...                      4  ...     Interrupt number = (0x1FC-Vector Address)/4. See Table 1-11. Interrupt     Vector Locations at RM(page 62-65).     For Example: Interrupt number of SCI0 = (0x1FC-0x19C)/4 = 0x18 = 24.     So you can use either form                interrupt VectorNumber_Vsci0 void SCI0_isr(void)     or                interrupt 24 void SCI0_isr(void)     or                interrupt ((0x1FC-0x19C)/4) void SCI0_isr(void)       Note: VectorNumber_Vsci0 is defined in mc9s12zvl32.h      
記事全体を表示
A project presents control of the HD44780 driven display where it is assumed that RW pin of the LCD is permanently connected to “Write” level (GND). The SW contains mirror(s) of the LCD display as array of characters stored within RAM. Both read and write function can be used because writing is performed to the display and also to the array. Read functions are directed to the character array stored within RAM.
記事全体を表示
Customers are sometimes asking for reference schematics, so here is a batch of minimal configurations for main representatives of S12(X) family. Attached is also document that should answer most common questions. Hope this will help. Lukas
記事全体を表示
S12 FAMILY DEVICES COP RECOGNITION CONSIDERATIONS SHOULD HELP YOU TO SET HW OF THE RESET PIN TO BE COP CORRECTLY RECOGNIZED The calculator can be found at S12 FAMILY DEVICES COP RECOGNITION CONSIDERATIONS - calculator.xlsx
記事全体を表示
The example demonstrates the COP watchdog reset on MC9S12ZVL32 microcontroller. The code can be used on any MagniV device based on S12Z core. The example project is created in CodeWarrior v10.6 (Eclipse IDE). The SW code has been tested on TRK-S12ZVL board.   * Brief description: The Phase Locked Loop (PLL) is set by default to PEI mode, so the bus clock is 6.25MHz based on 1MHz internal RC oscillator (IRC1M). The RGB LED (red) is used to indicate MCU runs after reset. When the RGB colour changes to green, the COP time-out period has started. After the period times out, the COP generates a reset and COPRF flag is set. After the reset, based on COPRF flag, the Blue LED is turned on indicating previous reset has been generated by COP watchdog. The COP time-out period is set to maximum (CPMUCOP register, bits CR[2:0]=7). The number of COPCLK cycles to time-out is 2^24 = 16777216. The COPCLK is based on IRCCLK (by default) with 1MHz clock frequency. The maximum COP time-out period in this case is approximately 16.78 seconds. - On the TRK-S12ZVL board:   Port P is used to drive RGB LED. Anode is connected to VDDX, a cathode to port  pin. Port P can be set as output (DDRP=0xFF) and logic zero on output enables LED.   - Reference documentation: MC9S12ZVL Family Reference Manual & Datasheet TRK-S12ZVL Board schematics
記事全体を表示
The ADC measurement is always relative – relative to your voltage reference. The most of the applications don't allow to use accurate and expensive voltage reference. In that case, VDDA is used as the reference for ADC measurement. Since the operational VSUP range starts from 3.5V and accuracy of the voltage regulator is limited, we should use internal bandgap reference for compensating ADC voltage results. The bandgap voltage VBG has a narrow variation over temperature and external voltage supply. The example shows how to compensate ADC results by additional bandgap voltage measurement.
記事全体を表示
Here is the example code demonstrating erase/write/read of internal EEPROM module integrated into MagniV devices such as S12ZVM, S12ZVC, S12ZVL etc.   Find detailed description in the project's main.c file.   The example project was created in CodeWarrior IDE v10.6.4 and tested on TRK-S12ZVL board.
記事全体を表示
CAN Standard ID, CAN Extended ID memories refreshment   A human is a creature forgetting things, procedures and a lot of useful principles in a very short time especially when it often jumps between different projects. I also solve the CAN interface filter setup issues occasionally and even I did it a lot of times I always have to think how to set the filter easily and fast. Because of this, on the basis of last experience, I created an excel sheet this year which provides me an easy return to my CAN filter memories. I am not sure it will be helpful for everyone as it is helpful for me, however, I am sharing..... Each of us has different thinking and ways of visualization so any idea for improvement is appreciated in advance.      
記事全体を表示
Hello everyone, In this post you are going to find the example codes that where mentioned during the "Learning to Easily Develop LIN-based Actuator Applications with Mixed-signal MCUs" webinar. In the "S12ZVMA_Webinar_ExampleCodes" package you are going to find the code for the S12ZVMA slave node, the code for the S12ZVL master node and the LIN configuration files (LDF and NPF's files).   SETUP CONFIGURATION: In the images below you can find the information you need to know to create the setup and get running your LIN network and the DC motor.   Note: Remember that in this code we are using the active configuration where the High Side Driver and the Low Side Driver are being used to control de motor.   Steps: Place jumper J21 in the position [3-2]. With this step, we are connecting the PHASE_A_HS with the PHASE_A_LS to get the active configuration. Connect one line of your DC motor to J30 (connect it in pin 2 or 3, do not use pin 1) and the other line to any GND point of your S12ZVMAEVB. Connect the master and the slave nodes using J6 jumper.     Best Regards, Atzel Collazo
記事全体を表示
This document includes in attachment excel file calculation that might be useful for those using the S12 MagniV for motor control and proper PLL setting in their projects.   Following parameters can be set and reused for different scenarios via attached excel sheet calculation for the S12 MagniV BLDC motor control applications: #define CPMU_REFDIV // PLL setting of ref. divider #define CPMU_SYNDIV // PLL setting of multiplier #define CPMU_POSTDIV // PLL setting of the post divider #define CPMU_REFFRQ // PLL setting of ref. frequency #define CPMU_VCOFRQ // PLL setting of VCO frequency #define ADC_TIM // setting of ADC timer #define MIN_ADC_TRIGGER_FIRST // setting of ADC trigger #define MIN_ADC_TRIGGER_SECOND // setting of ADC trigger #define PWM_MODULO // PMF module config. #define PWM_DEADTIME // PMF module config. #define TIM_PRESCALER // Timer prescaler #define TIMER_1MS // Setting of timer #define SCI_BAUDRATE // setting of SCI baud rate   This is how it can look for setting either internal or external clock: // PLL settings /* /* // Internal clock 1MHz, 100/50 MHz CPU/Bus clock, 8.33 MHz ADC clock #define _INTERNAL_CLOCK                        // 1 MHz internal clock is used #define    CPMU_REFDIV        0 #define    CPMU_SYNDIV        49 #define    CPMU_POSTDIV       0 #define    CPMU_REFFRQ        0 #define    CPMU_VCOFRQ        3 #define    ADC_TIM            2 #define    MIN_ADC_TRIGGER_FIRST     24 #define    MIN_ADC_TRIGGER_SECOND    144 #define    PWM_MODULO                5000 #define    PWM_DEADTIME              50 #define    TIM_PRESCALER      6         // Timer prescaler 64; 50 MHz/64 = 1.28 us #define    TIMER_1MS          781 #define    SCI_BAUDRATE       5208 */  // External clock 4MHz, 25/12.5 MHz CPU/Bus clock, 6.25 MHz ADC clock #define _EXTERNAL_CLOCK #define    CPMU_REFDIV        3 #define    CPMU_SYNDIV        24 #define    CPMU_POSTDIV       1 #define    CPMU_REFFRQ        0 #define    CPMU_VCOFRQ        1 #define    ADC_TIM            0 #define    MIN_ADC_TRIGGER_FIRST     8 #define    MIN_ADC_TRIGGER_SECOND    48 #define    PWM_MODULO                1250 #define    PWM_DEADTIME       13 #define    TIM_PRESCALER      4         // Timer prescaler 16; 12.5MHz/16 = 1.28 us #define    TIMER_1MS          781 #define    SCI_BAUDRATE       1302     It is used in following function for Clock, Reset and Power Management Unit configuration: //Clock, Reset and Power Management Unit configuration //* //*****************************************************************************/ void initCPMU(void) {     // Wait for stable supply after power up     while (GDUF_GLVLSF)         GDUF_GLVLSF = 1;      CPMUREFDIV_REFDIV = CPMU_REFDIV;     CPMUREFDIV_REFFRQ = CPMU_REFFRQ;     CPMUSYNR_SYNDIV = CPMU_SYNDIV;     CPMUSYNR_VCOFRQ = CPMU_VCOFRQ;     CPMUPOSTDIV_POSTDIV = CPMU_POSTDIV;  #ifdef _EXTERNAL_CLOCK     CPMUOSC_OSCE = 1;     while (CPMUIFLG_UPOSC == 0) {}; // Wait for oscillator to start up (UPOSC=1) and PLL to lock (LOCK=1) #endif      while (CPMUIFLG_LOCK == 0) {};     CPMURFLG  = 0x60;     //Clear PORF and LVRF }          Or setting of ADC clock for both ADC modules in ADC module configuration function:   //ADC0CTL_1 = 0;        ADC0TIM = ADC_TIM;          // clock: clk = fbus / (2x(reg.value + 1)) [0.25 - 8MHz]        //ADC1CTL_1 = 0;        ADC1TIM = ADC_TIM;          // clock: clk = fbus / (2x(reg.value + 1)) [0.25 - 8MHz]        All the rest of the corresponding registers settings can be found in the example for the BLDC motor control of 3-pase sensorless BLDC development kit with S12 MagniV in section download: MTRCKTSBNZVM128_SW: Complete motor control application software package for MTRCKTSBNZVM128
記事全体を表示
Here is the example code demonstrating erase/write/read of internal Flash module integrated into MagniV devices such as S12ZVM, S12ZVC, S12ZVL etc.   Find detailed description in the project's main.c file.   The example project was created in CodeWarrior IDE v10.6.4 and tested on TRK-S12ZVL board.
記事全体を表示
The package contains of AN5327_SW ported to S12ZVML-MINIBRD hardware. Just minor changes are introduced, such as removing a button control, moving the LED light to another pin and using internal oscillator. This is just a working version, it is NOT an official release!!! AN5327_SW_CW11_MINIBRD.ZIP CodeWarrior 11.0 and AMMCLib 1.1.13 or higher is required to run this example. If you are not sure about the AMMCLib version, please download the general AN5327_SW from the www.nxp.com/automcdevkits first, install it and then unzip and use the example above.
記事全体を表示
This example simulates ECC issue by cumulative write into the same EEPROM area without an erasing.   The EEPROM erase operation set all bits into log1. The EEPROM program operation may keep bit cells in log1 state or change it into log0 state, but not in opposite way.   The S12Z MCU EEPROM is protected by 22-Bit ECC Scheme. Every word (16bits) is protected by additional 6 bits with ECC checksum. The ECC values are not accessible for users. Every EEPROM reading triggers also ECC check by internal logic. The single bit error in user data may be corrected by ECC checksum. The double bit error cannot be corrected.   The ECC protection is implemented also at flash controller commands and results are signalling by MGSTAT bits.   The first case simulates Single-bit ECC error during reading. The MGSTAT bits after the second write are 0b10 due to fact that just 1 bit is different during write verification (correctable error)   The second case simulates Single-bit ECC error during reading. The MGSTAT bits after the second write are 0b11 due to fact that more than 1 bits are different during write verification (non-correctable error)   The third case simulates Double-bit ECC error during reading. The MGSTAT bits after the second write are 0b11 due to fact that more than 1 bits are different during write verification (non-correctable error)       The EEPROM patterns are selected for highlighted described behavior and they don't have any real meaning.   The cumulative write is not allowed for normal operation!!! The code from this example should be used only for design testing - not in production!!!   Please, see the prm file. Address range 0x100000-0x100001 is excluded from default EEPROM and is used as user EEPROM memory The size of EEPROM sectors is 2 bytes. The EEPROM_Program() function may program up to 4 words in single flash command.   Note: The EEPROM_Program() function was updated - erase verification is skipped     I hope it helps you. Radek
記事全体を表示
CAN setup calculator for S12(X) and MagniV devices.   I would like to share my CAN setup calculator I've been using for a few years. I’ll be glad if anyone who sees any discrepancy in calculation or values would contact me with comment or idea for improvement. Even I think the sheet is intuitive I’ll provide a few notes. 1) Entering input values a) fosc – defines frequency of input clocks for CAN peripheral. It can be either oscillator clock or bus clock in dependence what is used in application. Note: Because of CAN clock requirements I suggest to use oscillator clock as a source clock for CAN peripheral to meet oscillator precision parameter. The recommendation is based on the fact of that the PLL is usually used for bus clock generation and the PLL unlock parameter is usually out of clock specification. Especially un-lock parameter which can be observed and processed by PLL lock interrupt. Only for example, S12ZVC defines:   b) Physical Interface Tx+ Rx propagation delay – The parameter can be calculated from the data presented in the data sheet for given CAN transceiver. A few values are presented in the top of the sheet.   c) Required sample point - A good general rule is to set the sample point above 80%. Based on the experiences of the automotive industry, the selected sample point should be near the 80% value.   2) Output values   The results field show calculations for all combinations. The simplification, I use, is the max SJW is always used.   Lines containing correct values for bitrate setup are highlighted with orange color. The only thing which is not checked is sample point. You should check calculated “Sample point calculated” whether it corresponds to your requirements. There are two correct values of CANBTR0 and CANBTR1 for required bitrate but the bottom orange line meets exactly our requirement for sample point.
記事全体を表示
Work with pushbuttons and 7 segment display. Write assembly (ASM) and C programs for the HCS12, as well as to work with the pushbuttons and 7-segment display on the Dragon12-JR board.  The programs find the largest and smallest numbers from an arbitrary list of eight 8-bit unsigned numbers and displays them on the 7-segment display as outlined in the following.   1. Write a program to do the following, in both ASM and C. Do not use MINA, MINM, MAXA, and MAXM instructions.            a. Load an array of eight 8-bit unsigned numbers into RAM.            b. Find the largest of these numbers and store it.            c. Find the smallest of these numbers and store it.            d. Wait for the pushbuttons (S1 or S2) to be pressed.            e. The first time S1 is pressed, display the high nibble of the largest number; the second time S1 is pressed, display the low nibble of the largest number.                For example, if the largest number is 0x3F, the 7-segment display should show “3” the first time S1 is pressed and “F” the second time it is pressed.            f. Do the same for S2, except use the smallest number.  2. Explain why debouncing is used with switches. Optional: Implement software debouncing for switch used above.   Hints: These are unsigned numbers that your program will be searching through.  Make sure you are using the unsigned branch instructions in your ASM code. Your TA will be changing the numbers in your array to make sure it works for arbitrary 8-bit values. Please make sure the array is somewhere near the top of your program file. For interfacing to LEDs, 7 segment Displays, and pushbuttons see the schematic and manual of your development board. The type of the 7-segment LED on the Dragon12-JR board is common anode. All cathodes are driven individually by an output port and all anodes are internally connected together. The Dragon12-JR board uses port H to drive 7-segment cathodes. Skeleton files are provided to help you complete the asseignment. The 7-segment display communicates with the board via Port H whose address is $0260 (PTH).  Its data direction (input or output) is controlled by writing to Data Direction H register whose address is $0262 (DDRH). In order for PTH to be output (i.e. displaying something), you must set DDRH to $FF first (all bits high, all bits output).  The skeleton code does this for you this time. Almost every I/O port on the board works similarly to PTH; that is, you must set the direction of data on a corresponding data direction register before writing to or reading from it. The two pushbuttons (S1 and S2) are connected to PM6 and PM7. S1à PM6, S2à PM7 A subroutine that displays the low nibble of register A is included with the skeleton ASM code. Just store a value in register A and issue jsr seg7_out to display the low nibble of A. You are required to understand how it works and to write a similar routine for the C version of your code.   This document was generated from the following discussion: Professional Way to solve this HCS12 Dragon12-JR,Work with pushbottons and 7 segment display
記事全体を表示