A Library of Functions for HD44780 Based LCD Modules (no R/W) for S12Z devices

cancel
Showing results for 
Search instead for 
Did you mean: 

A Library of Functions for HD44780 Based LCD Modules (no R/W) for S12Z devices

No ratings

A Library of Functions for HD44780 Based LCD Modules (no R/W) for S12Z devices

A project presents control of the HD44780 driven display where it is assumed that RW pin of the LCD is permanently connected to “Write” level (GND). The SW contains mirror(s) of the LCD display as array of characters stored within RAM.

Both read and write function can be used because writing is performed to the display and also to the array. Read functions are directed to the character array stored within RAM.

Labels (1)
Attachments
Comments

This is another library which can be used: Tutorial: HD44780 Display Driver with NXP MCUXpresso SDK | MCU on Eclipse 

It supports 4bit and 8bit data bus with and without read/write.

Erich

Version history
Revision #:
1 of 1
Last update:
‎09-24-2016 09:46 AM
Updated by: