NXP Tech Blog - 8ページ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Tech Blog - 8ページ

omar_cruz
NXP Employee
NXP Employee

Focusing on low-power and fast wake up times, the K32 L2 MCU family – based on the Arm® Cortex®-M0+ - targets power-conscious end nodes and can enable a wide range of general purpose industrial and IoT applications. Today, the K32 L2 MCU family is being brought to market in a scalable set of packages, core performance and memory configurations, from 64KB to 512KB flash, and backed by unmatched enablement, led by NXP’s complementary suite of MCUXpresso software and tools with example projects utilizing IAR, Keil, and GCC based toolchains.

詳細を読む...

件数が多いもの
0 0 2,075
monicavelez
NXP Employee
NXP Employee

Innovation means being first. And with more than 20 years of firsts, NXP’s MCU portfolio has grown into a powerhouse of more than 200 Arm®-based MCU families scaling from low-power Cortex®-M0+ to high performance Cortex®-M7 crossover MCUs.

詳細を読む...

件数が多いもの
2 0 2,353
lpcxpresso_supp
NXP Employee
NXP Employee

MCUXpresso IDE is currently supported on macOS 10.12 to 10.14.

In macOS 10.15 (Catalina), Apple have introduced a new additional "signing" mechanism for software that is download outside of the Apple App Store, know as "Notarization". Currently MCUXpresso IDE for macOS is signed using NXP's Apple Developer ID, but has not yet gone through Apple's notarization process. This means that by default you will not be able to install if you are running macOS 10.15.

詳細を読む...

件数が多いもの
0 0 3,565
iWave
Contributor V

Have you ever checked your smartphone or your IoT device and received an alert for software updates? All you have to do is to simply accept the update when you have the network connectivity and the rest will be taken care of automatically by the software. Isn’t it simply amazing to be able to refresh your device, no matter where you are in the world? This update process is widely known as OTA (over the air).

OTA is a technology that manages software and lets you wirelessly upgrade the operating system/files of your platform.

詳細を読む...

件数が多いもの
0 0 2,347
lpcxpresso_supp
NXP Employee
NXP Employee

As part of the MCUXpresso IDE v11.0.1 release, we had to make some major changes to our LinkServer debugging mechanism to support the latest silicon revision of the LPC55xx family of devices (revision 1B) and the more secure debug request mechanism required by these parts. Such silicon is supplied on LPC55S69-EVK boards marked Revision A2 (or later) on the board silkscreen.

詳細を読む...

件数が多いもの
0 0 2,957
iWave
Contributor V

iWave systems recently launched a new SMARC System on Module (SOM) based on the powerful NXP® i.MX 8QuadMax applications processors. This high performance SOM features an intelligent blend of MPUs+MCU power in a single device and integrates heterogeneous multicore 64 bit ARM® processors (Dual Cortex® A72@ 1.8 GHz + Quad Cortex® A53 @ 1.2 GHz and Dual Cortex® -M4F @ 266 MHz), targeted for applications that demand advanced real-time processing, multi-media performance as well as in applications that requires simultaneous multi-OS operations. For more details refer to the link: i.MX8 QuadMax NXP SMARC SOM

詳細を読む...

件数が多いもの
0 0 3,455
Kathleen
NXP Employee
NXP Employee

Today I conclude my countdown of top reasons to use i.MX RT1010, and I wanted to end the blog series in the same way that it began – by talking about how to get started. It is has been  2 weeks since my first post, so hopefully by now you have found the $10.10 in your couch cushion to order your i.MX RT1010 EVK. Maybe you even already have the EVK on your desk and followed the instructions on the Getting Started webpage which leads you to download the software and tools. But what is MCUXpresso and how much does it cost?

詳細を読む...

件数が多いもの
0 0 2,127
Kathleen
NXP Employee
NXP Employee

Listen up everyone. We are winding down the countdown and my blog today is about audio. Many consumer products and embedded devices support various digital audio functions, and more and more engineers are looking for the MCU to support these functions, rather than needing to add a DSP or other dedicated solution.  The good news is that many MCUs now have the capabilities to support these basic audio tasks. But how do you choose an MCU that will give your product the price, performance, and design flexibility you need?

詳細を読む...

件数が多いもの
0 0 2,203
Kathleen
NXP Employee
NXP Employee

So you want to add a display to your product? You look at the i.MX RT series table and see that the i.MX RT1010 device does not have an LCD interface, so you immediately write it off. Not so fast!  Did you know that you can add a display to your i.MX RT1010 design through the I2C module? What’s great about the i.MX RT1010 is that we didn’t skimp on peripherals to hit that $1 price point. Even the pin muxing takes into account maximum usability for a variety of applications. But say you are working on a thermostat application and need the I2C module to connect to a variety of sensors instead. Based on yesterday’s blog, hopefully you immediately think of the FlexIO module.

詳細を読む...

件数が多いもの
1 0 2,315
Kathleen
NXP Employee
NXP Employee

Say for example, you are working on your industrial application using the i.MX RT1010 MCU and have everything designed out. You are using two UARTs for sensor interfaces, one UART for camera, and the fourth UART will be used for development and future debug. Then, your product marketer comes by and asks you to add Bluetooth to the product.


What can you do?  The i.MX RT1010 only supports 4 UARTs. Do you move to an i.MX RT1050 MCU since it has 8 UARTs? Do you add another external UART to your design?


Don’t fret! FlexIO to the rescue!

詳細を読む...

件数が多いもの
0 0 1,974
Kathleen
NXP Employee
NXP Employee

All engineers – and most anyone – love to make things spin, right? That explains the revenue made on those fidget spinners. The inventor is a genius! OK ok … now back to MCUs … the i.MX RT MCU motor control demos are some of the most highly viewed demos. So what makes the i.MX RT1010 device ideal for motor control applications? Is it the FlexPWM? The ADC? Or just the raw performance of this 500 MHz MCU? The answer – all of the above.  The i.MX RT1010 MCU is an ideal solution for a single motor and here’s why

詳細を読む...

件数が多いもの
0 1 3,314
vishakhadakhane
Contributor III

Hello, recently I have done Periph Blinky e.g. from LPCOpen library on MCUxpresso. I am using LPC1769 chip and I have toggled GPIO pin. In my case I have used buzzer pin i.e. Port 3 & Pin 25. Instead of using Timer delay I created a delay function i.e. void delay_ms(unsigned int ms). Here I am attaching the systick.c file. Hope it helpsSmiley Happy!!  

詳細を読む...

件数が多いもの
0 0 1,989
Kathleen
NXP Employee
NXP Employee

On what could be perceived as a low-cost MCU, it is nice to see that security was not compromised on the i.MX RT1010 device. In fact, the i.MX RT1010 MCU has the same security block that exists on many of the other i.MX RT products.

詳細を読む...

件数が多いもの
0 0 1,652
Kathleen
NXP Employee
NXP Employee

For today's blog, I am going to keep it short and direct it to the PCB layout engineers out there.  The i.MX RT1010 MCU designers want you to know that the utmost care was taken when designing the i.MX RT1010 device. Even if your company typically prioritizes product requirements over package requirements, NXP has you covered. During our package development, we do a number of pin-out iterations and a fanout exercise to make sure that the i.MX RT LQFP packages are easily laid out for 2-layer through-hole PCBs. 

詳細を読む...

件数が多いもの
0 0 1,527
Kathleen
NXP Employee
NXP Employee

Continuing with my countdown of top reasons to use i.MX RT1010 crossover MCU, today I want to talk about performance.  The performance of the i.MX RT series really pushes this portfolio to a classification of its own – crossover MCUs. Engineers can now enjoy the level of performance historically seen in the processor space, now in the MCU world – providing tremendous familiarity and usability for engineers. But just ask the rabbit from the Tortoise and the Hare fable, sometimes it is not enough just to be fast. You have to be smart too. Within the i.MX RT1010 family, several smart features are coupled together with the 500 MHz Arm® Cortex®-M7 core.

詳細を読む...

件数が多いもの
0 0 2,245
vishakhadakhane
Contributor III

Hello everyone, I am working on MCUxpresso and using LPC1769 controller. I am done with Led blinking in MCUxpresso. I have used flash magic to flash the hex file in controller using usb to ttl. But I faced a hex file issue while doing this project. So I thought I should share this with everyone who are facing the same issue. After compiling only .axf was getting created. For creating .hex file ,you need to do following settings

詳細を読む...

件数が多いもの
1 1 10.5K
Kathleen
NXP Employee
NXP Employee

Continuing with my 10-day countdown to top reasons to consider the i.MX RT1010, today we look at reason #9 -the unlimited memory capabilities of the i.MX RT1010.

Looking at the i.MX RT1010 crossover MCU, one might notice that there is no on-chip Flash memory. Where do you boot from? Where do you store your code? And is it safe? What about latency issues? The i.MX RT1010 MCU was designed to ensure maximum memory flexibility, while not sacrificing performance or security.

詳細を読む...

件数が多いもの
0 0 1,850
Kathleen
NXP Employee
NXP Employee

As explained in my blog yesterday, for the next 10 days, I will countdown 10 top reasons to consider the i.MX RT1010 for your next design.  Today we start with reason #10 -the EVK.  Since the first i.MX RT crossover MCU first launched in 2017, the EVK has been the board of choice for developers. Right-sized with the right level of features and capabilities

詳細を読む...

件数が多いもの
0 0 1,947
iWave
Contributor V

iWave Systems, a leading embedded solutions provider company based in Bangalore has successfully demonstrated Xen virtualization hypervisor on their i.MX8 QM SoC based System on Module. The  multi-core SOM comprises of 2x Arm® Cortex® -A72 @1.8 GHz and 4x Arm® Cortex®-A53 @1.2 GHz and 2x additional Cortex®-M4F @ 266 MHz, rendering a highly powerful  integrated solution on a SMARC R2.0 compatible module.

詳細を読む...

件数が多いもの
0 0 4,348
Kathleen
NXP Employee
NXP Employee

Though not widely publicized, the $1 price point of the newly announced i.MX RT1010 crossover MCU made me pause. My parents always told me that a dollar is not what it used to be, meaning that the value of a dollar today does not go nearly as far as it used to for them when they were growing up.

詳細を読む...

件数が多いもの
1 0 2,157
omar_cruz
NXP Employee
NXP Employee

Searching for a low-power, well-integrated but cost-sensitive MCU for your embedded designs? Look no further – the K32 L2 MCU family is for you!

詳細を読む...

件数が多いもの
1 0 32.7K
martinformanek-
NXP Employee
NXP Employee

Dear MCUXpresso user,

 

We have decided to remove “Configurations” page from MCUXpresso SDK Builder website (http://mcuxpresso.nxp.com) with the December update this year.

Details are summarized below about the existing Configurations page and how page’s functionality will replaced.

詳細を読む...

件数が多いもの
1 0 3,485
lpcxpresso_supp
NXP Employee
NXP Employee

An issue has been identified that impacts the debugging of older LPC devices using SEGGER Jlink via the version of MCUXpresso IDE v11.0.1 released on 4th September 2019.

This issue will be seen only when debugging an LPC device that use the IDE's Preinstalled part support i.e. parts that do not require an SDK - a debug operation via SEGGER Jlink will lead to an error as below:

詳細を読む...

件数が多いもの
2 0 12.9K
lpcxpresso_supp
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso IDE v11.0.1 (build 2563) is now available.

This is a maintenance release that builds upon the previous MCUXpresso IDE v11.0.0 release, and we recommend that all existing users download and install this new version. It also incorporates a minor update to the integrated MCUXpresso Config Tools.

詳細を読む...

件数が多いもの
0 0 4,828
KATE_WANG
NXP Employee
NXP Employee

Dear sdk developers,

During our development, more and more components are joining our sdk. It is necessary for the component sections recorded in yml data to follow a simple and effective naming convention, so that they can be well organized, identified and processed.

Here we provide the doc of Yml Data Record Component Naming Conventions, please kindly review and follow the rules in your future development.

詳細を読む...

件数が多いもの
0 0 1,538
raluca_popa
NXP Employee
NXP Employee

This tutorial demonstrates how to convert a Tensorflow model to TensorFlow Lite using post training quantization and run the inference on an i.MX8 board using the eIQ™ ML Software Development Environment. It uses a TensorFlow mobilenet_v1 model pre-trained with ImageNet.

NOTES:

1. Except for the section "Build Custom Application to Run the Inference" this tutorial can also be applied to any i.MX RT platform.

2. For more information on quantization check the 'QuantizationOverview.pdf' attached to this post.

詳細を読む...

件数が多いもの
6 0 7,992
lpcxpresso_supp
NXP Employee
NXP Employee

The Windows installer for SEGGER J-Link has changed behaviour for version after V6.44 i.e. after the version installed with V11.0.0 of the IDE. Previously each SEGGER installation was located in a versioned directory e.g. JLink_V644g, now each new installation will by default, write to C:\Program Files (x86)\SEGGER\JLink.

This change will only impact Windows users who manually install a later version of SEGGER J-Link for use within MCUXpresso IDE.

詳細を読む...

件数が多いもの
2 0 5,384
kuruibonny
Contributor III

I think this might be late since I was using Ubuntu 18.04 until recently when I upgraded to latest version 19.04

Tried to install Mcuxpresso IDE I encountered some dependency errors but managed to solved it. I had already replied to question about it but decided #to write main post about it.

詳細を読む...

件数が多いもの
0 0 5,111
CJarvis
NXP Employee
NXP Employee

In March of 2017, NXP released the debut version of the MCUXpresso SDK along with an IDE and set of Config Tools under the same MCUXpresso name.  Since that time we have seen an amazing response from developers downloading and using this suite of software and tools.  The number of MCUXpresso SDK downloads recently surpassed 100,000 unique downloads.

As the NXP and former Freescale microcontrollers were unified under one company, we knew we needed to provide a consistent and efficient software development platform – one that would allow you  the flexibility to develop on a wide range on NXP microcontrollers without the need to relearn a new software architecture or re-invent basic enablement functionality.

詳細を読む...

件数が多いもの
0 0 2,263
Ragan_Dunham
NXP Employee
NXP Employee

Machine Learning at the Edge:

eIQ Software for i.MX Applications Processors

Developing machine learning (ML) applications for embedded devices can be a daunting task. For the traditional embedded developer, the learning curve can be quite steep, as there are numerous decisions that must be made and new jargon that must be learned. Which framework should I choose? Which model best meets the requirements of my application and how do I know when it’s good enough? What “size” microcontroller or application processor do I need? The questions are many and figuring out how to get started can prove to be a challenge.

詳細を読む...

件数が多いもの
2 7 21K