NXP Tech Blog - 8ページ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Tech Blog - 8ページ

devonna_dorton
NXP Employee
NXP Employee

NXP's MCUXpresso Software and Tools has expanded to include a new Secure Provisioning Tool, support for integrated third software solutions and has major improvements in the user experience for software selection. This newly updated suite further augments the easy-to-use SDK, IDE and Configuration Tools for streamlined development with Arm® Cortex®-M cores, including NXP’s LPC and Kinetis MCUs and the  i.MX RT Crossover Processors. A (comprehensive) list of supported devices can be found in the MCUXpresso community here: https://community.nxp.com/docs/DOC-333073

 

MCUXpresso software and tools bring together the best of NXP’s software enablement (core technologies) and integrated solutions from select partners (enabling technologies) into one enablement ecosystem for a shared software experience across a broad set of Arm® Cortex®-M MCUs.

詳細を読む...

件数が多いもの
0 0 2,362
MeganHansen
NXP Employee
NXP Employee

New versions of MCUXpresso SDK, IDE, and Configuration Tools are now available, along with a new Secure Provisioning Tool.

詳細を読む...

件数が多いもの
0 0 2,814
petrstruzka
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso Config Tools v7 are now available.

MCUXpresso Configuration Tools is a product with set of tools that help users of all levels with a Cortex-M-based MCU solution.

Features

  • Available as Web, Desktop application and MCUXpresso IDE plug-ins
  • MCUXpresso SDK v2 support
  • Multicore support
  • GUI localized for English and Simplified Chinese
  • On-Demand device data download for latest features and support
  • Integrated directly within MCUXpresso IDE, standalone version supports other compilers and IDEs
  • Currently there are the following tools available

詳細を読む...

件数が多いもの
0 0 2,780
lpcxpresso_supp
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso IDE v11.1.0 (build 3209) is now available. This is a major new version of the IDE, and contains many new features and enhancements over the previous MCUXpresso IDE v11.0.1 and earlier releases.

詳細を読む...

件数が多いもの
2 0 6,802
omar_cruz
NXP Employee
NXP Employee

The 5V KE MCU series has been designed to maintain high reliability and robustness in harsh electrical noise environments primarily targeting white goods and industrial applications, but now extending its success to consumer applications where touch sensing, safety and motor control capabilities have become a “must have” in the embedded design. 

詳細を読む...

件数が多いもの
0 0 5,154
monicavelez
NXP Employee
NXP Employee

NXP understands that in addition to offering breakthrough innovations its ongoing investment and commitment to longevity is critical to being your trusted supplier. This paired with the continued demand and broad market use of NXP’s MCU portfolio makes it priority for us to extend the longevity1 on the following parts/families by an additional five years.

詳細を読む...

件数が多いもの
0 2 5,914
nxf33441
NXP Employee
NXP Employee

More products today include graphical user interfaces than ever before, and consumers have a growing expectation that they be visually appealing and intuitive to use. Luckily, NXP and its partners make the process of adding a GUI of any level of complexity to your product seamless.

詳細を読む...

件数が多いもの
0 0 7,688
Kathleen
NXP Employee
NXP Employee

Announced in October, the i.MX RT1170 is NXP’s latest break-through technology within the i.MX RT series of Crossover MCUs.  What makes the i.MX RT1170 so cutting edge?

詳細を読む...

件数が多いもの
0 0 2,636
jianfeichang
Contributor IV

开发板是imx8M mini,我们自己做的板子,使用官方镜像yocto 4.14.98,OV5640 mipi摄像头,验证及其测试:

root@imx8mmevk:~# uname -a
Linux imx8mmevk 4.14.98-imx_4.14.98_2.0.0_ga+g5d6cbea #1 SMP PREEMPT Thu Dec 12 08:23:58 UTC 2019 aarch64 aarch64 aarch64 GNU/Linux

我这里用的是I2C4的接口,所以设备树修改arch/arm64/boot/dts/freescale/fsl-imx8mm-evk.dts

詳細を読む...

件数が多いもの
1 0 6,069
omar_cruz
NXP Employee
NXP Employee

Based on the ultra-low-power Arm® Cortex ®-M0+ Core the LPC800 MCU series offers a range of memory, small footprint and low-pin options for basic microcontroller applications. By being fully compatible with the Cortex-M architecture and instruction set, this series efficiently handles 32-bit data, requiring less code, memory and 30% less dynamic power outperforming 8- and 16-bit MCUs.

詳細を読む...

件数が多いもの
0 0 2,683
nicasio
NXP Employee
NXP Employee

The next generation of machine interfaces is here. As embedded technology evolves, NXP continues to innovate with technologies like cloud-based/local voice control and face recognition for secure access/authentication. Resources for these technologies are abundant, but how can NXP continue to offer an efficient, easy, and quick path to development for people who do not want to reinvent the wheel? How do we make it easier to innovate?

 

Enter NXP’s turnkey, production-grade IoT ML/AI edge computing solutions. NXP provides the option of an integrated approach to development, with solutions that include out-of-box hardware, software, schematics, layouts, documentation, certifications, and BOMs to enable developers to add sensor-based capabilities into their design easily and quickly. The advantage is a faster time to market with the ability to leverage popular services like the Alexa Voice Service for AWS IoT Core Integration or compute completely offline when it comes to face recognition, for instance. 

詳細を読む...

件数が多いもの
0 0 2,201
Kathleen
NXP Employee
NXP Employee

A lot of discussion recently has been around the i.MX RT1010 crossover MCU -and why not?  It is the latest and greatest achievement for high-end crossover MCUs.  But, you probably noticed that the i.MX RT1010 MCU left off some features in order to keep the cost low.  So, what if you need a high performance MCU with all the bells and whistles?

詳細を読む...

件数が多いもの
0 0 7,143
omar_cruz
NXP Employee
NXP Employee

The LPC5500 MCU series, world’s first Arm® Cortex®-M33 based MCU series for the mass market, has introduced new levels of performance efficiency, advanced security and functionality in the MCU space. With up to 150Mhz of core frequency (dual-core options included), 32uA/MHz of active power consumption, and tightly couple accelerators for signal processing and cryptography, the LPC5500 MCU series has become a key player in consumer electronics, building control and automation, secure applications and Industrial IoT markets.

詳細を読む...

件数が多いもの
0 0 2,504
Kathleen
NXP Employee
NXP Employee

Launched in October, the i.MX RT1010 crossover MCU further expands NXP’s popular i.MX RT series and introduces the world to the next generation of low-cost, high-performance MCUs.

詳細を読む...

件数が多いもの
2 0 3,357
omar_cruz
NXP Employee
NXP Employee

Building upon the market success and broad adoption of the Kinetis MCU portfolio, the K32 L3 MCU family leverages the combination of high-efficiency and low-power capabilities of the Arm® Cortex®-M4 while adding another Cortex-M0+ providing new enhancements such as low-leakage power-optimized peripherals, a DC-DC converter, numerous serial communication interfaces and up to 1.25MB flash and 384KB of SRAM memory.  

詳細を読む...

件数が多いもの
0 0 2,546
omar_cruz
NXP Employee
NXP Employee

Focusing on low-power and fast wake up times, the K32 L2 MCU family – based on the Arm® Cortex®-M0+ - targets power-conscious end nodes and can enable a wide range of general purpose industrial and IoT applications. Today, the K32 L2 MCU family is being brought to market in a scalable set of packages, core performance and memory configurations, from 64KB to 512KB flash, and backed by unmatched enablement, led by NXP’s complementary suite of MCUXpresso software and tools with example projects utilizing IAR, Keil, and GCC based toolchains.

詳細を読む...

件数が多いもの
0 0 2,281
monicavelez
NXP Employee
NXP Employee

Innovation means being first. And with more than 20 years of firsts, NXP’s MCU portfolio has grown into a powerhouse of more than 200 Arm®-based MCU families scaling from low-power Cortex®-M0+ to high performance Cortex®-M7 crossover MCUs.

詳細を読む...

件数が多いもの
2 0 2,560
lpcxpresso_supp
NXP Employee
NXP Employee

MCUXpresso IDE is currently supported on macOS 10.12 to 10.14.

In macOS 10.15 (Catalina), Apple have introduced a new additional "signing" mechanism for software that is download outside of the Apple App Store, know as "Notarization". Currently MCUXpresso IDE for macOS is signed using NXP's Apple Developer ID, but has not yet gone through Apple's notarization process. This means that by default you will not be able to install if you are running macOS 10.15.

詳細を読む...

件数が多いもの
0 0 3,801
iWave
Contributor V

Have you ever checked your smartphone or your IoT device and received an alert for software updates? All you have to do is to simply accept the update when you have the network connectivity and the rest will be taken care of automatically by the software. Isn’t it simply amazing to be able to refresh your device, no matter where you are in the world? This update process is widely known as OTA (over the air).

OTA is a technology that manages software and lets you wirelessly upgrade the operating system/files of your platform.

詳細を読む...

件数が多いもの
0 0 2,451
lpcxpresso_supp
NXP Employee
NXP Employee

As part of the MCUXpresso IDE v11.0.1 release, we had to make some major changes to our LinkServer debugging mechanism to support the latest silicon revision of the LPC55xx family of devices (revision 1B) and the more secure debug request mechanism required by these parts. Such silicon is supplied on LPC55S69-EVK boards marked Revision A2 (or later) on the board silkscreen.

詳細を読む...

件数が多いもの
0 0 3,188
iWave
Contributor V

iWave systems recently launched a new SMARC System on Module (SOM) based on the powerful NXP® i.MX 8QuadMax applications processors. This high performance SOM features an intelligent blend of MPUs+MCU power in a single device and integrates heterogeneous multicore 64 bit ARM® processors (Dual Cortex® A72@ 1.8 GHz + Quad Cortex® A53 @ 1.2 GHz and Dual Cortex® -M4F @ 266 MHz), targeted for applications that demand advanced real-time processing, multi-media performance as well as in applications that requires simultaneous multi-OS operations. For more details refer to the link: i.MX8 QuadMax NXP SMARC SOM

詳細を読む...

件数が多いもの
0 0 3,647
Kathleen
NXP Employee
NXP Employee

Today I conclude my countdown of top reasons to use i.MX RT1010, and I wanted to end the blog series in the same way that it began – by talking about how to get started. It is has been  2 weeks since my first post, so hopefully by now you have found the $10.10 in your couch cushion to order your i.MX RT1010 EVK. Maybe you even already have the EVK on your desk and followed the instructions on the Getting Started webpage which leads you to download the software and tools. But what is MCUXpresso and how much does it cost?

詳細を読む...

件数が多いもの
0 0 2,367
Kathleen
NXP Employee
NXP Employee

Listen up everyone. We are winding down the countdown and my blog today is about audio. Many consumer products and embedded devices support various digital audio functions, and more and more engineers are looking for the MCU to support these functions, rather than needing to add a DSP or other dedicated solution.  The good news is that many MCUs now have the capabilities to support these basic audio tasks. But how do you choose an MCU that will give your product the price, performance, and design flexibility you need?

詳細を読む...

件数が多いもの
0 0 2,370
Kathleen
NXP Employee
NXP Employee

So you want to add a display to your product? You look at the i.MX RT series table and see that the i.MX RT1010 device does not have an LCD interface, so you immediately write it off. Not so fast!  Did you know that you can add a display to your i.MX RT1010 design through the I2C module? What’s great about the i.MX RT1010 is that we didn’t skimp on peripherals to hit that $1 price point. Even the pin muxing takes into account maximum usability for a variety of applications. But say you are working on a thermostat application and need the I2C module to connect to a variety of sensors instead. Based on yesterday’s blog, hopefully you immediately think of the FlexIO module.

詳細を読む...

件数が多いもの
1 0 2,526
Kathleen
NXP Employee
NXP Employee

Say for example, you are working on your industrial application using the i.MX RT1010 MCU and have everything designed out. You are using two UARTs for sensor interfaces, one UART for camera, and the fourth UART will be used for development and future debug. Then, your product marketer comes by and asks you to add Bluetooth to the product.


What can you do?  The i.MX RT1010 only supports 4 UARTs. Do you move to an i.MX RT1050 MCU since it has 8 UARTs? Do you add another external UART to your design?


Don’t fret! FlexIO to the rescue!

詳細を読む...

件数が多いもの
0 0 2,150
Kathleen
NXP Employee
NXP Employee

All engineers – and most anyone – love to make things spin, right? That explains the revenue made on those fidget spinners. The inventor is a genius! OK ok … now back to MCUs … the i.MX RT MCU motor control demos are some of the most highly viewed demos. So what makes the i.MX RT1010 device ideal for motor control applications? Is it the FlexPWM? The ADC? Or just the raw performance of this 500 MHz MCU? The answer – all of the above.  The i.MX RT1010 MCU is an ideal solution for a single motor and here’s why

詳細を読む...

件数が多いもの
0 1 3,543
vishakhadakhane
Contributor III

Hello, recently I have done Periph Blinky e.g. from LPCOpen library on MCUxpresso. I am using LPC1769 chip and I have toggled GPIO pin. In my case I have used buzzer pin i.e. Port 3 & Pin 25. Instead of using Timer delay I created a delay function i.e. void delay_ms(unsigned int ms). Here I am attaching the systick.c file. Hope it helpsSmiley Happy!!  

詳細を読む...

件数が多いもの
0 0 2,211
Kathleen
NXP Employee
NXP Employee

On what could be perceived as a low-cost MCU, it is nice to see that security was not compromised on the i.MX RT1010 device. In fact, the i.MX RT1010 MCU has the same security block that exists on many of the other i.MX RT products.

詳細を読む...

件数が多いもの
0 0 1,821
Kathleen
NXP Employee
NXP Employee

For today's blog, I am going to keep it short and direct it to the PCB layout engineers out there.  The i.MX RT1010 MCU designers want you to know that the utmost care was taken when designing the i.MX RT1010 device. Even if your company typically prioritizes product requirements over package requirements, NXP has you covered. During our package development, we do a number of pin-out iterations and a fanout exercise to make sure that the i.MX RT LQFP packages are easily laid out for 2-layer through-hole PCBs. 

詳細を読む...

件数が多いもの
0 0 1,690
Kathleen
NXP Employee
NXP Employee

Continuing with my countdown of top reasons to use i.MX RT1010 crossover MCU, today I want to talk about performance.  The performance of the i.MX RT series really pushes this portfolio to a classification of its own – crossover MCUs. Engineers can now enjoy the level of performance historically seen in the processor space, now in the MCU world – providing tremendous familiarity and usability for engineers. But just ask the rabbit from the Tortoise and the Hare fable, sometimes it is not enough just to be fast. You have to be smart too. Within the i.MX RT1010 family, several smart features are coupled together with the 500 MHz Arm® Cortex®-M7 core.

詳細を読む...

件数が多いもの
0 0 2,434