NXP Tech Blog - 2ページ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Tech Blog - 2ページ

CosminB05
NXP Employee
NXP Employee

An interactive tutorial on how to create your own MATLAB Simulink temperature sensor application by applying the model-based design approach, how to configure and use the i.MXRT1060 EVK using NXP MCUXpresso, a thermistor module and the IMXRT Toolbox.

詳細を読む...

件数が多いもの
2 0 6,517
Irina_Costachescu
NXP Employee
NXP Employee

The Local Interconnect Network (LIN) was developed as a complementally bus standard to the Controller Area Network (CAN bus) to address the need for a cost-efficient network for lower performance devices within the vehicle.  While the CAN network was already in place within vehicles, its high bandwidth and advanced error detection capabilities were overkill (and thus, cost-prohibitive) for lower performance applications such as seat and window controllers.

詳細を読む...

件数が多いもの
2 2 36.4K
Irina_Costachescu
NXP Employee
NXP Employee

CAN FD is an extension to the Classic CAN protocol that was developed to meet the needs of modern vehicles wherever-increasing numbers of embedded electronics are transmitting ever-increasing amounts of control and diagnostic data.  Because the original CAN specification has a maximum bandwidth limitation of 1 Mbps, data-dense activities like ECU flashing and advanced driver assistance systems (ADAS) ADAS applications were being impeded, forcing automotive manufacturers to add multiple CAN networks into newer vehicles.

詳細を読む...

件数が多いもの
2 0 21.3K
Irina_Costachescu
NXP Employee
NXP Employee

Communication between these subsystems is critical to ensure the reliability and safety demanded in the automotive market.  The Controller Area Network (CAN bus) is a message-based communication network standard that allows ECUs to communicate within a vehicle without the use of dedicated analog signal wires. 

詳細を読む...

件数が多いもの
16 0 84.2K
asim_zaidi
NXP Employee
NXP Employee

NXP PSIRT was informed by security researchers about two Denial of Service (DoS) vulnerabilities which can cause crashes or message-dependent deadlocks in certain Bluetooth Low Energy (Bluetooth LE) implementations of the MCUXpresso Software Development Kit (SDK). The specific software vulnerabilities are...

詳細を読む...

件数が多いもの
3 0 4,368