Tutorial: Booting the NXP i.MX RT from Micro SD Card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Tutorial: Booting the NXP i.MX RT from Micro SD Card

BlackNight
NXP Employee
NXP Employee
1 0 3,377

The following article is a step-by-step tutorial how to use the NXP MCUXpresso SDK & IDE to create a SD card bootable image on i.MX RT. It features the i.MX RT1050-EVK(B) but is with minor changes applicable to any other i.MX RT device:

Tutorial: Booting the NXP i.MX RT from Micro SD Card

  • Creating a project running in RAM
  • Generating S19 file
  • Running application in RAM
  • Creating SD card boot image with Flashloader and elftosb
  • Loading image to SD card with MfgTool
  • Booting i.MX from SD card image

sw7-on-i.mxrt1050-evkb-for-sd-card-boot-1.png

 

I hope you find it useful,

Erich