Overview of using the MIMXRT1170-EVK with MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Overview of using the MIMXRT1170-EVK with MCUXpresso IDE

lpcxpresso_supp
NXP Employee
NXP Employee
3 1 10K

Please find attached a document detailing various features related to using the IMXRT1170-EVK evaluation board with MCUXpresso IDE v11.4.x (or newer) and SDK v2.10.0 (or newer), including details of multicore debugging on this MCU.

Updated v1.2.0  29th September 2021

Updated to include a section on how to enable SWO trace on this MCU.

Updated v1.3.0  17th January 2023

Updated to reflect the most recent SDK and IDE versions, and to include a section about building and debugging SDRAM-based applications.

Updated v2.0.0  20th January 2023

Updated to include information about MIMXRT1170-EVKB board.

Updated v2.1.0  9th September 2024

Updated to include additional information about SWO trace configuration related to MIMXRT1170-EVKB board. Other minor additions.

 

Yours,

MCUXpresso IDE Support

1 Comment
jeremyzhou
NXP Employee
NXP Employee

Hi @Childe,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'd like to know more information about your issue, so I hope you can answer the below inquires.
1) Is the first time to debug the MIMXRT1170-EVK board?
1.1) If not, did the phenomenon happen before?
1.2) If yes, did you ever change the hardware setting of the board or not?
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------