NXP Designs ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Designs Knowledge Base

ディスカッション

ソート順:
Overview This NXP® reference design of a 3-phase sensorless PMSM vector control drive with a sliding mode observer (SMO) is targeted mainly for compressor control and other consumer and industrial applications. This cost-effective solution uses the NXP MC56F8013 device dedicated for motor control. Software written in C-code using some library algorithms Available for the MC56F8013 and MC56F8346 digital signal controllers Hardware-based on the NXP universal motor control h/w modules Features The system is designed to drive a three-phase PM synchronous motor. Application features are: 3-phase sensorless PMSM speed vector control (FOC) Sliding mode observer with adaptive velocity estimation Based on NXP ®  MC56F8013 (resp. 56F8346) controller Running on a 3-phase high voltage (230/115V) power stage FreeMASTER software control interface and monitor Block Diagrams Design Resources
記事全体を表示
  Overview The Point of Sale reference design demonstrates how the control, security, and connectivity features found on the NXP ®  MCF5329 ColdFire ®  MPU and MCS908QG8 MCU work together to create a secure Industrial Point of Sale System. Complete with an Open Source Embedded Linux® Software Solution, the Point of Sale Reference Design serves as a reference for any industrial design that requires flexible connectivity options, secure communication, or a human interface at a low cost and with a fast development cycle. Archived content is no longer updated and is made available for historical reference only.   Features The Point of Sale Reference Design was designed with the following considerations: Low system cost Easy and intuitive graphical user interface Multiple connectivity solutions to accommodate various POS system connectivity requirements Secure networking communications, transactions, and memory accesses Fast development cycle The Industrial Point of Sale Reference Design also features an Open Source Software Solution: µCLinux Operating System running on the MCF5329 Microprocessor NanoX Graphical User Interface (GUI) Configuration Tool running in the µCLinux environment Communication protocol for secure ethernet transactions MySQL Server Database used to store/access sales transactions       Code Generation Tools Model-Based Design Toolbox Printed Circuit Boards and Schematics Point of Sale Reference Design Schematics Point of Sale Gerber Files (Reference Design)
記事全体を表示
        S32G just support serial download a M7 image to run by internal rom codes, our S32G DS IDE have a flash tools to use this feature to burn the image to external device. So current image burn method will divide into 2 step: 1: burn a uboot into the external device by S32G DS flash tools. 2: reboot the codes with uboot and run with network to burn the linux image into external device.      which need two working place on manufacture line, and customer wish to have a one time on-line tools, which means we need use serial port to boot uboot directly but S32G rom codes do not support it.       We have a reference tools of S32V but which IP difference is big between on S32V and S32G, So we can not reuse it and have to develop a new one.       The development working include: 序号 开发工作 说明 开发者 1 开发 根据S32G的serial boot协议要求,开发PC端的串口工具来下载M7镜像 John.Li 2 开发 根据自定义协议要求,开发PC端的串口工具来下载A核Bootloader到SRAM中 John.Li 3 开发 根据自定义协议要求,开发M7镜像的串口接收与Checksum逻辑 John.Li 4 开发 修改M7镜像支持串口0 John.Li 5 开发 开发实现M7镜像的串口单字节同步收发函数 John.Li 6 开发 开发实现A53启动功能 John.Li 7 调试与Debug 调试解决串口接收乱码问题(Serial boot rom codes仍然在回送消息串口) John.Li 8 调试与Debug 提供 解决A核启动串口halt思路(Serial boot rom codes仍然占用串口) John.Li 9 调试与Debug 优化M7镜像,缩小大小 Tony.Zhang 10 调试与Debug 根据M7镜像和A核 Uboot在SRAM中的内存分配要求,重排M7镜像位置,避免冲突 Tony.Zhang 11 调试与Debug 在M7中初始化SRAM空间 Tony.Zhang 12 调试与Debug 在M7中设置SRAM可执行空间 Tony.Zhang 13 调试与Debug 调试解决由于cache没有及时回写导致的下载镜像错误的问题 Tony.Zhang 14 调试与Debug 集成,调优与文档 John.Li   Pls check the attachment for the doc/codes/binary release which include:    Release      |->M7: Linflexd_Uart_Ip_Example_S32G274A_M7: S32DS M7工程。      |->PC: s32gSerialBoot_Csharp: PC端的Visual Studio的C#的串口工具工程。      |->Test:      |    |-> 115200_bootloader.bin: S32DS M7工程编译出来的bin文件,波特率为115200      |    |-> 921600_bootloader.bin: S32DS M7工程编译出来的bin文件,波特率为921600      |    |->load_uboot.bat: 运行工具的批处理文件,运行成功后打开串口可以看到Uboot执行,默认使用的波特率是115299         |    |->readme.txt:其它测试命令 |    |->s32gSerialBoot.exe:编译出来的PC端串口工具 |    |->u-boot.bin: BSP29默认编译出来的u-boot.bin.      Product Category NXP Part Number URL Auto MPU     S32G274     https://www.nxp.com/s32g    
記事全体を表示
Linux kernel is not real time OS, while some applications is time sensitive tasks running in Linux environment, this request to extend the real time feature in common Linux kernel, and RT_PREEMPT is one of the methods to enable Linux kernel with real time processing requirement. But RT_PREEMPT is not accepted by kernel, so it needs extra effort to porting this patch-set to i.MX8M family products. This patch-set is based on L4.14.78 for i.MX8M products, customer need to apply patches based on this release.
記事全体を表示
  Overview   Vehicle-to-Everything (V2X) technology enables cars to communicate with their surroundings and makes driving safer and more efficient for everyone. By making the invisible visible, V2X warns the driver of road hazards, helping reduce traffic injuries and fatalities. In addition to improving safety, V2X helps to optimize traffic flow, reduce traffic congestion and lessen the environmental impact of transportation. V2X is a key component for full autonomous driving. V2X need message package signing & verification which need high CPU loading if used CPU. Qualcomm recommend their customers to use NXP i.MX8X/XL which have HSM as their modem’s companion chip. Two major components in the system: RSU (Road Side Unit) and OBU (On Board Unit). Both have similar system design, with minor differences. Block Diagram   v2x rsu.png v2x.png Product Category MCU/MPU Product URL 1 i.MX 8X Family – Arm® Cortex®-A35, 3D Graphics, 4K Video, DSP, Error Correcting Code on DDR  Product Description 1 Extending the scalable range of the i.MX 8 series, the i.MX 8X family is comprised of common subsystems and architecture from the higher-end i.MX 8 family, establishing a range of cost-performance scaling with pin-compatible options and a high level of software reuse. Product URL 2 https://www.nxp.com/design/development-boards/automotive-development-platforms/s32k-mcu-platforms/s32k144-evaluation-board:S32K144EVB  Product Description 2 The S32K144EVB is a low-cost evaluation and development board for general purpose automotive applications.   Category Transceivers Product URL 1 TJA1051: High-speed CAN transceiver  Product Description 1 The TJA1051 is a high-speed CAN transceiver that provides an interface between a Controller Area Network (CAN) protocol controller and the physical two-wire CAN bus. Product URL 2 TJA1101: 2nd generation Ethernet PHY Transceivers - IEEE 100BASE-T1 compliant  Product Description 2 TJA1101 is a high-performance single port, IEEE 100BASE-T1 compliant Ethernet PHY Transceiver.   Category Power Management Product URL PF8100-PF8200: 12-channel Power Management Integrated Circuit (PMIC) for High-Performance Processing Applications  Product Description The PF8100/PF8200 PMIC family is designed for high-performance processing applications such as infotainment, telematics, clusters, vehicle networking, ADAS, vision and sensor fusion.   Category Secure Element Product URL SXF1800: Secure Element IC for V2X Communication  Product Description SXF1800 is based on highly secure microcontroller used also to protect mobile payments, providing highest proven assets protection.   Category I2C interface Product URL 1 PCA9538: 8-bit I²C-bus and SMBus low power I/O port with interrupt and reset  Product Description 1 The PCA9538 is a 16-pin CMOS device that provides 8 bits of General Purpose parallel Input/Output (GPIO) expansion with interrupt and reset for I2C-bus/SMBus applications and was developed to enhance the NXP Semiconductors family of II2CC-bus I/O expanders. Product URL 2 PCT2075: I2C-Bus Fm+, 1 Degree C Accuracy, Digital Temperature Sensor And Thermal Watchdog  Product Description 2 The PCT2075 is a temperature-to-digital converter featuring ±1 °C accuracy over ‑25 °C to +100 °C range. Product URL 3 PCA85073A: Automotive tiny Real-Time Clock/Calendar with alarm function and I2C-bus  Product Description 3 The PCA85073A is a CMOS1 Real-Time Clock (RTC) and calendar optimized for low power consumption.   Category Wi-Fi Product URL 88W8964: 2.4/5 GHz Dual-Band 4x4 Wi-Fi® 5 (802.11ac) Access Solution  Product Description The 88W8964 features 160MHz bandwidth and Multi-User Multi-Input Multi-Output (MU-MIMO) while achieving 2.6 Gbit/s peak data rate for high speed, secure, and reliable access points and smart gateways.   Category V2X Modem Product URL RoadLINK® SAF5400 Single Chip Modem for V2X  Product Description The RoadLINK SAF5400 is an automotive-qualified single chip DSRC modem for V2X applications. The SAF5400 modem is able to receive and verify up to 2000 messages per second.
記事全体を表示
  Overview   Since 1996 in EU and since 2000 in Europe, the OBD (On-Board Diagnostics) is mandatory for all the cars manufactured. This protocol is used to verify the smoke emissions and check if any car is between the parameters stablished in every country. Also detect engine failures without need to check the engine manually, identifying accurately the problems reducing the repairing time and cost. OBD-II is a sort of computer which monitors emissions, mileage, speed, and other useful data. OBD-II is connected to the check engine light, which illuminates when the system detects a problem. Scan tools can be used to make sense of the diagnostic trouble codes and collect data on other aspects of vehicle’s performance.   Use Cases Hotspot in the CAR Geofences and speed limits Driving habits tracking Insurance and Rental Entertainment   Block Diagram Block-Diagram-OBDIICarScanner-PNG.png   Products Category Name MCU Product URL 1 MIMXRT1050-EVK: i.MX RT1050 Evaluation Kit Product Description 1 The i.MX RT1050 EVK is a 4-layer through-hole USB-powered PCB. At its heart lies the i.MX RT1050 crossover MCU, featuring NXP’s advanced implementation of the Arm® Cortex®-M7 core.   Category Name Serial Link Bus Product URL 1 KIT33660EFEVBE: Evaluation Kit - MC33660, ISO K Line Serial Link Product Description 1 The KIT33660 evaluation board supports the MC33660, a serial link bus interface device designed to provide bi-directional half-duplex communication interfacing in automotive diagnostic applications.   Category Name Transceiver Product URL 1 TJA1100HN: Evaluation Board, TJA1100HN 100BASE-T1 PHY Transceiver Product Description 1 The TJA1100HN customer evaluation board is a low-cost hardware development tool which supports the functional evaluation of the TJA1100HN 100BASE-T1 PHY transceiver.  
記事全体を表示
This doc explain bootloader secure boot feature and how to re-develop it to support: .FW update .OTP attribute access .IVT protect: 目录 1 参考资料 .................................................................... 2 2 S32G Secure Boot说明 ............................................. 2 2.1 IVT头格式与Secure Boot相关 ................................ 3 2.2 Secure Boot流程 .................................................... 3 2.3 Secure Boot配置 .................................................... 4 2.4 Secure Boot涉及到的HSE内容 ............................... 6 3 环境搭建 .................................................................... 7 3.1 搭建编译环境 .......................................................... 7 3.2 IVT镜像制造 ........................................................... 7 3.3 镜像烧写 ................................................................. 8 3.4 Bootloader Secure Boot测试 .................................. 8 4 Bootloader Secure Boot代码与功能说明 ................... 9 4.1 EB配置说明: ........................................................ 9 4.2 EB生成代码说明: ............................................... 15 5 定制1:HSE FW update .......................................... 22 5.1 代码开发 ............................................................... 22 5.2 测试 ...................................................................... 25 6 定制2:HSE OTP Attribute设置 ............................... 26 6.1 代码开发 ............................................................... 26 6.2 模拟测试 ............................................................... 33 7 定制3:IVT签名 ....................................................... 35 7.1 代码开发 ............................................................... 35 7.2 模拟测试 ............................................................... 40 Contents 1 Reference Materials .................................................. 2 2 S32G Secure Boot ..................................................... 3 2.1 IVT header format for the Secure Boot part .......... 3 2.2 Secure Boot Flow ................................................... 3 2.3 Secure Boot Configuration ..................................... 4 2.4 HSE background of Secure Boot ........................... 6 3 Build the Project ........................................................ 7 3.1 Build the Compiling Environment ........................... 7 3.2 Create IVT Image ................................................... 7 3.3 Burning Image ........................................................ 8 3.4 Bootloader Secure Boot Testing ............................ 9 4 Bootloader Secure Boot Codes and Function Description 9 4.1 EB Configuration .................................................... 9 4.2 EB output codes ................................................... 15 5 Customization 1:HSE FW update ......................... 22 5.1 Codes development ............................................. 23 5.2 Testing ................................................................. 26 6 Customization 2:HSE OTP Attribute Setting ......... 26 6.1 Code Development .............................................. 27 6.2 Simulation test ...................................................... 34 7 Customization 3:IVT Signature ............................. 36 7.1 Codes Development ............................................. 36 7.2 Simulation Testing ................................................ 40  
記事全体を表示
  Overview Hearables or smart headphones are highly integrated, truly wireless earbuds designed to improve audio experiences across a range of consumer and healthcare applications. Small form factors, ultra-light weight and wireless operation increase user comfort. The continued challenge for hearables is how to combine audio quality, user experience and better battery life in a tiny package while offering a multitude of possibilities, all of which demands digital signal processing. To simplify customer engineering efforts on prototype TWS earbud, NXP built an Application Development Kit. Customer just need plug and play to test the functionality and performance of earbud. The ADK demonstrated a stable audio streaming link from Bluetooth mobile phone to both ear. It can be used as a fundamental platform for customer to develop hearables. Features Fitness tracking (pedometer, heart rate, etc.) Local playback (mp3, wav…) Voice UI (command trigger, ON/OFF) Voice enhancement (argument hearing, be forming) Universal translator Block Diagram Block-Diagram-TrueWirelessEarbuds-PNG.png Products Category MCU Product URL LPC541XX: Low-Power Microcontrollers (MCUs) Based on Arm® Cortex®-M4 Cores With Optional Cortex®-M0+ Co-processor  Product Description The LPC541xx MCU family of single-core and dual-core MCUs are our next-generation of power efficient MCUs.   Category NFMI Radio Product URL NXH2266: NFMI radio for wireless audio and data streaming  Product Description The NXP® NXH2266 is a fully integrated single-chip solution that enables wireless audio streaming and data communication using Near Field Magnetic Induction (NFMI), a mature technology that has a proven track record in the hearing industry.   Category Audio Codec Product URL SGTL5000: Ultra-Low-Power Audio Codec  Product Description The SGTL5000 is a low-power stereo codec designed to provide a comprehensive audio solution for portable products that require line-in, mic-in, line-out, headphone-out and digital I/O.   Category NFC Product URL NTAG I2C plus: NFC Forum Type 2 Tag with I2C interface  Product Description The NTAG I2C plus combines a passive NFC interface with a contact I2C interface.   Category Accelerometer Product URL MMA8652FC: ±2g/±4g/±8g, Low g, 12-Bit Digital Accelerometer  Product Description The NXP® MMA8652FC 12-bit accelerometer has industry-leading performance in a small package.   Category Power Management Product URL MC34673: 1.2 A Single-Cell Li-Ion/Li-Polymer Battery Charger  Product Description The MC34673 is a cost-effective fully-integrated battery charger for Li-Ion or Li-Polymer batteries.   Category Voltage Level Translator Product URL GTL2005PW: Quad GTL/GTL+ to LVTTL/TTL bidirectional non-latched translator  Product Description The GTL2005 is a quad translating transceiver designed for 3.3 V system interface with a GTL/GTL+ bus.
記事全体を表示
This doc explain  where is the design resource and what they are of S32G in Chinese,  Contents as follows: 目录 1 www.nxp.com 官网资源 ............................................. 2 1.1 www.nxp.com Documentation ................................ 4 1.2 www.nxp.com Tools&Software ............................. 10 2 Flexera资源 ............................................................. 18 2.1 Automotive HW-S32G Evaluation Board .............. 21 2.2 Automotive HW-S32G GoldBox ........................... 22 2.3 Automotive HW-S32G RDB2(RDB不再说明) ....... 22 2.4 Automotive SW-S32G2 Standard Software.......... 23 2.5 Automotive SW-S32G2 reference Software ......... 28 2.6 Automotive SW-S32G2 Tools .............................. 30 3 Docstore资源 ........................................................... 31
記事全体を表示
    Description: Teensy 3.1 and Teensy-LC are a complete USB-based development tools featuring respectively the Kinetis 32-bit Cortex-M4 K20 and Cortex-M0+ KL26 devices running @ 72 and 48 MHz. Teensy 3.1 is equipped with 256KB flash and 64KB RAM. Teensy-LC board is equipped with 62KB flash and 8KB RAM.   Value Propositions * Very small footprint development tools * Very Low Cost dev tool * They are able to implement many different projects * Open source SDKs   Teensy board with very high extended-Arduino compatible performance levels and libraries taking advantage of Kinetis features like low power modes and internal DMA. Libraries for LED (WS2811) and 16bit 44.1kHz audio quality is where Makers go when they need quality, performance and small size. FEATURES Hardware Specifications Specification Teensy LC Teensy 3.0 Teensy 3.1 & 3.2 Units Processor MKL26Z64VFT4 32 bit ARM Cortex-M0+ 48 MHz MK20DX128 32 bit ARM Cortex-M4 48 MHz MK20DX256 32 bit ARM Cortex-M4 72 MHz Flash Memory 62 128 256 kbytes RAM Memory 8 16 64 kbytes EEPROM 1/8 (emu) 2 2 kbytes I/O 46, 5 Volt 34, 3.3 Volt 34, 3.3V, 5V tol Analog In 8 14 21 PWM 9 10 12 UART,I2C,SPI 1,1,1 3,1,1 3,2,1 Price $24.00 $19.00 $19.80 USD   Software Enablement Teensy 3.2 & 3.1: New Features https://www.pjrc.com/store/teensylc.html     RECOMMENDED PRODUCTS Product Description Kinetis K Microcontroller Kinetis L Microcontroller RESOURCES Title Type PJRC (Teensy Official Website) Web Page
記事全体を表示
  Overview NXP’s Motion Control and Robotics solution provides the computing performance, embedded connectivity, low latency and a real-time open source operating system to address the requirements for multi-axis motion control and robotics applications.  This solution is based on an i.MX RT1050, which controls four steppers motors that activates the different kind of movement of the robotic arm for the 3D printer to function. This solution also counts with the FreeMASTER GUI for easy debugging and a better presentation and control of the system. Use Cases Our robust product portfolio makes motor and robotics control more precise, secure and effective for the creation of end-products with applications like: 3D printers Industrial applications: Welding machines Material handling Painting and drilling Assembly machines Surgical assistants Block Diagram Block-Diagram-Robot ARM-PNG.png Products Category MCU Product URL i.MX RT1050 Crossover MCU with Arm® Cortex®-M7 core  Product Description The i.MX RT1050 is the industry's first crossover MCU and combines the high-performance and high level of integration on an applications processors with the ease of use and real-time functionality of a microcontroller.   Category Motor Driver Product URL GD3000: 3-Phase Brushless Motor Pre-Driver  Product Description The GD3000 is a gate driver IC for three-phase motor drive applications providing three half-bridge drivers, each capable of driving two N-channel MOSFETs.   Category Power Management Product URL PCA9412: 3.0 MHz, 300 mA, DC-to-DC boost converter  Product Description The PCA9412 and PCA9412A are highly efficient 3.0 MHz, 300 mA, step-up DC-to-DC converters.
記事全体を表示
本文为如下G2版本的升级篇,使用G3+更新的软件 目录 1    需要的软件与工具... 2 1.1  软件工具与文档... 2 1.2  开发说明... 3 2    测试软件安装编译说明... 3 2.1  安装LLCE Logger驱动... 3 2.2  编译LLCE驱动测试程序(以CAN Logger 为例) 4 2.3  Logger Demo功能说明... 5 2.4  M7 BootLoader ATF镜像冲突检查... 7 2.5  LLCE Logger Demo去掉CLOCK INIT. 9 2.6  LLCE Logger Demo去掉MCU 相关INIT. 10 2.7  LLCE Logger Demo程序去掉PORT INIT. 10 2.8  中断冲突说明... 10 2.9  去掉其它无用初始化... 11 3    Bootloader工程说明... 11 3.1  关掉XRDC支持... 12 3.2  关掉eMMC/SD支持(可选) 13 3.3  关掉secure boot(可选) 14 3.4  增加LLCE 驱动所需要的PORT 的初始化... 15 3.5  解决Bootloader,MCAL 与Linux 的clock 冲突... 16 3.6  配置A53 Boot sources: 34 3.7  配置M7 Boot sources: 36 3.8  关闭调试软断点... 37 3.9  编译Bootloader工程... 38 3.10 制造Bootloader的带IVT的镜像... 39 3.11 烧写镜像... 41 4    Linux LLCE logger功能修改... 42 4.1 ATF的修改... 42 4.2 Linux中关于LLCE配置... 44 4.3 LLCE相关初始化冲突说明... 45 5    测试... 46 5.1  硬件连接... 46 5.2  LLCE logger 测试过程... 46 S32G Boot customization doc how to run bootloader to run mcal&linux https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/S32G-Bootloader-Customzition/ta-p/1519838
記事全体を表示
This doc explain how to optimize the Linux boot time, Contents as follows: 目录 1 默认BSP28 Linux内核的启动时间分析和优化方向 ..... 2 2 UBoot的优化 .............................................................. 3 2.1 缩小Uboot的DTS尺寸 ............................................ 3 2.2 缩小Uboot的尺寸 .................................................... 4 2.3 去掉等待3S输入时间 .............................................. 4 2.4 配合内核修改的Uboot参数 ..................................... 4 2.5 关闭串口调试信息 .................................................. 5 2.6 MMC read的方法来读取内核和DTB ....................... 5 3 Kernal的优化 ............................................................. 5 3.1 DTB中去掉不用的驱动和代码 ................................. 5 3.2 内核中去掉不用的平台与驱动及相关代码 ............... 6 3.3 内核中去掉不用功能,缩小内核大小 ...................... 7 3.4 去掉initramfs支持 ................................................... 7 3.5 关闭调试信息 .......................................................... 7 3.6 提前eMMC驱动加载时间 ........................................ 7 3.7 将Kernel与DTB打包在一起..................................... 8 4 Rootfs+应用程序的优化 ............................................. 8 5 最终全部启动时间比较 ............................................. 12
記事全体を表示
         随着近年来人们对日常出行品质的提高,电动自行车(包括共享类)市场得到了飞速发展,其功能日趋复杂智能。作为电控部分的“三大件”,电驱,主控和仪表也在不断升级迭代,其中电驱发展经历了最早期的直流有刷电机驱动到直流无刷方波驱动再到如今的 FOC 正弦波驱动,主控从以前附属在电驱或者仪表里的边缘化概念到如今独立出来的中心化,仪表则从普通的段式 LED 显示到如今尺寸越来越大功能越来越丰富的彩屏显示,而相对应的负责沟通互联“三大件”的通信总线也从传统的单总线到 TTL UART 到 RS485 再到如今逐渐展露头脚的 CAN 总线。对于电动自行车这种大众型消费市场来说,这些电控部分的升级换代给MCU 带来新的机遇的同时也对其性能,外设资源和价格带来了极大挑战。基于此, 针对三大件之一的仪表市场,NXP 开发了一套基于高性价比 LPC5506 系列 MCU 的 E-Bike 迈速表中低端显示屏方案。 系统框图: calvinji_0-1663122165356.png 主要特性: 4.5v~85v宽范围电压输入,支持24v,36v和48v锂电池组电源直接接入; 主控LPC5506支持CAN通信,8080 16bit/8bit LCD接口,且封装为LQFP 10*10mm,利于仪表小型化; 支持3.5寸320*480 16bit及以下尺寸的TFT LCD显示屏,预留I2C接口的电阻屏触摸控制芯片; 支持开源免费的ZLG AWTK GUI和LittleVgl GUI框架; 板载光敏传感器,可用于根据环境光自动调节LCD背光亮度; 板载六轴Motion Sensor(MPU6050),可用于转把方向检测,防盗检测和自行车摔倒检测等; 板载GPS和BLE模块,可用于定位,精确授时校准,行车轨迹离线存储或者与手机蓝牙通信; 板载4MB SPI Flash,用于图片和字体资源,GPS坐标轨迹存储和其他重要信息存储; 预留了USB Type-C电源供电端口和调试串口,方便工程师调试。 软件环境:        当前版本的软件代码工程有三份,一份为基于ZLG AWTK GUI的完整E-Bike迈速表工程,可显示车速仪表盘,里程,档位和电池电压等行车参数,也可以进入简单的功能设置界面浏览当前系统信息,且支持通过指定的CAN帧格式更新当前GUI界面的参数信息。一份为基于NXP GUIGuider图形化工具设计开发的LVGL版本E-Bike迈速表工程,分为3个子界面显示车速和骑行状态等详细信息。第三份为移植到本参考设计上的LVGL官方Demo例程,里面包含了配置好的EZH驱动库和LittleVgl基本的设备输入输出框架,用户可以基于此例程灵活开发定制自己的LVGL based其他GUI应用。        目前基于ZLG AWTK和LVGL GUI的E-Bike迈速表显示屏方案在经过优化之后对主控MCU的资源的占用以及GUI整体刷新性能如下表1,由于两个工程所使用的GUI素材和布局不一样,所以不要对两者的资源占用和性能参数做对比。他们都可以满足大部分客户的应用需求(>15fps)。如果将显示屏的分辨率降低到320*240及以下小尺寸的情况下,整个系统的资源占用会相应的减小,刷新性能也会得到更大的提升。 表1 方案资源占用及GUI刷新性能(分辨率320*480 16bit) Demo Code Flash RAM Refresh Rate AWTK GUI Version 202KB 61KB 22fps LVGL GUI Version 206KB 78KB 17fps 写在最后:        本参考设计的初衷是针对E-Bike中低端仪表显示屏市场提供一个高性价比的选择,同时也可以作为一个对于显示,CAN通信和小封装有类似需求的平台性的参考方案推广,比如电摩,带显示屏的便携式医疗设备和工业IoT设备等,希望此方案能给市场带来更好的用户体验和高性价比的选择。 注:由于代码工程超过25M,不能上传到该Community,如有需要请联系NXP销售或FAE索取。
記事全体を表示
This post entry provides a detailed description of how to develop an NFC pairing solution for audio devices. For that, we will describe in detail an audio speaker prototype made by NXP. This post entry has been structured as follows: Use cases for Bluetooth and Wi-Fi pairing via NFC As the number of connected devices grow, the more important it becomes to connect them in a simple way. At the same, it is required to provide a consistent and pleasant user experience. NFC pairing is one popular NFC use case, just bringing two NFC-enabled devices close together is all it takes to create a connection. For instance: To connect to your TV, to transfer a video from your phone, or sharing screens between your tablet and the TV. To connect to your camera to transfer pictures. To connect your phone to a wireless speaker. To connect your new devices to the home network. To connect to your wearables to read your heart rate. Or, to set-up a multi-audio system with NFC. Precisely, this post will guide you through the implementation of the NFC pairing solution for a multi-audio system. Benefits offered by the NFC pairing solution There are several benefits to consider adding NFC to your consumer device. First, from the consumer perspective: It provides a faster and simpler way to link wireless devices, only one touch. The credentials for establishing this connection are exchanged in a secure way. The device is identified instantly, without conflicts. In addition, from the manufacturer perspective, the benefits come mainly from: Making the device more attractive, by adding a new feature. And making the device easier to use, reducing the cost associated to customer technical support. Overall, NFC pairing is an interesting solution since it combines the simple, one-touch setup of NFC with the higher speed, longer distance communication of BT or Wi-Fi networks Pair and unpair Bluetooth headsets with just a tap with NFC NFC pairing process steps To pair and send music to a BT headset is as simple as: Select and play a music track in our phone. Tap the BT headset with the phone. When doing so, the BT pairing credentials are exchanged securely via NFC without any manual settings. The phone automatically initiates a BT connection request. After a second, audio is streamed via BT to the headset without entering any manual configuration. Furthermore, this is not only restricted to phones and headsets, but in general between any two NFC-enabled devices. Therefore, it is also possible to pair and send music to two Bluetooth headsets at the same time, creating what is known as “a silent disco”. Again, the process is simple: First, tap the two headsets with NFC capabilities. When doing so, the headsets automatically exchange the pairing credentials. The headsets establish a BT connection. And audio is streamed between them without requiring any manual setting. Similarly, instead of creating a silent disco, wireless speakers can be paired together via NFC to create a multi-audio system.  As such, NFC offers a real one-touch solution. It works with any NFC phone and no dedicated app needs to be installed. NFC unpairing process steps To stop sending music and un-pair the headset is easy as well. A second tap is the only action required to disconnect the headsets. After the tap, the second headset automatically de-activates the audio streaming and switches off. Best of all, we have instant identification of the device to be disconnected. Therefore, zero chances to unpair the wrong device as might happen through the phone settings, where we can unintentionally pick the wrong one. Multi-audio wireless speaker demo with NFC pairing capabilities During the rest of this post, we will tear-down an NFC multi-audio wireless speaker prototype developed by NXP based on PN7120 NFC controller solution. Hardware architecture This demo consists of two speakers with the same components, and therefore, the same functionality. If we dismount one of the speakers, the components we can find in the device PCB are: A system on chip solution, with an application processor, embedded flash memory and BT wireless connectivity. A system crystal clock, the BT antenna and two audio speakers A power supply unit, which includes three 1.5V batteries providing a stable 1.8V output. A NFC reader module, based on PN7120 chip, with an integrated antenna and a compact form factor. Application circuit for Bluetooth power on by NFC triggering If we have a closer look to the power unit interface, we see that: The VBAT pin is directly connected to the batteries. (PN7120 it supports a wide range of power supply voltages, from 5.5V down to 2.75V) The pad supply (PVDD), for the host interface operation, is connected to the 1.8V from the PMU. A wake-up trigger is built so that the BT controller is powered when an RF-field is detected. Regarding the host interface between the NFC controller and the main system MCU: The PN7120 module is connected to the BT controller via I2C slave interface. It supports standard, fast and high speed I2C modes (100 kHz SCL, 400 kHz SCL, 3.4 MHz SCL) The corresponding pull-up resistors are connected on the data and clock lines (SDA and SCL). The IRQ pin is used for ensuring the data flow control between PN7150 and the BT controller. The VEN (RESET) pin, used for setting the device in hard power down mode.  And, in respect to the antenna interface: The PN7120 VGA package Some discrete components for the antenna matching And the antenna coil surrounding the PCB edge. Software architecture and NCI interface In this section, we detail the solution software stack and how the NFC application logic works within the overall system. Using the block diagram, we have added the software blocks in orange.First, the PN7120 module includes: The NCI firmware & transport mapping layer for I2C communication (nothing to take care of from the developer side, since this firmware already comes embedded in the chip). Similarly, the host controller side requires: The NCI driver & transport mapping layer to communicate with PN7120 On top of these layers, the application logic for the BT pairing is implemented. Finally, the BT stack for the audio streaming, , but this software piece is not detailed here as it is out of the scope of the NFC implementation. NFC controller interface (NCI) specification details NCI describes the internal interface between an NFC Controller and the main host platform (in this case, between PN7120 and the BT chip). NCI is defined by the NFC Forum organization. As such, it provides manufacturers with a standard interface they can use for whatever kind of NFC-enabled device they build (making integration easier, saving time and effort). The next figure represents the NCI architecture: At the bottom, we find the transport mapping blocks, which map the NCI protocol to an underlying physical connection (I2C, SPI, UART, etc) The NCI core defines the messages, commands and data format for the different communications On top, the NCI modules implement specific functionalities, like the RF discovery which configures the NFC controller to communicate with other NFC tags or devices. From the overall NCI architecture, this implementation makes use of: The transport mapping is the I2C block The RF discovery is configured so that the speaker iterates between the reader, card and P2P modes NFC controller interface: RF Discovery PN7120 firmware can combine the three NFC modes of operation using the RF Discovery as defined in NCI spec. The RF discovery is a cyclic activity which activates various modes of operation. This consists of a loop which alternates two phases: The polling and the listen phases. In the polling phase, the PN7150 acts as Reader or NFC Initiator for the P2P mode, searching for passive tags or an NFC target device. If no card or target was detected, it enters a listening phase, to potentially be activated as card or P2P target If no device to interact is detected in the polling or listening phase, it switches back to polling phase after a timeout. All RF technologies supported by PN7120 can be independently enabled within this discovery loop. However, the PN7120 is in poll phase generates RF field and consumes current. Therefore, the more technologies to be polled, the larger the average current consumption. Multi-audio speaker prototype: RF dscovery configuration To enable the speaker-to-speaker pairing functionality, each of the speakers needs: To have the capability to discover a remote speaker and initiate a pairing operation. Or the other way around, be discovered by a remote speaker to complete a pairing operation. To accomplish this, the speakers need to sequentially move from polling and listening phases. As such, the discovery loop configured in the application iterates between reader, P2P and card modes.During the polling phase, the speaker generates an RF field, and uses an NFC-A polling sequence looking for: A remote card or device in card emulation. If found, the NDEF data with the pairing info will be retrieved and processed. Next, it looks for a remote P2P device. If found, it pushes an NDEF message with the pairing info to this remote peer. On the other hand, during the listening phase, the speaker turns off its RF field and waits to be discovered by a remote device: If it is discovered while operating as P2P target, it will pull an NDEF message coming from the remote speaker. If it is discovered while operating in card mode, its NDEF message will be read by the remote speaker. The precise communication that takes place between the two speakers will differ every time. It will depend on the polling loop status of both speakers at the instant they are tapped. Application logic Until now, we have described how both speakers are discovered, and therefore, how they can start a communication to exchange pairing data via NFC. The next step is to  describe which data and which data format is used to exchange the pairing details. NFC Forum specifications The NFC Forum organization defined a set of specs explaining how to exchange pairing data over NFC in an interoperable way with just a tap, independent of the manufacturer and without installing any dedicated application for it. These are: Connection handover: This spec defines how two NFC devices can negotiate and activate an alternative communication carrier.  NDEF: The NDEF spec defines a message format to exchange data between NFC devices, including pairing data. Tag 1 Type to Tag 5 Type specs: These specs define how NFC devices can interact with five different types of tag technology. As a result, any NDEF message store in any of these five types of tags will be processed by any NFC-compliant device. NFC pairing: Static handover As mentioned earlier, how pairing data is transferred between the two speakers will depend on the discovery loop status. The static handover takes place when: One speaker is in reader mode / polling mode. (left hand side) The other speaker is in card mode / listening mode, showing a Type 4 Tag with an NDEF message on it (right hand side). The process is as follows: The speaker in reader mode activates RF field and generates a NFC-A polling sequence. The remote speaker in card mode responds to the polling command. The reader retrieves the NDEF data from the remote speaker, using the commands as defined in Type 4 tag NFC forum spec. The reader processes the carrier data from the NDEF message and establishes a BT connection according to BT protocol. The speaker in card emulation mode deploys a Handover Select NDEF record, advertising its BT carrier. In The NDEF message, we store: The BT device address (MAC address) Bluetooth local name (Friendly name for the user) Class of the device (e.g. headset, mobile, etc) This is the carrier data that will be used by the application to trigger the BT connection. After this proces, both devices start streaming music over BT. NFC pairing: Negotiated handover The other possibility is that when both speakers are tapped, they find themselves during the P2P operation. In such a situation, the pairing process will be conducted according to the Negotiated handover mechanism. One of them will take the role of initiator, the other the target role: The initiator will poll for target devices The target will respond to the initiator command The initiator will send a handover request message, with the carrier details The target will respond with a handover select message, indicating the selected carrier option. On the received data, the initiator will establish a connection according to BT protocol. After that, both devices start streaming audio over BT. In this case, both speakers exchange data with their alternative carrier capabilities, could be more than one. The initiator communicates to the target device its carrier capabilities with a Handover request record followed by an NDEF record per each available carrier (in this case, just one BT carrier). After that, the target replies to the initiator with the selected carrier to be used for the out of band data transfer. As before, the BT configuration in the NDEF message includes fields such as: BT address, device class, BT local name, and optional data if secure pairing according to BT spec is required.The key here is that, this negotiation protocol and these message formats are specified and defined in the NFC Forum specs, so they offer an interoperable solution for any compliant-platform Support package  This section details resources and information provided by NXP you can use to replicate your own multi-audio speaker solution with NFC pairing capabilities. PN71xx family of NFC controllers PN71xx family are solutions integrating an RF frontend together with an embedded microcontroller with dedicated FW and NCI interface. They fully comply with the NFC Forum, include Linux®, Android™, and WinIoT drivers and sample code for bare metal and RTOS integration. Additionally, they support direct supply from a battery, different power states and an ultra-low power polling loop. Their features make it ideal for NFC integration into any application, especially those with OS system. Hardware support From a hardware point of view, several demokits are available to evaluate PN71xx family. They interface into popular platforms, such as: Raspberry Pi BeagleBone Black Any board featuring an Arduino compatible header like LPCXpresso or Kinetis Freedom among others. In case you have to evaluate PN71xx into any other platform, these kits can be reused, The PN71xx board provides all required signal pins easily accessible so that you can design and build your own interface board for your target platform. Software support From a software support point of view,  device manufacturers can easily integrate PN71xx family in Linux, Android and Win IoT systems through the available SW drivers. But also, NXP supplies a set of code examples running on LPC and Kinetis MCUs for Bare metal RTOS integration. Precisely, the demo presented in this post, leverages on the NullOS/RTOS SW examples. The software example for PN71xx integration into RTOS / Bare metal system is made of 3 components: The NXP-NCI module offers an API for configuring, starting and processing the NFC device discovery The NDEF library offers an API for processing NDEF data over reader, card and p2p modes: The transport mapping layer providing HW abstraction for the host – NFC controller connection On top of it, developers can implement their own application. Available resources PN7120 product website: www.nxp.com/products/:PN7120 PN7120 demokits: www.nxp.com/products/:OM5577 PN7120 product website: http://www.nxp.com/products/:PN7150 PN7120 demokits: www.nxp.com/products/:OM5578 Reference source code and related documentation: https://www.nxp.com/doc/SW4325 and http://www.nxp.com/docs/en/application-note/AN11990.pdf  Video recorded session
記事全体を表示
Description A bicycle with an integrated electric motor and a rechargeable battery, making it an eco-friendly, zero-emission vehicle ideal for smart cities. An important feature of an E-Bike is that it must be reliable and can be used for long periods.   Block Diagram   Products Category Name 1: Microcontroller Product 1 URL 1 https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/ke-series-cortex-m4-m0-plus/kinetis-ke02-20-mhz-entry-level-microcontrollers-mcus-based-on-arm-cortex-m0-plus-core:KE02 Product 1 Description 1 The Kinetis KE02 includes a powerful array of analog, communication and timing and control peripherals with specific flash memory size and the pin count. The K02 acts as a low-power, high-robustness, and cost-effective microcontroller with one 6-channel FlexTimer/PWM and two 2-channel FlexTimer/PWM. Product 2 URL 1 Arm® Cortex®-M4|Kinetis® K64 120 MHz 32-bit MCUs | NXP  Product 2 Description 1 Kinetis ®  K64-120 MHz, 256 KB SRAM Microcontrollers (MCUs) based on Arm ®  Cortex ® -M4 Core   Category Name 2: Gate driver Product 1 URL 1 https://www.nxp.com/products/power-management/motor-and-solenoid-drivers/bldc-h-bridge-stepper/3-phase-brushless-motor-pre-driver:GD3000 Product 1 Description 1 The GD3000 is a gate driver IC for three-phase motor drive applications providing three half-bridge drivers, each capable of driving two N-channel MOSFETs.   Category Name 3: LED Driver Product URL 1 https://www.nxp.com/products/power-management/lighting-driver-and-controller-ics/ic-led-controllers/16-channel-fm-plus-ic-bus-57-ma-20-v-constant-current-led-driver:PCA9955BTW Product Description 1 The PCA9955B is an I2C-bus controlled 16-channel constant current LED driver optimized for dimming and blinking 57 mA Red/Green/Blue/Amber (RGBA) LEDs in amusement products. Each LED output has its own 8-bit resolution (256 steps) fixed frequency individual PWM controller that operates at 31.25 kHz with a duty cycle that is adjustable from 0 % to 100 % to allow the LED to be set to a specific brightness value.   Category Name 4: Logic USB Type-C Configuration Channel Product URL 1 https://www.nxp.com/products/interfaces/usb-interfaces/usb-type-c-true-plugn-play/usb-pd-phy-and-cc-logic/cc-logic-for-usb-type-c-applications:PTN5150 Product Description 1 PTN5150 is a small thin low power CC Logic chip supporting the USB Type-C connector application with Configuration Channel (CC) control logic detection and indication functions. The PTN5150 enables USB Type-C connector to be used in both host and device ends of the Type-C cable   Category Name 5: Current-Limited Power Switch Product URL 1 https://www.nxp.com/products/power-management/load-switches/usb-pd-and-type-c-current-limited-power-switch:NX5P3290UK Product Description 1 The NX5P3290 includes under-voltage lockout, over-temperature protection, and reverse current protection circuits to automatically isolate the switch terminals when a fault condition occurs.   Category Name 6: Secure Product 1 URL 1 A71CH | Plug and Trust for IoT | NXP  Product Description 1 Plug and Trust - The fast, easy way to deploy secure IoT connections   Category Name 7: NFC Product 1 URL 1 PN5180 | Full NFC Forum-compliant frontend IC | NXP  Product Description 1 Full NFC Forum-compliant frontend IC   Category Name 8: GPIO Expander Product 1 URL 1 PCAL6534 | Level translating GPIO Expander | NXP  Product Description 1 Ultra-low-voltage, level translating, 34-bit I2C-bus/SMBus I/O expander   Category Name 8: NFC smartcard Product 1 URL 1 https://www.nxp.com/products/rfid-nfc/mifare-hf/mifare-desfire/mifare-desfire-ev2:MIFARE_DESFIRE_EV2_2K_8K Product Description 1 Secure, contactless multi-application IC with an enhanced feature set for Smart City applications Related Documentation   Document URL Title https://www.nxp.com/docs/en/application-note/AN10439.pdf Wafer-level chip-scale package https://www.nxp.com/docs/en/application-note/AN5322.pdf AN5322, TPMS wheel location introduction and main concepts Training Training URL https://community.nxp.com/docs/DOC-341509 Related Demos from Communities URL Kinetis Microcontrollers  MCUXpresso SDK  MCUXpresso Software and Tools  UAV Speed Control with Kinetis KV5x Cortex-M7 MCU and GD3000 Motor Pre-Drivers   
記事全体を表示
This post entry provides a detailed description of how to port the NFC Reader Library to Kinetis K64F MCU. It is used a real porting example exercise to show the steps required to adapt the NFC Reader Library to a sample target MCU. The goal of this post is to serve as a guide for software developers requiring to port the NFC Reader Library to their MCU of choice for their designs. NFC Reader Library overview The NFC Reader Library is a software stack for creating and developing contactless applications for NXP’s NFC frontends and NFC controllers with customizable firmware. This library provides an API facilitates the most common operations required in NFC applications such as: reading or writing data into contactless cards, exchanging data with other NFC-enabled devices or emulating cards. The NFC Reader Library: It is based on a modular approach It has been designed with a flexible and multilayered architecture It is written in ANSI-C programming language It is supported in multiple design environments and platforms and it has been developed with a strong focus on portability. It is available for free download. The NFC Reader Library v5.02.00 currently supports: All our NFC frontends (CLRC663 plus PN5180) and PN7462 NFC controller. Their corresponding development boards, used as NXP reference HW (CLEV6630B, PNEV5180B, PNEV7662B) And built-in MCU support for LPC1769, LPC11U68, FRDM-K82F and Raspberry Pi. In addition, the release includes several examples to get familiar with the library and which can be used as reference for your developments and, it is also included an HTLM-based API documentation for all the components, which is generated from source-code annotations. NFC Reader Library architecture The NFC Reader Library is encapsulated into layers, differentiated by colors, and components, differentiated in boxes. From top to bottom, we have: The Application Layer (AL), which implements the command sets to interact with MIFARE cards and NFC tags. The NFC activity, which implements a configurable Discovery loop for the detection of contactless cards, NFC tags or other NFC devices. Next to it, the HCE and P2P components, for the emulation of Type 4 tags and P2P data exchange respectively. The protocol abstraction layer (PAL), which contains the RF protocol implementation of the ISO14443, Felica, vicinity and NFC standards. One level down, the hardware abstraction layer (HAL), which implements the drivers for controlling the NFC frontends RF interface and capabilities. Below, the Driver Abstraction Layer (DAL), newly introduced in the latest release, which implements the GPIO pinning, the timer configuration and the physical interface (BAL) between the host MCU and the reader IC. Finally, the OSAL module, in charge of abstracting the OS or RTOS specifics (handles tasks such as timers, events, semaphores and threads) This layered architecture is helpful for several reasons: The eleven software examples, the Application Layer (AL) and the Protocol Abstraction Layer (PAL) are HW-independent, so that can be used on top of any NFC frontend. The the Application Layer (AL), the Protocol Abstraction Layer (PAL) and the Hardware Abstraction Layer (HAL) are platform-independent, so that can run in any MCU without any additional change. In case the reader MCU is part of the built-in support, the examples can be directly imported and executed straight forward. On the other hand, in case the reader MCU is not supported by default, the major advantage is that only adaptations in the DAL and OSAL layers are required, while the rest of the layers can be used without any modification. The NFC Reader Library structure can be seen more clearly when imported in the MCUXpresso development environment. After completing the import wizard, all projects are listed in the “Project Explorer” window. As can be seen in the screenshot, it contains different folders: API documentation folder Driver Abstraction Layer FreeRTOS support The platform support (in the screenshot, corresponding to the LPC support) The software examples (11) The Reader Library implementation And the OS abstraction layer NFC Reader Library porting to FRDM-K64F steps In the existing NFC Reader Library v5.02.00 release there is no native support for Kinetis K64F. However, it is included a pre-compiled package for Kinetis K82F MCU. We use the K82F NFC Reader Library package as a reference project to start the porting to K64F MCU. This package can be downloaded from www.nxp.com/pages/:NFC-READER-LIBRARY. The steps required to port the library to Kinetis K64F are: Prearing the HW (i.e the pining between the Kinetis and the NFC reader board). Setting up the development environment (i.e workspace). Perfoming some changes in project configuration settings Performing some code modifications in the DAL and application code for adding Kinetis K64F support. NFC Reader Library porting to FRDM-K64F - Preparing the hardware The hardware used for this porting exercise is: A CLEV6630B board (CLRC663 plus) as an NFC transceiver  A FRDM-K64F board (Kinetis K64F) as host MCU, used to load and run the application logic. The CLRC663 plus evaluation board is connected by default to an LPC1769 µC via SPI. However, the board is made in such a way that the LPC1769 MCU can be bypassed to connect an external MCU easily. For doing so: Six resistors from the board need to be removed. These are highlighted in red. Use the SPI pin connectors available on the left hand side, on the board edge. Next, to connect the two boards together, the pining routing was done as follows: We use the Kinetis K64F jumper 2 pin line for the MOSI, MISO, chip select and clock lines of the SPI communication. The IRQ, interface selection and reset pins of CLRC663 plus are connected in jumper 1 pin line. And, one ground pin used for reference. Therefore no complex HW manipulation was required since all interfaces are easily accessible via dedicated headers or test points. NFC Reader Library porting to FRDM-K64F - Setting up the development environment Once the HW connection is prepared, we can move to setting up the development environment and workspace. Get the latest NFC Reader Library release From the software perspective, first we need to download the latest NFC Reader Library package. To do so: Go to NXP dot com slash pages slash NFC Reader Library (www.nxp.com/pages/:NFC-READER-LIBRARY) Go to the Downloads tab and click on the download button Click download on the NFC Reader Library for Kinetis K82Fpackage. Generate a downloadable SDK package for FRDM-K64F board As part of the NXP support, an SDK with drivers, middleware, RTOS demos and more is available for any of its Kinetis and LPC micros.We need to build the corresponding one to K64F SDK. For that: Navigate to www.mcuxpresso.nxp.com and select SDK builder option. Then, use the drop-down menus to customize your SDK configuration, middleware and optional software components be included in the package. Select Request build. In a few minutes, you will receive an email with a link to download the SDK package, very similar to the one showed in the figure below. Import the NFC Reader Library into MCUXpresso workspace Next step to configure the development environment is to import the library package in the workspace. The easiest way is to use the Quick Start Panel on the left hand side. Click on Import project from file system Then, browse the library package in your file system. Click Finish to import it all to your workspace. Install and link FRDM-K64F SDK into MCUXpresso workspace The last step is to import the K64F customized SDK we configured from the MCUXpresso tools. To do so: Just drag and drop the SDK into the installed SDKs tab of the MCUXpresso IDE. (It will appear in the bottom part, in the center) Import the SDK into the workspace and link it with the software examples. It will appear as another folder in the project explorer window. If the K64F SDK has been properly imported in the workspace, we should see a new drop-down menu for K64F. From there, we should select K64F and click Apply so that the memory details for K64F are set to the project example NFC Reader Library porting to FRDM-K64F - Project configuration changes At this point we have the hardware and the workspace for software development ready. In this step, we will start porting the NfcrdlibEx1_BasicDiscoveryLoop  software example provided as part of the NFC Reader Library release. Select FRDM-K64F SDK in the project MCU settings One of the first configurations to be changed is the project MCU settings. These settings indicate which target host device is running the application code. These settings can be found if: You right click on the project example > Properties In the left-hand list of the Properties window, open “C++ build” and select “MCU settings” In the right-hand panel, we can observe the corresponding settings for K82F micro. The left figure indicates the project configuration settings used by the default SW example prepared for K82F while the right figure indicates the final project configuration settings used by the SW example ported to K64F. Define FRDM-K64F SDK preprocessor symbols in the project After that, we need to change the compiler preprocessor settings, which can be found in C++Build > Settings. In the project examples of the NFC Reader Library, the conditional directives like #ifdef and #ifndef are used to include or exclude portions of the code from the actual compilation. The conditional codes are included in the program compilation only if the MACROs are defined in the project compiler preprocessor settings. In the left side we can see the defined macros for the original project. Among them, includes one which defines that the HW used is PN518 and K82F board. Therefore, in the ported project, we need to replace the macros corresponding to K82F with the new ones corresponding to K64F.  For instance, the PHDRIVER_K64_CLRC663 macro includes in the compilation the files related to the new HW used in the ported project (for the board pin and GPIO config, SPI settings or timers). Precisely, these files are included inside BoardSelection.h file in the Driver Abstraction Layer (DAL). Add include paths for FRDM-K64F SDK files When including header files into our project, the compiler must be told which directories must be searched to find those files. To do this: Open the project properties. In the left-hand list, open “C++ Build” and Select “Settings”. In the right-hand pane, choose the “Includes” section. Click the “Add icon”. In the left figure, we see the compiler include paths for the K82F SDK of the original example. In the ported example, the K64F SDK sources will not yet compile since we did not tell the compiler about all the new include paths. Therefore, we need to add the new include paths pointing to the K64F SDK and put them into the MCUXpresso IDE project. In the right figure, you can see the paths we included for this purpose. Mainly, these paths reference to the board system init, board drivers, CMSIS files and debug utils. Add include path for FRDM-K64F MCU assembler The last MCUXpresso settings to be changed is in the MCU Assembler. This can be found in the right-hand panel, choose the “MCU Assembler” and select “General”. In the original source code, a path is used to the K82F SDK. In the ported example, we just need to remove the previous include path and replace it with the corresponding one pointing to the K64F SDK in our workspace. NFC Reader Library porting to FRDM-K64F - Code changes So far, we have the HW, the development environment prepared and the project configuration settings changed. At this point, there are only a few code changes to be done before the porting is completed and the software example can be run in K64F. DAL driver adaptation for FRDM-K64F The layered architecture of the NFC Reader Library makes porting easier since only the lower drivers need to be adapted. This driver includes functions for: The physical link connection establishment between the CLRC663 plus and K64F The init functions for timers and interrupts so they are correctly used by the application layer. Going to the NfcrdlibEx1-BasicDiscovery loop project structure, it contains several folders. If we open the DAL > board folder, we can observe one source file per each supported platform (LPC with PN5180 and CLRC663, and the same for Raspberry Pi and Kinetis K82F). Our task for the porting would be to create an equivalent source file for the new supported board, the K64F together with the CLRC663 (e.g. Board_FRDM_K64FRc663.h). This file includes The related board pin and GPIO configurations The SPI configuration The timer configuration In addition, we need to include the board, pin_mux and clock config files. Use SDK examples to get FRDM-K64F board specific configuration Implementing these board specific files, in some cases, could be time consuming and may require experience. However, you do not need to do so but rather use the existing source files. For that, you can use any of the existing SDK software examples. You can easily import one SDK example by: Clicking the “Import SDK” example in the quick start menu > select the FRDM-K64F board. Selecting the demo example. Each example application has its own unique copy of the board, pin mux, and clock config files that you can reuse for the porting (Note: this process could be different depending on the MCU used). Add FRDM-K64F macro definitions in the source code Next, along the project tree, we need to add the #ifdef directives, indicating that K64F board files that need to be compiled. This is the case for: The BoardSelection.h file The ph_NxpBuild_App.h, which links the board with the reader IC by enabling the CLRC663 plus module in the HAL layer. The ph_AppInit.h so that the board is initialized when the reader device boots. Add FRDM-K64F CPU initialization code The ph_AppInit.h  file takes care of the code initialization and code specific to the HW used to run the example. As part of this ph_AppInit.h file, there is a function in charge of initialization the host MCU. Here, we need to implement the corresponding function for the K64F init, based on the SDK example source code selected earlier. If we look within this routine, we actually find functions for: Configuring the MCU clocks. Configuring the MCU pins. Configuring the interrupts (PIT). NFC Reader Library porting to FRDM-K64F: NfcrdlibEx1_BasicDiscoveryLoop execution After following the previous steps, the source code is succesfully ported to K64F. The following video demonstrates the correct execution of the NfcrdlibEx1_BasicDiscoveryLoop example in FRDM-K64F host MCU connected to CLRC663 plus NFC frontend (CLEV6630B). The video includes a webcam, which records the HW, including all the witing wiring between the K64F and the CLRC663 plus antenna. After the code is built and compiled, the video shows how some tags are tapped to validate that the example is working as expected (tag's UIDs are displayed in the MCUXpresso console). . General considerations to port the NFC Reader Library to your target MCU Overall, the general steps required to port the NFC Reader Library to your target MCU are: Adapt the MCU drivers to the DAL layer in the NFC Reader Library. This typically includes: timers, interrupts, pining and host interface configuration between the NFC reader and host MCU sides. Adapt the OS layer (i.e. you might need to port the FreeRTOS or to your target OS platform). Adapt the source code examples: project settings (macros, include paths, MCU configuration) and perform the required code modifications (Code for HW initialization, board files, etc). Available resources NFC Reader Library:  www.nxp.com/pages/:NFC-READER-LIBRARY CLRC663 plus: www.nxp.com/products/:CLRC66303HN CLRC663 plus development kit: www.nxp.com/demoboard/OM26630 FRDM-K64F board: www.nxp.com/demoboard/FRDM-K64F Video recorded session
記事全体を表示
  Overview With the expansion of IoT technologies, it is required to count with special devices that allow, to the users, to count with the necessary tools to develop IoT-related projects in order to acquire an edge that allows improvement and optimization in the execution of any task. Use Cases IoT Gateway / Communication HUB devices can be used to work with: Cloud Services Network commissioning Encrypted Data Storage Block Diagram Block-Diagram-IoT Gateway Communication HUB-PNG.png Product Category MCU Product URL LPC540XX: Power-Efficient Microcontrollers (MCUs) with Advanced Peripherals Based on Arm® Cortex®-M4 Core  Product Description Offering flashless design and security integration, the LPC540xx family of MCUs combines a 180 MHz Arm® Cortex®-M4 core with a power-efficient and unique architecture, advanced HMI and flexible communication peripherals for real-time performance in the next-generation IoT.   Category NFC Product URL CLRC663 plus family: High-performance NFC frontends  Product Description If you need high NFC performance or the lowest power consumption, use this remarkably efficient yet highly flexible frontend family to push your design further.   Category Secure Product URL A71CH: Plug and Trust - The fast, easy way to deploy secure IoT connections  Product Description A71CH is a ready-to-use secure element for IoT devices providing a root of trust at the IC level and delivers, chip-to-cloud security right out of the box, so you can safely connect to IoT clouds and services, including AWS, IBM Watson IoT™ Platform, and Google Cloud™ IoT Core without writing security code or exposing keys.   Category Wireless Product URL JN5169: ZigBee and IEEE802.15.4 wireless microcontroller with 512 kB Flash, 32 kB RAM  Product Description The JN5169 is an ultra low power, high performance wireless microcontroller suitable for ZigBee applications.
記事全体を表示
Overview New technologies added to existing applications like Elevators, help improve user experience, quality and safety. This application summary focuses on the human machine interface of the elevator in cabin control and floor control modules. NXP ®  technologies and products enhance different features, like NFC for access control, 2-wire Ethernet provides floor to floor connectivity, and PMICs provide power supply with safety features. With NXP’s wide connectivity portfolio, Elevators can have wireless cloud connectivity as back-up communication channel that supplement cellular radio communication for data logging, monitoring & maintenance or even to handle emergencies. Block Diagram Elevator Cabin Control Module Elevator Control Module Recommended Products Category Link MPU i.MX 8M Applications Processor | Arm® Cortex®-A53, Cortex-M4 | 4K display resolution | NXP  MCU i.MX RT1050 MCU/Applications Crossover MCU| Arm® Cortex-M7, 512KB SRAM | NXP  Audio Amp Audio Amplifiers | NXP  PMIC 12-channel configurable PMIC | NXP  LED Controller LED Drivers | NXP  CAN Transceiver TJA1051 | High-speed CAN Transceiver | NXP  Ethernet PHY Automotive Ethernet PHY Transceivers | NXP  MiFARE SAM MIFARE SAM AV3 | NXP  Signal Conditioner MSDI | NXP  CD1020|Multiple Switch Detect Interface | NXP  Contact Reader Low power single card reader | NXP  NFC Controller CLRC663 plus family | High-performance NFC frontends | NXP  MiFARE DESfire MIFARE DESFire | NXP  Safety Power Management FS4500 | fail silent safety SBC compliant grade1 & grade 0 automotive qualification | NXP  Voltage Level Translator Voltage Level Translators (Level Shifters) | NXP  Motor Drivers BLDC, H-Bridge, and Stepper Motor Drivers | NXP 
記事全体を表示
NXP Content: PN7462, NTAG I²C plus NXP Recommends: PN7462, NTAG I²C plus The NFC Cube is a universal demo with which all 3 basic NFC operation modes can be shown: Interaction between a device and a card or tag Interaction between 2 electronic devices (NFC as cable replacement) Interaction between a device and an NFC phone Value Propositions The NFC Cube is a universal NFC demo Support Under https://nxp.box.com/NFCcube you find more information and a video showing the NFC Cube in action.
記事全体を表示