Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
Example S32K312 ADC DS3.5 RTD300 *******************************************************************************  The purpose of this demo application is to present a usage of the  ADC_SAR IP Driver for the S32K3xx MCU.  The example uses the PIT0 trigger to trigger  conversions on ADC1.  ADC channels  are selected to be converted on  ADC-1:  ADC channel S10 is connected to board's potentiometer. #define ADC_SAR_USED_CH_BANDGAP 48U /* Internal Bandgap Channel */ #define ADC_SAR_USED_CH_POT_0 34U  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
查看全文
Connecting camera and LCD to i.MX RT EVKs This guide will walk through how to do connect the camera and LCD modules to i.MX RT boards and how to test to ensure the camera and LCD are connected properly. Update May 2022: There are now updated versions of these LCD panels that have an impact on software. See this post for more details. The physical connections are the same for both the original and new panels however so there are no changes to this guide. This first part of this guide is for the i.MX RT1050, i.MX RT1060, i.MX RT1064 EVKs. The second part of this guide is for i.MX RT595, i.MX RT1160 and i.MX RT1170 EVKs.  Part 1: Camera and LCD for i.MX RT1050, i.MX RT1060, and i.MX RT1064:  The camera used by the RT1050, RT1060, and RT1064 EVKs are the same. However this camera only comes with the RT1060 and RT1064 EVKs. There are alternatives available for the RT1050 as discussed in this blog post.  The LCD screen compatible with these boards is the RK043FN66HS-CTG  Camera:  1) The camera connector is on the front of the board. Flip the black connector up so it's 90 degrees from its original position.  2) Then slide in the flat ribbon connector of the camera 3) Flip the black connector back down. It should keep the ribbon cable snug. LCD: 1) On the back of the board, slide the black connector for the LCD ribbon forward. 2) Then slide in the flat LCD ribbon cable underneath the black connector. 3) Slide the black connector back to its original position. The cable should be snug. 4) Do the same for the touch controller connector and slide the black connector forward Then insert the cable between the black connector and the white top so that the cable is in the middle. It might take a few tries as its somewhat difficult. You could also use needle nose pliers to help guide in the cable but be careful about damaging the cable. 5) Then slide the black connector back to the original position. The cable should be snug. 6) It should look like the following when complete. Testing: 1) To test the camera and LCD, use the CSI driver examples in the MCUXpresso SDK.  2) The camera will likely be out of focus the first time you use it. Adjust it by rotating the lens clockwise until the image is in focus. You can use your fingers or some needle nose pliers. It could take up to two rotations and it should turn easily. Also remove the plastic cover.  3) To test the touch controller, use the emwin temperature control example in the MCUXpresso SDK Tape: 1) Once the LCD has been confirmed to work, you can use two layers of thick double sided foam tape to securely attach it to the board.  Part 2: Camera and LCD for i.MX 700, i.MX RT595, i.MX RT1160 and i.MX RT1170 EVKs:  The i.MX RT1160 and i.MX RT1170 EVKs both come with a OV5640 MIPI camera module in the box.  The LCD screen compatible with the i.MX RT1160, i.MX RT1170, i.MX RT595, and i.MX RT700 is the RK055HDMIPI4MA0 and it can be found here.  There are multiple alternative names for this panel and all these names refer to the exact same panel: RK055HDMIPI4MA0 RK055MHD091 RK055MHD091-CTG RK055MHD091A0-CTG Instructions for i.MX RT1170 are below: i.MX RT1170-EVK Camera:  1) The camera connector is on the front of the board at J2. It connects by simply pressing the camera down onto the connector. It takes a bit of force but should not be too difficult.  i.MX RT1170-EVK LCD: 1) On the back of the board, slide the black connector (J40) for the LCD ribbon forward towards the edge of the board.  2) Then carefully slide in the flat LCD ribbon cable into the connector. The blue writing should be facing up like in the photo. It should go above the black part of the connector that you just slid out, and under the white part of the connector.  3) Slide the black plastic connector back to its original position. The cable should be snug if pulled. It should look like the following:  i.MX RT1170-EVK Power: 1) If using the LCD, then the external power adapter must be used with the board. Connect the barrel connector to J43 on the board. 2) Also change the jumper on J38 to be on pins 1-2 so that it uses the external power.  3) Connect a micro-USB cable to J11, which will cause the board to enumerate as a COM port and as a debug interface for downloading and debugging code i.MX RT1170-EVK Camera and LCD Testing: 1) To test the camera and LCD, use the csi_mipi_rgb_cm7 driver example that can be found in the MCUXpresso SDK for i.MX RT1170. The camera input should be displayed on the LCD screen if everything is connected properly.   Re: Connecting camera and LCD to i.MX RT EVKs Thanks for this guide.
查看全文
S32 Design Studio for S32 Platform 3.3 を使用した実行中のターゲットへの接続 (アタッチ) 一般的なデバッグセッションは、コードをFlashにダウンロードし、main()以降でデバッグすることから始まります。ただし、すでに実行中のシステムを探索するには、コードの実行に影響を与えることなく、ターゲットMCUにデバッグ接続(アタッチ)を行うことができます(少なくとも、ユーザーがMCUの停止を選択するまでは)。   注: 実行中のターゲットのソース レベルのデバッグは、アタッチするプロジェクトのソースがターゲットで実行されているバイナリ コードと完全に一致する場合にのみ可能です。   ツールバーの [(Debug As)] ボタンをクリックし、ドロップダウン メニューから [Debug Configurations ] をクリックします。 [デバッグ構成] ダイアログ ボックスの左側のウィンドウで、プロジェクト設定で指定されたデバッグ インターフェイスを展開し、必要な起動構成をクリックします。 左側のウィンドウで構成をクリックすると、構成設定がタブにグループ化されて右側のウィンドウに表示されます。 PEmicro(ピーマイクロ) [スタートアップ] タブを選択し、次のように [実行中のターゲットにアタッチ] チェック ボックスを設定します。 デバッグ接続が確立されると、ターゲットは一時停止するまで実行を続けます。 セガーJリンク [デバッガー] タブを選択し、次のように [実行中のターゲットに接続] チェック ボックスを設定します。 残念ながら、この機能は現在サポートされていません。 デバッグ | フラッシュプログラミング Eclipse IDEの使用と設定
查看全文
How to use the NanoVNA for the board OM29263ADK      This document mainly describes how to use NanoNVA tool to do antenna tuning on OM29263ADK with CLEV663B/PN5180B board. Please refer to the application note AN12810(https://www.nxp.com/docs/en/application-note/AN12810.pdf) about the NanoVNA tool. And please refer the user manual UM11098 (https://www.nxp.com/docs/en/user-guide/UM11098.pdf) about OM29263ADK. After setting NanoVNA tool with reference to the above documents. Firstly, take the small antenna of OM29263ADK with CLEV663B as an example. The small antenna can be directly connected and used on the CLEV6630B。the antenna board can be directly connected to the CLEV6630B without any additional modification, after the original antenna had been removed (cut off). The result of the antenna tuning with NanoVNA tool as the below: Second, take the small antenna of OM29263ADK with PN5180B board as an example. Follow the UM11098 steps as the below: (a) the EMC filter cut off frequency must be adjusted, and (b) the DPC and related features should be disabled, since the antenna is asymmetrically tuned and the DPC is not used. (a) The original antenna uses a symmetrical tuning, which uses an EMC filter with L0 = 470nH and C0 = 253pF (220pF + 33pF). The inductor as well as the first part of the capacitance (220pF) are assembled on the main board. To operate the OM29263ADK antenna, the C0 (220pF) on the PNEV5180B must be replaced by a 68pF. (b) The DPC and its related features should be disabled to operate an asymmetrical antenna. If can’t get the card information please refer to the AN11740’s related steps to achieve a good sensitivity of RxP/RxN path. The result of the antenna tuning with NanoVNA tool as the below: The whole process of the small antennas tuning of OM29263ADK with CLEV66B/PN5180 with NanoVNA is completed. PS: It is the similar with the steps for the large antennas tuning of OM29263ADK with CLEV66B/PN5180 with NanoVNA.  
查看全文
S32G2 support guide S32G2 support guide (rev0.1, 070521) 1. If you have any technical issues encountered when using NXP S32G-VNP-RDB2 or S32G-VNP-GLDBOX, these can be discussed and covered on the S32G product forum. 2. You can also submit your ticket through the nxp.com website here 3. We also provide professional services and support as per cases beyond standard supports, please contact your NXP sales representative in your region for more options
查看全文
NXP Model-Based Design Toolbox for S32M2xx – version 1.0.0 Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for S32M2xx – version 1.0.0 RTM The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32M2xx version 1.0.0. This release supports automatic code generation for S32M2xx peripherals and applications prototyping from MATLAB/Simulink for NXP S32M2xx Automotive Microprocessors. This new product adds support for S32M41, S32M242, S32M43,  S32M244, S32M274, S32M276 MCUs and part of their peripherals, based on RTD MCAL components (ADC, AE, DIO, CAN, DPGA, GDU, GPT, MCL, PWM, MCU, PORT, QDEC, UART). In this release, we have also added support for FreeMASTER, AMMCLib, and MATLAB support for the latest versions. The product comes with over 60 examples, covering all supported peripherals, and Simulink simulation modes Software-in-the-Loop, Processor-in-the-Loop, and External Mode. Target audience: This product is part of the Automotive SW – S32M2 Standard Software Package. FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=3785898 Technical Support: NXP Model-Based Design Toolbox for S32M2xx issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt     Release Content Automatic C code generation from MATLAB® for NXP S32M2xx derivatives: S32M241 S32M242 S32M243 S32M244 S32M274 S32M276 Support for the following peripherals (MCAL components): ADC AE DIO CAN DPGA GDU GPT MCL PWM MCU PORT QDEC UART Provides 2 modes of operation: Basic – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced – using S32 Configuration Tool or EB Tresos to configure peripherals/pins/clocks Integrates the Automotive Math and Motor Control Library version 1.1.34: All functions in the Automotive Math and Motor Control Functions Library v1.1.34 are supported as blocks for simulation and embedded target code generation. Integration with FreeMASTER We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications. Support for MATLAB® versions R2021a R2021b R2022a R2022b R2023a R2023b Support for custom board initialization Toolbox generates the components’ peripherals initialization function calls as configured in the Board Initialization window, which can be customized to each Simulink model. This feature allows users to set a custom order for the components initialization, the insertion of the Custom code sequences, or share the custom initialization with multiple Simulink models via the Export and Import functionality.     Support for custom default project configuration The toolbox provides support for users to create their custom default project configurations. This could be very useful when having a custom board design – only needing to create the hardware configuration once. After it is saved as a custom default project, it can be used for every model that is being developed. Integration with S32 Config Tools version v1.7:     Integration with S32 Design Studio The toolbox automatically generates the _Config folder, next to the Simulink model location, providing the user the opportunity to easily import the generated code from Simulink into S32 Design Studio. Each time the code is generated, the _Config folder is updated with the new changes. The toolbox also provides a mechanism to launch an S32 Design Studio instance, with the imported generated code project in the Project Explorer tab from S32DS. Simulation modes: We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) External mode Support for profiling in PIL mode: Examples for every peripheral/function supported: We have added over 60 examples, including: CDD Blocks (Ae, Dpga, Gdu, Mcl, Qdec) Communication (Can, Uart) AMMCLib IO Blocks (Adc, Dio, Pwm) ISR Blocks (Hardware Interrupt Handler) MCAL Blocks (Gpt) Utility Blocks (FreeMASTER) Software-in-the-Loop / Processor-in-the-Loop / External mode For more details, features, and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32M2xx MCUs and evaluation board solutions out-of-the-box with: Model-Based Design Toolbox for S32M2xx version 1.0.0 is fully integrated with MATLAB® environment in terms of installation:   Target Audience This release (1.0.0) is intended for technology demonstration, evaluation purposes, and prototyping of S32M2xx MCUs and Evaluation Boards.   Useful Resources Examples, Training, and Support: https://community.nxp.com/community/mbdt Re: NXP Model-Based Design Toolbox for S32M2xx – version 1.0.0 When I click on the following "Go to NXP Download Site" button: It redirects me to the page below: Can you provide a location that I can download the S32M2xx Model-Based Design Toolbox? Re: NXP Model-Based Design Toolbox for S32M2xx – version 1.0.0 S32M2 ,with out   externel boost   power is  ? 回复: NXP Model-Based Design Toolbox for S32M2xx – version 1.0.0 And I still can't find the correct URL when I click on the link on this Matlab script. 回复: NXP Model-Based Design Toolbox for S32M2xx – version 1.0.0 Hello, I have encountered the same problem. Clicking on this link https://nxp.flexnetoperations.com/control/frse/download?element=3785898 will still redirect me to the account information interface, and I cannot find the correct URL. Also, I have logged into my own account before that. First,I click on this link: Then, The result is that the correct URL cannot be redirected. Re: NXP Model-Based Design Toolbox for S32M2xx – version 1.0.0 Hello @SmallWhite , It takes a little while for us after a release to update all the documentation on the NXP.com website. The Release Notes alongside the Quick Start Guide for the MBDT for S32M2xx are available on the FlexNET Location url: here:  https://nxp.flexnetoperations.com/control/frse/download?element=3785898 Please login on the NXP.COM before accessing this link. 回复: NXP Model-Based Design Toolbox for S32M2xx – version 1.0.0 When I click the urls in this passage,I will always redirect to my personal page taht I can not go to the true urls. And I wonder is there a quick reference guide for s32m244 like this ?
查看全文
Audio demo over AVB/TSN network on i.MX8DXL 1.  Introduction 1.1.        Purpose This application note introduces a procedure of how to port AVB/TSN stack and run referring feature demos on i.MX8DXL board. This can help users who want to run AVB/TSN demos to quickly understand and customized their own codes. Since many of the standards are only for TSN switch/bridges and i.MX8DXL is design to be a TSN/AVB endpoint, the demos did not implement a full stack or full standards. They only demonstrated the basic end-to-end point (talker to listener) A/V streaming without bridge or switch. The software used for example in this documentation are based on the opensource such as gstreamer and alsa utils. 1.2.        Overview 1.2.1.     AVB/TSN AVB (Audio Video Bridging) is a common name for the set of technical standards which provide improved synchronization, low-latency, and reliability for switched ethernet network. AVB was initially developed by the IEEE Audio Video Bridging task group of the IEEE 802.1 standards committee. In November 2012, AVB group was renamed to TSN (Time-Sensitive Networking) task group to reflect the expanded scope of its work, which is to provide the specifications that will allow time-synchronized low latency streaming services through IEEE 802 networks. The referring standards shows as follows:   TSN protocol additions QoS components supported in HW TSN MAC + SW driver Managed Object components expose i/f to allow support of standardized network config protocols (local & remote) Transport API to allow other transport layer to use TSN QoS Stack extensions to map traffic priority to application task scheduling Real Time, gPTP based, Best Effort 1.2.2.     Demo introduction   The two streams are defined as below to grantee time sensitive (sub-microsecond synchronization), low latency and bandwidth on the ethernet: Stream A: SR class A, AVTP Audio Format, PCM 16-bit sample, 48 kHz, stereo, 12 frames per AVTPDU. Stream B: SR class B, AVTP Compressed Video Format, H.264 profile High, 1920x1080, 30 fps. The two TSN streams would be allocated into different TC (traffic control) class for egress. Different TC class would be mapped to different hardware queues with specific DMA channel which supported by ENET_OoS IP. The demos were built by follow blocks:   Linux Traffic Control: streams egress control Linux ptp: clock sync in network Libavtp: Time Sensitive Applications AV Transport protocol Gstreamer: avtp plugin uses the libavtp to transmit and receive AVTP audio/video (audio pcm, video h264).   1.2.3.     Traffic control Multiply queue qdiscs + CBS: The CBS class is actually handled by hardware IP to select which queue for transmitting.   CBS parameters come straight from the IEEE 802.1Q-2018 specification. They are the following: idleSlope: rate credits are accumulated when queue isn’t transmitting; sendSlope: rate credits are spent when queue is transmitting; hiCredit: maximum amount of credits the queue is allowed to have; loCredit: minimum amount of credits the queue is allowed to have;   2.  Build demo 2.1.        Build yocto $ DISTRO=fsl-imx-xwayland MACHINE=imx8dxlevk source imx-setup-release.sh -b ./xwayland $ bitbake imx-image-full Prepare a SD card and burn it with the built out images. 2.2.        Rebuild kernel Rebuild the kernel after applying the 0001-qenet-add-queue-avoid-panic.patch, and overwrite the Image and imx8dxl-evk.dtb on the boot partition of the SD card. 2.3.        Install the toolchain $ bitbake -f fsl-image-validation-imx -c populate_sdk $ sh tmp/deploy/sdk/fsl-imx-xwayland-glibc-x86_64-fsl-image-validation-imx-aarch64-imx8dxlevk-toolchain-5.4-zeus.sh The toolchain would be installed into /opt/fsl-imx-xwayland/5.4-zeus 2.4.        Create a install folder $ mkdir Create a folder to install all of the shared libraries, binaries and configure files which built out manually in this doc. After built done, you should copy all of the contents in this folder to target board root. 2.5.        Build libavtp $ source /opt/fsl-imx-xwayland/5.4-zeus/environment-setup-aarch64-poky-linux $ git clone https://github.com/Avnu/libavtp.git $ cd libavtp $ meson build --prefix= /usr $ ninja -C build Copy the built out .so and .pc into the toolchain rootfs: $ sudo cp build/libavtp.so* /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/lib $ sudo cp build/meson-private/*.pc /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/lib/pkgconfig/ Copy the .so into the install folder: $ cp build/libavtp.so* /usr/lib/ To make sure you have avtp package installed correctly:     $ pkg-config --list-all | grep avtp 2.6.        Build ALSA aaf plugin $ cd /tmp/work/aarch64-poky-linux/alsa-plugins/1.1.9-r0/alsa-plugins-1.1.9 $ ./configure --build=x86_64-linux --host=aarch64-poky-linux --target=aarch64-poky-linux --prefix= /usr --disable-silent-rules --disable-dependency-tracking --with-libtool-sysroot= /xwayland/tmp/work/aarch64-poky-linux/alsa-plugins/1.1.9-r0/recipe-sysroot --disable-static --enable-aaf --disable-jack --disable-libav --disable-maemo-plugin --disable-maemo-resource-manager --enable-pulseaudio --enable-samplerate --with-speex=lib $ make $ make install 2.7.        Build Gstreamer AVTP plugins (1.17.x) 2.7.1.     Build Gstreamer core $ git clone https://gitlab.freedesktop.org/gstreamer/gstreamer.git $ patch -p1 < gstreamer-1.0-pass-build.patch $ meson build --prefix= /usr $ ninja -C build $ sudo ninja -C build install After Gstreamer is installed into , please fix the “prefix” path in the .pc files by, and copy to the toolchain folders: $ cd $ grep -lR ./lib/pkgconfig/ | xargs sed -i 's/ /\/usr/g' $ cp -rf ./usr/* /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/ 2.7.2.     Build gst-plugins-base $ git clone https://gitlab.freedesktop.org/gstreamer/gst-plugins-base.git $ cd gst-plugins-base $ patch -p1 < gst-plugins-base-pass-build.patch $ meson build --prefix= /usr $ ninja -C build $ sudo ninja -C build install 2.7.3.     Build gst-plugins-bad $ git clone https://gitlab.freedesktop.org/gstreamer/gst-plugins-bad.git $ cd gst-plugins-bad $ meson build --prefix= /usr $ ninja -C build $ sudo ninja -C build install   After gst-plugins-base and gst-plugins-bad installed into , please fix the “prefix” path in the .pc files and copy them into the toolchain folders: $ cd $ grep -lR ./lib/pkgconfig/ | xargs sed -i 's/ /\/usr/g' $ cp -rf ./usr/* /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/ 2.8.        Build H.264 SW plugins 2.8.1.     Build x264 As the yocto actually has the x264 recipes, but not included in our bblayers, we need to copy the x264 source into our bblayers path under /source to build: $ cp -rf ./poky/meta/recipes-multimedia/x264 ./meta-openembedded/meta-multimedia/recipes-multimedia/ $ vi ./meta-openembedded/meta-multimedia/recipes-multimedia/x264_git.bb Remove the LICENSE_FLAGS line $ bitbake -f x264 -c do_install $ sudo cp -rf tmp/work/aarch64-poky-linux/x264/r2917+gitAUTOINC+72db437770-r0/image/usr/* /opt/fsl-imx-xwayland/5.4-zeus/sysroots/aarch64-poky-linux/usr/ 2.8.2.     Build gst-plugins-ugly $ git clone https://gitlab.freedesktop.org/gstreamer/gst-plugins-ugly.git $ cd gst-plugins-ugly $ meson build --prefix= /usr $ ninja -C build $ sudo ninja -C build install 2.8.3.     Build libav $ cp -rf poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-libav meta-openembedded/meta-multimedia/recipes-multimedia/gstreamer-1.0/ Remove the LICENSE_FLAGS line $ vim ./poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-libav_1.16.2.bb $ bitbake -f gstreamer1.0-libav -c do_install $ cp /opt/samba/nxf39444/imx-yocto-bsp-i.mx8dxl/xwayland/tmp/work/aarch64-poky-linux/gstreamer1.0-libav/1.16.2-r0/image/usr/lib/gstreamer-1.0/libgstlibav.so /usr/lib/gstreamer-1.0 2.8.4.     Install binaries Final step is to copy all of your built out files from into your board / root, and boot up the board. $ export GST_PLUGIN_PATH=/usr/lib/gstreamer-1.0/ $ gst-inspect-1.0 To check if the above Gstreamer plugins we built out can be found by gst-instpect. 3.  System Setup 3.1.        VLAN The ENTE_QoS is assigned to eth0 instance. So create eth0.5 for vlan id 5: $ ip link add link eth0 name eth0.5 type vlan id 5 egress-qos-map 2:2 3:3 $ ip link set eth0.5 up 3.2.        Qdiscs The TSN control plane is implemented through the TC (Traffic Control) system. The transmission algorithms specified in the FQTSS (Forwarding and Queuing for Time-Sensitive Streams) chapter of IEEE 802.1Q-2018 are supported via TC Qdiscs (Queuing Discipline). 3.2.1.     MQPRIO qdisc $ tc qdisc add dev eth0 parent root handle 100 mqprio num_tc 3 map 0 0 2 1 0 0 0 0 0 0 0 0 0 0 0 0 queues 1@0 1@1 1@2 hw 1 3.2.2.     CBS qdisc Q1 CBS for audio, Q2 CBS for video: $ tc qdisc replace dev eth0 parent 100:3 handle 888 cbs idleslope 3648 sendslope -996352 hicredit 12 locredit -113 offload 1 $ tc qdisc replace dev eth0 parent 100:2 handle 777 cbs idleslope 98688 sendslope -901312 hicredit 153 locredit -1389 offload 1 3.2.3.     TimeSync Run the ptp4l and phc2sys in background, and use check_clocks to check the ptp sync works. $ ptp4l -i eth0 -f ./gPTP.cfg --step_threshold=1 & $ pmc -u -b 0 -t 1 "SET GRANDMASTER_SETTINGS_NP clockClass 248 clockAccuracy 0xfe offsetScaledLogVariance 0xffff currentUtcOffset 37 leap61 0 leap59 0 currentUtcOffsetValid 1 ptpTimescale 1 timeTraceable 1 frequencyTraceable 0 timeSource 0xa0" $ ./check_clocks -d eth0 4.  Run demo 4.1.        ALSA AAF audio To run the alsa AAF demo, please add aaf0 and converter0 plugin device into /etc/asound.conf: pcm.aaf0 {    type aaf    ifname eth0.5    addr 01:AA:AA:AA:AA:AA    prio 2    streamid AA:BB:CC:DD:EE:FF:000B    mtt 50000    time_uncertainty 1000    frames_per_pdu 12    ptime_tolerance 100 } pcm.converter0 {    type linear    slave {                  pcm "hw:0,0"                  format S16_LE    } } The “aaf0” plugin device defines the ethernet interface which AAF runs on, the socket priority which mapping to Traffic Class in kernel TC, the stream-id for the aaf streaming. The “converter0” plugin device is used for convert the S16_BE format to S16_LE for the wm8960 PCM audio. Select one device as AVB talker, and run: $ speaker-test -p 25000 -F S16_BE -c 2 -r 48000 -D aaf0 Select one device as AVB listener, and run: $ arecord -F 25000 -t raw -f S16_BE -c 2 -r 48000 -D aaf0 | aplay -F 25000 -t raw -f S16_BE -c 2 -r 48000 -D converter0 You can hear the sound on the listener device. You can also check which qdisc queue is used for AAF by: $ tc -s qdisc 4.2.        Gstreamer AAF audio Select one device as AVB talker, and run: $ gst-launch-1.0 clockselect. \( clock-id=realtime audiotestsrc samplesperbuffer=12 is-live=true ! audio/x-raw,format=S16BE,channels=2,rate=48000 ! avtpaafpay mtt=50000000 tu=1000000 streamid=0xAABBCCDDEEFF000B processing-deadline=0 ! avtpsink ifname=eth0.5 address=06:98:c0:22:df:35 priority=3 processing-deadline=0 \) Select one device as AVB listener, and run: $ gst-launch-1.0 clockselect. \( clock-id=realtime avtpsrc ifname=eth0.5 ! avtpaafdepay streamid=0xAABBCCDDEEFF000B ! queue max-size-bytes=0 max-size-buffers=0 max-size-time=0 ! audioconvert ! audioresample !  alsasink device="hw:0,0" \) 5.  Packet sniffer Use tcpdump on board to dump the L2 ethernet packet: $ tcpdump -i eth0 ether proto 0x22f0 -w dump.pcap The AVTP ether protocol code is 0x22f0 embedded inside the ether frame, or you can use "vlan 5" VLAN id for tcpdump parameters to dump. Then open this dump.pcap in the windows/Linux PC by the wireshark tool, it will automatically show the protocol inside the package, it can also parser the IEEE1722 (AVTP) CVF/AFF package header as below:   To measure the package latency from transmit port (talker) to receive port (listener), you can use the tcpdump on both end-points. And compare the Epoch Time the packet dumped: "Epoch Time: 1596252905.688243000 seconds". The delta of the epoch time of the same packet is around 100us~500us. This latency actually includes the AF_PACKET clone cost in kernel netfilter, also the tcpdump application schedule latency.   6.  Revision history summarizes the changes done to this document since the initial release. Table2. Revision history Revision number Date Substantive changes 1 5/2021 Initial release  
查看全文
MCUXpresso IDE v11.9.0 Now Available We are pleased to announce that MCUXpresso IDE v11.9.0 (build 2144) is now available. This is a major new version of the IDE and contains new features, enhancements and bug fixes over the previous versions, including latest announced MCUXpresso IDE v11.8.1.  Installer Downloads  To download the installers for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/ide/download   Documentation  Additional information can be found in the updated User Guide and other documentation, which can be accessed from the built in help system available via IDE's Help menu and in PDF form from within the installation directory.   Notification of future releases  To receive notifications about future releases, please follow: MCUXpresso IDE - Release History    Summary of Changes - version 11.9.0 - January 2024 Upgraded: Eclipse version to 2023.06 (Eclipse Platform 4.28.0 / CDT 11.2.0). Upgraded: MCUXpresso IDE integrated with OpenJDK Runtime Environment Temurin-17.0.7+7. Upgraded: GNU ARM Embedded Toolchain to version 12.3.Rel1. Note. Debugging info is enforced to DWARF version 4 ("-gdwarf-4"). Upgraded: ARM CMSIS-Pack Eclipse Plug-ins 2.9.0. Upgraded: Newer SEGGER J-Link software (v7.94b). Upgraded: Newer PEmicro plugin (v5.7.6). Upgraded: Version v15 of MCUXpresso Config Tools. Added: Initial support for MCXN2xx devices and FRDM-MCXN236 board. Feature: [MCXN9xx] Update debug support for A1 silicon. Feature: [App Code Hub] The IDE now offers views and wizards that allow users to import projects by directly interacting with Application Code Hub website. Feature is accessible through the File -> Import -> Application Code Hub wizard, the dedicated Quickstart link, by opening the view using Window -> Show View -> Other -> Application Code Hub, or by using Help -> Additional Resources -> Application Code Hub menu entry. Feature: [SDK Integration] Synchronization with SDK v2.15.abc and manifest schema version 3.14. Feature: [SDK Integration] Support complex dependencies for board, core, device, toolchain, compiler. Feature: [SDK Integration] Support new "template" type of SDK component containing predefined code snippets, visible to users in the UI of new project wizard and component manager to allow users to add the files with the snippets into projects. Also, added CLI support for this type by "use.all.templates" property for the "example.build" and "project.build" commands. By default, the option is set to false, so no template source is added to the project. Feature: [SDK Integration] Existing Import Remote SDK Git repository flow improved - a wizard is now used to clone and import the SDK. Feature: [SDK Integration] Automatic import of plugin SDKs from previous IDEs versions when upgrading to newer version. Feature: [SDK Integration] Add "change.sdk.roots" command in CLI mode that allows updating the built-in SDK search locations. Feature: [RT1160/RT1170/RT1020] Update flashloaders to work with non-default dummy cycle values. Feature: LinkServer debug solution is now installed by the MCUXpresso IDE installer as a separate tool and support files from the IDE that were LinkServer-specific are now part of the actual LinkServer package. The IDE implicitly uses the automatically installed LinkServer but a custom LinkServer can be configured using the Preferences page. A symbolic link to the installed LinkServer is also created inside the IDE layout (see /ide/LinkServer). Improvement: [IDE] Make Welcome page theme-aware and create content for dark theme.  Improvement: [IDE] Speed-up automatic generation of Makefiles. Improvement: [Windows installer] Disabled maximum path length limitation. Improvement: [Windows installer] Install J-Link USB drivers on Windows (starting with J-Link V7.92l installer, drivers are no longer installed by default) Improvement: [SDK Integration] Reduced GitHub SDK loading time when starting IDE. Improvement: [NPW/Manage SDK Components] Optimized component selection, minimizing time and eliminating freezes when selecting several components. Improvement: [NPW] Performance improvements when changing core selection. Fixed: [IDE] Too many identical confirmation windows appear if a required (by project) SDK is not installed. Fixed: [IDE] J-Link RAM debug sessions fail to set PC and SP correctly. Fixed: [IDE / Toolchain integration] The IDE automatically switches to using response files inside the generated linker command, for command lines exceeding 32K in length. Behavior is specific to Windows hosts, where there's a 32K length limit for a command line. Fixed: [IDE / Toolchain integration] Archiver ends with error when lots of object files are passed to the tool. IDE now passes object files through response files when command line exceeds 32K in length. Fixed: [SDK Integration] Recreating or uninstalling a GitHub SDK deletes the manifest file from the repository and breaks the SDK. Fixed: [NPW] Link section memory range used by secondary Multicore project specified during project creation is not reflected in final project settings. Fixed: [RT1180 B0] Semihosting PRINTF does not work properly with LinkServer when heap is located in cacheable memory. Fixed: [RT1180 B0] Connect script leaves DMA4 controller with error status indication.   Known issues  Please follow the KnownIssues.txt file from installation layout for a detailed list.
查看全文
i.MX6DQ Register Programming Aids Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response. These are the detailed programming aids for the registers associated with MMDC DDR3 and LPDDR2 initialization for the MX6DQ SoC. The last sheet formats the register settings for use with ARM RealView ICE. It can also be used with the windows executable for the DDR Stress Test. This programming aid was used for internal NXP boards. i.MX6Dual i.MX6Quad
查看全文
Running code from external memory with MCX N94x The MCX  N series are MCUs with an integrated flash memory like many traditional MCU series. Having an embedded flash memory is particularly useful, as facilitates board design, development, simplifies BOM, software development.  However, the size of the embedded flash might not meet applications required memory footprint. Some customers simply need more flash memory. For example, Graphical applications require store large image buffers in a non-volatile memory. Data logger devices that need to store large amounts of data. Or heavy inference models for object recognition.  Applications that need to store backup versions of their firmware or are way too complex and big. To solve this requirement the MCX N94x provides the capability to interface a great variety of wider and external memories. There are several traditional options to expand flash storage, but the one we are addressing is the use of external NOR  flash memories. To access an external memory the MCX N94x integrates modules that support external memory interfacing, those are  FlexIO and the FlexSPI. The FlexSPI module is capable of communicating with several kinds of memories. One of them is the Serial NOR flash which can be used as booting device. The goal of this article is to present the solution of a customer case scenario: How to run code from an external flash memory. Demonstrating the flexibility of the MCX N94x platform as well as introducing several tools, peripherals, and concepts that a developer will need to be familiar with while developing an application that runs from an external flash memory. The below figure illustrates the goal of this article, Run code from an external flash memory. The same hello world application can be run from the internal and external memory, for example, a NOR serial QuadSPI memory, without any functionality changes. The core simply will fetch and execute the instructions, using dedicated peripherals like FlexSPI. Figure 1 Executing same code from internal memory vs external memory. The MCX N94x series integrates a FlexSPI module, which enables running code from an external NOR flash memory. Figure 2 MCX N94x block diagram To follow this article, you will need the FRDM-MCXN947 Development board. Which is the evaluation board for the MCX N94x and N54x MCUs. The FRDM-MCXN947 integrates a W25Q64JVSSIQ QuadSPI flash memory. Therefore, this platform is perfect for creating an application that runs from an external flash memory. Figure 3 External NOR flash memory on FRDM-MCXN947 Boot, PFR, and SPSDK With the boot ROM  that the MCX  N integrates you can erase, program, and read the on-chip or external flash memory, which means you can use the boot ROM to download a boot image into the on-chip or external flash memory via the ISP interfaces. This article shows how to load a customized led_blinky demo, from the SDK  to the external flash memory using the boot ROM. However, other application projects may be used as well. Also, the boot ROM takes responsibility for the boot flow. It selects whether to boot from on-chip flash memory, external flash memory, or ISP mode.  The figure below shows an extremely simplified boot flow, which gives an overall understanding of the chip boot flow.  For more details on the boot flow mechanism refer to the section Top-level boot flow of the MCX Nx4x Reference manual. Figure 4 Simplified boot Flow After the reset handling routine, the boot ROM will take control of the chip’s boot flow. It will begin with pertinent chip’s initialization. Then will check the status of the ISP pin. If the ISP pin is currently asserted, the ISP boot handling routine will be executed. ISP or  In-system programming is an execution mode where the boot ROM will wait for commands from an external host, over protocols like UART or USB, to do actions like read and write the chip memory, burn fuses, and many more. If the ISP pin is not asserted, the boot ROM will continue to determine the boot mode. Boot mode can be controlled with the CMPA[BOOT_SOURCE] bit of the CMPA of the PFR or eFUSES. If  CMPA[BOOT_SOURCE]= 01b the boot ROM will run FlexSPI NOR boot handling routine. If CMPA[BOOT_SOURCE] is 00b or 11b internal flash memory handling routine is executed. After the boot mode selection, the image will be validated. If it is not valid, for example, is not present in memory, is corrupted, or does not have proper format,  the ISP boot handling routine is executed. If the image is valid, finally the boot ROM will perform the jump to the user´s application. The default boot flow is by internal flash, most of the SDK examples will be configured to boot from internal flash, as CMPA[BOOT_SOURCE] equals zero by default, or when CMPA area is erased. According to the Simplified bot Flow diagram, we need to make boot ROM go to FlexSPI NOR boot handling routine, to boot from the external flash. Therefore, we need to make   CMPA[BOOT_SOURCE] = 01b. The PFR holds critical boot and security settings that are monitored by the boot ROM after every reset. As just described earlier, the CMPA area can be used to control boot mode. Therefore, PFR areas need to be carefully configured, as they control boot flow and also security features of the chip. The below figure shows a very minimalistic representation of the PFR containing the CMPA, next to the internal flash. Figure 5 PFR's CMPA area For specific details of the PFR  please refer to the MCXNx4x_IFR.xlsx, attached to the MCX Nx4x Reference Manual. To facilitate writing into the CMPA and other areas of the  PFR, signing applications, burning fuses.  programming applications, NXP already developed several host command tools, APIs, and applications and integrated into a python tool called SPSDK. The below figure shows all the tools contained by the SPSDK. To get  details on the SPSDK and description of APIs, Applications, and tools  refer to SPSDK documentation at  https://spsdk.readthedocs.io/en/latest/spsdk.html# Figure 6 SPSDK API modules, applications, and tools The above figure highlights 3 applications, provided by the SPSDK,  that is going to be used to configure the chip to boot from the external flash memory those are: nxpdebugmbox, PRF, and BLHOST. Detailed step-by-step usage of these applications will be described later on.  The nxpdebugmbox application sends interfaces with the chip’s debug mailbox over SWD. The purpose of this tool is set MCU into ISP mode, without having to set low ISP pin,  also to make a mass erase to the chip's memory and PFR. Once the MCU enters ISP mode the host PC will be able to communicate with the boot ROM over UART or USB protocols. This enables the use of PFR and BLHOST applications. The PFR application will be used to write the CMPA[BOOT_SOURCE] = 01b and enable FlexSPI, port to probe and let the chip communicate with the external flash, in the CMPA area of the PFR. The BLHOST application will be used to erase the chip and program application image, in this particular case,  a led_blinky demo.  External Serial NOR flash interfacing The following terms are critical to understand how we can execute code in an external NOR flash memory with the MCX N94x. First of all, Execute-in-Place refers to the capability that the MCU core has to fetch and execute instructions directly from the external memory. It refers to the capability that an MCU has to execute code from the flash memory instead of an internal and traditional flash. To do XIP the MCX  N94x requires a capable peripheral with the ability to fetch instructions from the external memory. The FlexSPI module is capable of doing this. The FlexSPI does support several types of external memories. One of them is Serial NOR Flash. To interface the external memory with the FlexSPI supports SPI. SPI is an excellent serial protocol for short-distance and high-speed communications. The term QuadSPI could be simply understood as an implementation of the SPI protocol, where instead of having a single Data line, there are 4 data lines. SPI also supports two, and eight data lines. Flexible Serial Peripheral Interface (FlexSPI) memory controller supports connection to external serial NOR, NAND, and RAMs. It supports two SPI channels and up to four external devices. Each channel supports Single/Dual/Quad/Octal mode data transfer (1/2/4/8 bidirectional data lines). Flexible sequence engine (LUT table) to support various vendor devices (serial NOR, serial NAND, HyperBus, FPGA, etc). Memory-mapped read/write access by AHB Bus AHB RX Buffer implemented to reduce read latency. Total AHB RX Buffer size: 1024 Kbytes 8 flexible and configurable buffers in AHB RX Buffer Software triggered Flash read/write access by IP Bus IP RX FIFO implemented to buffer all read data from External device. FIFO size: 1024 Bytes IP TX FIFO implemented to buffer all Write data to External device. FIFO size: 1024 Bytes DMA support to fill IP TX FIFO DMA support to read IP RX FIFO Figure 7 FlexSPI block diagram FlexSPI system memory map regions are remapped to different addresses at the FlexSPI sub-module: Figure 8 FlexSPI memory map FlexSPI can support serial devices compliant with JESD216. Pre-requisites You will need the following Hardware: FRDM-MCXN947 evaluation board. USB C cable. Windows or Linux PC. You will need to install the following Software. MCUXpresso IDE v11.9.0 or above.  FRDM-MCXN947 SDK v2.15.0 or above.  SPSDK and python.   SPSDK installation and virtual environment We recommend to run the SPSDK on a python virtual environment, as this simplifies the installation of the SPSDK. Before proceeding with installation steps for the SPSDK we recommend to create a folder in your computer. This is where the virtual environment will be running, the SPSDK tools will be called,  and all the files generated by the SPSDK will be stored. Open a terminal, command, or Power Shell prompt  and navigate to your folder and follow the SPSDK installation  commands listed in this guide: Installation Guide — SPSDK documentation            To double check installation of the SPSDK run the following command in your virtual environment. spsdk --version         This figure shows the example of this command and the spsdk version used for this document. Figure 9 SPSDK version.  Setup  This chapter describes all steps to generate and boot an image from the external memory.  To run the commands listed in this document you will need use your python’s virtual environment. Use the virtual environment you created during SPSDK installation.  PFR settings This section describes the settings that need to be done in the MCX N94x PFR and bootable image.      Create CMPA and CFPA yaml  templates   In the following steps, we are going to focus on editing CMPA area since it contains boot-related fields for external execution.  CFPA area is not required to be edited.            Note:The commands used to generate the templates are based on ‘pfr’ tool  For details on the capabilities of these commands, visit: User Guide - pfr — SPSDK documentation First we are going to use pfr to create our yml CMPA/CFPA templates. These templates contain only the default configurations specified for the CMPA and CFPA areas of  device. If the command run successful the templates will be generated. As shown in figure this figures Figure 10 Yaml template created. Edit the CMPA and CFPA yaml templates Open CMPA   template in any text editor and follow the below steps. Set DEFAULT_BOOT_SOURCE to FLEXSPI_FLASH_XIP_0b01 Set FLEXSPI_AUTO_PROBE   to ENABLE Save the changes in the CMPA template.      Create and write the  CMPA and CFPA binaries       After editing the cmpa yaml, you will generate the CMPA/CFPA binaries from the yml templates.   Import and edit image This section shows how to create an XIP bootable image from the  MCUXpresso SDK  led_blinky example.  Import the led_blinky demo from the SDK.  Click on “Import SDK example(s)…” (1), then search and select the FRDM-MCXN947 (2), and click “Next” (3). Inside the “SDK import wizard” search and select the “led_blinky  demo (4) and click on “Finish” (5) Figure 11 Import the blinky example.  Once the demo project is imported open the project properties. Do a right-click in the project’s name (1), then click on “Properties” option (2) and open the project properties(3) Figure 12 Project ´properties Navigate to the Properties> C/C++ Build > MCU settings section Figure 13 MCU settings window Make sure that there are two  Flash areas for the external memory: QSPI_FLASH and             QSPI_FCB as shown in Figure 14. If the areas are missing add them as shown in the next step. Figure 14 External flash areas in the linker. Add the two flash areas for the  QSPI_FLASH and QSPI_FCB in the “Memory details” table, the move them to the Top.  Click in “Add Flash”  (1) twice, then click on “Move selected memory up in table” (2), the two newly created flash areas should be placed at the top. Note: Moving a memory area to the top of the “Memory details” table indicates the linker that text and data should be placed preferably in that area. Update the newly created flash areas name and parameters with the ones from the below table. Type Name Alias Location Size Driver Flash QSPI_FLASH Flash 0x80001000 0xFFFF000 MCXN9xx_SFDP_FlexSPI.cfx Flash QSPI_FCB Flash 2 0x80000400 0x400 MCXN9xx_SFDP_FlexSPI.cfx   Make sure that the flash areas match the ones shown in the Figure 15. Figure 15 Configured flash areas  Click “Build” (1), once compilation is finished, should return 0 errors (2). Figure 16 Successfully compiled image.                                      Note: You should see that the QSPI_FLASH section is being used and that the PROGRAM_FLASH section is not. Generate the binary. Navigate to the project’s debug folder and locate generated .axf (1). Then do a right-click in the .axf, and click on Binary utilities > Create Binary. Figure 17 Create binary. 7 The binary should appear in the debug folder. Get  easily get the binary location by doing a right click on the binary and navigating to  “Show in>System Explorer” Figure 18 Get created binary with ease. 8. Paste the binary into the workspace where you created the cmpa_bin.bin. This step is only to simplify the commands shown later on. Erase and ISP mode entry      ISP (In system programming ) is a mode where a host is able to instruct the ROM bootloader to program a new image or the PFR. The which holds the CMPA field with our configuration to do XIP from the external flash memory. Basically, the Host computer sends commands to the ROM bootloader to program the PFR using NXP’s BLHOST. To enter into ISP mode there are two options: ISP pin entry and Debugger mailbox. ISP pin entry requires keeping ISP pin asserted during reset sequence and de-asserting this pin after reset has been completed. Debugger mailbox only requires to use of a SWD debugger to make the ROM entry ISP mode. To enter into ISP mode over ISP pins follow is necessary keep ISP pin asserted during reset sequence and de-assert this pin after reset has been completed. To use the debugger mailbox is only needed having a debugger. For simplicity, the communication protocol will be USB. However, UART can be used as well. Erase the flash memory and enter ISP mode using the nxpdebugmbox. Proceed to run each command nxpdebugmbox erase  nxpdebugmbox ispmode -m 0 This figure shows the expected output when running the two commands from above. This operation will erase the contents on the internal and external flash memory. Also the PFR contents. Repeating this operation can be useful to get the chip to boot from internal flash memory. Note:  nxpdebugmbox commands need to be run using a SWD-JTAG debugger. For this example on-board debugger of the FRDM-MCXN947 is used. Ping rom Bootloader  Run the following command to ping the rom Bootloader, this way we can ensure that the device was set correctly in ISP mode. blhost  -t 2000 -p COMxxx,115200 -j -- get-property 1 Figure 19 Ping rom Bootloader From now on, an external debugger is not strictly required. The communication with the rom bootloader can be done over UART or USB. For simplicity, the UART protocol-based commands are used from now on in the rest of this document. Write  image and PFR and run demo We are going to follow the steps to write image.  1 Write CMPA binary. pfr write -p COMxxx,115200 -t cmpa -f mcxn9xx -b cmpa_bin.bin 2 Write CFPA binary. pfr write -p COM140,115200 -t cfpa -f mcxn9xx -b cfpa_bin.bin 3 Provide FlexSPI flash memory configuration blhost  -t 2000 -p COMxxx,115200 -- fill-memory 0x20000000 0x04 0xc0000405 4 Configure and fill memory. blhost  -t 2000 -p COMxxx,115200 -- configure-memory 0x09 0x20000000 blhost  -t 2000 -p COMxxx,115200 -- fill-memory 0x20003000 0x04 0xf000000f 5 Erase flash blhost  -t 2000 -p COMxxx,115200 -- flash-erase-region 0x80000000 0x100000 6 Configure memory. blhost  -t 2000 -p COMxxx,115200 -- configure-memory 0x09 0x20003000  7 Write image. blhost  -t 2000 -p COMxxx,115200 write-memory 0x80001000 frdmmcxn947_led_blinky.bin 8 Reset. blhost  -t 2000 -p COMxxx,115200 reset You might use this command or directly press the reset button from the FRDM board. The below image shows the successful execution of each command. Your FRDM-MCXN947  should be blinking by now. Figure 20 Successful image write and reset. Once the board is reset you will notice that the loaded example will begin to execute.  Double-check execution from external flash  To double-check that the image is executing from the external flash you can use the disassembly view from MCUXpresso. 1  Attach the debugger to the running target and place a breakpoint at any part of the code. Figure 21 Attach debugger to a running target. Once your debug probe is discovered, click “OK.” Halt the processor execution. Use the debug button. Figure 22 halt execution. Reset processor. Use the “Restart button”. The program should be stop at the first line of the main function. Figure 23 Breakpoint at main. Find and open the disassembly view. Click on “Instruction Stepping Mode” button or search for disassembly. Any option will open the MCUXpresso “Disassembly” view. Figure 24 Open "Disassembly" view Processor must be running at 0x8000_0000 address space. On the disassembly view you can check that the instructions are executed from address on the range of 0x8000_xxxx which is assigned for external flash. Figure 25 Running code from external flash. If you want to return the device to run from internal memory, then you need to go back to default values. If there are no modifications, to the ones shown in this document,  to the CMPA and CMPA areas, the nxpdebugmbox command can be executed. Board Design Boot ROM|Booting | Flash Clock|Timers Core and Memory MCXA MCXN
查看全文
S32G_How_to_Put_A53_to_WFI Chinese version S32G的partition off流程要求核稳定的进 入到WFI状态,本文说明如何修改Linux内核, 在A53 Linux关机或kernel panic时,如何让所 有A53 Core进入WFI。 目录 1 背景说明与参考资料 .................................................. 2 1.1 背景说明 ................................................................. 2 1.2 参考资料 ................................................................. 5 1.3 测试工具 ................................................................. 6 2 Panic ......................................................................... 7 2.1 Panic代码流程分析 ................................................. 7 2.2 BSP30修改说明(Non-ATF) ................................... 10 2.3 BSP36修改说明(ATF) .......................................... 15 3 Poweoff ................................................................... 17 3.1 Poweroff代码流程分析 ......................................... 17 3.2 BSP30修改说明(Non-ATF) ................................... 19 3.3 BSP36修改说明(ATF) .......................................... 20 4 Reboot情况说明 ....................................................... 20 5 STR情况说明 ........................................................... 21 Contents 1    Background and Reference. 2 1.1  Background. 2 1.2  Reference materials. 5 1.3  Test Tools. 6 2    Panic. 7 2.1  Panic code flow analysis. 7 2.2  BSP30 Modification (Non-ATF) 10 2.3  BSP36 Modification (ATF) 16 3    Poweoff 18 3.1  Poweroff code analysis. 18 3.2  BSP30 Modification (Non-ATF) 20 3.3  BSP36 Modification (ATF) 21 4    Reboot Description. 21 5    STR Description. 21 Automotive
查看全文
Example S32K344 PIT TRGMUX ADC DS3.5 RTD300 *******************************************************************************  The purpose of this demo application is to present a usage of   configure TRGMUX to select triggers for staring Normal/Injected chain conversion. Select PIT0_Ch0 as the hardware trigger source of ADC1_Ch34 & Ch48 via TRGMUX and two LEDs to show the trigger Sequence. ADC1_Ch34 is connected to board's potentiometer,Ch38 is bandgap channel.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q257 * MCU: S32K344 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: OpenSDA * Target: internal_FLASH ******************************************************************************** Re: Example S32K344 PIT TRGMUX ADC DS3.5 RTD300 Thanks for sharing. Is there any example with MCAL drivers?
查看全文
Using SEC Tool Config and Program Image to External Flash Ⅰ、Introduction The MCUXpresso Secure Provisioning Tool (SEC) tool is a GUI-based application provided to simplify generation and provisioning of bootable executables on NXP MCU platforms. The latest version of SEC v8 adds FCB configuration function to help users program image to external flash. The MCX N94x family is a typical product series of MCX. A controller with a flexible serial peripheral interface (FlexSPI) that supports external memory. The external flash has a large storage capacity, high flexibility. It is relatively independent of the replacement or upgrade of the main chip, and has high reliability and lifecycle. This article focuses on how to use SEC tools to configure and program MCXN947 external flash quickly and easily. Ⅱ、Configuration steps This article uses the FRDM-MCXN947 board as an example to configure FCB and download an external flash image. Hardware requirements: FRDM-MCXN947 board、Type-C USB cable Software requirements: MCUXpresso Secure Provisioning Tool | NXP Semiconductors Step1. Create new workspace  After opening the software, click File->New Workspace, select "MCX N94x/N54x" -> MCXN947 -> Click "create". Refer to the following figure: Step2. Connection with Target Processor Enter ISP mode:Press and hold SW3(ISP key) => Press and release SW1 (RESET key) => Release SW3 Go to your workspace and click “Target”->Connection, the Connection with Target Processor window is displayed. Here, we make Connection through UART and select port and baud rate. Refer to the following figure: We can click "Test connection" to check whether the connection is successful. If the connection is successful, the result will display "OK". Refer to the following figure: Step3. Boot memory configuration Next we need to configure FCB. Click on "Target"-> Boot Memory… ,The Boot memory configuration window is displayed. First we need to select the Boot memory type, this part allows selection of the boot memory type, and optionally instance. The selection contains all memory types but unsupported types are disabled. FlexSPI NOR flash can be configured in two ways: By using the flashloader/ROM based simple configuration in the Boot Memory Configuration dialog or By using the complete FCB (FCB binary), which can be prepared from the boot device configuration as well, or via MCUXpresso IDE by adding the FCB component into Peripheral Drivers in Peripherals tools, where the full configuration can be specified. Here we use a simple configuration, click "FlexSPI NOR-simplified", on this Predefined template, select W25Q64JW and click apply. Then, corresponding parameters on W25Q64JW will be automatically created on Boot memory configuration parameters. Normally, keep the default value. Refer to the following figure: We use "Test the configuration" to check whether the configuration is correct. After clicking "Test", the script will pop up to run automatically, and "SUCCESS" will be displayed after running. Refer to the following figure: Then click "convert to FCB" and the "convert to FCB" dialog box will pop up. Keep the default position of "FCB file path". Select "Apply the converted FCB as boot device configuration" and click "convert". The script automatically runs and generates "converted_fcb.bin". The FlexSPI NOR-complete FCB window is displayed. Refer to the following figure: The generated converted_fcb.bin file is automatically loaded to FCB file for runtime and FCB File for write. Click "Test" and "SUCCESS" will be displayed. Click "OK" to close the window. Refer to the following figure: Step4. Build image After completing the above operations, we need to load the .s19 or .hex file generated by MCUXpresso IDE into the Source executable image. Note: The start address of the external flash of the project needs to be changed to 0x80001000. This section does not explain how to change the start address. For details, see “How to config booting from external flash”. After the file is loaded, the start address is automatically identified. If the start address is not 0x80001000, you cannot "built image". Then click on "built image". Refer to the following figure: After completing the built image, "SUCCECC: built image" will be displayed. Click "close". Refer to the following figure: Step5. Write image We can see that the required .bin file has been generated automatically in "write image", or we can import the corresponding .bin file we wrote by "import". The Image path file will be automatically loaded. Click "write image" to run the script automatically. After the file is successfully written, "SUCCESS: write image" is displayed. Refer to the following figure: Finally, by pressing the RESET key on the board to exit ISP mode, we completed the configuration and downloaded the external flash image. Ⅲ、Summarize We use SEC Tool to configure FCB and download external flash images via GUI. This is just a simple method, and users can choose different ways according to their requirements. Boot ROM|Booting | Flash MCXN
查看全文
i.MX 8Mまたはi.MX 93で32ビットのアプリケーションをビルドして実行 次のセットアップは i.MX 93 で行われます。i.MX 8M に対しても同じ手順が有効であり、従うことができます。 前提条件 Yocto 環境を準備してください。 $ mkdir imx-yocto-bsp $ cd imx-yocto-bsp $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-langdale -m imx-6.1.1-1.0.0.xml $ repo sync ビルド環境を設定してください。 $ DISTRO=fsl-imx-wayland MACHINE=imx93-11x11-lpddr4x-evk source imx-setup-release.sh -b build-imx93 イメージに32ビットのメモリのサポートを追加する i.MX 8Mまたはi.MX 93の場合、multilib構成を使用して、64ビットOS上で32ビット・アプリケーションのビルドをサポートできます。Multilibは、さまざまなターゲットの最適化やアーキテクチャ・フォーマットのライブラリを構築し、それらを組み合わせて1つのシステムのイメージに集約できます。 32ビット・アプリケーションをビルドするには、conf/local.conf内に以下のステートメントが必要です。設定で、メインのマシン・タイプとして64ビット・マシンを指定し、multilib:lib32を追加します。ここで、これらのライブラリはarmv7athf-neonチューニングでコンパイルされ、lib32パッケージがイメージに含められます。 # Define multilib target require conf/multilib.conf MULTILIBS = "multilib:lib32" DEFAULTTUNE:virtclass-multilib-lib32 = "armv7athf-neon" # Add the multilib packages to the image IMAGE_INSTALL:append = " lib32-glibc lib32-libgcc lib32-libstdc++" Multilibは、Debianパッケージ管理ではサポートされていません。RPMシステムが必要です。デフォルトのRPMに移行するには、conf/local.conf内の2行のパッケージ管理行を確認し、コメントアウトしてください。 PACKAGE_CLASSES = "package_deb" EXTRA_IMAGE_FEATURES += "package-management" イメージをビルドします。 bitbake imx-image-core 32ビットアプリケーションをクロスコンパイルする このセクションでは、Linux SDKを使用して、シンプルなCアプリケーションを32ビットのバイナリにクロスコンパイルする方法を説明します。 ツール、ツールチェーン、およびホストマシンに配置するためにコンパイルする小さなサイズのrootfsを含むSDKを生成します。 DISTRO=fsl-imx-wayland MACHINE=imx93-11x11-lpddr4x-evk bitbake core-image-minimal -c populate_sdk ビルドを行う前に、次のコマンドを使用してSDK環境を設定します。 source /opt/fsl-imx-wayland/6.1-langdale/environment-setup-armv7at2hf-neon-pokymllib32-linux-gnueabi シンプルなHello Worldアプリケーションを実装します。 cat hello_world_32.c #include int main() { printf("Hello, World!"); return 0; } $CC hello_world_32.c -o hello_world_32 ファイル・タイプを確認します。 $ file hello_world_32 hello_world_32: ELF 32-bit LSB shared object, ARM, EABI5 version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-armhf.so.3, BuildID[sha1]=0a5042a0309858e0b10b12175a155cfbfb4c6a80, for GNU/Linux 3.2.0, with debug_info, not stripped バイナリをLinuxのrootfsにコピーしてください。 i.MX 93でアプリケーションを実行する ボードをブートして、アプリケーションを実行します。 root@imx93-11x11-lpddr4x-evk:~# ./hello_world_32 Hello, World!
查看全文
GPSダイナミックリンクライブラリをAndroidシステムのサービスとして追加 症状 お客様は、AndroidシステムのサービスとしてGPSダイナミックリンクライブラリを追加したいと考えていますが、Android SEポリシーで許可することはできません。 診断 お客様が正しい設定ファイルを設定しませんでした。 解決策 (1)ファイルandroid_build/device/fsl/imx8q/mek_8q/mek_8q.mkを開きます。GNSSサービスを追加 # GNSS HAL のPUALPRODUCT_PACKAGES += \[email protected]\[email protected]サービス (2)ファイルandroid_build/device/fsl/imx8q/mek_8q/manifest.xmlを開き、gnss hidlを追加します  android.hardware.gnsshwbinder 1.0 IGnss デフォルト (3)ファイルandroid_build/device/fsl/imx8q/mek_8q/BoardConfig.mkを開きます。足す #GNSS PUALBOARD_HAS_GPS_HARDWARE := 真 (4) android_build/device/fsl/imx8q/mek_8q/ueventd.freescale.rc ファイルを開きます。足す /dev/ttyLP1 0660 システム gps Selinux の権限を追加する device/fsl/imx8q/sepolicy/system_server.te に追加します。 許可 hal_gnss_default vndbinder_device:chr_file {read }; テストを追加した後、書き込み、オープンなどの権限の問題もあり、一度にすべてを追加します。 許可 hal_gnss_default vndbinder_device:chr_file {open read write execute getattr create ioctl map};
查看全文
Documents and Examples for S12(X) and S12 MagniV devices S12(X) S12 MagniV DOCUMENTS CAN setup calculator for S12(X) and MagniV devices  S12(X) MCU Security  S12(X) devices reference schematics  Useful documents for building own CAN bootloader  How-to Add missing derivatives to CodeWarrior Classic HCS12(X) 5.2 (Unofficial Method)  DOCUMENTS S12Z constant, variable, code allocation in CodeWarrior   BLDC 6-step control speed scaling using S12ZVM  MagniV Power Dissipation Calculator  MTRCKTSBNZVM128 vs MTRCKTSPNZVM128 kit motor  S12ZVM configuration for the motor control applications  Software for S12ZVM motor control kits  DEVKIT-ZVL128 EVB review  S12 family devices - COP recognition consideration calculator  MagniV PLL calculator  Bus-Off Handling in MSCAN EXAMPLES CAN Standard ID and CAN Extended ID for S12(X) and MagniV devices, memories refreshment  S12XD, S12XE - External BUS design - Addendum To AN2708  S12X Examples Pack  TIC-S12-XDP512-FLASH-E_W-CW47  S12X_Interrupt_catcher (catch all unexpected interrupts)  API example code for S12G  Read paged const in S12  EXAMPLES How to get device ID and write program once field without programming application to the S12Z device in the CodeWarrior (Eclipse)  CAN Standard ID and CAN Extended ID for S12(X) and MagniV devices, memories refreshment  S12Z Protection Override  S12ZVC IFR Program Once Field  S12Z: Simulating ECC errors at EEPROM by cumulative write  S12Z: Simulating ECC errors at RAM by debug access  S12Z: Simulating ECC errors at Flash by cumulative write  S12Z SW example of COP Watchdog Reset  S12Z Interrupt catcher for unexpected interrupts  S12Z voltage measurement  S12Z EEPROM example code  S12Z Flash example code  Autonomous Clock Trimming SW example for MagniV devices  BATS Voltage Supply Sense example code for MagniV devices  High-Voltage Input (HVI) SW examples for MagniV devices  SW examples for MagniV S12ZVC and S12ZVL devices  PWM example code for S12ZVL  S12ZVL-TIM-FrequencyMeasurement-V1_0-CW106-TIC-EXAMPLE  SW example of Security feature with Backdoor Access Key option for S12ZVL  Example S12ZVL ADC0 triggered by TIM0 OC updates PWM duty cycle  S12ZVM clock module and PLL configuration - SW examples  Low power mode example code for S12ZVC  Single / double bit RAM ECC error example code at S12ZVC  S12ZVML-MINIBRD software ported from AN5327  Example: S12ZVC192-ACMP-POT-CW107  Example codes form "Easily Develop LIN-based Actuator Applications with Mixed-signal MCUs" webinar 
查看全文
How to use Bluetooth on i.MX8M boards How to use Bluetooth on i.MX8M boards This article introduces how to connect a device via Bluetooth to the i.MX8M family of boards. The steps shown in this document were done using the i.MX8M Plus. Start Bluetooth First, enable the BT service and start it. If systemctl refuses to start or enable these services, consider using the force option -f at the end of the following commands: systemctl enable bluetooth.service systemctl start bluetooth.service Check status of BT. It should be active and running: systemctl status bluetooth You should see "Running" on Status: ● bluetooth.service - Bluetooth service Loaded: loaded (/lib/systemd/system/bluetooth.service; enabled; vendor preset: enabled) Active: active (running) since Mon 2021-11-29 19:41:18 UTC; 4s ago Docs: man:bluetoothd(8) Main PID: 710 (bluetoothd) Status: "Running" Tasks: 1 Memory: 1.9M CGroup: /system.slice/bluetooth.service └─710 /usr/libexec/bluetooth/bluetoothd Nov 29 19:41:18 imx8mpevk systemd[1]: Starting Bluetooth service... Nov 29 19:41:18 imx8mpevk systemd[1]: Started Bluetooth service. Load Wi-Fi To use the Bluetooth, it is necessary first to load the Wi-Fi, otherwise it won't be possible to load BT firmware. To do this, use the following steps: modprobe moal mod_para=nxp/wifi_mod_para.conf wpa_passphrase SSID SSID_PASSWD >> /etc/wpa_supplicant.conf wpa_supplicant -d -B -i mlan0 -c /etc/wpa_supplicant.conf -Dnl80211 Up to this point, you should be able to use BT, however, if you want to continue connecting to a network using Wi-Fi, you can use the following steps. Otherwise, skip the following and go to the next section. Run below command: connmanctl Connect to Wi-Fi: connmanctl> enable wifi connmanctl> scan wifi #This should list the networks: connmanctl> services connmanctl> agent on connmanctl> connect wifi_ _managed_psk #Enter password of wifi network Passphrase? connmanctl> quit Now that Wi-Fi is connected, BT can be used. Select serial port for Bluetooth Show serial ports available on the system (each board has different devices): dmesg | grep tty i.MX8M Plus shows these results: [ 0.000000] Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk2p2 rootwait rw [ 0.166330] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 29, base_baud = 5000000) is a IMX [ 0.166815] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 30, base_baud = 5000000) is a IMX [ 0.167185] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 31, base_baud = 1500000) is a IMX [ 1.189285] printk: console [ttymxc1] enabled [ 4.160356] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling. [ 7.171005] audit: type=1006 audit(1605328853.412:2): pid=665 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1 For this article, the ttymxc0 port was selected. To attach the device port and set the baudrate (115200 for this case) run the following commands, where hciconfig is used to configure BT device and up opens and initializes HCI device: hciattach ttymxc0 any 115200 flow hciconfig hci0 up hciconfig  After running the commands above, you should see this: hci0: Type: Primary Bus: UART BD Address: 00:E9:3A:0D:C7:80 ACL MTU: 1016:5 SCO MTU: 120:6 UP RUNNING RX bytes:1424 acl:0 sco:0 events:82 errors:0 TX bytes:1218 acl:0 sco:0 commands:82 errors:0 Now you can manage BT with bluetoothctl. Connect device To start bluetoothctl run the following command: bluetoothctl Scan for devices: [bluetooth]# power on [bluetooth]# default-agent [bluetooth]# pairable on #Start scanning for devices: [bluetooth]# scan on You should see the discovered devices: [CHG] Controller 00:E9:3A:0D:C7:80 Discovering: yes [NEW] Device E0:89:7E:86:47:47 E0-89-7E-86-47-47 [NEW] Device 59:80:27:7E:98:A2 59-80-27-7E-98-A2 [NEW] Device EC:81:93:51:FE:66 EC-81-93-51-FE-66 [NEW] Device 50:32:37:D0:A5:B8 50-32-37-D0-A5-B8 [NEW] Device 2C:DD:64:A1:B2:48 2C-DD-64-A1-B2-48 [NEW] Device 08:66:98:EF:B6:C5 08-66-98-EF-B6-C5 ... ... Wait for the system to find the device you want to pair and use the following command: #Use the corresponding address from your device [bluetooth]# pair 88:29:9C:59:BC:F6 Confirm the passkey both in the i.MX8M board and device. If all steps were done successfully you should see now the name of your connected device instead of [bluetooth]#. To stop scanning, the scan off command can be used. To see connected devices and information, use the following commands: #A galaxy S10+ was connected to the i.MX8M Plus [Galaxy S10+]# devices [Galaxy S10+]# info This article introduces how to connect a device via Bluetooth to the i.MX8M family of boards. i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlus i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Linux
查看全文
How to use FreeMaster SDKs in S32K3 RTD 0.9.0 Some customers inquire how to use FreeMASTER with S32K3. But there is no exists example projects which demonstrate usage of the FreeMASTER serial communication driver in S32K3 Real Time Drivers at the moment. So this article will introduce how to use FreeMaster SDKs in S32K3 RTD 0.9.0. Download S32DS \ S32K3 Development Package \ RTD (SDK) \ FreeMASTER Driver Login your account on NXP website, and download the S32K3 Standard software from TOOLS &SOFTWARE of S32K3 webpage. If you have already installed the S32DS3.4 \ S32K3 Development Package 3.4.0 \ RTD 0.9.0, then you can skip the following part and start directly from 4.Install FreeMASTER Driver 3.0 for S32K3 Install S32K3 Development Package 3.4.0 After install the S32 Design Studio v3.4, we should install S32K3 Development Package 3.4.0(SW32K3_S32DS_3.4.0_D2012.zip): go to menu "Help" -> "Install New Software" and click on "Add..." button Here we uncheck S32 Design Studio S32K3 SDK (RTD S32K3 0.8.1), because we will install the newer version S32K3 RTD 0.9.0 later. Install S32K3 Real Time Drivers Version 0.9.0 S32K3 Real Time Drivers Version 0.9.0 can be installed by refer the Offline Package Installation Setup of S32DS Extensions & Updates: Explanation and How To Use. Install FreeMASTER Driver 3.0 for S32K3 Attach FreeMASTER_S32K3 to S32K344_UART_Printf_Sample_090_34 The reason for choosing the S32K344_UART_Printf_Sample_090_34 project to demonstrate the combination of FreeMaster SDKs is that the project has already configured the LPUART of the S32K3X4EVB-Q257 development board. Select LPUART peripheral as host communication Through the description in the Requirements and Release Description chapter of FreeMASTER Driver Release Notes(FMSTRS32K3RN), we can see that currently only UART interface is supported. The S32K3 FreeMASTER 3.0 version 1.0.0 only support NXP GCC 6.3 or 9.2 for ARM at the moment, but the latest S32K3 Real Time Drivers Version 1.0.0 is based on NXP GCC 10.2.0. This is the reason why RTD 0.9.0 is selected in this article.  The README.txt also shows that: Current package provides FreeMASTER Communication Driver support for S32K344 over LPUART module   LPUART13 is selected in this project for S32K3X4EVB-Q257, so we need to define the base address for FreeMASTER: #define FMSTR_LPUART_BASE           0x404A0000 Modify the main function according to the README.txt: Connect FreeMASTER3.1 to S32K3X4EVB-Q257 board Here we can see that the FreeMASTER3.1 is connected to S32K3X4EVB-Q257 board.
查看全文
RW612 WiFi Init stuck on HAL_ImuLinkIsUp() I am trying to run the MQTT example on a custom board. The module used is ublox IRIS-W106-30B. I followed the instructions to use j-link to install the wifi fw blob serperatly. However, I am getting stuck in an infinite loop in WPL_Init().   I was also unable to initialize the BLE due to similar issue. SDK 25.09.00 using MCUXpresso  Re: RW612 WiFi Init stuck on HAL_ImuLinkIsUp() Yes, I am able to run my normal application code, log to UART etc.  Re: RW612 WiFi Init stuck on HAL_ImuLinkIsUp() Hi, Are you able to test a simple Hello World example? Also, have you already applied the required modifications to enable your module? Please refer to the following article for guidance. Regards, Daniel.
查看全文
Not able to Download S32K3 Standard Software Not able to download  Re: Not able to Download S32K3 Standard Software Hello, I have just download it with no issues. Try different browse, clear cookies, etc... Download itself is working properly on NXP side. Best regards, Peter
查看全文