1789282_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1789282_en-US

1789282_en-US

Example S32K312 ADC DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of the
 ADC_SAR IP Driver for the S32K3xx MCU.

 The example uses the PIT0 trigger to trigger  conversions on ADC1.  ADC channels
 are selected to be converted on  ADC-1:
 ADC channel S10 is connected to board's potentiometer.

#define ADC_SAR_USED_CH_BANDGAP 48U /* Internal Bandgap Channel */
#define ADC_SAR_USED_CH_POT_0 34U



 ------------------------------------------------------------------------------
* Test HW: S32K3X2EVB-Q172
* MCU: S32K312
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

Dinesh_Guleria_0-1705393272443.png
Dinesh_Guleria_1-1705393287863.png


Dinesh_Guleria_2-1705393446888.png

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-19-2025 03:45 AM
更新者: