Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
Not able to run 3rd party android/system app over AAOS in mek_imx8 (Please Contact car service) Hello, I have successfully generated an Android image from 14.0.0_1.1.0_AUTO_SOURCE PLATFORM_VERSION=14 PRODUCT_INCLUDE_TAGS=com.android.mainline TARGET_PRODUCT=mek_8q_car TARGET_BUILD_VARIANT=eng TARGET_ARCH=arm64 BUILD_ID=UQ1A.231205.015 However, I'm not able to run a 3rd party nor system app. So, here: - Install a 3er party using adb - Install a 3rd party app using the aaos  as module. I got this messsage (Please Contact car services): The API that it acesses: Same happes if I try with a system app  Here, I'm not really sure if there something that I need to activate in the aaos build. I logcat both with kitchen sunk and this test app. However, I'm not really sure what's going on.  I think that maybe this is something straightforward that I'm not able to figure out. Thanks in advance Android i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlus Re: Not able to run 3rd party android/system app over AAOS in mek_imx8 (Please Contact car service) Hi Reymor, What display are you currently using? We’re looking for a similar type of large display. Could you please let us know which vendor you’re purchasing it from? Re: Not able to run 3rd party android/system app over AAOS in mek_imx8 (Please Contact car service) Hello, You are trying to access an exclusively apps you need go with the vendor or you can contact google android for this. Regards
查看全文
TJA1103A フォロワー/リーダー 私はTJA1103AをMIIモードで使用しており、片側はMPC5777C(FEC MAC)に、もう片側は100BASE-T1経由でdSPACEに接続しています。 TJA1103 データシート (Rev.3.0)は、2つの異なる文脈で出現するためです。 1. 表18(ピンストラップ、その他グループ):LEADER/FOLLOWERは、自律モードおよび極性補正とともにCONFIG5/CONFIG6で設定されます。 2. ポート機能レジスタ(ビット8~11):MII_LEADER_ABILITY、MII_FOLLOWER_ABILITY、RMII_LEADER_ABILITY、RMII_FOLLOWER_ABILITY — ここで「リーダー」は、TXC/RXCクロック(MIIクロック方向)を出力するPHYを指します。 私の質問:表18のLEADER/FOLLOWERは、以下を指しますか? (a) MDIリンク上の100BASE-T1タイミングマスター/スレーブの役割(PHYがツイストペア上のラインクロックを提供する)、または (b)MACとPHY間のMII/RMIIクロックの方向? 同じような曖昧さに遭遇した人はいますか? ご説明いただければ幸いです。 Re: TJA1103A Follower/Leader よろしくお願い申し上げます。 Re: TJA1103A Follower/Leader TJA1103データシートの表18にあるLEADER/FOLLOWER設定は、MDIツイストペアインターフェース上の100BASE-T1リンクタイミングのマスター/スレーブの役割(つまり、物理リンクのラインタイミングを提供するPHY)を指します。対照的に、ポート機能レジスタのLEADER/FOLLOWERビットは、MACとPHY間のMII/RMIIクロックの方向を示します。したがって、同じ用語が使用されていますが、表18はワイヤ上のリンクレベルのタイミングに関するものであり、レジスタビットはMACへのインターフェースクロックに関するものです。
查看全文
LPC55S06:在应用程序内确定生命周期属性 您好, 我目前正在尝试在 LPC55S06 控制器上进行安全启动,想知道:是否可以在不进入引导加载程序的情况下从用户应用程序(非引导加载程序上下文)访问等效的 API 来确定生命周期状态(属性 17,如下所述)? 例如,我在 status_t 中看到这样的状态返回代码:kStatus_FLASH_SealedFfrRegion (137) 但我认为应该有更好的方法来确定生命周期状态,而不是尝试对密封的 ffr 区域执行闪存操作,并评估返回代码 == kStatus_FLASH_SealedFfrRegion (137)。此外,我在 SDK 中也没有找到相关的应用程序接口(使用 SDK 26.03). 根据UM11126第 8 章表 420: 生命周期状态: 标签17 (11h) 表示是否启用了 Flash 网络安全: 0x5aa55aa5-设备处于开发生命周期 0xc33cc33c-设备处于部署生命周期 目前通过 blhost 获取值: blhost -p , -- get-property 17 谢谢您! LPC55xx Re: LPC55S06: Determine Lifecycle property In-App 你好卡洛斯, 最酷的个人资料照片! 感谢您的快速回答,这个解决方法对我有用。 Re: LPC55S06: Determine Lifecycle property In-App 你好@sjrzcis 谢谢您的帖子! 生命周期值只能通过引导加载程序读取。用户应用程序中没有访问该参数的 API。 对于可能由此导致的不便,我们深感抱歉。 作为一种解决方法,我建议在图像中添加一个自定义参数以指示设备的生命周期状态。
查看全文
複数のCAN RXを使用し、異なるメッセージIDで送信したい 複数のCAN-Rxメッセージを使用したいのですが、同じメッセージを異なるID経由で送信する必要があります。動作するモデルをお持ちの方がいらっしゃいましたら、こちらで共有してください。 Re: I want to use multiple can rx and send with different message Id こんにちは、 @Sachinkumarar15 さん。 RTDパッケージ内には、シンプルなFlexCAN構成の既存のサンプルがあり、さらにコミュニティにもいくつかの追加サンプルがあります。 [RTD600 MCAL & IP] S32K3X4EVB-T172 FlexCAN 割り込みのサンプル / ポーリング 例:S32K344 FlexCAN_Ip TX/RX/EnhanceRXFIFO DMAテスト S32DS3.5 RTD400 複数のIDを受信および送信するように変更できます。受信(Rx)の場合は、Rxフィルターを変更するだけで済み、送信(Tx)の場合は、同じTxデータを再利用してmsg_idを変更できます。 よろしくお願いします、 ジュリアン
查看全文
LPC55S06: Determine Lifecycle property In-App Hi there, I am currently experimenting with secure boot on a LPC55S06 controller and wanted to know: is there is an equivalent API accessible from user application (non-bootloader context) to determine the Lifecycle state (property 17, described below), without entering the bootloader? For instance, I saw this status return code: kStatus_FLASH_SealedFfrRegion (137) in status_t But I think there should be a better way to determine the lifecycle state than trying to do a flash operation on the sealed ffr region and evaluating that the return code == kStatus_FLASH_SealedFfrRegion (137). Also I see no API in the SDK for this (using SDK 26.03). According to UM11126 Chapter 8, Table 420: LifeCycleState: Tag: 17 (11h) Indicates whether Flash security is enabled: 0x5aa55aa5 - Device is in development lifecyle 0xc33cc33c - Device is in deployment lifecycle Currently getting the value through blhost: blhost -p , -- get-property 17 Thanks! LPC55xx Re: LPC55S06: Determine Lifecycle property In-App Hello Carlos, coolest profile pic! Thanks for the quick answer, this workaround works for me. Re: LPC55S06: Determine Lifecycle property In-App Hi @sjrzcis  Thanks for your post! The Lifecycle value can only be read through the bootloader. There is no API available to access this parameter from the user application. We apologize for any inconvenience this may cause. As a workaround, I recommend adding a custom parameter to your image to indicate the device’s lifecycle state.
查看全文
S32K344 - DMAスキャッターギャザーを使用してADCマルチチャネル値を取得する方法 私のプロジェクトでは、ADC0/ADC1/ADC2モジュールに分散配置された50個のADCチャネルを使用しました。各モジュール内のADCチャネルはランダムに配置されており、連続チャネルと不連続チャネルが混在していた。ADCモジュールはスキャンモードを使用し、起動後は中断やMCUの介入なしに、継続的にADC変換を実行します。チャネルのすべてのADCサンプリング値は、DMAモジュールを介して関連するメモリアドレス(dma_adc_value [50]など)に転送されます。スキャッターギャザーコレクタの設定方法が理解しにくく、ソースアドレス(ADC結果レジスタ)、デスティネーションアドレス、オフセット、マイナーループ、メジャーループの設定方法がわかりません。私はS32プラットフォーム3.5、RTD3.0.0、およびS32K344 MCU用のS32 Design Studioを使用しています。関連アプリケーションのリファレンスルーチンはありますか?ありがとう! Re: S32K344-how to use DMA scatter gather get adc multi channel value こんにちは、@blue0432 さん。 MCTPTX1AK324 SWサンプルコードを参照してください: S32K324トリプル永久磁石同期モータ制御(PMSM)リファレンスデザインボード これは、PWM同期と位相依存型ADCリストのための散乱収集を設定します。 ただし、ADCの設定については、コミュニティ資料を参照することもできます。スキャッターギャザーの設定よりも、そちらの方が役に立つと思います。 例 S32K312 PIT BTCU パラレル ADC FIFO DMA DS3.5 RTD300 例 S32K344 PIT BTCU パラレル ADC FIFO DMA DS3.5 RTD300 ADCパラレル変換 一般的な解決策は、BCTUリスト/FIFOを使用してDMA結果配列にデータを供給することです。S32K3 ADCは、複数のADCインスタンスに対応するMPC(多重並列変換)もサポートしています。 最後に、 S32K3XX SAR-ADC、BCTU、TRGMUXのトレーニングプレゼンテーションをご参照ください。 よろしくお願いします、 ジュリアン
查看全文
S32K344-how to use DMA scatter gather get adc multi channel value In my project, 50 ADC channels were used, distributed in ADC0/ADC1/ADC2 modules. The ADC channels in each module were randomly distributed, with some continuous and some discontinuous. The ADC module uses scanning mode and continuously performs ADC conversion after startup, without any interruption or MCU involvement. All ADC sampling values of channels are transferred to the associated memory address (such as dma_ adc_value [50]) through the DMA module. It is difficult to understand how to configure the scatter gather collector and do not know how to configure the source address (ADC result register), destination address, offset,  minor loop, and major loop. I am using S32 Design Studio for S32 Platform 3.5, RTD3.0.0, and S32K344 MCU. Do you have any reference routines for related applications? Thank you! Re: S32K344-how to use DMA scatter gather get adc multi channel value Hi @blue0432, You can refer to the MCTPTX1AK324 SW example code: S32K324 Triple Permanent Magnet Synchronous Motor Control (PMSM) Reference Design Board  It configures scatter gather for PWM synchronization and phase‑dependent ADC lists. However, you can refer to some community material for ADC configuration, which I think will serve you better than scatter gather configuration: Example S32K312 PIT BTCU parallel ADC FIFO DMA DS3.5 RTD300 Example S32K344 PIT BTCU parallel ADC FIFO DMA DS3.5 RTD300 ADC parallel conversion Usual solution is BCTU list/FIFO feeding a DMA result array. S32K3 ADC also supports MPC (Multiple Parallel Conversion) for more than 1 ADC instance: Lastly, you can refer to the S32K3XX SAR-ADC, BCTU AND TRGMUX Training presentation. Best regards, Julián
查看全文
使用 PEMicro 调试的 S32M2xx 是否支持 DEBUG_RAM? 是否计划在S32M2系列上支持 DEBUG_RAM 与 PEMicro 调试? 我从 S32 Design Studio 3.6.0 中看到公告称 Lauterbach 调试器支持该功能,但我找不到 PEMicro 调试工具支持该功能。
查看全文
S32M276 - RTDを使用した定数1秒リセットループ(MCU_HSE_SWT_RST_RESET)6.0.0 こんにちは、 S32M276をベースにしたカスタムボードと、RTD 6.0.0を使用しているNXP公式開発ボードの両方で、リセットループが継続的に発生する問題が発生しています。 観察された行動: JTAGデバッガを接続すると、アプリケーションは予期しないリセットなしに正常に動作します。デバッガを再接続し、MCU/RGMステータスレジスタを介してリセット理由を調べると、リセット原因はMCU_HSE_SWT_RST_RESETであることが特定されます。 HSEウォッチドッグ(HSE_WDT)に関連付けられたリセットカウンタは、サイクルごとに増加します。 デバッガーを取り外して電源を入れ直すと、デバイスは約1秒ごとにリセットループに入ります。 現在の構成: MCU: S32M276 RTDバージョン:6.0.0 MCU_HSE_SWT_RST_RESETの具体的なトリガーについてご説明いただけますでしょうか? - RTD 6.0.0 において、この HSE 管理リセットを無効にするか、WDT を適切に保守するための推奨手順は何ですか? よろしくお願いします。 - ミゲル・マルケス Re: S32M276 - Constant 1s reset Loop (MCU_HSE_SWT_RST_RESET) using RTD 6.0.0 フォーラムでさらに調査した結果、以下の情報が問題のデバッグに役立つ可能性があると考えました。(これはコネクテッドでの情報です。) UT0レジスタ値 DCMUTS値 UTESTメモリ開始: Re: S32M276 - Constant 1s reset Loop (MCU_HSE_SWT_RST_RESET) using RTD 6.0.0 こんにちは、@Miguel_Marquez_Schaeffler さん。 詳細な説明と追加のデバッグ情報をありがとうございました。 あなたの説明からすると、これは時計の設定の問題のようですね。通常、この動作はクロック比率が守られていない場合に発生します。 [s32k312]RTD 機能によるリセット理由の読み取り、HSE_SWT_RST は機能リセット後に発生します。 - NXP コミュニティ。 S32M27XRMの第21.7.2章に記載されているクロックモードに従っていることを確認してもらえますか?具体的には、HSE_CLK 構成を確認してください:解決済み: S32K312 flexcan サンプルが電源リセット時に実行されない - NXP コミュニティ。 よろしくお願いします、 ジュリアン Re: S32M276 - Constant 1s reset Loop (MCU_HSE_SWT_RST_RESET) using RTD 6.0.0 解決策は、HSEクロックを120MHzから60MHzに事前にスケーリングすることだった。
查看全文
S32DS for PA v2.1のライセンスが間もなく期限切れになりますので、延長をお願いします。 こんにちは、 私のS32DS for PA v2.1のライセンスが間もなく期限切れになります。 メンテナンス期間の延長にご協力ください。 どうもありがとう。 Re: S32DS for PA v2.1 license will expire soon, please extend こんにちは、 PA v2.1用のS32DSライセンスの有効期限が延長されました。以前使用していたコードを使って、S32DSを再度有効化してください。
查看全文
i.MX8MM – Kernel logo support with DRM / GKI (fb/simplefb issue) Hi, I am working on i.MX8MM (Android 12, kernel 5.15, GKI) and trying to implement a kernel-level logo. Since FBDEV is not supported in Android 12, I attempted to enable CONFIG_FB=y CONFIG_FB_EFI=y CONFIG_LOGO=y and use a framebuffer/simplefb-based approach. However, I am facing the following issues: * Kernel crashes when adding the framebuffer node * simplefb/simpledrm is not working as expected * Display drivers (LCDIF + MIPI DSI) are built as GKI modules Because of this, I am unable to display any logo during the kernel phase. I also tried to retain the U-Boot logo during the kernel transition by disabling video shutdown (video_link_shut_down), as suggested in some references. However, the display still goes blank (white/black) before the Android boot animation starts. I have attached a video for reference. **Platform details:** * SoC: i.MX8MM * Display pipeline: LCDIF + MIPI DSI (ili9881c panel) * Display driver: DRM/KMS (no FBDEV) * Kernel: 5.15 (Android GKI) **Questions:** 1. What is the recommended approach to implement a kernel logo using DRM (without FBDEV)? 2. Does NXP BSP support simplefb/simpledrm for Android 12? Thanks. i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.MX8MM – Kernel logo support with DRM / GKI (fb/simplefb issue) Hello, Please note that Android 12 + GKI + DRM/KMS does not support a classic kernel logo, if you want to have an image early on boot you may use Uboot bootloader logo, using a bmp image. Best regards/Saludos, Aldo.
查看全文
如何将 M7 内核的主频设置为 400M 根据芯片手册,如果不将M7内核重置为400M的工作频率,哪些方面会受到影响?这在 EB 项目的什么地方起作用?   Re: How to set the main frequency of the M7 core to 400M Hi,sdx111 根据手册信息,400 MHz 是最大工作频率(Max),没有规定最低必须运行在 400 MHz。参考例程中默认设置为M7时钟为XBAR_CLK 400M。 您们实际工程中遇到什么问题,或者有什么担忧吗? BR Joey Re: How to set the main frequency of the M7 core to 400M 你好,sdx111 感谢您与我们联系。 我已收到您的问题,并将帮助您进行检查。 BR 乔伊 Re: How to set the main frequency of the M7 core to 400M 嗯,我想问一下BSP35.0的关于时钟树的设置只在ATF中吗?在linux中会有吗?如果在ATF中,是在哪个目录下,就比如CGM0MUX0的相关设置,我可能需要更改一下,因为双核启动后时钟貌似被更改了 Re: How to set the main frequency of the M7 core to 400M Hi,sdx111 A核时钟主要在ATF中定义,主要在arm-trusted-firmware\fdts\s32cc.dtsi设备树文件中定义时钟属性。uboot和Kernel中不排除有驱动少数情况下会调整时钟。 我可能需要更改一下,因为双核启动后时钟貌似被更改了。 >>>建议从先ATF修改,多数情况下应该都是可以的。 BR Joey Re: How to set the main frequency of the M7 core to 400M 我看了一下这个文件的XBAR_2X的时钟设置是0呢?是我看的有问题吗?还是另有其他地方设置? Re: How to set the main frequency of the M7 core to 400M Hi,sdx111 应该在初始化早期阶段设置的XBAR_2X时钟,请参考以下代码内容,S32GEN1_XBAR_2X_FRE被定义为了固定值。 int s32gen1_get_early_clks_freqs(struct siul2_freq_mapping *mapping) { ...     /* User defined values */     if (mapping->a53_freq > S32GEN1_A53_FREQ) {         mapping->a53_freq = S32GEN1_A53_FREQ;         mapping->arm_pll_vco_freq = S32GEN1_ARM_PLL_VCO_FREQ;         mapping->arm_pll_phi0_freq = S32GEN1_ARM_PLL_PHI0_FREQ;         mapping->xbar_2x_freq = S32GEN1_XBAR_2X_FREQ;     }   请问您具体需要修改哪个时钟呢?    BR Joey   Re: How to set the main frequency of the M7 core to 400M Hi,sdx111 关于XBAR的时钟,如果您使用S32G2的话,尝试修改一下这个值。 BR Joey Re: How to set the main frequency of the M7 core to 400M 就是想要更改CGM0MUX0寄存器的值还有XBAR的时钟
查看全文
S32K312 Mini-EVB - 无法进入调试模式,GDB 服务器连接失败 问题描述 S32K312 Mini-EVB 以前可以正确调试,但现在无法进入调试模式。GDB 服务器 无法与目标处理器建立连接。 错误消息: " 启动 PortsCinet Debug_Flash 遇到了问题-服务启动序列中出现错误 " "GDB 服务器无法与目标处理器建立连接。请检查您的连接和 电源,验证包括调试配置在内的启动配置设置是否准确。" --- 已尝试的故障排除步骤: 1。已选中 PEmicro 连接助手: -已检测到板:USB1 上的 Multilink Universal Rev A -已选择 " Auto " 连接速度 -已启用 " 重置后和与目标通信之前出现延迟 " -构建成功完成,出错 0,警告 0 2。尝试使用通用多链路固件更新实用程序 (v9.90.00.00) 进行固件更新: -硬件类型:多链路通用-低成本调试接口-设备:Multilink Universal Rev C (PEM647663)(ARM 配置) -架构:ARM -固件文件:usbmlfsufarmens.1152(自动选择) -结果:上次结果 = 成功(固件更新成功完成) 3.二手 Pemicro JTAG/ARM 恢复实用程序(在 S32DS 中): -检测到的接口硬件使用旧固件: -所需固件:200.240-原始固件:7.95 -更新固件:9.10 -现有 INCT 固件 " 选项 " block... -结果:闪存擦除失败,结果 > 5000:固件更新失败。重试? 4.Used P&E Kinetis Recovery Utility (v0.02): - Interface Libaries Version: 1.06.00.00 - Detected:USB1:Multilink Universal Rev C (PEM647663) - 通信:SWD - 电缆版本:341 - 状态:"持续尝试停止处理器。请尝试重启主板直到此操作 成功为止 " -对主板进行电源循环未解决问题 --- 意见: -电脑检测到调试器硬件(Multilink Universal) -编译过程没有错误地完成 -通过 P & E Utility 进行固件更新显示 " 成功 " 但恢复实用程序显示固件不匹配(必需: 200.240 与原始版本:7.95) -即使在多次通电后处理器也无法暂停 -在此问题开始之前,板工作正常 --- 问题: 1. 2. 当 S32K312 MCU 处于这种状态时,是否有特定的顺序来恢复它? 3.Multilink 调试器和 S32K312 目标机之间是否可能存在固件版本冲突? 4. 对于这种情况,是否建议使用其他恢复程序或工具? Re: S32K312 Mini-EVB - Unable to enter debug mode, GDB Server connection failure 我已经在这里回答过了,我相信是同一个主题: https://community.nxp.com/t5/S32K/S32K312MINI-EVB-Unable-to-enter-debug-mode-Cannot-halt-processor/m-p/2349362/highlight/false#M57862
查看全文
[不正行為] 投稿者: @RishavKaaraTech / 掲示板: TapLinx-SDK / 報告者: kwsxxcwi kwsxxcwi は、 @RishavKaaraTech が投稿した 「RFIDDiscover ツールを入手したが、その使い方はわからない」という 投稿を以下の理由で報告しました。 理由:裸体または性行為 詳細: イモバンFedexでの配送のみ イモバンプリペイド不要で購入 合法的にイモバンをオンラインで注文する イモバン処方箋不要 海外 imovane処方箋なしで一晩中 購入イモバン処方箋なし サウジアラビアアラビア シルダルド 価格 イモバネ byimovane オンラインで COD を利用できます イモバンを購入したい イモバンの注文方法 イモバン翌日配送 次のイモバンの購入場所 最安値plrice imovane いいえ処方箋翌日イモバン 購入割引イモバンカスタムhrt イモバンはどこで買えますか imovane代金引換 イモバンを購入したい サウジアラビアアラビア シルダルド 価格 イモバネ 合法的にイモバンをオンラインで注文する イモバンをオンラインで合法的に注文する can私はイモバンを注文します 次にイモバンを注文する場所 購入私たちからのimovane 割引イモバンをオンラインで購入する いいえ処方箋イモバン Fedex 配送 安全イモバン アメリカのオンライン薬局 イモバンを購入したい いいえ処方箋翌日イモバン イモバンを購入したい イモバンを翌日配送で注文 イモバンを購入したい imovaneプリペイド不要で購入 ausイモバン注文 イモバンを翌日配送で購入 割引本物のイモヴァネ イモバン外国からの処方箋なし イモヴェイン2mg 安い 処方箋なしでイモバンをオンラインで購入 イモバンFedexでの配送のみ 投稿リンク: https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/RFIDDiscover-tool-acquired-but-how-to-use-it/mp/2164324#M205 投稿者: @RishavKaaraTech |作成者に電子メールを送信する 報告者: kwsxxcwi |メールによる報告 報告された投稿には3件の返信があります。
查看全文
[不正行為] 投稿者: @RishavKaaraTech / ボード: TapLinx-SDK / 報告者: zhvaoq zhvaoq は、 @RishavKaaraTech が投稿した 「RFIDDiscover ツールを入手したが、その使い方はわからない」という 投稿を以下の理由で報告しました。 理由:スパム 詳細: 割引エクセロン英国セール リアル一般的なエクセロン エクセロン処方箋不要、代金引換可 購入ブランド エクセロン オレゴン 低価格エクセロン 方法エクセロンを注文する 安いエクセロン50mgの価格(ロンドンデリー) 欲しいエクセロンを注文する 購入エクセロン3mgフェデックス can私はエクセロン錠を購入しました 購入ペット用エクセロン 安いエクセロン50mgの価格(ロンドンデリー) エクセロンを次に注文する場所 エクセロン無料の処方薬 エクセロンカナダで購入 処方箋不要の格安オンラインエクセロン 海外エクセロンをオンラインで注文する canエクセロンを注文します 購入エクセロン インターネット検索 購入エクセロン ウェストバージニア 次のエクセロンの注文先 エクセロンカナダで購入 エクセロン処方薬の副作用 注文オンラインエクセロン代金引換 エクセロンnrg 取引 購入エクセロン アトランタ アメリカ オンラインエクセロンの合法的な配送 安いエクセロン50mgの価格(ロンドンデリー) 購入エクセロン・トロント どのようにエクセロンを購入する エクセロンは購入できますか エクセロンの購入方法 次のエクセロンの購入場所 エクセロンカナダで購入 エクセロン処方箋不要、代金引換可 ジェネリックエクセロン最安値 can私はエクセロン1を購入します 購入エクセロン ウェストバージニア 次のエクセロンはどこで購入できますか エクセロンインドの薬局 投稿リンク: https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/RFIDDiscover-tool-acquired-but-how-to-use-it/mp/2164324#M205 投稿者: @RishavKaaraTech |作成者に電子メールを送信する 報告者: zhvaoq |メールによる報告 報告された投稿には3件の返信があります。
查看全文
[不正行為] 投稿者: @RishavKaaraTech / 掲示板: TapLinx-SDK / 報告者: oqgmavfu oqgmavfu は、 @RishavKaaraTech が投稿した 「RFIDDiscover ツールを入手したが、その使い方はわからない」という 投稿を以下の理由で報告しました。 理由:ヘイトスピーチ 詳細: カナダでゾピクロンをオンラインで購入 購入ゾピクロン オーストラリア いいえ処方箋ゾピクロンをフェデックスで発送 ゾピクロンを次に購入できる場所 ゾピクロン翌日配送 Fed Ex ゾピクロン土曜日配達代金引換 ゾピクロンを次に購入する場所 購入ゾピクロン ドミニカ共和国 ゾピクロン代金引換オンライン注文 欲しいゾピクロンを購入する 注文ゾピクロンを代金引換でオンラインで購入 ジェネリックゾピクロン処方箋不要翌日配送 canゾピクロンを購入します 購入ゾピクロン セントポール 注文ゾピクロン オクラホマシティ ゾピクロンを注文したい 購入処方箋なしでゾピクロンを入手 購入処方箋なしでゾピクロンを入手 安全にゾピクロンをオンラインで購入 ゾピクロン代金引換購入 canゾピクロンを購入します 購入ゾピクロンオンラインオーストラリア ジェネリックゾピクロンが安い 購入ゾピクロンのオンライン処方 購入ゾピクロンを代金引換でオンラインで購入 ゾピクロン、処方箋不要、一晩中 ゾピクロンの注文方法 購入ゾピクロン バーモント codゾピクロン 安全にゾピクロンをオンラインで購入する ゾピクロン代金引換 ゾピクロンを注文したい ゾピクロンを購入する方法 欲しいゾピクロンを購入する 注文ゾピクロンを代金引換でオンラインで購入 %E2%ゾピクロンをモンペリエで購入 タラゾピクロン canゾピクロンを注文します どこでゾピクロンを購入できますか? https://museusvalenciades.grupotecopy.es/en/node/2467 "> 処方箋鎮痛剤ゾピクロン 投稿リンク: https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/RFIDDiscover-tool-acquired-but-how-to-use-it/mp/2164324#M205 投稿者: @RishavKaaraTech |作成者に電子メールを送信する 報告者: oqgmavfu |メールによる報告 報告された投稿には3件の返信があります。
查看全文
lpc4078 eeprom page erase clarification required I'm using an LPC4078 and MCUXpresso and experimenting with storing values in Eeprom. I want to write a few bytes in the middle of a page without clearing the whole page. Looking in the datasheet, it says that after writing the data to be written int he page register, it still has to be programmed into non-volatile memeory and that is done with the erase/program operation. Does the Erase/Program operation erase the whole page or just the area of the page I have new data for, and how does it know? - the address setting for Erase/Program ignores the 6 lsbs so it only knows the page. The UM10562.pdf isn't explicitly clear on this matter. Thanks Alex Re: lpc4078 eeprom page erase clarification required I attach a workspace with the mentioned project in it. I ran it on an LPC4078 using a lpc-link2 debugger. (I couldn't be bothered to get semihosting to work, so I used breakpoints and inspected the data) Re: lpc4078 eeprom page erase clarification required Hello @alex_conway  For LPC4078 EEPROM, the minimum erase/program unit is one page (64 bytes). Therefore, each erase/program operation will erase the entire page. If you want to write only a few bytes, please first read the whole page, then modify the required bytes, and finally perform an erase/program operation on the page. You can test this on your side.   Thank you.   BR Alice Re: lpc4078 eeprom page erase clarification required Hi Alice, My experiments demonstrate otherwise: I wrote a small program using the lpc_board_ea_devkin_4088 library and the periph_eeprom demo project to start me up. I erase a page of Eeprom and read it back. To my surprise the results are all '\0' instead of 0xFF Then I write 'ABCDEFG\0' to address 0 in that page and read the page back. I receive 'ABCDEFG\0' Then I write 'ABCDEFG\0' to address 7 in that page and read the page back. I receive 'ABCDEFGABCDEFG\0' This is all as expected except for two things: 1. after erasing the eeprom reads 0 2. looking at the implementation of Chip_EEPROM_Write() is can seem no read-modify-erase-write sequence. There is only Chip_EEPROM_WritePageRegister followed by Chip_EEPROM_EraseProgramPag. This is why I asked the question. Thanks Alex Re: lpc4078 eeprom page erase clarification required I've got semihosting to work after adding a newline to all my printf strings! Also clearer evidence of everything I have said: Erasing sets Eeprom to 0x00 The code does not perform a read-modify-erase-write sequence, just erase-write. The LPC4078 seems to only erase the locations that are written to when erasing. I would really like clarification on this. Thanks Alex
查看全文
T2081 SGMIIは電源の再投入後に動作しなくなります。 件名:電源再投入後のT2081 SGMIIの問題 こんにちは、 私は、RCW構成がDEに設定され、SGMIIがSerDesレーン7に構成されているT2081プロセッサで作業しています。 電源投入直後、SGMIIインターフェースは正常に動作し、問題なくリンクが確立されます。しかし、電源サイクル(電源をオフにしてからオンにする)を実行すると、動作が不安定になる。 SGMIIリンクが確立されたようです(リンクがUPとして検出されます)。 しかし、ネットワーク通信が失敗します(pingが通りません)。 2~3回電源を入れ直すと、インターフェースは再び正常に動作するようになります。 その後、電源のオンオフを繰り返すたびに、この問題が断続的に発生する。 この挙動はデターミニスティックではなく、ランダムに見える。 その他詳細: この基板は伝導冷却式のヒートシンクを使用しています。 サイクル間で構成に変更は加えられません。 この問題は電源のオンオフ後にのみ発生し、初期起動時には発生しません。 考えられる原因の特定やデバッグ手順の提案にご協力いただけますでしょうか? よろしくお願いいたします。 ラビンドラ・アルミリ。 QorIQ T2デバイス Re: T2081 SGMII is not working after a power cycle. こんにちは、 T2081 SGMIIインターフェースで発生している、電源再投入後にリンクが「UP」状態であるにもかかわらずデータが流れない(pingが応答しない)という不安定な動作は、プロセッサのSerDes/FMan(フレームマネージャ)と外部PHY間の同期またはリセットタイミングの不一致が原因であることが多いです。   考えられる原因 SerDes リセット/再初期化が不完全: 電源サイクル中に残留電圧または不適切なリセットタイミングにより、SerDes PLL またはレーンが未定義の状態 になることがあります。SerDesが、内部PHY/PCS(物理符号化サブレイヤー)が完全に同期する前にリンクが確立されたと判断した場合、FManはパケットをサイレントに破棄します。 PHY ストラップイン/初期化の不一致: PHY は、コールドブート と比較して、電源サイクルの急速な移行中に誤ったブートストラップ値をラッチしている可能性があります。これにより、PHYがMACへのリンクを報告しているにもかかわらず、内部のSGMII自動ネゴシエーションが実際には完了していない状態が発生する可能性があります。 FMan クロック/ソフトリセットの問題: T2081 の既知のエラータ (A-007273 など) によると、特定の イーサネット MAC クロックが移行中に無効または不安定になると、FMan ソフトリセットが正しく完了しない可能性があります  。 電圧/電力シーケンス: 伝導冷却ヒートシンクを使用しているため、電源サイクル中の熱膨張と収縮により、特に SerDes PLL 電源フィルタ で、はんだ付け不良や電力供給の問題が明らかになることがあります。   推奨されるデバッグ手順 CDRロックの確認:SerDesレーン制御およびステータスレジスタを読み取ります。pingが失敗した場合はCDR_LCKビットを確認してください  。設定されていない場合、リンク層が接続が確立されていると判断していても、SerDesは受信データストリームをロックしていません。 SGMIIステータスレジスタの検証:SGMII MDIOレジスタ空間にアクセスします。具体的には、MDIO_SGMII_SR(ステータスレジスタ)をチェックして、リンクステータスがPCSレベル で本当に有効かどうかを確認します。 ループバックテストを実行します。問題がSerDesまたはPHYのどちらにあるかを特定するには、 LaneBTCSR3[LPBK_EN]=01  を設定して内部ループバックを有効にします。ループバック経由でpingできる場合は、問題は外部(PHYまたは信号完全性)にある可能性が高いです。ループバックが失敗した場合は、問題はT2081 SerDes/FManの内部にあります。 レジスタダンプ: 「合格」CASEと「不合格」CASEでSerDes、PCS、およびFManレジスタの完全なダンプを実行して、電源サイクルによって引き起こされる構成のずれを特定します  。 電源レールを監視します: オシロスコープを使用して、電源サイクル中に SerDes PLL 電源レーンをプローブし、初期起動時 と異なる可能性のあるグリッチや遅い立ち上がり時間を確認します。 よろしくお願いします。 Re: T2081 SGMII is not working after a power cycle. こんにちは、 別の掲示板でも同じ問題を確認しました。この場合、PCIブリッジが検出されていません。 どちらのシナリオにおいても、問題は高温時のみ発生する。 温度が60℃に達する前に電源を再起動すれば、システムは正常に動作します。しかし、温度が60℃を超えた後にハードリブート(電源のオンオフ)を実行すると、ボードによって動作が異なります。 一方の基板では、 SGMII(SerDes経由で接続)が機能しません。 もう一方のボードでは、 PCIブリッジが検出されません。 よろしくお願いいたします。 ラビンドラ・アルミリ
查看全文
i.MX6UL (TX6UL) eLCDIF: デバイスツリー内のクロック周波数はmxsfbドライバによって無視されます 説明:私はTX6UL (i.MX6UL) モジュールを使用しており、デバイスツリーのノードを変更することでディスプレイのクロック周波数を調整しようとしています。しかしながら、タイミングノード内のパラメータ「クロック周波数」の数値を変更しても物理的な影響がない一方で、異なるポーチパラメータを切り替えると影響があるという状況に遭遇しました。 テスト対象ノード: 「A { クロック周波数 = <0x01c9c380>; (10進数: 30000000) hactive = <0x00000320>; (10進数: 800) vactive = <0x000001e0>; (10進数: 480) hback-porch = <0x00000028>; (10進数: 40) hsync-len = <0x00000030>; (10進数: 48) hfront-porch = <0x00000028>; (dec:40) vback-porch = <0x0000001d>; (10進数: 29) vsync-len = <0x00000003>; (10進数: 3) vfront-porch = <0x0000000d>; (10進数: 13) hsync-active = <0x00000000>; (dec: 0) vsync-active = <0x00000000>; (dec: 0) 非アクティブ = <0x00000001>; (10進数: 1) pixelclk-active = <0x00000000>; (dec: 0) };“ 「B { クロック周波数 = <0x017d7840>; (10進数: 25000000) hactive = <0x00000320>; (10進数: 800) vactive = <0x000001e0>; (10進数: 480) hback-porch = <0x00000028>; (10進数: 40) hsync-len = <0x00000030>; (10進数: 48) hfront-porch = <0x00000028>; (10進数: 40) vback-porch = <0x0000001d>; (10進数: 29) vsync-len = <0x00000003>; (10進数: 3) vfront-porch = <0x0000000d>; (10進数: 13) hsync-active = <0x00000000>; (dec: 0) vsync-active = <0x00000000>; (dec: 0) 非アクティブ = <0x00000001>; (10進数: 1) pixelclk-active = <0x00000000>; (dec: 0) };“ 「C { クロック周波数 = <0x017d7840>; (10進数: 25000000) hactive = <0x00000320>; (10進数: 800) vactive = <0x000001e0>; (10進数: 480) hback-porch = <0x00000008>; (dec: 😎 hsync-len = <0x00000004>; (dec: 4) hfront-porch = <0x00000008>; (dec: 😎 vback-porch = <0x00000010>; (10進数: 16) vsync-len = <0x00000004>; (10進数: 4) vfront-porch = <0x00000010>; (10進数: 16) hsync-active = <0x00000000>; (dec: 0) vsync-active = <0x00000000>; (dec: 0) 非アクティブ = <0x00000001>; (10進数: 1) pixelclk-active = <0x00000000>; (dec: 0) };“ 「D { クロック周波数 = <0x01c9c380>; (10進数: 30000000) hactive = <0x00000320>; (10進数: 800) vactive = <0x000001e0>; (10進数: 480) hback-porch = <0x00000008>; (dec: 😎 hsync-len = <0x00000004>; (dec: 4) hfront-porch = <0x00000008>; (dec: 😎 vback-porch = <0x00000010>; (10進数: 16) vsync-len = <0x00000004>; (10進数: 4) vfront-porch = <0x00000010>; (10進数: 16) hsync-active = <0x00000000>; (dec: 0) vsync-active = <0x00000000>; (dec: 0) 非アクティブ = <0x00000001>; (10進数: 1) pixelclk-active = <0x00000000>; (dec: 0) };“ 観察された行動: AとBを組み合わせると、クロック周波数は27MHzとなる。 BとCは25MHzのクロック周波数で動作する。 質問: ドライバがクロック周波数パラメータを無視するのはなぜですか? AとBのポーチパラメータを使用しつつ、CとDのように25MHzのクロック周波数を実現するにはどうすればよいでしょうか? ドライバが約60FPSのリフレッシュレートを実現しようとしているようですが、なぜでしょうか?リフレッシュレートを変更してクロック周波数を25MHzにするにはどうすればよいですか? 環境: モジュール: Ka-Ro TX6UL ドライバー: mxsfb Re: i.MX6UL (TX6UL) eLCDIF: clock-frequency in Device Tree ignored by mxsfb driver こんにちは、 @ArbeitEr1860 お元気でお過ごしのことと思います。 i.MX Linuxユーザーガイドの4.4.1.3章で説明されているように、「mmcargs」変数に何らかの引数を渡してみてください。 よろしくお願いいたします。 サラス。
查看全文
Is the eMMC IP used in S32R45 the same as that in i.MX? Does the i.MX USDHC interface support S32G (S32G and i.MX share the same IP)? Is the IP used in S32R45 the same as that in i.MX? How to enable the eMMC driver for S32R45? Re: Is the eMMC IP used in S32R45 the same as that in i.MX? Hello, @sinetech  Thanks for the post. The S32G and some of the i.MX SOCs use same USDHC drivers, the IP used is similar. For S32R related questions, I suggest posting it to the following board: https://community.nxp.com/t5/Other-NXP-Products/bd-p/other The S32R engineers would provide more accurate answers directly. BR Chenyin  回复: Is the eMMC IP used in S32R45 the same as that in i.MX? linux-release-bsp37.0
查看全文