Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
mma8653fc PL_STATUS returns 0XFF I can read and write the registers, but when i read the STATUS register i receive 0xFF. The same applys to the PL_STATUS, it returns 0xFF. The orientation of the display has no influence on the status.  Re: mma8653fc PL_STATUS returns 0XFF Hi Phillip, To be able to read correct data from the PL_STATUS register (0x10), the Portrait/Landscape function needs to be enabled by setting the PL_EN bit in the PL_CFG register (0x11). So please make sure you have the Portrait/Landscape function enabled in order to get right data from the PL_STATUS register. If you have it enabled, please post here your source code so that we can review it. You might also find useful my simple example code I have written for the FXLS8471Q. Best regards, Tomas    
查看全文
NTM88 board What would these LF and RF be? Are two antennas necessary? Where can I find the schematic or gerber of this attached slide plate? Pressure Sensors Re: NTM88 board Hello, L5---LF  E1---RF The LF receiver block allows the TPMS to receive signals at 125kHz. The RF transmitter generates a radio frequency (RF) signal to send the data. You will find the Schematic and Gerber files in the following link: NTM88 sub-GHz Schematic and Gerber files
查看全文
TPMS - FSLTMPSRCV8000 Hello, I'm from the technical university Clausthal. In the past we got some samples of the tire pressure measurement system. We got 4 sensors and one device that can be connected to the PC via USB. Unfortunately we did not got any documentation abaout this so I have some serious trouble getting this to work. My broblem is that i am not able to get any information about this "FSLTMPSRCV8000". Pluged into the PC it is an unknown device VID_C1CA&PID_0005. Can anyone tell me what device actually is and how i can use it? Thanks Pressure Sensors Re: TPMS - FSLTMPSRCV8000 Hello Nicholas, I will be helping you at the Technical Service Request 1-4194544644. Any update about your issue, please refer to the service mentioned. Thank you for your interest in Freescale. Have an excellent. David
查看全文
Effect of perfluorocarbon liquids on the silicone gel of the MPXV7205. Why can't I get real tech support like from a real company?y can't I reach Effect of perfluorocarbon liquids on the silicone gel of the MPXV7205. Why can't I get real tech support like from a real company? Re: Effect of perfluorocarbon liquids on the silicone gel of the MPXV7205. Why can't I get real tech support like from a real company?y can't I reach Hello Nate, We do not recommend the MPXV7025 to become in direct contact with any kind of liquid substance or corrosive gases which would damage the gel and cause the sensor to become out of specification. The strain gauge and the electronic circuitry for calibration and compensation are protected by a nitride layer but the aluminum bonding pads which provide electrical connections between the leadframe and the gauge are not protected, in order to make the bonding feasible. The complete die is also protected with a silicone gel. This gel is not fully hermetic, although we use much better gel for our newer types of pressure sensors, water or any other fluid can penetrate the gel and can reach the die. When the sensor die is in contact with water e.g., oxydoreduction reactions between Al/Al3+ and water start as soon as the sensor is biased. After some working hours, or maybe days, the aluminum pad of the supply pin is destroyed, so that an open circuit on the Vcc pin occurs. This is an aluminum corrosion phenomena. But the corrosion phenomena is stopped when the sensor supply voltage is switched off. There are also some other failure causes like galvanic corrosion, but the Mean Time To Failure (MTTF) due to these other causes much longer than the MTTF caused by electrocorrosion of the Vcc pad. Therefore electrocorrosion is the major failure cause, and they are permanent. I would also recommend taking a closer look at our AN3728 about media compatibility. If you have any further questions and do not want to use this forum, you can contact our technical support team by following these steps. 1) Go to http://www.nxp.com/support/sales-and-support:SUPPORTHOME. 2) On the bottom of the page under Submit new tickets, click "Hardware & Software". 3) Register with your business email to access NXP technical online support. 4) A verification email will be sent to your account. Click the link embedded in that email to verify your access. 5) On the NXP online support page, select Contact Support from the top menu and click “Submit a new case” to start the process. I hope it helps. Regards, Tomas PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
查看全文
FRDM-FXS-MULTI-BへのBluetooth接続に関する問題 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> デスクトップ コンピューター (外付け USB Bluetooth ドングル) に FRDM-FXS-MULTI-B を Bluetooth で接続する際に問題が発生しています。 KL-25 ボードのファームウェアをフラッシュし、ボードを積み重ねた後、Blueradio をデスクトップとペアリングすると、2 つの COM ポートが表示されます。ただし、センサ Fusion Toolbox (自動検出と手動ポート選択の両方を使用) を実行しようとすると、何も起こりません。Bluetooth COM ポートの 1 つを手動で選択すると、自動検出ボタンの横にある赤い円が青に変わりますが、ボードのイメージは変わりません。また、他のタブにはデータが表示されません。 Bluetooth 無線をオフにして、ボードを USB ケーブルで接続すると、Toolbox は USB COM ポートを使用してシームレスに実行されます。 スマートフォンで Android アプリを実行できません (Google Play ではアプリがスマートフォンと互換性がないと表示されます) が、VT100 ターミナル エミュレーター (Blueterm) を試しました。blueradio に接続すると、ターミナル画面に文字が表示され始め、Bluetooth 無線の横にある青い LED も点灯しました。 何が起こっているのか、何かアイデアはありますか?私は CSR Bluetooth ドングルを使用しており、Windows の汎用ドライバと同じチップセットのドライバの両方で試しました。Windows 7 では、表示されるポートは COM18 と COM19 です。 よろしくお願いいたします。 センシング・プラットフォーム Re: Problems connecting Bluetooth to FRDM-FXS-MULTI-B <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 返信に時間がかかりすぎて申し訳ありません。今のところ、MULTI ボードの Bluetooth 無線に PIN を割り当てる方法がわかりません。 Re: Problems connecting Bluetooth to FRDM-FXS-MULTI-B <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、アントニオ。 同意します。これは Windows/Bluetooth スタック/USB ドングルの問題のように思えます。固定 PIN を要求する Bluetooth ファームウェア アップデートを見つけることができましたか? また、それは機能しましたか? ありがとうございます モーリーン Re: Problems connecting Bluetooth to FRDM-FXS-MULTI-B <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、デイビッド。 回答に時間がかかってしまい申し訳ありません。私は他のプロジェクトに取り組んでいました。 まず、J6 ピン 2-3 のジャンパーを忘れていました。しかし、それを修正した後でもBluetoothでは動作しませんでした。Bluetooth 無線をオフにし (J7 のジャンパーを取り外す)、SDA COM ポートを使用して SDA USB ケーブルを接続すると、完璧に動作します。つまり、センサ ボードが接続されていれば、デモ プログラムは完璧に動作します。 いくつかのフォーラムで確認したところ、Windows 7 および 8 では、PIN を使用せずに Bluetooth 無線をペアリングすると (これが該当します)、COM ポートは作成されますが、開くことができないことがわかりました。デモ プログラムはすべてのポートをスキャンしますが、スキャンの途中でしばらく停止することがわかります。COM ポートを開こうとして、タイムアウト後に先へ進むようです。 Realterm を使用してポートを開こうとしましたが、ポートを開こうとするとエラーが発生します。したがって、私の問題は Windows 7/8 の Bluetooth スタックに関連する問題のようです。つまり、Windows 7/8 を使用している場合、ポートは作成されますが、ボード無線をペアリングするときに PIN が必要ないため、開くことができません。 おそらく、Bluetooth 無線設定のファームウェア アップデートが機能するでしょう。無線が固定の PIN (たとえば 0000) を要求する場合は、機能するはずです。ラジオのドキュメントをチェックして、それが可能かどうか確認してみます。 それでは。 アントニオ Re: Problems connecting Bluetooth to FRDM-FXS-MULTI-B <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、アントニオ。 FRDM-KL25Z と FRDM-FXS-MULTI-B を動作させる方法は次のとおりです。 FRDM-KL25Z SDA USBコネクタにUSBケーブルを接続しました。 私の Win7 ノートPCには、リムーバブル ストレージ デバイスが表示されます。 次に、Xtrinsic デモ S-Record を FRDM-KL25Z (E: ) ストレージ ドライブにドラッグ アンド ドロップしました。 C:\Freescale\Freescale Xtrinsic FXLS8471Q デモンストレーション\Freedom Images\fxls8471q_CLI_27SEP2013.srec Windowsの「デバイス マネージャー」のポート フォルダーを見ると、次のようになります。 これは、OpenSDA が動作していることを確認するのに役立ちます。私のはCOM72として列挙されました。 プログラムが完了したら、FRDM-KL25Z SDA USB コネクタ (この USB はオンボードの K20 デバッガー MCU に接続されています) から USB ケーブルを外し、再度接続してパワーオン リセット (POR) を実行します。 115200 ボー、8 ビット、1 ストップ、パリティなしで OpenSDA COMx (私の場合は COM72) を使用してターミナル ウィンドウを開きます。 開いたら Enter キーを押すと、ターミナルに次のように表示されます。 これは、Xtrinsic Freedom ボードからの通信チャネルが VCOM CDC プロトコルを使用して OpenSDA デバッガー インターフェイスを通過していることを示しています。 次に、ターミナル ウィンドウを切断するか閉じて、デモ アプリケーションを開きます。 C:\Freescale\Freescale Xtrinsic FXLS8471Q Demonstation\Freescale Xtrinsic FXLS8471Q Demo.exe この Xtrinsic アプリケーションは、COM ポートをスニッフィングして、FRDM-FXS-MULTI-B にコネクテッドなポートを探します。完了するとアプリケーションが開き、次のようになります。 Freedom ボードを持ち上げて回転させたり振ったりして、3 軸データを確認します。 デモを終了…切断SDA USBコネクタ用のUSBケーブル。 Bluetooth を動作させるには、FXLS8471QDEMOSWUG.pdf の指示に従う必要がありました。 簡単に言うと (しゃれですみません)、FRDM-FXS-MULTI-B ボードに次のジャンパーを追加する必要があります。 J6ピン2-3 J7オン(ピン1-2) J22オン(ピン1-2) SW1 オン。 「デバイス マネージャー」に戻り、USB ケーブルをいずれかの USB コネクタに再接続して、Freedom システムの POR を実行します。 「デバイス マネージャー」ウィンドウで、「アクション」→「ハードウェア変更のスキャン」を実行し、少し待ちます--> (30 秒未満)。 PC は新しいハードウェアをスキャンし、BlueTooth COM ポートを見つけて表示します。私のはこんな感じです: ターミナル アプリケーションを低い番号の COM ポート (私の場合は COM81) で開き、Enter キーを押します。 次のように表示されます。 コマンドリストを表示するには「?」を入力します。 これで、BlueTooth COM ポートが動作していることがわかりました。ここで、ターミナル ソフトウェア アプリケーションを切断するか、終了します。 C:\Freescale\Freescale Xtrinsic FXLS8471Q Demonstation\Freescale Xtrinsic FXLS8471Q Demo.exe を開きます。 Xtrinsic プロトコルが動作している COM ポートを検索し、以前と同じようにデータを表示できます。 最後に…Bluetooth COM 用に構成されている場合は、COM に OpenSDA ポートを使用しないでください。そうしないと、競合の問題が発生する可能性があります。これが、COM ポートも列挙される SDA USB コネクタではなく、KL25Z USB に USB ケーブルを接続してシステムに電源を供給した主な理由です。 これがお役に立てば幸いです。 よろしくお願いいたします。 デビッド Re: Problems connecting Bluetooth to FRDM-FXS-MULTI-B <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、 これまでのところ、私の PC でセンサ フュージョン ツールボックスを実行することはできませんでした。別のデバイスで Android アプリを試してみました (Google Play ではアプリが私のスマートフォンと互換性がないと表示されます...)なぜか不思議です。私は Android 4.1 を使用していますが、他のデバイスは別のブランドですが、同じバージョンを使用しており、問題なく動作します。 これまで試してみたところ、Windows Bluetooth スタックは BlueRadio モジュール用の仮想 COM ポートを作成しているようですが、何らかの理由でこのポートを開くことができません。私は、ボードから何かが送信されているかどうかを確認するために realterm を使用しようとした後、この結論に達しました (スマートフォンの Android VT100 ターミナル アプリを使用してこれを実行したところ、機能しました)。realterm を使用すると、COM ポートを開くことができないというメッセージのみが表示されました。 現在の問題は、実際には Windows - Bluetooth スタック - USB ドングルの非互換性にあるようです。 他にもこのような問題を抱えた人はいますか? Re: Problems connecting Bluetooth to FRDM-FXS-MULTI-B <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、トーマス。 まず、Android アプリは私のスマートフォンと互換性がないと Google が言っているので、試していません (なぜでしょうか...)。スマートフォンで VT100 シリアル ターミナル アプリを使用して、ボードの Bluetooth 無線が送信されているかどうかを確認してみました。スマートフォンがボードからデータを受信していることを確認しました。 PC 側に関しては、あらゆることを試しました。すべてのデバイス (blueradio と opensda) を削除し、blueradio を再度ペアリングしましたが、何も変わりませんでした。 インストール中に何か間違ったことをしたのかもしれません。ノードロックライセンスがインストールされていない可能性があります。しかし、OpenSDA シリアルポートを使用するとなぜ動作するのでしょうか? 何かご意見はございますか? Re: Problems connecting Bluetooth to FRDM-FXS-MULTI-B <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、モーレン。 最初にボードを PC の Bluetooth とペアリングしようとしましたが、成功しませんでした。その後、スマートフォンにアプリをインストールしようとしましたが、Play ストアではアプリがデバイスと互換性がないと表示されます。SO、VT100ターミナルアプリ(Blueterm)を使用して、スマートフォンのCOMポートを開いてみたところ、データ転送ができました(スマートフォンのターミナル画面に文字が表示されました)。 OpenSDA から USB シリアルを使用して PC にデータを転送することもできます。ボードの Bluetooth を PC とスマートフォンの両方に同時に接続していないことは確かです。すべてのテストは、他のデバイスに接続する前にペアリングしてからペアリングを解除して行いました。 トーマスの提案を試してみて、何が起こるか見てみましょう。ご返信ありがとうございます。 アントニオ Re: Problems connecting Bluetooth to FRDM-FXS-MULTI-B <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、アントニオ。 ターミナルに接続したとき、それは PC 上ですか、それとも Android デバイス用のターミナル アプリがありますか?BlueRadio を複数のデバイス (PC と Android デバイスなど) に同時にペアリングしようとしていないことを確認してください。PC ツールボックスを動作させようとしている場合は、Android デバイスの Bluetooth を無効にし、Freedom ボードを POR してから、PC ツールボックスを開くことをお勧めします。 マウレン Re: Problems connecting Bluetooth to FRDM-FXS-MULTI-B <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、アントニオ。 PCの場合:まず、Windows 7の「デバイスとプリンター」ダイアログから、インストールされているBluetoothデバイスを削除することをお勧めします。既存のデバイスを右クリックし、「デバイスの削除」を選択します。デバイスマネージャーで「ポート」を展開し、OpenSDAまたはBluetoothポートをすべて削除します(「デバイスのドライバーソフトウェアを削除する」チェックボックスはオンにしないでください)。その後、「デバイスとプリンター」に戻り、ボードのペアリングを行います。その後、ツールを再度お試しください。こちらもご覧ください: https://community.freescale.com/thread/322592 Androidの場合:「最近使ったアプリケーション」リストでアプリケーションを右にスワイプして完全に終了してください。古いプロセスが残っていると問題が発生する可能性があります。http: //www.freescale.com/sensorfusionには、問題解決に役立つ動画も掲載されています。ページ右側の「動画で見る」リンクをクリックしてください。Bluetoothのトラブルに特化した動画があります。 お役に立てれば幸いです。 よろしくお願いいたします。 トーマス 追伸: 私の回答がご質問の解決に役立った場合は、「正解」または「役に立った」と評価してください。ありがとうございます。
查看全文
Media Resistant Gel on MPXA6115AC6U I see that the MPXAZ6115A is now obsolete, but there is an identical part the MPXA6115AC6U. One difference from the data sheet is the MPXAZ6115A  has media resistant gel and the MPXA6115AC6U does not. What is the purpose/function of the media resistant gel? Pressure Sensors Re: Media Resistant Gel on MPXA6115AC6U Hi Erich, From the MPXAZ6115A series, the following packaged options are still available as shown on the MPXx6115 Buy/Parametrics website: MPXAZ6115AC6T1 MPXAZ6115AP MPXAZ6115APT1  Their media resistant gel die coat and durable polymer package provide an improved media resistant barrier that allows the sensor to operate reliably in high humidity conditions as well as environments containing common automotive media. More information can be found in this discussion. Regards, Tomas PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.
查看全文
MAG3110 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 同じ PCB に 4 つの MAG3110 を配置したいのですが、センサ間に最小距離があるかどうか知りたいです。 よろしくお願い申し上げます。 磁気センサ Re: MAG3110 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 助けてくれてありがとう。2個で試してみます。 よろしくお願い申し上げます。 よろしくお願いいたします。 Re: MAG3110 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、キム・ダット・トランさん。 同じ PCB 上に 4 つの磁力計を互いに近づけて配置すれば、問題は発生しないと思います (私たちは、数十個の MAG3110 を可能な限り近づけて配置した PCB を開発しましたが、問題は発生しませんでした)。電流トレースが漂遊磁界を発生させないようにレイアウトに注意してください。 MAG3110 のレイアウト推奨事項に関する有用な情報は、アプリケーション ノートAN4247に記載されています。 すてきな一日を、 ホセ・レイエス ----------------------------------------------------------------------------------------------------------------------- 注: この投稿で質問が解決した場合は、「正解」ボタンをクリックしてください。ありがとう! -----------------------------------------------------------------------------------------------------------------------
查看全文
MPXA6115AC6U 上的抗介质凝胶 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我发现 MPXAZ6115A 已经过时,但还有一个相同的部件MPXA6115AC6U。 数据表上的一个区别是,MPXAZ6115A具有抗介质凝胶,而MPXA6115AC6U 没有。 耐介质凝胶的目的/功能是什么? 压力传感器 Re: Media Resistant Gel on MPXA6115AC6U <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,埃里希、 在 MPXAZ6115A 系列中,以下软件包选项仍然可用,如 mpxx6115 购买/参数化网站上所示: MPXAZ6115AC6T1 MPXAZ6115AP MPXAZ6115APT1 它们的耐介质凝胶模具涂层和耐用的聚合物封装提供了改进的耐介质屏障,使传感器能够在高湿度条件下以及包含普通汽车介质的环境中可靠地运行。更多信息请参见本讨论。 此致, 托马斯 PS: 如果我的回答有助于解决您的问题,请标记为"正确" 或 "有帮助"。谢谢。
查看全文
MPX5700DPセンサの製品寿命はどのくらいですか? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは。私たちのチームはMPX5700DPセンサーを使用して差圧を測定していますが、図のように変化します(圧力は1秒間に約5回変化します)。この場合、センサーは100万回の変化をサポートできますか?あるいは、何回までサポートできますか?よろしくお願いします!@@ 圧力センサ Re: How about of the product’s lifetime of MPX5700DP sensor <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ありがとう!すでにセールスとサポートにメッセージを送信しました。 Re: How about of the product’s lifetime of MPX5700DP sensor <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、 要求された情報を取得するには、Freescale Web 経由でサービス リクエストを作成できます。 セールスとサポート|フリースケール すてきな一日を。 デビッド
查看全文
ISF2P2_K22F_MQX_SF_PROJ Outputting Incorrect Data? Hello, Using KDS 3.2.0 and SDK 1.2.0. I followed all the steps to update KDS and update Processor Expert with ISF2P2_PEx.PEupd. I know the hardware is ok because when I download FSFK-K22F-AGM01-GL-NED.bin (from the Sensor Fusion GUI) to flash the board the GUI display works great!   However, when I program the board with the SF2P2_K22F_MQX_SF_PROJ the GUI does not display the board orientation properly because the data being sent to the GUI is not right. Here is a screen shot using the "working program", FSFK-K22F-AGM01-GL-NED.bin:   And below is a ("not working") screen shot using ISF2P2_K22F_MQX_SF_PROJ: The Inclination Delta should be 66.7 degrees and the Field Strength is 55.2uT for my location. The working program matches these values almost exactly but ISF2P2_K22F_MQX_SF_PROJ is way off with an Inclination Delta at 45.4 degrees. I also noticed that the hard iron vector is different between the two, and should be about the same since it is the same hardware. Right?   I could go on comparing screen shots, but the point is that something is not right. The Gyro Stabilized Compass is not working correctly at all. North is not anywhere near North and when the board is moved the displayed motion does not reflect the motion of the hardware.   Q1. Has anyone gotten ISF2P2_K22F_MQX_SF_PROJ to work properly? Q2. Regarding the .bin I mentioned above (FSFK-K22F-AGM01-GL-NED.bin) that works great. Is the project that  generated that file available? Q3. Is there a Gyro Stabilized Compass example that uses Bare Metal?   Thanks, Mark Intelligent Sensing Framework Re: ISF2P2_K22F_MQX_SF_PROJ Outputting Incorrect Data? Mark, I just looked at the ISF SF build with one of our other engineers, and confirm I am seeing weirdness in a couple places.  I don't like the gyro numbers and magnetic buffer updating doesn't look right to me.  If you are in a hurry, I would suggest you download the "standalone" sensor fusion V5.00 release at nxp.com/sensorfusion.  That is the version that was used to build the binaries that the Sensor Fusion Toolbox flashes to the board. In the meantime, we'll dig into the ISF implementation issues and get back with you when we know more. Regards, Mike Re: ISF2P2_K22F_MQX_SF_PROJ Outputting Incorrect Data? Hey Dave, Sorry for the delay in getting back. I was stuck again for a few hours with not being able to launch the debugger in KDS. I was getting the familiar, "error in services launch sequence". This time the cure was to kill the P&E Multilink GDB Server: pegdbserver_console in windows task manager. And voila, it works again. Whew! I was not using Freedom Sensor Toolbox Rev 2.3.2. However, I did try that one and the results are the same. Thanks, Mark Re: ISF2P2_K22F_MQX_SF_PROJ Outputting Incorrect Data? Hi Mark, I assume you are running the Freedom Sensor Toolbox Rev 2.3.2 that is shown on the Downloads tab at nxp.com/isf?  We also provide a stand-alone open source version of the Sensor Fusion and a stand-alone GUI, but it doesn't work with ISF 2.2 at this point. Dave...
查看全文
MPxx5004 temperature ratings. The temperature rating numbers are confusing for this series of sensors.  There is the "Ambient Operating Temperature (Min-Max) (°C)" value of -40 to 100 from the Product selector.  That looks good to me.  But then there are two numbers on the datasheet Absolute Maximum Ratings table: Storage Temperature of -30 to 100 °C and Operating temperature of 0 to 85 °C.  Which is it? My application would be in an environment -40 to 85 °C, but the sensor would only be read when the temperature was in the 0-60 °C range (it would always be powered). Robert Pressure Sensors Re: MPxx5004 temperature ratings. Hello Robert, Exposing the MPxx5004 to -40 °C is beyond the spec limits of the device so although the sensor may work fine for your application, we cannot guarantee the sensor will operate properly. The issue is the Gel inside the sensor can stiffen at temperatures below -30 °C. The stiffening can cause the wire bonds to break. There is a guard band associated with this so depending how often, how long and much below -30 °C the device is exposed to, the sensor may be okay for your application. You would have to do your own testing and validation. Best regards, Tomas
查看全文
用于 FXLS8962AF 的断路器/库? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我对这种超低功耗 3 轴加速度计很感兴趣,但我找不到可以入手的东西。 是否计划设立分会场和/或图书馆? Re: Breakout / Library for FXLS8962AF ? 嗨,托马斯、 用于 imx 平台的 fxls8962af 驱动程序准备好了吗? 如果不是,请告诉我上市日期。因为我们急需为客户提供软件支持。 顺祝商祺! 酋长 Re: Breakout / Library for FXLS8962AF ? 嗨,托马斯、 用于 imx 平台的 fxls8962af 驱动程序准备好了吗? 如果不是,请告诉我上市日期。因为我们急需为客户提供软件支持。 顺祝商祺! 酋长 Re: Breakout / Library for FXLS8962AF ? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,Yann、 FXLS89xx加速度计系列尚未完全发布,目前预计上市日期为2021年第一季度。 评估板的数量非常有限,需要我们的营销团队的批准。 在 MCUXpresso 中创建的驱动程序和代码示例可根据标准支持请求提供。 顺祝商祺! 托马斯
查看全文
タイヤ空気圧モニターセンサー (TPMS) MPXx85/86xxD のファームウェア ドキュメントはありますか? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 私は MPXY8500B チップ用の最初のアプリケーションを開発しようとしています。Freescale の Web サイトからデータシートを入手しましたが、そこにはファームウェア ルーチン (TPMS_RESET、TPMS_READ_VOLTAGE) とルーチンのアドレスがリストされているだけで、各ルーチンの完全な詳細 (パラメータ、予想される戻り値、ルーチンの副作用など) は示されていません。これらのルーチンの関数プロトタイプのリストはどこで見つけることができますか?さらに良いことに、ソースコードはどこにありますか? 圧力センサ Re: Firmware documentation for Tire Pressure Monitor Sensor (TPMS) MPXx85/86xxD? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、ジョナサン。 残念ながら、要求された情報は NDA ライセンス契約の対象であり、送信する権限がありません。この種の文書を取得するには、営業担当者、FAE、または代理店に**お問い合わせください**。 「MPXx85/86xxxD 組み込みファームウェア ユーザー ガイド」を要求してください。 よろしくお願いいたします。 ホセ
查看全文
FXOS8700 accelerometer only function does not work sometimes. My FXOS8700 sensor is applied on MX6 based android platform. When both of acc and mag sensor in FXOS8700 enabled, everything okay. But when I only enable accelerometer in FXOS8700, it's g value in 3-axis won't be updated sometimes. Driver is from Freescale (attached files). Anyone got similar issue? Original Attachment has been moved to: fxos8700.h.zip Original Attachment has been moved to: fxos8700.c.zip Re: FXOS8700 accelerometer only function does not work sometimes. Hi Jamesbone, Thanks for the reply.since we are using i.Mx 6solo processor in our project. we need support for FXOS8700CQ accelerometer source code.kindly oblige. Regards Re: FXOS8700 accelerometer only function does not work sometimes. You download the BSP for the WandBoard from the FSL site? right? Because this is not the official FSL BSP, which it is only for the SABRE SDP, SDB and Auto. Re: FXOS8700 accelerometer only function does not work sometimes. Hi Raymond, Yes , the code is availble in free scale. Me also same issue. I also working on FXOS8700CQ sensor. O.S: Kernel 3.0.35 Board : Wand board i.Mx6 solo Multimedia processor Re: FXOS8700 accelerometer only function does not work sometimes. Hi , The same issue. The source code is avilble on freescale. I also tries it. At initial stage it is working minimum time like generating events for 20sec. Now I am not getting any out put. No error messages. probe is calling fine. presently I am working on i.Mx 6solo ; Linux version:3.0.35; wand board. If any one have proper solution/source code for this ? Re: FXOS8700 accelerometer only function does not work sometimes. Does anyone got this similar issue ? Re: FXOS8700 accelerometer only function does not work sometimes. This driver is fetched from FreeScale. Our board is a custom board based on MX6Q SabreSD. Acc and Mag function are verified. This issue is reported recently by our TE. Re: FXOS8700 accelerometer only function does not work sometimes. Hello Raymond, Can you please tell me where do you get this source code?,  Because in the Freescale Official Boards with i.MX6 there is no FXOS8700, which makes me the doubt if the driver has been tested and it is just and add on to the BSP of a custom board.  Can you please clarify if this is the case? Have a great day, Jaime ----------------------------------------------------------------------------------------------------------------------- Note: If this post answers your question, please click the Correct Answer button. Thank you! -----------------------------------------------------------------------------------------------------------------------
查看全文
Freedom 传感器工具箱 - 无法下载固件 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好 我拼命想让 Freedom Sensor Toolbox (CE) (v2.0.0.) 与 FRDM-K64F 底座和 FRDM-STBC-AGM01 子卡一起运行。 我做了 DAPLink 的所有更新,但仍然收到错误信息: "固件下载不成功。请参见《STB-CE 用户指南》[...]" 当我插上设备时,我看到一个 FRDM-K64FD 设备而且 details.txt 包含以下信息: # DAPLink 固件 - 参见 https://mbed.com/daplink 唯一 ID:0240000033904e4500293013912700142041000097969900 HIC ID:97969900 自动重置:0 允许自动化:0 溢出检测:0 Daplink 模式:接口 接口版本:0244 Bootloader 版本:0244 Git 安全散列算法 (SHA):5f9092d41cfd6601fef7b3b467fe8f8767b01f84 本地模组:1 USB 接口:MSD、CDC、HID Bootloader CRC:0x251003d3 接口 CRC:0x0676bc5d 重装次数:0 谁能帮帮我?我真的需要把这些东西弄好,否则传感器就会从评估中消失,那就太遗憾了... 非常感谢您! Re: Freedom Sensor Toolbox - Firmware download not possible <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,马蒂亚斯、 您想运行哪个图形用户界面演示? 有 3 种硬件可供选择: 你可以尝试手动刷新 K64F 演示固件,只需将 & 拖放到 FRDM-K64FD 驱动器中相应的二进制文件即可。 二进制文件位于 F reedom Sensor Toolbox (CE)\ Projects 安装文件夹中: C:\Program Files (x86)\NXP\Freedom Sensor Toolbox (CE)\Projects\FXAS21002 Gyroscope Demo\Firmwares\ISSDK\FRDM-K64F_FRDM-STBC-AGM01_21002_2.0.bin C:\Program Files (x86)\NXP\Freedom Sensor Toolbox (CE)\Projects\FXOS8700 6-axis (Accel, Mag) Demo\Firmwares\ISSDK\FRDM-K64F_FRDM-STBC-AGM01_8700_2.0.bin C:\Program Files (x86)\NXP\Freedom Sensor Toolbox (CE)\Projects\9 Axis Orientation Sensor Demo\Firmwares\ISSDK\FRDM-K64F_FRDM-STBC-AGM01_Orient_2.0.bin 然后上市 FSTB (CE) 并运行关联的 GUI。 让我知道这是否解决了你的问题。 再见,雅克
查看全文
MAG3110 AUTO_MRST_EN Hello,   I am using the MAG3110 in trigger mode. I want to know if I set the AUTO_MRST_EN during the device initialization if the setting sticks or do I have to set it every time I trigger a measurement? Thanks Deric Re: MAG3110 AUTO_MRST_EN Hello Deric, There is no need to set the AUTO_MRST_EN bit every time you trigger a new measurement, it remains set in both the triggered and continuous measurement modes. Regards, Tomas PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
查看全文
SPI write problems on an own reflown FXOS8700 I have reflowed an FXOS8700 to my own development card as an breakout to be able to use it in a project. I am now unsure if it works proper or not. Is the possibility to read but not write a sign of a burnt FXOS8700 in the reflow process???? SPI setting are CPOL=0 and CPHA=0: I have no problem to read from an address, but problem to read back what was written. This is my sequence of SPI commands:     // WHO AM I     SPI_ReadFXOS(WHO_AM_I, rbuf, 1);     sprintf_P(buffer_0, PSTR("\r\n::WHO AM I = 0x%X\r\n\r\n"), rbuf[0]);     uart_puts(buffer_0); => 0xC7     // Temperature     SPI_ReadFXOS(TEMP, rbuf, 1);     sprintf_P(buffer_0, PSTR("\r\n::TEMP = %i\r\n\r\n"), rbuf[0]);     uart_puts(buffer_0); => 21 Both above works as aspected!!!!     // Acc + Mag TEST     SPI_WriteFXOS(CTRL_REG1, 0x00);        // Set to standby mode     SPI_ReadFXOS(CTRL_REG1, rbuf, 1);     sprintf_P(buffer_0, PSTR("\r\n::CTRL_REG1 = 0x%X\r\n\r\n"), rbuf[0]);     uart_puts(buffer_0);     SPI_WriteFXOS(M_CTRL_REG1, 0x1F);    // 200 Hz hybrid mode     SPI_ReadFXOS(M_CTRL_REG1, rbuf, 1);     sprintf_P(buffer_0, PSTR("\r\n::M_CTRL_REG1 = 0x%X\r\n\r\n"), rbuf[0]);     uart_puts(buffer_0); => 0x00 Writing to M_CTRL_REG1 does not work but gives 0x00 back ...... Accelerometers Magnetic Sensors Re: SPI write problems on an own reflown FXOS8700 Thanks a bizillion times Tomas! You are my hero and made my day, truly I had used a macro (atmega8) in as if it returned the first bit as set, and it stayed to the second byte ... Now all three modules work just fine!!!! Best Regards, Hans-Henrik P.S: For anyone interested in atmega8 code looks like: // Set FXOS8700 in SPI mode void init_spi(void) {     FXOS_SS_ENABLE;  // To open tri-state buffer and set MISO high     MISO_HI;                    // SPI init demands SA0/MOSI high during reset     FXOS_RESET_HI;     // Active high     _delay_ms(1);             // ??     FXOS_RESET_LO;     _delay_ms(1);              // FXOS8700 Datasheet defines 1ms wait after reset [p.19]     FXOS_SS_DISABLE; } // Read values from register FXOS8700 void SPI_ReadFXOS(uint8_t reg, volatile uint8_t* rbuf, uint8_t len) {     FXOS_SS_ENABLE;     ATOMIC_BLOCK(ATOMIC_RESTORESTATE) {         SPDR = cbi(reg,7);                    // Transmit; clear bit 7 for reading + 7 bits of register address         while(!(SPSR & 1<         SPDR = reg;                            // Transmit bit 7 of register address         while(!(SPSR & 1<         for(uint8_t i=0; i             SPDR = 0x00;                    // Transmit             while(!(SPSR & 1<             rbuf[i] = SPDR;                    // Clear SPIF flag 2/2         }     }     FXOS_SS_DISABLE;                // 2) For ISR context switcher which re-enable SPI unit } // Write value to register FXOS8700                                       <------------------------- ineffektiv loop void SPI_WriteFXOS(uint8_t reg, uint8_t val) {     FXOS_SS_ENABLE;     uint8_t reg1 = reg;     sbi(reg1,7);     uint8_t wbuf[3] = {reg1, reg, val}; // Two bytes for write bit and address     ATOMIC_BLOCK(ATOMIC_RESTORESTATE) {         for(uint8_t i=0; i<3; i++) {             SPDR = wbuf[i];                    // Transmit             while(!(SPSR & 1<         }     }     FXOS_SS_DISABLE;                // 2) For ISR context switcher which re-enable SPI unit } Re: SPI write problems on an own reflown FXOS8700 Just for illustration, here is an example of writing/reading the value of 0x3D to/from the CTRL_REG1 (0x2A): Best regards, Tomas Re: SPI write problems on an own reflown FXOS8700 Hi Hans-Henrik, It seems like your both write sequences are not correct. The order of the bits is as follows: Byte 0: R/W, ADDR[6], ADDR[5], ADDR[4], ADDR[3], ADDR[2], ADDR[1], ADDR[0] Byte 1: ADDR[7], X, X, X, X, X, X, X Byte 2: DATA[7], DATA[6], DATA[5], DATA[4], DATA[3], DATA[2], DATA[1], DATA[0] The first byte you are sending is correct, but the MSB bit of the second byte (ADDR[7]) should be "0" and not "1". So instead of sending 0xDB, 0xDB, 0x1F, try to send 0xDB, 0x00, 0x1F. Then send 0x5B, 0x00, 0x00 to read back 0x1F from the M_CTRL_REG1 register. Hope it helps. Best regards, Tomas Re: SPI write problems on an own reflown FXOS8700 Now I have reflowed another two FXOS8700 vary carefully, and both of them show identical characteristics. It is not possible to write to a register and than read it back, what can possible be wrong??
查看全文
NTM88 example code Hello, We are an engineering company currently working on a project involving the NTM88 sensor family. We are interested in using these sensors in a TPMS application. Could you kindly open a support ticket on our behalf or connect us with the relevant technical team for further assistance regarding product selection, development tools, and integration? We appreciate your support. Best regards, AISET TECHNOLOGY Co. Inc. Pressure Sensors Re: NTM88 example code Hello Wolke_Trailer_Systems Of course! My entire team will be gland to help you. But you need to open the ticket, this action is required on your part to confirm identity and by protocol If you want a more private help with your issue please open the thicket here: https://support.nxp.com/s/?language=en_US You can find our code examples in the software session on our official NTM88 page. I hope this information has helped you, please let me know if you need help with anything else. Have a great day and best of luck.
查看全文
E-Compass ソフトウェア、AN4676、AN4681 などを探しています。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 私は、E-Compass ソフトウェアと、それに付属するとされるアプリケーション ノート (AN4676、AN4681、AN4684、AN4685、AN4696、AN4697、AN4698、AN4699、AN4700、AN4706、AN4709 など) を探しています。 E-Compassソフトウェアのページは、例えば以下の説明には記載されていない新しいセンサーフュージョンツールキットにのみ誘導しているようです。「磁気キャリブレーションを備えた傾き補正電子コンパス用ソフトウェア」( http://cache.freescale.com/files/sensors/doc/fact_sheet/eCompassFS.pdf ) には、特にこれらのアプリケーション ノートは含まれていません。 センサ・フュージョン Re: Looking for E-Compass software, AN4676, AN4681, etc. <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 「しかし、結局のところ、このようなアプリケーションには、ハードウェアとインターフェースするドライバーが必要になります。」 概念的にはそれは逆で、ソフトウェア パッケージがハードウェア選択プロセスを推進しているように見えますが、それが常に悪いことというわけではありません。 はい、明らかに、組み込み関連チップにはハードウェアとソフトウェアのインターフェースがあります。 私は、自社製品にデザインを施すハードウェアを購入しようとベンダーを訪問します。 私が確認したいのは、そのハードウェアがどれだけ簡単に使用できるかということです。 ベンダー A とベンダー B のどちらを使用するかを決定するために何かをインストールする必要があることは、チップの使用方法を単純に確認するための問題です。 あなたが「ドライバ」について言及したという事実自体が、どのチップを使用するかを決めるのが過度に複雑であるという警告を私に与えます。 ご存知のとおり、アプリケーション ノートが役立つのはまさにこの点です。 すべてが 1 か所にパッケージ化されているのは良いことです。センサ フュージョンがいかに複雑であるかは理解していますが、カルマン フィルターの定数などを調べるのに、あまりにも多くの時間を費やしてきました。 Re: Looking for E-Compass software, AN4676, AN4681, etc. <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ボブ、 バージョン 7.00 は、可能な限りプラットフォームに依存しません。しかし、結局のところ、このようなアプリケーションには、ハードウェアとインターフェースするドライバが必要になります。ハードウェアを変更する場合は、ドライバを交換する必要があります。他に方法はないのです。 私は、Freescale/NXP の一般的なドキュメントに関して、皆さんの意見に一部同意します。そのため、センサー フュージョン アプリのノート、データシート、ユーザー ガイドはすべてソフトウェアにバンドルされています。このトピックは複雑なので、私たちはこのパッケージに多大な労力を費やし、できるだけ理解しやすいものにするよう努めています。ただし、これらのいずれかを利用するには、ダウンロードする必要があります。 センサ フュージョン コードの SDK 構造内の場所を確認するには、 https://community.nxp.com/thread/444092の下部にある私の最後の投稿を参照してください。 Mike Re: Looking for E-Compass software, AN4676, AN4681, etc. <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 「プラットフォームに依存しない C コード」が、この疑問が生じる理由の 1 つです。 あなたの返信には、「プラットフォームに依存しない C コード」がオプションであるようには聞こえませんでしたか? おそらく、無限にネストされたヘッダー ファイル内のこれらのツールから抽象化の抽象化を削除した後に、「完全なソース コード」が利用可能になるということでしょうか。公平を期すために言うと、私は 7.00 を見たことはなく、古いツールから見たコードでの過去の経験に基づいて作業を進めています。 App Notes が公開されると、コードは App Notes で利用可能になり、引き続き利用可能になります。 数十年前に Motorola が公開したアプリケーション ノートや関連コードは、最近の Freescale/NXP のものよりも簡単に見つけられることがよくあります。:-( Re: Looking for E-Compass software, AN4676, AN4681, etc. <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このコミュニティの読者の誰もが、この情報がhttp://www.nxp.com/sensorfusionで入手可能であることに気づいていないことに驚いています。それは何年もそこにあり、私は定期的に人々にそれを紹介します。傾き補正 eCompass は、当社のオープン ソース センサ フュージョン ライブラリの標準コンポーネントです。2 つのバージョンがあります。バージョン 5.00 は、CodeWarrior、KDS、および Processor Expert に基づく少し古いツールチェーンを対象としています。バージョン 5.00 は、上記の URL にある別のインストーラーを介してダウンロードおよびインストールされます。バージョン 7.00 は KDS、IAR、Allolic をサポートしており、MCUXpresso SDK (旧 KSDK) をベースにしています。7.00 は、Welcome to MCUXpresso | MCUXpresso Config Toolsでビルドできる FRDM-K64F および FRDM-K22F の SDK の一部として提供されます (SDK をビルドするときに、FreeRTOS および ISSDK オプションを必ずチェックしてください)。どちらにも、詳細なドキュメント、完全なソース コード、特定の NXP ボード用のビルド済みプロジェクトが含まれています。他のハードウェアに移植する必要がある場合は、バージョン 7.00 から始めることをお勧めします。それを念頭に置いて再設計され、バージョン 5.00 に加えていくつかの追加機能が含まれています。 よろしくお願いいたします。 Mike Re: Looking for E-Compass software, AN4676, AN4681, etc. <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、エリックとアニル: 私はちょうど電子コンパスのソリューションを探し始めたところですが、皆さんと同じ問題を抱えていることがわかりました。私の最初の観察からすると、これらのチップから X、Y、Z を抽出し、便利で読み取り可能なコンパスの方向を作成する、機能的で便利なプラットフォームに依存しない C コードは、意図的に隠されているか、現実には存在しないか、Samsung、Apple、Ford Motors などの大手企業 (おそらく、e-Compass ソリューションを作成するために多大な研究開発費を費やした) の機密情報であるか、または「学生の課題として残されている」かのいずれかです。率直に言って、私はこの業界に完全に失望しています。この業界は「インダストリアル アプリケーション」ではなく「ドローンとゲームと趣味人」によって推進されているように思われます。私は、InvenSense、Bosch、STMicro、NXP など、「傾き補正」機能付き e-Compass を謳うメーカーを調べましたが、これらのデバイスは傾き補正が「可能」かもしれないが、そのようなすぐに利用できるソフトウェア ソリューションは実際には存在しないという結論に達しました。おそらく誰かが私の間違いを証明できるだろうが、それまでは、私はこの業界を「マーケティングの誇大宣伝」のトップに位置づけるつもりだ。 Re: Looking for E-Compass software, AN4676, AN4681, etc. <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、 また、eCompass の方向を取得するために同じ FXOS チップを使用しています。 問題は解決しましたか?私も同じ問題に直面しています。加速度センサの x、y、z と磁気の x、y、z データから RAW 値を取得しています。回転、ピッチ、ロールを変換できます。 しかし、eCompass の 0 ~ 360 度の方向値が必要です。RAW 値を使用して数式を適用する方法。私はジャイロを使用しておらず、加速度と磁気の値のみをfxosチップから取得しています。 0、90、180、270、360 の角度計算を取得または計算するための参照 C コードを入手しましたか。 よろしくお願いいたします アニル Re: Looking for E-Compass software, AN4676, AN4681, etc. <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> プラットフォームに依存しないソース コードを含むこのようなソフトウェア パッケージは、Windows 固有の自己解凍型アーカイブではなく、ZIP ファイルなどのプラットフォームに依存しない配布形式で提供されると便利です。Windows を実行しているシステムに何らかの形でアクセスできない人はおそらくほとんどいないでしょうが、一部の人にとってはあまり便利ではありません。私は Linux 上で Kinetis Design Studio を使用していますが、非常にうまく動作します (Linux バージョンを提供していただきありがとうございます)。 ありがとう! エリック Re: Looking for E-Compass software, AN4676, AN4681, etc. <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> どうやら、ダウンロードにアプリのノートが含まれていなかったため、私は混乱してしまったようです。いくつか同等のものが存在するようですが、私が知る限り、AN4698「CPU、フラッシュ、および RAM ベンチマーク」や AN4681「加速度センサと磁力計センサを使用した仮想ジャイロの実装」には同等のものはありません。また、データシートに記載されている「実際のセンサに接続する前にターゲット プロセッサですぐに検証できるようにシミュレートされた加速度センサおよび磁力計ドライバが提供されています」という記述も見つかりませんでした。また、KDS でコンパイルしても「合計コード サイズが 10 KB 未満」にはなりません。これにより、ダウンロードが適切ではなかったこと、また、完全なセンサー フュージョン パッケージに比べてよりシンプルな eCompass パッケージが存在することが考えられました。 AN4681 を入手できなかったのは特に残念です。これは非常に興味深く、役に立つ可能性もあるように思えました。 よろしくお願いします! エリック Re: Looking for E-Compass software, AN4676, AN4681, etc. <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、エリックさん。 「eCompass ソフトウェア パッケージ」とは何のことですか? ダウンロード リンクは [ダウンロード] タブの下にあります。その名前は " XTRINSIC_FUSION_LIB_KINMCU " です。これは、Kinetis MCU 用の eCompass ライブラリのコピーをインストールする実行可能ファイルです。 磁気キャリブレーションアルゴリズムは、Sourcesフォルダのどこかにあり、その名前は「magnetic.c」です。そのパスは次のようになります。 INSTALLATION_PATH\Codewarrior\FRDM_KL46Z\Sources\magnetic.c 残念ながら、ご参照のアプリケーション ノートは現在入手できず、eCompass ファクトシートも古くなっています。ご不便をおかけして申し訳ございません。ただし、必要なドキュメントはすべて、「インストール パス」の「docs」フォルダにあります。 お役に立てれば幸いです。 -ジョシュ Re: Looking for E-Compass software, AN4676, AN4681, etc. <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> はい、私はそのページを見つけました。そのページから私が言及した PDF を入手したのですが、私が知る限り、そのページのリンクのどれもが実際の eCompass ソフトウェア パッケージ (アプリケーション ノートを含む) のダウンロードにはつながりませんでした。一方、リンクの少なくとも 1 つはセンサー フュージョンのダウンロードにつながります。 おそらく私が鈍感なだけかもしれませんが、見つけることができません。ダウンロードできるのであれば、正しいダウンロードにたどり着くための正確な URL または正確なクリック順序が必要です。 よろしくお願いします! エリック Re: Looking for E-Compass software, AN4676, AN4681, etc. <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、エリックさん。 eCompass ソフトウェアの Web ページは次のとおりです。 http://www.freescale.com/ecompass Sensor Fusion のホームページ: http://www.freescale.com/sensorfusion -ジョシュ
查看全文
FXAS21002C 陀螺仪未通过自检 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 亲爱的同事们 在我们目前的项目中,我们计划使用 FXAS21002C 陀螺仪。印刷电路板是根据布局建议设计的,我们已经制造了几个原型。 但是,它们似乎都已失效,因为它们未通过X和Y轴的自检(值超出指定范围),并且尽管板在测试期间没有移动,但它会读取角度移动。Z 轴没问题,代码在围绕恩智浦的突破而构建的旧原型上运行良好。 会有什么问题呢? 此外,勘误文件FXAS21002CER指出,新的芯片修订版应解决 SPI 问题。如何确定新的修订?我们芯片的追溯日期代码为 FCSA。 谢谢! 亚当-海因里希 陀螺仪 Re: FXAS21002C gyro does not pass self-test <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Dobrý den Adame、 关于自测,我要求我们的设备组对此发表评论。 您或您的代理商可以下订单申请固定部件。它们没有特殊的 P/N,但 WW32'2015 对应的数据代码是 "DF"(xDFx)。WW33'2015 是 "DG",WW34 是 "DH "等。WW1'2016 则为 "EA"。如果您只需要一些样品,请告诉我,我可以直接提供。 S pozdravem、 托马斯 Re: FXAS21002C gyro does not pass self-test <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Dobrý den、 感谢您的快速回复。是的,它们超出了范围。精确的自检输出值为:X 489,Y 635(Z 为 16952,保持在指定范围内)。 我们如何从代理商那里订购固定芯片?新的 FXAS21002 是否有一些特殊的 P/N? Díky、 ADAM Re: FXAS21002C gyro does not pass self-test <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 亲爱的亚当 能否请您在此公布自检时得到的数值?是否超出了下图所示的指定范围? 陀螺仪偏移取决于温度、方向和加速度,其典型值为 ±50 LSBs @ ±2000 dps 范围: 零件标记中的"CS" 表示 2015 年第 19 周,因此您的旧零件存在 SPI 问题,详情见下文 FXAS21002CER. 顺祝商祺! 托马斯
查看全文