343660_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

343660_en-US

343660_en-US

Media Resistant Gel on MPXA6115AC6U

I see that the MPXAZ6115A is now obsolete, but there is an identical part the MPXA6115AC6U.

One difference from the data sheet is the MPXAZ6115A  has media resistant gel and the MPXA6115AC6U does not.


What is the purpose/function of the media resistant gel?

Pressure SensorsRe: Media Resistant Gel on MPXA6115AC6U

Hi Erich,

From the MPXAZ6115A series, the following packaged options are still available as shown on the MPXx6115 Buy/Parametrics website:

MPXAZ6115AC6T1

MPXAZ6115AP

MPXAZ6115APT1 


MPXAZ6115A Availability.JPG.jpg


Their media resistant gel die coat and durable polymer package provide an improved media resistant barrier that allows the sensor to operate reliably in high humidity conditions as well as environments containing common automotive media. More information can be found in this discussion.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

标记 (1)
无评分
版本历史
最后更新:
‎02-04-2026 07:21 AM
更新人: