Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
AFT05MP075N 需要 222mhz 的阻抗 我想知道 AFT05MP075N 频率为 222mhz。 虚拟测试 Re: Need impedance for AFT05MP075N at 222mhz 您好 恐怕我们没有 AFT05MP075N 的222MHZ特性数据。整个阻抗测量过程既费力又费时,因为必须对每个感兴趣的频率进行重复测量。请注意,允许进行表征的频率范围是电路调谐的频率范围。对于其他频率,必须设计和建造额外的测试电路,这就解释了为什么有时很难让半导体制造商为特殊工作条件(例如不同的频率、不同的功率级或不同的工作电压)提供阻抗数据。
View full article
BURY / MB:EB Tresos 配置,用于 S32K342 中加密驱动程序的新代码删除 团队 直接客户BURY在集成恩智浦上天向Bury发布的新的Code Drop S32K3XX_S32M27x_P20_CD01时面临着EB Tresos的配置问题。 客户怀疑交付的代码掉落具有与原始代码相同的模块 ID,因此 EB Tresos 无法将其识别为更新。 是否有任何变通方法可以正确配置,以获得更新加密驱动程序的可见性? 附上客户反馈和发送给客户的如何下载此代码 Drop 的说明。 BSSM 合同:否 客户公司*:BURY 项目名称*:835_069 Mercedes 50W WCH EPP (Huawei) https://nxp.lightning.force.com/lightning/r/Opportunity/0062p00001VNuIDAA1/view 客户联络点* (姓名& 电子邮件):Sebastian Draus [email protected] 软件& 硬件信息: 基于 S32K342 的 MWCT2D16 代码包信息*:RTD4.0.0 AS 4.4.0 硬件*(板/芯片组/平台):客户自己的板 SW 版本*: EB TRESOS 许可证 优先级:高 RTD 安全加密 资料来源直接客户 Re: BURY / MB: EB Tresos configuration for new Code Drop of Crypto Driver in S32K342 @Mateusz_Choromanski 在我 看来,客户同时安装了 P20 和 P24,而 EB Tresos 无法重新识别新的代码包。 请让他们按照以下步骤卸载旧代码包 P20: 1.前往 EB Tresos 目录:EB\ tresos\ links 此文件夹包含所有已安装代码包的路径。查找并删除 .link 文件 这将使 EB Tresos 断开与已安装的 RTD P20 的链接。 1.1 其他步骤:你可以通过访问已安装的 RTD 目录来永久卸载旧的 RTD 软件包-> uninst.exe 2.重新启动 EB Tresos。前往帮助 > EB Tresos 详情...> 模块注册表 确保只有 1 个加密代码包版本 P24 而不是 P20 和 P24  
View full article
编译 MPC5775K 外部中断时遇到的错误 亲爱的先生 当我为 MPC5775K 编译外部中断程序时,参考示例"Example-MPC5775K-PIT-ISR-v1_0-GHS614" ,使用 S32DS Power2.1、我遇到了这些错误的编译结果(图 1)。这些错误(图 2 和图 3)来自文件"Vector_SW_VLE - Z4.s" 。文件没有被编辑过,但为什么会出现这些错误?如何解决这些问题? 谢谢,并致以问候。 Re: Errors met when compiling external interrupt for MPC5775K 非常感谢。您的建议非常有帮助! 谢谢& 。 Re: Errors met when compiling external interrupt for MPC5775K 你好@yongzhiliu "Example-MPC5775K-PIT-ISR-v1_0-GHS614" 如后缀所示,这是一个用于 GreenHills MULTI IDE 而非 S32 Design Studio 的项目。语法不同。 有必要在 S32DS 中创建新项目,并使用 S32DS 项目中的启动文件和中断/异常相关文件。 您可以查看以下项目,了解如何在 S32DS 中处理中断: https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5775K-DSPI-with-interrupts-S32DS-1-0/ta-p/1119830 其他例子可在此处找到: https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5-software-example-list/ta-p/1102445 最重要的是,MPC5775K 并不面向大众市场,无法订购。因此,我们不为该设备提供支持。请访问这样或更新的替换网站: https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32r-radar-processing/radar-microcontroller:S32R294 问候, Lukas
View full article
LPCScrypt not running on Windows 11 25H2 [LPCScrypt version 2.1.3_83] For booting and flashing an old LPC1857 we use LPCScrypt for updating device firmware. Since Windows 11 25H2 LPCScrypt is broken: calling it on the command line (ie PowerShell) leads to "Error: Error from CreateProcess: The system cannot find the file specified" Sysinternal's Process Monitor leads to the assumption that LPCScrypt is performing a wmi query by using "wmic path Win32_PnPEntity where (service like '%usbser%' and name like '%lpc%') get.exe". But wmic is declared deprecated since 2016 and had been removed from Windows 11 since 25H2 (see Windows Management Instrumentation Command-line (WMIC) removal from Windows - Microsoft Support) Request to NXP dev team: Is this issue known yet? How to get it to work in the future? Re: LPCScrypt not running on Windows 11 25H2 Hi ErichStyger, you are right. By upgrading from Windows 10 wmic is kept in Windows 11. But I had to setup a fresh Windows 11 system and came accross that issue. Re: LPCScrypt not running on Windows 11 25H2 Thank you for the information. My workaround was to add wmic support to Windows 11 as follows open system settings as an administrator, go to optional features (...further features...) and add wmic  or by using "DISM /Online /Add-Capability /CapabilityName:WMIC" [see Install WMIC to a Windows 11 computer - Microsoft Q&A] Regards, Mathias Re: LPCScrypt not running on Windows 11 25H2 Probably because I have upgraded from Win10 to Win11, I still have WMIC on my machine: Re: LPCScrypt not running on Windows 11 25H2 I recently upgraded from Win10 to Win11 25H2. But so far, I have not seen an issue with LPCScrypt (yet). Using the one packaged with LinkServer v25.9.134 (see below) Updating my LPC-Link2 with LPCScrypt worked fine. Not an expert on WMIC, but according to the information it is gone in 25H2, chatGTP suggested to copy wmic.exe and wmic.exe.mui from an older Windows version to 25H2. NXP is aware of the issue, and there might be an updated LPCScrypt in a next LinkServer release. Re: LPCScrypt not running on Windows 11 25H2 Hello @mathiasmonse  Thanks for your question. If WMIC support is removed, yes, you can try to install it. Or  use an earlier Windows version or to run LPCScrypt on Linux or macOS. BR Alice
View full article
S32K3 HSE: Export EDDSA Public Key I am able to generate an ED25519 key pair with the Key Generation Service, and I would like to be able to export the public key later with the Key Export Service. However, the HSE returns a HSE_SRV_RSP_NOT_ALLOWED when I attempt to export the public key. When I generate the key I use the following parameters: Service ID: HSE_SRV_ID_KEY_GENERATE targetKeyHandle = key_handle; keyInfo: keyFlags = HSE_KF_USAGE_SIGN | HSE_KF_USAGE_VERIFY | HSE_KF_ACCESS_EXPORTABLE keyBitLen = HSE_KEY256_BITS keyCounter = 0 smrFlags = 0 keyType = HSE_KEY_TYPE_ECC_PAIR specific.eccCurveId = HSE_EC_25519_ED25519 keyGenScheme = HSE_KEY_GEN_ECC_KEY_PAIR sch.eccKey.pPubKey = (HOST_ADDR)pub_key_output_ptr; And when I export the key: Service ID: HSE_SRV_ID_EXPORT_KEY targetKeyHandle = key_handle; // Same Key Handle keyInfo: keyFlags = HSE_KF_USAGE_VERIFY | HSE_KF_ACCESS_EXPORTABLE keyBitLen = HSE_KEY256_BITS keyCounter = 0 smrFlags = 0 keyType = HSE_KEY_TYPE_ECC_PAIR specific.eccCurveId = HSE_EC_25519_ED25519 pKey[0] = (HOST_ADDR)pub_key_output_ptr; pKeyLen[0] = (HOST_ADDR)&g_identity_key_len;   Are there any parameter's that are missing or configured incorrectly? Re: S32K3 HSE: Export EDDSA Public Key Thank you Lukas, I was missing setting the HSE_INVALID_KEY_HANDLE's. I see now in the header files: Must be set to #HSE_INVALID_KEY_HANDLE if not used. Re: S32K3 HSE: Export EDDSA Public Key Hi @MHan  I can see nothing wrong in those parameters. Because the public ECC key is exported in plain and not authenticated, did you configured cipherKeyHandle and authKeyHandle as HSE_INVALID_KEY_HANDLE (0xFFFFFFFF)? Setting of HSE_INVALID_KEY_HANDLE to these key handles ensures that authentication and encryption parameters are ignored. Also try to disable data cache to confirm it is not cache issue. Regards, Lukas
View full article
s32k1:同じFTMチャネルでPWM周波数とデューティサイクルを測定する方法 こんにちは、 S32K1xxとFTM 入力キャプチャを使用して PWM 信号を測定しています。 現在、1 つのチャネル (例: FTM0_CH1) を使用して周波数を取得できます。 同じチャネルを使用して周波数とデューティ サイクルの両方を測定するにはどうすればよいでしょうか? SDK またはプロセッサ Expert 構成を使用して、同じ FTM チャネル内でエッジ (立ち上がり/立ち下がり) を切り替えることは可能ですか? 例や推奨方法があれば教えていただけると幸いです。 よろしくお願いします! Re: s32k1:How to measure PWM frequency and duty cycle on the same FTM channel こんにちは、レオさん。返信ありがとうございます。 現在のプロジェクトでは、 S32 Design Studio for Arm v2.2 そして S32SDK_S32K1xx_RTM_3.0.0なので、最新の IDEs または SDKs バージョンにアップグレードするのは便利ではありません。 ご提供いただいたサンプルをダウンロードし、それをどのように設定すれば良いか理解しました。 デューティサイクル そして 周期測定。しかし、私の主な疑問は、どのように使用するかということです 単一チャネル 両方を測定する PWMデューティサイクルと周期 同時に、つまり、両方の例を 1 つに結合する方法です。 デューティ サイクルと周期測定の両方の例を一緒に実装する方法が見つからなかったSO、コード内のキャプチャ エッジ (立ち上がり/立ち下がり) を切り替えて測定を実行してみました。 このアプローチが許容可能または推奨されるかどうかを確認してください。 static uint32_t read_ts32_ch2(void) { uint32_t ovf_before = g_ftm_ovf; (void)FTM0->CONTROLS[2].CnSC; // Clear CHF step 1 uint32_t cap32 = FTM0->CONTROLS[2].CnV; // Clear CHF step 2 & get timestamp uint16_t cap16 = (uint16_t)(cap32 & 0xFFFFu); // Only the lower 16 bits are valid uint32_t ovf_after = g_ftm_ovf; // If overflow occurred after capture and cap16 is small, // assume the capture happened before the overflow and apply compensation if ((ovf_after != ovf_before) && (cap16 < 0x8000u)) { ovf_before++; } return (ovf_before << 16) | cap16; } #if 1 // Function works but sometimes has errors due to edge-switching jitter void FTM0_CH2_Input_Detect(void) { uint32_t cap_ts = read_ts32_ch2(); // Captured channel counter value //bool PwmIOStatus = FTM_DRV_GetChnEventStatus(FTM0,2); // ---------- Rising edge ---------- //if (PwmIOStatus & (1u << 2)) //{ if(!waiting_fall) { /* ---------- Rising edge ---------- */ rise_prev = rise_curr; rise_curr = cap_ts; /* Arm the next edge: falling edge */ waiting_fall = 1; FTM0->CONTROLS[2].CnSC = (FTM0->CONTROLS[2].CnSC & ~(FTM_CnSC_ELSA_MASK | FTM_CnSC_ELSB_MASK)) | (FTM_CnSC_ELSB_MASK); if (got_first_rise) { period_cnt = (uint32_t)(rise_curr - rise_prev); if (period_cnt == 0u) { got_first_rise = 0; } /* Protection */ else { pwm_freq_hz = frequency / period_cnt; } } else { got_first_rise = 1; } } else { /* ---------- Falling edge ---------- */ fall_curr = cap_ts; /* Switch back to rising edge */ waiting_fall = 0; FTM0->CONTROLS[2].CnSC = (FTM0->CONTROLS[2].CnSC & ~(FTM_CnSC_ELSA_MASK | FTM_CnSC_ELSB_MASK)) | (FTM_CnSC_ELSA_MASK); if (got_first_rise && (fall_curr >= rise_curr)) { high_cnt = (uint32_t)(fall_curr - rise_curr); if ((period_cnt != 0) && (pwm_freq_hz != 0)) { // duty_pct = ((float)high_cnt * 100.0f) / (float)period_cnt; new_sample = 1; } } } /* Redundant flag clear */ // FTM0->STATUS = (1u << 2); //} } 回复: s32k1:How to measure PWM frequency and duty cycle on the same FTM channel こんにちは、レオさん。返信ありがとうございます。 現在のプロジェクトでは、 S32 Design Studio for Arm v2.2とS32SDK_S32K1xx_RTM_3.0.0を使用しているSO、最新の IDEs または SDKs バージョンにアップグレードするのは便利ではありません。 ご提供いただいた例をダウンロードし、デューティ サイクルと周期の測定を取得するように構成する方法を理解しました。しかし、私の主な疑問は、 1 つのチャネルを使用してPWM デューティ サイクルと周期の両方を同時に測定する方法、つまり、両方の例を 1 つに組み合わせる方法です。 デューティ サイクルと周期測定の両方の例を一緒に実装する方法が見つからなかったSO、コード内のキャプチャ エッジ (立ち上がり/立ち下がり) を切り替えて測定を実行してみました。 このアプローチが許容可能または推奨されるかどうかを確認してください。 static uint32_t read_ts32_ch2(void) { uint32_t ovf_before = g_ftm_ovf; (void)FTM0->CONTROLS[2].CnSC; // Clear CHF step 1 uint32_t cap32 = FTM0->CONTROLS[2].CnV; // Clear CHF step 2 & get timestamp uint16_t cap16 = (uint16_t)(cap32 & 0xFFFFu); // Only the lower 16 bits are valid uint32_t ovf_after = g_ftm_ovf; // If overflow occurred after capture and cap16 is small, // assume the capture happened before the overflow and apply compensation if ((ovf_after != ovf_before) && (cap16 < 0x8000u)) { ovf_before++; } return (ovf_before << 16) | cap16; } #if 1 // Function works but sometimes has errors due to edge-switching jitter void FTM0_CH2_Input_Detect(void) { uint32_t cap_ts = read_ts32_ch2(); // Captured channel counter value //bool PwmIOStatus = FTM_DRV_GetChnEventStatus(FTM0,2); // ---------- Rising edge ---------- //if (PwmIOStatus & (1u << 2)) //{ if(!waiting_fall) { /* ---------- Rising edge ---------- */ rise_prev = rise_curr; rise_curr = cap_ts; /* Arm the next edge: falling edge */ waiting_fall = 1; FTM0->CONTROLS[2].CnSC = (FTM0->CONTROLS[2].CnSC & ~(FTM_CnSC_ELSA_MASK | FTM_CnSC_ELSB_MASK)) | (FTM_CnSC_ELSB_MASK); if (got_first_rise) { period_cnt = (uint32_t)(rise_curr - rise_prev); if (period_cnt == 0u) { got_first_rise = 0; } /* Protection */ else { pwm_freq_hz = frequency / period_cnt; } } else { got_first_rise = 1; } } else { /* ---------- Falling edge ---------- */ fall_curr = cap_ts; /* Switch back to rising edge */ waiting_fall = 0; FTM0->CONTROLS[2].CnSC = (FTM0->CONTROLS[2].CnSC & ~(FTM_CnSC_ELSA_MASK | FTM_CnSC_ELSB_MASK)) | (FTM_CnSC_ELSA_MASK); if (got_first_rise && (fall_curr >= rise_curr)) { high_cnt = (uint32_t)(fall_curr - rise_curr); if ((period_cnt != 0) && (pwm_freq_hz != 0)) { // duty_pct = ((float)high_cnt * 100.0f) / (float)period_cnt; new_sample = 1; } } } /* Redundant flag clear */ // FTM0->STATUS = (1u << 2); //} } Re: s32k1:How to measure PWM frequency and duty cycle on the same FTM channel 当社製品にご興味をお持ちいただき、また当社コミュニティに貢献していただき、ありがとうございます。 RTD の最新バージョンに更新すると、最近のバグ修正とパフォーマンスの向上のメリットが得られます。現在使用しているバージョンは数リリース前のものなので、安定性と互換性に影響する可能性があります。RTD を最新の状態に保つことで、最新の機能や拡張機能にアクセスできるようになります。 S32K1xx シリーズを使用した開発では、最新の S32DS および RTD バージョンを使用することをお勧めします。 • S32 Design Studio 3.6.4 – Windows/Linux • S32K1_S32M24X リアルタイム・ドライバ AUTOSAR R21-11 バージョン 3.0.0 IDEをダウンロードするには、 S32プラットフォーム用のS32 Design Studioページにアクセスしてください-> ダウンロード -> S32 Design Studio 3.6.4 – Windows/Linux RTD をダウンロードするには、 S32K1ページ-> デザイン リソース -> ソフトウェア -> S32K1 用リアルタイム・ドライバ -> オートモーティブ SW - S32K1_S32M24x - Cortex-M 用リアルタイム・ドライバにアクセスしてください。 各SWへのインストールフロー/詳細についてはリリースノートをご確認ください。 … SW をインストールしたら、デューティ サイクルと周期の測定については添付の例を参照できます。 ftm0_ch0 (PTD15) を PWM として、ftm1_ch2 (PTC14) を ICU として設定します。SO、テストのために接続してください。さらに、PTD16 はデバッグ目的のためだけに、測定開始前と測定停止後に切り替わります。 式タブで結果を確認します: デューティサイクルの例 期間の例 次の RTD を使用して例が構築およびテストされました。 - S32K1_S32M24X リアルタイム・ドライバ AUTOSAR R21-11 バージョン 3.0.0 この情報が役に立つことを願います。リアルタイム・ドライバ (RTD) の使用に関してさらに質問がある場合は、お気軽にお問い合わせください。
View full article
I.MX 93 FRDMがhello_worldでクラッシュする こんにちは、 ダウンロードしたバージョン: https://github.com/nxp-real-time-edge-sw/heterogeneous-multicore/tree/main(v2.9-202407) 起動すると、数秒間動作しますが、その後常に同じ場所でクラッシュします (これにより、u-boot がリセットされます)。スクリーンショットを参照してください。いつも同じ場所でクラッシュするのは普通ですか? よろしくお願いします、 Re: I.MX 93 FRDM crashes on hello_world 再、 プレビルドはこちら: (Linux 6.12.34_2.1.0): https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX FRDM-IMX93 をフラッシュするには UUU を使用します。 Linux の起動を停止して u-boot に入り、次のコマンドを入力します。 ファットロード mmc 1:0 0xD0000000 hello_world_ca55_RTOS0_UART2.bin dcache フラッシュ; icache フラッシュ; CPU リリース 1 0xD0000000 ファットロード mmc 1:0 0xD1000000 hello_world_ca55_RTOS1_UART1.bin dcache フラッシュ; icache フラッシュ; 0xD1000000 に移動 それでは正常に動作しています!!! そこで、FRDM-IMX93 用の私のツールチェーンを使用して u-boot をビルドする方法と、それを UUU でフラッシュするスクリプトを調べてもらえますか? よろしくお願いいたします。 Re: I.MX 93 FRDM crashes on hello_world こんにちは、 まず、今日は 異種マルチコア v3.2-202507 すると結果は同じになります。 hello_world の例のビルドを作成する手順は次のとおりです。 ./CMSIS_5-Real-Time-Edge-v3.2-202507.zip を解凍します。 ./FreeRTOS-Kernel-Real-Time-Edge-v3.2-202507.zip を解凍します。 ./heterogeneous-multicore-Real-Time-Edge-v3.2-202507.zip を解凍します。 ./lwip-Real-Time-Edge-v3.2-202507.zip を解凍します。 ./mcuxsdk-middleware-multicore-Real-Time-Edge-v3.2-202507.zip を解凍します。 ./mcux-sdk-Real-Time-Edge-v3.2-202507.zip を解凍します。 ./rpmsg-lite-Real-Time-Edge-v3.2-202507.zip を解凍します。 ./soem-Real-Time-Edge-v3.2-202507.zip を解凍します。 mv ./FreeRTOS-Kernel-Real-Time-Edge-v3.2-202507 ./FreeRTOS-Kernel mv ./heterogeneous-multicore-Real-Time-Edge-v3.2-202507 ./heterogeneous-multicore mv ./mcux-sdk-リアルタイムエッジ-v3.2-202507 ./mcux-sdk mv ./CMSIS_5-リアルタイムエッジ-v3.2-202507 ./mcux-sdk/CMSIS mkdir ミドルウェア mv ./mcuxsdk-middleware-multicore-リアルタイムエッジ-v3.2-202507 ./middleware/multicore mv ./lwip-リアルタイムエッジ-v3.2-202507 ./middleware/lwip mv ./rpmsg-lite-リアルタイムエッジ-v3.2-202507 ./middleware/multicore/rpmsg_lite mv ./soem-Real-Time-Edge-v3.2-202507 ./middleware/soem エラーがない場合は echo でインストールが成功しました。SO、インストールを試みます… コアのエコー: cd ./異種マルチコア ARMGCC_DIR=~/toolchains/arm-gnu-toolchain-12.2.rel1-x86_64-aarch64-none-elf/ をエクスポートします。 ./build_apps.sh a-core mcimx93evk_ca55 フリートス m コアのエコー: ARMGCC_DIR=~/toolchains/arm-gnu-toolchain-12.2.rel1-x86_64-arm-none-eabi/ をエクスポートします。 ./build_apps.sh m-core mcimx93evk_cm33 フリートス エコー、掃除しましょう…: ./build_apps.sh クリーン エコー終了 SO、よろしければリンクをご覧ください: https://github.com/nxp-real-time-edge-sw/heterogeneous-multicore/releases/tag/Real-Time-Edge-v3.2-202507 https://github.com/nxp-mcuxpresso/mcux-sdk/releases/tag/Real-Time-Edge-v3.2-202507 https://github.com/nxp-mcuxpresso/FreeRTOS-Kernel/releases/tag/Real-Time-Edge-v3.2-202507 https://github.com/nxp-mcuxpresso/lwip/releases/tag/Real-Time-Edge-v3.2-202507 https://github.com/nxp-mcuxpresso/mcuxsdk-middleware-multicore/releases/tag/Real-Time-Edge-v3.2-202507 https://github.com/nxp-mcuxpresso/rpmsg-lite/releases/tag/Real-Time-Edge-v3.2-202507 https://github.com/nxp-real-time-edge-sw/soem/releases/tag/Real-Time-Edge-v3.2-202507 https://github.com/nxp-mcuxpresso/CMSIS_5/releases/tag/Real-Time-Edge-v3.2-202507 この場合のビルドは問題ありません: .binをアップロードするにはimx93 では SD カードを使用し、コンピューターから直接イメージを書き込み、SD を評価ボードに接続します。 SO、ここで私の画像を見ることができます: 次に、表示されている U-Boot について説明します。 リポジトリはこちらです: https://github.com/u-boot/u-boot/releases/tag/v2025.10 次にこれもダウンロードします: https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.21.bin https://github.com/nxp-imx/imx-atf/tree/lf_v2.8 https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-sentinel-0.11.bin このドキュメントを使用して続行します: https://docs.u-boot.org/en/latest/board/nxp/imx93_frdm.html しかし、ここでは、次の 2 つのコマンドにツールチェーンを使用します。 PLAT=imx93 CROSS_COMPILE=/ホーム/tcouille/toolchains/Arm-gnu-toolchain-12.2.rel1-x86_64-aarch64-none-elf/bin/aarch64-none-elf- bl31 を作成します。 そして : $ export CROSS_COMPILE=/home/tcouille/toolchains/arm-gnu-toolchain-12.2.rel1-x86_64-aarch64-none-elf/bin/aarch64-none-elf- $ make imx93_frdm_defconfig $ make 次に、UUU を使用します: : https://github.com/nxp-imx/mfgtools/releases/tag/uuu_1.5.201 次のように入力します: ./uuu -v -b emmc_all .\flash.bin このコマンドを入力して、2 つの cortex-A で 2 つの hello_world サンプルを起動します。 ファットロード mmc 1:0 0xD0000000 hello_world_ca55_RTOS0_UART2.bin dcache フラッシュ; icache フラッシュ; CPU リリース 1 0xD0000000 ファットロード mmc 1:0 0xD1000000 hello_world_ca55_RTOS1_UART1.bin dcache フラッシュ; icache フラッシュ; 0xD1000000 に移動 そして数秒後、u-boot がリセットされます... よろしくお願いいたします。 Re: I.MX 93 FRDM crashes on hello_world こんにちは、 このボードのスクリプトをCANますか: mcimx93evk_ca55 ここで再現を試みるテスト対象の uboot のバージョン。 敬具
View full article
S32DS 3.6.4 can't found RTD Hello! Recently, I installed S32DS 3.6.4 & RTD 6.0.0. However, when I attempt to create a new app project, I am unable to select RTD. How can I fix it? Re: S32DS 3.6.4 can't found RTD Thank you for your interest in our products and for contributing to our community. According to RTD 6.0.0 Release Notes: So when you create a new project, please make sure you select NXP GCC 10.2.0 in the following step: I hope this information is helpful.
View full article
OPWMCB Mode in eMIOS – Lead vs. Trail Edge Hi I’ve been working with eMIOS PWM IP in OPWMCB mode and wanted to understand the practical difference between these two configurations: EMIOS_PWM_IP_MODE_OPWMCB_TRAIL_EDGE EMIOS_PWM_IP_MODE_OPWMCB_LEAD_EDGE To investigate, I created a simple test project and observed the output signals. Surprisingly, I couldn’t see any noticeable difference between the two modes on the waveform. Here’s my setup: Time base: Channel 23 Channels: CH1 and CH2 generating center-aligned PWM The same time base also triggers the ADC at the middle of the period for current sampling. My questions: What is the actual difference between these two OPWMCB modes? Under what conditions does this difference become visible? For my design (center-aligned PWM with ADC sampling at mid-period), which mode is best and why? Looking forward to your insights and explanations! Re: OPWMCB Mode in eMIOS – Lead vs. Trail Edge Thank you for your interest in our products and for contributing to our community. Regarding your questions: 1&2 .- The main difference is noted with deadtime insertion. The trail edge mode increasing high time. Alternatively, by selecting the lead edge mode, deadtime insertion decrease high time. For more details, please refer to 6.4. OPWMCB example project section of S32M27x/S32K3 – eMIOS Usage. On the other hand, it could also affect the flag event (I don't remember having tried it.), and therefore the interrupt and triggering support. For reference consult 6.6. PWM design considerations section. And please test it on your own taking as reference the 6.1 OPWMB example project. 3.- Such topic is addressed in https://community.nxp.com/t5/S32K/Design-Strategy-for-Complementary-PWM-Generation-for-motor/td-p/2170567 I hope this information is helpful.
View full article
项目无法作为 IAR EW 导出 我按照"HOWTO: Export S32DS Project to IAR EW (S32K14x/S32K11x)" 中的说明操作,但在"Export" 中找不到"Project Info Export Wizard" 选项。 Re: The project cannot be exported as IAR EW 你好、 这一功能在配备处理器专家的旧版 S32DS 中也有。我对 IAR Workbench 不熟悉,但我想您可以将项目作为 ProjectInfo.xml 导入 WB IDE。
View full article
How Do You Ensure Reliability and Redundancy in Large Enterprise Storage Environments? Hello everyone, As our enterprise storage needs grow, maintaining high reliability, redundancy, and performance is more important than ever. We’re actively exploring best practices to ensure our enterprise storage infrastructure remains both resilient and efficient, with minimal risk of data loss or downtime. I’d love to hear from others managing large-scale storage environments. What strategies and technologies have you found to be the most effective in ensuring reliability and redundancy? Here are a few specific areas I’m interested in: RAID configurations: Which RAID level works best for large environments and why? Data replication: How do you ensure fast and reliable replication? Backup strategies: How often do you back up critical data, and do you leverage cloud or offsite solutions? Disaster recovery: Tips for designing a robust disaster recovery plan? Fault tolerance: How do you effectively manage hardware failure or network issues? Automation: How does automation play a role in improving reliability? Looking forward to hearing your thoughts and experiences!
View full article
RT1176 custom board no access to LPUART1 or JTAG/SWD ... I have a custom board, that is very close to the EVKB board, except no USB or MIPI. I cannot seem to access serial downloader mode to use the Secure Provisioning Tool via UART, nor obtain any access via JTAG/SWD for programming. The chip seems to be working, on that there is an ON/OFF button that when held for 5 seconds, or whatever the length is, powers the chip off, and then pressing the button again powers it on. I've double-triple checked everything, and it nearly matches the EVKB board, however one things I noticed that was not done was to connect VDD_MIPI_* or VDD_USB_* to anything, again, as the board doesn't use MIPI or USB. Could not connecting those power pins be causing the problems I'm having with accessing UART or JTAG/SWD? Re: RT1176 custom board no access to LPUART1 or JTAG/SWD ... The image I posted is from that red circled area, and I am using the exact components, values as detailed in the EVKB there. Re: RT1176 custom board no access to LPUART1 or JTAG/SWD ... Hi @application_ninja , In MIMXRT1170-EVKB board  , RC delay time is 30000*0.00000022=0.0066s  =6.6ms. Please check your board, if your board use the same RC delay circuit, Please use an oscilloscope to measure the signal circled in red in the image. Best Regards Re: RT1176 custom board no access to LPUART1 or JTAG/SWD ... As an FYI, this is what my delay circuit looks like...  Blue being DCDC_IN and yellow being DCDC_PSWITCH. Re: RT1176 custom board no access to LPUART1 or JTAG/SWD ... Not sure what you mean by: "VDD_SNVS_DIG is internal LDO output.", so is 0v output correct for this, or not? My custom board is nearly identical to the EVKB except for not using MIPI/USB/AUDIO. I've gone over things many times, just cannot figure out why I cannot get it into serial downloader mode nor use JTAG/SWD to program it. Re: RT1176 custom board no access to LPUART1 or JTAG/SWD ... Hi @application_ninja , VDD_SNVS_DIG is  internal LDO output. 1: I suggest you can compare your customed board with MIMXRT1170-EVKB board, check the difference. 2: If you have MIMXRT1170-EVKB board, did you try modify the MIMXRT1170-EVKB board same as your customed board? Best Regards Re: RT1176 custom board no access to LPUART1 or JTAG/SWD ... Apparently VDD_SNVS_DIG is low, and controlled by software, so my design is correct? https://www.nxp.com/docs/en/data-sheet/IMXRT1170BCEC.pdf "The power rail VDD_SNVS_DIG is controlled by software." Re: RT1176 custom board no access to LPUART1 or JTAG/SWD ... OK, so it's looking like I'm not getting anything on VDD_SNVS_DIG, not sure why, but any thoughts as to what could cause this off hand? Re: RT1176 custom board no access to LPUART1 or JTAG/SWD ... That was going to be my next steps, however quite difficult to test / probe, thus my first questions to see if not connecting those VDD_MIPI_* and VDD_USB_* could be the cause, since everything else seems to power up correctly and I get correct voltages everywhere. Thank you. Re: RT1176 custom board no access to LPUART1 or JTAG/SWD ... Hi @application_ninja , Could you use an oscilloscope to check if the power-up sequence is normal, especially the RC delay circuit?  Best Regards MayLiu Re: RT1176 custom board no access to LPUART1 or JTAG/SWD ... Yes, thank you, I have verified all that, I have a positive voltage on BOOT_CFG_0, and have positive voltage on the RXD LPUART1 pin coming from the chip, so everything appears as though it should be working, but I get nothing from the secure provisioning tool, nor from the sdphost tool. All my power rails look good, proper voltages, my ONOFF button works, reset button, just really stumped as to why I cannot program / read the chip. Re: RT1176 custom board no access to LPUART1 or JTAG/SWD ... Hi @application_ninja , Thanks for your updated information. First, I suggest you follow the HDUG recommended design for your customed hardware development board. Second, please check the Boot Mode pins settings of your custom development board. If you want use the Secure Provisioning Tool via UART, you need set as serial downloader mode. Third,  Only LPUART1 support serial downloader mode. Wish it helps you. Best Regards MayLiu Re: RT1176 custom board no access to LPUART1 or JTAG/SWD ... Yes, I am aware of that document, but that does not answer my question, and as you have confirmed what the document states, those are "recommendations", they are not listed as "requirements" for proper board operation. So going by the way you have stated and the documentation reads, as "recommended" they do not have to be performed for proper board  / chip operation. Which leads back to my question, could not doing these "recommendations" cause the problems I am seeing? Re: RT1176 custom board no access to LPUART1 or JTAG/SWD ... Hi @application_ninja , Thank you so much for your interest in our products and for using our community. In MIMXRT1170HDUG, it describe that Unused pins recommendation  https://www.nxp.com/webapp/Download?colCode=MIMXRT1170HDUG Please follow the  Recommended connections for unused analog interfaces. Wish it helps you. If you still have question about it, please kindly let me know.  Best Regards MayLiu
View full article
Inference Degradation on i.MX95 Neutron NPU Dear NXP Technical Support Team, We are currently developing a pose estimation model using ResNet as the backbone, and are considering deploying it on a product based on the i.MX95 platfo However, we are encountering significant degradation in inference accuracy when running quantized models on the Neutron NPU. Our investigation revealed that even with standard classification models, quantized models that perform correctly on the CPU show degraded results after conversion for NPU execution. This issue also affects ResNet, which we use as our backbone. Through partial NPU assignment testing using neutron-converter, we confirmed that the degradation occurs when layers other than specific Conv2D layers are assigned to the NPU. We would appreciate your insights regarding the following: What could be the cause of the inference degradation? For example, quantization or conversion parameter issues, hardware limitations of the NPU, or bugs in the neutron-converter. Are there any known issues related to this problem? For example, bugs in BSP 6.12.20 or eIQ Toolkit 1.16.0, known limitations when running ResNet models on the NPU, or any other documented issues with the i.MX95 NPU. What countermeasures can we take to mitigate this issue? Development Environment Hardware: i.MX95 EVK BSP Version: 6.12.20_2.0.0(NXP) eIQ Toolkit: 1.16.0 (Windows) Model Conversion Pipeline PyTorch → ONNX: torch.onnx (opset version 15) ONNX → TensorFlow (.pb): PINTO0309/onnx2tf INT8 Quantization: tensorflow.lite.TFLiteConverter (version 2.12.0) NPU Conversion: neutron-converter (version 2.0.2+0X0cebb80a) Inference Results When executing on the NPU, the inference accuracy drops drastically. We tested with quantized models of MobileNetV2 and ResNet18 (from torchvision) using ImageNetV2 (500 samples): model float32 CPU Accuracy (Top1 / Top5) int8 CPU Accuracy (Top1 / Top5) int8 NPU Accuracy (Top1 / Top5) MobileNetV2 70.2% / 89.4% 68.4% / 88.6% 0.2% / 0.8% ResNet18 64.0% / 86.6% 63.6% / 87.4% 0.0% / 0.6% Additional Test We performed partial NPU assignment tests using the --include-operators option in neutron-converter on the quantized ResNet18 model. We observed that assigning layers other than specific Conv2D layers to the NPU leads to inference degradation. case NPU assignment result Accuracy Top1 / Top5 Baseline none (all CPU) ー(baseline) 63.6 / 87.4 % Case 1 all bad 0.0 / 0.6 % Case 2 Conv2D layers which in/out shape is [1×56×56×64] good 64.0 / 87.4 % Case 3 Case 2 + Add layers bad 0.0 / 0.6 % Case 4 Case 2 + other Conv2D layers bad 0.0 / 0.8 % Thank you so much for your support. Best regards, Ryosuke Re: Inference Degradation on i.MX95 Neutron NPU Hello, Please note that the i.MX95 is still in pre-production stage so we cannot offer support to it, please contact your local NXP Sales/NXP FAE for further assistance. Best regards/Saludos, Aldo.
View full article
SJA1110 による IGMP スヌーピング こんにちは、 私は S32G と SJA1110 で bsp43 を実行しており、IGMP スヌーピングを有効にしてマルチキャスト ストリームを動的にルーティングしようとしています。IGMP に関連するいくつかの固有の問題を特定しましたが、解決方法がわかりません。IGMP スヌーピングを無効にすると、マルチキャスト パケットがスイッチに溢れるようになることを確認しました。SO、IGMP スヌーピング オプションが何かを実行しているということです... ただし、これは予期された動作ではありません。 マルチキャストトラフィックは常に、列挙された最も低いアクティブポートに転送されます。 ポート 3 のノードが IGMP 経由のトラフィックを要求し、ポート 4 から出力されるストリームは、ポート 1 がトラフィックを要求したかのように、ポート 1 から出力されます (そのリンクがアクティブな場合)。ポート 1 のリンクがアクティブでない場合、そのリンクがアクティブであればトラフィックはポート 2 に転送されます。 mdbを使用してトラフィックを手動でルーティングすることはできますが、IGMPスヌーピングがこれを自動的に管理することを期待しています。 マルチキャストクエリーを有効にしても、スイッチポートからメンバーシップクエリーが出力されない DSAブリッジインターフェースにはIGMPクエリがありますが、スイッチにコネクテッドされた他のリンクにはIGMPクエリが表示されません。 ブリッジ ポートからの IGMP クエリをトラップし、スイッチ ポートにリダイレクトするための tc ルールを設定する必要があるのではないかと思います。 これが Linux 構成の問題なのか、スイッチ ハードウェアの制限なのかはわかりません。 ご提案があればよろしくお願いします。
View full article
S32 Design Studio v3.6.x および LQFP パッケージ用の S32K39x ピンツール こんにちは、 既存の例をインポートすることと、S32K396 用の RTD 6 QLP01 を使用して新しいアプリケーション プロジェクトを生成することの両方を試しました。 ピン ツールのグラフィック表示は BGA パッケージでは見栄えが良いのですが、パッケージを 176LQFP に変更すると、LQFP パッケージの上部にピンがなくなります (すべて左、右、下部にあります)。 これは対処が予定されている問題ですか、それとも私のインストールの問題ですか? ありがとうございます! Re: S32 Design Studio v3.6.x and S32K39x Pins tool for LQFP package バグレポートが S32 Design Studio チームに送信されました。彼らはこのバグを確認し、FUTUREリリースで修正する予定です。 Re: S32 Design Studio v3.6.x and S32K39x Pins tool for LQFP package ハイ この問題を報告していただきありがとうございます。この問題は S32DS チームに報告済みです。返答が届き次第お知らせします。 現在、ピンのポジショニングが正しく表示されていません。S32K396RM (Rev. 4 11 2024).pdf のS32K36_IOMUX.xlsxファイルのS32K396_176lqfp_EPを参照してください。正しいピンのポジショニング。 よろしくお願いします、 ロビン --------------------------------------------------------------------------------- 注記: - この投稿があなたの質問への回答である場合は、「解決策として承認」ボタンをクリックしてください。ありがとう! - Threadは最後の投稿から7週間フォローされます。それ以降の返信は無視されます。 後ほど関連する質問がある場合は、新しいThreadを開いて、閉じたThreadを参照してください。 ---------------------------------------------------------------------------------
View full article
门禁卡 晚上好。我购买了 Mifare Plus X(2K/4K)卡。当我尝试将它们升级到网络安全级别 SL3 时,我收到一条错误消息,提示该卡的网络安全级别为 SL1。要升级到 SL3,我需要在 SL1 卡初始化时设置的 AES 密钥。有可能获得它们吗? Re: Access cards 您好, MIFARE Plus S 状态设置为不再生产。MIFARE Plus产品组合的重点产品是MIFARE Plus EV2。 要获得有关MIFARE Plus S和X的更多支持,请通过代理商网络联系您的当地代理商|恩智浦半导体。 不便之处,敬请原谅。 Eduardo。 Re: Access cards 下午好。保护卡片免受黑客攻击和伪造。它们将用于人员出入控制系统。 我尝试使用 MIFARE Plus S та MIFARE Plus X。 我无法将它们提高到 SL3 网络安全级别。 Re: Access cards 您好, 能否请您说明在项目中使用 MIFARE Plus X 的原因?您申请的目的是什么? 支持 MIFARE Plus X 的资源受到限制,并根据 NDA(保密协议)进行保密。有关此部分的更多信息,请通过代理商网络联系您的本地代理商|恩智浦半导体。 Eduardo。 Re: Access cards 下午好,是的,卡片是个性化的。该制造商只生产使用恩智浦芯片的卡。 制造商没有关于卡片个性化代码的信息。 Re: Access cards 下午好,是的,卡片是个性化的。该制造商只生产使用恩智浦芯片的卡。 制造商没有关于卡片个性化代码的信息。 Re: Access cards 你好@Serhii91 希望你一切顺利。 请确认您使用的是否是已个性化的卡片?如果是这样,请联系卡片制造商/发行商,尝试获得更多有关个人化过程中使用的密钥的信息。 Eduardo。
View full article
S32K35X8EVBとADTJA1101 これらのボードを Sabre コネクタと一緒に起動するのに苦労しています。言い換えが含まれていると思われるこの投稿を見つけました。何をする必要があるのか分かりません。データシートと比較すると、その投稿では選択と混合が行われているようです。 現在、RMII とリセット ピンについて言及しているすべてのピンが Config ツールからマップされています。SMI と通信でき、ID レジスタを確認できました。RMII を使用するために次に何が必要なのかわかりません。また、ツール内でのリファレンス クロックの設定内容や、変更する抵抗リンクについても不明です。何かアドバイスをCANますか? https://community.nxp.com/t5/S32K/S32K3X8EVB-Q289-rework-for-RMII/mp/2023038#M44835
View full article
S32 Design Studio for S32 Platform v.3.5 Activation Code I want to install S32DS version 3.5, but I can't find the activation code, and it says I don't need the activation code to activate it.
View full article
S32 Design Studio for S32 Platform v.3.5 激活码 想安装S32DS3.5版本,找不到激活码,提示不需要激活码激活
View full article
S32Z2 Python script error issue Dear;        The customer uses NXP S32Z2 to design a real-time computing board, and the IDE uses NXP S32DS. 3.6.3. Currently, during debugging, occasional S32Z2 Python script error issues occur, with the specific phenomenon being "failure during execution of Python script", as shown in Figure 1. The relevant error log information is as follows:         540,987 1-list-features 541,001 1^done,features=["frozen-varobjs","pending-breakpoints","thread-info","data-read-memory-byte\ s","breakpoint-notifications","ada-task-info","language-option","info-gdb-mi-command","undefined-com\ mand-error-code","exec-run-start-option","data-disassemble-a-option","simple-values-ref-types","pyth\ on"] 541,002 (gdb) 541,142 2-list-thread-groups 541,142 3-gdb-version 541,150 2^done,groups=[{id="i1",type="process"}] 541,150 (gdb) 541,151 ~"GNU gdb (GDB src=ga98a3c7ad40 bld=ga98a3c7ad40 ) 15.1\n" 541,151 ~"Copyright (C) 2024 Free Software Foundation, Inc.\n" 541,151 ~"License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>\nThis is fre\ e software: you are free to change and redistribute it.\nThere is NO WARRANTY, to the extent permitt\ ed by law." 541,151 ~"\nType \"show copying\" and \"show warranty\" for details.\n" 541,151 ~"This GDB was configured as \"--host=x86_64-w64-mingw32 --target=arm-none-eabi\".\n" 541,151 ~"Type \"show configuration\" for configuration details.\n" 541,151 ~"For bug reporting instructions, please see:\n" 541,151 ~"<https://www.gnu.org/software/gdb/bugs/>.\n" 541,151 ~"Find the GDB manual and other documentation resources online at:\n <" 541,151 ~"http://www.gnu.org/software/gdb/documentation/>.\n\n" 541,151 ~"For help, type \"help\".\n" 541,151 ~"Type \"apropos word\" to search for commands related to \"word\".\n" 541,151 3^done 541,151 (gdb) 541,151 4-environment-cd C:/Users/developer/Desktop/MyWorkspace/modifiedPlatform/100713_PLT_COM_S32Z\ 280_R52_Core 541,166 4^done 541,166 (gdb) 541,166 5-gdb-set breakpoint pending on 541,166 5^done 541,167 (gdb) 541,167 6-gdb-set detach-on-fork on 541,167 6^done 541,167 (gdb) 541,167 7-enable-pretty-printing 541,167 7^done 541,167 (gdb) 541,167 8-gdb-set python print-stack none 541,167 8^done 541,167 (gdb) 541,168 9-gdb-set print object on 541,168 9^done 541,168 (gdb) 541,168 10-gdb-set print sevenbit-strings on 541,169 10^done 541,169 (gdb) 541,169 11-gdb-set host-charset UTF-8 541,169 11^done 541,169 (gdb) 541,169 12-gdb-set target-charset GBK 541,170 12^done 541,170 (gdb) 541,170 13-gdb-set target-wide-charset UTF-16 541,170 13^done 541,170 (gdb) 541,170 14-gdb-set dprintf-style call 541,170 14^done 541,170 (gdb) 541,170 15source .gdbinit 541,171 &"source .gdbinit\n" 541,171 &".gdbinit: No such file or directory.\n" 541,171 15^error,msg=".gdbinit: No such file or directory." 541,171 (gdb) 541,171 16-gdb-set mi-async off 541,171 16^done 541,171 (gdb) 541,172 17-gdb-set record full stop-at-limit off 541,173 17^done 541,173 (gdb) 541,173 18-gdb-set auto-solib-add on 541,173 18^done 541,173 (gdb) 541,174 19-gdb-set substitute-path C:\\Users\\tgp\\Documents\\Platform_SW_git\\COM_Lane\\COM_PFCC_S3\ 2Z280_Platform_SW_Core_R52\\Debug_RAM/../Project_Settings/Startup_Code/ C:\\Users\\developer\\Deskto\ p\\MyWorkspace\\modifiedPlatform\\100713_PLT_COM_S32Z280_R52_Core\\Project_Settings\\Startup_Code\\ 541,174 20-gdb-set substitute-path C:\\Users\\tgp\\Documents\\Platform_SW_git\\COM_Lane\\COM_PFCC_S3\ 2Z280_Platform_SW_Core_R52\\Debug_RAM/../include/ C:\\Users\\developer\\Desktop\\MyWorkspace\\modifi\ edPlatform\\100713_PLT_COM_S32Z280_R52_Core\\include\\ 541,204 21-gdb-set substitute-path C:\\Users\\tgp\\Documents\\Platform_SW_git\\COM_Lane\\COM_PFCC_S3\ 541,204 19^done 541,204 (gdb) 2Z280_Platform_SW_Core_R52\\Debug_RAM/../src/ C:\\Users\\developer\\Desktop\\MyWorkspace\\modifiedPl\ atform\\100713_PLT_COM_S32Z280_R52_Core\\src\\ 541,205 20^done 541,205 (gdb) 541,206 21^done 541,206 (gdb) 541,207 22py _IS_LOGGING_ENABLED = True 541,207 23py _REMOTE_TIMEOUT = 30 541,207 24py _CORE_NAME = "S32Z280_R52_0_0" 541,207 25py _SOC_NAME = "S32Z280" 541,207 26py _GDB_SERVER_PORT = 45000 541,207 27py _JTAG_SPEED = 16000 541,207 28py _RESET_DELAY = 0 541,207 29py _PROBE_IP = "s32dbg:usb#00:04:9f:08:bc:b1" 541,207 30py _CCS_IP = "127.0.0.1" 541,207 31py _CCS_PORT = 41475 541,207 32source C:\NXP\S32DS.3.6.3\eclipse\../S32DS/tools/S32Debugger/Debugger/scripts/s32z2e2/s32z\ 2e2_attach.py 541,234 &"py _IS_LOGGING_ENABLED = True\n" 541,234 22^done 541,234 (gdb) 541,235 &"py _REMOTE_TIMEOUT = 30\n" 541,235 23^done 541,235 (gdb) 541,235 &"py _CORE_NAME = \"S32Z280_R52_0_0\"\n" 541,235 24^done 541,235 (gdb) 541,235 &"py _SOC_NAME = \"S32Z280\"\n" 541,235 25^done 541,235 (gdb) 541,236 &"py _GDB_SERVER_PORT = 45000\n" 541,236 26^done 541,236 (gdb) 541,236 &"py _JTAG_SPEED = 16000\n" 541,236 27^done 541,236 (gdb) 541,236 &"py _RESET_DELAY = 0\n" 541,236 28^done 541,236 (gdb) 541,237 &"py _PROBE_IP = \"s32dbg:usb#00:04:9f:08:bc:b1\"\n" 541,237 29^done 541,237 (gdb) 541,237 &"py _CCS_IP = \"127.0.0.1\"\n" 541,238 30^done 541,238 (gdb) 541,238 &"py _CCS_PORT = 41475\n" 541,238 31^done 541,238 (gdb) 541,238 &"source C:\\NXP\\S32DS.3.6.3\\eclipse\\../S32DS/tools/S32Debugger/Debugger/scripts/s32z2e2/\ s32z2e2_attach.py\n" 541,300 =cmd-param-changed,param="pagination",value="off" 541,306 32^done 541,306 (gdb) 541,306 33py board_init() 541,306 &"py board_init()\n" 541,307 ~"... board_init() skipped.\n" 541,307 33^done 541,307 (gdb) 541,307 34py core_init() 541,331 &"py core_init()\n" 541,331 ~"Selected CORE=S32Z280_R52_0_0\n" 541,347 ~"Primary session connecting...\n" 541,360 =cmd-param-changed,param="remotetimeout",value="30" 545,535 ~"^Error:Target connection failed. Please re-check the settings." 545,535 ~"Processor: S32S250" 545,535 ~"Probe: S32 Debugger TAP (usb#00:04:9f:08:bc:b1)" 545,535 ~"[CCS: Bus error]" 545,535 ~"//" 545,535 ~"Additional error details:" 545,535 ~"[GTA: target access error]" 545,535 ~":GtaTaErr(1303)" 545,535 ~" File \" \", line 1, in " 545,535 ~" File \"C:\\NXP\\S32DS.3.6.3\\eclipse\\../S32DS/tools/S32Debugger/Debugger/scripts/s32z2e\ 2/s32z2e2_attach.py\", line 80, in core_init" 545,536 ~" connect()" 545,536 ~" File \"C:\\NXP\\S32DS.3.6.3\\eclipse\\../S32DS/tools/S32Debugger/Debugger/scripts/s32z2e\ 2/s32z2e2_attach.py\", line 52, in connect" 545,536 ~" gta_lib.establish_connection(" 545,536 ~" File \"C:\\NXP\\S32DS.3.6.3\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32z2e2//../u\ tils\\gta_lib.py\", line 89, in establish_connection" 545,536 ~" return connect(" 545,536 ~" File \"C:\\NXP\\S32DS.3.6.3\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32z2e2//../u\ tils\\errors.py\", line 275, in wrapper" 545,537 ~" v = func(*args, **kwargs)" 545,537 ~" File \"C:\\NXP\\S32DS.3.6.3\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32z2e2//../u\ tils\\gta_lib.py\", line 152, in connect" 545,537 ~" gdb_exec(\"monitor ctx connect\", from_tty=True, errcode=ErrorCode.ConnectError).unwra\ p()" 545,537 ~" File \"C:\\NXP\\S32DS.3.6.3\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32z2e2//../u\ tils\\mem_reg_utils.py\", line 65, in wrapper" 545,538 ~" result = Result(Error(value, str(error_msg)))"      The red part shows an error in the debugging tool link. Is this Python script a configuration issue or a problem with the GDB tool? Please help analyze it. If there is a configuration error, is there a script file updated with Python? Thank you! Re: S32Z2 Python script error issue Hi Chenyin, When my program stalls, I try to connect to the target board via the Probe to observe the error context. However, I often encounter connection errors #1303 or #101. What do these errors (1303 and 101) mean about the processor's state? Restarting the target device might resolve the Probe connection issue, but it also destroys the error context. This is why I want to understand the reason of error #1303 and #101. thanks for any help!
View full article