2189425_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2189425_en-US

2189425_en-US

S32K3 HSE: Export EDDSA Public Key

I am able to generate an ED25519 key pair with the Key Generation Service, and I would like to be able to export the public key later with the Key Export Service. However, the HSE returns a HSE_SRV_RSP_NOT_ALLOWED when I attempt to export the public key.

When I generate the key I use the following parameters:
Service ID: HSE_SRV_ID_KEY_GENERATE

targetKeyHandle = key_handle;

keyInfo:
keyFlags = HSE_KF_USAGE_SIGN | HSE_KF_USAGE_VERIFY | HSE_KF_ACCESS_EXPORTABLE
keyBitLen = HSE_KEY256_BITS
keyCounter = 0
smrFlags = 0
keyType = HSE_KEY_TYPE_ECC_PAIR
specific.eccCurveId = HSE_EC_25519_ED25519

keyGenScheme = HSE_KEY_GEN_ECC_KEY_PAIR

sch.eccKey.pPubKey = (HOST_ADDR)pub_key_output_ptr;

And when I export the key:

Service ID: HSE_SRV_ID_EXPORT_KEY

targetKeyHandle = key_handle; // Same Key Handle

keyInfo:
keyFlags = HSE_KF_USAGE_VERIFY | HSE_KF_ACCESS_EXPORTABLE
keyBitLen = HSE_KEY256_BITS
keyCounter = 0
smrFlags = 0
keyType = HSE_KEY_TYPE_ECC_PAIR
specific.eccCurveId = HSE_EC_25519_ED25519

pKey[0] = (HOST_ADDR)pub_key_output_ptr;
pKeyLen[0] = (HOST_ADDR)&g_identity_key_len;
 
Are there any parameter's that are missing or configured incorrectly?

Re: S32K3 HSE: Export EDDSA Public Key

Thank you Lukas, I was missing setting the HSE_INVALID_KEY_HANDLE's.

I see now in the header files: Must be set to #HSE_INVALID_KEY_HANDLE if not used.

Re: S32K3 HSE: Export EDDSA Public Key

Hi @MHan 

I can see nothing wrong in those parameters. Because the public ECC key is exported in plain and not authenticated, did you configured cipherKeyHandle and authKeyHandle as HSE_INVALID_KEY_HANDLE (0xFFFFFFFF)? Setting of HSE_INVALID_KEY_HANDLE to these key handles ensures that authentication and encryption parameters are ignored.
Also try to disable data cache to confirm it is not cache issue.

Regards,
Lukas

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 05:29 AM
Updated by: