FRDM-K66F microSD f_opendir never returns: stuck in SDMMC_OSAEventWait Board: FRDM-K66F. SDK: 2.11.0 (541 2022-01-14) I'm using the SD library to read and write files to an SD card. I'm using "baremetal" instead of an RTOS; I mention this because the definition for KOSA_StatusIdle says: KOSA_StatusIdle = MAKE_STATUS(kStatusGroup_OSA, 3), /*!< Used for bare metal only, the wait object is not ready and timeout still not occur */ My program is trying to f_opendir(), after verifying that the card exists, successful calls to f_mount(), and f_chdrive(), and it's hanging in this function: status_t SDMMC_OSAEventWait(void *eventHandle, uint32_t eventType, uint32_t timeoutMilliseconds, uint32_t *event) { assert(eventHandle != NULL); osa_status_t status = KOSA_StatusError; #if defined(SDMMC_OSA_POLLING_EVENT_BY_SEMPHORE) && SDMMC_OSA_POLLING_EVENT_BY_SEMPHORE while (true) { status = OSA_SemaphoreWait(&(((sdmmc_osa_event_t *)eventHandle)->handle), timeoutMilliseconds); if (KOSA_StatusTimeout == status) { break; } if (KOSA_StatusSuccess == status) { (void)SDMMC_OSAEventGet(eventHandle, eventType, event); if ((*event & eventType) != 0U) { return kStatus_Success; } } } #endif return kStatus_Fail; } This while() loop never exits because "timeoutMilliseconds" never decreases - the value passed in is a define: SDMMCHOST_TRANSFER_COMPLETE_TIMEOUT, rather than a variable - which might eventually lead to a time out, and the loop condition doesn't check for KOSA_StatusIdle. Before the point at which the program hangs, the semaphore is evidently properly created and removed: I've followed the semaphore value as it's increased and decreased in the Expression panel. However, at some point, OSA_SemaphorePost() is no longer called, so semCount isn't increased, and OSA_SemaphoreWait() just keeps returning KOSA_StatusIdle. Here's the call stack when it's stuck in this loop: Thread #1 57005 (Suspended : Breakpoint) OSA_SemaphoreWait() at fsl_os_abstraction_bm.c:584 0x616e SDMMC_OSAEventWait() at fsl_sdmmc_osa.c:69 0x3268 SDMMCHOST_TransferFunction() at fsl_sdmmc_host.c:299 0x8524 SD_SendScr() at fsl_sd.c:814 0x16e0 sdcard_init() at fsl_sd.c:2,033 0x2cbe SD_CardInit() at fsl_sd.c:2,085 0x2d96 SD_Init() at fsl_sd.c:2,268 0x307a sd_disk_initialize() at fsl_sd_disk.c:145 0x374c disk_initialize() at diskio.c:117 0x87ba mount_volume() at ff.c:3,376 0x3c02 f_opendir() at ff.c:4,544 0x953c prepareSDForWrite() at MK66F18_Van_Gizmo_v02.c:340 0xa9a measureAccelerometer() at MK66F18_Van_Gizmo_v02.c:353 0xaee main() at MK66F18_Van_Gizmo_v02.c:416 0xc8c How can I get either the timeout value to decrease, while time is physically passing, or get the semaphore count increased so the loop continues to work properly until f_opendir() completes? Also, here's a shot of the g_sd variable, at the time it enters the endless loop: Re: FRDM-K66F microSD f_opendir never returns: stuck in SDMMC_OSAEventWait XuZhang, I ran my copy of the sdcard_fatfs example program, which is probably identical to what you posted, and it did work, curiously, and when I added the "PRINTF" statements to the SDK example for the semaphore waits, the output looked similar to yours. Puzzling. I then went through all of the files in the two projects to see if the SDKs were somehow different: they were not. I checked the pull-up and pull-down statuses in the Pins perspective: the SDK example manually sets them "pull-up," and mine were "ignore." I changed mine, but it didn't make a difference. I checked the clock configuration - maybe a system clock of 120MHz was incorrect for the SD card; I dunno - and that had no change. Finally, since I couldn't find any other differences, I added the SYSMPU SDK module and the call to SYSMPU_Enable(SYSMPU, false); in the main initialization block. That did it. My semaphore counts were increasing and decreasing as in your example, and f_opendir() returned successfully. I've no idea what SYSMPU does, and I haven't seen it before when dealing with the FRDMK66 board, but that was the trick, evidently. I'm marking this as "solved." Thanks for your help. Re: FRDM-K66F microSD f_opendir never returns: stuck in SDMMC_OSAEventWait Can I ask what kind of SD card you used? And how was it formatted: ExFAT, or MS-DOS / FAT? I know it shouldn't matter, but I'm seeing different results in the same code if I use different SD cards. The one that fails with ACMD51, is a 2GB Lexar formatted as FAT-32; and the other is a 64GB SanDisk formatted as ExFAT. That one fails at SD_AllSendCid() line 2005, in sdcard_init() / fsl_sd.c. Re: FRDM-K66F microSD f_opendir never returns: stuck in SDMMC_OSAEventWait Hi , aaronm
I experimented with the MK66FN2M0xxx18 development board and the "frdmk66f_sdcard_fatfs" program in the SDK. It didn't seem to hang in SDMMC_OSAEventWait. I tried to print out the values of timeoutMilliseconds and semCount and found that the value of semCount was changing, and the return value of the OSA_SemaphoreWait() function was KOSA_StatusSuccess.
The location of adding the test output function is as shown below.
XuZhang_0-1720425194756.png
XuZhang_1-1720425207689.png
I can see the output results as shown in this figure, which outputs the values of timeoutMilliseconds and semCount during the program execution, and creates files in the SD card.
XuZhang_2-1720425294428.png
I have attached the program, I hope this can help you.
BR
XuZhang Re: FRDM-K66F microSD f_opendir never returns: stuck in SDMMC_OSAEventWait Further info: This is locking up in sdcard_init() -> SD_SendScr(), or when we run SD command ACMD51, Read the SD Configuration Register (SCR). When I stepped through the commands from SD_SendSCR(), I notice it doesn't trigger an SDHC interrupt, like the previous commands, such as SD_SendRca(), or SD_SendCsd(). These function trigger interrupts, which is where the semaphore counter is increased before reaching SDMMC_OSAEventWait(). What is the problem with SD_SendScr()? Just in case it matters, I'm not specifically using DMA in this application. Does that make a difference?
View full article