Example MPC5748G PretendedNetworkingCAN S32DS_1.0 ******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed * frequency * * * Mode transition to LPU_STOP is executed. CAN_0 is configured to wake up from * LPU_STOP to LPU_RUN using message with standard IDE = 0 as a wake up * preselected matching criteria. After wake up from LPU_STOP, user * LED1 is blinking. * * Modified files: mem.ld, sections.ld, startup.s, added file z2_restart.s * * * ------------------------------------------------------------------------------ * Test HW: MPC5748G-324DS, MPC574xG Motherboard * MCU: PPC5748GMMN6A 1N81M * Fsys: PLL0 160MHz * Debugger: Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * Target: internal_FLASH (debug mode, release mode) * EVB connection: Default * * * ******************************************************************************** ******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed * frequency * * * Mode transition to LPU_STOP is executed. CAN_0 is configured to wake up from * LPU_STOP to LPU_RUN using message with standard IDE = 0 as a wake up * preselected matching criteria. After wake up from LPU_STOP, user * LED1 is blinking. * * Modified files: mem.ld, sections.ld, startup.s, added file z2_restart.s * * * ------------------------------------------------------------------------------ * Test HW: MPC5748G-324DS, MPC574xG Motherboard * MCU: PPC5748GMMN6A 1N81M * Fsys: PLL0 160MHz * Debugger: Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * Target: internal_FLASH (debug mode, release mode) * EVB connection: Default * * * ******************************************************************************** General Re: Example MPC5748G PretendedNetworkingCAN S32DS_1.0 Hi, Can I use U-multilink to test this code?When I use this tool, I can not debug properly.
View full article