Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
FTF-HMB-N1961 - 高级线程实验室 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> <meta http-equiv="Content-Type" content="text/html; charset=utf-8" />
查看全文
i.mx8M EVK board encoder and decoder i.mx8M evk board has HW decoder and SW encoder, this document introduce how to use HW decoder and SW encoder the bsp is the latest version L4.14.78, the environment is : $ DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland $ bitbake fsl-image-validation-imx   For the 4.14.78, we don’t use mfgtool anymore, customer can use uuu.exe to program the image to the board, the uuu.exe can be found from https://github.com/NXPmicro/mfgtools/releases Here we use emmc as media, I attached the kerel_emmc.uuu for reference Open the cmd.exe, then use the command “uuu.exe kernel_emmc.uuu” to download the image to the emmc on the board as the picture shows When the board boot up, don’t forget to change the image and fdt_file as you want, for example, I use Image-imx8mqevk.bin as image name  and Image-fsl-imx8mq-evk.dtb as my fdt file, you can choose different image and fdt file as uuu file mentions. 1) Decoding   For play the video, we can use three solution to support this a) gplay-1.0 test.mp4 b) gst-launch-1.0 playbin uri=file:///mnt/sdcard/test.mp4 c) gst-launch-1.0 filesrc location=test.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! vpudec ! autovideosink For play the two different video to the different display, current imx8M evk board supports dual hdmi output, in the uboot command: setenv fdt_file Image-fsl-imx8mq-evk-dual-display.dtb saveenv Use the command as below:    gst-launch-1.0 playbin uri=file:///test1.mp4 playbin uri=file:///test2.mp4 video-sink="glimagesink display-master=false display-slave=true" 2) Encoding Because imx8M evk don’t have hardware encoding, so we need to add the SW plugins in the bsp   a)add the commands as below in the /build/conf/local.conf "CORE_IMAGE-EXTRA_INSTALL += "gstreamer1.0-plugins-ugly-meta packagegroup-fsl-gsstreamer1.0-commercial gst-ffmpeg" LICENSE_FLAGS_WHITELIST = "commercial""        b)Create the new txt file and add “PACKAGECONFIG_mx8mq = "x264"”in the file        c)Rename the file as 0-plugins-ugly_%.bbappend and put this file under /sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-multimedia/gstreamer        d)Build the image you want, then download the new rootfs file in the board, use the command “gst-inspect-1.0 | grep x264” i.MX 8M | i.MX 8M Mini | i.MX 8M Nano
查看全文
some useful tips about S32DS for ARM v2018.R1 IDE and S32K1xx development Dear all, I'd like to share some useful tips about S32DS for ARM v2018.R1 IDE and S32K1xx development  in Chinese as below: 《S32DS使用Tips--SDK使用常见问题(FAQ)答疑》; 《S32K SDK使用详解之S32 SDK软件编程思想详解》; 《S32K SDK使用详解之S32 SDK软件架构详解》; 《 S32K1xx系列MCU使用Tips--功能介绍及软件开发和硬件设计FAQ》; 《 S32K1xx系列MCU使用Tips--Flash加密后不断复位无法连接调试器的问题解决》; 《S32DS使用Tips--S32DS for Power V1.2 链接文件和启动过程详解》; 《S32K1xx系列MCU使用Tips之SDK软件架构和使用详解》; 《S32DS使用Tips--SDK使用常见问题(FAQ)答疑》; 《S32DS IDE使用Tips--应用工程调试常见问题(FAQ)答疑》; 《 S32DS 使用Tips之S32DS for Power不同版本之间的GNU工具链差异与外设寄存器位域访问问题总结》; 《 S32DS使用Tips之S32DS for Power v1.1应用工程升级到v1.2重新编译运行程序跑飞问题解决》; 《S32DS 使用tips--S32DS for ARM v1.3工程到S32DS for ARM V2.0迁移升级方法和注意事项》; 《  S32DS 使用 tips--工程属性配置(编译选项和C编译器、汇编器及链接器设置)》; 《 S32DS使用Tips--如何编译生成和调用静态库》; 《S32DS使用Tips--如何通过创建新的编译目标(Build Target)在同一个S32DS工程中同时编译静态库和应用程序》; 《 S32DS使用Tips--如何配置和使能Attach功能定位软件程序bug和完成bootloader与应用程序工程的联合调试》; 《 CodeWarrior与S32DS IDE使用 Tips之如何在应用工程中保留定义但未使用的全局常量、变量(用于参数标定)》; 《 S32DS 使用 tips--使用Flash from file下载S19或elf文件》; 《S32DS for ARM v2018.R1安装IAR Eclipse插件调用IAR工具链开发S32K系列MCU应用程序详解》 For more contents, please follow below link: “汽车电子expert成长之路”微信公众号最新最全原创技术分享文章列表 ; Hope this can help you and have a nice day~! Best regard, Enwei Hu(胡恩伟) General Re: some useful tips about S32DS for ARM v2018.R1 IDE and S32K1xx development Updates the lastest techncial sharing articles list(By Nov 15th, 2019) as below: 1. 《汽车电子ECU bootloader开发》系列   《汽车电子ECU bootloader开发要点详解》; 《汽车电子ECU bootloader开发之S32K144的CAN bootloader开发详解(工程源代码开源供大家参考)》; 《汽车电子ECU bootloader开发开发之S32K1xx系列MCU bootloader开发要点详解》;      《汽车电子ECU BootLoader开发之基于CAN总线通信的MPC574xP系列MCU bootloader开发详解》;       《汽车电子ECU BootLoader开发之基于CAN总线通信的S12(X) 系列MCU独立NVM驱动安全bootloader》;       《 浅谈嵌入式软件开发之Qorivva MPC57xx和S32R系列多核MCU启动配置与bootloader开发要点详解》; 《 Qorivva MPC56xx系列MCU启动过程全解析(基于CW IDE应用工程--EAB I、链接文件、启动文件和map文件)》; 《浅谈嵌入式MCU软件开发之startup过程详解(从复位向量到main函数之前的准备工作)》; 《浅谈嵌入式MCU软件开发之S32K1xx系列MCU启动过程及重映射代码到RAM中运行方法详解》; 《CodeWarrior IDE使用Tips之利用prm链接文件实现储存器数据填充和代码编译结果CRC校验和自动生成详解》; 《汽车电子ECU BootLoader开发》系列相关文章链接与资源汇总;   2. 《浅谈嵌入式MCU软硬件开发》系列 《 浅谈嵌入式MCU开发中的三个常见误区》;       《 浅谈嵌入式 MCU 软件开发之应用工程的堆与栈》;       《 浅谈嵌入式MCU软件开发之中断优先级与中断嵌套》;       《 浅谈嵌入式MCU软件开发之代码风格与代码优化》; 《浅谈嵌入式MCU软件开发之内存分配详解--链接文件与map文件中段的分配使用和使用注意事项》; 《浅谈嵌入式MCU硬件设计之MCU最小系统电路》; 《浅谈嵌入式MCU软件开发之startup过程详解(从复位向量到main函数之前的准备工作)》; 《浅谈嵌入式MCU软件开发之S32K1xx系列MCU启动过程及重映射代码到RAM中运行方法详解》; 《浅谈嵌入式MCU软件开发之S32K1xx系列MCU CPU内核性能优化方法详解》; 《浅谈嵌入式软件开发之Qorivva MPC57xx和S32R系列多核MCU启动配置与bootloader开发要点详解》; 《浅谈嵌入式系统软件开发之S32K1xx系列MCU的MPU配置与使用详解》; 《浅谈嵌入式软件开发之MagniV S12Z系列MCU内核Machine Exception异常原理与恢复》; 《浅谈嵌入式软件开发之重定向标准输入输出设备使用printf()函数格式化输出调试信息(基于S32DS IDE和MPC5744P)》; 《浅谈嵌入式MCU软件开发之startup过程详解(在CodeWarrior 5.1 中实现RAM自定义初始化)》; 《嵌入式软件开发之S12(X)系列MCU的far和near函数指针调用详解(S12G128 CW 5.x Project)》; 《浅谈嵌入式MCU软件开发之S12(X)系列MCU 中断ISR在CodeWarrior 5.1 IDE 中的三种写法》; 《浅谈嵌入式软件开发之Qorivva MPC56/57xx系列MCU的Power e200内核寄存器功能和内核调试技巧介绍》; 《嵌入式软件开发之调试器(Debugger)使用--PEMicro Multilink功能介绍与使用FAQ 》; 《浅谈嵌入式MCU软件开发之MCU芯片内部Bandgap参考电压(带隙基准)和集成温度传感器的工作原理和使用详解》; 《浅谈嵌入式MCU软件开发之条件断点的设置与使用详解(以S32DS IDE + U-Multink debugger为例介绍)》; 《浅谈嵌入式软件开发之使用Srecord工具实现S19文件数据填充和CRC校验和自动计算与存储方法详解》; 《浅谈嵌入式MCU软件开发之使用makefile脚本编译和调试NXP S32 SDK应用工程详解》;   3.   《外设使用Tips》系列   《S32K1xx系列MCU使用Tips之SDK软件架构和使用详解》;      《S12(X)系列MCU的片上存储器资源与分页访问机制详解(一) 》;       《S12(X)系列MCU的片上存储器资源与分页访问机制详解(二)》;     《S12(X)系列MCU的加密(Secure)原理和解密(Unsecure)方法》; 《 Qorivva MPC56xx系列MCU的Flash加密解密原理与工程实现方法详解》;      《使用 Cyclone 离线编程器对 S12(X)和 MagniV S12Z 系列 MCU 片上 NVM 编程》;        《 S32K1xx系列MCU使用Tips--功能介绍及软件开发和硬件设计FAQ》;        《 S32K1xx系列MCU使用Tips--Flash加密后不断复位无法连接调试器的问题解决》; 《S32K14x系列MCU使用Tips之硬件FPU特性介绍和使用详解》; 《外设使用Tips之Qorivva MPC56xx_57xx系列MCU内核异常(IVORx)与IRQ中断处理详解》; 《外设使用Tips之Qorivva MPC56xx/57xx系列MCU的模式控制与切换(片上外设资源使能与功耗控制)》; 《外设使用Tips之MCU内部集成IRC时钟工作原理、特性和trim原理及方法详解(以KEA系列MCU的ICS为例)》; 《外设使用Tips之S12G系列MCU Startup之前的复位过程详解(COP看门狗复位和时钟监测复位中断识别与处理)》;        《外设使用Tips之MPC57xx系列MCU C55 Flash模块详解及其SSD(标准软件驱动)使用》;       《 外设使用Tips之MSCAN接收ID滤波器设置》;        《外设使用Tips之TIM定时器使用FAQ和使用经验》;       《 外设使用Tips之MPC574xP系列汽车级MCU的SWT看门狗定时器配置与使用》;       《NXP汽车MCU开发详解之《 KEA系列汽车MCU开发指南》》;  《S32K1xx系列MCU应用指南之芯片锁死(lockup)复位原因分析与恢复方法详解》; 《关于使用J-LINK开发S32K1xx系列MCU应用程序的使用说明和注意事项》;   4. 《S32K SDK使用详解》系列   《S32K SDK使用详解之S32 SDK软件编程思想详解》; 《S32K SDK使用详解之S32 SDK软件架构详解》; 《S32K SDK使用详解之Keil MDK开发S32K1xx系列MCU应用程序(使用Processor Expert配置SDK)》; 《S32K SDK使用详解之GHS Multi(Eclipse插件)开发S32K1xx系列MCU应用程序(使用PE配置SDK)》; 《浅谈嵌入式MCU软件开发之使用makefile脚本编译和调试NXP S32 SDK应用工程详解》; 《浅谈嵌入式MCU软件开发之S32K1xx系列MCU CPU内核性能优化方法详解》; 《S32DS GNU GCC编译优化选项与配置方法详解及S32 SDK代码编译优化选项设置建议》; 《《S32K系列MCU应用开发详解》直播ppt高清pdf版本下载与直播视频回放链接》; 《S32DS使用Tips--SDK使用常见问题(FAQ)答疑》;   5. 《S32K1xx应用指南》系列   《S32K1xx系列MCU应用指南之芯片锁死(lockup)复位原因分析与恢复方法详解》; 《S32K1xx系列MCU应用指南之存储器ECC功能使用详解(一)》; 《S32K1xx系列MCU应用指南之存储器ECC功能使用详解(二)》; 《S32K1xx系列MCU应用指南之RTC模块使用详解》; 《S32K1xx系列MCU应用开发指南之IAR toolchain样例工程及使用常见问题(FAQ)》;   6. 《细说汽车电子通信总线》系列 《细说汽车电子通信总线之CAN 2.0 总线协议详解》; 《细说汽车电子通信总线之CAN-FD 总线协议详解》; 《细说汽车电子通信总线之LIN总线协议详解》; 《细说汽车电子通信总线之常见汽车电子串行通信总线(CAN、LIN、DSI、ISO-9141、SWCAN、J 1850)对比》;   7. 《S32DS IDE使用Tips》系列     《S32DS使用Tips--S32DS for Power V1.2 链接文件和启动过程详解》; 《S32K1xx系列MCU使用Tips之SDK软件架构和使用详解》;  《S32DS GNU GCC编译优化选项与配置方法详解及S32 SDK代码编译优化选项设置建议》; 《S32DS IDE使用Tips--应用程序开发实战实用技巧总结与详解(工欲善其事必先利其器)》; 《S32DS使用Tips--SDK使用常见问题(FAQ)答疑》; 《S32DS IDE使用Tips--应用工程调试常见问题(FAQ)答疑》;       《S32DS 使用Tips之S32DS for Power不同版本之间的GNU工具链差异与外设寄存器位域访问问题总结》;       《S32DS使用Tips之S32DS for Power v1.1应用工程升级到v1.2重新编译运行程序跑飞问题解决》;     《S32DS 使用tips--S32DS for ARM v1.3工程到S32DS for ARM V2.0迁移升级方法和注意事项》;       《 S32DS 使用 tips--工程属性配置(编译选项和C编译器、汇编器及链接器设置)》;       《 S32DS使用Tips--如何编译生成和调用静态库》;      《S32DS使用Tips--如何通过创建新的编译目标(Build Target)在同一个S32DS工程中同时编译静态库和应用程序》;      《 S32DS使用Tips--如何配置和使能Attach功能定位软件程序bug和完成bootloader与应用程序工程的联合调试》; 《 CodeWarrior与S32DS IDE使用 Tips之如何在应用工程中保留定义但未使用的全局常量、变量(用于参数标定)》;       《 S32DS 使用 tips--使用Flash from file下载S19或elf文件》; 《S32DS for ARM v2018.R1安装IAR Eclipse插件调用IAR工具链开发S32K系列MCU应用程序详解》; 《浅谈嵌入式MCU软件开发之条件断点的设置与使用详解(以S32DS IDE + U-Multink debugger为例介绍)》; 《S32DS IDE使用Tips之配置objcopy选项生成S3行的S19文件和指定每行S19文件的最大数据长度的方法和步骤详解》;   8. 《CodeWarrior IDE使用Tips》系列   《CodeWarrior IDE使用tips之bug定位绝技--hotsync与attach调试》; 《CodeWarrior IDE使用Tips之Qorivva MPC56xx新建应用工程选项、调试高级选项及下载过程控脚本详解》; 《CodeWarrior IDE使用tips之prm链接文件详解(自定义存储器分区以及自定义RAM数据初始化与在RAM中运行函数)》; 《CodeWarrior IDE使用Tips-Qorivva MPC56xx应用工程map文件全解析(CW 2.10/10.x )》;       《 CodeWarrior IDE使用tips之map文件详解》;      《 CodeWarrior IDE 版本选择与 License功能(feature)和价格,授权形式差异、激活方法与安装使用》; 《CodeWarrior IDE使用Tips之利用Hiwave读取S12(X)系列MCU片上NVM命令脚本(CW 5.x IDE)》;       《 CodeWarrior IDE使用Tips-如何编译生成和调用静态库》;      《 CodeWarrior与S32DS IDE使用 Tips之如何在应用工程中保留定义但未使用的全局常量、变量(用于参数标定)》;      《 CodeWarrior IDE使用Tips之如何通过prm文件指定汇编代码函数、全局变量和常量的储存地址》;      《CodeWarrior IDE使用Tips之利用prm链接文件实现储存器数据填充和代码编译结果CRC校验和自动生成详解》; 《CodeWarrior IDE使用Tips之burner工具使用详解(实现不同类型存储器地址间的转换和NVM编程格式文件的输出)》; 《CodeWarrior IDE使用Tips--使用burner将elf文件转换生成HEX和BIN文件的方法和步骤详解》; 《CodeWarrior IDE使用Tips之利用Hiwave读取S12(X)系列MCU片上NVM命令脚本(CW 5.x IDE)》;    9.   《汽车ECU参数标定》系列   汽车ECU参数标定之配置e200系列CPU内核MMU实现Qorivva MPC56xx_57xx系列MCU的参数在线实时标定》;   《汽车ECU参数标定之配置Overlay RAM实现Qorivva MPC57xx系列MCU参数在线标定和代码重映射原理和方法详解》; 《CodeWarrior IDE使用Tips之如何通过prm文件指定汇编代码函数、全局变量和常量的储存地址》; 《CodeWarrior与S32DS IDE使用 Tips之如何在应用工程中保留定义但未使用的全局常量、变量(用于参数标定)》; 《CodeWarrior IDE使用tips之prm链接文件详解(自定义存储器分区以及自定义RAM数据初始化与在RAM中运行函数)》; 《CodeWarrior IDE使用tips之map文件详解》; 《S32DS使用Tips--S32DS for Power V1.2 链接文件和启动过程详解》;   10.  《答疑解惑》系列 《《疑难答疑》之S12G系列MCU使用Hiwave和BDM调试器debug时无法使用逻辑地址查看和保存P-flash问题的解决》; 《《疑难答疑》之S32DS IDE调试启动过程详解与调试目标复位方法和步骤详解》; 《《答疑解惑》之S12(X)系列MCU的CodeWarrior 5.x应用工程下载调试过程详解以及如何保护NVM存储器不被擦除》;   11. 《产线批量Flash编程与ESD/EOS保护》系列 《使用 Cyclone 离线编程器对 S12(X)和 MagniV S12Z 系列 MCU 片上 NVM 编程》; 《使用Cyclone 离线编程器对S32K1系列MCU进行NVM(P-Flash, D-Flash和EEE)编程的方法与步骤详解》;       12.  其他   《汽车电子expert成长之路微信公众号原创技术分享文章集合2017~2018年下载》; 《汽车电子expert成长之路”微信公众号最新最全原创技术分享文章列表》; 《汽车以太网(100BASE-T1)转工业以太网(100BASE-TX)转换器工作原理介绍》; 《好消息!使用关键词回复功能找到感兴趣的公众号原创技术文章》; 《原创技术文章高清PDF版分享链接(限时7天),欢迎下载》; 《历史文章分类列表目录(点击文章标题即可直接跳转阅读,截止2019年6月15日)》; 《历史文章分类列表目录(点击文章标题即可直接跳转阅读,截止2019年7月15日)》; 《历史文章分类列表目录(点击文章标题即可直接跳转阅读,截止2019年8月15日)》; 《历史文章分类列表目录(点击文章标题即可直接跳转阅读,截止2019年9月15日)》; 《历史文章分类列表目录(点击文章标题即可直接跳转阅读,截止2019年10月15日)》; 《给大家拜年了--这份大礼,请务必收下!--公众号原创技术文章阅读链接整理与分享》;   Best regard, Enwei Hu(胡恩伟)
查看全文
MCUXpressoソフトウェアとツールによるFreeRTOS™の最適化 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションでは、Segger SystemViewやPercepio Tracealizerなどのツールを含むMCUXpresso SDKとIDEを使用してFreeRTOS™アプリケーションを最適化する方法を示します。このセッションでは、構成設定によるRTOSの最適化、NXP Kernel Awarenessを使用したスタックとランタイムの検査、Segger RTTとSystemViewを使用したリアルタイムデータのストリーミング、RTOSとアプリケーショントレースを使用したシステムパフォーマンスの分析と最適化について説明します。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションでは、Segger SystemViewやPercepio Tracealizerなどのツールを含むMCUXpresso SDKとIDEを使用してFreeRTOS™アプリケーションを最適化する方法を示します。このセッションでは、構成設定によるRTOSの最適化、NXP Kernel Awarenessを使用したスタックとランタイムの検査、Segger RTTとSystemViewを使用したリアルタイムデータのストリーミング、RTOSとアプリケーショントレースを使用したシステムパフォーマンスの分析と最適化について説明します。
查看全文
AFV10700H Highest Power Density 750 W L Band RF LDMOS Transistor Demo NXP boasts about power and prowess in the industry’s highest power density in LDMOS technology with a compact 750 W 1.3 x 2.55 inch reference circuit. See this demo for how our transistors deliver highest RF output power for automatic dependent surveillance – broadcast (ADS-B), identification friend-or-foe (IFF), and distance measuring equipment (DME) systems. Product AFV10700H|700 W Pulse, 1030-1090 MHz, 52 V|NXP (50V LDMOS, 750 W Peak, Gain 17dB, Efficiency 58%) Link www.nxp.com/RFPower Communications Infrastructure
查看全文
i.MX RT系列 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 介绍 i.MX RT 产品和汽车合格变体,适用于需要实时处理和低物料清单的多媒体应用。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 介绍 i.MX RT 产品和汽车合格变体,适用于需要实时处理和低物料清单的多媒体应用。
查看全文
TARS_里程碑_3 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 在此视频中,您可以看到我们用来每 10 秒将传感器数据引入数据库的 Python 草图的运行模式、数据库本身和网页,该网页以精美的格式显示存储在数据库中的信息(最后一条,每 15 秒刷新一次)以及描述温度、湿度和压力随时间变化的 3 个图表。 (在 “我的视频” 中查看) 2017 年 Linux 嵌入式挑战赛
查看全文
DES-N1989 Hands-On Workshop: Hands-On with the SCM-i.MX 6Dual6Quad Quick Start Board Learn how to effectively use the integrated SPI-NOR flash on the SCM-i.MX 6Dual/6Quad. Topics covered will include the characteristics of a Linux image that will fit entirely into 16 MB SPI-NOR, and examples for how to leverage the SPI-NOR along with external boot sources such as eMMC. Attendees will also get to try multiple scenarios using the Quick Start board. Learn how to effectively use the integrated SPI-NOR flash on the SCM-i.MX 6Dual/6Quad. Topics covered will include the characteristics of a Linux image that will fit entirely into 16 MB SPI-NOR, and examples for how to leverage the SPI-NOR along with external boot sources such as eMMC. Attendees will also get to try multiple scenarios using the Quick Start board. Design | Software & Services
查看全文
i.MX 8シリーズ:eCockpitシミュレータ(バーチャルリアリティ) <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 最先端のeCockpitに座るのはどんな感じですか?バーチャルリアリティヘッドセットを装着して見つけてください!ここでは、HUD、クラスター、インフォテインメント、後部座席エンターテイメントシステムの4つのディスプレイからのライブビデオコンテンツが、単一の i.MX 8アプリケーションプロセッサからリアルタイムで処理およびストリーミングされるため、仮想世界と現実世界が出会います。 i.MX 8シリーズは、想像もしなかった方法でインタラクションを変革します   NXP製品の推奨 i.MX 8 ARMCortex-A53プロセッサ|NXPの  モバイル
查看全文
DES-N2044 TQ 系统:如何充分利用处理器板 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 在集成设计中使用处理器是一种方法。使用嵌入式模块是另一种方法,可以加快设计速度、降低设计风险并降低设计成本。不同的模块供应商将提供什么支持?如果使用嵌入式模块,有哪些限制和约束?市场概述和选择嵌入式模块供应商的指南。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 在集成设计中使用处理器是一种方法。使用嵌入式模块是另一种方法,可以加快设计速度、降低设计风险并降低设计成本。不同的模块供应商将提供什么支持?如果使用嵌入式模块,有哪些限制和约束?市场概述和选择嵌入式模块供应商的指南。 设计 | 软件与服务
查看全文
INS-N1913 改进型集成电路间 I3C 标准 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 现代汽车不仅仅是交通工具,它还提供舒适的加热和制冷系统、导航系统、娱乐系统、以及众多关于汽车健康和性能的数据。 包括您省油的情况或何时进行保养。 向驾驶员和乘客展示所有这些数据 --且无论是大白天还是大黑夜,不论温度如何,均不影响驾驶,这是一个很大的挑战。 我们同时讨论让仪表板保持简单、可读和有用的液晶显示器(LCD)和发光二极管(LED)组件解决方案。 观看视频演示 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 现代汽车不仅仅是交通工具,它还提供舒适的加热和制冷系统、导航系统、娱乐系统、以及众多关于汽车健康和性能的数据。 包括您省油的情况或何时进行保养。 向驾驶员和乘客展示所有这些数据 --且无论是大白天还是大黑夜,不论温度如何,均不影响驾驶,这是一个很大的挑战。 我们同时讨论让仪表板保持简单、可读和有用的液晶显示器(LCD)和发光二极管(LED)组件解决方案。 观看视频演示 洞察与创新
查看全文
如何使用微量缓冲液(MTB) <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 分享一些如何使用微迹缓冲区的信息。
查看全文
NET-N1883 QorIQ LS2088AおよびLS1088A向けのODPおよびDPDKの詳細 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ODP と DPDK は、さまざまなネットワーク プロセッサ アーキテクチャで使用されるデータプレーンの API の標準セットを定義するオープンソース プロジェクトです。このセッションでは、標準のDPDKおよびODP APIが、特定のパケット処理要素(パケットIO、分類、スケジューリング、暗号化など)のNXPデータパスアクセラレーションにどのようにマッピングされているかについて詳しく説明します。また、NXP SoCSで追加のパフォーマンスを得るためのさまざまな可能なAPI拡張も提案します。このプレゼンテーションでは、ODPとDPDKが仮想化環境に必要なインフラストラクチャを提供する方法について説明します。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ODP と DPDK は、さまざまなネットワーク プロセッサ アーキテクチャで使用されるデータプレーンの API の標準セットを定義するオープンソース プロジェクトです。このセッションでは、標準のDPDKおよびODP APIが、特定のパケット処理要素(パケットIO、分類、スケジューリング、暗号化など)のNXPデータパスアクセラレーションにどのようにマッピングされているかについて詳しく説明します。また、NXP SoCSで追加のパフォーマンスを得るためのさまざまな可能なAPI拡張も提案します。このプレゼンテーションでは、ODPとDPDKが仮想化環境に必要なインフラストラクチャを提供する方法について説明します。 スマートネットワーク
查看全文
INS-N2024 半导体 101-102 集成电路的功能和制造 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 许多从事电子行业的人员需要具备半导体元件的基本知识,以便理解制造周期、半导体工厂整合和故障分析结果等问题。本次会议面向非技术受众,并对半导体器件及其制造方法进行了高层次的概述。讲座首先简要概述了半导体器件的工作原理。演示的大部分内容描述了半导体器件的通用制造流程,重点强调了所用设备/设施的复杂性和所需的处理时间。 观看视频演示 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 许多从事电子行业的人员需要具备半导体元件的基本知识,以便理解制造周期、半导体工厂整合和故障分析结果等问题。本次会议面向非技术受众,并对半导体器件及其制造方法进行了高层次的概述。讲座首先简要概述了半导体器件的工作原理。演示的大部分内容描述了半导体器件的通用制造流程,重点强调了所用设备/设施的复杂性和所需的处理时间。 观看视频演示 洞察与创新 回复:INS-N2024 半导体 101-102 集成电路的功能和制造 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 关于组装封装工艺流程,请告知第63页,第二行表示工艺流程的箭头是保留的。应该是:等离子清洁-->引线键合-->模具-->模具后固化......
查看全文
AUT-N1797 MagniV モータ制御用統合ソリューション <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 従来のMCU機能と高電圧アナログ部品を1つのチップに組み合わせることで、システムコストを節約できます。品質を向上させ、設置面積を削減する統合ソリューション。ここでは、ウィンドウリフト、サンルーフ、スライドドアなどのクロージャーソリューション向けのS12 MagniV MCUファミリの概要を示します。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 従来のMCU機能と高電圧アナログ部品を1つのチップに組み合わせることで、システムコストを節約できます。品質を向上させ、設置面積を削減する統合ソリューション。ここでは、ウィンドウリフト、サンルーフ、スライドドアなどのクロージャーソリューション向けのS12 MagniV MCUファミリの概要を示します。 セキュアなコネクテッド&自動運転車
查看全文
MQX FlashX 驱动程序 – 如何编写 FlexNVM? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 1. 关于 FlexNVM 和 FlashX 的一些基本问题和解答。 1.1 什么是 FlexNVM? FlexNVM 是额外的独立闪存块,可用作数据闪存、模拟 EEPROM 的非易失性存储器或两者的组合。我将重点介绍本文档中的第一个选项——FlexNVM 将简单地用作数据闪存。 您可以在部件编号的专用位置包含“X”的 MCU 部件中找到 FlexNVM。例如: MK64F X 512VMD12 包含 1 个程序闪存块 (512 KB) 和 1 个 FlexNVM 块 (128 KB) MK64F N 1M0VMD12 仅包含 2 个程序闪存块(每个 512 KB)。 有关 FlexNVM 和闪存块的更多详细信息,请参阅您的 MCU 参考手册。例如“闪存大小”章节。 1.2 什么是FlashX? MQX FlashX 驱动程序提供写入和读取内部闪存的能力。不幸的是,FlexNVM 内存在默认状态下仅部分受支持——一些 BSP 已经实现了模拟 EEPROM(flexnvm 示例代码)的配置和功能。有关更多详细信息,请查看c:\Freescale\Freescale_MQX_4_2\doc\mqx文件夹中的MQX_IO_User_Guide.pdf 。 1.3 我可以将不带 FlexNVM 的 MCU BSP 用于我自己的带有带 FlexNVM 的 MCU 的主板吗? 不建议这么做。但是,您可以使用此 BSP 作为您自己的板 BSP 的基础。请检查MQX_BSP_Cloning_Wizard_Getting_Started.pdf ,MQX_BSP_Porting_Guide.pdf和MQX_BSP_Porting_Example_User_Guide.pdf文档位于C:\Freescale\Freescale_MQX_4_2\doc文件夹中。 1.4 我可以在我的 KSDK 项目中使用 FlashX 吗? 不幸的是,FlashX 驱动程序没有在 KSDK 中实现。KSDK 包含其自己的用于 C90TFS/FTFx Flash 系列的标准软件驱动程序 (SSD),然而,这只是低级驱动程序,没有像 FlashX 驱动程序那样的高级抽象层。 2. 更新 MQX FlashX 驱动程序以支持 FlexNVM 的过程。 2.1 请备份以下文件: user_config.h 、 .h ,init_flashx.c文件flash_ftfl.c和flash_ftfe.c文件。注意: user_config.h , .h 和 init_flashx.c是 BSP 代码的一部分。 2.2 在user_config.h中启用 FlashX文件定义: #定义 BSPCFG_ENABLE_FLASHX 1 2.3 更新.h 文件: 2.3.1 请检查 MCU 参考手册并根据需要更新 BSP_INTERNAL_FLASH_BASE、BSP_INTERNAL_FLASH_SIZE、BSP_INTERNAL_FLASH_SECTOR_SIZE。通常,当使用不带 FlexNVM 的 BSP 作为自己的 BSP 的基础时,我们必须减少 BSP_INTERNAL_FLASH_SIZE。 2.3.2添加将在内存映射中定义 FlexNVM 的新宏。例如: #定义 BSP_INTERNAL_FLEXNVM_BASE 0x10000000 #定义 BSP_FLEXNVM_SECTOR_SIZE 0x400 #定义 BSP_INTERNAL_FLEXNVM_SIZE 0x00008000 2.4 更新 BSP 文件夹中的init_flashx.c : 2.4.1 将 FlexNVM 文件块添加到 _bsp_flashx_file_blocks[] 表中。例如: // 数据闪存文件块 { “dflash”,BSP_INTERNAL_FLEXNVM_BASE,(uint32_t)(BSP_INTERNAL_FLEXNVM_BASE + BSP_INTERNAL_FLEXNVM_SIZE - 1)}, 参数为{文件块名称,起始地址,结束地址}。 注意:这是纯软件接口;地址范围不需要适合物理闪存块参数。您可以根据需要组织文件块。 2.4.2如果您使用非 FlexNVM BSP 作为您自己的 BSP 的基础,则必须更改 KinetisX 设备的硬件块图。请在_bsp_flashx_init 结构中将_flashx_kinetisN_block_map 更改为_flashx_kinetisX_block_map。 2.5 更新flash_ftfl.c或flash_ftfe.c文件: 2.5.1 查看 MCU 参考手册,了解您的 MCU 是否具有 FTFL 或 FTFE 闪存模块,并选择适当的文件进行编辑。 2.5.2将 FlexNVM 内存块添加到 _flashx_kinetisX_block_map[] 表中。例如: { BSP_INTERNAL_FLEXNVM_SIZE / BSP_FLEXNVM_SECTOR_SIZE,(_mem_size)BSP_INTERNAL_FLEXNVM_BASE,BSP_FLEXNVM_SECTOR_SIZE }, // FlexNVM 块 参数为{扇区数,起始地址,扇区大小}。 注意:这是物理硬件内存块的描述;地址范围必须适合物理闪存块参数。 2.5.3现在我们必须修复 FlexNVM 地址的问题。程序闪存和 FlexNVM 闪存均通过 FTFL_FCCOBn / FTFE_FCCOBn 寄存器进行编程,其中 FCCOB1.. FCCOB3 包含 24 位格式的地址。因此,我们不能直接使用 FlexNVM 地址——由于 FlexNVM 基数为 0x10000000,它们不适合 24 位。 FTFL/FTFE 模块指定 24 位地址中的最高有效位(位 23)将用于区分程序闪存和 FlexNVM 闪存。例如,我们可以使用这样的代码: //设置第23位,当FlexNVM闪存地址 如果(write_addr&BSP_INTERNAL_FLEXNVM_BASE)     { 写入地址 = 写入地址 | (1 << 23);     }   并在写入 command_array[] 之前将此代码添加到必要的函数中( command_array[]的内容将用于填充 FTFL_FCCOBn / FTFE_FCCOBn 寄存器)。 为了 FlashX 示例代码的基本工作,至少需要更新 ftfl_flash_erase_sector()/ftfe_flash_erase_sector() 和 ftfl_flash_write_sector()/ftfe_flash_write_sector() 函数。 2.6.完成这些更改后,您可以尝试使用flash_demo.c中的 FlashX 示例代码您只需打开 FlexNVM 文件块而不是默认程序闪存文件块。例如: //#define FLASH_NAME“flashx:bank0” #define FLASH_NAME“flashx:dflash” 在附件文件中,您可以找到 MQX4.2.0 和 MK20DX72 MCU 的修改示例。 3. 如何重写 Flash - 一般说明: Flash数据在编程之前必须处于已擦除状态。 不允许对位进行累计编程(添加更多0)。 对于 FTFL 和 FTFE 模块,我们通过对齐的短语(通常为 64 位)对闪存进行编程。如果我们想要按更小的块(例如按字节)进行编程,FTFL 模块将允许您写入此短语,即使不推荐这样做。但FTFE模块如果第二次写入同一个相位,将会引起总线故障。因此,更改已写入的 FTFE 短语中的数据的唯一安全方法是擦除整个扇区并重写数据。因此,请对 FTFE 模块使用 ioctl 命令 FLASH_IOCTL_ENABLE_SECTOR_CACHE。当目标区域(与短语对齐)为空白时,在完整扇区写入和部分扇区覆盖的情况下不需要扇区缓存分配。 回复:MQX FlashX 驱动程序 – 如何编写 FlexNVM? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,Shridhar, 对于 FlexNVM: 您还必须编辑 flash_ftfl.c 中的 _flashx_kinetisX_block_map[] 表文件并添加 FlexNVM 块的描述。 对于 FlexRAM: 您在断电之前是否使用过刷新/关闭功能? 如何使用 FlexRAM 的示例可以在这里找到 c:\Freescale\Freescale_MQX_4_2\mqx\examples\flexnvm 在我们启用 EEPROM 仿真之前,目标 FlexRAM 内存范围的工作方式与“标准”RAM 相同。 当然,您必须选择是否将 FlexNVM 内存用作数据闪存、模拟 EEPROM,或者您可以将 FlexNVM 内存分成两部分并使用两个选项(在这种情况下,必须相应地更新内存范围)。 无论如何,空 MCU 上具有默认设置的 FlexNVM 内存可用作数据闪存,而 FlexRAM 可用作“标准”RAM。如果您想使用模拟 EEPROM(FlexRAM),则必须为其配置 FlexNVM 内存(程序分区命令和设置 FlexRAM 功能命令)。查看 flexnvm 示例代码...
查看全文
DragonFlame_TechnicalReport.pdf Technical report from Team Dragon Flame from Mexico prepared for The Freescale Cup WW Finals 2015 Technical report from Team Dragon Flame from Mexico prepared for The Freescale Cup WW Finals 2015
查看全文
TFC2015 UCDavis 团队 Chucksgon 最终报告 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> TFC2015 UCDavis 团队 Chucksgon 最终报告 感谢LanceHalsted的分享​ <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> TFC2015 UCDavis 团队 Chucksgon 最终报告 感谢Lance Halsted的分享​ 飞思卡尔杯内容 学生项目
查看全文
Freetech工具介绍,基于KE02 PWM实现高精度ADC转换及实现简单音频 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 由 Freetech 呈现 基于 ARM ®技术的 DwF Kinetis MCU 研讨会 - 天津 - 2015 年 3 月 19 日 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 由 Freetech 呈现 基于 ARM ®技术的 DwF Kinetis MCU 研讨会 - 天津 - 2015 年 3 月 19 日 Kinetis Cortex ® -M 微控制器
查看全文
.sdcardをダウンロードi.MX6sx SabreSDB for MFGToolのイメージ <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 私はタスク#4 - デプロイとテストまでYoctoトレーニングに従いました。そして、私はここで立ち往生しました。 .sdcardをダウンロードできません画像をSDカードに貼り付けます。最初にフォーマットする必要がありますか?それは真新しいです。 sudo dd if=core-image-base-imx6solosabresd.sdcard of=/dev/sdb1 bs=1M が私には動作しなかったため、ボード上の SD から起動できませんでした。ボードのスイッチはSD4から起動するように設定されています。imx6solosabresd は solox に使用するのに適したマシンですか?local.conf ファイルに MACHINE=imx6sxsabersd を設定しようとしましたが、エラーメッセージが表示されました (タスク #2)。 だからこそ、MFGToolを試してみたいのです。ボードをSD3から起動するように設定して、「ダウンロードモード」に切り替えられるようにしました。MFGToolを実行すると、HID準拠のベンダー定義のデバイスが表示されますが、デバイスが接続されていませんと表示されます。 このドキュメントは、次のディスカッションから作成されました。
查看全文