Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
料金の初期化時間について NXPのエキスパートの方、こんにちは。S32K312のフィード初期化時間に問題があり、ご相談させていただきたいのですが。詳細は以下のとおりです。 プライマリとスタンバイの2つのデータストレージクラスタグループを設定しました。スタンバイはプライマリのバックアップです。合計19個のブロックが設定され、これらのブロックはプライマリとスタンバイの両方に保存されます。ソフトウェアバージョンはMcal RTD4.0.0 HF02で、バーストモードが有効になっています。 Chenxu1_0-1785460201957.png 試験方法: 電源投入時に初期化時刻が出力され(Mem_43_INFLS_Initt()、MemAcc_Initt()、Fee_Init() を呼び出した後、Fee_GetStatus() インターフェースが MEMIF_IDLE を返すまで待機)、すべてのブロックにデータが一度書き込まれます。 試験結果は以下のとおりです。 パワーアップアイテムの数 初期化時間(ミリ秒) 例示する 1 8 2 15 3 23 4 40 5 48 6 57 7 65 8 74 9 82 10 90 11 99 12 107 13 115 14 124 15 133 16 141 17 149 18 158 19 166 20 175 21 183 22 192 23 200 24 209 25 217 26 226 27 234 28 8 クラスタページング 上記のテスト結果から、各増分にかかる時間が非常に速く変化することが分かりました。そこで、初期時間を計算する式が存在するかどうか、また、その式を最適化できるかどうかをお伺いしたいと思います。 Re: 关于FEE初始化时间 こんにちは@Chenxu1 FEEドライバのドキュメントには初期化時間を計算するための公式は提供されていません。初期化時間は、保存されているデータ量、レコード数、クラスタの復旧やスワップが必要かどうかなど、FEEストレージの実際の状態によって異なります。初期化性能を向上させる主な構成パラメータはFeeDataBufferSizeであり、バッファが大きいほどFls_MainFunctionサイクルあたりより多くのデータを処理できます。詳細は「Please Fee ユーザーマニュアル」をご覧ください。より現実的な見積もりを行うには、初期化時間を、FEEを長時間使用し、複数回の書き込みサイクルを行った後の対象構成で測定する必要があります。 よろしくお願いいたします。 ルーカス Re: 关于FEE初始化时间 こんにちは、 現在、16バイトを書き込むと、次の初期化に2ミリ秒余計に時間がかかります。この時点では、ページ切り替えは発生せず、単に再初期化して16バイトを再度読み込むだけなので、2ミリ秒余計に時間がかかります。これは普通のことですか? Re: 关于FEE初始化时间 はい、この件についてはここで何度か議論されています。例えば: https://community.nxp.com/t5/S32K/S32K312-FEE-FLS-INIT-time/m-p/2024041 よろしくお願いいたします。 ルーカス
記事全体を表示
Assistance Required with SPI Communication on NBP8FD4ST1 Pressure Sensor Hi, I am using the NBP8FD4ST1 pressure sensor with the S32K146 microcontroller. The CS_B/WAKE-UP pin of the sensor is connected to a GPIO pin on the microcontroller. The logic analyzer signal mapping is as follows: D0 → SCLK D1 → CS_B D3 → READY D5 → MISO D7 → MOSI During the communication sequence, when I pull the CS_B pin low to request SPI communication, the READY pin is asserted as expected. After READY goes high, I send the SPIOPS register read command (0x00E1). However, the sensor always returns 0x0000 on MISO. As a result, the firmware validation fails, and the CS_B pin is subsequently driven high to terminate the transaction. Could you please help me understand whether my SPI communication sequence is correct or if I am missing any required step, such as the wake-up sequence, dummy transfer, or SPIOPS handling described in the datasheet? I have also attached the logic analyzer screenshots for reference. Thank you in advance for your support. Best regards, Pratyusha. Pratyusha_0-1783666219816.png Pressure Sensors Re: Assistance Required with SPI Communication on NBP8FD4ST1 Pressure Sensor Hi Pratyusha, Please note that NXP's MEMS Sensors business, including pressure sensors such as the NBP8FD4ST1, has been transferred to STMicroelectronics. Effective February 2, 2026, technical support, product documentation and development activities for these sensors are now handled by STM. As a result, we are unfortunately no longer able to provide technical support for the NBP8FD4ST1. I recommend that you contact STM directly through their support channels or community forum, where the sensor experts can assist you with your implementation and communication troubleshooting. BRs, Tomas Re: Assistance Required with SPI Communication on NBP8FD4ST1 Pressure Sensor from your chart D0 → SCLK, there is no clock signal when you read SPIOPS? Re: Assistance Required with SPI Communication on NBP8FD4ST1 Pressure Sensor @suncongjohnson Thanks for your reply. I have configured the SPI peripheral for 16-bit transfers, so I expect 16 SCLK pulses to be generated for each SPI transaction. However, when issuing the SPIOPS read command, no SCLK signal is generated on the D0 (SCLK) line. const lpspi_master_config_t lpspiCom1_MasterConfig0 = { .bitsPerSec = 1000000U, .whichPcs = LPSPI_PCS0, .pcsPolarity = LPSPI_ACTIVE_LOW, .isPcsContinuous = true, .bitcount = 16U, .lpspiSrcClk = 8000000U, .clkPhase = LPSPI_CLOCK_PHASE_1ST_EDGE, .clkPolarity = LPSPI_SCK_ACTIVE_HIGH, .lsbFirst = false, .transferType = LPSPI_USING_INTERRUPTS, .rxDMAChannel = 255, .txDMAChannel = 255, .callback = NULL, .callbackParam = NULL, };
記事全体を表示
如何将配置文件放入 S32DS 中进行版本、调试……项目 I just started with AUTOSAR and I have S32K144EVB I want to find instructions on how to use Tresos to generate config file and put it in S32DS for debug, build... Can anyone tell exactly where I should start from where? Re: How to put config file to S32DS for build, debug.... project 对于任何使用 S32DS 并试图正确设置版本和调试配置的人来说,这都是一个很有帮助的问题。查阅了一些相关资料(包括普特南法院判决书参考,引用)后,我发现配置步骤更容易遵循。关键似乎在于正确放置配置文件并确保项目设置指向该文件。如果能提供一个清晰的步骤示例,对于初学者来说就更容易理解了。 Re: How to put config file to S32DS for build, debug.... project 所得税的概念涉及对个人、公司、合伙企业和其他实体所赚取的收入进行评估和征税。 Re: How to put config file to S32DS for build, debug.... project 从现有项目文件生成新项目。构造 3. 调试是第五个。最终目的地。9……我们的 IDE 和开发环境 Eclipse 将开始加载。然后……转到“文件”>“新建”>“S32DS 应用程序项目”……导航到版本配置中的 (1) C/C++ 构建、(2) 设置和 (3) 目标处理器。 [[ ## completed ## ] Re: How to put config file to S32DS for build, debug.... project 从现有项目文件创建项目。3. 建筑物。5. 调试。6. 终端。9……它将开始加载我们将用于编写和测试代码的Eclipse环境和IDE。然后,它会……文件>新建>S32DS应用程序项目……在版本设置中,转到(1)C/C++版本,(2)设置,(3)目标处理器
記事全体を表示
How to put config file to S32DS for build, debug.... project I just started with AUTOSAR and I have S32K144EVB I want to find instructions on how to use Tresos to generate config file and put it in S32DS for debug, build... Can anyone tell exactly where I should start from where? Re: How to put config file to S32DS for build, debug.... project This is a helpful question for anyone working with S32DS and trying to get the build and debug setup right. I found the configuration steps easier to follow after checking a few related resources including Putnam Court Judgments for reference. The key seems to be placing the config file correctly and ensuring the project settings point to it. A clear step-by-step example would make this even easier for beginners to follow. Re: How to put config file to S32DS for build, debug.... project The concept of income tax involves the assessment and taxation of income earned by individuals to get help, corporations, partnerships, and other entities. Re: How to put config file to S32DS for build, debug.... project Generation of a new project from an existing project file. Construction 3. Debugging is the fifth. A final destination. 9 ... Our IDE and development environment, Eclipse, will begin to load. This will then... Go to File > New >S32DS Application Project... Navigate to (1) C/C++ Build, (2) Settings, and (3) Target Processor in the build's configuration. Re: How to put config file to S32DS for build, debug.... project Creating a project from existing project file. 3. Building. 5. Debugging. 6. Terminal. 9 ... It will begin to load the eclipse environment and IDE we will be using to write and test code. It will then ... File > New >S32DS Application Project ... In the build settings, go to (1) C/C++ Build, (2) Settings, (3) Target Processor
記事全体を表示
关于FEE初始化时间 Hi,NXP专家,我遇到一个S32K312 FEE初始化的时间想咨询一下,描述如下: 我配置了2个fee存储的clustergroup,一个主区,一个备区,备区是主区的备份,共配置了19个block,block同时存储在主区和备区中。软件版本Mcal RTD4.0.0 HF02,使能了Burst mode。 Chenxu1_0-1785460201957.png 测试方法: 上电时打印初始化时间(调用Mem_43_INFLS_Initt(),MemAcc_Initt(),Fee_Init()后等待Fee_GetStatus()接口返回MEMIF_IDLE),所有block写入一次数据 测试结果如下: 上电次数 初始化时间(ms) 说明 1 8 2 15 3 23 4 40 5 48 6 57 7 65 8 74 9 82 10 90 11 99 12 107 13 115 14 124 15 133 16 141 17 149 18 158 19 166 20 175 21 183 22 192 23 200 24 209 25 217 26 226 27 234 28 8 Cluster换页 根据以上实测发现每次递增的时间变化很快,所以想咨询一下有没有初始胡时间的计算公式、是否可以优化? Re: 关于FEE初始化时间 嗨@Chenxu1 FEE驱动程序文档中没有提供计算初始化时间的公式。初始化时间取决于 FEE 存储的实际状态,例如存储的数据量、记录数,以及是否需要任何集群恢复或交换。能够提高初始化性能的主要配置参数是 FeeDataBufferSize,因为更大的缓冲区允许每个 Fls_MainFunction 周期处理更多的数据。详情请参阅收费用户手册。为了进行实际的估计,应该在长时间使用 FEE 和多次写入周期后,在目标配置上测量初始化时间。 此致, Lukas Re: 关于FEE初始化时间 是的,这个问题之前已经讨论过好几次了。例如: https://community.nxp.com/t5/S32K/S32K312-FEE-FLS-INIT-time/m-p/2024041 此致, Lukas Re: 关于FEE初始化时间 你好, 目前,写入 16 字节会导致下次初始化时间延长 2 毫秒。此时不涉及页面切换——只是重新初始化并再次读取 16 个字节,这会增加 2 毫秒。这正常吗?
記事全体を表示
MX8-DSI-OLED1 Display part No and sequence. Hi Team, We are planning to use MX8-DSI-OLED1 accessory in our custom board as well. Could you please share the display part no and if there is any power sequence to be maintained. Re: MX8-DSI-OLED1 Display part No and sequence. Hi Team, Any updates on this? Re: MX8-DSI-OLED1 Display part No and sequence. Hello, Could you share what kind of information you are looking for? The display for the MX8-DSI-OLED1A (raydium rm67199) is a MIPI-DSI OLED display with touch support. Following are some key features: • 5.49" FHD (1080p@60fps) AMOLED display • 16.7 M (RGB*8bits) display color • Touch screen • 4-lane MIPI-DSI interface for display • I2C interface for touch and control Also, note that for this part there is not much information we can share. Best regards/Saludos, Aldo. Re: MX8-DSI-OLED1 Display part No and sequence. Hi @AldoG I would like to understand if there is any power up sequence to be followed for these rails. VDD_1V8 VEXT_3V3 VDD_5V
記事全体を表示
圧力センサのSPI通信に関する支援NBP8FD4ST1必要 こんにちは、 S32K146マイクロコントローラでNBP8FD4ST1圧力センサーを使っています。センサーの CS_B/WAKE-UP ピンはマイクロコントローラのGPIOピンに接続されています。 ロジックアナライザの信号マッピングは以下のとおりです。 D0 → SCLK D1 → CS_B D3 → 準備完了 D5 → MISO D7 → MOSI 通信シーケンス中に、 CS_BピンをローレベルにプルダウンしてSPI通信を要求すると、 READYピンは期待どおりにアサートされます。READYがハイになった後、 SPIOPSレジスタ読み取りコマンド(0x00E1)を送信します。しかし、MISOではセンサーは常に 0x0000 戻ってしまいます。その結果、ファームウェアの検証が失敗し、CS_Bピンがハイレベルに駆動されてトランザクションが終了します。 私のSPI通信シーケンスが正しいのか、それともデータシートに記載されているウェイクアップシーケンス、ダミー転送、SPIOPS処理など、必要なステップを見落としているのか教えていただけますか? 参考までに、ロジックアナライザのスクリーンショットも添付しました。 サポートにあらかじめ感謝いたします。 よろしくお願いします、 プラチューシャ。 Pratyusha_0-1783666219816.png 圧力センサ Re: Assistance Required with SPI Communication on NBP8FD4ST1 Pressure Sensor こんにちは、プラティウシャさん。 なお、NXPのMEMSセンサ事業、NBP8FD4ST1などの圧力センサはSTMicroelectronicsに移管されました。2026年2月2日付で、これらのセンサの技術サポート、製品ドキュメント、開発活動はSTMが担当しています。その結果、残念ながらNBP8FD4ST1の技術サポートは提供できません。 サポートチャネルやコミュニティフォーラムを通じて直接STMに連絡することをお勧めします。センサの専門家が実装やコミュニケーションのトラブルシューティングをサポートいたします。 BRs、トーマス Re: Assistance Required with SPI Communication on NBP8FD4ST1 Pressure Sensor あなたのチャートのD0→SCLKから、SPIOPSを読み取る際にクロック信号がないということでしょうか? Re: Assistance Required with SPI Communication on NBP8FD4ST1 Pressure Sensor @suncongjohnsonご返信ありがとうございます。SPIペリフェラルは16ビット転送に設定しているので、SPIトランザクションごとに16回のSCLKパルスが生成されると予想しています。しかし、SPIOPSの読み取りコマンドを発行しても、D0(SCLK)ラインにはSCLK信号が生成されません。 const lpspi_master_config_t lpspiCom1_MasterConfig0 = { .bitsPerSec= 1000000U、 .whichPcs= LPSPI_PCS0、 .pcs極性= LPSPI_ACTIVE_LOW、 .isPcsContinuous= 真、 .bitcount= 16U、 .lpspiSrcClk= 8000000U、 .clkPhase= LPSPI_CLOCK_PHASE_1ST_EDGE、 .clkPolarity= LPSPI_SCK_ACTIVE_HIGH、 .lsbFirst= 偽、 .transferType= LPSPI_USING_INTERRUPTS、 .rxDMAChannel= 255、 .txDMAChannel= 255、 。折り返し電話= NULL、 .callbackParam= NULL、 };
記事全体を表示
i.MXRT685S:通过 HS SPI 总线从外部闪存启动 我有一个外部 SPI 或非 闪存设备,通过 HS SPI 总线接口(Flexcomm 14)连接到 RT685s。我想从这个闪存设备启动;但是,我了解到只有 FlexSPI 启动、SD 启动和 eMMC 启动这三种主启动选项。是否可以使用高速 SPI 总线(Flexcomm 14)从该外部闪存启动?如果是这样,我需要遵循哪些要求/设置步骤才能执行此操作? Re: i.MXRT685S: Boot from external flash via HS SPI bus 以下是一些关于NOR启动的应用笔记,供您参考。 AN12751 如何从 QSPI Flash 启用恢复启动 AN12773 如何从串行 或非 Flash 启用主启动 Re: i.MXRT685S: Boot from external flash via HS SPI bus 嗨@lgibarra9 , 使用 FC14 的高速 SPI 总线无法从外部 SPI 或非 Flash 启动。除了运行时 SPI 通信外,该总线还可以在 MCU 处于 ISP 模式时下载图像。但是,对于从外部闪存进行正常启动操作而言,高速 SPI 总线不是一个选项,因此您的 SPI NOR 闪存应该连接到 FlexSPI 总线。 BR, 埃德温。
記事全体を表示
ビルド、デバッグ、プロジェクトのためにS32DSに設定ファイルを配置する方法 I just started with AUTOSAR and I have S32K144EVB I want to find instructions on how to use Tresos to generate config file and put it in S32DS for debug, build... Can anyone tell exactly where I should start from where? Re: How to put config file to S32DS for build, debug.... project これは、S32DS を扱っていて、ビルドとデバッグの設定を正しく行おうとしている人にとって、非常に役立つ質問です。参考資料としてパットナム裁判判例集などいくつかの関連資料を確認したところ、設定手順がより分かりやすくなった。重要なのは、設定ファイルを正しい場所に配置し、プロジェクト設定がそのファイルを指していることを確認することのようです。明確な手順を示す例があれば、初心者でもさらに理解しやすくなるでしょう。 Re: How to put config file to S32DS for build, debug.... project 所得税の概念は、個人、法人、パートナーシップ、その他の事業体が得た所得を評価し、課税することを含みます。 Re: How to put config file to S32DS for build, debug.... project 既存のプロジェクトファイルから新しいプロジェクトを生成する。構築 3. デバッグは 5 番目です。最終目的地。9 ...私たちのIDEsと開発環境であるEclipseが読み込みを開始します。これ なら...新しい>S32DSアプリケーションプロジェクト>ファイルへ移動...ビルドの設定で(1) C/C++ビルド、(2) 設定、(3) ターゲットプロセッサへ移動します。 Re: How to put config file to S32DS for build, debug.... project 既存のプロジェクトファイルから新しいプロジェクトを作成します。3. ビルディング。5. デバッグ。6. ターミナル。9 ...Eclipse環境とIDEの読み込みが始まり、コードを書 いたりテストしたりします。そうすれば...ファイル>新>S32DSアプリケーションプロジェクト...ビルド設定で、(1) C/C++ビルド、(2) 設定、(3) ターゲットプロセッサに進みます
記事全体を表示
RW612 - PM4 电流异常。 专家们好 我们最近在一些量产产品中使用了 u-blox W10 模块。不过,我们发现不同模块的 PM4 电流消耗量差别很大,从约 300 µA 到 1 mA 不等。 为了进一步调查,我使用两个 FRDM-RW612 开发套件进行了测试,没有进行任何返工或修改,并使用恩智浦 SDK v25.6.0 中的电源管理器测试(裸机)示例应用程序对两个套件进行了编程。 在 DK1 上,通过 JP9 测量电流,PM4 的电流消耗约为 400 µA,符合预期。 在 DK2 上,在完全相同的测试条件下,PM4 的电流消耗约为 1 mA。我重复了 120 次测试,结果始终如一。 有趣的是,当我给 DK2 吹热风时,PM4 电流下降到 ~400 µA(正常值)。但冷却几分钟后,电流又回升到 ~1 mA。再次注入热空气会使电流暂时回落。 请问我该如何分析这个问题?我使用的是官方开发工具包和未修改的示例代码,可以可靠地重现该问题。 Re: RW612 - PM4 current is abnormal. 嗨,丹尼尔 这款 K.O. 板上的黄色电缆用于测量 VPA 的电流,电阻为 0 欧姆 (R218)。 WeiliWang_0-1758787079290.png 此外,我还发送了一条私人信息。 你能检查一下吗? Re: RW612 - PM4 current is abnormal. 您好, 我使用 2 个 FRDM-RW612 板测试了 25.09 SDK 的电源管理器测试。 尽管如此,我还是得到了预期的结果。 DanielRuvalcaba_4-1758773852825.png 测量在 JP9 上进行。 你能告诉我你的 KO FRDM 板上的电缆是干什么用的? 此致, 丹尼尔 Re: RW612 - PM4 current is abnormal. 嗨,丹尼尔 用于测量 VPA 电流的 K.O. 板黄色电缆。 我去掉了用于测量 VPA 电流的 R218 WeiliWang_0-1758687668677.png Re: RW612 - PM4 current is abnormal. 您好, 抱歉耽搁了。 目前我还没有办法测量电流消耗,但明天应该可以做到。请给我一些时间来收集测量数据。 顺便问一下,您能告诉我 KO FRDM 中的电缆是做什么用的吗? 此致, 丹尼尔 Re: RW612 - PM4 current is abnormal. 嗨,丹尼尔 下面是另一个更新: 我们使用了 uBlox IRIS-W106-30B 模块。 我们打开屏蔽罩,测量了 ublox IRIS-W106-30B 模块在特定测试条件下的漏电流情况(K.O.情况)。我们发现 VPA 处的漏电流为 657 微安。 因此,根据实验结果,FRDM612 和 ublox IRIS-W106-30B 的漏电流源似乎是从 VPA 吸收的电流。 Re: RW612 - PM4 current is abnormal. 嗨,丹尼尔 我的 FRDM 照片如下: WeiliWang_0-1758328990924.png WeiliWang_1-1758329028621.png WeiliWang_2-1758329081576.png WeiliWang_3-1758329134480.png Re: RW612 - PM4 current is abnormal. 您好, 您能分享一下 FRDM 的照片吗? 我们正在检查。请给我一些时间,等我有了最新进展再与大家分享。 此致, 丹尼尔 Re: RW612 - PM4 current is abnormal. 嗨,丹尼尔 我已经确定了 700µA"间隙电流" ;测量结果显示,该电流来自 VPA 引脚。这个问题可以通过软件更新或补丁解决吗?我们已经从 U-blox 购买了 1560 台设备,我们的客户即将在六个不同的国家进行射频认证。我想知道这个问题能否得到解决。 有可能用补丁解决这个问题吗? WeiliWang_0-1758251280118.png Re: RW612 - PM4 current is abnormal. 嗨,丹尼尔 我还测试了 PM3 模式 对于 PM3 模式。 FRDM612 都是一样的。 PM3 的电流消耗约为 0.96mA 然而,当进入 PM4 模式时,有问题的 FRDM612 将变为 1.19mA,而正常 FRDM 约为 0.47mA Re: RW612 - PM4 current is abnormal. 嗨,丹尼尔 对不起,JP9:474mA 应更正为 474uA,而不是 mA。 此外,我还查看了 JP9 之后的电源树,除了 JP7 和 JP5。 如果我想进一步分析,是否可以只测量 R218 和 R196 来确定功耗源?测量这两条路径的功率树对您有帮助吗? 我已在附件中上传了 FRDM612 原理图。 FRDM-RW612-SCH.pdf WeiliWang_0-1758180854622.png Re: RW612 - PM4 current is abnormal. 你好、 感谢您提供如此详细的信息。我只想确定我完全理解了你的设置。 我这边需要做一些测试。 同时,请确认这是否是错字:" 这意味着我的漏电流约为 800mA "。这些不是800uA 吗? 您还提到"在 DK1 上,通过 JP9 测量电流,PM4 的电流消耗约为400 µA,符合预期。" 。但您还提到"FRDM1(正常情况下),JP9:474mA,JP5:21uA,JP7:444uA。" 。JP9 上的测量值是 474uA 而不是 474mA? 此致, 丹尼尔 Re: RW612 - PM4 current is abnormal. 嗨,丹尼尔 你的理解非常正确。 我研究过 AN14464。 我用三个电流表测量了 JP9、JP5 和 JP7。 结果如下 FRDM1(正常情况下) JP9:474mA JP5:21uA JP7:444uA。 FRDM2(K.O 外壳) JP9:1.26mAJP5:21uA JP7:448uA. 在 K.O. 的案例中,我注意到 JP9 消耗了 1.26mA 电流,但 JP5 和 JP7 加起来消耗了 469uA 电流。这意味着我有大约800mA的漏电流来自JP9节点下方的某个地方。 您有什么建议可以让我尝试排除故障吗? 我们使用的是 Ublox W10,也遇到了这个问题。 我们已经进行了一些小规模生产。 413 模块的电流消耗在 300 至 500uA 之间。 70 个模块的电流消耗在 501 至 800uA 之间。 32 个模块的电流消耗在 801 至 900uA 之间。 15 个模块的电流消耗在 901 至 1050uA 之间。 Re: RW612 - PM4 current is abnormal. 您好, 能否请您帮我确认以下内容? 您在两个 FRDM 板上使用相同的示例进行了相同的测试。 FRDM 1 显示电流消耗正常,甚至在热空气作用下也是如此。 在正常情况下,FRDM 2 比 FRDM 1 多消耗约 1 mA 电流,但当使用热空气时,其电流消耗会下降到与 FRDM 1 相当。 我的理解正确吗? 作为参考,我建议看看 AN14464。 致: Daniel Re: RW612 - PM4 current is abnormal. 这个问题最终解决了吗? 我在基于 RW612 的模块上也看到了类似的情况。在 PM3 中,VDD 总电流消耗为 318 µA,而在 PM4 中,VDD 总电流消耗增加到 425 µA。我直接测量了VPA电流,发现PM3中的VPA电流为877 nA,而PM4中的VPA电流为330 µA。
記事全体を表示
MX8-DSI-OLED1 ディスプレイの部品番号とシーケンス。 こんにちは、チームのみなさん。 カスタムボードにはMX8-DSI-OLED1アクセサリーも使用する予定です。 ディスプレイの部品番号と、維持すべき電源順序があれば教えていただけますか? Re: MX8-DSI-OLED1 Display part No and sequence. こんにちは、 どのような情報をお探しですか? MX8-DSI-OLED1A(raydium rm67199)のディスプレイは、タッチ対応のMIPI-DSI OLEDディスプレイです。以下は主な特徴です: • 5.49インチFHD(1080p@60fps)AMOLEDディスプレイ • 16.7 M(RGB*8ビット)表示色 ・タッチスクリーン • 表示用の4レーンMIPI-DSIインターフェース ・タッチおよび制御のためのI2Cインターフェース また、この部分については共有できる情報があまり多くないことにご注意ください。 よろしくお願いいたします。 アルド。 Re: MX8-DSI-OLED1 Display part No and sequence. チームの皆さん、こんにちは。 この件について何か進展はありますか? Re: MX8-DSI-OLED1 Display part No and sequence. こんにちは、 @AldoGさん これらのレールに電源を入れる際の順序があるかどうかを知りたいです。 VDD_1V8 VEXT_3V3 VDD_5V
記事全体を表示
i.MXRT685S: HS SPIバス経由で外部フラッシュからブート 私はRT685sのHS SPIバスインターフェース(Flexcomm 14)に接続した外部SPI NORフラッシュデバイスを使っています。このフラッシュデバイスから起動したいのですが、マスターブートのオプションはFlexSPIブート、SDブート、eMMCブートしかないと読みました。高速SPIバス(Flexcomm 14)を使用して、この外部フラッシュメモリから起動することは可能ですか?もしSOなら、実行するためにどのような要件やセットアップ手順に従うべきでしょうか? Re: i.MXRT685S: Boot from external flash via HS SPI bus 以下はNORブート用の参考となるアプリケーションノートです AN12751 QSPIフラッシュからのリカバリブートを有効にする方法 AN12773 シリアルNORフラッシュからのマスターブートを有効にする方法 Re: i.MXRT685S: Boot from external flash via HS SPI bus こんにちは、@lgibarra9 さん。 FC14の高速SPIバスを使用して、外部SPI NORフラッシュからブートすることはできません。このバスは(実行時SPI通信以外にも)MCUがISPモードの際にイメージをダウンロードするために使用できます。しかし、外部フラッシュからの通常の起動動作では高速SPIバスは使えないため、SPI NORフラッシュはFlexSPIバスにコネクテッドすべきです。 BR、 エドウィン。
記事全体を表示
S32K311 LCUの立ち上がり/立ち下がりフィルタのデッドタイムが、2µsから1µsに短縮されることがあります。 こんにちは、NXP チームの皆様、 私はRTD 5.0を搭載したS32K311を使用しています。 PWM信号はeMIOS0によって生成され、 LCU0の出力に直接送られます。 eMIOS0_CH0 -> LCU0_OUT0 eMIOS0_CH1 -> LCU0_OUT1 eMIOS0_CH2 -> LCU0_OUT2 eMIOS0_CH3 -> LCU0_OUT3 eMIOS0_CH4 -> LCU0_OUT4 eMIOS0_CH5 -> LCU0_OUT5   LCUは、立ち上がり/立ち下がりフィルタを使用してデッドタイムを挿入するように構成されています。   設定 MCU:S32K311 RTDバージョン:5.0 PWMソース: eMIOS0 デッドタイム生成:LCU上昇/下降フィルタ ハイサイドチャネルのライズフィルター = 192 ローサイドチャネルのフォールフィルター = 192 設定デッドタイム = 2 µs 観察された行動 ほとんどのスイッチングイベントは、予想 される2μsのデッドタイムを生み出します。 しかし、時折、一方の遷移(立ち上がりエッジまたは立ち下がりエッジ)のデッドタイムが、2 µs ではなく約1 µsしかない場合があります。これは、PWM周波数とデューティサイクルが変化しない状態で断続的に発生します。 添付のロジックアナライザのキャプチャ画像に、この動作が示されています。 質問 LCUの上昇/下降フィルターを使用した場合、このような変動は想定されるものですか? eMIOSの出力とLCUフィルタの間には、同期に関する要件はありますか? LCUフィルターは内部同期やクロックドメイン交差によってプログラム遅延を時折短縮することはありますか? S32K311の立ち上がり/立ち下がりフィルタに関して、既知の制限事項や不具合はありますか? 何かアドバイスをいただければ幸いです。 よろしくお願いします。 Re: S32K311 LCU Rise/Fall Filter Deadtime Occasionally Reduced from 2 µs to 1 µs こんにちは、 Esakkiさん。 1. あなたの値 192 = 2 µs  LCUフィルターのティック値は約: 2us / 192 = 10.4167 ns -> 1/ 10.4167 ns = 96MHz、 有効なLCU/周辺クロックやプリスケーラが変化したり、想定と異なるクロックが選択された場合、実際の遅延は変わります。 2. オシロスコープを用いてテストする方が正確で、波形は外部静電容量リアクタンスに関連しています。大きな静電容量リアクタンスも波形の不安定性を引き起こすことがあります。
記事全体を表示
RW612 - PM4電流が異常です。 こんにちは、エキスパートの皆さん。 当社では最近、一部の量産製品に u-blox W10 モジュールを採用しています。ただし、PM4 の電流消費量はモジュールごとに大きく異なり、約 300 µA から最大 1 mA の範囲であることがわかりました。 さらに調査するために、手直しや変更を加えずに 2 つの FRDM-RW612 開発キットでテストし、両方を NXP SDKs v25.6.0 の Power Manager Test (ベアメタル) サンプル アプリケーションでプログラムしました。 DK1 で JP9 を介して電流を測定すると、PM4 の電流消費量は約 400 µA であり、これは予想どおりです。 DK2 では、まったく同じテスト条件下で、PM4 の電流消費量は約 1 mA です。このテストを 120 回繰り返しましたが、結果は常に同じでした。 興味深いことに、DK2 に熱風を当てると、PM4 の電流が約 400 µA (正常値) に低下しました。しかし、数分間冷却すると、電流は再び約 1 mA まで上昇しました。再び熱風を当てると、電流は一時的に低下します。 この問題をどのように分析すればよいかアドバイスをいただけませんか?公式開発キットと変更されていないサンプルコードを使用しており、問題を確実に再現CANます。 Re: RW612 - PM4 current is abnormal. こんにちは、ダニエル。 この KO ボード上の黄色のケーブルは、0 オームの抵抗 (R218) を持つ VPA の電流を測定するために使用されます。 WeiliWang_0-1758787079290.png また、プライベートメッセージも送りました。 確認していただけますか? Re: RW612 - PM4 current is abnormal. こんにちは、 2 つの FRDM-RW612 ボードを使用して、25.09 SDK で電源マネージャ テストをテストしました。 それでも、どちらも期待通りの結果が得られました。 DanielRuvalcaba_4-1758773852825.png 測定はJP9で行います。 KO FRDM ボード内のケーブルの用途を教えてください。 よろしくお願いいたします。 ダニエル。 Re: RW612 - PM4 current is abnormal. こんにちは、ダニエル。 VPA 電流を測定するための KO ボードの黄色いケーブル。 VPA電流を測定するためにR218を取り外しました WeiliWang_0-1758687668677.png Re: RW612 - PM4 current is abnormal. こんにちは、 遅れてごめんなさい。 現時点では電流消費量を測定する方法がありませんが、明日には測定できるようになるはずです。測定値を収集するのに少し時間をください。 ところで、KO FRDM 内のケーブルの用途を教えていただけますか? よろしくお願いいたします。 ダニエル。 Re: RW612 - PM4 current is abnormal. こんにちは、ダニエル。 もう一つのアップデートは次のとおりです: uBlox IRIS-W106-30Bモジュールを使用しました。 シールドカバーを開けて、特定のテスト条件(KO)でublox IRIS-W106-30Bモジュールの電流漏れを測定しました。CASE)。VPA で 657 µA の電流漏れを発見しました。 したがって、実験結果に基づくと、FRDM612 と ublox IRIS-W106-30B の両方における漏れ電流の発生源は、VPA から引き出される電流であると考えられます。 Re: RW612 - PM4 current is abnormal. こんにちは、ダニエル。 私のFRDMの写真は以下の通りです。 WeiliWang_0-1758328990924.png WeiliWang_1-1758329028621.png WeiliWang_2-1758329081576.png WeiliWang_3-1758329134480.png Re: RW612 - PM4 current is abnormal. こんにちは、 FRDM の写真を共有していただけますか? これを確認中です。更新情報を共有するまで、しばらくお待ちください。 よろしくお願いいたします。 ダニエル。 Re: RW612 - PM4 current is abnormal. こんにちは、ダニエル。 700µA の「ギャップ電流」を特定しました。測定結果から、この電流は VPA ピンから引き出されていることがわかっています。この問題はソフトウェアのアップデートやパッチで解決CANものなのでしょうか?当社はすでに U-blox から 1560 台を購入しており、顧客は 6 か国で RF 認証を受ける予定です。この問題が解決CANかどうかを知る必要があります。 パッチを使用してこの問題を解決することは可能ですか? WeiliWang_0-1758251280118.png Re: RW612 - PM4 current is abnormal. こんにちは、ダニエル。 PM3モードも試してみました PM3モード用。 FRDM612は両方とも同じです。 PM3の消費電流は約0.96mA しかし、PM4モードに入ると、問題のあるFRDM612は1.19mAになりますが、通常のFRDMは約0.47mAです。 Re: RW612 - PM4 current is abnormal. こんにちは、ダニエル。 申し訳ありませんが、JP9: 474mA は mA ではなく 474uA に修正する必要があります。 また、JP7とJP5を除く、JP9以降のパワーツリーも調べました。 これをさらに分析したい場合、電力消費源を特定するために R218 と R196 のみを測定することはCANますか?これら 2 つのパスの電力ツリーを測定すると役立ちますか? FRDM612 の回路図を添付ファイルにアップロードしました。 FRDM-RW612-SCH.pdf WeiliWang_0-1758180854622.png Re: RW612 - PM4 current is abnormal. こんにちは、 詳しい情報をありがとうございます。私はあなたの設定を完全に理解していることを確認したいだけです。 私の側でいくつかテストを行う必要があります。 一方、これがタイプミスであるかどうかを確認してください:「これは、約800mAの漏れがあることを意味します。」これらは800uAではないですか? また、「 DK1 では、JP9 を通じて電流を測定すると、PM4 の電流消費は約400 µAで、予想どおりです。」とも述べられています。しかし、「 FRDM1(OK CASE) JP9:474mA JP5:21uA JP7:444uA 」とも言及されています。JP9 の測定値は 474mA ではなく 474uA ですか? よろしくお願いいたします。 ダニエル。 Re: RW612 - PM4 current is abnormal. こんにちは、ダニエル。 あなたの理解は非常に正しいです。 AN14464を勉強しました。 JP9、JP5、JP7を測定するために3つの電流計を使用しました。 結果は次のとおりです。 FRDM1(正常CASE) JP9:474mA JP5:21uA JP7:444uA。 FRDM2(KO CASE)JP9:1.26mAJP5:21uA JP7:448uA。 KO の CASE、JP9 の消費電流は 1.26mA でしたが、JP5 と JP7 を合わせると 469uA でした。これは、JP9 ノードの下のどこかから約 800mA の漏れが発生していることを意味します。 トラブルシューティングのために試すことができる提案はありますか? Ublox W10 を使用していますが、この問題が発生しています。 小規模な生産も行いました。 413 モジュールの電流消費量は 300 ~ 500 uA です。 70 個のモジュールの電流消費量は 501 ~ 800 uA です。 32 個のモジュールの電流消費量は 801 ~ 900 uA です。 15 個のモジュールの電流消費量は 901 ~ 1050 uA です。 Re: RW612 - PM4 current is abnormal. こんにちは、 以下の点について確認させていただけますでしょうか? 2 つの FRDM ボードで同じ例を使用して同じテストを実行しました。 FRDM 1 熱風を当てても正常な電流消費を示します。 FRDM2 通常の状態では FRDM 1 よりも約 1 mA 多く消費しますが、熱風を当てると消費電流が FRDM 1 と同程度まで低下します。 私の理解は正しいでしょうか? 参考までに、AN14464 をご覧になることをお勧めします。 よろしくお願いいたします。 ダニエル Re: RW612 - PM4 current is abnormal. この問題は解決されたのでしょうか? RW612ベースのモジュールでも同様の挙動が見られます。PM3では、VDDの総消費電流は318µAですが、PM4では425µAに増加します。私はVPA電流を直接測定し、PM3では877 nA、PM4では330 µAという値を確認した。
記事全体を表示
S32K311 LCU 上升/下降滤波器死区时间偶尔会从 2 µs 缩短至 1 µs 您好,NXP团队: 我正在使用带有RTD 5.0的S32K311 。 PWM信号由eMIOS0生成,并直接路由至LCU0输出端: eMIOS0_CH0 -> LCU0_OUT0 eMIOS0_CH1 -> LCU0_OUT1 eMIOS0_CH2 -> LCU0_OUT2 eMIOS0_CH3 -> LCU0_OUT3 eMIOS0_CH4 -> LCU0_OUT4 eMIOS0_CH5 -> LCU0_OUT5   LCU 配置为使用上升/下降滤波器插入死区时间。   配置 MCU:S32K311 RTD 版本:5.0 PWM源:eMIOS0 死区生成:LCU 上升/下降滤波器 高侧通道上升滤波器 = 192 低侧通道的跌落滤波器 = 192 配置的死区时间 = 2 微秒 观察到的行为 大多数切换事件都会产生预期的2 µs 死区时间。 然而,偶尔会出现一个转换(上升沿或下降沿)只有大约1 µs死区时间,而不是 2 µs。这种情况会间歇性地发生,而 PWM 频率和占空比保持不变。 附件中的逻辑分析仪捕获图像显示了这种现象。 问题 使用 LCU 上升/下降滤波器时,这种变化是否正常? eMIOS 输出和 LCU 滤波器之间是否存在同步要求? LCU滤波器是否会因内部同步或时钟功能域交叉而偶尔缩短编程延迟? S32K311 的上升/下降滤波器是否存在任何已知的限制或错误? 任何指导都将不胜感激。 谢谢! Re: S32K311 LCU Rise/Fall Filter Deadtime Occasionally Reduced from 2 µs to 1 µs 您好@Esakki 1. 您的值 192 = 2 µs  这意味着 LCU 滤波器的滴答时间约为: 2微秒 / 192 = 10.4167 ns -> 1/ 10.4167 ns = 96MHz, 如果有效的 LCU/外设时钟或预分频器发生变化,或者选择的时钟与假定的时钟不同,则实际延迟会发生变化。 2.使用示波器进行测试更加准确,波形与外部容抗有关;较大的容抗也会导致波形不稳定。
記事全体を表示
MX8-DSI-OLED1 显示屏部件号和序列号。 大家好, 我们也计划在我们的定制板中使用 MX8-DSI-OLED1 配件。 请问能否提供一下显示屏的零件编号,以及是否有任何需要保持的电源顺序? Re: MX8-DSI-OLED1 Display part No and sequence. 你好, 您能告诉我您想了解哪方面的信息吗? MX8-DSI-OLED1A(raydium rm67199)的显示屏是支持触摸的 MIPI-DSI OLED 显示屏。以下是一些主要特点: • 5.49 英寸 FHD (1080p@60fps) AMOLED 显示屏 • 1670万色(RGB*8位)显示颜色 • 触摸屏 • 用于显示器的 4 通道 MIPI-DSI 接口 • 用于触摸和控制的 I2C 接口 另外,请注意,关于这部分内容,我们能分享的信息不多。 此致敬礼/Saludos, 阿尔多。 Re: MX8-DSI-OLED1 Display part No and sequence. 大家好, 这件事有任何进展吗? Re: MX8-DSI-OLED1 Display part No and sequence. 嗨@AldoG 我想了解这些轨道上电是否有任何需要遵循的顺序。 VDD_1V8 VEXT_3V3 VDD_5V
記事全体を表示
Eat-Sleep-Code-Repeat: Automotive Control Systems Using FRDM-A-S32K3XX Microcontrollers 1. Overview This article is the umbrella entry point for a series of automotive embedded workshops built on the FRDM-A-S32K3xx microcontroller family. It groups together five hands-on modules — Lights, Brakes, Steering, Comfort, and Transmission — each demonstrating a different real-world automotive function that a modern Body Control Module (BCM), Chassis ECU, or Powertrain ECU would implement in production vehicles. All five modules share the same educational philosophy: they take a simple, low-risk hardware setup (FRDM board + FRDM-K64 Click Shield + a few MikroE Click modules) and use it to teach the core embedded concepts that underlie automotive software: analog and digital signal acquisition, real-time processing, actuator control, and safety-aware system design. Together they cover the most common peripherals of the S32K3 family — ADC, GPIO, PWM, FlexIO, LPI2C, eMIOS — and expose students to the same tool-chain used by NXP customers: S32 Design Studio 3.6.5, the S32K3 Real-Time Drivers (RTD), the Application Code Hub (ACH), and the underlying Automotive Software Package. Learning philosophy — Eat-Sleep-Code-Repeat The whole workshop series is designed around the Eat-Sleep-Code-Repeat initiative — a learn-by-doing culture where students continuously iterate on real hardware, break things, fix them, refactor, and re-flash until the concepts stick. Every module is small enough to be completed in one lab session, yet rich enough to leave room for extensions (state machines, filtering, CAN networking, closed-loop control, safety fall-backs). Concepts covered across the series Analog sensing: potentiometers, force sensors, resistor-ladder buttons → ADC conversion, scaling, debouncing. Digital I/O: GPIO input handling (buttons, switches), GPIO output sequencing (stepper coils). Actuation: PWM-based motor speed control (DC motors, fans), PWM-based servo positioning, WS2812 LED driving through FlexIO. Communication: I²C configuration of external PWM drivers (Servo Click / PCA9685). Control patterns: continuous mapping, threshold-based decisions, state machines, safety interlocks. Automotive concepts: Body Control Module (BCM) behavior, functional safety (ISO 26262), fail-safe defaults, redundancy considerations. What this article gives you Each of the next five sections provides a short summary of one module — what it demonstrates, which hardware it uses, which peripherals are involved, and a direct link to the full detailed workshop article. Students should read this page first to understand where each module fits in the bigger picture, then dive into the individual articles for step-by-step instructions. 2. Vehicle Lighting Control The Lights module implements a simplified automotive lighting system that mirrors the behavior of a real vehicle Body Control Module. Six buttons on the Analog Key Click command different lighting functions — low beam, high beam, left/right turn signals, brake lights, and hazard lights — all displayed in real time on a 16-LED 4x4 RGB Click matrix. Key learning points Multi-button decoding on a single ADC channel (resistor-ladder input). Software debouncing and command decoding. Driving WS2812 LEDs through FlexIO (precise sub-microsecond timing without CPU load). BCM safety interlocks: high beam requires low beam ON; hazards synchronize left + right turn signals; high beam state preserved between blink cycles. Peripherals used: ADC0, FlexIO, GPIO. Boards: FRDM-A-S32K312 or FRDM-A-S32K344. Reference project:Automotive Lighting Control Using FRDM-A-S32K3XX Microcontrollers - NXP Community lighting_k344_gif.gif Demo: Vehicle Lighting Control on FRDM-A-S32K344 Automotive relevance: lighting is one of the most safety-critical driver-visibility functions in modern vehicles — this module teaches how a real BCM manages dependencies, blinking patterns, and fail-safe defaults. 3. Brake Status Monitoring The Brakes module implements a simplified brake status monitoring system where a Force Click sensor simulates the driver's brake-pedal pressure. As pressure increases, the ADC value grows and the application progressively lights up the 4x4 RGB Click LEDs in green → yellow → orange → red, providing immediate visual feedback of the current braking level. Key learning points Continuous analog sensor acquisition through ADC. Threshold-based decision logic: converting a raw ADC value into discrete alert levels. Driving the RGB LED matrix through FlexIO to reflect the current system state. Introduction to real-time monitoring and safety-oriented visual feedback. Peripherals used: ADC0, FlexIO. Boards: FRDM-A-S32K312 or FRDM-A-S32K344. Reference project: Automotive Brake Control Using FRDM-A-S32K3XX Microcontrollers - NXP Community brakes_k344_gif.gif Demo: Brake Status Monitoring on FRDM-A-S32K344 Automotive relevance: brake status is a core input for many downstream ECUs (ABS, ESC, hill-hold, brake lights). This module teaches the fundamental pattern of sensor → threshold → visual/electrical output that appears everywhere in automotive software. 4. Assisted Steering Control The Steering module demonstrates a simplified Electric Power Steering (EPS) / steer-by-wire concept. A POT Click potentiometer simulates the steering-wheel angle; the MCU reads it through ADC, scales it linearly, and generates a PWM command through the Servo Click (configured over I²C) that positions a Micro Servo SG 180° in real time. Key learning points Analog input scaling and linear mapping (ADC range → servo angle range). Using an external PWM controller configured over I²C (LPI2C1) — a common embedded pattern that offloads timing-critical work. Working with the Output Enable (OE) pin for safe-stop behavior. Understanding the actuation chain sensor → MCU → PWM → actuator. Peripherals used: ADC0, LPI2C1, GPIO. Boards: FRDM-A-S32K312 or FRDM-A-S32K344. Reference projects: Automotive Steering Control Using FRDM-A-S32K3XX Microcontrollers - NXP Community steering_k344_gif.gif Demo: PWM-Based Steering Control on FRDM-A-S32K344 Automotive relevance: steering is a strictly safety-relevant function (ISO 26262 typically classifies it as ASIL C or D). This module introduces the concepts behind EPS and steer-by-wire and lays the foundation for future work with redundant sensors and fault detection. 5. Vehicle Comfort Control The Comfort module implements two independent comfort functions typical of vehicle body electronics: cabin cooling (a 5 V fan driven through a DC Motor 2 Click using PWM) and electric window control (a NEMA17 stepper motor driven through an H-Bridge Click using full-step GPIO sequencing). On-board push-buttons act as the driver's HVAC and window switches. Key learning points PWM motor speed control (fan simulation). Stepper motor full-step sequencing (A → B → C → D and reverse) through four GPIO outputs. Handling multiple independent actuators from a single MCU without blocking. Introduction to window anti-pinch and other real BCM safety concepts. Peripherals used: GPIO, eMIOS (PWM). Boards: FRDM-A-S32K344 (only). Reference project: Automotive Comfort Control Using FRDM-A-S32K344 Microcontrollers - NXP Community comfort_k344_gif.gif Demo: Vehicle Comfort Control on FRDM-A-S32K344 Automotive relevance: comfort systems (HVAC, windows, mirrors, seats) form a huge share of modern body electronics. This module shows how one ECU can coordinate multiple actuators of different types (rotational-speed and positional) using the same S32K3 platform. 6. Transmission Control The Transmission module demonstrates a continuous, proportional transmission control concept. A POT Click potentiometer represents the driver's acceleration command; the MCU samples it, applies linear scaling, and simultaneously drives two actuators: a Servo Click + Micro Servo that simulates the transmission selector position, and a DC Motor 2 Click + DC motor whose speed reflects the powertrain response. Key learning points Dual-actuator control from a single analog input (one MCU commands both servo angle and DC motor speed in parallel). Linear signal mapping to two different PWM ranges simultaneously. Combining I²C-configured PWM (Servo Click) and eMIOS-generated PWM (DC Motor 2 Click) in the same application. Understanding continuous vs. discrete control and how continuous mapping better mirrors real automotive behavior. Peripherals used: ADC0, LPI2C1, eMIOS. Boards: FRDM-A-S32K344 (only). Reference project: Automotive Transmission Control Using FRDM-A-S32K344 Microcontrollers - NXP Community transmission_k344_gif.gif Demo: Transmission Control on FRDM-A-S32K344 Automotive relevance: transmission control is part of the powertrain domain and requires deterministic response and safety-aware design. This module introduces the concepts and prepares students for more advanced topics such as closed-loop control, transmission-mode logic (P/R/N/D), and CAN networking with the engine ECU. 7. Conclusion Together, these five modules give students a complete tour of what a modern Body Control Module, Chassis ECU, and Powertrain ECU actually do in a vehicle — from reading sensors and buttons, through processing and safety interlocks, to driving lights, motors, and actuators. Each module can be studied independently, but the real value emerges when they are viewed as pieces of one coherent picture: the same MCU family (S32K3), the same tool-chain (S32 Design Studio + Application Code Hub), the same hardware base (FRDM-A-S32Kxxx + FRDM-K64 Click Shield + MikroE Click modules), applied to five different automotive domains. The series is intentionally aligned with the Eat-Sleep-Code-Repeat philosophy: start with a working example, then experiment — add filtering, replace polling with interrupts, introduce a state machine, add CAN communication, or refactor for functional safety. Every extension is a step closer to the way production automotive software is actually written. Recommended learning path: Lights — simplest, teaches ADC, FlexIO and BCM logic. Brakes — introduces continuous sensor thresholds. Steering — adds I²C-controlled PWM and actuator positioning. Comfort — multi-actuator, dual-technology control (PWM + stepper). Transmission — combines everything into a proportional, dual-actuator system. If you have questions, suggestions for improvement, or ideas for new modules that could extend this series, please leave a comment below — feedback from students and instructors is what keeps the workshops relevant and up to date.
記事全体を表示
Automotive Comfort Control Using FRDM-A-S32K344 Microcontrollers 1. Overview This module demonstrates how to implement a vehicle comfort control system using GPIO, PWM, and stepper motor sequencing on NXP S32K3 microcontrollers. The application reads user inputs from push-buttons and translates them into two independent comfort functions: a DC motor that simulates a cabin cooling fan (regulated through PWM) and a stepper motor that simulates an electric window mechanism (driven through GPIO coil sequencing). Both actuators react in real time, mimicking how comfort body-control modules work in modern vehicles. This example is based on the Application Code Hub demonstration for: Vehicle Comfort Control for FRDM-A-S32K344 In this workshop, on-board push-buttons simulate the driver's comfort commands. When the student presses a button, the MCU reads the input through GPIO, decodes the requested action, and drives the associated actuator: a PWM duty cycle is generated for the DC Motor 2 Click (regulating the fan speed), or a full-step coil sequence is generated through GPIO outputs to the H-Bridge Click (moving the NEMA17 stepper motor up or down). Beyond the technical implementation, the course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples. 2. Learning Scope After completing this course, participants should be able to:   Understand a basic vehicle comfort control system and the ideas behind HVAC regulation and electric window control. Use on-board push-buttons as simulated driver comfort commands. Read digital inputs using the GPIO peripheral and understand debouncing considerations. Generate PWM signals to regulate DC motor speed (fan simulation). Implement a full-step drive sequence (A → B → C → D) to control a stepper motor. Configure the DC Motor 2 Click and H-Bridge Click boards over the mikroBUS interface. Recognize the actuation data flow: user input → MCU processing → PWM / GPIO actuation. Import, build, flash, and debug an ACH project in S32 Design Studio 3.6.5. Understand why comfort functions are relevant in modern automotive body electronics. 3. System Architecture The three elements capture exactly the basic idea of the system in the demo: Input: Push-buttons (on-board buttons simulate driver comfort commands) Processing: S32K3 MCU (reads GPIO, decodes the command, drives the correct actuator) Output: Dual actuation (DC motor via PWM for the fan, stepper motor via GPIO sequencing for the window) This matches the classic flow of an embedded body-control system: user input → processing → actuator. Functional Flow The system operates continuously as follows: The user presses a button that corresponds to a comfort action The GPIO peripheral reads the button state The application decodes the command (fan control or window movement) Depending on the command, the MCU generates either a PWM signal or a stepper coil sequence The DC motor changes speed, or the stepper motor rotates in the requested direction This loop runs continuously to ensure real-time comfort control. Comfort_Control_Application.png Vehicle Comfort Control Application Architecture 4. Key Concepts 4.1 GPIO (General-Purpose Input/Output) The push-buttons on the FRDM-A-S32K344 board are connected to GPIO input pins. The MCU polls (or reads on interrupt) the pin state and interprets a logic transition as a user command. GPIO is also used as output for the stepper motor coil control signals, driving the H-Bridge Click inputs. GPIO handling is the foundation of automotive user-interface processing — used for buttons, switches, ignition detection, and many others. 4.2 PWM — Pulse-Width Modulation and Fan Speed Control PWM switches a digital output on and off at a fixed frequency, varying the duty cycle (the fraction of time the signal is high). A DC motor interprets the average voltage produced by this PWM as a proportional rotational speed. In this demo, the S32K344 generates PWM on a mikroBUS pin that drives the DC Motor 2 Click, which in turn powers the 5 V fan motor. Increasing the duty cycle increases fan speed; decreasing it slows the fan down — a typical pattern used in cabin ventilation and HVAC systems. 4.3 DC Motor Direction and H-Bridge Concept The DC Motor 2 Click integrates an H-Bridge driver that can be configured for forward, reverse, brake, or coast modes. The MCU controls the direction pins and applies PWM on the enable input to regulate speed. This is exactly the same principle used in real automotive fan modules, where a low-side or full-bridge driver is switched at kilohertz frequency to obtain smooth speed control without dissipating power in a series resistor. 4.4 Stepper Motor Full-Step Sequencing A stepper motor like the NEMA17 rotates in fixed angular increments (typically 1.8° per step) when its coils are energized in the correct order. The MCU generates a repeating four-phase pattern (A → B → C → D) on four GPIO pins connected to the H-Bridge Click. Reversing the sequence (D → C → B → A) reverses the direction. The step frequency directly determines rotation speed, and counting the number of steps gives an open-loop position estimate — the exact behavior needed to simulate an electric window moving up or down. 4.5 Push-Buttons as Comfort Commands The on-board buttons are a simplified, safe stand-in for the physical HVAC and window switches found in a real vehicle. The student presses them by hand, the GPIO state changes, the MCU decodes the command, and the corresponding actuator reacts. This isolates the student from real body-electronics wiring while preserving the full software logic. 4.6 Data Flow at a Glance Button press → GPIO input → command decoding → selection of actuator (fan or window) → PWM duty cycle update or stepper coil sequence advance → motor response. This direct chain from the student's finger to the actuator shaft is the main educational value of the demo. 5. Hardware and Software Setup Required Hardware Component Image Purpose FRDM-A-S32K344 FRDM-A-S32K344FRDM-A-S32K344 MCU platform used to run the comfort control application and drive the connected peripherals. FRDM-K64 Click Shield FRDM K64 click shieldFRDM K64 click shield mikroBUS expansion board used to connect Click modules to the FRDM platform. DC Motor 2 Click DC Motor 2 ClickDC Motor 2 Click H-Bridge driver board used to control DC motor speed and direction via PWM. H-Bridge Click H-Bridge ClickH-Bridge Click Dual H-Bridge driver used to sequence the stepper motor coils. 5 V Fan Motor 5V Fan Motor5V Fan Motor Actuator used to simulate the vehicle cabin cooling fan controlled through PWM. Stepper Motor NEMA17 Stepper Motor Nema17Stepper Motor Nema17 Actuator used to simulate the electric window mechanism through step sequencing. USB-C  — Provides power and enables programming and debugging of the system. The example application demonstrates how these peripherals are connected to the MCU pins and used to simulate cabin cooling and electric window control. Vehicle Comfort Control Full Setup on FRDM-A-S32K344 Comfort Full SetupComfort Full Setup Software Environment S32 Design Studio IDE S32K3 Real-Time Drivers (RTD) S32K3 Automotive Software Package Application Code Hub project import Vehicle Comfort Control for FRDM-A-S32K344 6. Implementation Guide Step Action Sub-steps Expected Result 1 Import the Project Open S32 Design Studio Select “Import project from Application Code Hub” Search for the vehicle comfort control demo Use the GitHub link for automatic configuration Select main branch Import project Project successfully appears in workspace 2 Build the Application Right-click project Select “Update Code and Build Project” Confirm SDK component management Build completes with no errors and generates .elf file 3 Connect Hardware Connect USB cable and external 12 V supply Attach FRDM-K64 Click Shield, DC Motor 2 Click and H-Bridge Click Wire the 5 V fan motor and NEMA17 stepper motor Verify wiring before powering the system Board is powered and detected by IDE 4 Flash and Run Open Debug Configurations Select “debug_flash_pemicro” Start debugging Application runs continuously 5 Functional Validation Press the fan control buttons Observe DC motor speed change Press the window up/down buttons Observe stepper motor movement and direction Fan speed and window motion follow user commands in real time 7. Signal Behavior and Control Logic The Vehicle Comfort Control application drives two independent actuators from a single S32K344 MCU: a DC fan motor controlled through a PWM signal for cooling, and a stepper motor controlled through a 4-channel GPIO sequence for electric window movement. User inputs (SW2 and SW3) are read by the MCU, which then generates the appropriate signal type for each actuator. The two diagrams below describe the signal behavior and control logic for each subsystem. 7.1 Cooling System – Fan Speed Control (PWM) Comfort_Fan_PWM.png Figure: Fan speed control mapping. The MCU generates a PWM signal on the EMIOS channel to drive the DC fan motor through the DC MOTOR 2 Click board. Each SW2 press increments the duty cycle by one step (0 % → 33 % → 67 % → 100 %) and each SW3 press decrements it, so fan speed is directly proportional to duty cycle. Duty Counts represent the raw PWM compare values (period = 20000 counts). When the fan is fully stopped, the TB6593FNG driver is automatically put into low-power sleep mode to prevent wasted current through the windings. 7.2 Window System – Stepper Motor Full-Step Sequencing Direction Step # Coil A (PTA13) Coil B (PTD0) Coil C (PTA3) Coil D (PTC10) Active Pair UP (SW2 pressed) 1 ON OFF ON OFF AC 2 OFF ON ON OFF BC 3 OFF ON OFF ON BD 4 ON OFF OFF ON AD DOWN (SW3 pressed) 1 ON OFF OFF ON AD 2 OFF ON OFF ON BD 3 OFF ON ON OFF BC 4 ON ON OFF OFF AC Table: Stepper motor full-step sequencing for window control. The MCU drives the stepper motor through four GPIO lines connected to the H-Bridge Click board, using dual-coil activation (two coils energised per step) to maximise torque. Pressing SW2 executes the Up sequence AC → BC → BD → AD (window moves up), while SW3 executes the reversed Down sequence AD → BD → BC → AC (window moves down). Each press advances the motor by one full step with a 3 ms delay, and the coil pair remains energised as long as the button is held. When no button is pressed, all coils are de-energised to prevent motor winding overheating during idle periods. 8. Troubleshooting Issue Possible Actions Board Not Detected Check USB cable and drivers Verify debugger connection Restart IDE Fan Does Not Spin Verify PWM configuration and duty cycle Check DC Motor 2 Click wiring and enable pins Ensure the 5 V motor supply is present Stepper Not Moving Verify GPIO output configuration for coil pins Check H-Bridge Click wiring and coil order Confirm the step delay is not too short (motor stalls) Stepper Rotates Wrong Direction Invert the coil sequence in software (A→B→C→D vs D→C→B→A) Swap one coil pair on the H-Bridge output Buttons Not Responding Verify GPIO input configuration and pull-up/pull-down Add software debouncing Check that the correct button pins are mapped 9. Extending the Application The basic implementation can be extended in several ways: Feedback-Based Control Add temperature or Hall-effect sensors for closed-loop fan speed regulation Add end-stop switches or encoders for accurate window position tracking Automatic Comfort Modes Implement predefined climate or ventilation profiles Trigger comfort actions based on sensor thresholds CAN Communication Enable communication with other vehicle ECUs (e.g., HVAC master, door module) Receive comfort commands over the vehicle network Diagnostic Functions Add fault detection for stuck motors, over-current or open loads Expose diagnostic status via LEDs or debug UART Position Memory Store and restore window or fan positions in non-volatile memory Recall the last comfort state after each power-up State Machine Implementation A more advanced approach is to implement a state machine: Idle Active Fault 10. Safety Context This example reflects key automotive principles: Continuous monitoring of driver commands Immediate response to control signals Reliable actuator control for both speed and position In real systems: Redundancy is required for safety-relevant functions (e.g., anti-pinch on windows) Fault detection mechanisms are implemented (over-current, stall, over-temperature) Systems must comply with ISO 26262 (functional safety standard) where applicable Modern comfort modules also implement anti-pinch protection on power windows, ensuring the motor stops or reverses when an obstruction is detected — a safety-critical requirement for real vehicles. 11. Conclusion This module demonstrates how a simple embedded system can implement vehicle comfort control using GPIO inputs, PWM outputs, and stepper motor sequencing on the S32K344 platform. It shows how: Digital user inputs are acquired through GPIO Commands are decoded and processed in real time A DC motor is controlled using PWM for smooth speed regulation A stepper motor is controlled using a full-step coil sequence for precise positioning Result on FRDM-A-S32K344 Comfort ResultComfort Result The course provides a strong foundation for more advanced systems, including feedback-based control, CAN networking, diagnostics, and safety-oriented designs typical of automotive body-control modules. The course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples.
記事全体を表示
Automotive Lighting Control Using FRDM-A-S32K3XX Microcontrollers 1. Overview This module demonstrates how to implement a vehicle lighting control system using analog input acquisition and FlexIO-based LED driving on NXP S32K3 microcontrollers. The application reads analog inputs from the Analog Key Click module (six push-buttons, each generating a distinct voltage level) and converts them into commands that drive a 4x4 RGB LED matrix. Each button press activates a specific lighting function — low beam, high beam, turn signals, brake lights, or hazard lights — while safety interlocks and blinking patterns run continuously in the background, mimicking how a real automotive Body Control Module (BCM) manages vehicle lighting. This example is based on Application Code Hub demonstrations for: Vehicle Lighting Control for Daylight and Hazard Signals on FRDM-A-S32K344 Vehicle Lighting Control for Daylight and Hazard Signals on FRDM-A-S32K312 In this workshop, the Analog Key Click simulates six vehicle lighting controls. When the student presses a button, an analog voltage proportional to the pressed key is read by the MCU through the ADC (with software debouncing), decoded into a specific lighting command, and translated into an RGB pattern generated by the FlexIO peripheral. The 4x4 RGB Click then displays the corresponding automotive lighting behavior in real time — warm white for low beams, cool white for high beams, blinking amber for turn signals and hazards, and red for brake lights. Beyond the technical implementation, the course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples. 2. Learning Scope After completing this course, participants should be able to:   Understand a basic vehicle lighting control system and the ideas behind an automotive Body Control Module (BCM). Use the Analog Key Click as a simulated multi-button user interface (six inputs on a single analog line). Acquire analog values (0–3.3 V) using the ADC and understand how multiple buttons share one channel through voltage division. Perform software debouncing and decode which button was pressed based on ADC value ranges. Drive an RGB LED matrix using the FlexIO peripheral, generating precise timing for WS2812-style LEDs. Implement safety interlocks between lighting functions (e.g., high beam requires low beam ON). Implement continuous background patterns such as blinking turn signals and synchronized hazards. Recognize the actuation data flow: analog input → ADC → command decoding → FlexIO LED output. Import, build, flash, and debug an ACH project in S32 Design Studio 3.6.5. Understand why lighting functions are relevant for automotive safety and driver visibility. 3. System Architecture The three elements capture exactly the basic idea of the system in the demo: Input: Analog Key Click (six buttons T1–T6, each generating a distinct analog voltage level) Processing: S32K3 MCU (reads the ADC, decodes the button, applies BCM logic, updates the LED state) Output: 4x4 RGB Click (16-LED matrix driven by FlexIO to display lighting patterns) This matches the classic flow of an embedded body-control system: sensor → processing → actuator. Functional Flow The system operates continuously as follows: The user presses a button on the Analog Key Click (T1–T6) Each button generates a distinct analog voltage on the shared output line The ADC samples the voltage and converts it into a digital value The application decodes which button was pressed (with debouncing) The BCM logic applies interlocks and dependencies (e.g., high beam requires low beam) The FlexIO peripheral drives the RGB Click LEDs with the corresponding color pattern This loop runs continuously to ensure real-time lighting control, with blinking patterns and safety interlocks maintained in the background. System_Architecture_Lights.pngVehicle Lighting Control Application Architecture  4. Key Concepts 4.1 ADC (Analog-to-Digital Converter) The Analog Key Click outputs 0–3.3 V on a single analog line, with each button generating a specific voltage step. The ADC samples this voltage on ADC0_P0 (pin PTD1) at regular intervals and quantizes it into a digital code (a 12-bit ADC produces values between 0 and 4095). Each button corresponds to a specific value range, allowing six digital inputs to be read through a single ADC channel. ADC acquisition is the foundation of automotive sensing — used for switches, buttons, sensors, and many others. 4.2 Analog Multi-Button Decoding Instead of using six separate GPIO pins, the Analog Key Click uses a resistor ladder that produces a different voltage for each button press. The application performs software debouncing (multiple ADC samples must agree before a press is confirmed) and then compares the ADC value against predefined thresholds to identify which button (T1–T6) was pressed. This technique is common in automotive steering-wheel controls, where many buttons share a single analog line to save wiring and pins. 4.3 FlexIO — Driving the RGB Click LEDs FlexIO is a highly flexible peripheral on S32K3 that can emulate serial protocols like WS2812/NeoPixel. The RGB Click uses individually addressable LEDs that require precise timing (~800 kHz with strict pulse widths). FlexIO on PTA13 (FlexIO_D8) generates this waveform in hardware, without loading the CPU. Each of the 16 LEDs receives its color data through a serial stream, allowing independent control of color and brightness per LED. 4.4 RGB LED Mapping and Lighting Zones The 16 LEDs of the RGB Click are logically grouped into automotive lighting zones: LEDs 13, 14 → Low Beam Headlights (warm white) LEDs 8, 9, 10, 11 → High Beam Headlights (cool white) LEDs 0, 12 → Left Turn Signal (blinking amber) LEDs 3, 15 → Right Turn Signal (blinking amber) LEDs 1, 2, 5, 6 → Brake Lights (red) LEDs 0, 3, 12, 15 → Hazard Lights (synchronized blinking amber) 4.5 BCM Safety Interlocks and State Dependencies The application implements safety logic typical of a real Body Control Module: high beam can only be activated when low beam is already ON; turning OFF the low beam automatically disables the high beam; hazard lights synchronize left and right turn signals simultaneously; high beam state is preserved during hazard blinking and restored between cycles. These interlocks illustrate how real automotive lighting logic prevents unsafe combinations and preserves driver intent. 4.6 Data Flow at a Glance Button press → analog voltage on shared line → ADC sample → software debouncing → button decoding → BCM logic (interlocks + dependencies) → FlexIO WS2812 output stream → RGB LED color update. This direct chain from the student's finger to the LEDs is the main educational value of the demo. 5. Hardware and Software Setup Required Hardware Component Image Purpose FRDM-A-S32K312 FRDM-A-S32K312.png Alternative MCU platform used to run the lighting application and process user inputs. FRDM-A-S32K344 S32K344MINI-EVB.png Alternative MCU platform used to run the lighting application and control connected peripherals. FRDM-K64 Click Shield frdm-k64-click.jpg mikroBUS expansion board used to connect Click modules to the FRDM platform. Analog Key Click analog-click.jpg Six-button analog module used to simulate the vehicle lighting controls (headlights, indicators, brakes, hazards). 4x4 RGB Click 4x4-rgb-click.jpg 16-LED RGB matrix used to display the automotive lighting patterns in real time. USB-C / 12 V supply — Provides power and enables programming and debugging of the system through a single USB-C connection. The example applications demonstrate how these peripherals are connected to the MCU pins and used to simulate a complete vehicle lighting control system. Vehicle Lighting Control on FRDM-A-S32K312 Vehicle Lighting Control on FRDM-A-S32K344 Lights_k312.png Lights_k344.png Software Environment S32 Design Studio IDE S32K3 Automotive Software Package Application Code Hub project import Vehicle Lighting Control for Daylight and Hazard Signals on FRDM-A-S32K344 Vehicle Lighting Control for Daylight and Hazard Signals on FRDM-A-S32K312 6. Implementation Guide Step Action Sub-steps Expected Result 1 Import the Project Open S32 Design Studio 3.6.5 Select “Import project from Application Code Hub” Search for “Lighting” Select the desired project for your FRDM board Use the GitHub link for automatic configuration Select main branch Import project Project successfully appears in workspace 2 Build the Application Right-click project Select “Update Code and Build Project” Confirm SDK component management Build completes with no errors and generates .elf file 3 Connect Hardware Connect USB-C cable (and 12 V supply for FRDM-A-S32K312) Attach FRDM-K64 Click Shield, Analog Key Click and 4x4 RGB Click Verify wiring on PTA13 (FlexIO) and PTD1 (ADC) Board is powered and detected by IDE 4 Flash and Run Open Debug Configurations Select “debug_flash_pemicro” Start debugging Application runs continuously; LEDs perform startup test sequence 5 Functional Validation Press buttons T1–T6 on the Analog Key Click Observe corresponding LED patterns on the RGB Click Verify safety interlocks (high beam requires low beam) Verify continuous blinking on turn signals and hazards RGB LEDs display the correct automotive lighting patterns for each button 7. Signal Behavior and Control Logic   The following diagram illustrates how each user input on the Analog Key Click is mapped to a specific lighting function and to the individual LEDs of the 4×4 RGB Click matrix. Each button (T1–T6) triggers a unique combination of LEDs, colors, and patterns, reproducing the behavior of a simplified automotive lighting system.   Led_Matrix_Mapping.png  The MCU continuously monitors the analog input from the Analog Key Click and decodes which button is pressed. Based on the detected input, the application activates the corresponding lighting function by driving the assigned LEDs on the 4×4 RGB Click through the FlexIO serial interface. Steady functions (Low Beam, High Beam, Brake) keep the associated LEDs constantly ON, while directional functions (Left Turn, Right Turn, Hazard) toggle the LEDs at approximately 1 Hz to reproduce the blinking behavior of real vehicle indicators. Additional control rules — such as High Beam requiring Low Beam to be active, or Hazard Lights preserving and restoring the High Beam state — reflect the interdependencies found in a real automotive body control module. 8. Troubleshooting Issue Possible Actions Board Not Detected Check USB-C cable and drivers Verify debugger connection Restart IDE No LEDs Lighting Up Verify FlexIO configuration on PTA13 Check 3.3 V and GND wiring on RGB Click Confirm data-line wiring to IN1 Buttons Not Detected Verify ADC0_P0 configuration on PTD1 Check 3.3 V and GND wiring on Analog Key Click Confirm software debouncing thresholds Wrong Button Triggered Recalibrate ADC value ranges for each button Verify power supply stability (3.3 V) Check for noise on the analog line Incorrect LED Colors or Timing Verify FlexIO clock configuration (WS2812 timing) Check LED index → color mapping in code Ensure RGB order (GRB vs. RGB) matches the LED type High Beam Not Activating Ensure low beam (T1) is ON first — BCM interlock Check application logic for beam dependencies 9. Extending the Application The basic implementation can be extended in several ways: Additional Lighting Functions Add fog lights, parking lights, or daytime running lights (DRL) Simulate reverse lights that activate when a specific input is triggered Adaptive Front Lighting Integrate a steering angle input (e.g., POT Click) to swivel the headlights Simulate cornering lights that turn on when indicators are active Ambient Light Sensing Add a light sensor to automatically enable low beams at dusk Implement smooth dimming between day and night modes Brake Light Enhancements Add an emergency brake flashing pattern for hard braking Implement a third brake light (single LED, always ON with brakes) CAN Communication Enable communication with other vehicle ECUs (e.g., BCM master, doors) Receive lighting commands over the vehicle network State Machine Implementation A more advanced approach is to implement a formal state machine covering: Off DRL / Parking Low Beam High Beam Hazard / Fault 10. Safety Context This example reflects key automotive principles: Continuous monitoring of driver input Immediate response to control signals Reliable actuator (LED) control with predictable timing Safety interlocks between lighting functions (high beam requires low beam) In real systems: Redundancy is required for safety-relevant functions (e.g., brake lights, hazards) Fault detection mechanisms are implemented (open lamp, short circuit, overcurrent) Systems must comply with ISO 26262 (functional safety standard) Vehicle lighting is one of the most safety-critical automotive functions because it directly affects driver visibility and vehicle conspicuity. Modern Body Control Modules implement extensive diagnostics, backup lighting strategies, and fail-safe defaults (e.g., hazard lights activated on power-loss recovery). 11. Conclusion This module demonstrates how a simple embedded system can implement complete vehicle lighting control using ADC input and FlexIO output on the S32K3 platform. It shows how: Multiple digital inputs can share a single analog line through resistor-ladder decoding Analog data is acquired, debounced and processed in real time Complex automotive lighting patterns are controlled through FlexIO-driven WS2812 LEDs Safety interlocks and background blinking patterns are managed by BCM-style logic Result on FRDM-A-S32K312 Result on FRDM-A-S32K344 FRDM-A-S32K312FRDM-A-S32K312 FRDM-A-S32K344FRDM-A-S32K344 The course provides a strong foundation for more advanced systems, including adaptive lighting, CAN networking, ambient sensing, and safety-oriented designs typical of automotive body-control modules.
記事全体を表示
Automotive Brake Control Using FRDM-A-S32K3XX Microcontrollers 1. Overview This article demonstrates how to implement a brake status monitoring system using NXP S32K3 microcontrollers. The solution is based on Application Code Hub examples for S32K344 and S32K312 platforms and showcases how real-time sensor data can be used to detect braking events and trigger visual feedback. This is based on the following Application Code Hub demonstrations: Brake-Control-Monitoring-FRDM-A-S32K312 Brake-Control-Monitoring-FRDM-A-S32K344 The application simulates braking conditions using a sensor input and provides immediate system response via an LED indicator. Such systems are commonly used in automotive environments to improve system awareness and support safety-related functionality.   Beyond teaching technical concepts, the course promotes the Eat-Sleep-Code-Repeat methodology as a core learning principle. Students are encouraged to continuously explore, implement, test, and enhance automotive embedded applications using real hardware and practical examples, reinforcing knowledge through repetition, experimentation, and hands-on problem solving. 2. Learning Scope This article covers both practical implementation and core embedded concepts, including: Reading analog signals using ADC Processing real-time signals Controlling outputs using GPIO Implementing decision logic based on thresholds Understanding signal flow in embedded systems 3. System Architecture The application is built around a simple but representative embedded system: Input: Analog sensor (force / brake simulation) Processing: S32K3 microcontroller Output: LED indicator Functional Flow The sensor generates an analog signal proportional to applied force The ADC converts the analog signal into a digital value The software evaluates the value against defined thresholds The system updates the output (LED) based on braking state Brake Monitoring Application ArchitectureBrake Monitoring Application Architecture 4. Key Concepts Analog Signal Acquisition (ADC) Sensors typically output analog values that must be digitized for processing. The ADC periodically samples this signal and produces a digital representation used by the application logic. Typical interpretation: Low value → no braking activity High value → braking detected Real-Time Signal Processing The system continuously reads sensor data and reacts immediately. This is essential in automotive contexts where delayed responses may impact system behavior. Output Control Using GPIO The LED output reflects the system state: OFF → no braking detected ON → braking condition detected In extended implementations, multiple states or patterns can be used. 5. Hardware and Software Setup Required Hardware Component Image Purpose FRDM-A-S32K312 FRDM-A-S32K312FRDM-A-S32K312 Alternative MCU platform used to run the brake application and process brake inputs. FRDM-A-S32K344 FRDM-A-S32K344FRDM-A-S32K344 Alternative MCU platform used to run the brake application and control connected peripherals. FRDM K64 click shield                  frdm-k64-click mikroBUS expansion adapter that connects Click modules to the FRDM board Force Click (or similar analog sensor module)                          Force ClickForce Click Simulates the brake pedal by producing an analog signal proportional to applied pressure 4x4 RGB Click (LED output)                         4X4 RGB Click4X4 RGB Click Displays real-time brake status through colored LED patterns (green → yellow → orange → red) USB cable / power supply — Powers the FRDM board and provides debug connectivity to the PC The example applications demonstrate how these peripherals are connected to the MCU pins and used to simulate brake inputs and outputs. Brake Control Monitoring on FRDM-A-S32K312 Brake Control Monitoring on FRDM-A-S32K344 Brake Control Monitoring on FRDM-A-S32K312Brake Control Monitoring on FRDM-A-S32K312 Brake Control Monitoring on FRDM-A-S32K344Brake Control Monitoring on FRDM-A-S32K344 Software Environment S32 Design Studio S32K3 Automotive Software Package Application Code Hub project import Brake-Control-Monitoring-FRDM-A-S32K312 Brake-Control-Monitoring-FRDM-A-S32K344 6. Implementation Guide Step Action Sub-steps Expected Result 1 Import the Project Open S32 Design Studio Use “Import project from Application Code Hub” Locate the brake monitoring example Import and configure the project Project is successfully loaded into the workspace 2 Build the Application Compile the project Resolve any dependency issues if needed No compilation errors 3 Connect Hardware Connect the development board via USB Attach sensor and LED modules Ensure correct pin connections Board is powered and detected by the IDE 4 Flash and Run Program the MCU Start execution Application runs continuously 5 Functional Validation Apply pressure to the sensor Observe LED behavior LED activates when braking condition is detected 7. Signal Behavior and Threshold Logic The application relies on threshold-based decision logic: If ADC value < threshold → no brake If ADC value ≥ threshold → brake active Signal vs Threshold Diagram Designer (4).png 8. Troubleshooting Issue Possible Actions Board Not Detected Verify USB cable and drivers Check debugger connection Restart IDE No Output Response Validate GPIO configuration Check LED connections Confirm code execution Incorrect Sensor Readings Verify ADC configuration Inspect sensor wiring Confirm scaling and thresholds 9. Extending the Application The basic implementation can be extended in several ways: Multi-Level Brake Detection Define multiple thresholds: Low → normal Medium → moderate braking High → emergency braking Noise Filtering Apply software filtering to stabilize readings Avoid false triggering from sensor noise Timing-Based Logic Add debounce or delay mechanisms Require sustained input before triggering State Machine Implementation A more advanced approach is to implement a state machine: Idle Braking Emergency 10. Safety Context Although simplified, this application reflects concepts used in automotive safety systems: Continuous monitoring of input signals Immediate response to changes Clear indication of system state In real systems, additional mechanisms are required: Redundancy Fault detection Compliance with safety standards (e.g., ISO 26262) 11. Conclusion This example demonstrates how a simple embedded application can model a real-world automotive use case. By combining ADC input, real-time processing, and GPIO output, it highlights the core principles behind monitoring functions in automotive ECUs. Result on FRDM-A-S32K312 Result on FRDM-A-S32K344 Result on FRDM-A-S32k312Result on FRDM-A-S32k312 Result on FRDM-A-S32K344Result on FRDM-A-S32K344 The course provides a foundation for more advanced designs, including multi-state logic, filtering techniques, and safety-focused extensions. The course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples.
記事全体を表示