Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
HOWTO: Install GHS Compiler Plugin S32 Design Studio (S32DS) supports Eclipse plug-in of Green Hills Software (GHS) compiler to compile S32DS projects via GHS compiler. This document describes how to install this plug-in and enable GHS in the new project wizard. After the GHS Eclipse plug-in is installed successfully, you can be able to create and build S32DS project using GHS compiler under S32DS Eclipse environment if the device and SDKs support GHS compiler. Installation instructions To able to use GHS compiler, you need to make sure that GHS compiler is installed with a valid license. Follow the steps below to install eclipse plugin: Install GHS Eclipse plug-in On S32DS graphical user interface, go to menu "Help" -> "Install New Software" DanielBarbu_0-1724323738892.jpeg In the "Install" dialog appears, click on "Add" button. In the "Add Repository" dialogappears, click on "Local". Navigate to the eclipse directory located in your MULTI compiler installation(eg: C:\ghs\comp_202114\eclipse) DanielBarbu_1-1724323981927.png In the Name box, enter "GHS Eclipse". Click on "Add" button. DanielBarbu_2-1724324072313.png  In the Name/Version list, expand the Green Hills MULTI for Eclipse item. Select GreenHills MULTI for Eclipse corresponding to your target architecture(eg: Green Hills MULTI for Eclipse(ARM) and Green Hills MULTI for Eclipse(ARM64)). If you have MULTI licenses for more than one architecture, you can select all the targets you are licensed for. Click Next until you see the license acceptance page. DanielBarbu_3-1724324146518.png  If you accept the terms of the feature license, select I accept the terms in the license agreement. And click on "Finish" button. DanielBarbu_4-1724324257519.png If the Security Warning window appears, click on "Install anyway". DanielBarbu_5-1724324310392.png In the "Software Updates" dialog box appears, click on "Restart Now" to restart S32DS.- Go to "Window" -> select "Preference" -> "S32 Design Studio for S32 Platform" -> "S32DS Variables". Set your GHS installation path for S32DS_GHS_PATH variable (ex "C:\ghs\comp_202114"). DanielBarbu_6-1724324374973.png Create new S32DS project using GHS in the project wizard. Now you can create a new S32DS project and select GHS toolchain for the device andSDKs support GHS toolchain. DanielBarbu_7-1724324414370.png And you can see the GHS settings are showed in the S32DS project properties. All_options_white_bg.png Re: HOWTO: Install GHS Compiler Plugin Hello NXP team, I have tried the above procedure and its not working, It is a simple test project. Created a simple project, using pins tool, updated the code , and tried to build all. here is the commander and linker options generated with new project. GHS C Compiler for ARM Standalone-  ccarm Options- -preprocess_assembly_files -list --no_slash_comment -C99 --no_exceptions --gnu_asm --unsigned_fields --unsigned_chars --no_short_enum --ghstd=last --prototype_errors -Wimplicit-int --incorrect_pragma_warnings -Wshadow -Wtrigraphs -Wundef -G -dwarf2 -Osize -DS32K344 -DGHS -DENABLE_FPU -DMPU_ENABLE -DI_CACHE_ENABLE -DD_CACHE_ENABLE -DCPU_S32K344 -DS32K3XX -DCPU_CORTEX_M7 -IC:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/generate/include -IC:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/RTD/include -I"C:\NXP\S32DS.3.5\eclipse\../S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M30I0R0/header" -I"C:\NXP\S32DS.3.5\eclipse\/../S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M30I0R0//header/" -I"C:\NXP\S32DS.3.5\eclipse\/../S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M30I0R0//include/" -I"C:\NXP\S32DS.3.5\eclipse\/../S32DS/software/PlatformSDK_S32K3/RTD/Platform_TS_T40D34M30I0R0//include/" -I"C:\NXP\S32DS.3.5\eclipse\/../S32DS/software/PlatformSDK_S32K3/RTD/Platform_TS_T40D34M30I0R0//startup/include/" -I"C:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/board" -keeptempfiles -littleendian -cpu=cortexm7 -fpu=vfpv5_d16 -fsingle -thumb --no_commons GHS C Linker for ARM Standalone ccarm options -  --gnu_asm -g -dwarf2 -Wl,-keep=C40_Ip_AccessCode -Wl,-v -T "C:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/Project_Settings/Linker_Files/linker_flash_s32k344.ld" -e Reset_Handler -delete -ignore_debug_references -map -keepmap -Mn -nostartfiles -I"C:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/board" -larch -lstartup -lind_sd -L"C:\ghs\comp_202354_1fp_x64_ForNXP\lib\thumb2" -cpu=cortexm7 -thumb
記事全体を表示
HOWTO: GHSコンパイラ・プラグインのインストール方法 S32 Design Studio(S32DS)は、Green Hills Software(GHS)コンパイラのEclipseプラグインをサポートしており、GHSコンパイラを使用してS32DSプロジェクトをコンパイルできます。本ドキュメントでは、このプラグインをインストールする方法と、新規プロジェクト・ウィザードでGHSを有効にする方法を説明します。 GHS Eclipse プラグインが正常にインストールされると、デバイスと SDK が GHS コンパイラをサポートしている場合、S32DS Eclipse 環境で GHS コンパイラを使用して S32DS プロジェクトを作成およびビルドできるようになります。 インストール手順 GHS コンパイラを使用するには、有効なライセンスでインストールされていることを確認する必要があります。Eclipse プラグインをインストールするには、以下の手順に従ってください。 GHS Eclipseプラグインのインストール S32DSのグラフィカル・ユーザー・インターフェースで、メニューの「Help(ヘルプ)」->「Install New Software(新規ソフトウェアをインストール)」を選択します。 DanielBarbu_0-1724323738892.jpeg 表示される「Install(インストール)」ダイアログで、「Add(追加)」ボタンをクリックします。表示される「Add Repository(リポジトリを追加)」ダイアログで、「Local(ローカル)」をクリックします。MULTIコンパイラのインストール先にあるeclipseディレクトリに移動します(例: C:\ghs\comp_202114\eclipse) DanielBarbu_1-1724323981927.png 「Name(名前)」ボックスに「GHS Eclipse」と入力します。「Add(追加)」ボタンをクリックします。 DanielBarbu_2-1724324072313.png 名前/バージョンのリストで、Green Hills MULTI for Eclipseの項目を展開します。ターゲットのアーキテクチャに合致するGreen Hills MULTI for Eclipseを選択します(例:Green Hills MULTI for Eclipse(ARM)とGreen Hills MULTI for Eclipse(ARM64))。複数のアーキテクチャに対してMULTIライセンスを保有している場合は、ライセンスが適用されるすべてのターゲットを選択できます。「Next(次へ)」をクリックして、ライセンスの同意ページまで移動します。 DanielBarbu_3-1724324146518.png 機能ライセンスの条項に同意する場合は、「I accept the terms in the license agreement(ライセンス契約の条項に同意します)」を選択します。「Finish(完了)」ボタンをクリックします。 DanielBarbu_4-1724324257519.png セキュリティ警告ウィンドウが表示された場合は、「Install anyway」をクリックしてください。 DanielBarbu_5-1724324310392.png 表示される「Software Updates(ソフトウェア・アップデート)」ダイアログ・ボックスで、「Restart Now(今すぐ再起動)」をクリックして、S32DSを再起動します。「Window(ウィンドウ)」->「Preference(環境設定)」->「S32 Design Studio for S32 Platform」->「S32DS Variables(S32DS変数)」を選択します。S32DS_GHS_PATH変数にGHSのインストール・パスを設定します(例:「C:\ghs\comp_202114」)。 DanielBarbu_6-1724324374973.png プロジェクトウィザードでGHSを使用して新しいS32DSプロジェクトを作成してください。 こうして、GHSツールチェーンをサポートするデバイスを対象として、S32DSプロジェクトを新規作成し、GHSツールチェーンを選択できるようになりました。 DanielBarbu_7-1724324414370.png また、画面を見ると、S32DSプロジェクトのプロパティにGHS設定が表示されています。 DanielBarbu_8-1724324493234.png Re: HOWTO: GHSコンパイラ・プラグインのインストール方法 NXPチームの皆様、こんにちは。 上記の手順を試しましたが、うまくいきません。簡単なテスト・プロジェクトで試しています。 ピンツールを使用して簡単なプロジェクトを作成し、コードを更新し、すべてをビルドしようとしました。 新規プロジェクトで生成されたコマンドとリンカのオプションは次のとおりです。 GHS C ARMスタンドアロン用コンパイラ ccarm Options- -preprocess_assembly_files -list --no_slash_comment -C99 --no_exceptions --gnu_asm --unsigned_fields --unsigned_chars --no_short_enum --ghstd=last --prototype_errors -Wimplicit-int --incorrect_pragma_warnings -Wshadow -Wtrigraphs -Wundef -G -dwarf2 -Osize -DS32K344 -DGHS -DENABLE_FPU -DMPU_ENABLE -DI_CACHE_ENABLE -DD_CACHE_ENABLE -DCPU_S32K344 -DS32K3XX -DCPU_CORTEX_M7 -IC:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/generate/include -IC:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/RTD/include -I"C:\NXP\S32DS.3.5\eclipse\../S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M30I0R0/header" -I"C:\NXP\S32DS.3.5\eclipse\/../S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M30I0R0//header/" -I"C:\NXP\S32DS.3.5\eclipse\/../S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M30I0R0//include/" -I"C:\NXP\S32DS.3.5\eclipse\/../S32DS/software/PlatformSDK_S32K3/RTD/Platform_TS_T40D34M30I0R0//include/" -I"C:\NXP\S32DS.3.5\eclipse\/../S32DS/software/PlatformSDK_S32K3/RTD/Platform_TS_T40D34M30I0R0//startup/include/" -I"C:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/board" -keeptempfiles -littleendian -cpu=cortexm7 -fpu=vfpv5_d16 -fsingle -thumb --no_commons GHS C ARMスタンドアロン用リンカー ccarm オプション - --gnu_asm -g -dwarf2 -Wl,-keep=C40_Ip_AccessCode -Wl,-v -T "C:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/Project_Settings/Linker_Files/linker_flash_s32k344.ld" -e Reset_Handler -delete -ignore_debug_references -map -keepmap -Mn -nostartfiles -I"C:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/board" -larch -lstartup -lind_sd -L"C:\ghs\comp_202354_1fp_x64_ForNXP\lib\thumb2" -cpu=cortexm7 -thumb
記事全体を表示
操作方式:安装 GHS 编译器插件 S32 设计工作室(S32DS)支持 Green Hills Software(GHS)编译器的 Eclipse 插件,可通过 GHS 编译器来编译 S32DS 项目。本文档介绍如何安装该插件以及在新建项目向导中启用 GHS。 GHS Eclipse 插件成功安装后,若器件和 SDK 支持 GHS 编译器,你就可以在 S32DS Eclipse 环境下使用 GHS 编译器创建并构建 S32DS 项目。 安装说明 要使用 GHS 编译器,您需要确保 GHS 编译器已安装并拥有有效的许可证。请按照以下步骤安装 Eclipse 插件: 安装 GHS Eclipse 插件 在S32DS图形用户界面中,进入菜单"Help" -> "Install New Software" DanielBarbu_0-1724323738892.jpeg 在弹出的 “Install”(安装)对话框中,点击 “Add”(添加)按钮。在弹出的 “Add Repository”(添加仓库)对话框中,点击 “Local”(本地)。导航至您的 MULTI 编译器安装目录下的 eclipse 文件夹(例如:C:\ghs\comp_202114\eclipse)。 DanielBarbu_1-1724323981927.png 在 “名称” 框中,输入 “GHS Eclipse”。点击 “添加” 按钮。 DanielBarbu_2-1724324072313.png 在 “名称 / 版本” 列表中,展开 “Green Hills MULTI for Eclipse” 项。选择与您的目标架构对应的 “Green Hills MULTI for Eclipse”(例如:Green Hills MULTI for Eclipse (ARM) 和 Green Hills MULTI for Eclipse (ARM64))。如果您拥有多个架构的 MULTI 许可证,可以选择所有已获得许可的目标架构。点击 “下一步”,直至出现许可协议接受页面。 DanielBarbu_3-1724324146518.png 如果您接受该功能许可条款,请选择 “我接受许可协议中的条款”,然后点击 “完成” 按钮。 DanielBarbu_4-1724324257519.png 如果出现 “安全警告” 窗口,请点击 “仍然安装”。 DanielBarbu_5-1724324310392.png 在弹出的 “软件更新” 对话框中,点击 “立即重启” 以重启 S32DS。-依次进入 “Window”-> 选择 “Preference”-> “S32 Design Studio for S32 Platform”-> “S32DS Variables”。为 S32DS_GHS_PATH 变量设置您的 GHS 安装路径(例如 “C:\ghs\comp_202114”)。 DanielBarbu_6-1724324374973.png 在项目向导中使用GHS创建新的S32DS项目。 现在,您可以创建一个新的 S32DS 项目,并为支持 GHS 工具链的器件和 SDK 选择 GHS 工具链。 DanielBarbu_7-1724324414370.png 您可以看到GHS设置显示在S32DS项目属性中。 DanielBarbu_8-1724324493234.png 回复:如何安装 GHS 编译器插件 您好,NXP团队, 我已尝试上述步骤,但无法正常运行,这只是一个简单的测试项目。 创建了一个简单的项目,使用 pins 工具,更新了代码,并尝试构建所有。 以下是新项目生成的编译器和链接器选项。 ARM 独立式 GHS C 编译器 - ccarm 选项- -preprocess_assembly_files -list --no_slash_comment -C99 --no_exceptions --gnu_asm --unsigned_fields --unsigned_chars --no_short_enum --ghstd=last --prototype_errors -Wimplicit-int --incorrect_pragma_warnings -Wshadow -Wtrigraphs -Wundef -G -dwarf2 -Osize -DS32K344 -DGHS -DENABLE_FPU -DMPU_ENABLE -DI_CACHE_ENABLE -DD_CACHE_ENABLE -DCPU_S32K344 -DS32K3XX -DCPU_CORTEX_M7 -IC:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/generate/include -IC:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/RTD/include -I"C:\NXP\S32DS.3.5\eclipse\../S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M30I0R0/header" -I"C:\NXP\S32DS.3.5\eclipse\/../S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M30I0R0//header/" -I"C:\NXP\S32DS.3.5\eclipse\/../S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M30I0R0//include/" -I"C:\NXP\S32DS.3.5\eclipse\/../S32DS/software/PlatformSDK_S32K3/RTD/Platform_TS_T40D34M30I0R0//include/" -I"C:\NXP\S32DS.3.5\eclipse\/../S32DS/software/PlatformSDK_S32K3/RTD/Platform_TS_T40D34M30I0R0//startup/include/" -I"C:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/board" -keeptempfiles -littleendian -cpu=cortexm7 -fpu=vfpv5_d16 -fsingle -thumb --no_commons ARM 独立式 GHS C 链接器 ccarm 选项 - --gnu_asm -g -dwarf2 -Wl,-keep=C40_Ip_AccessCode -Wl,-v -T "C:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/Project_Settings/Linker_Files/linker_flash_s32k344.ld" -e Reset_Handler -delete -ignore_debug_references -map -keepmap -Mn -nostartfiles -I"C:\Users\ganheg1\workspaceS32DS.3.5\GHS_Test/board" -larch -lstartup -lind_sd -L"C:\ghs\comp_202354_1fp_x64_ForNXP\lib\thumb2" -cpu=cortexm7 -thumb
記事全体を表示
S32DS ARM 2.2 issue After installing S32DSARM 2.2 on Windows 11, the following error message appears. The default project cannot be opened either. Re: S32DS ARM 2.2 issue Hi@ yeSerrui After installing S32 DS, you also need to install the RTM SDK, as shown below. Senlent_1-1785739865237.png In the project browsing box on the left, right-click "new" to select the included example. Senlent_0-1785739821338.png
記事全体を表示
インターネットにコネクテッドではないコンピュータでGUI Guiderを起動できない こんにちは。私の開発用コンピュータはインターネットに接続されていません。GUI Guider をダウンロードし、プログラムを起動すると、インターネット接続を探し、NXP アカウントにログインするように求められます。GUI Guider を実行するにはなぜインターネット接続が必要なのですか?インターネットに接続されていないコンピューターでツールを起動する方法はありますか? ありがとうございます ジョー Re: Unable to Launch GUI Guider on non-internet connected computer こんにちは@joseph_lindula すでにメールで返信させていただきました。 ご理解いただきありがとうございます。 BR ハリー Re: Unable to Launch GUI Guider on non-internet connected computer また、インターネット接続していないパソコンからGui Guiderを動かしたいとも思っています。 CAN 解決策を公に共有していただき、皆がSO恩恵を受けられるようにしてください。 よろしくお願いします。
記事全体を表示
NFC Cockpit 下载 大家好!不好意思问个傻问题,请问哪里可以下载适用于我的CLRC 663的NFC Cockpit? 软件页面上找不到相关信息: Screenshot_474.png
記事全体を表示
NXP MIMXRT1062DVL6Bに関するヘルプ/質問 NXP MIMXRT1062DVL6B おもちゃのデザインについて。 ユニット番号:NXP MIMXRT1062DVL6B に関して 強力な600MHz CortexM7を搭載しているので、私には必要以上の性能かもしれません。 私はそれを2語のフレーズを認識するためだけに利用しています。VIT + 2つのマイク+カスタムウェイクフレーズを安定して動作させる、最も安価なNXPプロセッサはありますか? ご相談のため、[email protected]までメールをいただければ幸いです。 Re: NXP MIMXRT1062DVL6B help/questions こんにちは、 @toy_maker さん。 ご質問ありがとうございます! VITが提供するサポート対象部品番号のリストを参照してください。 Gavin_Jia_0-1785724846969.png また、このスレッドの議論も参考になるはずです:https://community.nxp.com/t5/MCX-Microcontrollers/Wake-Word-and-Voice-command-engines/m-p/2054222 MCXNに関する詳細情報については、関連するコミュニティフォーラムに質問を投稿することをお勧めします。ありがとう! よろしくお願いします、 ギャビン
記事全体を表示
LPC55xx API Hello, for a new project I want to use LPC550x microcontroller with IAR Embedded Workbench: in the past I have used other LPC MCU (LPC1317, LPC1788, LPC1788) Now i read everywhere that some functions can be managed only by using API but I don't understand how to use them; are these function available only with MCUXPRESSO? I would like to avoid API and write my own code but I don't fine the C code of these API. For example CAP BANK for oscillators are only documented with API so if I don't use API I can't use these CAP BANK. Is it correct? I have a big confusion in my mind about this. Can anyone help me? It's for my job Best regards. Re: LPC55xx API Hello @Lor75  For newer NXP MCUs, including the LPC55xx series, we recommend using the MCUXpresso SDK drivers, which include both APIs and source code. You can download the SDK from: https://mcuxpresso.nxp.com/builder?hw=LPCXpresso55S06&rel=943  For detailed instructions, please refer to: https://www.nxp.com/document/guide/getting-started-with-the-lpc55s06-evk-evaluation-board:GS-LPC55S06-EVK?section=get-software   Additionally, the LPC55xx series is supported by MCUXpresso IDE, which is free to use with no restrictions on functionality or code size. You can download MCUXpresso IDE from: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE  If still have any question, please feel free to contact me. Thank you.  BR Alice
記事全体を表示
LPC55xx API こんにちは、 新しいプロジェクトでは、LPC550xマイクロコントローラとIAR Embedded Workbenchを使いたいと考えています。過去には他のLPC MCU(LPC1317、LPC1788、LPC1788)を使っていました どこでも「APIでしか管理できない関数もある」と読んだのですが、どう使えばいいのか分かりません。これらの機能はMCUXPRESSOでしか使えないのでしょうか? APIを使わずに自分でコードを書きたいのですが、これらのAPIのC言語コードが見つかりません。例えば、オシレーター用のCAP BANKはAPIでしかドキュメント化されていないので、APIを使わなければこれらのCAP BANKは使えません。それは正しいですか? これについて、私は大きな混乱を抱えています。 どなたか助けてくれませんか?仕事のためです よろしくお願いいたします。 Re: LPC55xx API こんにちは、 @Lor75さん LPC55xxシリーズを含む新しいNXP MCUでは、APIとソースコードの両方を含むMCUXpresso SDKドライバの使用を推奨します。 SDKは以下からダウンロードできます: https://mcuxpresso.nxp.com/builder?hw=LPCXpresso55S06&rel=943  詳細な手順については、以下を参照してください。 https://www.nxp.com/document/guide/getting-started-with-the-lpc55s06-evk-evaluation-board:GS-LPC55S06-EVK?section=get-software さらに、LPC55xxシリーズはMCUXpresso IDEでサポートされており、機能やコードサイズに制限なく無料で使用できます。 MCUXpresso IDEは以下からダウンロードできます: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE  もし質問があれば、どうぞ気軽にお問い合わせください。ありがとう。 BR アリス
記事全体を表示
NXP MIMXRT1062DVL6B 帮助/问题 NXP MIMXRT1062DVL6B 关于玩具设计。 关于您的设备编号:NXP MIMXRT1062DVL6B 它配备了强大的 600MHz CortexM7 处理器,这可能超出了我的需求。 我用它来识别两个单词的短语。NXP 是否有价格最低的处理器能够可靠地运行 VIT + 两个麦克风 + 自定义唤醒词? 欢迎通过电子邮件联系,以便我们进一步讨论:[email protected] Re: NXP MIMXRT1062DVL6B help/questions 嗨@toy_maker , 谢谢你的提问! 请参考VIT提供的受支持零件编号列表。 Gavin_Jia_0-1785724846969.png 此外,这个帖子里的讨论应该会有帮助: https://community.nxp.com/t5/MCX-Microcontrollers/Wake-Word-and-Voice-command-engines/mp/2054222 有关 MCXN 的更多信息,我们建议您在相关的社区论坛中发布您的问题。谢谢你! 此致, 加文
記事全体を表示
NXP MIMXRT1062DVL6B help/questions NXP MIMXRT1062DVL6B regarding toy design. In regards to your unit number: NXP MIMXRT1062DVL6B a powerful 600MHz CortexM7 and it may be more then I need. I am using it to only to recognize a two word phrase. IS there a least expensive NXP processor that can reliably run VIT + two microphones + a custom wake phrase? Would appreciate an email to discuss: [email protected] Re: NXP MIMXRT1062DVL6B help/questions Hi @toy_maker , Thanks for your questions! Please refer to the list of supported part numbers provided by VIT. Gavin_Jia_0-1785724846969.png Also, the discussion in this thread should be helpful: https://community.nxp.com/t5/MCX-Microcontrollers/Wake-Word-and-Voice-command-engines/m-p/2054222 For more information about MCXN, we recommend that you post your question in the relevant community forum. Thank you! Best regards, Gavin
記事全体を表示
NFC Cockpit download Hi all! Sorry for stupid question, but where i can download NFC Cockpit  for my CLRC 663? Cant see on software page : Screenshot_474.png
記事全体を表示
NXP layoffs? Apparently a lot of people were laid off yesterday and more layoffs are coming this week and next. Anyone know anything about this? Power
記事全体を表示
S32DS ARM 2.2 issue windows 11 安装S32DSARM 2.2安装后提示以下错误  也打开不了默认的 工程 Re: S32DS ARM 2.2 issue Hi@yeSerrui 安装完S32 DS,还需要安装RTM SDK,如下所示 Senlent_1-1785739865237.png 在左侧工程浏览框中,右键new可选择自带的例程 Senlent_0-1785739821338.png
記事全体を表示
NFC Cockpitのダウンロード こんにちは、みんな!馬鹿な質問で申し訳ありませんが、CLRC 663用のNFCコックピットはどこでダウンロードできますか? ソフトウェアページには見当たりません: Screenshot_474.png
記事全体を表示
Unable to Launch GUI Guider on non-internet connected computer Hello, my development computer is not connected to the internet. I downloaded GUI Guider and when I launch the program it is looking for a internet connection and wants me to log into my NXP account. Why is it necessary for GUI Guider to have an internet connection to run? Is their a way to launch the tool on a computer that does not have an internet connection? Thanks, Joe Re: Unable to Launch GUI Guider on non-internet connected computer Hi @joseph_lindula  I have already replied to you via email. Thanks for your understanding. BR Harry Re: Unable to Launch GUI Guider on non-internet connected computer I would also like to run Gui Guider from a non internet connected computer. Can you please share the solution publicly so we can all benefit? Thank you.
記事全体を表示
LPC55xx API 你好, 我打算在一个新项目中使用 LPC550x 微控制器和 IAR Embedded Workbench:过去我使用过其他 LPC MCU(LPC1317、LPC1788、LPC1788)。 现在我看到很多资料都说有些功能只能通过 API 来实现,但我不知道该如何使用它们;这些功能是否只有 MCUXPRESSO 才有? 我想避免使用 API 而自己编写代码,但我找不到这些 API 的 C 代码。例如,振荡器的 CAP BANK 仅通过 API 进行了文档说明,因此如果我不使用 API,就无法使用这些 CAP BANK。这样说对吗? 我对此感到非常困惑。 请问有人能帮帮我吗?这是为了我的工作 顺祝商祺! Re: LPC55xx API 你好@Lor75 对于较新的 NXP MCU,包括 LPC55xx 系列,我们建议使用 MCUXpresso SDK 驱动程序,其中包含 API 和源代码。 您可以从以下位置下载 SDK: https://mcuxpresso.nxp.com/builder?hw=LPCXpresso55S06&rel=943  详细说明请参阅: https://www.nxp.com/document/guide/getting-started-with-the-lpc55s06-evk-evaluation-board:GS-LPC55S06-EVK?section=get-software 此外,MCUXpresso IDE 支持 LPC55xx 系列,并且免费使用,对功能或代码大小没有任何限制。 您可以从以下网址下载 MCUXpresso IDE: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE  如果您还有任何疑问,请随时与我联系。谢谢。 BR 爱丽丝
記事全体を表示
NXPのレイオフ? 昨日、多くの人が解雇されたようで、今週と来週もさらに多くの解雇が予定されている。これについて何か知っている人はいますか? パワー
記事全体を表示
无法在未连接互联网的计算机上启动 GUI Guider 你好,我的开发电脑无法连接互联网。我下载了GUI Guider,当我启动该程序时,它正在寻找互联网连接,并希望我登录我的恩智浦账户。为什么 GUI Guider 需要连接互联网才能运行?它们是在没有互联网连接的计算机上上市该工具的一种方法吗? 谢谢! 乔 Re: Unable to Launch GUI Guider on non-internet connected computer 你好@约瑟夫-林杜拉 我已经通过电子邮件回复了您。 感谢您的理解。 BR 哈利 Re: Unable to Launch GUI Guider on non-internet connected computer 我还想在未连接互联网的计算机上运行 GUI Guider。 您能否公开分享一下解决方案,以便我们大家都能受益? 谢谢!
記事全体を表示
恩智浦裁员? 显然,昨天很多人被裁员,而且本周和下周还会有更多人被裁员。有人知道这件事吗? 电源
記事全体を表示