Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
i.MX8QXP-回路図レビュー こんにちは、NXP チームの皆様、 私たちは i.MX8QXP を使用してカスタム ボードを作成しており、回路図部分は完成しています。ピア レビュー用に回路図を非公開で送信するにはどうすればよいでしょうか。 Re: i.MX8QXP-Schematic review こんにちは@abhi400 ! NXP サポートにお問い合わせいただきありがとうございます。 回路図を共有するには、サポート チケットを開き、以下のリンクを使用してファイルをアップロードしてください。 NXPサポート よろしくお願いします、 チャビラ
View full article
看门狗定时器 MIMXRT1042XJM5B 的引脚配置 亲爱的团队 我们在即将到来的项目中使用 MIMXRT1042XJM5B,我们正在寻找 Watch Dog Timer 的引脚排列,在那里可以对其进行配置,请与我们联系 期待您的来信、 此致, Bhavesh Re: Pin configuration for Watch Dog timer MIMXRT1042XJM5B 你好@bhaveshtirex、 非常感谢您关注我们的产品并使用我们的社区。 关于"我们在即将开始的项目中使用 MIMXRT1042XJM5B,我们正在查找 Watch Dog Timer 的引脚输出,它可以在哪里配置" ,在 IMXRT1040RM 中,有一些关于 WDOG 外部信号的说明。 至于如何配置引脚,您可以使用 MCUXPresso IDE 中的引脚工具 希望它能帮到你。 如果您还有疑问,请告诉我。 祝你愉快 敬上 MayLiu
View full article
我在哪里可以买到 NXPS32G 的邮箱和共享内存驱动程序 Arm Cortex-A53 Re: Where do i get the Mailbox and Shared memory Driver for NXPS32G Arm Cortex-A53 嗨,pnp1kor 感谢您与我们联系。 能否向我们提供更多信息? 您使用的是 RDB2 还是 RDB3?您想获得 IPCF 的信息吗? BR 乔伊
View full article
i.MX 8X secure boot - keys for two parties rather than one - Yocto Linux How is the following Secure Boot / Chain of Trust scenario usually handled? What are the precedents? In most of the documentation/examples, the scenario is simple: the same company creates the device and the application software, sells the device with application software on it, and only their keys need to be accommodated. However in our case: we manufacture i.MX 8X based devices. Our customers develop software applications for the devices, and then sell the devices with software to their customers. Our keys are in the AHAB SRK. But we also need to accommodate our customers keys somewhere, so that they can sign their software updates... We supply our customers with the SDK produced by Yocto, and the Linux rootfs. Our customers don't perform Yocto builds themselves. They build their application software using the SDK. What precedents are there for how this scenario is usually handled, in terms of secure boot and whose keys are stored where? What is the terminology for the different parties? Thank you Peter Security Re: i.MX 8X secure boot - keys for two parties rather than one - Yocto Linux Please let me know if you not received yet. Regards Harvey Re: i.MX 8X secure boot - keys for two parties rather than one - Yocto Linux Hi @Harvey021. Thank you. Where can I find the internal system emails please? I've looked under Private Messages / Inbox, but that is empty? Re: i.MX 8X secure boot - keys for two parties rather than one - Yocto Linux Hi  @petero5  I've sent you internal system emails. Regards Harvey Re: i.MX 8X secure boot - keys for two parties rather than one - Yocto Linux Hi @Harvey021 thank you, yes we are using CST with HSM. But are still looking for best practices re chain of trust involving two companies, rather than one: Company A manufactures the device, builds the Yocto SDK and the FIT image, U-Boot, Linux kernel and rootfs. Company B receives the above and develops an application (and creates the application partition). If A writes the SRKs and closes the device, then B can trust that the device and images have not been tampered with on the way to them. But there needs to be a way to enroll B's public key for the application partition, or include that in the chain of trust? Thank you Peter Re: i.MX 8X secure boot - keys for two parties rather than one - Yocto Linux The section <7.3 Using CST with Hardware Security Module> of CST User Guide can be a reference for you. You can download the guide from IMX_CST_TOOL  Regards Harvey
View full article
imxrt1170 EVKB こんにちは、 現在、開発には i.MXRT1170 EVKB を使用しており、ポーリング モードで正常に機能している evkbmimxrt1170_enet_txrx_transfer_cm7_100M の例を使用しています。ただし、代わりに割り込み (ISR) モードで動作するように変更したいと考えています。 これを実装する方法を誰か教えていただけませんか? ご回答をお待ちしています。 Re: imxrt1170 EVKB わかりました。やってみます。 ありがとうございます パルト Re: imxrt1170 EVKB こんにちは、 最新の SDK のすべての関連例については、 https://github.com/nxp-mcuxpresso/mcuxsdk-examples/tree/release/25.06.00/driver_examples/enetをご覧ください。 txrx_multiring_transfer からの割り込みをサポートする例があるようです: https://github.com/nxp-mcuxpresso/mcuxsdk-examples/blob/release/25.06.00/driver_examples/enet/txrx_multiring_transfer/enet_txrx_multiring_transfer.c#L347   しかし、それは 1G enet のようです。https://mcuxpresso.nxp.com/mcuxsdk/latest/html/examples/driver_examples/enet_1g/txrx_multiring_transfer/readme.html
View full article
CD1020 汽车资格证书 CD1020 数据表上报告说:"该恩智浦产品已通过汽车应用认证。" 您是否确认 MC33CD1020AES 符合 AEC-Q100 / Q101 标准?你是否有任何文件证明这一说法? 谢谢! 此致, 安德烈亚 Re: CD1020 automotive qualification 感谢您的咨询。 MC33CD1020AES/R2 设备的认证符合 AEC-Q100G(1 级)标准。 这一点已在 PPAP 中说明。 希望对你有所帮助。
View full article
ウォッチドッグタイマーMIMXRT1042XJM5Bのピン構成 親愛なるチームの皆様、 今後のプロジェクトでMIMXRT1042XJM5Bを使用する予定です。ウォッチドッグタイマーのピン配置を探しています。設定できる場所を教えてください。 ご連絡をお待ちしております。 よろしくお願いいたします。 バヴェシュ Re: Pin configuration for Watch Dog timer MIMXRT1042XJM5B こんにちは@bhaveshtirex 、 弊社の製品にご興味をお持ちいただき、またコミュニティをご利用いただき誠にありがとうございます。 「今後のプロジェクトで MIMXRT1042XJM5B を使用する予定で、ウォッチ ドッグ タイマーを設定 CAN ピン配置を探しています」に関して、IMXRT1040RM には WDOG 外部信号に関する説明がいくつかあります。 ピンの設定方法については、MCUXPresso IDEsのピンツールを使用することができます。 お役に立てれば幸いです。 まだ質問がある場合は、お気軽にご連絡ください。 素敵な一日をお過ごしください! よろしくお願いします メイリュー
View full article
imxrt1170 EVKB 您好, 我们目前正在使用 i.mxrt1170 EVKB 进行开发,并正在使用 evkbmimxrt1170_enet_txrx_txrx_transfer_cm7_100M 示例,该示例在轮询模式下运行良好。不过,我们希望将其修改为在中断(ISR)模式下运行。 有人能指导我们如何实施吗? 谢谢! Re: imxrt1170 EVKB 好的,我会试试的。 谢谢! Parth Re: imxrt1170 EVKB 您好, 请参阅最新 SDK 中的所有相关示例https://github.com/nxp-mcuxpresso/mcuxsdk-examples/tree/release/25.06.00/driver_examples/enet 似乎有一个示例支持来自 txrx_multiring_transfer 的中断:https://github.com/nxp-mcuxpresso/mcuxsdk-examples/blob/release/25.06.00/driver_examples/enet/txrx_multiring_transfer/enet_txrx_multiring_transfer.c#L347   但似乎是 1G enet。 https://mcuxpresso.nxp.com/mcuxsdk/latest/html/examples/driver_examples/enet_1g/txrx_multiring_transfer/readme.html
View full article
KW45 RSSI計算 NXPチームの皆様、こんにちは。 UI アプリケーションを使用してデータを受信しています。ble パケットを送信するペリフェラルからの RSSI 値を計算したいのですが、可能ですか? ペリフェラルから BLE 経由でデータを送信しており、送信 RSSI の意味、つまりペリフェラルから UI アプリに送信しているデータの RSSI 値を計算したいと考えています。 SDKs の例を確認すると、関数が 1 つあります。 #Gap_ReadRssi (デバイスID)を定義します Gap_ReadRadioPowerLevel(g Rssi _c, (デバイスID)) これをペリフェラル側で使用した場合、機能しますか?そうでない場合、ペリフェラル側から RSSI を計算する方法はありますか。   通信と制御(I3C | I2C | SPI | FlexCAN | イーサネット | FlexIO) 開発ボード Re: KW45 RSSI calculation こんにちは、 あなたの調子が良いといいのですが。RSSI (受信信号強度インジケータ) は、トランスミッタではなく、接続のレシーバ側で読み取られます。 Gap_ReadRadioPowerLevel で使用できるさまざまな gapRadioPowerLevelReadType_t を確認できます。 よろしくお願いいたします。 リカルド
View full article
S32G: FreeRTOS SMP サポートに関する質問 こんにちは、チームの皆さん お客様: クアンタ プラットフォーム: S32G3 モジュール: FreeRTOS SMP サポート Quanta は、 FreeRTOS_4_0_3_CD3パッケージに SMP サポート付きの FreeRTOS v11 の例を投資しており、S32G3 Cortex-M7 プラットフォームでの SMP サポートの実装の詳細を知りたいと考えています。 1. S32G3 の Cortex-M7 コアで SMP を有効にして管理する方法。 2. SMP サポートの実際の範囲はどの程度ですか (例: タスクのスケジュール設定、同期、コア間通信)。 3. キャッシュ コヒーレンスがハードウェアでサポートされているか、または実装でキャッシュを完全に無効にする必要があるかどうか。 どうぞよろしくお願いいたします。 よろしくお願いいたします。 レオ RTOS Re: S32G: Questions about FreeRTOS SMP support こんにちは@congnguyenhuu @lequana2 サポートありがとうございます。これらの回答をお客様にフィードバックします。 BR、 レオ Re: S32G: Questions about FreeRTOS SMP support こんにちは@LeoLiAPこの情報はあなたの質問に対する解決策であるとマークしておきます。不明な点があればフィードバックしていただければマークを外します。 Re: S32G: Questions about FreeRTOS SMP support こんにちは@LeoLiAP 、 1.リリース4.0.3CD3 には、SMP の組み込みサポートを提供する S32DS サンプルFreeRTOS_SMP_Example_S32G399が含まれています。SMP を有効にするために追加の構成は必要ありません。S32DS構成で SMP の有効化と管理が実行され、すぐに使用できます。 2. S32G SMP は、タスク スケジューラ、キュー、セマフォなどの API をサポートします。 コア間通信では、コア間の信号伝達、コアの再スケジュールのトリガーにコア間割り込みを使用しますが、ストリーム バッファー、メッセージ バッファー API はまだサポートされていません。 上記に記載されていない残りの API については、まだテストが行われておらず、動作が保証されていません。 3. キャッシュを有効にすると、S32G SMP CAN が動作します。 FPU が有効になっている場合はサポートされません。 ご質問がありましたら、どうぞお気軽にお尋ねください。 よろしくお願いします、 コング
View full article
S32K118 中的非对称算法库支持 你好 要使用带有 cSec 部分的 S32K118,我想知道恩智浦是否为非对称网络安全算法提供了任何库,(主要需要 ed25519ph) 如果是,我可以从哪里快速集成并进行烟雾测试和性能检查。 如果没有,是否有适用于 S32K118 的第三方库? 谢谢您! Re: asymmetric algorithm library support in S32K118 嗨@zzzzz 恩智浦 S32K1 系列微控制器中的 cSEC(加密服务引擎——压缩)模块不支持任何非对称加密算法,包括 RSA、ECC、Ed25519 等。 1.网上有很多实现 Ed25519ph 的轻量级 C 语言库,但由于我们没有测试过,所以不能向您推荐。 2。如果性能或网络安全要求很高,可以考虑通过 SPI/I2C 接口连接支持非对称加密的外部安全芯片(例如恩智浦 A71CH 或 ATECC608A)。
View full article
S32G:有关 FreeRTOS SMP 支持的问题 各位队员好、 客户:广达 平台:S32G3 模块:FreeRTOS SMP 支持 广达正在我们的FreeRTOS_4_0_3_CD3代码包中投资支持SMP的FreeRTO S v11示例,他们想知道在 S32G3 Cortex-M7平台上支持SMP的实现细节。 1.如何在 S32G3 的 Cortex-M7 内核上启用和管理 SMP; 2. SMP 支持的实际范围(如任务调度、同步、内核间通信); 3. 硬件是否支持高速缓存一致性,或者实施过程中是否需要完全禁用高速缓存。 提前感谢您的支持。 顺祝商祺! 狮子座 实时操作系统 Re: S32G: Questions about FreeRTOS SMP support 你好@congnguyenhuu @lequana2 感谢您的支持。我会将这些答复反馈给客户。 BR、 狮子座 Re: S32G: Questions about FreeRTOS SMP support 你好@LeoLiAP我将标记此信息为您问题的解决方案。如果有不清楚的地方,请反馈给我,我将取消标记。 Re: S32G: Questions about FreeRTOS SMP support 你好@LeoLiAP、 1. 随着 4.0.3 版本的发布CD3,我们加入了 S32DS 示例 FreeRTOS_SMP_Example_S32G399,它为 SMP 提供了内置支持。启用 SMP 无需额外配置,只需在 S32DS 配置中启用和管理 SMP 即可使用。 2.S32G SMP 应支持任务调度器、队列和 Semaphore 等 API。 对于内核间通信,使用内核间中断进行内核间信号,触发信号重新调度内核,尚不支持流缓冲区、消息缓冲区 API。 以上未提及的其余 API 我们尚未测试,不能确保正常工作。 3.启用缓存后,S32G SMP 可正常工作。 启用 FPU 时不支持。 欢迎你们提出任何问题。 致以最崇高的敬意, Cong
View full article
NXPS32G Arm Cortex-A53用のメールボックスと共有メモリドライバはどこで入手できますか? Re: Where do i get the Mailbox and Shared memory Driver for NXPS32G Arm Cortex-A53 こんにちは、 pnp1kor お問い合わせいただきありがとうございます。 さらに詳しい情報を教えていただけますか? RDB2 と RDB3 のどちらを使用していますか?IPCF の情報を取得しますか? BR ジョーイ
View full article
imxrt1170 EVKB Hi, We are currently using the i.MXRT1170 EVKB for our development and working with the evkbmimxrt1170_enet_txrx_transfer_cm7_100M example, which is functioning well in polling mode. However, we would like to modify it to operate in interrupt (ISR) mode instead. Could someone guide us on how to implement this? Thank you! Re: imxrt1170 EVKB Okay, i will try that. Thanks, Parth Re: imxrt1170 EVKB Hi, Please see All related examples from the latest SDK https://github.com/nxp-mcuxpresso/mcuxsdk-examples/tree/release/25.06.00/driver_examples/enet  It seems there is an example which supported Interrupt from txrx_multiring_transfer:  https://github.com/nxp-mcuxpresso/mcuxsdk-examples/blob/release/25.06.00/driver_examples/enet/txrx_multiring_transfer/enet_txrx_multiring_transfer.c#L347    But it seems for 1G enet. https://mcuxpresso.nxp.com/mcuxsdk/latest/html/examples/driver_examples/enet_1g/txrx_multiring_transfer/readme.html 
View full article
CD1020 オートモーティブ資格 CD1020 のデータシートには、次のように記載されています。「この NXP 製品は、オートモーティブ アプリケーションでの使用が認定されています。」「 MC33CD1020AES が AEC-Q100 / Q101 認定を受けていることを確認していますか?この声明が記された文書はありますか? ありがとうございます よろしくお願いいたします。 アンドレア Re: CD1020 automotive qualification お問い合わせいただきありがとうございます。 MC33CD1020AES/R2 デバイスの認定は、AEC-Q100G (グレード 1) に準拠しています。 これはPPAPに記載されています。 お役に立てれば幸いです。
View full article
i.MX8QXP-系统回顾 您好,NXP团队: 我们正在使用i.mx8QXP制作定制板,原理图部分已经完成了,我怎样才能私下发送原理图供同行评审。 Re: i.MX8QXP-Schematic review 你好@abhi400! 感谢您联系恩智浦支持中心! 要共享您的原理图,请打开支持票据并使用下面的链接上传文件: 恩智浦支持 致以最崇高的敬意, Chavira
View full article
i.MX 8X 安全启动-两方而不是一方的密钥-Yocto Linux 通常如何处理以下安全启动/信任链场景?有什么先例? 在大多数文档/示例中,场景很简单:同一家公司创建设备和应用程序软件,出售带有应用程序软件的设备,只需要存放密钥。 但是,就我们而言:我们生产基于i.MX 8X的设备。我们的客户为设备开发软件应用程序,然后将带有软件的设备出售给客户。 我们的钥匙在 AHAB SRK。但是,我们还需要在某个地方为客户提供密钥,以便他们可以签署软件更新... 我们为客户提供 Yocto 开发的 SDK 和 Linux rootfs。我们的客户不会自己执行 Yocto 版本。他们使用 SDK 版本应用程序软件。 就安全启动以及谁的密钥存储在哪里而言,通常如何处理这种情况有哪些先例?各方的术语是什么? 谢谢 Peter 安全 Re: i.MX 8X secure boot - keys for two parties rather than one - Yocto Linux 如果您还没有收到,请通知我。 此致 哈维 Re: i.MX 8X secure boot - keys for two parties rather than one - Yocto Linux 嗨,@Harvey021。谢谢。请问在哪里可以找到内部系统邮件?我查看了 "私人信息"/"收件箱",但里面是空的? Re: i.MX 8X secure boot - keys for two parties rather than one - Yocto Linux 你好@petero5 我已向您发送了内部系统邮件。 此致 哈维 Re: i.MX 8X secure boot - keys for two parties rather than one - Yocto Linux 你好@Harvey021谢谢,是的,我们使用的是带有 HSM 的 CST。 但我们仍在寻找最佳实践,即涉及两家公司而不是一家公司的信任链: A 公司制造该设备,构建 Yocto SDK 和 FIT 映像、U-启动、Linux 内核和 rootfs。 B 公司收到上述内容并开发应用程序(并创建应用程序分区)。 如果 A 写入 SRK 并关闭设备,则 B 可以相信设备和图像在发往它们的途中没有被篡改。 但是否需要一种方法来为应用分区注册 B 的公钥,或者将其纳入信任链? 谢谢 Peter Re: i.MX 8X secure boot - keys for two parties rather than one - Yocto Linux <7.3将 CST 与 CST 用户指南的硬件网络安全模块 > 一起使用可以作为参考。 您可以从IMX_CST_TOOL下载指南。 此致 哈维
View full article
MCXA153 ADC 触发信号 尊敬的各位, 我正在开发一个基于 MCXA153VLH 微处理器的项目。 它需要定期对输入的模拟电压进行采样。我想用计时器来触发信号 ADC 开始转换。 我知道 MCXA153VLH 微处理器的 ADC 模块最多支持 4 个硬件触发信号,但我无法弄清楚硬件外设与其特定触发信号之间的对应关系。 通过分析 SDK 提供的演示软件,我了解到触发信号 1 与引脚生成的 IRQ 相关联。哪个触发信号与计时器相关联? 感谢您的帮助与合作 问好 Re: MCXA153 ADC TRIGGER 你好@_Ferrari_ 很抱歉这么晚才回复您。 幸运的是,我已经在你的另一个主题中为你解答了这个问题。 如果还有人遇到同样的问题,请参阅: https://community.nxp.com/t5/MCX-Microcontrollers/MCXA153VLH-ADC-trigger/td-p/2155041 BR 爱丽丝
View full article
Where do i get the Mailbox and Shared memory Driver for NXPS32G Arm Cortex-A53 Re: Where do i get the Mailbox and Shared memory Driver for NXPS32G Arm Cortex-A53 hi,pnp1kor Thank you for contacting us. Could you please share more information to us? are you using the RDB2 or RDB3? Do you want to get the information of IPCF? BR Joey 
View full article
S32G: Questions about FreeRTOS SMP support Hi Teams, Customer: Quanta Platform: S32G3 Module: FreeRTOS SMP support The Quanta is investing example of FreeRTOS v11 with SMP support in our FreeRTOS_4_0_3_CD3 package and they would like to know implementation details of SMP support on the S32G3 Cortex-M7 platform. 1. How SMP is enabled and managed on the Cortex-M7 cores of the S32G3; 2. What is the actual extent of SMP support (e.g., task scheduling, synchronization, inter-core communication); 3. Whether cache coherence is supported by hardware, or if the implementation requires disabling caches entirely. Thanks for your support in advance. Best Regards, Leo RTOS Re: S32G: Questions about FreeRTOS SMP support Hi @congnguyenhuu @lequana2  Thanks for your support. I will feedback these answer to customer.  BR, Leo Re: S32G: Questions about FreeRTOS SMP support Hi @LeoLiAP I shall mark this information is solution for your question. If any unclear, please feedback and I shall unmark it. Re: S32G: Questions about FreeRTOS SMP support Hi @LeoLiAP , 1. With release 4.0.3 CD3, we’ve included the S32DS sample FreeRTOS_SMP_Example_S32G399, which provides built-in support for SMP. No additional configuration is required to enable SMP, enabling and managing SMP done on S32DS configuration, it's ready to use. 2. S32G SMP shall be supported APIs task scheduler, Queue and Semaphore. For inter-core communication, used inter-core interrupts for signaling between cores, triggering rescheduling cores, haven't yet supported Stream Buffer, Msg Buffer APIs. The remaining APIs that are not mentioned above, we have not tested yet, not ensure working.  3. S32G SMP can work when enabling cache. Not support with FPU enabled. You're welcome to bring up any questions. Best Regards, Cong
View full article