Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
FreeMaster 无法集成 GUI Guider。 各位 FreeMASTER 网页上指出 GUI Giider 支持在 FreeMASTER 中创建小部件,但目前可用的 FreeMASTER 版本为 2.01,并且视频中也提到了这一点: https://community.nxp.com/t5/MCUXpresso-Training-Hub/FreeMASTER-Gui-Guider-integration/ta-p/1924225 请说明如何将 GUI Guider 集成到 FreeMASTER 中,但是 GUI Guider 2.01 中既没有“FreeMASTER 服务器链接”,也没有任何关于 FreeMASTER 配置的参考资料。此外,FREEMaster 不支持 NODE Red(仅轻量版支持)。所以,在FreeMaster中无法创建美观的小部件。 这样说对吗? 看待 保罗 FreeMASTER 中是否可以使用 GUI Guider?如果可以,该如何操作?你能帮我找到相关的视频/应用说明吗? 谢谢 保罗
查看全文
Kinetis (KW3x/4x, MCX W7x and MCX W23) One Wireless Connectivity Power Profile Tool This page is dedicated to the Kinetis (KW3x/4x, MCX W7x & MCX W23) One Connectivity Power Profile Tool. It contains all different standalone connectivity power profiling tools in one. It will help you to estimate the power consumption in your application (Automotive or IIoT) and evaluate the battery life time of your solution. This page content a dedicated power profile tool 'One Wireless Connectivity Power Profiling Tool' which includes: Bluetooth LE : Available in this new tool New: KW43 (Automotive) and MCX W70 (IIoT) products in standalone based on simulation. Products will be available begin 2027. KW3x/KW4x (Automotive) and MCX W7x (IIoT) products in standalone. MCX W23 (IIoT) product in standalone. K32W0/QN9090, KW41, QN9080 products in standalone. MCX W71 & W72 product in standalone (IIoT). 802.15.4 Matter & ZED : Available in this new tool. MCX W71 & W72 product in standalone (IIoT). New: MCX W70 product in standalone (IIoT) based on simulation. Bluetooth LE Channel Sounding Localization (Automotive): Available in this new tool. SmartFob application (Automotive): BLE/KW45/47 + UWB Ranger4/5 + SE + motion sensor: Available in this new tool. Active anchor use case (Automotive): BLE CS (KW47) Anchor + Digital Key or Keyfob : Available in this new tool. Save the OneConnectivity_Power_profiling_tool_SDK_26_06_date.zip file in your disk, unzip it and launch One_Wireless_Connectivity_Power_profiling_tool_SDK_26_06.html. page overview: Product: JN518X Product: K32W0 Product: K32W1 Product: KW 34|35|36 Product: KW 37|38|39 Product: KW41Z |31Z | 21Z Product: QN9080|SIP Product: QN9090|30 Product: UWB NCJ29D5 Protocol: BLE -> connectivity Protocol: Matter Protocol: Zigbee Re: Kinetis (KW3x/4x, MCX W7x and MCX W23) One Wireless Connectivity Power Profile Tool Hi @stephen_t , Application Note is on the way to explain how to use this new tool. Find a draft version attached. It covers Bluetooth LE part for the moment. Re: Kinetis (KW3x/4x, MCX W7x and MCX W23) One Wireless Connectivity Power Profile Tool Hello , Suppose if we need to design a digital keyfob which combine KW45+NCJ29D5/6+SecureEngine how to use this tool. Any guidance document avatilable will be helpful. Re: Kinetis (KW3x/4x, MCX W7x and MCX W23) One Wireless Connectivity Power Profile Tool @christophe_menard  Thank you very much  for the draft document , will be interested in the final version also as it will help to correctly configure UWB and SE. Regards Stephen
查看全文
NDA Question Hello NXP, Can only companies apply for NDA for SJA1105PQRS_SDS datasheet ? I'm an independent developing motor controls solutions. I may form a company in the future.
查看全文
S32K344 Kicadの記号とパッケージ こんにちは、 S32K344 MCUファミリー用のKiCadライブラリ(回路図記号、フットプリント、3Dモデル(STEP)などは利用可能でしょうか? ありがとう。 Re: S32K344 Kicad symbols and footprints ありがとう。 そこで、kicadのシンボル、フットプリント、3Dモデルを自分で設計しなければならないと考えています。 Re: S32K344 Kicad symbols and footprints こんにちは、 @manu_fenixecu さん。 S32K3の場合、CADENCE Allegro用の3D STEPファイルや記号とパッケージを提供しています。ハードウェア設計パッケージでご覧いただけます: https://www.nxp.com/webapp/Download?colCode=S32K3_HW-DesignPackage よろしくお願いいたします。 ルーカス
查看全文
S32K344 KiCad符号和封装 你好, 是否有适用于 S32K344 MCU 系列的 KiCad 库,包括原理图符号、封装和 3D 模型(STEP)? 谢谢。 Re: S32K344 Kicad symbols and footprints 谢谢。 所以我想我必须自己设计 KiCad 符号、封装和 3D 模型。 Re: S32K344 Kicad symbols and footprints 你好@manu_fenixecu 对于 S32K3,我们提供 CADENCE Allegro 的 3D STEP 文件、符号和封装。可以在硬件设计包中找到: https://www.nxp.com/webapp/Download?colCode=S32K3_HW-DesignPackage 此致, Lukas
查看全文
PTN3460 支持 大家好, PTN3460I 的数据手册中提到了“I2C 总线实用程序和固件及 EDID 更新编程指南”文档。我找不到与I2C总线实用程序和EDID更新工具相关的文档。 此外,我们能否使用 DP Aux 刷新 PTN3460I 的内部闪存?如果是这样,是否有相应的工具?PTN3460(Flash-over-AUX)工具仅用于固件更新,还是也可用于EDID更新? Re: PTN3460 Support 您好, PTN3460I 数据手册中引用的文档“I2C 总线实用程序和固件及 EDID 更新编程指南”对应于 AN11606 – PTN3460I 编程指南(适用于 PTN3460I)和 AN11128 – PTN3460 编程指南(适用于商用 PTN3460)。两者均可在NXP.com上公开获取: AN11606 – PTN3460I 编程指南(修订版 1.4) — 涵盖 I²C 总线配置表结构、EDID 编程(最多 7 个 EDID 数据结构)、所有寄存器定义,以及通过 I²C 将 EDID 和配置数据写入 PTN3460I 内部闪存的逐步程序。 AN11128 – PTN3460 编程指南(修订版 1.8) — 商用 PTN3460BS 变体的等效文档。 关于您提出的有关 DP AUX 接口和 Flash-over-AUX (FoA) 工具的问题: 通过 DP AUX 接口对内部闪存进行编程:是的,PTN3460I 支持通过 DP AUX 通道对其内部闪存进行编程。可以通过 I²C 总线接口或 DP AUX 访问寄存器。 Flash-over-AUX (FoA) 工具范围:PTN3460/PTN3460I 有两种独立的 FoA 工具: FoA 固件更新程序(PTN3460IBS 固件 F2 的独立工具)——专门用于通过 DP AUX 通道进行固件版本升级。 FoA EDID 更新程序 — 一个专门用于通过 DP AUX 通道进行 EDID 更新的独立实用程序。 请查收下方附件。 BRs,托马斯
查看全文
CLEV6630B eval board(OM26630FDK) I got PDf files of CLEV6630B eval board(OM26630FDK) can I get altium pcb files of the same for use in our custom design? Re: CLEV6630B eval board(OM26630FDK) Hello @R_Tony, Hope you are doing well. My apologies, the only design files available for this device are the CLRC6630B schematics and layout, available in PDF format. I apologize for the inconvenience. Regards, Eduardo.
查看全文
FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external device; Subject: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external device; suspect conflict with onboard tri-radio module (MAYA-W27x) Hi NXP team, I'm trying to bring up an external SPI device (Waveshare 2-CH CAN HAT(https://www.waveshare.com/wiki/2-CH_CAN_HAT), dual MCP2515) on the FRDM-IMX93 board's EXPI 40-pin header (P11), using LPSPI3 (GPIO_IO08–11, matching the RPi-compatible pin positions). I've confirmed the HAT itself is fully functional (tested and working on a genuine Raspberry Pi with the standard dtoverlay=mcp2515 configuration). Board / BSP: FRDM-IMX93, model NXP FRDM-IMX93 NXP i.MX Release Distro 6.18-whinlatter, kernel 6.18.2-1.0.0-gf49f45233f7b What I've configured (all verified correct at the device tree level): Overlay adds mcp2515@0/mcp2515@1 under &lpspi3, with cs-gpios = <&gpio2 8 1>, <&gpio2 7 1>; (GPIO_IO08/GPIO_IO07), matching the GPIO-based CS pattern I found in NXP's own upstream patch for a similar FRDM-IMX93 SPI3 peripheral (pixpaper display overlay). Extended &pinctrl_lpspi3 to mux GPIO_IO07 (CS1) as GPIO, since it was previously (MUX UNCLAIMED) in /sys/kernel/debug/pinctrl/. Disabled the pre-existing spidev0 node that was conflicting with CS0. Enabled reg_vexp_3v3/reg_vexp_5v (regulator-always-on) — these were disabled by default and the EXPI header had no power without this. Confirmed /dev/spidev2.0 is created and pinmux shows correct function assignment (lpspi3grp) on all 4 SPI pins. Symptom: mcp251x driver always fails: spi2.0: Cannot initialize MCP2515. Wrong wiring? (err=19) and spi2.1: MCP251x didn't enter in conf mode after reset (err=110) — completely unchanged across every device-tree variation above. Raw SPI-level test with spidev_test (compatible lwn,bk4) on /dev/spidev2.0: RX buffer returns byte-for-byte identical data regardless of whether MOSI/MISO are physically shorted (loopback), left open, or bridged with a shunt. This suggests the SPI3 signals present at P11 header pins 19/21/23/24 are not being reflected in the controller's actual bus activity — i.e., the signals may not be reaching the header at all, or something else is interfering. Suspected root cause: Per UM12181 (FRDM-IMX93 Board User Manual, Section 2.11 "Tri-radio module interface"), the SPI3 signals (CLK, MOSI, MISO, CS0 — multiplexed on GPIO_IO08-11) are shared between the onboard MAYA-W27x tri-radio module and the M.2 connector, via a bidirectional 1.8V level translator (U729), resistor-selected. The document doesn't clarify whether/how the EXPI header (P11) is electrically isolated from this shared path when SPI3 alternate function is driven from the SoC side. Question: Is P11's exposure of GPIO_IO08-11 electrically independent of the U729 translator/tri-radio path, or does using SPI3 on P11 require any additional configuration (e.g., disabling the tri-radio module, GPIO expander bits, or resistor rework) to route/isolate the signal to the header correctly? Is there a validated reference device tree (similar to imx93-11x11-evk-lpspi.dts for the EVK) for using LPSPI3 externally on the FRDM-IMX93 board specifically? Could a schematic excerpt for the SPI3/U729 signal path be shared to confirm the P11 connection topology? Thanks in advance for your help. Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi FRDM-IMX93: No signal is output to the LPSPI3 (P11 EXPI header) SCK pin Issue I am trying to operate an external SPI device (2× MCP2515 CAN) using LPSPI3 (GPIO_IO08-11, spi@42550000) on the P11 EXPI header. The driver is active, and the peripheral appears to be running “internally,” but no signal is being output to the physical SCK pin (GPIO_IO11). Evidence The overlay is applied without errors; spi2.0/spi2.1 are registered in the SPI core. Power, pinctrl, pinctrl-assert-gpios, cs-gpios, and clock source—all are correct and have been verified. CS0 (same bank, GPIO alternate function, mode=0) works flawlessly—pulses are visible with both a multimeter and a logic analyzer. SCK (mode=1, native LPSPI3_SCK) is completely flat/0V on the logic analyzer—whether the HAT is connected or not, it makes no difference in the continuous trigger loop. Nevertheless, LPSPI3’s IRQ (GIC 97) is actually being triggered in /proc/interrupts (a single transfer attempt generated over 220 interrupts) — the peripheral’s internal logic (status/IER registers) is active. Reading the LPSPI3 base address (0x42550000) with /dev/mem returns a “Bus error” — but flexcan2 (0x425b0000), which is running on the same bus, also returns the same error, meaning this is a general /dev/mem limitation, not specific to LPSPI3 (ruled out via the control group). The DMA theory was tested and ruled out: when overriding dmas with an invalid phandle, the driver fell back to PIO with the message “dma setup error -19, use pio,” but the SCK signal still did not appear. The `clk_ignore_unused` boot argument also made no difference. Conclusion The internal logic of the LPSPI3 peripheral is working (generating interrupts), but the SCK signal never reaches the external pin (GPIO_IO11)—while CS0 (GPIO mode) in the same pinctrl group outputs correctly, SCK (native LPSPI3 alternate function) does not. This appears to point to a configuration detail related to the pad driver/silicon or a configuration detail that NXP should be aware of, which cannot be explained by the device tree or software. Question On the FRDM-IMX93, is there an additional hardware/firmware enable step outside the device tree for LPSPI3_SCK (GPIO_IO11, native alternate function) via P11? There is a known example where LPSPI3 works with the same pins on the i.MX93 EVK (community.nxp.com/t5/i-MX-Processors/iMX93AUTO-EVK-SPI-Configuration-for-QCA7006AQ)—could there be a difference specific to the FRDM? Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi If anything is missing, I can add it. root@imx93-11x11-lpddr4x-frdm:/sys/firmware/devicetree/base# ls '#address-cells' clock-osc-24m firmware mcp2515_clock pmu regulator-hmisc-vddio regulator-vexp-3v3 soc@0 usbphynop2 '#size-cells' clock-osc-32k imx93-lpm memory psci regulator-usdhc2 regulator-vexp-5v sound-mqs usdhc3_pwrseq __symbols__ compatible interrupt-controller@48000000 model regulator-adc-vref regulator-usdhc3 remoteproc-cm33 sw-keys aliases cpus interrupt-parent mqs1 regulator-avdd regulator-vdd-12v reserved-memory thermal-zones chosen display-subsystem ldb-display-controller mqs2 regulator-can2-stby regulator-vdd-5p0v secure-enclave timer clock-ext1 ethosu ldb-phy name regulator-dvdd regulator-vddo serial-number usbphynop1 Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi No, the imx93-11x11-frdm.dts file is the original; I edited the mcp2515-can-hat.dtbo overlay file, https://www.waveshare.com/wiki/2-CH_CAN_HAT, I only changed INT_1 from the default GPIO_25 to GPIO_24 (physical pin 18). Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi Hello @irfanktm  Hope you are doing very well. Actually, there are a direct connections between the i.MX93 FRDM PADs and the P11 GPIO_IO08-IO11 Pines: Manuel_Salas_0-1789421014211.pngManuel_Salas_0-1789421014211.pngManuel_Salas_0-1789421014211.pngManuel_Salas_0-1789421014211.pngManuel_Salas_0-1789421014211.pngManuel_Salas_0-1789421014211.pngManuel_Salas_0-1789421014211.pngManuel_Salas_0-1789421014211.png Could you please share steps to reproduce it by my side? Best regards, Salas. Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi Hello @irfanktm  I just made some test by my side: Manuel_Salas_0-1789495251012.pngManuel_Salas_0-1789495251012.pngManuel_Salas_0-1789495251012.pngManuel_Salas_0-1789495251012.pngManuel_Salas_0-1789495251012.pngManuel_Salas_0-1789495251012.pngManuel_Salas_0-1789495251012.png SPI us working well in my i.MX93 FRDM. Manuel_Salas_1-1789495295645.pngManuel_Salas_1-1789495295645.pngManuel_Salas_1-1789495295645.pngManuel_Salas_1-1789495295645.pngManuel_Salas_1-1789495295645.pngManuel_Salas_1-1789495295645.pngManuel_Salas_1-1789495295645.png I have the same environment as you. One more question. Do yo have voltage in your 3V3 and 5V pines of the i.MX93 FRDM board? If not, please take a look to the below link to enable the regulators of the board: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Enable-3-3-V-and-5-V-Regulators-for-Expansion-Header-on-i-MX9/ta-p/2299415 Best regards, Salas. Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi According to the logs, it makes me think you are trying to access to the SPI device over spidev_test, but the device is being handle by the MCP driver. What I need to know is the entire device tree (.dts) that you are using, like: imx93-11x11-frdm.dts Also, if you modified it, please let me know your modifications. Also, I will try to get an mcp2515 CAN module to try the integration by my side. Best regards, Salas. Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi Please kindly share your entire device tree. Or just the related to the lpspi3 node and pinmux. Best regards, Salas. Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi Yes, I have 3.3v and 5V at the p11 header, Why I have errors? imx93-11x11-lpddr4x-frdm login: root root@imx93-11x11-lpddr4x-frdm:~# dmesg | grep -iE 'mcp251|lpspi3' [ 8.989639] mcp251x: no symbol version for module_layout [ 10.032864] mcp251x spi2.1: MCP251x didn't enter in conf mode after reset [ 10.033021] mcp251x spi2.1: Probe failed, err=110 [ 10.033034] mcp251x spi2.1: probe with driver mcp251x failed with error -110 [ 10.074097] mcp251x spi2.0: Cannot initialize MCP2515. Wrong wiring? [ 10.074256] mcp251x spi2.0: Probe failed, err=19 root@imx93-11x11-lpddr4x-frdm:~# ip link show 1: lo: mtu 65536 qdisc noqueue state UNKNOWN mode DEFAULT group default qlen 1000 link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00 2: eth0: mtu 1500 qdisc mq state DOWN mode DEFAULT group default qlen 1000 link/ether 90:a9:f7:80:42:26 brd ff:ff:ff:ff:ff:ff 3: eth1: mtu 1500 qdisc mq state DOWN mode DEFAULT group default qlen 1000 link/ether 90:a9:f7:80:42:27 brd ff:ff:ff:ff:ff:ff 4: mlan0: mtu 1500 qdisc mq state UP mode DORMANT group default qlen 1000 link/ether 80:a1:97:50:4e:0d brd ff:ff:ff:ff:ff:ff 5: uap0: mtu 1500 qdisc noop state DOWN mode DEFAULT group default qlen 1000 link/ether 82:a1:97:50:4f:0d brd ff:ff:ff:ff:ff:ff 6: wfd0: mtu 1500 qdisc noop state DOWN mode DEFAULT group default qlen 1000 link/ether 82:a1:97:50:4e:0d brd ff:ff:ff:ff:ff:ff 7: can0: mtu 16 qdisc noop state DOWN mode DEFAULT group default qlen 10 link/can Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi Technical Support Request — MCP2515 on i.MX93 LPSPI3 Multiple MCP2515 CAN controllers (3 units tested, 2 different manufacturers/boards, 8/16 MHz crystals) connected to an i.MX93-11X11-LPDDR4X-FRDM board via LPSPI3 (SPI2) intermittently fail to reach Configuration mode after reset (CANSTAT should read 0x80). Environment: kernel 6.18.2 (NXP downstream), CONFIG_SPI_FSL_LPSPI built-in, ERR051608 prescale fix present. Device tree / pinctrl verified correct (LPSPI3 SIN/SOUT/SCK properly muxed, CS via cs-gpios). Logic-analyzer captures confirm MOSI/SCK/CS are generated correctly and consistently by the host. Key observation: On a freshly opened spidev handle, the very first RESET + CANSTAT read succeeds (~0x80) roughly 50–60% of the time, with consistent ~2–6 ms timing. If additional RESET+read cycles are issued on the same, still-open SPI file descriptor, they consistently fail afterward, settling into a repeatable ~10–11 ms periodic pattern of fixed values (0x00 / 0xFF / 0xFB) that never reaches 0x80 again. This same failure signature is reproduced across all 3 physical MCP2515 units and 2 different board designs, ruling out a single defective chip/module. Adding inter-transfer delay (delay_usecs), a dummy 'flush' SPI transfer, and increasing the gap between cycles to 100 ms did not change the outcome (0/10 success once the pattern starts). VDD, GND, RESET pin and idle MISO level are all confirmed healthy (3.3 V) throughout. The mainline mcp251x kernel driver's own probe() shows the same instability: 5 consecutive bind attempts (unbind/clear driver_override/bind) all failed, alternating between err=-19 ("Wrong wiring?") and err=-110 ("didn't enter in conf mode after reset") in a regular, non-random pattern. This pattern (good on first transfer after open, then a fixed repeatable failure signature on subsequent transfers within the same session — reproduced by the kernel driver's own probe as well) suggests a state that is not being fully cleared between consecutive LPSPI3 transfers/CS cycles, rather than a defect in the MCP2515 units themselves. Question for NXP: is this consistent with a known LPSPI3 (i.MX93) behavior — e.g. FIFO/CS state not resetting cleanly between back-to-back transfers on the same SPI file descriptor — and is there a recommended driver-level workaround (e.g. required delay, FIFO flush, or CS handling) beyond ERR051608? Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi Technical Support Request MCP2515 (Microchip) SPI communication failure on i.MX93 (NXP) SPI2/LPSPI3 1. Summary Two MCP2515 CAN controllers (Waveshare 2-CH CAN HAT, MCP2515-I/SO, 16 MHz crystal) connected to an i.MX93-11X11-LPDDR4X-FRDM board via LPSPI3 (SPI2, CS0/CS1) never enter Configuration mode after power-up or SPI/hardware reset. All register reads return fixed, non-varying values instead of the expected CANSTAT = 0x80. The kernel mcp251x driver consistently reports probe failure (err=-110 "didn't enter in conf mode after reset", or err=-19 "Wrong wiring?"). 2. Environment SoM/board: i.MX93-11X11-LPDDR4X-FRDM Kernel: 6.18.2-1.0.0-gf49f45233f7b (NXP downstream), CONFIG_SPI_FSL_LPSPI=y (built-in), ERR051608 prescale fix already present SPI bus: LPSPI3 (spi@42550000), 2 chip selects, custom device tree overlay (16 MHz fixed-clock, IRQ GPIO3-23 / GPIO3-24) CAN modules: Waveshare 2-CH CAN HAT, MCP2515-I/SO, marking "E3 2335BK5" (genuine Microchip marking format) Driver: mcp251x (mainline), tested against kernel driver and a custom spidev-based test utility 3. Troubleshooting performed Corrected device tree overlay target (&spi1/&lpspi3 vs. incorrect &spi2 label) — overlay now applies correctly, mcp2515 child nodes present in live DT Verified LPSPI3 pinctrl, cs-gpios, interrupt-parent/GPIO mapping against running device tree — all correct Verified master-side SPI signal integrity with a logic analyzer: MOSI, SCK and CS are generated correctly and consistently by the i.MX93 in several captures Confirmed VDD = 3.3V and idle MISO = 3.3V on both CAN modules (no short to GND) Confirmed RESET pin (pin 17, SOIC-18) = 3.3V (inactive) on both modules Tested SPI Mode 0,0 and Mode 1,1 (CPOL/CPHA), 100 kHz-8 MHz clock — no change in behavior Added 10k pull-up resistors on CS0/CS1 to resolve MISO bus contention between the two parallel MCP2515 devices — this stabilized (but did not correct) the readback data Custom spidev test tool: RESET instruction + immediate/continuous CANSTAT polling (1 ms interval, 300 ms window) after reset — CANSTAT settles instantly to a fixed value and never reaches 0x80 Forced WRITE to CANCTRL (0x80) followed by READ — readback is unaffected by the write, indicating the SPI transaction is not being processed by the CAN controller logic 4. Key observation CS0 device: CANSTAT/CANCTRL/all registers consistently read back 0x00 (100% repeatable across dozens of reset+read cycles, independent of register address, SPI mode, or written value). CS1 device: CANSTAT/CANCTRL/all registers consistently read back 0xFF (100% repeatable, MISO never toggles during the transaction). Both devices show clean, correctly-timed MOSI/SCK/CS from the master, but return a fixed value regardless of instruction, address, or CS pull configuration — this pattern is not explained by SPI mode/timing/wiring on the host side and is consistent with the MCP2515 CAN core never leaving its post-reset/oscillator-not-stable state. 5. Request Given the host-side SPI signaling has been verified correct by logic analyzer and the device tree / kernel driver configuration is confirmed correct, we would like guidance on: Whether this failure signature (fixed register readback, CANSTAT never = 0x80) is consistent with a known MCP2515 crystal/oscillator start-up issue, and recommended oscilloscope/verification procedure for OSC1/OSC2 Whether there are known compatibility issues between MCP2515 and i.MX93 LPSPI (beyond ERR051608, already addressed) Recommended next diagnostic steps or RMA process if a hardware defect in the MCP2515 modules is suspected Please let us know if additional logic analyzer captures, device tree files, or kernel logs would help. Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi MCP2515 / i.MX93 LPSPI3 — Root-Cause Update Follow-up to our earlier report. A new, isolating test now points away from the MCP2515 modules entirely and toward the i.MX93 LPSPI3 SPI controller / driver. Test performed: Using a userspace spidev tool, we repeatedly issue RESET + CANSTAT-read cycles on LPSPI3 (500 kHz, Mode 0) while varying only the physical state of the MISO line: MISO wired to a real MCP2515 chip: unstable, rarely reaches the expected 0x80. MISO physically disconnected (floating, no chip attached): a structured, repeating byte pattern (0x00 / 0xFF / 0xFB) still appears, with ~10–11 ms periodicity. MISO tied to GND through a 10kΩ resistor: the same repeating pattern still appears, essentially unchanged. MISO shorted directly to GND (~0Ω): the pattern disappears completely — reads become a flat, constant 0x00. Key finding: The exact same byte sequence, with millisecond-for-millisecond identical timing, reappears across independent runs (different process IDs, different times) and across different physical MISO conditions (disconnected vs. 10kΩ pulldown vs. connected to a real chip). The SPI ioctl() call itself returns success (no error) every time — this is not a failed transfer being masked; real data is being clocked in on every call. Interpretation: A genuinely floating or resistor-loaded input pin should not reproduce an identical, host-independent bit pattern down to the millisecond across separate process invocations. This level of determinism suggests the byte values being read back are not representative of the actual MCP2515 SO/MISO line, but are instead coming from a fixed, repeatable internal state of the LPSPI3 peripheral or its Linux driver (e.g., stale RX FIFO content, or a fixed pattern read regardless of the input pin's real logic level) — only a hard short to GND overrides it. Question for NXP: could LPSPI3 (or its Linux driver, spi-fsl-lpspi) under certain conditions return fixed/stale RX FIFO content instead of the pin's real sampled value? Is there a known erratum or driver behavior that would explain a deterministic, wiring-independent readback pattern like this? Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi Hello dear @irfanktm  Please take a look to the post I made for your case: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/2-CH-CAN-HAT-with-FRDM-IMX93/ta-p/2415467 There is explained how you can use the 2-Channel CAN HAT in our BSP and i.MX93 FRDM. Best regards, Salas.
查看全文
为 IMX8 Nano 处理器实现 USB 尝试为 imx8 nano 实现 USB 功能,评估板布局显示 ID 引脚为浮空导线。它能在主机模式下工作吗?因为主机模式下 id 必须等于 0。 Re: implementing usb for imx8 nano processor 你好@Jayesh2408 希望你一切都好。 是的,只要通过软件强制控制器行为,浮空 ID 引脚在仅主机模式下也能完美工作。 您只需将设备树中的dr_mode属性从“ otg ”更改为“ host ”即可: &usbotg1 { dr_mode = "host"; hnp-disable; srp-disable; adp-disable; usb-role-switch; disable-over-current; samsung,picophy-pre-emp-curr-control = <3>; samsung,picophy-dc-vol-level-adjust = <7>; status = "okay"; port { usb1_drd_sw: endpoint { remote-endpoint = <&typec1_dr_sw>; }; }; }; 顺祝商祺! 萨拉斯。
查看全文
IMX8ナノプロセッサ向けのUSB実装 iMX8 NanoにUSBを実装しようとしていますが、評価ボードのレイアウトではIDピンの配線がフローティング状態になっています。ホストモードでも動作しますか?ホストモードではidを0にする必要があるからです。 Re: implementing usb for imx8 nano processor こんにちは、@Jayesh2408さん お元気でお過ごしのことと思います。 はい、フローティングIDピンはホストオンリーモードでは、ソフトウェアでコントローラーの動作を強制すれば問題なく動作します。 デバイスツリーの dr_mode プロパティを「otg」から「host」に変更すればいいです。 &usbotg1 { dr_mode = "host"; hnp-disable; srp-disable; adp-disable; usb-role-switch; disable-over-current; samsung,picophy-pre-emp-curr-control = <3>; samsung,picophy-dc-vol-level-adjust = <7>; status = "okay"; port { usb1_drd_sw: endpoint { remote-endpoint = <&typec1_dr_sw>; }; }; }; よろしくお願いいたします。 サラス。
查看全文
i.MX93 power sequencing I am designing a low power PCB based around the i.MX93 and its recommended PMIC (PCA9451). The AN13917 power consumption measurement document suggests that in its lowest power mode (section 6.7.8) the SoC+DRAM power consumption should be ~174mW. However, the current measurements in the document are taken after the PMIC, so do not include any efficiency losses.  When calculating the actual expected power consumption, the vdd_ana_0p8 rail stands out as a very high consumer of energy. The 16.5mA current draw on this rail causes 69mW dissipation in the PMIC LDO (from a 5V input). This is ~60% of the efficiency losses. I would like to power this rail from a separate SMPS module (TI TPSM82821) to reduce these losses, however the i.MX93 datasheet has no definition of Tstep or Toff_step in the power rail sequencing requirements. Are there actually any timing requirements, or only sequencing? Would it be sensible to use VDD_SOC as the enable trigger (via a comparator) for the external SMPS, or are there better options to use? I'm assuming that the 0V8 will discharge faster than VDD_SOC during power down as the TPMS82821 has an output active discharge function. Re: i.MX93 power sequencing Hello, There is a time for Tstep or Toff_step in Table 6. PWRUP mode: tSTEP (Time to next power rail ON from prev rail POK):  2 ms tOFF_STEP (Time to next power rail off from prev rail off): 8 ms Also, you can use VDD_SOC as reference to trigger external regulator in power-up/power-off sequences. Best regards.
查看全文
Ara2 Windows 工厂测试/运行时软件包不可用 我正在 Windows 系统上使用 Ara2 PCIe 加速器。硬件检测正确,PCIe/DMA 初始化成功,AraProxyService 正在运行。但是,设备初始化失败,并出现以下错误: 设备上的固件版本不支持:0,请更新固件。 当前环境: 固件版本:14.34.0.0 代理版本:1.1.0.0 SysAPI:1.1.56.0 Windows ARA2 用户指南提到了 factory-test-package-windows.zip 文件和 Qwen Windows 演示包,但我无法通过文章获取这些附件。 NXP 的某位工作人员能否提供 Ara2 的最新 Windows 工厂测试包以及与之匹配的运行时/固件包? 目前,这导致无法在正在运行的 Windows 部署中验证加速器。
查看全文
i.MX8QXP – Prevent normal boot after interrupted USB flashing on Yocto Scarthgap with A/B partitions Hi NXP Team, The installed UUU executable reports: libuuu_1.5.21-0-g1f42172 We use: sudo uuu -b emmc_all ~/Downloads/flash.bin *.wic The built-in emmc_all script writes the complete .wic image using: FB: flash -raw2sparse all _image It then writes the bootloader, configures eMMC boot selection, and finishes with FB: done. The script contains no explicit persistent flash-in-progress completion metadata handling or readback hash verification step. If flashing is interrupted during the .wic write, the cluster can subsequently boot and display the updated HMI. We suspect that an existing usable bootloader and sufficient written boot,rootfs content permit this, but the selected slot and completeness of its contents are not yet confirmed. Please advise how to add a power-loss-tolerant completion check that blocks normal boot from both slots after interrupted factory flashing, while preserving USB recovery. The metadata must remain valid independently of the full .wic write and bootloader update. Re: i.MX8QXP – Prevent normal boot after interrupted USB flashing on Yocto Scarthgap with A/B partit Hello,  An official solution is not implemented but you can customize the uuu script, the built-in emmc_all flow is simply a UUU script based on Fastboot and U-Boot commands, and it can be modified or replaced by a custom uuu.auto file. U-Boot commands can also be executed through FB: ucmd. This means you should add custom steps such as setting a "flash in progress" flag before programming and clearing it only after verification succeeds.  U-Boot Boot Count / Boot Limit The U-Boot tree includes support for: CONFIG_BOOTCOUNT_LIMIT bootcount bootlimit altbootcmd CONFIG_BOOTCOUNT_FS When bootcount exceeds bootlimit, U-Boot executes altbootcmd instead of the normal bootcmd. This mechanism can be used to redirect the system to a recovery mode such as Fastboot Boot Count Limit — Das U-Boot unknown version documentation
查看全文
i.MX8QXP – A/BパーティションでYocto ScarthgapのUSBフラッシュが中断された後の通常起動を防ぐ こんにちは、NXP チームの皆様、 インストールされたUUU実行ファイルは以下を報告します。 libuuu_1.5.21-0-g1f42172 私たちは以下を使用しています: sudo uuu -b emmc_all ~/Downloads/flash.bin *.wic 組み込みのemmc_allスクリプトは、以下の方法で完全な.wicイメージを書き込みます。 FB: flash -raw2sparse all _image その後、ブートローダーを書き込み、eMMCブート選択を設定し、FB: doneで終了します。 このスクリプトには、進行中のフラッシュ処理完了メタデータの明示的な処理や、読み戻しハッシュの検証手順は含まれていません。 .wic の実行中にフラッシュが中断された場合writeすると、クラスタはその後起動し、更新されたHMIを表示できます。既存の使用可能なブートローダーと、十分な量のboot、rootfsの内容が書き込まれていればこれが可能になると思われますが、選択されたスロットとその内容の完全性はまだ確認されていません。 工場出荷時フラッシュが中断された後、両方のスロットからの通常起動をブロックしつつ、USBリカバリ機能を維持するための、電源喪失耐性のある完了チェックを追加する方法について教えてください。メタデータは、完全な.wicファイルとは独立して有効でなければならない。書き込みとブートローダーのアップデート。 Re: i.MX8QXP – Prevent normal boot after interrupted USB flashing on Yocto Scarthgap with A/B partit こんにちは、 公式の解決策は実装されていませんが、uuuスクリプトをカスタマイズでき、組み込みのemmc_allフローはFastbootやU-Bootコマンドに基づくUUUスクリプトで、カスタムのuuu.autoファイルで修正または置き換えが可能です。U-BootコマンドはFB: ucmdを通じても実行可能です。つまり、プログラミング前に「フラッシュ処理中」フラグを設定し、検証が成功した後にのみそのフラグを解除するなど、カスタム手順を追加する必要があるということです。 U-Bootの起動回数/起動制限 U-Bootツリーには以下のサポートが含まれています: CONFIG_BOOTCOUNT_LIMIT ブートカウント ブート制限 altbootcmd CONFIG_BOOTCOUNT_FS ブート回数がブート制限を超えると、U-Bootは通常のbootcmdの代わりにaltbootcmdを実行します。この仕組みは、システムをFastbootのようなリリバリモードにリダイレクトするために使用できます ブートカウント制限 — Das U-Boot 不明バージョンドキュメント
查看全文
Ara2 Windows factory-test/runtime package unavailable I’m working with an Ara2 PCIe Accelerator on Windows. The hardware is detected correctly, PCIe/DMA initialization succeeds, and the AraProxyService is running. However, device initialization fails with the following error: Unsupported firmware version on device: 0 please update firmware. Current environment: Firmware: 14.34.0.0 Proxy: 1.1.0.0 SysAPI: 1.1.56.0 The Windows ARA2 User Guide references the factory-test-package-windows.zip file and the Qwen Windows demo package, but those attachments are not available to me through the article. Could someone from NXP please provide access to the current Windows factory-test package and the matching runtime/firmware package for the Ara2? This is currently blocking validation of the accelerator in an active Windows deployment.
查看全文
implementing usb for imx8 nano processor trying to implement usb for imx8 nano, the eval board layout shows floating wire for Id pin. will it work for host mode? because id need to be =0 for host mode. Re: implementing usb for imx8 nano processor Hello @Jayesh2408  Hope you are doing very well. Yes, a floating ID pin will work perfectly fine for host-only mode, provided you force the controller behavior via software. You can just change the dr_mode property in device tree from "otg" to "host": &usbotg1 { dr_mode = "host"; hnp-disable; srp-disable; adp-disable; usb-role-switch; disable-over-current; samsung,picophy-pre-emp-curr-control = <3>; samsung,picophy-dc-vol-level-adjust = <7>; status = "okay"; port { usb1_drd_sw: endpoint { remote-endpoint = <&typec1_dr_sw>; }; }; }; Best regards, Salas.
查看全文
FRDM-IMX93 — LPSPI3/EXPI (P11) SPI 引脚无法与任何外部设备产生有效的 SPI 通信; 主题:FRDM-IMX93 — LPSPI3/EXPI (P11) SPI 引脚无法与任何外部设备产生有效的 SPI 通信;怀疑与板载三频模块 (MAYA-W27x) 冲突 NXP团队您好, 我正在尝试启动一个外部SPI设备(Waveshare 2通道CAN HAT( https://www.waveshare.com/wiki/2-CH_CAN_HAT )),在 FRDM-IMX93 板的 EXPI 40 针接头 (P11) 上使用 LPSPI3 (GPIO_IO08–11,与 RPi 兼容的引脚位置匹配) 连接双 MCP2515)。我已经确认 HAT 本身功能齐全(在具有标准 dtoverlay=mcp2515 配置的真正 Raspberry Pi 上进行了测试并运行正常)。 板/电路板支持包。 FRDM-IMX93,型号 NXP FRDM-IMX93 NXP i.MX 发布发行版 6.18-whinlatter,内核版本 6.18.2-1.0.0-gf49f45233f7b 我已配置好(所有配置均已在设备树级别验证正确): Overlay 在 &lpspi3 下添加了 mcp2515@0/mcp2515@1,其中 cs-gpios = <&gpio2 8 1>, <&gpio2 7 1>; (GPIO_IO08/GPIO_IO07),与我在 NXP 自己的上游补丁中找到的基于 GPIO 的 CS 模式相匹配,该补丁用于类似的 FRDM-IMX93 SPI3 外设(pixpaper 显示覆盖层)。 将 &pinctrl_lpspi3 扩展为将 GPIO_IO07 (CS1) 复用为 GPIO,因为它之前在 /sys/kernel/debug/pinctrl/ 中是 (MUX UNCLAIMED)。 禁用了与 CS0 冲突的已存在的 spidev0 节点。 启用 reg_vexp_3v3/reg_vexp_5v(稳压器始终开启)——这些默认是禁用的,如果没有这些,EXPI 标头将无法供电。 已确认 /dev/spidev2.0 已创建,引脚复用显示所有 4 个 SPI 引脚上的功能分配 (lpspi3grp) 正确。 症状: mcp251x 驱动程序始终失败:spi2.0:无法初始化MCP2515。接线错误?(错误代码=19)和 spi2.1:RESET后 MCP251x 未进入配置模式(错误代码=110)——以上所有设备树变体均完全不变。 使用 spidev_test(兼容 lwn、bk4)对 /dev/spidev2.0 进行原始 SPI 级测试:无论 MOSI/MISO 是物理短路(环回)、开路还是用分流器桥接,RX 缓冲区都会返回逐字节相同的数据。这表明 P11 接头引脚 19/21/23/24 处的 SPI3 信号没有反映在控制器的实际总线活动中——也就是说,这些信号可能根本没有到达接头,或者有其他东西在干扰。 疑似根本原因: 根据 UM12181(FRDM-IMX93 板用户手册,第 2.11 节“三射频模块接口”),SPI3 信号(CLK、MOSI、MISO、CS0 — 在 GPIO_IO08-11 上复用)通过双向 1.8V 电平转换器 (U729)(电阻选择)在板载 MAYA-W27x 三射频模块和 M.2 连接器之间共享。该文档没有说明当 SPI3 备用功能由 SoC 端驱动时,EXPI 接头 (P11) 是否/如何与此共享路径电气隔离。 问题: P11 的 GPIO_IO08-11 引脚在电气上是否独立于 U729 转换器/三路无线电路径?或者,在 P11 上使用 SPI3 是否需要任何额外的配置(例如,禁用三路无线电模块、GPIO 扩展位或电阻器改造)才能正确地将信号路由/隔离到接头? 是否有经过验证的参考设备树(类似于 EVK 的 imx93-11x11-evk-lpspi.dts),专门用于在 FRDM-IMX93 板上外部使用 LPSPI3? 能否提供 SPI3/U729 信号路径的原理图片段,以确认 P11 连接拓扑结构? 提前感谢您的帮助。 Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi 如果有什么遗漏,我可以补充。 root@imx93-11x11-lpddr4x-frdm:/sys/firmware/devicetree/base# ls '#address-cells' clock-osc-24m 固件 mcp2515_clock pmu regulator-hmisc-vddio regulator-vexp-3v3 soc@0 usbphynop2 '#size-cells' clock-osc-32k imx93-lpm memory psci regulator-usdhc2 regulator-vexp-5v sound-mqs usdhc3_pwrseq __symbols__兼容中断控制器@48000000 型号 regulator-adc-vref regulator-usdhc3 remoteproc-cm33 sw-keys 别名 cpus 中断父级 mqs1 稳压器-avdd 稳压器-vdd-12v 保留内存 热区 选定的显示子系统 ldb-display-controller mqs2 regulator-can2-stby regulator-vdd-5p0v secure-enclave timer clock-ext1 ethosu ldb-phy 名称 regulator-dvdd regulator-vddo 序列号 usbphynop1 Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi 是的,我在p11接头上测得3.3V和5V电压。 为什么我的电脑会出现错误? imx93-11x11-lpddr4x-frdm 登录:root root@imx93-11x11-lpddr4x-frdm:~# dmesg | grep -iE 'mcp251|lpspi3' [ 8.989639] mcp251x:模块布局没有符号版本 [ 10.032864] mcp251x spi2.1:MCP251x RESET 后未进入配置模式 [ 10.033021] mcp251x spi2.1:探测失败,错误代码=110 [ 10.033034] mcp251x spi2.1:使用驱动程序 mcp251x 进行探测失败,错误代码为 -110 [ 10.074097] mcp251x spi2.0:无法初始化 MCP2515。接线错误? [ 10.074256] mcp251x spi2.0:探测失败,错误代码=19 root@imx93-11x11-lpddr4x-frdm:~# ip link show 1: lo: mtu 65536 qdisc noqueue state UNKNOWN mode DEFAULT group default qlen 1000 链接/回环 00:00:00:00:00:00 brd 00:00:00:00:00:00 2: eth0: mtu 1500 qdisc mq 状态 DOWN 模式 DEFAULT 组 default qlen 1000 链接/以太 90:a9:f7:80:42:26 brd ff:ff:ff:ff:ff:ff 3: eth1: mtu 1500 qdisc mq 状态 DOWN 模式 DEFAULT 组 default qlen 1000 链接/以太 90:a9:f7:80:42:27 brd ff:ff:ff:ff:ff:ff 4: mlan0: mtu 1500 qdisc mq 状态 UP 模式 DORMANT 组 default qlen 1000 链接/以太 80:a1:97:50:4e:0d brd ff:ff:ff:ff:ff:ff 5: uap0: <广播,组播> mtu 1500 qdisc noop 状态 DOWN 模式 DEFAULT 组 default qlen 1000 链路/以太网 82:a1:97:50:4f:0d brd ff:ff:ff:ff:ff:ff 6: wfd0: <广播,组播> mtu 1500 qdisc noop 状态 DOWN 模式 DEFAULT 组 default qlen 1000 链接/以太 82:a1:97:50:4e:0d brd ff:ff:ff:ff:ff:ff 7: can0: mtu 16 qdisc noop 状态 DOWN 模式 DEFAULT 组 default qlen 10 链接/罐 Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi FRDM-IMX93:LPSPI3(P11 EXPI 接头)SCK 引脚无信号输出 问题 我正在尝试使用 P11 EXPI 接头上的 LPSPI3 (GPIO_IO08-11, spi@42550000) 操作外部 SPI 设备 (2× MCP2515 CAN)。驱动程序处于活动状态,外设似乎正在“内部”运行,但没有信号输出到物理 SCK 引脚 (GPIO_IO11)。 证据 覆盖层应用无误;spi2.0/spi2.1 已在 SPI 内核中注册。 电源、引脚控制、引脚控制断言-GPIOS、CS-GPIOS 和时钟源——全部正确,并且已经过验证。 CS0(同一组,GPIO 交替功能,模式=0)工作完美——用万用表和逻辑分析仪都能看到脉冲。 在逻辑分析仪上,SCK(模式=1,原生 LPSPI3_SCK)完全平坦/0V——无论 HAT 是否连接,对连续触发回路都没有影响。 然而,LPSPI3 的 IRQ(GIC 97)实际上是在 /proc/interrupts 中触发的(一次传输尝试产生了 220 次中断)——外设的内部逻辑(状态/IER 寄存器)处于活动状态。 使用 /dev/mem 读取 LPSPI3 基地址 (0x42550000) 时返回“总线错误”——但是运行在同一总线上的 flexcan2 (0x425b0000) 也返回相同的错误,这意味着这是 /dev/mem 的一般限制,而不是 LPSPI3 特有的限制(已通过控制组排除)。 DMA 理论经过测试并被排除:当使用无效句柄覆盖 dmas 时,驱动程序回退到 PIO 并显示消息“dma 设置错误 -19,请使用 pio”,但 SCK 信号仍然没有出现。 `clk_ignore_unused` 启动参数也没有任何作用。 结束语 LPSPI3 外设的内部逻辑正在工作(产生中断),但 SCK 信号始终无法到达外部引脚 (GPIO_IO11)——尽管同一引脚控制组中的 CS0(GPIO 模式)输出正确,但 SCK(LPSPI3 原生替代功能)却无法输出。这似乎指向与焊盘驱动器/硅相关的配置细节,或者指向 NXP 应该了解的配置细节,而这些细节无法通过设备树或软件来解释。 问题 在 FRDM-IMX93 上,是否需要在设备树之外通过 P11 为 LPSPI3_SCK(GPIO_IO11,本机替代功能)添加额外的硬件/固件使能步骤? 已知有一个例子表明,LPSPI3 可以使用 i.MX93 EVK 上的相同引脚(community.nxp.com/t5/i-MX-Processors/iMX93AUTO-EVK-SPI-Configuration-for-QCA7006AQ)——可能FRDM是否存在特殊差异? Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi 根据日志,我怀疑您尝试通过 spidev_test 访问 SPI 设备,但该设备由 MCP 驱动程序处理。 我需要知道的是您使用的完整设备树(.dts)文件,例如: imx93-11x11-frdm.dts 另外,如果您对它进行了修改,请告诉我您的修改之处。 另外,我也会尝试弄一个 mcp2515 CAN 模块,以便我这边进行集成测试。 顺祝商祺! 萨拉斯。 Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi 你好@irfanktm 希望你一切都好。 实际上,i.MX93 FRDM PAD 与 P11 GPIO_IO08-IO11 引脚之间存在直接连接: Manuel_Salas_0-1789421014211.pngManuel_Salas_0-1789421014211.pngManuel_Salas_0-1789421014211.pngManuel_Salas_0-1789421014211.pngManuel_Salas_0-1789421014211.pngManuel_Salas_0-1789421014211.png曼努埃尔_萨拉斯_0-1789421014211.png 能否请您提供一下重现问题的步骤? 顺祝商祺! 萨拉斯。 Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi 你好@irfanktm 我刚才做了一些测试: Manuel_Salas_0-1789495251012.pngManuel_Salas_0-1789495251012.pngManuel_Salas_0-1789495251012.pngManuel_Salas_0-1789495251012.pngManuel_Salas_0-1789495251012.png曼努埃尔_萨拉斯_0-1789495251012.png 我的 i.MX93 FRDM 上的 SPI 工作正常。 Manuel_Salas_1-1789495295645.pngManuel_Salas_1-1789495295645.pngManuel_Salas_1-1789495295645.pngManuel_Salas_1-1789495295645.pngManuel_Salas_1-1789495295645.png曼努埃尔_萨拉斯_1-1789495295645.png 我的环境和你一样。 最后一个问题。 你的i.MX93 FRDM板的3V3和5V引脚有电压吗? 如果不行,请点击以下链接启用董事会监管功能: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Enable-3-3-V-and-5-V-Regulators-for-Expansion-Header-on-i-MX9/ta-p/2299415 顺祝商祺! 萨拉斯。 Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi 请您提供完整的设备树。 或者只是与 lpspi3 节点和引脚复用相关的。 顺祝商祺! 萨拉斯。 Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi 不,imx93-11x11-frdm.dts 文件是原始文件;我编辑了 mcp2515-can-hat.dtbo 覆盖文件, https://www.waveshare.com/wiki/2-CH_CAN_HAT我只将 INT_1 从默认的 GPIO_25 改为 GPIO_24(物理引脚 18)。 Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi 技术支持请求 MCP2515(Microchip)SPI 通信故障,i.MX93(NXP)SPI2/LPSPI3 1. 总结 两个 MCP2515 CAN 控制器(Waveshare 2-CH CAN HAT、MCP2515-I/SO、16 MHz 晶振)通过 LPSPI3(SPI2、CS0/CS1)连接到 i.MX93-11X11-LPDDR4X-FRDM 板,上电或 SPI/硬件 RESET 后始终无法进入配置模式。所有寄存器读取都返回固定不变的值,而不是预期的 CANSTAT = 0x80。内核 mcp251x 驱动程序持续报告探测失败(err=-110“RESET 后未进入配置模式”,或 err=-19“接线错误?”)。 2. 环境 SoM/板:i.MX93-11X11-LPDDR4X-FRDM 内核:6.18.2-1.0.0-gf49f45233f7b(NXP 下游),CONFIG_SPI_FSL_LPSPI=y(内置),ERR051608 预分频修复程序已存在 SPI 总线:LPSPI3 (spi@42550000),2 个片选信号,自定义设备树覆盖(16 MHz 固定时钟,IRQ GPIO3-23 / GPIO3-24) CAN 模块:Waveshare 2 通道 CAN HAT,MCP2515-I/SO,标记“E3 2335BK5”(Microchip 原装标记格式) 驱动程序:mcp251x(主线),已使用内核驱动程序和基于 spidev 的自定义测试工具进行测试。 3. 已执行的故障排除 已更正设备树覆盖目标(&spi1/&lpspi3 与错误的 &spi2 标签相比)——覆盖现在已正确应用,mcp2515 子节点已存在于实时设备树中 已根据运行中的设备树验证 LPSPI3 pinctrl、cs-gpios 和 interrupt-parent/GPIO 映射——全部正确 使用逻辑分析仪验证了主端SPI信号的完整性:在多次捕获中,i.MX93均能正确且一致地生成MOSI、SCK和CS信号。 已确认两个 CAN 模块的 VDD = 3.3V 和空闲 MISO = 3.3V(无对地短路) 已确认两个模块的 RESET 引脚(引脚 17,SOIC-18)均为 3.3V(未激活) 测试了 SPI 模式 0,0 和模式 1,1 (CPOL/CPHA),时钟频率为 100 kHz 至 8 MHz — 行为未发生变化 在 CS0/CS1 上添加了 10k 上拉电阻,以解决两个并联 MCP2515 器件之间的 MISO 总线争用问题——这稳定了(但并未纠正)回读数据。 自定义 spidev 测试工具:RESET 指令 + 复位后立即/连续轮询 CANSTAT(1 毫秒间隔,300 毫秒窗口)— CANSTAT 立即稳定到一个固定值,且永远不会达到 0x80。 强制写入 CANCTRL (0x80) 后执行读取操作——读取操作不受写入操作的影响,表明 SPI 事务未被 CAN 控制器逻辑处理。 4. 关键观察 CS0 设备:CANSTAT/CANCTRL/所有寄存器始终读取回 0x00(在数十次复位+读取周期中 100% 可重复,与寄存器地址、SPI 模式或写入值无关)。 CS1 设备:CANSTAT/CANCTRL/所有寄存器始终读取回 0xFF(100% 可重复,MISO 在事务处理期间从不翻转)。 两个设备均显示来自主控端的干净、时序正确的 MOSI/SCK/CS,但无论指令、地址或 CS 拉取配置如何,都返回一个固定值——这种模式无法用主机端的 SPI 模式/时序/接线来解释,并且与 MCP2515 CAN 内核永远不会离开其复位后/振荡器不稳定状态一致。 5. 请求 鉴于逻辑分析仪已验证主机端 SPI 信号传输正确,且设备树/内核驱动程序配置也已确认正确,我们希望获得以下方面的指导: 此故障特征(固定寄存器回读,CANSTAT 始终不等于 0x80)是否与已知的 MCP2515 晶振(晶体振荡器)启动问题一致,以及 OSC1/OSC2 的推荐示波器/验证程序。 MCP2515 和 i.MX93 LPSPI 之间是否存在已知的兼容性问题(除已解决的 ERR051608 之外) 如果怀疑MCP2515模块存在硬件缺陷,建议采取以下后续诊断步骤或RMA流程。 如果您需要提供额外的逻辑分析仪捕获文件、设备树文件或内核日志,请告知我们。 Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi MCP2515 / i.MX93 LPSPI3 — 根本原因更新 这是我们之前报告的后续报道。一项新的隔离测试现在完全指向了 i.MX93 LPSPI3 SPI 控制器/驱动程序,而不是 MCP2515 模块。 已执行测试: 使用用户空间 spidev 工具,我们反复对 LPSPI3(500 kHz,模式 0)发出 RESET + CANSTAT 读取周期,同时仅改变 MISO 线的物理状态: MISO 连接到真正的 MCP2515 芯片:不稳定,很少达到预期的 0x80。 MISO 物理断开(浮空,未连接芯片):仍会出现结构化的重复字节模式(0x00 / 0xFF / 0xFB),周期约为 10-11 毫秒。 MISO 通过 10kΩ 电阻连接到 GND:仍然出现相同的重复模式,基本没有改变。 MISO 直接短接到 GND (~0Ω):图案完全消失——读取结果变为平坦的恒定值 0x00。 主要发现: 完全相同的字节序列,毫秒级的时序完全相同,在不同的运行(不同的进程 ID、不同的时间)和不同的物理 MISO 条件(断开连接、10kΩ 下拉电阻、连接到真实芯片)中反复出现。SPI ioctl() 调用本身每次都会返回成功(无错误)——这不是被掩盖的传输失败;每次调用都会将真实数据记录到时钟中。 解释: 真正浮空或电阻负载的输入引脚不应该在不同的进程调用中精确到毫秒地重现与主机无关的相同位模式。这种确定性表明,读取回来的字节值并不代表实际的 MCP2515 SO/MISO 线,而是来自 LPSPI3 外设或其 Linux 驱动程序的固定、可重复的内部状态(例如,过时的 RX FIFO 内容,或者无论输入引脚的实际逻辑电平如何,读取的固定模式)——只有硬短路到 GND 才能覆盖它。 向 NXP 提出问题:在某些情况下,LPSPI3(或其 Linux 驱动程序 spi-fsl-lpspi)是否会返回固定/过时的 RX FIFO 内容,而不是引脚的实际采样值?是否存在已知的错误或驱动程序行为可以解释这种确定性的、与线路无关的读取模式? Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi 技术支持请求 — i.MX93 LPSPI3 上的 MCP2515 多个 MCP2515 CAN 控制器(测试了 3 个单元,2 个不同的制造商/板,8/16 MHz 晶振)通过 LPSPI3 (SPI2) 连接到 i.MX93-11X11-LPDDR4X-FRDM 板,RESET后间歇性地无法进入配置模式(CANSTAT 应读取 0x80)。 环境:内核 6.18.2(NXP 下游),CONFIG_SPI_FSL_LPSPI 内置,ERR051608 预分频修复已存在。设备树/引脚控制已验证正确(LPSPI3 SIN/SOUT/SCK 已正确复用,CS 通过 cs-gpios)。逻辑分析仪捕获结果证实主机能够正确且一致地生成 MOSI/SCK/CS。 关键观察结果: 对于新打开的 spidev 句柄,第一次 RESET + CANSTAT 读取操作大约有 50-60% 的概率成功(~0x80),且计时稳定在 2-6 毫秒左右。 如果对同一个仍然打开的 SPI 文件描述符发出额外的 RESET+读取周期,则之后会持续失败,并稳定为可重复的 ~10-11 毫秒周期性固定值 (0x00 / 0xFF / 0xFB) 模式,永远不会再次达到 0x80。 所有 3 个物理 MCP2515 单元和 2 种不同的电路板设计都出现了相同的故障特征,排除了单个芯片/模块存在缺陷的可能性。 添加传输间延迟(delay_usecs)、虚拟“刷新”SPI 传输,并将周期之间的间隔增加到 100 毫秒,结果都没有改变(一旦模式开始,成功率就为 0/10)。 VDD、GND、RESET 引脚和空闲 MISO 电平均已确认正常(3.3 V)。 主线 mcp251x 内核驱动程序自身的 probe() 也显示出同样的不稳定性:连续 5 次绑定尝试(取消绑定/清除 driver_override/绑定)全部失败,错误信息在 err=-19(“接线错误?”)和 err=-110(“重置后未进入配置模式”)之间交替出现,且模式具有规律性,并非随机性。 这种模式(打开后第一次传输正常,然后在同一会话中的后续传输中出现固定的可重复故障特征——内核驱动程序自己的探测也重现了该故障)表明,连续的 LPSPI3 传输/CS 周期之间没有完全清除状态,而不是 MCP2515 单元本身存在缺陷。 向 NXP 提出的问题:这是否与已知的 LPSPI3 (i.MX93) 行为一致——例如:在同一 SPI 文件描述符上连续进行数据传输时,FIFO/CS 状态无法干净地重置——是否有推荐的驱动程序级解决方法(例如,使用 FIFO/CS 进行数据交换)?除了 ERR051608 之外,还需要延迟、FIFO 刷新或 CS 处理吗? Re: FRDM-IMX93 — LPSPI3/EXPI (P11) SPI pins produce no valid SPI transactions with any external devi 你好,亲爱的@irfanktm 请查看我针对您的情况发布的帖子: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/2-CH-CAN-HAT-with-FRDM-IMX93/ta-p/2415467 本文解释了如何在我们的 电路板支持包 和 i.MX93 FRDM 中使用2 通道 CAN HAT 。 顺祝商祺! 萨拉斯。
查看全文
Ara2 Windows ファクトリーテスト/ランタイムパッケージが利用できません 私はWindowsでAra2 PCIeアクセラレータを使っています。ハードウェアは正しく検出され、PCIe/DMAの初期化は成功し、AraProxyServiceが実行されています。しかし、デバイスの初期化は、以下のエラーで失敗します。 デバイスのファームウェアバージョンがサポートされていません:0。ファームウェアをアップデートしてください。 現在の環境: ファームウェア: 14.34.0.0 プロキシ: 1.1.0.0 SysAPI: 1.1.56.0 Windows ARA2ユーザーガイドにはfactory-test-package-windows.zipファイルとQwen Windowsデモパッケージが記載されていますが、記事ではそれらの添付ファイルは入手できません。 NXPのどなたか、現在のWindows工場出荷時テストパッケージとAra2対応のランタイム/ファームウェアパッケージへのアクセスを提供していただけませんか? 現在、これによりアクティブなWindows展開中のアクセラレータの検証がブロックされています。
查看全文
i.MX8QXP – 防止在 Yocto Scarthgap 系统上使用 A/B 分区时,USB 刷写中断后无法正常启动 您好,NXP团队: 已安装的 UUU 可执行文件报告: libuuu_1.5.21-0-g1f42172 我们使用: sudo uuu -b emmc_all ~/Downloads/flash.bin *.wic 内置的 emmc_all 脚本使用以下命令写入完整的 .wic 镜像: FB:flash -raw2sparse 所有_image 然后写入引导加载程序,配置 eMMC 引导选择,最后显示 FB: done。 该脚本不包含显式的持久性闪存进行中完成元数据处理或回读哈希验证步骤。 如果在 .wic 期间闪光灯闪烁中断写入后,集群即可启动并显示更新后的 HMI。我们怀疑现有的可用引导加载程序和足够的已写入启动、根文件系统内容允许这样做,但所选插槽及其内容的完整性尚未得到确认。 请问如何添加一个断电容错完成检查,在工厂刷机中断后阻止从两个插槽正常启动,同时保留 USB 恢复功能?元数据必须独立于完整的 .wic 文件保持有效。写入和引导加载程序更新。 Re: i.MX8QXP – Prevent normal boot after interrupted USB flashing on Yocto Scarthgap with A/B partit 你好, 虽然没有官方的解决方案,但您可以自定义 uuu 脚本,内置的 emmc_all 流程只是一个基于 Fastboot 和 U-Boot 命令的 UUU 脚本,它可以被修改或替换为自定义的 uuu.auto 文件。U-Boot 命令也可以通过 FB:ucmd 执行。这意味着您应该添加自定义步骤,例如在编程前设置“闪存正在进行中”标志,并在验证成功后才清除该标志。 U-Boot 启动次数/启动限制 U-Boot 库包含对以下功能的支持: 配置启动次数限制 启动计数 启动限制 altbootcmd 配置启动计数_FS 当启动次数超过启动限制时,U-Boot 会执行 altbootcmd 而不是正常的 bootcmd。此机制可用于将系统重定向到恢复模式,例如 Fastboot 模式。 启动次数限制 — Das U-Boot 未知版本文档
查看全文
CLEV6630B評価ボード(OM26630FDK) 評価ボード(OM26630FDK)のPDfファイルCLEV6630B入手しましたが、カスタム設計で使うために同じAltiumのPCBファイルを入手できますか? Re: CLEV6630B eval board(OM26630FDK) こんにちは、 @R_Tony さん。 あなたの調子が良いといいのですが。 申し訳ありませんが、このデバイスで利用可能な設計ファイルはPDF形式の CLRC6630B回路図とレイアウトのみです。 ご迷惑をおかけして申し訳ございません。 よろしくお願いいたします。 エドゥアルド。
查看全文