Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
RT1189 - 2 octal 166MHz HyperRAMs on SPI1 to create 16-bit wide bus? The RT1180 RM shows a Parallel FlexSPI configuration wherein two octal HyperBus memories on SPI1 to A_D7..0 and B_D7..0 to form a 16 bit wide bus.  See pages 2243 & 2244, Table 196, 6th row down which is the only entry where Effective Bus Size is listed as 16bit.  If this actually works, the max data transfer rate should be 166 MHz x 2 bytes x 2 transfers per clock period = 644 MB/s. Has anyone tried this configuration? If yes, does it work and what was the actual performance? Thanks! Re: RT1189 - 2 octal 166MHz HyperRAMs on SPI1 to create 16-bit wide bus? Hi @DoubleD , Thanks for your interest in NXP MIMXRT series! RM lists the 2×8b parallel connection mode for FLEXSPI1, but no verified RT1180 dual-HyperRAM 16-bit parallel example/benchmark was found in public resources like SDK demos or ANSW. And theoretical raw line rate is 664 MB/s, but it must not be used as guaranteed bandwidth. This use case may require users to test it on a custom board. We apologize for any inconvenience this may cause at this stage. Best regards, Gavin Re: RT1189 - 2 octal 166MHz HyperRAMs on SPI1 to create 16-bit wide bus? Update: The previous reply based on the description in RM. Afterward, I reconfirmed this with internal team of experts, and the conclusion is as follows: 1. FlexSPI1 supports this connection method; 2. However, performance cannot reach the theoretical upper limit. It is only about 20% to 30% faster than a single-chip HyperRAM. Best regards, Gavin
記事全体を表示
S32K342、HSE、設置に関する問題 S32K342カスタムボード + PEmicro。S32K344_HSE_FW_INSTALL サンプルを S32K342 に移植しました。ビルドは正常に完了し、S32K342.mac のリセットも完了しますが、 main に到達する前にコードが Default_Handler (BusFault/HardFault) にトラップされ、起動時に失敗します。ピンクは0.13.0_2.40.0 FULL_MEMです。S32K342では、どのようなスタートアップ/リンカーの変更が必要ですか? Re: S32K342, HSE , installation issues 最近似たような問題に直面したので、使用済みのライブラリ(セミホスティングなど)が原因かもしれません。newlib_nano を選択してください(I/O なし) それ以外の場合、S32K344_HSE_FW_INSTALLを別の派生製品に移植するのは非常に簡単です。S32K342のスタートアップコードとレジスタ定義を使用する必要があります。
記事全体を表示
Default workspace Hello, I'm using MCUXpressoIDE v.24.9.25 (I know I could run a newer version, but for some reasons, I need to run 24.9.25). As I can see in "C:\NXP\MCUXpressoIDE_24.9.25\ide\configuration\config.ini", osgi.instance.area.default is "@user.home/Documents/MCUXpressoIDE_24.9.25/workspace", so it's correct. However, if I close Windows user session and open a new one with other user, when I run MCUXpressoIDE, the default workspace is the workspace of the first user, so I need to change to the second workspace directory because each user have their own directory. It seems that osgi.instance.area.default is not working fine, because @user.home/Documents/MCUXpressoIDE_24.9.25/workspace should be the home of each user, but always takes the first login user. How could I reconfigure this? Thanks. #mcux Re: Default workspace Hello, Could you help us confirm if you have the cell "Use this as the default and do not ask again" enable?  If you tick the Use this as the default and do not ask again option, then MCUXpresso IDE always starts up with the chosen workspace opened; I would recommend on not having this box checked to select the Workspace You could add the other workspace for User 2 and keep it in Recent workspaces, so you can select your desired workspace before the app open Also, In Tab Window> Preferences> General>Startup and Shutdown>Workspaces Enable the Prompt for workspace on startup. Best Regards, Luis
記事全体を表示
Ezurio Sona NX611 support in MCUXpresso SDK Hello, Is Ezurio Sona NX611 wireless card supported in MCUXpresso SDK FreeRTOS? As it's using base NXP IW611 radio, I think it should be supported, right? Re: Ezurio Sona NX611 support in MCUXpresso SDK Hello, Hope you are doing well. I would recommend checking directly on the configuration of any of our SDK examples, the supported modules. For example, in the wifi_cli for iMX RT1170, you can find these modules:   If you are looking for any other module, you would need to add the specific support at your own, taking as a base the available enablement for IW61x. Best Regards, Ricardo Re: Ezurio Sona NX611 support in MCUXpresso SDK Thank you. How do I add the specific support for the module? I see there are specific settings for each module in mcuxsdk/components/wifi_bt_module/ /tx_pwr_limits . Also there are multiple calibration data headers in mcuxsdk/middleware/wifi_nxp/incl/, for example, wifi_cal_data_override.h which has the following text: "Customer can override the data of ext_cal_data[] to set specific antenna calibration data". How do I set these (power limits and calibration data) correctly for a new module? Is there a comprehensive manual for adding support for a new wireless module? Mine is based on IW611, so I guess I can take NXP IW611-MURATA-2DL-M2 as a reference but how do I know if I need to change any values?   Re: Ezurio Sona NX611 support in MCUXpresso SDK Thank you @Ricardo_Zamora . I selected NXP-IW611-MURATA-2DL-M2 card, as Ezurio Sona NX611 uses the same chip (IW611) and I thought it should work. However, when the SDK code tries to download the firmware to the wireless card, I get: 09/07/2026 13:04:32.589 [RX] - [FW Download] Start to download firmware from 0x60143230: 727 09/07/2026 13:04:38.560 [RX] - [wifi_io] Error: SDIO - FW Ready Registers not set [wifi] Error: sd_wifi_init failed. status code -1 [wlcm] Error: wifi init/reinit failed. status code -1 [!] WPL_Init: Failed, error: 1 I understand that Sona NX611 is not in the list of supported modules but I had the impression that it should still work given that it shares the wireless chip model, IW611, with one of the supported boards. Re: Ezurio Sona NX611 support in MCUXpresso SDK Hello, I would recommend going with Ezurio for specific support for their module. Implementation may vary from module partners. Regards, Ricardo
記事全体を表示
S32k322 ADC Configuration Issue I am using three ADC channel is configured for current sensing using BCTU interrupt(CTU mode is configured to trigger mode) and remaining ADC channels are configured in Normal chain method for voltage and temperature sensing. During this configuration voltage and temperature sensing is working as expected but current sensor is sensing raw values with noise so we are getting abnormal spike in current control. Also we have changed the Ctu mode from trigger to control mode ,in current sensor channel raw value noise is reduced. But other channel configured in normal channel were not working. Our expectation is to work with single ADC peripheral(ADC0) in current sensing using BCTU trigger as well as voltage and temperature sensing in normal chain method without any spike. Note: Our hardware is designed with configuration (i.e Current sensor channels is configuration is as follows, P7-ADC0,P2 and P3 -ADC1 for reading in BCTU method. Followed by remaining ADC channels configured to normal chain method(ADC0 - X0,X1,S19 and ADC1-P0,P2,P3,P1,S10) S32 SDK for S32K1 S32 SDK for S32V Re: S32k322 ADC Configuration Issue Hi@praveen_ext I believe this is the exact same issue you're facing. https://community.nxp.com/t5/S32K/Difference-in-ADC-noise-between-BCTU-Control-Mode-and-Trigger/td-p/2384122 From the screenshot you provided, it seems you haven't made any changes to my previous reply. I've already informed you that there's a problem with your ADC clock divider configuration, Also, are you sure your external clock is 25MHz? If you've checked these two points and the problem persists after testing, you can try modifying the ADC channel's sampling time. This option allows you to modify the sampling time; you can try increasing the sampling time and testing again. Re: S32k322 ADC Configuration Issue Hi @Senlent , I have also same issue which you mentioned above. Our external oscillator clock is 25 MHz. According to the S32K322 datasheet, the ADC supports up to 80 MHz, so I have configured a prescaler of 2. I also configured the sampling time to 1.2 microseconds and set the BCTU mode to trigger mode. However, we are still getting noisy data when executing the BCTU method and the normal chain method simultaneously on the same ADC0 peripheral. Is there a workaround or an alternative method to safely run both on the same ADC0 peripheral? Re: S32k322 ADC Configuration Issue Hi@praveen_ext Aren't you the same company? You're asking the exact same questions. https://community.nxp.com/t5/S32K/Difference-in-ADC-noise-between-BCTU-Control-Mode-and-Trigger/m-p/2384122#M59412 It seems you haven't been reading my answer carefully. This is the third time I've told you that your clock divider settings are incorrect. For 160MHz, you need to set them to 2 and 4. Re: S32k322 ADC Configuration Issue Hi @Senlent , I have also same issue which you mentioned above. Our external oscillator clock is 25 MHz. According to the S32K322 datasheet, the ADC supports up to 80 MHz, so I have configured a prescaler of 2. I also configured the sampling time to 1.2 microseconds and set the BCTU mode to trigger mode. However, we are still getting noisy data when executing the BCTU method and the normal chain method simultaneously on the same ADC0 peripheral. Is there a workaround or an alternative method to safely run both on the same ADC0 peripheral? In the meantime, I reduced the Instance 1 clock frequency to 40 MHz and configured the sampling time to 1.2 microseconds. Following these changes, the measured values from the BCTU are no longer showing noise. Adc_Raw_Val_Ph3 connceted with sensor remainig two values in floating. RwaeVal - configured normal chain Re: S32k322 ADC Configuration Issue Hi @Senlent , We tested the previous suggestions, but the issue is still not resolved. After further configuration and verification, I have attached the updated test data and configuration images below. kindly assist us where we missed. ADC0 ADC1 Re: S32k322 ADC Configuration Issue Hi@praveen_ext Share your project and i will test it on myside,
記事全体を表示
ディスプレイのタッチ入力がプライマリディスプレイに正しくマッピングされていません 私たちは、LVDSからHDMIへのアダプターカードを使って、i.MX 8 QuadMax MEK CPUボードのプライマリディスプレイで2台のディスプレイを設定し、タッチを有効にしようとしています。タッチ入力にはUSB Type-Cコネクタ(J17)を使用しています。 以下に、我々が得た観察結果を示します。 タッチ入力をプライマリディスプレイに接続しても、入力は認識されるものの、マッピングされません。しかし、それをセカンダリディスプレイに接続すると、タッチ入力は完璧に動作します。 回避策として、ディスプレイポートを入れ替えました。つまり、プライマリポートとセカンダリポートを相互に接続しました。すると、セカンダリースクリーンはプライマリースクリーンと同じ解像度になってしまうため、私たちのプロジェクトには理想的ではありません。 以下に、受信した応答とログを示します。     $ adb shell dumpsys SurfaceFlinger --display-id  ディスプレイ 4632668096568543232 (HWC ディスプレイ 0): ポート=0 pnpId=RTK ディスプレイ名="WaveShare"[15.6]  ディスプレイ 4624778001127622657 (HWC ディスプレイ 1): ポート=1 pnpId=KTC ディスプレイ名="WaveShare"[12.3] 【タッチ入力をメインディスプレイへ】 $ adb shell getevent -i | grep location  場所: "imx-sc-pwrkey/input0"    adb shell getevent -i  デバイス1を追加: /dev/input/event0  バス:0019  ベンダー0000  製品0000  バージョン0000  名前: "sc-powerkey"  場所: "imx-sc-pwrkey/input0"  id: ""  バージョン: 1.0.1    イベント情報:  キー(0001):0074  入力プロパティ:  【タッチ入力をセカンダリディスプレイへ】  $adb shell getevent -i | grep location  場所:「USB-XHCI-HCD.1.Auto-1/input0」  場所: "imx-sc-pwrkey/input0"    adb shell getevent -i  デバイス1を追加: /dev/input/event1  バス:0003  ベンダー0712  製品000a  バージョン0111  名前: "HID 0712:000a"  場所:「USB-XHCI-HCD.1.Auto-1/input0」  id: ""  バージョン: 1.0.1    イベント情報:  凡例(0001):014a  ABS (0003): 0000 : 値 0、最小値 0、最大値 1920、ファジー 0、フラット 0、解像度 4  0001 : 値 0、最小値 0、最大値 720、ファジー 0、フラット 0、解像度 2  002f : 値 0、最小値 0、最大値 9、ファジー 0、フラット 0、解像度 0  0035 : 値 0、最小値 0、最大値 1920、ファジー 0、フラット 0、解像度 4  0036 : 値 0、最小値 0、最大値 720、ファジー 0、フラット 0、解像度 2  0039 : 値 0、最小値 0、最大値 65535、ファジー 0、フラット 0、解像度 0  MSC (0004): 0005  入力プロパティ:  入力プロパティダイレクト  デバイス2を追加: /dev/input/event0  バス:0019  ベンダー0000  製品0000  バージョン0000  名前: "sc-powerkey"  場所: "imx-sc-pwrkey/input0"  id: ""  バージョン: 1.0.1    イベント情報:  キー(0001):0074  入力プロパティ:  Re: Display Touch input not mapped properly with primary display こんにちは、 基板のどのポートがディスプレイのタッチ入力に接続されているか、そしてどのポートがADBアクセスに使われているのか教えていただけますか? できるだけ早くご返信ください。 ありがとうございます。 Re: Display Touch input not mapped properly with primary display こんにちは@Zhiming_Liuさん 解決策をありがとうございました。タッチマッピングが正しく設定できました。 同じブロッカーを持っている人のために、 1)「input-port-associations.xml」は/vendor/etcにあります。 2)コマンド $getevent -i | grep location を使用してディスプレイの入力構成を確認します。 3) 次に、XMLファイルに記載されているディスプレイの設定を変更します。 Re: Display Touch input not mapped properly with primary display こんにちは、 @adithysm65さん AOSPのinput-port-associations.xmlファイルを変更してみましたか? https://github.com/nxp-imx-android/android-imx_device_fsl/blob/android-13.0.0_2.2.0/imx8q/mek_8q/input-port-associations.xml
記事全体を表示
默认工作区 你好, 我正在使用MCUXpressoIDE v.24.9.25 (我知道我可以运行更新的版本,但由于某些原因,我需要运行 24.9.25)。正如我在“C:\NXP\MCUXpressoIDE_24.9.25\ide\configuration\config.ini”中看到的那样,osgi.instance.area.default为“@user.home/Documents/MCUXpressoIDE_24.9.25/workspace”,所以是正确的。 但是,如果我关闭 Windows 用户会话并使用其他用户打开一个新会话,当我运行 MCUXpressoIDE 时,默认工作区是第一个用户的工作区,所以我需要切换到第二个工作区目录,因为每个用户都有自己的目录。 osgi.instance.area.default似乎工作不正常,因为@user .home/Documents/MCUXpressoIDE_24.9.25/workspace 应该是每个用户的家目录,但它总是获取第一个登录用户的家目录。 我该如何重新配置它? 谢谢。 #mcux Re: Default workspace 你好, 请问您是否已启用“将此设置为默认值,不再询问”单元格选项? 如果勾选“将此用作默认值且不再询问”选项,MCUXpresso IDE 将始终启动并打开所选工作区;我建议不要勾选此框来选择工作区。 您可以为用户 2 添加另一个工作区,并将其保留在“最近使用的工作区”中,这样您就可以在打开应用程序之前选择所需的工作区。 另外,在“选项卡窗口”>“首选项”>“常规”>“启动和关闭”>“工作区”中 启用启动时提示选择工作区。 此致敬礼,路易斯
記事全体を表示
S32k322 ADCの設定に関する問題 私は3つのADCチャネルをBCTU割り込みで電流検知用に設定しています(CTUモードはトリガーモードに設定)。残りのADCチャネルは電圧と温度検知用にノーマルチェーン方式で設定しています。 この構成中、電圧と温度の検知は正常に動作していますが、電流センサがノイズを含む生値を感知しているため、電流制御に異常なスパイクが発生しています。また、CTUモードをトリガーモードからコントロールモードに変更し、現在のセンサーチャネルでは生値ノイズが減少しました。しかし、通常のチャネルで設定された他のチャネルは動作しませんでした。 私たちの期待は、BCTUトリガーを用いた電流検出において単一ADCペリフェラル(ADC0)と、通常の連鎖方法での電圧および温度検出をスパイクなしで処理することです。 注:当社のハードウェアは設定(例:電流センサーチャネルは以下の通り、BCTU方式での読み取り用にP7-ADC0、P2、P3-ADC1)で設計されています。その後、通常のチェーン方法(ADC0 - X0,X1,S19およびADC1-P0,P2,P3,P1,S10)で設定された残りのADCチャネルが続きます S32 SDK for S32K1 S32 SDK for S32V Re: S32k322 ADC Configuration Issue こんにちは、@ praveen_ext これはまさにあなたが直面している問題と同じだと思います。 https://community.nxp.com/t5/S32K/Difference-in-ADC-noise-between-BCTU-Control-Mode-and-Trigger/td-p/2384122 あなたが提供してくれたスクリーンショットを見る限り、私の以前の返信に何も変更を加えていないようですね。 既にお伝えしたとおり、ADCクロック分周器の設定に問題があります。 また、外部クロックが25MHzであることは確かですか? この2点を確認しても問題が解決しない場合は、ADCチャネルのサンプリング時間を変更してみてください。 このオプションではサンプリング時間を調整できます。サンプリング時間を延ばして再度テストしてみるのもいいでしょう。 Re: S32k322 ADC Configuration Issue こんにちは、 @Senlent さん。 私も上記で述べられたのと同じ問題を抱えています。 当社の外部発振器クロックは25MHzです。S32K322のデータシートによると、ADCは最大80MHzをサポートしているので、プリスケーラーは2に設定しています。また、サンプリング時間を1.2マイクロ秒に設定し、BCTUモードをトリガーモードに設定しました。しかし、同じADC0ペリフェラルでBCTU法とノーマルチェーン法を同時に実行しても、依然としてノイズの多いデータが得られます。同じADC0ペリフェラルで両方を安全に動かす回避策や代替方法はありますか? Re: S32k322 ADC Configuration Issue こんにちは、 @Senlent さん。 私も上記で述べられたのと同じ問題を抱えています。 外部発振器のクロックは25MHzです。S32K322のデータシートによると、ADCは最大80MHzをサポートしているので、プリスケーラーは2MHzに設定しています。また、サンプリング時間を1.2マイクロ秒に設定し、BCTUモードをトリガーモードに設定しました。しかし、同じADC0ペリフェラルでBCTU方法とノーマルチェーン方法を同時に実行しても、依然としてノイズの多いデータが得られます。同じADC0ペリフェラルで両方を安全に動かす回避策や代替方法はありますか? その間、インスタンス1のクロック周波数を40MHzに下げ、サンプリング時間を1.2マイクロ秒に設定しました。これらの変更後、BCTUからの測定値にはノイズが見られなくなった。 Adc_Raw_Val_Ph3センサーと一致し、浮動している2つの値を保持しています。 RwaeVal - 通常のチェーンを設定済み Re: S32k322 ADC Configuration Issue こんにちは、@ praveen_ext 同じ会社じゃないの?あなたも全く同じ質問をしていますね。 https://community.nxp.com/t5/S32K/Difference-in-ADC-noise-between-BCTU-Control-Mode-and-Trigger/mp/2384122#M59412 私の回答をよく読んでいないようですね。 時計の分周器の設定が間違っていると、これで3度目ですよ。 160MHzの場合は、2と4に設定する必要があります。 Re: S32k322 ADC Configuration Issue こんにちは、 @Senlent さん。 以前に提案された方法を試してみましたが、問題はまだ解決していません。さらなる設定と検証を行った後、更新されたテストデータと設定イメージを以下に添付します。 我々が見落とした点があれば、ご指摘いただければ幸いです。 ADC0 ADC 1 Re: S32k322 ADC Configuration Issue こんにちは、@ praveen_ext プロジェクトを共有していただければ、こちらでテストしてみます。
記事全体を表示
Solyball Cooling Ace 专为现代生活而设计 当气温升高时,保持舒适的室内环境成为许多人的首要任务。无论是在家、办公室还是个人工作空间,过高的温度都会影响注意力、放松度和整体舒适度。Solyball 正是为此提供了一个便捷实用的解决方案。Solyball 的设计兼顾便携性、简洁性和现代生活方式,是一款小巧的降温设备,可帮助用户在各种室内环境中营造更舒适的氛围。 Solyball 最显著的特点之一 是其轻巧便携的设计。与笨重难搬或占用大量空间的大型制冷系统不同,Solyball 体积小巧,几乎可以完美融入任何房间。其便携性使用户能够轻松地将其从一个地方搬到另一个地方,从而满足全天候不同需求。无论您是在家办公、在客厅放松,还是准备享受一夜安眠,Solyball 都可以放置在任何您需要额外舒适感的地方。 Solyball 的多功能性 使其成为各种室内环境的理想之选。在卧室里,它有助于在温暖的夜晚营造更舒适的氛围。舒适的睡眠环境对整体健康至关重要,而小巧的降温设备可以提升您的睡眠体验。Solyball 尺寸适中,可轻松放置在床头柜或其他平面上,不会造成空间杂乱。 对于专业人士和远程办公人员来说, Solyball能帮助他们保持舒适的工作空间,从而显著提高工作效率。室内温度过高有时会影响专注力,难以集中精力完成工作。Solyball 提供了一种切实可行的提升工作舒适度的方法,帮助用户在一天中营造更加愉悦的工作环境。其小巧的体积使其可以方便地放置在办公桌或工作台上,而不会占用过多空间。 Solyball的便利性也体现在客厅和家庭共享空间中。这些区域通常是人们聚集的中心场所,他们会在这里看电视、阅读、社交或放松身心。将 Solyball 融入这些空间,用户可以在日常活动中享受更舒适的氛围。其现代外观确保它能与现代家居装饰自然融合。
記事全体を表示
FRDM MCX A266のピン設定ツールが見つかりません サイト内のピン設定ツールが見つかりません。 FRDMトレーニング Re: Can't find pin configuration tool for FRDM MCX A266 こんにちは、 これは、ツールを使い始める際に役立つ情報です。 MCUXpresso設定ツールのクイックスタートガイド MCUXpresso設定ツールユーザーガイド(IDE) 必要な情報やツールがあればお知らせください。 敬具、ルイス Re: Can't find pin configuration tool for FRDM MCX A266 https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-config-tools-pins-clocks-and-peripherals:MCUXpresso-Config-Toolsが見つかりました Re: Can't find pin configuration tool for FRDM MCX A266 ご返信ありがとうございます。 可能であれば、これらのツールのステップバイステップ設定の例を教えていただけると助かります。 Re: Can't find pin configuration tool for FRDM MCX A266 こんにちは、 何を達成したいのかによりますが、どのプロセスにアシスタントが必要なのか確認または説明してもらえますか? また、ユーザーガイドのMCUXpresso設定ツールユーザーガイド(IDE)第3章には、手順や写真が付いており、ツールの機能にリダイレクトして設定に合わせて調整できます。 敬具、ルイス Re: Can't find pin configuration tool for FRDM MCX A266 はい、お願いします。私が今やろうとしているのは、ごくシンプルなことです。 4つのDACチャネルと4つのADCチャネルを定義します。 それらを内部の4つのADCチャネルにルーティングしてループを閉じます。 それらの信号が届いたことを確認し、入力数を掛け合わせます。 再度掛け合わせて、パフォーマンスを測定してください。 デバッグおよび結果表示のために、USB経由のシリアル通信でログ出力を行うように設定してください。
記事全体を表示
S32DS issue regarding the reference to external files Currently, we are using the demo project. The files in the SDK/platform/drivers/src directory of the project folder are external linked files, which makes it difficult for me to share the project with others as I cannot locate these files. I wonder if there is any way to mount the linked files into the project (excluding the method of copying them one by one). Re: S32DS issue regarding the reference to external files Hello @NXP2 , This is expected behavior for older SDK-based S32DS projects. Some SDK driver files are added as Eclipse linked resources, so they are shown in the project tree, but the physical files remain in the installed SDK package location.   For sharing such a project, the recommended approach is to provide the project together with the exact S32DS/SDK package version required on the other PC. If a fully self-contained project is needed, the SDK files must be copied into the project and the linked resources/build paths updated accordingly.   Please note that newer RTD-based projects generated by S32 Configuration Tools copy the required/generated driver files into the project automatically during the Update Code step. Best regards, Pavel Re: S32DS issue regarding the reference to external files The currently used version is S32SDK_S32K1XX_RTM_4.0.2. As shown in the following figure, the two files come from different folders. Do we need to set anything for this? Re: S32DS issue regarding the reference to external files Hello @NXP2 , What version of SDK for which S32K family do you use? Best regards, Pavel
記事全体を表示
显示屏触摸输入未正确映射到主显示屏 我们正在尝试使用 LVDS 转 HDMI 适配器卡为 i.MX 8 QuadMax MEK CPU 板设置两个显示器,并在主显示器上启用触摸功能。我们使用 USB Type-C 连接器 (J17) 进行触摸输入。 以下是我们观察到的情况: 触摸输入可以被识别,但是当我们将触摸输入连接到主显示器时,它无法进行映射。但是,当我们将其连接到辅助显示器时,触摸输入功能就完全正常了。 作为权宜之计,我们交换了显示端口,即主端口与副端口互换。副屏幕的分辨率与主屏幕相同,这对于我们的项目来说并不理想。 以下是收到的回复和日志。     $ adb shell dumpsys SurfaceFlinger --display-id  显示 4632668096568543232 (HWC 显示 0): port=0 pnpId=RTK displayName="WaveShare"[15.6]  显示器 4624778001127622657(HWC 显示器 1):端口=1 pnpId=KTC 显示名称="WaveShare"[12.3] [触摸输入到主显示屏] $ adb shell getevent -i | grep location  位置:"imx-sc-pwrkey/input0"    adb shell getevent -i  添加设备 1:/dev/input/event0    总线:      0019  供应商 0000  产品 0000  版本 0000  名称:"sc-powerkey"  位置:"imx-sc-pwrkey/input0"  ID: ””  版本:1.0.1  事件:  密钥 (0001): 0074  输入属性:  [触摸输入到辅助显示屏]  $adb shell getevent -i | grep location  位置:“usb-xhci-hcd.1.auto-1/input0”  位置:"imx-sc-pwrkey/input0"    adb shell getevent -i  添加设备 1:/dev/input/event1    总线:      0003  供应商 0712  产品 000a  版本 0111  名称:“HID 0712:000a”  位置:“usb-xhci-hcd.1.auto-1/input0”  ID: ””  版本:1.0.1  事件:  密钥 (0001): 014a  ABS (0003): 0000:值 0,最小值 0,最大值 1920,模糊度 0,平坦度 0,分辨率 4  0001:值 0,最小值 0,最大值 720,模糊度 0,平坦度 0,分辨率 2  002f:值 0,最小值 0,最大值 9,模糊度 0,平坦度 0,分辨率 0  0035:值 0,最小值 0,最大值 1920,模糊度 0,平坦度 0,分辨率 4  0036:值 0,最小值 0,最大值 720,模糊度 0,平坦度 0,分辨率 2  0039:值 0,最小值 0,最大值 65535,模糊度 0,平坦度 0,分辨率 0  MSC (0004): 0005  输入属性:  输入属性直接  添加设备 2:/dev/input/event0    总线:      0019  供应商 0000  产品 0000  版本 0000  名称:"sc-powerkey"  位置:"imx-sc-pwrkey/input0"  ID: ””  版本:1.0.1  事件:  密钥 (0001): 0074  输入属性:  Re: Display Touch input not mapped properly with primary display 你好, 请问主板上哪个端口连接到显示屏的触摸输入,哪个端口用于 ADB 访问? 请尽快回复。 谢谢。 Re: Display Touch input not mapped properly with primary display 你好@Zhiming_Liu , 谢谢你的解答,触摸映射设置已经正确了。 仅供有同样困扰的人参考。 1)“input-port-associations.xml”位于/vendor/etc下。 2)使用命令 $getevent -i | grep location 检查显示器的输入配置。 3)现在更改 xml 文件中提到的显示配置。 Re: Display Touch input not mapped properly with primary display 嗨@adithysm65 您是否尝试过在AOSP中修改input-port-associations.xml文件? https://github.com/nxp-imx-android/android-imx_device_fsl/blob/android-13.0.0_2.2.0/imx8q/mek_8q/input-port-associations.xml
記事全体を表示
Display Touch input not mapped properly with primary display We are attempting to set up two displays and enable touch on the primary display for the i.MX 8 QuadMax MEK CPU Board using an LVDS to HDMI Adapter Card. We are using a USB Type-C connector (J17) for the touch input. Here are the observations we have made: The input is recognized but is not getting mapped when we connect the touch input to the primary display. However, when we connect it to the secondary display, the touch input works perfectly. As a workaround, we interchanged the display ports, i.e., primary to secondary and vice versa. The secondary screen then takes up the resolution of the primary screen, which is not ideal for our project. Following are the responses and logs received.     $ adb shell dumpsys SurfaceFlinger --display-id  Display 4632668096568543232 (HWC display 0): port=0 pnpId=RTK displayName="WaveShare"[15.6]  Display 4624778001127622657 (HWC display 1): port=1 pnpId=KTC displayName="WaveShare"[12.3]   [Touch input to primary display]  $ adb shell getevent -i | grep location    location: "imx-sc-pwrkey/input0"    adb shell getevent -i   add device 1: /dev/input/event0    bus:      0019    vendor    0000    product   0000    version   0000    name:     "sc-powerkey"    location: "imx-sc-pwrkey/input0"    id:       ""    version:  1.0.1    events:      KEY (0001): 0074     input props:        [Touch input to secondary display]  $adb shell getevent -i | grep location    location: "usb-xhci-hcd.1.auto-1/input0"    location: "imx-sc-pwrkey/input0"    adb shell getevent -i   add device 1: /dev/input/event1    bus:      0003    vendor    0712    product   000a    version   0111    name:     "HID 0712:000a"    location: "usb-xhci-hcd.1.auto-1/input0"    id:       ""    version:  1.0.1    events:      KEY (0001): 014a       ABS (0003): 0000  : value 0, min 0, max 1920, fuzz 0, flat 0, resolution 4                  0001  : value 0, min 0, max 720, fuzz 0, flat 0, resolution 2                  002f  : value 0, min 0, max 9, fuzz 0, flat 0, resolution 0                  0035  : value 0, min 0, max 1920, fuzz 0, flat 0, resolution 4                  0036  : value 0, min 0, max 720, fuzz 0, flat 0, resolution 2                  0039  : value 0, min 0, max 65535, fuzz 0, flat 0, resolution 0      MSC (0004): 0005     input props:      INPUT_PROP_DIRECT  add device 2: /dev/input/event0    bus:      0019    vendor    0000    product   0000    version   0000    name:     "sc-powerkey"    location: "imx-sc-pwrkey/input0"    id:       ""    version:  1.0.1    events:      KEY (0001): 0074     input props:        Re: Display Touch input not mapped properly with primary display Hi, Could you please let me know which port on the board is connected to the touch input for the displays, and which port is being used for ADB access? Please reply as soon as possible. Thanks. Re: Display Touch input not mapped properly with primary display Hello @Zhiming_Liu , Thanks for the solution,got the touch mapping right. Just for someone with same blocker, 1)The 'input-port-associations.xml' is located under  /vendor/etc. 2)Check the input configuration of the display using the command $getevent -i | grep location. 3)Now change the configurations of the display mentioned under the xml file. Re: Display Touch input not mapped properly with primary display Hi @adithysm65  Have you tried to modify the input-port-associations.xml file in aosp? https://github.com/nxp-imx-android/android-imx_device_fsl/blob/android-13.0.0_2.2.0/imx8q/mek_8q/input-port-associations.xml
記事全体を表示
Solyball Cooling Aceは、現代の生活に合わせて設計されています。 ソリーボール:気温が上がり始めると、多くの人にとって快適な室内環境を維持することが優先事項となります。自宅でもオフィスでも、個人の作業スペースでも、過度の熱は集中力やリラックス、全体的な快適さに影響を及ぼします。ここでSolyballが便利で実用的な解決策を提供します。携帯性、シンプルさ、そして現代的な生活を念頭に置いて設計されたSolyballは、さまざまな屋内環境でより快適な雰囲気を作り出すためのコンパクトな冷却装置です。 One of the most notable features of ソリボール は、軽量でポータブルなデザインです。大型の冷却システムが移動が難しかったり、十分なスペースを必要とするのに対し、ソリボールはほぼどんな部屋にも快適に収まるほどコンパクトです。ポータブルな性質により、ユーザーは一つの場所から別の場所へ簡単に持ち運べ、必要に応じて一日中使うのに適しています。ホームオフィスで作業している場合でも、リビングルームでくつろいでいる場合でも、安らかな睡眠の準備をしている場合でも、Solyballは快適さを求めるあらゆる場所に配置できます。 The versatility of Solyball makes it a valuable addition to many different indoor environments. In bedrooms, it can help create a more enjoyable atmosphere during warm evenings. Comfortable sleeping conditions are important for overall well-being, and a compact cooling device can contribute to a more pleasant bedtime experience. Solyball's convenient size allows it to fit neatly on a bedside table or nearby surface without creating clutter. プロフェッショナルやリモートワーカーにとって、Solyballは快適な作業環境を維持することが生産性に不可欠です。室内の暖かさは、時にタスクや責任に集中し続けるのが難しいことがあります。Solyballは作業中の快適さを向上させる実用的な方法を提供し、ユーザーが一日を通じてより快適な環境を作り出すのに役立ちます。コンパクトなサイズのおかげで、机やワークステーションに置いても無駄なスペースを取ることなく快適に置けます。 Solyballのリビングルームや共有のファミリースペースも、Solyballの利便性の恩恵を受けられます。これらのエリアは、人々がテレビを見たり、読書をしたり、交流したり、ただリラックスしたりする中心的な集まりの場として機能します。Solyballをこれらの空間に取り入れることで、ユーザーは日常生活をより快適な環境で過ごすことができます。モダンな外観により、現代的なインテリアと自然に調和しています。
記事全体を表示
S32DS 问题涉及对外部文件的引用 目前,我们正在使用演示项目。项目文件夹 SDK/platform/drivers/src 目录中的文件是外部链接文件,这让我很难与他人共享该项目,因为我找不到这些文件。我想知道是否有办法将链接的文件挂载到项目中(不包括逐个复制的方法)。 Re: S32DS issue regarding the reference to external files 您好@NXP2 , 这是基于旧版 SDK 的 S32DS 项目的预期行为。一些 SDK 驱动程序文件被添加为 Eclipse 链接资源,因此它们会显示在项目树中,但物理文件仍然保留在已安装的 SDK 包位置。   对于共享此类项目,建议的方法是将项目与另一台 PC 上所需的确切 S32DS/SDK 代码包,软件包版本一起提供。如果需要完全独立的项目,则必须将 SDK 文件复制到项目中,并相应地更新链接的资源/版本路径。   请注意,由 S32 配置工具生成的较新的基于 RTD 的项目会在更新代码步骤期间自动将所需/生成的驱动程序文件复制到项目中。 顺祝商祺! 帕维尔 Re: S32DS issue regarding the reference to external files 目前使用的版本是 S32SDK_S32K1XX_RTM_4.0.2。如下图所示,这两个文件来自不同的文件夹。我们需要为此做任何设置吗? Re: S32DS issue regarding the reference to external files 您好@NXP2 , 您使用的是哪个版本的SDK,对应哪个S32K系列? 顺祝商祺! 帕维尔
記事全体を表示
i.MX8QM上のAAOS 15における複数ディスプレイのタッチ入力設定 チームの皆さん、こんにちは。 私はi.MX8QMボードで10.1インチのHDMI LCD(E)タッチスクリーンディスプレイを使用しています。これらのディスプレイを基板に適切に接続し、各ディスプレイのタッチ入力を設定する方法について、ご指導をお願いします。具体的には、タッチ入力(USB)を接続するために基板上のどのポートやインターフェースを使うべきかを理解したいです。さらに、Android Automotiveシステム内の各タッチ入力を対応するディスプレイに正しくマッピングする方法も助けが必要です。 ありがとうございます。 Re: Touch Input Configuration for Multiple Displays in AAOS 15 on i.MX8QM こんにちは、 i.MX 8QuadMaxは最大4台のディスプレイに対応しています: 以下の4つのディスプレイ(HDMI_TX、LVDS0_CH0、LVDS1_CH0、MIPI_DSI1)から、2~4個のディスプレイを任意の組み合わせで使用できます。 以下の4つのディスプレイ(LVDS0_CH0、LVDS1_CH0、MIPI_DSI0、MIPI_DSI1)から2~4個のディスプレイを任意の組み合わせで使用できます。 入力設定については、Android Automotive User's Guideの8.3.3.1セクション「ディスプレイポートと入力ポートのバインド」を参照してください。 よろしくお願いいたします。 Re: Touch Input Configuration for Multiple Displays in AAOS 15 on i.MX8QM よろしくお願いします。
記事全体を表示
FRDM i.MX 93 你好。我打算在一个项目中使用 FRDM i.MX 93,该项目需要 Linux 操作系统,并通过 RS232、SPI 和 I2C 端口控制其他设备。 我看到有一个用于 USB 调试的 UART 端口,还有另一个 UART 端口、I2C 端口和 SPI 端口可以使用吗?   Re: FRDM i.MX 93 嗨@alberto83 是的,IMX93 有 8 个 UART 接口、8 个 I²C 接口和 8 个 SPI 接口。 有关 imx93 FRDM 的更多信息,您可以参考以下链接: https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM-IMX93 BR
記事全体を表示
S32DSにおける外部ファイル参照に関する問題 現在、私たちはデモプロジェクトを使用しています。プロジェクトフォルダのSDK/platform/drivers/srcディレクトリにあるファイルは外部リンクファイルであり、これらのファイルが見つからず、他の人と共有するのが難しいです。リンクされたファイルをプロジェクトにマウントする方法はありますか(一つずつコピーする方法は除きますが)。 Re: S32DS issue regarding the reference to external files こんにちは、 @NXP2 さん、 これは古いSDKベースのS32DSプロジェクトで予想される動作です。一部のSDKsドライバファイルはEclipseにリンクされたリソースとして追加され、プロジェクトツリーには表示されますが、物理ファイルはインストール済みSDKパッケージの場所に残ります。   このようなプロジェクトを共有する場合、推奨される方法は、もう一方のPCで必要な正確なS32DS/SDKパッケージバージョンをプロジェクトに提供することです。完全に自己完結型のプロジェクトが必要な場合は、SDKファイルをプロジェクトにコピーし、リンクされたリソースやビルドパスを適切に更新する必要があります。   なお、S32構成ツールによって生成される新しいRTDベースのプロジェクトは、Update Codeステップ中に必要な/生成済みドライバーファイルを自動的にプロジェクトにコピーします。 よろしくお願いいたします。 パベル Re: S32DS issue regarding the reference to external files 現在使用されているバージョンはS32SDK_S32K1XX_RTM_4.0.2です。次の図に示すように、2つのファイルは異なるフォルダから取得されています。これに関して何か設定する必要はありますか? Re: S32DS issue regarding the reference to external files こんにちは、 @NXP2 さん、 どのS32KファミリでどのバージョンのSDKを使っていますか? よろしくお願いいたします。 パベル
記事全体を表示
Can't find pin configuration tool for FRDM MCX A266 Can't find on site pin configuration tool. FRDM-Training Re: Can't find pin configuration tool for FRDM MCX A266 Hello, This is some helpful information if you are starting with the tool Quick Start Guide for MCUXpresso Config Tools MCUXpresso Config Tools User's Guide (IDE) If there is information or tools that you need to look for, let us know Best Regards, Luis Re: Can't find pin configuration tool for FRDM MCX A266 Found https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-config-tools-pins-clocks-and-peripherals:MCUXpresso-Config-Tools Re: Can't find pin configuration tool for FRDM MCX A266 Thanks for your reply. Will glad if you could point me to howto step by step configuration examples of those tools if possible. Re: Can't find pin configuration tool for FRDM MCX A266 Hello, It would depend on what are you trying to achieve, if you could confirm or describe what process do you need assistant for? Also, the User guide MCUXpresso Config Tools User's Guide (IDE) Chapter 3 is Pin Configuration Instructions with steps and photos that can redirect you to the tool functionalities and match your configuration. Best Regards, Luis Re: Can't find pin configuration tool for FRDM MCX A266 Yes, please. What I'm trying to do is something simple at this point. Define 4 DAC and 4 ADC channels. Route them to the 4 ADC channels internally to close the loop. Test that those signals arrived, then multiply the number of inputs. Multiply again and measure performance. Define log prints to serial over USB for debugging and results presentation.
記事全体を表示
S32k322 ADC配置问题 我使用了三个 ADC 通道,配置为使用 BCTU 中断进行电流检测(CTU 模式配置为触发模式),其余 ADC 通道配置为正常链式方法进行电压和温度检测。 在此配置下,电压和温度传感工作正常,但电流传感器检测到的是带有噪声的原始值,因此电流控制中会出现异常尖峰。此外,我们将 Ctu 模式从触发模式改为控制模式,目前传感器通道的原始值噪声有所降低。但是,正常频道中配置的其他频道却无法工作。 我们期望使用单个 ADC 外设 (ADC0) 进行电流检测,采用 BCTU 触发,并采用常规链式方法进行电压和温度检测,而不会出现任何尖峰。 注意:我们的硬件设计有配置(即当前传感器通道配置如下,P7-ADC0、P2 和 P3-ADC1 用于 BCTU 方法读取)。接下来,其余ADC通道配置为正常链式方法(ADC0 - X0、X1、S19 和 ADC1 - P0、P2、P3、P1、S10) S32K1系列的S32SDK S32V 的 S32 SDK Re: S32k322 ADC Configuration Issue 你好@ praveen_ext 我相信你遇到的问题和这个一模一样。 https://community.nxp.com/t5/S32K/Difference-in-ADC-noise-between-BCTU-Control-Mode-and-Trigger/td-p/2384122 从你提供的截图来看,你似乎没有对我之前的回复做任何修改。 我已经告知过你,你的ADC时钟分频器配置存在问题。 另外,你确定你的外部时钟频率是 25MHz 吗? 如果您已经检查了这两点,并且在测试后问题仍然存在,您可以尝试修改 ADC 通道的采样时间。 此选项允许您修改采样时间;您可以尝试增加采样时间并再次进行测试。 Re: S32k322 ADC Configuration Issue 嗨@Senlent , 我也有和你上面提到的同样的问题。 我们的外部振荡器时钟频率为 25 MHz。根据 S32K322 数据手册,ADC 支持高达 80 MHz 的频率,所以我将预分频器配置为 2。我还将采样时间配置为 1.2 微秒,并将 BCTU 模式设置为触发信号模式。但是,当在同一个 ADC0 外设上同时执行 BCTU 方法和普通链方法时,我们仍然会得到噪声数据。是否有变通方法或替代方法可以安全地在同一个 ADC0 外设上运行这两个程序? Re: S32k322 ADC Configuration Issue 你好@ praveen_ext 你们不就是同一家公司吗?你问的也是同样的问题。 https://community.nxp.com/t5/S32K/Difference-in-ADC-noise-between-BCTU-Control-Mode-and-Trigger/mp/2384122#M59412 看来你没有仔细阅读我的回答。 这是我第三次告诉你,你的时钟分频器设置不正确。 对于 160MHz,你需要将它们设置为 2 和 4。 Re: S32k322 ADC Configuration Issue 嗨@Senlent , 我也有和你上面提到的同样的问题。 我们的外部振荡器时钟频率为 25 MHz。根据 S32K322 数据手册,ADC 支持最高 80 MHz 的频率,所以我将预分频器设置为 2。我还将采样时间设置为 1.2 微秒,并将 BCTU 模式设置为触发模式。但是,当在同一个 ADC0 外设上同时执行 BCTU 方法和常规链式方法时,仍然会得到噪声数据。是否有解决方法或替代方法可以安全地在同一个 ADC0 外设上运行这两种方法? 与此同时,我将实例 1 的时钟频率降低到 40 MHz,并将采样时间配置为 1.2 微秒。经过这些改变后,BCTU 的测量值不再显示噪声。 Adc_Raw_Val_Ph3 与传感器连接,两个值仍然处于浮空。 RwaeVal - 配置正常链 Re: S32k322 ADC Configuration Issue 嗨@Senlent , 我们测试了之前的建议,但问题仍然没有解决。经过进一步配置和验证,我已将更新后的测试数据和配置图片附在下面。 请您帮忙指出我们遗漏的地方。 ADC0 ADC1 Re: S32k322 ADC Configuration Issue 你好@ praveen_ext 请分享您的项目,我将在我的环境中进行测试。
記事全体を表示