Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
i.MX 8M Plus:VPUは4K H.264の短いクリップを1080p HDMIディスプレイにダウンスケールして再生できますか? 皆さんこんにちは。i.MX 8M Plusボードを使用して、1080pのHDMIディスプレイ上で短いMP4クリップ(それぞれ4~10秒、H.264、3840x2160、24fps)をループ再生することを検討しています。これらのクリップは、例えば Veo3 AI上のGemini Omni Flashモデルなど、AI動画ジェネレーターから来ており、最大4Kまでエクスポートできます(開示:私はGoogleとは提携していない独立サービス、Veo3 AIと仕事をしています)。 設定を行う前に、その方法を確認しておきたいと思います。私が考えていたのは、このようなパイプラインです。 gst-launch-1.0 filesrc location=clip.mp4 ! qtdemux ! h264parse ! vpudec ! imxvideoconvert_g2d ! video/x-raw,width=1920,height=1080 ! waylandsink 質問: 8M Plus VPUは4K H.264をリアルタイムで24fpsでデコードできますか?それともクリップを1080pにトランスコードしてからボードにコピーしたほうが良いのでしょうか? imxvideoconvert_g2dは4Kから1080pへのダウンスケールに適した要素でしょうか、それともwaylandsinkへのゼロコピーパスが存在するのでしょうか? クリップのプレイリストをループ再生する場合、ファイル間に黒いフレームが表示されないようにするための推奨される方法はありますか? アドバイスをいただければ幸いです。 Re: i.MX 8M Plus: can the VPU play 4K H.264 short clips downscaled to a 1080p HDMI display? こんにちは、 @ethancaldwell 1. imx8mp vpuはハードウェア制限なしで4K動画をデコードできますが、1080pのパフォーマンスのみ保証し、私たちはSWの制限を1080pに設定しました。4K解像度を使用する必要がある場合は、ソースコードを変更する必要があります。SO、クリップを1080pにトランスコードする方が良いです。 2. スケーリングにはimxvideoconvert_g2dを使用してください。 3. 現在、`gst-launch`において複数のファイルをシームレスに切り替えるための公式な直接的な解決策は存在しません。複数のファイルを事前に1つの長い動画に多重化し、その単一ファイルをループ再生するように設定することをお勧めします。 B.R
View full article
FRDM-IMX93 Boot Hangs at "M33 prepare ok" due to JSC DDR (JSL4BAG167ZAMF) Incompatibility Hi NXP Community, I am currently working with the FRDM-IMX93 development board and using the official Flexbuild tool (lsdk2606) to build a Debian system. However, I am encountering a boot hang issue that I suspect is related to a hardware change on the board. 1. The Issue: After flashing the built images to an SD card and booting the board, the system hangs after the following SPL logs. There is no further output: text 编辑       1U-Boot SPL 2025.04 (Oct 14 2026 - 09:56:14 +0800)2PMIC: PCA9451A 3PMIC: Over Drive Voltage Mode 4DDR: 3733MTS 5DDR: 3733MTS 6M33 prepare ok 2. Root Cause Analysis: I noticed that the DDR chip on my FRDM-IMX93 board is a JSC LPDDR4X (Part Number: JSL4BAG167ZAMF), which differs from the original Micron DDR specified in the schematics. By analyzing the U-Boot source code (board/freescale/imx93_frdm/spl.c and Makefile), I found that the default lpddr4x_2gb_timing.c provided by Flexbuild is likely tailored for Micron DDR. When U-Boot attempts to initialize the JSC DDR using these Micron timings at 3733MTS, the initialization fails (the ddr_init() loop runs twice without printing "found DRAM ... matched"). Consequently, the Cortex-M33 core hangs when it tries to access the uninitialized/unstable DDR memory. 3. Questions: Does NXP provide an updated U-Boot BSP or specific LPDDR4X timing files (lpddr4x_2gb_timing.c) officially validated for the JSC DDR (JSL4BAG167ZAMF) on the FRDM-IMX93 board? If there is no pre-built timing file, could you provide the recommended DDR parameters (e.g., ODT, Vref, tRFC, etc.) for this specific JSC chip, or point me to the correct Config Tools template? Are there any known errata or hardware revisions for FRDM-IMX93 regarding this DDR vendor change that require specific software patches? Any guidance or official timing files would be highly appreciated. Thank you! Re: FRDM-IMX93 Boot Hangs at "M33 prepare ok" due to JSC DDR (JSL4BAG167ZAMF) Incompatibil Hi, Thank you so much for the quick and helpful response! I checked our U-Boot source tree and confirmed that the commit you referenced (4c35a6086aed) was indeed missing. After applying this update to add support for the JSC JSL4BAG167ZAMF 2CS LPDDR4X device, the issue has been fully resolved and the board is now working as expected. Re: FRDM-IMX93 Boot Hangs at "M33 prepare ok" due to JSC DDR (JSL4BAG167ZAMF) Incompatibil Could you please check whether the following update is included in your U-Boot source tree? https://github.com/nxp-imx/uboot-imx/commit/4c35a6086aedca2f6220382920242ad81ae372f6 This update adds support for the JSC JSL4BAG167ZAMF 2CS LPDDR4X device used on newer FRDM-IMX93 boards. If this update is not included in your current U-Boot version, it may be related to the issue you are seeing. Thanks.
View full article
74AHC1G04GWのVOHおよびVOL特性に関する質問 74AHC1G04GWのVOHおよびVOL特性について質問があります。 データシートによると、VOHとVOLの仕様は出力電流8mAで規定されている。 しかし、実際の出力電流が8mA未満の場合、VOHとVOLをどのように決定または推定すればよいのか分かりません。 8 mA未満の出力電流でのVOHとVOLを推定する特徴曲線、参考データ、または推奨される方法を教えていただけますか? このような低電流条件下での設計計算に推奨されるVOHおよびVOLの値があれば、ぜひ教えてください。
View full article
FRDM-IMX93 启动卡在“M33 prepare ok”处,原因是 JSC DDR (JSL4BAG167ZAMF) 不兼容。 NXP社区的各位好, 我目前正在使用 FRDM-IMX93 开发板,并使用官方的 Flexbuild 工具 (lsdk2606) 版本 Debian 系统。但是,我遇到了启动卡住的问题,我怀疑这与开发板上的硬件改动有关。 1. 问题: 将构建好的镜像文件烧录到 SD 卡并启动开发板后,系统在输出以下 SPL 日志后卡死,没有其他输出: 文字 编辑       1U-Boot SPL 2025.04 (Oct 14 2026 - 09:56:14 +0800)2PMIC: PCA9451A 3PMIC: Over Drive Voltage Mode 4DDR: 3733MTS 5DDR: 3733MTS 6M33 prepare ok 2. 根本原因分析: 我注意到我的FRDM-IMX93主板上的DDR芯片是 JSC LPDDR4X(部件号:JSL4BAG167ZAMF) ,与原理图中指定的原始 Micron DDR 不同。 通过分析 U-启动 源代码( 板/freescale/imx93_frdm/spl.c) 和 Makefile ),我发现默认 lpddr4x_2gb_timing.c Flexbuild 提供的配置很可能是针对 Micron DDR 定制的。当 U-启动 尝试使用这些 Micron 时序(3733MTS)初始化 JSC DDR 时,初始化失败( ddr_init() 循环运行两次,但均未打印“找到 动态随机存取存储器\(DRAM\) ... 匹配”信息。因此,Cortex-M33 内核在尝试访问未初始化/不稳定的 DDR 内存时会挂起。 3. 问题: NXP 是否 为 FRDM-IMX93 板上的 JSC DDR (JSL4BAG167ZAMF) 提供官方验证的更新版 U-Boot BSP 或特定的 LPDDR4X 时序文件 ( lpddr4x_2gb_timing.c)? 如果没有预先构建的时序文件,能否提供该特定 JSC 芯片的推荐 DDR 参数(例如 ODT、Vref、tRFC 等),或者指出正确的配置工具模板? FRDM-IMX93 是否有任何已知的勘误或硬件修订(与 DDR 供应商变更有关),需要特定的软件补丁? 任何指导或官方计时文件都将不胜感激。谢谢你! Re: FRDM-IMX93 Boot Hangs at "M33 prepare ok" due to JSC DDR (JSL4BAG167ZAMF) Incompatibil 您好,非常感谢您的快速回复和帮助!我检查了我们的 U-Boot 源代码树,并确认您引用的提交(4c35a6086aed)确实缺失。在应用此更新以添加对 JSC JSL4BAG167ZAMF 2CS LPDDR4X 设备的支持后,该问题已完全解决,板现在可以正常工作。 Re: FRDM-IMX93 Boot Hangs at "M33 prepare ok" due to JSC DDR (JSL4BAG167ZAMF) Incompatibil 请检查一下您的 U-Boot 源代码树中是否包含了以下更新? https://github.com/nxp-imx/uboot-imx/commit/4c35a6086aedca2f6220382920242ad81ae372f6 本次更新增加了对新型 FRDM-IMX93 板卡上使用的 JSC JSL4BAG167ZAMF 2CS LPDDR4X 设备的支持。 如果您的当前 U-Boot 版本中未包含此更新,则可能与您遇到的问题有关。 谢谢。
View full article
Question about VOH and VOL characteristics of 74AHC1G04GW I have a question regarding the VOH and VOL characteristics of the 74AHC1G04GW. According to the datasheet, the VOH and VOL specifications are provided at an output current of 8 mA. However, I am not sure how to determine or estimate the VOH and VOL when the actual output current is less than 8 mA. Could you please provide any characteristic curves, reference data, or a recommended method for estimating VOH and VOL at output currents below 8 mA? If there are recommended VOH and VOL values to use for design calculations under such low-current conditions, please let me know.
View full article
S32K3 UTESTプログラムでハードフォルトが発生する こんにちは、 JTAGやデバッグのアクセスを制限するために、S32K312に16バイトのパスワード(HSEなし)を設定して制限するテストアプリケーションを作成しようとしています。以前は2段階のアプローチをとっていました。1つのプログラムでパスワードを設定し、もう1つのプログラムでライフサイクルを進めるという方法で、これはうまく機能していたようです。 現在、両方を一つのシーケンスにまとめて最終的にメインアプリケーションに統合しようとしていますが、パスワードをプログラムしようとするとMCUがハードフォルトを発生させる問題に直面しています。 パスワードをプログラムしようとする前にパスワードは設定されておらず(全0xFF)、ハードフォールトが生成されたもののパスワードは実際にプログラムされていることを確認できます。これが以前の2段階の方法がうまくいった理由だと思います。最初の段階がハードフォールしても気づかず、単に2段階をプログラムしたはずです。 以下は私のコードスニペットです。なお、起動スクリプト内でライフサイクル構成ワードのアドレスも設定しており、これはIVTに含めるようにしています。起動スクリプトやリンカーには、他に一切変更は加えられていません。 #define MASTER_ID (0U) #define CUST_DB_PSWD_A_ADDR (0x1B000080U) #define CUST_DB_PSWD_A_SECTOR (C40_UTEST_ARRAY_0_S000) #define CUST_DB_PSWD_A_LENGTH (16U) #define LC_CONFIGURATION_WORD_ADDR (0x005A6000) #define LC_CONFIGURATION_WORD_SECTOR (C40_CODE_ARRAY_0_BLOCK_1_S211) #define LC_CONFIGURATION_WORD_LENGTH (8U) uint8_t cust_db_pswd_a[CUST_DB_PSWD_A_LENGTH] __attribute__((aligned(4))) = { 0x35, 0x2E, 0x04, 0x92, 0x65, 0x25, 0x09, 0x23, 0x35, 0x2E, 0x04, 0x92, 0x65, 0x25, 0x09, 0x23 }; uint8_t lc_configuration_word[LC_CONFIGURATION_WORD_LENGTH] __attribute__((aligned(4))) = { 0xBA, 0xBA, 0xBA, 0xBA, 0x0, 0x0, 0x0, 0x0 }; /* Minimum data length 8 bytes */ int main(void) { Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); C40_Ip_Init(&C40_Ip_InitCfg); /* PROGRAMMING ADKP */ if (C40_Ip_GetLock(CUST_DB_PSWD_A_SECTOR) == C40_IP_STATUS_SECTOR_PROTECTED) { C40_Ip_ClearLock(CUST_DB_PSWD_A_SECTOR, MASTER_ID); } C40_Ip_MainInterfaceWrite(CUST_DB_PSWD_A_ADDR, CUST_DB_PSWD_A_LENGTH, cust_db_pswd_a, MASTER_ID); /* Hardfaults here, but UTEST program is actually successful */ while (C40_Ip_MainInterfaceWriteStatus() == C40_IP_STATUS_BUSY) ; /* ADVANCING LC */ if (C40_Ip_GetLock(LC_CONFIGURATION_WORD_SECTOR) == C40_IP_STATUS_SECTOR_PROTECTED) { C40_Ip_ClearLock(LC_CONFIGURATION_WORD_SECTOR, MASTER_ID); } C40_Ip_MainInterfaceSectorErase(LC_CONFIGURATION_WORD_SECTOR, MASTER_ID); while (C40_Ip_MainInterfaceSectorEraseStatus() == C40_IP_STATUS_BUSY) ; C40_Ip_MainInterfaceWrite(LC_CONFIGURATION_WORD_ADDR, LC_CONFIGURATION_WORD_LENGTH, lc_configuration_word, MASTER_ID); while (C40_Ip_MainInterfaceWriteStatus() == C40_IP_STATUS_BUSY) ; while (true) ; return 0U; } 私の.mex設定は以下のとおりです。 私が何か間違っている点があれば、ご意見をお聞かせください。 よろしくお願いいたします。 ハリーシュS Re: S32K3 UTEST program generates hardfault ハイ アドレス 0x402EC004 の「 21.7.1.3 モジュール構成ステータス (MCRS) 」の値を確認してください。MCRS[RWE] = 1 の場合、前回の読み取り中に RWW エラーが発生したことを意味します。 それでは、「 s32k312 でフラッシュが消去されたときに C40_Ip_MainInterfaceHVJobStatus API でハードフォルトが発生する」の議論をお読みください。 よろしくお願いいたします ロビン Re: S32K3 UTEST program generates hardfault こんにちは、 @Robin_Shen さん。 ご返信ありがとうございます。ご指摘のとおり、RWWのエラーでした。 UTESTセクションは別のブロックで、フラッシュ消去やプログラム機能はフラッシュから動くと思っていましたが、どうやらそうではなかったようです。機能をRAMに移動させたことで問題が解決しました。 よろしくお願いいたします。 ハリーシュS
View full article
i.MX 8M Plus:VPU 能否播放降频至 1080p HDMI 显示器的 4K H.264 短片? 大家好,我们正在考虑使用 i.MX 8M Plus 板在 1080p HDMI 显示器上循环播放短 MP4 片段(每个 4-10 秒,H.264,3840x2160,24 fps)。这些片段来自 AI 视频生成器,例如Veo3 AI 上的 Gemini Omni Flash 模型,它可以导出高达 4K 分辨率的视频(声明:我与 Veo3 AI 合作,这是一个独立的服务,与 Google 无关)。 在进行设置之前,我想先确认一下方法。我设想的就是这样的管道: gst-launch-1.0 filesrc location=clip.mp4 ! qtdemux ! h264parse ! vpudec ! imxvideoconvert_g2d ! video/x-raw,width=1920,height=1080 ! waylandsink 问题: 8M Plus VPU 能否实时解码 24 fps 的 4K H.264 视频,还是最好在复制到板卡之前将视频片段转码为 1080p? imxvideoconvert_g2d 是将 4K 降采样到 1080p 的正确元素吗?或者是否存在无需复制即可使用 waylandsink 的方法? 循环播放视频片段列表时,有没有推荐的方法可以避免文件之间出现黑帧? 感谢您提供的任何建议。 Re: i.MX 8M Plus: can the VPU play 4K H.264 short clips downscaled to a 1080p HDMI display? 嗨@ethancaldwell 1. imx8mp vpu 可以解码 4K 视频而没有硬件限制,但只能保证 1080p 的性能,因此我们通过软件将其限制在了 1080p。如果必须使用 4K 分辨率,则需要修改源代码。所以,最好将视频片段转码为 1080p。 2. 请使用 imxvideoconvert_g2d 进行缩放。 3. 目前,`gst-用上市,不用发布` 中还没有官方的、直接的解决方案来实现多个文件之间的无缝切换。建议事先将多个文件合并成一个长视频,然后将该单个文件设置为循环播放。 B.R
View full article
关于PCA82C251T/YM,118的VOL特性的问题 我有一个关于 PCA82C251T/YM,118 的 VOL 特性的问题。 根据数据手册,最大电压 VOL 在输出电流为 10 mA 时为 1.5 V,在输出电流为 1 mA 时为 0.2 × VCC。 但是,当实际输出电流小于 1 mA 时,我不知道如何确定或估计 VOL。 请问能否提供一些特性曲线、参考数据或推荐的方法来估算输出电流低于 1 mA 时的 VOL? 如果在这种低电流条件下进行设计计算时有推荐的 VOL 值,请告诉我。 Re: Question about VOL characteristics of PCA82C251T/YM,118 嗨 yoshiki11457901 51 对于IVN产品,除随附的数据表外,我们不提供其他参数。 因此,对于电流小于 1 mA 的情况,您可以参考 I4 = 1 mA 测试条件下的 VOL 值。
View full article
S32K3 UTEST 程序产生硬故障 你好, 我正在尝试创建一个测试应用程序,通过为 S32K312 设置 16 字节密码(不使用 HSE)来限制 JTAG/调试访问。之前我采用的是两阶段方法——一个程序用于设置密码,另一个程序用于推进生命周期,这种方法似乎运行良好。 我现在正尝试将两者合并成一个序列,以便最终集成到我的主应用程序中,但我遇到了问题,当我尝试对密码进行编程时,MCU 会产生硬故障。 我可以确认,在尝试设置密码之前,没有设置密码(全程 0xFF),即使产生了硬故障,密码实际上也已经设置好了——这一定是我的前两阶段方法奏效的原因,因为即使第一阶段出现硬故障,我也不会注意到,只会简单地设置第二阶段。 以下是我的代码片段。请注意,我还在启动脚本中设置了生命周期配置字地址,以便将其包含在 IVT 中。启动脚本或链接器没有其他修改。 #define MASTER_ID (0U) #define CUST_DB_PSWD_A_ADDR (0x1B000080U) #define CUST_DB_PSWD_A_SECTOR (C40_UTEST_ARRAY_0_S000) #define CUST_DB_PSWD_A_LENGTH (16U) #define LC_CONFIGURATION_WORD_ADDR (0x005A6000) #define LC_CONFIGURATION_WORD_SECTOR (C40_CODE_ARRAY_0_BLOCK_1_S211) #define LC_CONFIGURATION_WORD_LENGTH (8U) uint8_t cust_db_pswd_a[CUST_DB_PSWD_A_LENGTH] __attribute__((aligned(4))) = { 0x35, 0x2E, 0x04, 0x92, 0x65, 0x25, 0x09, 0x23, 0x35, 0x2E, 0x04, 0x92, 0x65, 0x25, 0x09, 0x23 }; uint8_t lc_configuration_word[LC_CONFIGURATION_WORD_LENGTH] __attribute__((aligned(4))) = { 0xBA, 0xBA, 0xBA, 0xBA, 0x0, 0x0, 0x0, 0x0 }; /* Minimum data length 8 bytes */ int main(void) { Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); C40_Ip_Init(&C40_Ip_InitCfg); /* PROGRAMMING ADKP */ if (C40_Ip_GetLock(CUST_DB_PSWD_A_SECTOR) == C40_IP_STATUS_SECTOR_PROTECTED) { C40_Ip_ClearLock(CUST_DB_PSWD_A_SECTOR, MASTER_ID); } C40_Ip_MainInterfaceWrite(CUST_DB_PSWD_A_ADDR, CUST_DB_PSWD_A_LENGTH, cust_db_pswd_a, MASTER_ID); /* Hardfaults here, but UTEST program is actually successful */ while (C40_Ip_MainInterfaceWriteStatus() == C40_IP_STATUS_BUSY) ; /* ADVANCING LC */ if (C40_Ip_GetLock(LC_CONFIGURATION_WORD_SECTOR) == C40_IP_STATUS_SECTOR_PROTECTED) { C40_Ip_ClearLock(LC_CONFIGURATION_WORD_SECTOR, MASTER_ID); } C40_Ip_MainInterfaceSectorErase(LC_CONFIGURATION_WORD_SECTOR, MASTER_ID); while (C40_Ip_MainInterfaceSectorEraseStatus() == C40_IP_STATUS_BUSY) ; C40_Ip_MainInterfaceWrite(LC_CONFIGURATION_WORD_ADDR, LC_CONFIGURATION_WORD_LENGTH, lc_configuration_word, MASTER_ID); while (C40_Ip_MainInterfaceWriteStatus() == C40_IP_STATUS_BUSY) ; while (true) ; return 0U; } 我的 .mex配置如下—— 请问我哪里做错了? 此致敬礼, 哈里什·S Re: S32K3 UTEST program generates hardfault HI 请检查地址 0x402EC004 处的“ 21.7.1.3 模块配置状态 (MCRS) ”的值。如果 MCRS[RWE] = 1,则表示在之前的读取过程中发生了 RWW 错误。 然后请阅读“当 s32k312 中的 flash 被擦除时,C40_Ip_MainInterfaceHVJobStatus api 出现硬故障”中的讨论。 此致敬礼, Robin Re: S32K3 UTEST program generates hardfault 你好@Robin_Shen , 感谢您的回复——正如您所说,这确实是 RWW 错误。 我原以为 UTEST 部分是一个不同的模块,因此可以从闪存运行闪存擦除/编程功能,但显然并非如此。将函数移到内存中解决了我的问题。 此致, 哈里什·S
View full article
S32K3 UTEST program generates hardfault Hello, I am trying to create a test application to restrict JTAG/debug access by setting a 16 byte password (without HSE) for an S32K312. Previously my approach was 2 staged - I had one program to set the password, and another to advance the lifecycle, and this seemingly worked fine. I am now trying to combine both into a single sequence to integrate into my main application eventually, but I am facing issues where the MCU generates a hardfault when I try to program the password. I can confirm that before trying to program the password, there is no password set (0xFF throughout) and even though a hardfault was generated, the password has actually been programmed - this must have been why my previous 2 staged approach worked, as even if the first stage hardfaulted, I would not have noticed and simply programmed the second stage. Below is my code snippet. Do note that I have also set the lifecycle configuration word address in the startup script, to be included in the IVT. There are no other modifications to the startup script or linker. #define MASTER_ID (0U) #define CUST_DB_PSWD_A_ADDR (0x1B000080U) #define CUST_DB_PSWD_A_SECTOR (C40_UTEST_ARRAY_0_S000) #define CUST_DB_PSWD_A_LENGTH (16U) #define LC_CONFIGURATION_WORD_ADDR (0x005A6000) #define LC_CONFIGURATION_WORD_SECTOR (C40_CODE_ARRAY_0_BLOCK_1_S211) #define LC_CONFIGURATION_WORD_LENGTH (8U) uint8_t cust_db_pswd_a[CUST_DB_PSWD_A_LENGTH] __attribute__((aligned(4))) = { 0x35, 0x2E, 0x04, 0x92, 0x65, 0x25, 0x09, 0x23, 0x35, 0x2E, 0x04, 0x92, 0x65, 0x25, 0x09, 0x23 }; uint8_t lc_configuration_word[LC_CONFIGURATION_WORD_LENGTH] __attribute__((aligned(4))) = { 0xBA, 0xBA, 0xBA, 0xBA, 0x0, 0x0, 0x0, 0x0 }; /* Minimum data length 8 bytes */ int main(void) { Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); C40_Ip_Init(&C40_Ip_InitCfg); /* PROGRAMMING ADKP */ if (C40_Ip_GetLock(CUST_DB_PSWD_A_SECTOR) == C40_IP_STATUS_SECTOR_PROTECTED) { C40_Ip_ClearLock(CUST_DB_PSWD_A_SECTOR, MASTER_ID); } C40_Ip_MainInterfaceWrite(CUST_DB_PSWD_A_ADDR, CUST_DB_PSWD_A_LENGTH, cust_db_pswd_a, MASTER_ID); /* Hardfaults here, but UTEST program is actually successful */ while (C40_Ip_MainInterfaceWriteStatus() == C40_IP_STATUS_BUSY) ; /* ADVANCING LC */ if (C40_Ip_GetLock(LC_CONFIGURATION_WORD_SECTOR) == C40_IP_STATUS_SECTOR_PROTECTED) { C40_Ip_ClearLock(LC_CONFIGURATION_WORD_SECTOR, MASTER_ID); } C40_Ip_MainInterfaceSectorErase(LC_CONFIGURATION_WORD_SECTOR, MASTER_ID); while (C40_Ip_MainInterfaceSectorEraseStatus() == C40_IP_STATUS_BUSY) ; C40_Ip_MainInterfaceWrite(LC_CONFIGURATION_WORD_ADDR, LC_CONFIGURATION_WORD_LENGTH, lc_configuration_word, MASTER_ID); while (C40_Ip_MainInterfaceWriteStatus() == C40_IP_STATUS_BUSY) ; while (true) ; return 0U; }   my .mex configuration is as such -  Any inputs as to what I am doing wrong? With regards, Hareesh S Re: S32K3 UTEST program generates hardfault Hi Please check the value of "21.7.1.3 Module Configuration Status (MCRS)" at address 0x402EC004.  If MCRS[RWE] = 1, it means that an RWW error occurred during a previous read. Then please read the discussion in  "Hard Fault in C40_Ip_MainInterfaceHVJobStatus api when flash is erase in s32k312". Best Regards, Robin Re: S32K3 UTEST program generates hardfault Hello @Robin_Shen, Thanks for reverting back - It was indeed a RWW error as you had suggested. I assumed the UTEST section was a different block and hence flash erase/program functions could run from flash but apparently not. Moving the functions to RAM solved my issues. With regards, Hareesh S
View full article
i.MX 8M Plus: can the VPU play 4K H.264 short clips downscaled to a 1080p HDMI display? Hi all, we are looking at using an i.MX 8M Plus board to loop short MP4 clips (4–10 seconds each, H.264, 3840x2160 at 24 fps) on a 1080p HDMI display. The clips come from an AI video generator, e.g. the Gemini Omni Flash model on Veo3 AI, which exports up to 4K (disclosure: I work with Veo3 AI, an independent service, not affiliated with Google). Before setting this up I would like to check the approach. A pipeline like this is what I had in mind: gst-launch-1.0 filesrc location=clip.mp4 ! qtdemux ! h264parse ! vpudec ! imxvideoconvert_g2d ! video/x-raw,width=1920,height=1080 ! waylandsink Questions: Can the 8M Plus VPU decode 4K H.264 at 24 fps in real time, or is it better to transcode the clips to 1080p before copying them to the board? Is imxvideoconvert_g2d the right element for the 4K to 1080p downscale, or is there a zero-copy path into waylandsink? For looping a playlist of clips, is there a recommended way to avoid a black frame between files? Thanks for any pointers. Re: i.MX 8M Plus: can the VPU play 4K H.264 short clips downscaled to a 1080p HDMI display? Hi @ethancaldwell  1. imx8mp vpu can decoding 4K video without HW limitation, but only guarantee 1080p performance, and we did SW limitation to 1080p. If you must use 4K, you need to change the source code. So, it's better to transcode the clips to 1080p. 2. please use imxvideoconvert_g2d for scaling. 3. Currently, there is no official, direct solution for seamless switching between multiple files in `gst-launch`. It is recommended to mux multiple files into a single long video beforehand, and then set that single file to play on a loop. B.R
View full article
i.MX 适用于安卓车载主机 – 兼容性,电路板支持包。 产品型号:i.MX 8M Plus / i.MX 95 / i.MX 8QuadXPlus / i.MX 8QuadMax 你好, 我们正在评估 NXP i.MX 应用处理器(i.MX 8M Plus、i.MX 95、i.MX 8QuadXPlus / 8QuadMax),以用于基于 Android 的售后汽车主机。我们想了解哪个部件最符合我们的需求,以及价格和支持条款。如果以上产品均不合适,请从恩智浦的产品组合中推荐其他适合我们开发的替代部件。 产品要求 平台 - Android (AOSP) 13 或更高版本,并包含电路板支持包。源代码(引导加载程序、内核、HAL) - 4 GB DDR4/LPDDR4、64 GB eMMC - 八核处理器(或同等性能的处理器) 优先考虑工业级(-40 至 85 °C)或汽车级(AEC-Q100)温度等级。 展示 - 9英寸1280×800面板,首选LVDS接口(MIPI DSI接口亦可) - 通过 I2C 实现电容式触摸 - 显示颜色调整(对比度、饱和度、色温) 相机和视频 - 通过外部4通道解码器,使用MIPI CSI-2(虚拟通道)连接4个AHD 720p/1080p摄像头,实现360°环绕视角。 - 通过 CVBS 解码器支持 CVBS 倒车摄像头、前置/右摄像头和 AV-IN 视频输入 - 支持 H.264/H.265 1080p 解码;支持多流 H.264 编码,用于前后摄像头录制(例如 4 × 720p) - 具备用于 2D/3D 360° 拼接的 GPU 功能 声音的 - 支持 I2S/TDM(至少一个 8 通道 TDM 端口,共 3 个端口),用于多通道编解码器、FM/AM 调谐器和蓝牙语音 - S/PDIF 输出 - 音频处理,包括 8 段均衡器、跨界、低音炮滤波器和回声消除(请问 HiFi4 DSP 及其软件框架是否可以在 Android 系统下用于此功能) 连接和 I/O - 3 个 USB 2.0 接口(其中一个支持 OTG 功能),用于手机投屏、媒体播放和配件连接。 - 用于 Wi-Fi/蓝牙模块(2.4/5 GHz,蓝牙 5.0 双连接)的 SDIO - 5 个 UART 接口(车载接口盒、附件、蓝牙 HCI、GNSS、调试) - 3 个 I2C 接口、1 个 SPI 接口、2 个以上的 SAR-ADC 通道、3 个 PWM 接口、约 20 个 GPIO 接口 - 可选的:4G LTE(集成或通过 USB/PCIe 模块) 应用功能(请注明您的平台上任何可用或可授权的软件) - 支持 Apple CarPlay 和 Android Auto(有线/无线),手机镜像 - 360°环绕视图(AVM)库 - 音频DSP/音效包 请求提供的信息 1. 以上各部件是否符合我们的要求,以及您推荐的部件 2. 数据手册、硬件设计指南、参考原理图和推荐的电源管理集成电路/存储器 3. Android 电路板支持包。:可用版本(AOSP 和 Android Automotive)、内核版本、路线图、源代码可用性以及提供方式(公开下载、保密协议、许可协议) 4. 任何 SDK 许可费或单位版税(包括 HiFi4 DSP 软件) 5. 评估套件/SOM的可用性、价格和交货时间 6. SoC(或SOM)年产量分别为1万、5万和10万颗时的单价,另加最小起订量和交货周期。 7. 产品寿命/供应承诺 8. 技术支持模式,以及在印度的设计合作伙伴或代理商 谢谢! 此致, 诗条门·托马斯 Re: i.MX for Android car head unit – suitability, BSP 你好, 根据所述要求,我会将i.MX 95和i.MX 8QuadMax列入候选名单。最佳选择主要取决于相机/视频性能还是 HiFi4/音频和汽车软件成熟度哪个才是首要考虑因素。 i.MX95 i.MX 95 是相机和视频工作负载的最佳选择。它提供: 最多六个 Cortex-A55 应用核心 4K H.264/H.265 视频编码和解码 ISP 支持通过 MIPI 虚拟通道连接多个 1080p 流和最多八个摄像头。 支持两个四通道 MIPI-CSI 接口、LVDS 显示和 MIPI-DSI 显示。 多种 UART 和 I2C 接口、ADC 输入、15 通道 I2S/TDM 以及 S/PDIF 接口 汽车和扩展工业温度选项 这使其非常适合四通道 AHD 解码器、CVBS 解码器输入、环绕视图处理和多流录制,前提是所选解码器通过支持的 CSI-2/V4L2 或 Android 摄像头接口公开其流。 选择前需要核实的几点: 确切的 AHD/CVBS 解码器及其 Android 摄像头或 EVS 驱动程序支持 摄像机配置是否在可用车道带宽内使用 CSI 虚拟通道 如果显示器选择 MIPI-DSI,则 MIPI-CSI/DSI 多路复用会比较复杂;LVDS 可能会释放更多 CSI 资源。 由于处理器文档中列出了两个定时器/PWM模块,因此需要三个PWM输出。 HiFi4 DSP 可用性。i.MX 95 的文档中没有列出 HiFi4 DSP,因此音频算法可能需要在应用程序核心或实时核心上运行,或者在外部音频 DSP 上运行。 产品信息: i.MX 95 i.MX8QM 如果汽车认证、HiFi4 音频处理、外围设备覆盖范围和 Android Automotive 功能是主要优先事项,那么 i.MX 8QuadMax 是更好的选择。它提供: 两个 Cortex-A72 应用核心和四个 Cortex-A53 应用核心,外加两个 Cortex-M4F 核心 符合汽车行业 AEC-Q100 标准的订购选项 硬件视频、图形和摄像头处理,支持多摄像头输入 HiFi4 DSP、多个 SAI/ESAI 接口以及用于多声道音频设计的 S/PDIF 接口 具备满足所述车辆接口要求的充足 UART、I2C、SPI、PWM 和 ADC 资源 NXP Android Automotive 在 i.MX 8QuadMax 换成产品名,如“i.mx8-mek是……” 上的支持 主要的缺点是它的架构比 i.MX 95 更老,因此应该使用完整的四摄像头、CVBS、环视和录制工作负载来衡量可用的视频处理和 CPU 裕量。还必须检查确切的摄像头解码器、同时流数和 Android 摄像头集成情况。 产品信息: i.MX 8 应用处理器 i.MX8MPlus i.MX 8M Plus 对工业多媒体设计很有吸引力,因为它包括 HiFi4、LVDS/MIPI-DSI、两个 MIPI-CSI 接口以及 1080p 级 H.264/H.265 视频支持。但是,它有四个 Cortex-A53 内核,是工业级而非汽车级认证,并且只有两个 CSI 摄像头接口。因此,与 i.MX 95 或 i.MX 8QuadMax 相比,它不太适合满足完整的多摄像头车载单元需求。 产品信息: i.MX 8M Plus i.MX8QXP i.MX 8QuadXPlus 提供四个 Cortex-A35 内核和一个 Cortex-M4F 内核,以及多媒体、显示、摄像头和 HiFi4 功能。但是,它的 CPU 性能低于要求的级别。与 i.MX 8QuadMax 和 i.MX 95 相比,它也不是目前首选的 Android Automotive 平台。 Android 电路板支持包。 NXP 的公开 Android 电路板支持包。页面目前列出了对 i.MX 8M Plus、i.MX 8QuadMax/8QuadXPlus 和 i.MX 95 评估平台的 Android 16 支持。构建源代码包和文档通过 NXP 软件门户提供。应确认所选版本的确切源代码和二进制文件覆盖范围、许可条款以及生产再分发权。 目前公开的 Android Automotive 资料主要集中在 i.MX 8QuadMax 和 i.MX 95 平台上。Android Automotive 支持与 Android Auto 手机投影应加以区分。 适用于 i.MX 应用处理器的 Android 电路板支持包 适用于 i.MX 应用处理器的 Android Automotive 电路板支持包。 Apple CarPlay、Android Auto 手机投影、无线连接、AVM/环视库、音频效果包和 HiFi4 软件框架可能需要单独的认证、合作伙伴软件、专业服务或商业许可。不应仅仅因为 SoC 支持所需的硬件接口就假定它们会被包含在内。 总之,选拔路径如下: 如果 HiFi4、汽车认证、音频 I/O、PWM 资源和已建立的 Android Automotive 路径是主要决策因素,请选择 i.MX 8QuadMax。 如果摄像机/视频性能、未来处理裕量和虚拟通道摄像机支持更为重要,并且可以接受外部音频 DSP 或软件音频实现,则选择 i.MX 95。 只有在降低摄像头数量、性能和汽车要求的情况下,才将 i.MX 8M Plus 和 i.MX 8QuadXPlus 作为备选方案。 此致敬礼/Saludos, 阿尔多。
View full article
S32K3をリセットすると、fs26もリセットされますか? S32K3とFS26を使用している場合、電源投入時にFS26とS32K3の初期化が正常に完了し、FS26は通常モードに入ります。この状態でソフトウェアを使用してソフトリセットを実行した場合、ソフトリセット完了後、初期化プロセス中にFS26を再度初期化する必要はありますか? ご指導をお願いいたします。ありがとうございます。 Re: S32K3复位,会让fs26复位吗? はい、どうもありがとうございました! Re: S32K3复位,会让fs26复位吗? 基本的には以上です。 Re: S32K3复位,会让fs26复位吗? S32K3の初期化処理中は、S32K3によってプルダウンされます。初期化が完了するとプルダウンは解除されます。つまり、必ず初期化状態になります。 Re: S32K3复位,会让fs26复位吗? FS26のRSTBが外部からの力によって強制的にローレベルに引き下げられた場合、INIT状態に入ります。また、8秒以上ローレベルに引き下げられた場合、ディープFSモードに入ります。 Re: S32K3复位,会让fs26复位吗? 通常モードに入った後は、FS26レジスタは変更しません。ソフトリセット処理中は、S32K3のRSTBが変化します。このピンはFS26にも接続されており、FS26はこのピンの変化に基づいて関連する動作を実行します。 Re: S32K3复位,会让fs26复位吗? こんにちは、 zuozuo S32Kのみがリセットされ、FS26レジスタの値が変更されず、FS26が正常な状態のままであれば、FS26を初期化する必要はありません。
View full article
PN7220 Currently, we are observing failures in certain NFC XTS test cases on the supported PN7XX chips. Could you please clarify if Google plans to remove the relevant Type B and Type F Card Emulation test items from future XTS test suites? Also, has NXP confirmed this specific aspect with Google? Re: PN7220 Hello @Max4  For the PN7220, you can apply to NXP for a waiver statement and submit it to Google for testing. Best Rgeards, kelly
View full article
MCU (S32k312) to MC33664 (Network Isolator) to MC33771C(AFE) Comms No Response Diagnostics: Hello Everyone, Currently I am working on a BMS design.  The Main components/design highlights are: 1. MCU: S32k312 2. Network Isolator: MC33664 3. AFE: MC33771 4. Communication mode: TPL Isolation is as shown below: Also,  MCU to MC33664 Comms from Dual SPI.  MC33664 to MC33771C is TPL.  SPI Configuration is set as follows:     1. Wakeup Sequence:    Wake up sequence is pulling the VCOM high keeping it stable at 5V.  2. First Command  First command is a Software Reset command through Global Write with CID set to 0x00.    This is followed by Second Command after a 500 mS delay.  3. Second Command  Second command is a read command to read the Init (0x01) Register to verify the comms.    Second command is failing because it is expected to read 2 frames of 6 Bytes i.e. the echo and the read response but only echo is generated but not the read response.  4. Read Command and Read Response on the TPL Line:    The first pulse train shown in this image is the echo of the read command sent which is properly translated to SPI by MC33664. The second pulse train the actual response from the AFE on the TPL which the MC33664 is failing to translate to the SPI. The visual difference here is that the voltage levels of the echo and read response are different on the TPL which is a suspect to investigate.  Additional Diagnostic Signal Captures:  RDTX+ and RDTX- before the isolator.    2. RDTX+ and RDTX- after the isolator.      Conclusion:  The TPL comms are accepted by the AFE and is producing the responses but the MC33664 is not translating the responses back to SPI RX line which is causing communication timeout failure.  Please help !! Thank you in advance. Re: MCU (S32k312) to MC33664 (Network Isolator) to MC33771C(AFE) Comms No Response Diagnostics: Hello, Please verify that the wake-up is generated through the MC33664 CSB_TX timing after enabling the MC33664, rather than by forcing VCOM high. Since the AFE response appears on the TPL line, please focus next on the MC33664 receive path and check CSB_RX, SCLK_RX, DATA_RX, SPI mode, 48-bit frame timing, and the signal at both the MC33664 SPI RX pins and the S32K312 pins.  Please note that we do not have a ready made, tested software and evaluation-board combination for the exact S32K312 + MC33664 + MC33771C configuration, so the SPI driver and dual-SPI receive implementation require application specific validation.
View full article
PN7220 現在、サポートされているPN7XXチップの特定のNFC XTSテストケースで故障が確認されています。今後のXTSテストスイートから、関連するType BおよびType Fカードエミュレーションテスト項目を削除する予定があるのか、ご確認いただけますか?また、NXPはこの点についてGoogleと確認済みでしょうか? Re: PN7220 こんにちは、 @Max4さん PN7220については、NXPに免除申請書を申請し、Googleに提出してテストを受けることができます。 よろしくお願いいたします。 ケリー
View full article
Androidカーヘッドユニット i.MX – 適合性、BSP 部品番号:i.MX 8M Plus / i.MX 95 / i.MX 8QuadXPlus / i.MX 8QuadMax こんにちは、 私たちは、Androidベースのアフターマーケットカーヘッドユニット用に、NXP i.MX アプリケーションプロセッサ(i.MX 8M Plus、i.MX 95、i.MX 8QuadXPlus / 8QuadMax)を評価しています。どの部品が最も私たちの要件に合っているのか、価格やサポート条件についても知りたいと思っています。これらのいずれも適切でない場合は、NXPの製品ポートフォリオの中から、弊社の開発に適した代替部品をご提案ください。 製品要件 プラットフォーム - Android (AOSP) 13以降、BSPソース(ブートローダー、カーネル、HALs)を使用 - 4GB DDR4/LPDDR4、64GB eMMC - オクタコアクラスCPU(または同等の性能) - インダストリアル(-40〜85°C)またはオートモーティブ(AEC-Q100)温度グレードが推奨されます 画面 - 9インチ、1280×800ピクセルのパネル、LVDS推奨(MIPI DSIも可) - I2C経由の静電容量式タッチ - ディスプレイの色調整(コントラスト、彩度、色温度) カメラとビデオ - 4台× AHD 720p/1080pカメラを、MIPI CSI-2(仮想チャネル)で外部4チャネルデコーダー経由で360°サラウンドビューを使用。 - CVBSバックカメラ、前後カメラ、CVBSデコーダーによるAV-INビデオ - H.264/H.265 1080pデコード;前後録画用のマルチストリームH.264エンコード(例:4×720p) - 2D/3Dの360°ステッチング対応GPU機能 オーディオ - I2S/TDM(少なくとも1つの8チャネルTDMポート、合計3ポート)はマルチチャネルコーデック、FM/AMチューナー、Bluetooth音声用 - S/PDIF出力 - 8バンドEQ、クロスオーバー、サブウーファーフィルター、エコーキャンセリングのオーディオプロセッシング(Android上でHiFi4 DSPおよびそのソフトウェアフレームワークが使用可能かご確認ください) コネクティビティとI/O - 3 × USB 2.0(1つのOTG)で電話プロジェクション、プレスリリース、製品ニュース、アクセサリ用 - Wi-Fi/Bluetoothモジュール用のSDIO(2.4/5 GHz、BT 5.0デュアル接続) - 5 × UART(車載インターフェースボックス、アクセサリ、BT HCI、GNSS、DEBUG) - 3 × I2C、1 × SPI、2+ SAR-ADCチャネル、3× PWM、~20 GPIO - オプション:4G LTE(統合型またはUSB/PCIeモジュール経由) アプリケーションの機能(プラットフォーム上で利用可能なまたはライセンス可能なソフトウェアを記載してください) - Apple CarPlayおよびAndroid 車載(有線/無線)、電話ミラーリング - 360°サラウンドビュー(AVM)ライブラリ - オーディオDSP/効果音パッケージ 情報提供 1. 上記の各部品が当社の要件および推奨する部分に適合していること 2. データシート、ハードウェアデザインガイド、参照回路図および推奨PMIC/メモリ 3. Android BSP:利用可能なバージョン(AOSPおよびAndroid オートモーティブ)、カーネルバージョン、ロードマップ、ソースの入手可能性、および提供方法(公開ダウンロード、NDA、ライセンス契約) 4. SDKsのライセンス料やユニットごとのロイヤリティ(HiFi4 DSPソフトウェアを含む) 5. 評価キット/SOMの入手可能性、価格およびリードタイム 6. SoC(またはSOM)のユニット価格(年間10K、50K、100Kユニット)、さらにMOQおよびリードタイム 7. 製品の耐久性/供給コミットメント 8. 技術サポートモデルおよびインドにおけるデザインパートナーまたは代理店 よろしくお願いします。 よろしくお願いします、 四条門トーマス Re: i.MX for Android car head unit – suitability, BSP こんにちは、 記載された要件に基づくと、 i.MX 95とi.MX 8QuadMaxを候補として挙げます。最適な選択は主にカメラ/映像性能かHiFi4/オーディオ・自動車ソフトウェアの成熟度のどちらが優先度が高いかによります。 i.MX95 i.MX 95は、カメラおよびビデオ撮影のワークロードにおいて最も有力な候補である。提供するもの: 最大6つのCortex-A55アプリケーションコア 4K H.264/H.265ビデオのエンコードとデコード 複数の1080pストリームと最大8台のカメラをMIPI仮想チャネル経由でサポートするISP 2つの4レーンMIPI-CSIインターフェース、LVDSディスプレイサポート、MIPI-DSIディスプレイサポート 複数のUARTおよびI2Cインターフェース、ADC入力、15レーンI2S/TDM、S/PDIF オートモーティブおよび拡張インダストリアル用の温度オプション これにより、選択されたデコーダーが対応するCSI-2/V4L2またはAndroidカメラインターフェースを通じてストリームを露出すれば、4チャネルAHDデコーダー、CVBSデコーダー入力、サラウンドビュープロセッシング、マルチストリーム録画に適しています。 選択する前に確認すべき点: 正確なAHD/CVBSデコーダーとAndroidカメラまたはEVSドライバのサポート カメラ構成が利用可能なレーン帯域幅内でCSI仮想チャネルを使用しているかどうか MIPI-DSIがディスプレイに選択された場合、MIPI-CSI/DSI多重化が行われます。LVDSを使用すると、より多くのCSIリソースが利用可能になる可能性があります。 プロセッサのドキュメントには2つのタイマー/PWMブロックが記載されているため、3つのPWM出力の要件があります HiFi4 DSPの利用可能性。i.MX 95のドキュメントにはHiFi4 DSPが記載されていないため、オーディオアルゴリズムはアプリケーションコアやリアルタイムコア、または外部オーディオDSP上で動作する必要がある場合があります 製品情報: i.MX 95 i.MX8QM i.MX 8QuadMaxは、自動車認証、HiFi4オーディオプロセッシング、ペリフェラルカバレッジ、Android オートモーティブのイネーブルメントが主な優先事項である場合により適しています。提供するもの: Cortex-A72 2基とCortex-A53アプリケーションコア4基、さらにCortex-M4Fコア 2基 オートモーティブAEC-Q100対応ご注文オプション ハードウェアビデオ、グラフィックス、カメラプロセッシング、複数のカメラ入力に対応しています HiFi4 DSP、複数のSAI/ESAIインターフェース、そしてマルチチャネルオーディオデザイン用のS/PDIF対応 車載インターフェース要件を満たすために十分なUART、I2C、SPI、PWM、ADCリソース NXP Android オートモーティブの i.MX 8QuadMax MEKサポート 主なトレードオフは、i.MX 95よりも古いアーキテクチャであるため、利用可能なビデオプロセッシングやCPUの余裕は、4カメラ、CVBS、サラウンドビュー、録画の全負荷と合わせて測定されるべきだということです。カメラのデコーダー、同時配信数、Androidカメラとの連携も確認する必要があります。 製品情報: i.MX 8アプリケーションプロセッサ i.MX8MPlus i.MX 8M Plusは、HiFi4、LVDS/MIPI-DSI、2つのMIPI-CSIインターフェース、1080pクラスのH.264/H.265ビデオサポートを含むため、インダストリアルマルチメディアデザインに魅力的です。しかし、4つのCortex-A53コアを搭載しており、オートモーティブではなく、インダストリアルの認証で、CSIカメラインターフェースは2つだけです。したがって、i.MX 95やi.MX 8QuadMaxに比べて、完全なマルチカメラヘッドユニットの要件には適していません。 製品情報: i.MX 8M Plus i.MX8QXP i.MX 8QuadXPlusは、4つのCortex-A35コアと1つのCortex-M4Fコアを備え、マルチメディア、ディスプレイ、カメラ、HiFi4機能を備えています。しかし、そのCPU性能は要求されたクラスを下回っている。また、i.MX 8QuadMaxや i.MX 95と比べて現在のAndroid Automotiveプラットフォームとしては推奨されていません。 Android BSP NXPの公開Android BSPページでは、現在 i.MX 8M Plus、i.MX 8QuadMax/8QuadXPlus、i.MX 95の評価プラットフォームに対するAndroid 16サポートが掲載されています。ビルドソースパッケージやドキュメントはNXPソフトウェアポータルを通じて提供されています。選択したリリースについて、正確なソースコードとバイナリの提供範囲、ライセンス条項、および製品版の再配布権を確認する必要があります。 現在公開されているAndroid オートモーティブの資料は、i.MX 8QuadMaxおよび i.MX 95プラットフォームに焦点を当てています。Android オートモーティブのサポートは、Android 車載の電話プロジェクションとは区別されるべきです。 i.MX アプリケーションプロセッサ向けAndroid BSP Android オートモーティブ BSP for i.MXアプリケーション・プロセッサ Apple CarPlay、Android 車載の電話プロジェクション、ワイヤレス・コネクティビティ、AVM/サラウンドビューライブラリ、オーディオエフェクトパッケージ、HiFi4ソフトウェアフレームワークは、別途認証、パートナーソフトウェア、プロフェッショナルサービス、または商用ライセンスを必要とする場合があります。SoCが必要なハードウェアインターフェースをサポートしているからといって、それらが含まれていると考えるべきではありません。 要約すると、選考プロセスは以下のようになります。 HiFi4、自動車資格、オーディオI/O、PWMリソース、確立されたAndroid オートモーティブの経路が主な判断要素であれば、8QuadMax i.MX 選択してください。 カメラ/映像性能、FUTUREのプロセッシング余裕、仮想チャネルカメラのサポートがより重要で、外部オーディオDSPやソフトウェアオーディオ実装が許容される場合は i.MX 95を選択してください。 カメラ数、性能、オートモーティブ要件が減った場合 i.MX、8M Plusと i.MX 8QuadXPlusは副次オプションとして残しておくのが良いでしょう。 よろしくお願いいたします。 アルド。
View full article
PN7220 目前,我们发现支持的 PN7XX 芯片在某些 NFC XTS 测试用例中出现故障。请问谷歌是否计划从未来的 XTS 测试套件中移除相关的 B 型和 F 型卡模拟测试项?另外,NXP是否已向谷歌确认过这一具体方面? Re: PN7220 你好@Max4 对于 PN7220,您可以向 NXP 申请豁免声明,并将其提交给 Google 进行测试。 此致敬礼, 凯莉
View full article
MCU (S32k312) 至 MC33664 (网络隔离器) 至 MC33771C (AFE) 通信无响应诊断: 大家好, 目前我正在进行电池管理系统(BMS)的设计工作。 主要元器件/设计亮点如下: 1. MCU:S32k312 2. 网络隔离器:MC33664 3. AFE:MC33771 4. 通信方式:TPL 隔离情况如下所示: 还, MCU 与 MC33664 通过双 SPI 进行通信。 MC33664 至 MC33771C 是 TPL。 SPI配置设置如下:    1.唤醒序列:    唤醒序列将 VCOM 拉高,使其稳定在 5V。  2. 第一条命令  第一个命令是通过全局写入执行的软件 RESET 命令,CID 设置为 0x00。    随后,在延迟 500 毫秒后发出第二个命令。  3. 第二条命令  第二条命令是读取 Init (0x01) 寄存器的READ命令,用于验证通信。    第二个命令失败,因为它应该读取 2 个 6 字节的帧,即回显和读取响应,但只生成了回显,没有生成读取响应。  4. 在 TPL 线上READ命令和读取响应:    图中显示的第一组脉冲是发送的READ命令的回波,MC33664 已将其正确翻译为 SPI 信号。第二组脉冲是 TPL 上 AFE 的实际响应,MC33664 未能将其翻译为 SPI 信号。此处的视觉差异在于 TPL 上回波和读取响应的电压等级不同,这可能是需要调查的原因。  其他诊断信号捕获:  隔离器之前的 RDTX+ 和 RDTX-。    2. 隔离器后的 RDTX+ 和 RDTX-。      结论:  AFE 接受 TPL 通信并产生响应,但 MC33664 没有将响应已翻译回 SPI RX 线,导致通信超时失败。  请帮帮我!! 先感谢您。 Re: MCU (S32k312) to MC33664 (Network Isolator) to MC33771C(AFE) Comms No Response Diagnostics: 你好, 请验证在启用 MC33664 后,是否通过 MC33664 CSB_TX 时序产生唤醒,而不是通过强制 VCOM 为高电平产生唤醒。 由于AFE响应出现在TPL线上,接下来请重点检查MC33664接收路径,并检查CSB_RX、SCLK_RX、DATA_RX、SPI模式、48位帧时序,以及MC33664 SPI RX引脚和S32K312引脚上的信号。 请注意,我们没有针对 S32K312 + MC33664 + MC33771C 配置的现成、经过测试的软件和评估板组合,因此 SPI 驱动程序和双 SPI 接收实现需要针对特定应用进行验证。
View full article
Will resetting the S32K3 cause the fs26 to reset? Now, using S32K3 and FS26, during power-on, the initialization of FS26 and S32K3 is completed normally, and FS26 enters normal mode. If I use software to perform a soft reset at this time, after the soft reset is completed, is it necessary to initialize FS26 again during the initialization process? Requesting guidance, thank you. Re: S32K3复位,会让fs26复位吗? Okay, thank you very much! Re: S32K3复位,会让fs26复位吗? That's basically it. Re: S32K3复位,会让fs26复位吗? During the initialization process of S32K3, it will be pulled low by S32K3. It will be released after the initialization is completed. In other words, it will definitely be brought to the init state. Re: S32K3复位,会让fs26复位吗? If the RSTB of FS26 is forcibly pulled low by an external force, it will enter the INIT state; or if it is pulled low for more than 8 seconds, it will enter Deep FS mode. Re: S32K3复位,会让fs26复位吗? After entering normal mode, I will not modify the FS26 register. During the soft reset process, the RSTB of the S32K3 will change. This pin is also connected to the FS26, and the FS26 will perform related actions based on the change of this pin. Re: S32K3复位,会让fs26复位吗? Hi zuozuo If only the S32K is reset without changing the FS26 register value, and FS26 is still in normal state, then there is no need to initialize FS26.
View full article