Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
NXP i.MX93 EVKのNPU温度と使用率を取得する方法 私はi.MX93 EVKを使っており、Ethos-UのNPU温度と稼働率(負荷)を実行時に監視したいのですが、このデータをどうやって取得できますか? 目的は、AIモデルの推論中にハードウェアパラメータを監視することです。 i.MX8MPlusで以下のパラメータを監視できます。i.MX93でも同様のことを実現したいです。 8Mプラス RAM=$(free -m | awk '/Mem:/ {print $3}') CPU_LOAD=$(vmstat 1 2 | tail -1 | awk '{print 100 - $15}') CPU_TEMP=$(awk '{print $1/1000}' /sys/class/thermal/thermal_zone0/temp 2>/dev/null || echo "N/A") GPU_TEMP=$(awk '{print $1/1000}' /sys/class/thermal/thermal_zone1/temp 2>/dev/null || echo "${CPU_TEMP}") GPU_LOAD=$(cat /sys/kernel/debug/gc/load 2>/dev/null | awk '/load/ {gsub("%","",$3); if (max=="" || $3>max) max=$3} END {if (max!="") print max "%"; else print "N/A"}') i.MX93 RAM=$(free -m | awk '/Mem:/ {print $3}') CPU_LOAD=$(vmstat 1 2 | tail -1 | awk '{print 100 - $15}') CPU_TEMP=$(awk '{print $1/1000}' /sys/class/thermal/thermal_zone0/temp) i.MX93 NPU(ethos-u)のGPU_LOADとGPU_TEMPをどうやって監視できますか? Linux Re: How to get NPU Temperature and utilization for NXP i.MX93 EVK こんにちは、@sonal-acldigital i.MX 8M Plusも i.MX 93も、NPU温度をリアルタイムで監視する方法を提供していません。 - imx8MP、thermal_zone0はCPUの温度を表し、thermal_zone1はSoCの温度を表します。 - imx93、thermal_zone0はCPUの温度を表します。 - NPU、 nputopのようなツールは存在しません。 パフォーマンスチューニングに関する情報については、セクション7.1.2を参照してください。「ハードウェアアクセラレータのプロファイリング」、 MLユーザーガイドに収録。 B.R Re: How to get NPU Temperature and utilization for NXP i.MX93 EVK @pengyong_zhang i.MX 8M Plusとi.MX 93の熱ゾーンについてご説明いただきありがとうございます。以下の点を明確にしていただけますか? i.MX8MPLUS 1. GPU温度: 個別のGPU温度を読み取る専用のシステムパス(/sys/class/thermal/thermal/thermal_zoneX/temp)はありますか?それともソックサーマルゾーン(thermal_zone1)だけでカバーされているのでしょうか? 2. GPU負荷: /sys/kernel/debug/gc/loadを読み込むことがGPU負荷の確認の標準的な方法ですか?それともMLユーザーガイドのセクション7.1.2に詳述されている手順も必要ですか? i.MX93: NPUの負荷と温度を監視するネイティブツール(nputopなど)がないため、次の点について質問させてください。推論の実行をNPUにオフロードした場合とCPUのみで実行した場合のCPU負荷の減少を測定することで、相対的なNPU使用率を導き出すことは妥当でしょうか? もしこの方法が推奨されていない場合、推論実行中のNPU活動を推定するために使える代替のドライバーノードやパフォーマンスカウンターはありますか? Re: How to get NPU Temperature and utilization for NXP i.MX93 EVK こんにちは、@sonal-acldigital 返信が遅くなり申し訳ありません。最近、ひどいウイルス性の風邪にかかり、しばらくの間高熱が続きました。今日やっと熱が下がった。 1.GPU温度を読み取る専用の経路はありません。 2. はい、/sys/kernel/debug/gc/loadによるGPU負荷監視が現在の方法です。 IMX93: NPU使用率は、プロファイリングを用いてご自身で計算する必要があります。 B.R
View full article
KW45: Intermittent Wire ACK Fault During Programming/Debugging and Flash Erase Failure Hi Team, I am currently working with a KW45-based custom board and facing an intermittent issue during programming and debugging the firmware. I have tested the board with both a SEGGER J-Link and an NXP MCU-Link debug probe, and the issue occurs with both probes. The custom board has the same boot configuration as the KW45 EVK, and the JTAG/SWD connections have also been checked and appear to be correct. However, I am seeing the following behaviour: When I try to dump or program a known-working application: Sometimes the application is programmed successfully, but after programming or starting a debug session, the device eventually jumps to a fault address. The debugger then halts at that location. During some programming or dumping attempts, I receive a Wire ACK fault. At other times, MCUXpresso reports: Error while executing the MI command I also tried to erase the flash from MCUXpresso, but the flash erase operation itself does not complete successfully. Checks already performed JTAG/SWD connections have been checked and appear to be correct. The issue was tested with both a SEGGER J-Link and an NXP MCU-Link debug probe. Boot configuration has been compared with the KW45 EVK. I am using a known-working application for testing. The issue is intermittent: programming sometimes succeeds, but at other times a Wire ACK fault or MI command error occurs. Flash erase has also been attempted, but it does not complete successfully. My questions What could cause the KW45 to: Intermittently report a Wire ACK fault while dumping or programming code? Report Error while executing the MI command? Jump or halt at an unexpected or invalid memory address after programming? Fail even when attempting a full flash erase? Since the issue includes intermittent Wire ACK faults and failure during flash erase, I suspect this may be related to the debug interface, SWD/JTAG signal integrity, power-supply stability, reset sequence, flash controller state, device security/configuration, boot configuration, or another hardware-level issue rather than the application itself. Could you please suggest the recommended procedure to: Recover or erase the KW45 device. Verify that the debug interface is functioning correctly. Check whether the device is secured or in a state that prevents normal programming. Determine whether the Wire ACK fault is caused by the target hardware, debug probe, power/reset behavior, or SWD/JTAG signal integrity. I can provide the following information if required: MCUXpresso IDE version: 25.6.1 Debug probes tested: SEGGER J-Link and NXP MCU-Link Complete error log, including the Wire ACK fault details Debug console output Schematic of the JTAG/SWD and boot connections SWD/JTAG clock frequency Power-supply and reset configuration Memory/register information from the failed state Any guidance on the recommended troubleshooting steps would be greatly appreciated. Thanks in advance. Re: KW45: Intermittent Wire ACK Fault During Programming/Debugging and Flash Erase Failure Hi Ma'am, Thank you for your detailed response. Regarding the hardware details: BOOT_CFG (PTA4) pull-down: Yes, the BOOT_CFG (PTA4) net has a pull-down resistor to GND on our custom board. VDD_SYS and VDD_CORE decoupling capacitors: Yes, the required decoupling capacitors are populated on the board. I have attached the relevant schematic sections/images showing the VDD_SYS and VDD_CORE connections and decoupling capacitors. Meanwhile, I will proceed with the steps you suggested to access the device through ISP mode and will try the blhost commands to check the device state and perform the mass erase. Regarding the application that was previously running: The application is based on FreeRTOS and integrates the following peripherals/modules: FreeRTOS LPSPI0 with DMA GPIO LPSPI1 with FIFO WDOG Regarding the low-power question, I did not intentionally use any specific low-power example in the application. I will perform the ISP recovery procedure and let you know the results, particularly for: get-property 1 get-property 07 flash-erase-all flash-erase-all 2 Please let me know if there are any additional hardware checks or measurements you recommend while I perform these tests. Prashanth1_0-1789454497591.pngPrashanth1_0-1789454497591.png Prashanth1_1-1789454501864.pngPrashanth1_1-1789454501864.png Thanks again for your support. Best regards, Prashanth Re: KW45: Intermittent Wire ACK Fault During Programming/Debugging and Flash Erase Failure Hello, hope you are doing well.   Firstly, could you please confirm some hardware details from your custom board: Does the BOOT_CFG (PTA4) net have a pull-down resistor to GND? Are the VDD_SYS and VDD_CORE decoupling capacitors populated? As these are required to provide a feedback path and maintain voltage stability on the internal regulator output.   To attempt to recover the device, please try the following steps: Are you able to access your device through ISP mode? For this, pull BOOT_CONFIG (PTA4) high during reset to force the device into ISP mode (on a KW47-EVK this is SW4) Once in ISP mode, open a command prompt and run the following commands: # Confirms ROM bootloader communication is working, a successful response confirms the device is reachable via ISP blhost.exe -p COMX get-property 1 # Reveals whether the device is in OEM_OPEN or a secured lifecycle state blhost.exe -p COMX get-property 07 # Perform a mass erase of the CM33 and NBU Program Flash blhost.exe -p COMX flash-erase-all blhost.exe -p COMX flash-erase-all 2 Afterwards, you could try running a hello_world or BLE example to make sure the board is working properly. Also, just to confirm, which application did you run previously? Did you test with any low power examples? It is also possible that the device entered a low‑power state, disabling the SWD debug interface during low-power operation, which would prevent LinkServer or J-Link from connecting normally Best regards, Sofia.
View full article
PCA9450 Buck Voltage outside tolerance We use a PCA9450BHNY to supply an i.MX8 Nano. During production testing, we measure the Voltage of Buck 1 (V_0V95_SOC) and Buck2 (V_0V85_ARM) an check the voltage Limits of 0.85V +/- 2%. During this test, the CPU stops and the flash is unprogrammed. Beginning in August 2026 the Voltage rises and violates the upper limit at some boards. Not only the individual Voltages of a board rises, also the mean value of thousands of boards. There was an PCN (202502007F01 : PCA9450 / MP90 Dual Wafer Fabrication Source Expansion from SSMC to PSMC) last year (25.04.2025) Can the new wafer fab a possible source of the problem? i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: PCA9450 Buck Voltage outside tolerance Hello! Thank you for your patience. I’m currently checking this internally and will get back to you as soon as I have an update. Re: PCA9450 Buck Voltage outside tolerance An internal investigation revealed that the problem was caused by worn test probes contacting the test points on the printed circuit board. We replaced the test probes, and the voltages are now within the permissible range.
View full article
How to get NPU Temperature and utilization for NXP i.MX93 EVK I am using i.MX93 EVK and want to monitor the Ethos-U NPU temperature & utilization(load) at runtime how can I get this data ? The agenda is to monitor the HW-parameters during the inference of AI-models. I could monitor the below parameters using i.MX8MPlus I want to achieve the similar for i.MX93. 8MPlus RAM=$(free -m | awk '/Mem:/ {print $3}') CPU_LOAD=$(vmstat 1 2 | tail -1 | awk '{print 100 - $15}') CPU_TEMP=$(awk '{print $1/1000}' /sys/class/thermal/thermal_zone0/temp 2>/dev/null || echo "N/A") GPU_TEMP=$(awk '{print $1/1000}' /sys/class/thermal/thermal_zone1/temp 2>/dev/null || echo "${CPU_TEMP}") GPU_LOAD=$(cat /sys/kernel/debug/gc/load 2>/dev/null | awk '/load/ {gsub("%","",$3); if (max=="" || $3>max) max=$3} END {if (max!="") print max "%"; else print "N/A"}') I.mx93 RAM=$(free -m | awk '/Mem:/ {print $3}') CPU_LOAD=$(vmstat 1 2 | tail -1 | awk '{print 100 - $15}') CPU_TEMP=$(awk '{print $1/1000}' /sys/class/thermal/thermal_zone0/temp) How can I monitor the GPU_LOAD & GPU_TEMP for i.MX93 npu(ethos-u) ? Linux Re: How to get NPU Temperature and utilization for NXP i.MX93 EVK Hi @sonal-acldigital  Neither the i.MX 8M Plus nor the i.MX 93 offers a method to monitor NPU temperature in real time. - imx8MP, thermal_zone0 represents the cpu-thermal temperature ,thermal_zone1 represents the soc-thermal temperature. - imx93, thermal_zone0 represents the cpu-thermal temperature. - NPU, There is no such tool like nputop. For information on performance tuning, please refer to Section 7.1.2, "Profiling for Hardware Accelerators," in the ML User Guide. B.R Re: How to get NPU Temperature and utilization for NXP i.MX93 EVK @pengyong_zhang Thanks for clarifying the thermal zones for the i.MX 8M Plus and i.MX 93. Could you please clarify the following: i.MX8MPLUS 1. GPU Temperature: Is there a dedicated system path (like /sys/class/thermal/thermal_zoneX/temp) to read individual GPU temperatures, or is it covered solely under the soc-thermal zone (thermal_zone1)? 2. GPU Load: Is reading /sys/kernel/debug/gc/load the standard method for checking GPU load, or is the process detailed in Section 7.1.2 of the ML User Guide required for this as well? i.MX93: Since there is no native tool (like nputop) to monitor NPU load and temperature, we would like to ask: Is it valid to derive relative NPU utilization by measuring the reduction in CPU load when offloading inference execution to the NPU vs. running on the CPU alone? If this method isn't recommended, is there any alternative driver node or performance counter we can use to estimate NPU activity during an inference run? Re: How to get NPU Temperature and utilization for NXP i.MX93 EVK Hi @sonal-acldigital  Sorry for the late reply. I recently had a severe viral cold and had a high fever for a while. The fever just broke today. 1. There is no dedicated path to read the GPU temperature. 2. Yes, GPU load monitoring via /sys/kernel/debug/gc/load is the current method. IMX93: You need to calculate the NPU utilization yourself using profiling. B.R
View full article
KW45:プログラミング/デバッグ中の断続的なワイヤACK障害およびフラッシュ消去失敗 チームの皆さん、こんにちは。 現在、KW45ベースのカスタムボードを使用しているのですが、ファームウェアのプログラミングとデバッグ中に断続的な問題が発生しています。 SEGGER J-LinkとNXP MCU-Linkのデバッグプローブの両方で基板をテストしましたが、問題は両方のプローブで発生しました。 このカスタムボードはKW45 EVKと同じブート構成を採用しており、JTAG/SWD接続も確認済みで、問題ないようです。 しかし、以下のような挙動が見られます。 動作が確認されているアプリケーションをダンプしたりプログラムしたりしようとすると: 時にはアプリケーションが成功裏にプログラムされますが、プログラムやデバッグセッション開始後、デバイスは最終的にフォールトアドレスにジャンプします。 デバッガーはその場所で停止します。 プログラミングやダンプ処理中に、ワイヤACKフォルトが発生することがあります。 MCUXpressoは、別の時には次のように報告している。 MIコマンドの実行中にエラーが発生しました。 MCUXpressoからフラッシュメモリを消去しようと試みましたが、フラッシュメモリの消去操作自体が正常に完了しませんでした。 既に実施済みのチェック JTAG/SWD接続を確認したところ、問題ないようです。 この問題はSEGGER J-LinkとNXP MCU-Linkデバッグプローブの両方でテストされました。 ブート構成はKW45 EVKと比較された。 テストには動作が確認されているアプリケーションを使っています。 この問題は断続的に発生します。プログラミングが成功することもありますが、ワイヤACKエラーやMIコマンドエラーが発生することもあります。 フラッシュメモリの消去も試みましたが、正常に完了しませんでした。 私の質問 KW45がコードのダンプやプログラミング中に断続的にWire ACKの故障を報告する原因は何でしょうか? MIコマンドの実行中にエラーを報告しますか? プログラミング後に、予期しないまたは無効なメモリ アドレスにジャンプまたは停止する? フラッシュメモリの完全消去を試みても失敗する? 問題には断続的なWire ACKの故障やフラッシュ消去時の故障が含まれているため、これはデバッグインターフェース、SWD/JTAGの信号整合性、電源の安定性、リセットシーケンス、フラッシュコントローラの状態、デバイスのセキュリティ/設定、起動設定、あるいは他のハードウェアレベルの問題に関連しているのではないかと疑っています。 以下のような推奨される手順を教えていただけますか: KW45デバイスを復元または消去します。 デバッグインターフェースが正しく動作しているか確認してください。 デバイスがセキュリティ保護されているか、または通常のプログラミングを妨げる状態になっていないかを確認してください。 ワイヤACK障害が、ターゲットハードウェア、デバッグプローブ、電源/リセット動作、またはSWD/JTAG信号の完全性のいずれかに起因するものかどうかを判断します。 必要に応じて以下の情報を提供できます。 MCUXpresso IDE バージョン:25.6.1 テストしたデバッグプローブ:SEGGER J-LinkおよびNXP MCU-Linkです ワイヤACK障害の詳細を含む完全なエラーログ デバッグコンソール出力 JTAG/SWDおよびブート接続の概略図 SWD/JTAGクロック周波数 電源およびリセット設定 障害状態からのメモリ/レジスタ情報 推奨されるトラブルシューティング手順についてご教示いただければ大変ありがたいです。 よろしくお願いいたします。 Re: KW45: Intermittent Wire ACK Fault During Programming/Debugging and Flash Erase Failure こんにちは、奥様。 詳細なご回答をありがとうございました。 ハードウェアの詳細について: BOOT_CFG (PTA4) プルダウン:はい、当社のカスタムボードでは、BOOT_CFG (PTA4) ネットにGNDへのプルダウン抵抗が接続されています。 VDD_SYSおよびVDD_COREデカップリングコンデンサ:はい、必要なデカップリングコンデンサは基板上に実装されています。VDD_SYSとVDD_COREの接続およびデカップリングコンデンサを示す関連する回路図の断面図/画像を添付しました。 その間に、ISP モードで デバイスにアクセスするための手順を進め、blhostコマンドでデバイスの状態を確認し、大量消去を実行してみます。 以前に実行されていたアプリケーションについて: このアプリケーションは FreeRTOS をベースにしており、以下のペリフェラル/モジュールを統合しています: FreeRTOS DMA対応LPSPI0 汎用I/O (GPIO) LPSPI1(FIFO付き) WDOG 低消費電力の質問については、アプリケーションで特定の低消費電力の例を意図的に使ったわけではありません。 ISP復旧手順を実行し、結果をお知らせします。特に以下の点についてお知らせします。 get-property 1 get-property 07 フラッシュ消去 フラッシュ消去2 これらのテストを実施する際に、他に推奨するハードウェアのチェックや測定があればお知らせください。 Prashanth1_0-1789454497591.pngプラシャンス1_0-1789454497591.png Prashanth1_1-1789454501864.pngプラシャンス1_1-1789454501864.png 改めてサポートありがとうございます。 よろしくお願いします、 プラシャント Re: KW45: Intermittent Wire ACK Fault During Programming/Debugging and Flash Erase Failure こんにちは、お元気でお過ごしでしょうか。   まず最初に、カスタムボードのハードウェア詳細を確認していただけますか: BOOT_CFG(PTA4)ネットにはGNDへのプルダウン抵抗が接続されていますか?VDD_SYSおよびVDD_COREのデカップリングコンデンサは実装されていますか?これらは、フィードバック経路を提供し、内部レギュレータ出力の電圧安定性を維持するために必要となる。   デバイスの復旧を試みるには、以下の手順をお試しください。 ISPモードでデバイスにアクセスできますか?そのためには、リセット中にBOOT_CONFIG(PTA4)をハイレベルにプルアップして、デバイスをISPモードに強制的に切り替えます(KW47-EVKの場合はSW4です)。 ISPモードに入ったら、コマンドプロンプトを開き、以下のコマンドを実行します。 # Confirms ROM bootloader communication is working, a successful response confirms the device is reachable via ISP blhost.exe -p COMX get-property 1 # Reveals whether the device is in OEM_OPEN or a secured lifecycle state blhost.exe -p COMX get-property 07 # Perform a mass erase of the CM33 and NBU Program Flash blhost.exe -p COMX flash-erase-all blhost.exe -p COMX flash-erase-all 2 その後、hello_worldやBLEの例を試して、基板が正常に動作しているか確認してみてください。 念のため確認ですが、以前どのアプリケーションを実行しましたか?低消費電力のサンプルでもテストしましたか?また、デバイスが低消費電力状態に入り、低消費電力運転中にSWDデバッグインターフェースが無効化され、LinkServerやJ-Linkが正常に接続できなくなる可能性もあります よろしくお願いします、 ソフィア。
View full article
PCA9450 バック電圧の許容範囲外 i.MX8 Nanoへの電源供給にはPCA9450BHNYを使用しています。 生産テスト中に、Buck 1 (V_0V95_SOC) と Buck2 (V_0V85_ARM) の電圧を測定し、0.85V +/- 2% の電圧制限を確認します。 このテスト中は、CPUは停止し、フラッシュメモリはプログラムされていない状態になります。 2026年8月から電圧が上昇し、一部の基板で上限値を超えます。 個々の基板の電圧が上昇するだけでなく、数千枚の基板の平均値も上昇する。 PCN (202502007F01 : PCA9450 / MP90 デュアルウェハ製造ソース拡張) がありました 昨年(2025年4月25日)SSMCからPSMCへ 新しいウェハーファブが問題の原因になり得るのでしょうか? i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: PCA9450 Buck Voltage outside tolerance こんにちは! ご辛抱いただきありがとうございます。現在社内で確認中です。最新情報が入り次第、ご連絡いたします。 Re: PCA9450 Buck Voltage outside tolerance 社内調査の結果、問題の原因は、摩耗したテストプローブがプリント基板上のテストポイントに接触したことにあると判明した。テストプローブを交換したところ、電圧は許容範囲内になりました。
View full article
FRDM-IMX95のサスペンド時の消費電力を可能な限り低く抑える FRDM-IMX95ボードでサスペンドモード時の消費電力を可能な限り低く抑える方法についてのガイダンスをお探しですか?ベアメタルm7コードを使用し、a55sをオフにすることで、約2.2Wまで消費電力を下げることができました。これは、エキスパンダー/PHY/PD_NETC の電源を完全に切った後の状態です。FRDM-IMX95はどのくらい低く設定できるのでしょうか? FRDMトレーニング Re: Lowest possible SUSPEND power consumption of FRDM-IMX95 最新の調査結果を自分の投稿に追記します…EXT_5V0とEXT_3V3_PWR_ENをオフにしてみましたが、それ以上の改善は見られませんでした。次にDDRセルフリフレッシュをテストしたところ、約193mA/1.1Wまで下げることができました。できればもっと値下げしたいのですが…。 Re: Lowest possible SUSPEND power consumption of FRDM-IMX95 当社の i.MX 95消費電力測定を参照し、参照できる低消費電力のユースケースが多数あります。 i.MX 95の消費電力測定 Re: Lowest possible SUSPEND power consumption of FRDM-IMX95 これ閉めていいよ。低電力モードをすべて確実にテストでき、必要な結果を得ることができました。
View full article
KW45:编程/调试期间间歇性线路确认故障和闪存擦除失败 大家好, 我目前正在使用基于 KW45 的定制板,在固件编程和调试过程中遇到了间歇性问题。 我分别使用 SEGGER J-Link 和 NXP MCU-Link 调试探针测试了该电路板,两种探针都出现了该问题。 定制板的启动配置与 KW45 EVK 相同,JTAG/SWD 连接也已检查,看起来是正确的。 然而,我发现出现了以下情况: 当我尝试转储或编程一个已知可以正常运行的应用程序时: 有时应用程序编程成功,但在编程或启动调试会话后,设备最终会跳转到故障地址。 调试器随后在该位置停止。 在某些编程或转储尝试过程中,我收到 Wire ACK 故障。 MCUXpresso 在其他时候报道: 执行 MI 命令时出错 我还尝试使用 MCUXpresso 擦除闪存,但闪存擦除操作本身并未成功完成。 已执行的检查 已检查 JTAG/SWD 连接,连接似乎正常。 我们使用 SEGGER J-Link 和 NXP MCU-Link 调试探针测试了该问题。 已将启动配置与 KW45 EVK 进行了比较。 我使用一个已知可以正常运行的应用程序进行测试。 该问题是间歇性的:有时编程成功,但有时会出现 Wire ACK 故障或 MI 命令错误。 也尝试过闪存擦除,但未能成功完成。 我的问题 什么原因会导致 KW45 在转储或编程代码时间歇性地报告 Wire ACK 故障? 执行 MI 命令时出错? 编程后跳转到或停止在意外或无效的内存地址? 即使尝试完全擦除闪存也失败了吗? 由于该问题包括间歇性 Wire ACK 故障和闪存擦除期间的故障,我怀疑这可能与调试接口、SWD/JTAG 信号完整性、电源稳定性、RESET 序列、闪存控制器状态、设备安全/配置、启动配置或其他硬件级问题有关,而不是应用程序本身的问题。 请问您能否提供以下方面的推荐操作流程: 恢复或擦除 KW45 设备。 确认调试接口功能正常。 检查设备是否已锁定或处于阻止正常编程的状态。 确定 Wire ACK 故障是由目标硬件、调试探针、电源/复位行为还是 SWD/JTAG 信号完整性引起的。 如有需要,我可以提供以下信息: MCUXpresso IDE 版本:25.6.1 测试的调试探针:SEGGER J-Link 和 NXP MCU-Link 完整的错误日志,包括 Wire ACK 故障详情。 调试控制台输出 JTAG/SWD 和启动连接示意图 SWD/JTAG时钟频率 电源和 RESET 配置 来自故障状态的内存/寄存器信息 非常感谢您能提供任何故障排除步骤方面的指导。 先行致谢。 Re: KW45: Intermittent Wire ACK Fault During Programming/Debugging and Flash Erase Failure 你好,希望你一切都好。   首先,请您确认一下您定制主板的一些硬件细节: BOOT_CFG (PTA4) 网络是否有下拉电阻连接到 GND?VDD_SYS 和 VDD_CORE 去耦电容是否已安装?因为这些是提供反馈通路并维持内部稳压器输出电压稳定性所必需的。   要尝试恢复设备,请尝试以下步骤: 您能否通过 ISP 模式访问您的设备?为此,在 RESET 期间将 BOOT_CONFIG (PTA4) 拉高,以强制设备进入 ISP 模式(在 KW47-EVK 上,这是 SW4)。 进入ISP模式后,打开命令提示符并运行以下命令: # Confirms ROM bootloader communication is working, a successful response confirms the device is reachable via ISP blhost.exe -p COMX get-property 1 # Reveals whether the device is in OEM_OPEN or a secured lifecycle state blhost.exe -p COMX get-property 07 # Perform a mass erase of the CM33 and NBU Program Flash blhost.exe -p COMX flash-erase-all blhost.exe -p COMX flash-erase-all 2 之后,您可以尝试运行 hello_world 或 BLE 示例,以确保电路板正常工作。 另外,请确认一下,您之前运行的是哪个应用程序?你有没有用低功耗的例子进行测试?设备也可能进入了低功耗状态,在低功耗运行期间禁用了SWD调试接口,这将导致LinkServer或J-Link无法正常连接。 此致, 索菲亚。 Re: KW45: Intermittent Wire ACK Fault During Programming/Debugging and Flash Erase Failure 您好,女士。 感谢您的详细回复。 关于硬件细节: BOOT_CFG (PTA4) 下拉:是的,我们定制的板上的 BOOT_CFG (PTA4) 网络有一个下拉电阻连接到 GND。 VDD_SYS 和 VDD_CORE 去耦电容:是的,所需的去耦电容已安装在板上。我已附上相关的原理图部分/图像,显示了VDD_SYS 和 VDD_CORE 的连接以及去耦电容。 同时,我将按照您建议的步骤,通过ISP 模式访问设备,并尝试使用 blhost 命令检查设备状态并执行批量擦除。 关于之前运行的应用程序: 该应用程序基于FreeRTOS ,并集成了以下外设/模块: FreeRTOS LPSPI0 带 DMA 通用IO LPSPI1 带 FIFO WDOG 关于低功耗问题,我在应用中并没有特意使用任何具体的低功耗示例。 我将执行 ISP 恢复程序,并告知您结果,特别是以下方面: 获取属性 1 获取属性 07 全部擦除 全部擦除 2 如果您建议在进行这些测试时进行任何其他硬件检查或测量,请告诉我。 普拉山斯1_0-1789454497591.png Prashanth1_1-1789454501864.png 再次感谢您的支持。 此致, 普拉桑特
View full article
如何获取 NXP i.MX93 EVK 的 NPU 温度和利用率 我正在使用 i.MX93 EVK,想要监控 Ethos-U NPU 在运行时的温度和利用率(负载),请问如何获取这些数据? 本次议程旨在监测人工智能模型推理过程中的硬件参数。 我可以使用 i.MX8MPlus 监测以下参数,我想在 i.MX93 中实现类似的功能。 8MPlus RAM=$(free -m | awk '/Mem:/ {print $3}') CPU_LOAD=$(vmstat 1 2 | tail -1 | awk '{print 100 - $15}') CPU_TEMP=$(awk '{print $1/1000}' /sys/class/thermal/thermal_zone0/temp 2>/dev/null || echo "N/A") GPU_TEMP=$(awk '{print $1/1000}' /sys/class/thermal/thermal_zone1/temp 2>/dev/null || echo "${CPU_TEMP}") GPU_LOAD=$(cat /sys/kernel/debug/gc/load 2>/dev/null | awk '/load/ {gsub("%", "$3"); if (max== || $3>max) max=$3} END {if (max!=) print max "%"; else print "N/A"}') i.MX 93 RAM=$(free -m | awk '/Mem:/ {print $3}') CPU_LOAD=$(vmstat 1 2 | tail -1 | awk '{print 100 - $15}') CPU_TEMP=$(awk '{print $1/1000}' /sys/class/thermal/thermal_zone0/temp) 如何监测 i.MX93 npu(ethos-u) 的 GPU_LOAD 和 GPU_TEMP? Linux Re: How to get NPU Temperature and utilization for NXP i.MX93 EVK 你好@sonal-acldigital i.MX 8M Plus 和 i.MX 93 都没有提供实时监测 NPU 温度的方法。 - imx8MP,thermal_zone0 表示 CPU 温度,thermal_zone1 表示 SoC 温度。 - imx93,thermal_zone0 表示 CPU 温度。 - NPU,没有像 nputop 这样的工具。 有关性能调优的信息,请参阅第 7.1.2 节。《机器学习用户指南》中的“硬件加速器性能分析”。 B.R Re: How to get NPU Temperature and utilization for NXP i.MX93 EVK @pengyong_zhang感谢您澄清 i.MX 8M Plus 和 i.MX 93 的热区划分。请您澄清以下问题: i.MX8MPLUS 1. GPU 温度:是否有专门的系统路径(如 /sys/class/thermal/thermal_zoneX/temp)来读取单个 GPU 温度,还是仅包含在 soc-thermal 区域(thermal_zone1)中? 2. GPU 负载:读取 /sys/kernel/debug/gc/load 是检查 GPU 负载的标准方法吗?还是也需要按照 ML 用户指南第 7.1.2 节中详述的过程进行检查? i.MX93: 由于没有像 nputop 这样的原生工具来监测 NPU 负载和温度,我们想问:将推理执行卸载到 NPU 与单独在 CPU 上运行相比,通过测量 CPU 负载的减少量来推导出相对 NPU 利用率是否有效? 如果这种方法不推荐,是否有其他驱动节点或性能计数器可以用来估算推理运行期间的 NPU 活动? Re: How to get NPU Temperature and utilization for NXP i.MX93 EVK 你好@sonal-acldigital 抱歉回复晚了。我前段时间得了重感冒,还持续高烧了一段时间。今天刚退烧。 1.没有专用的路径来读取GPU温度。 2. 是的,目前通过 /sys/kernel/debug/gc/load 进行 GPU 负载监控的方法就是如此。 IMX93: 您需要使用性能分析自行计算 NPU 利用率。 B.R
View full article
PCA9450降压电压外部容差 我们使用 PCA9450BHNY 为 i.MX8 Nano 供电。 在生产测试期间,我们测量 Buck 1 (V_0V95_SOC) 和 Buck2 (V_0V85_ARM) 的电压,并检查电压限制为 0.85V +/- 2%。 在此测试期间,CPU 停止运行,闪存未编程。 从 2026 年 8 月开始,某些电路板上的电压升高并违反了上限。 不仅单个电路板的电压升高,而且数千个电路板的平均电压也升高了。 存在一个 PCN(202502007F01:PCA9450 / MP90 双晶圆制造源扩展) 去年(2025年4月25日)从SSMC到PSMC 新的晶圆厂会不会是问题的根源? i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: PCA9450 Buck Voltage outside tolerance 您好! 感谢您的耐心等待。我目前正在内部核实此事,一旦有最新消息,我会立即回复您。 Re: PCA9450 Buck Voltage outside tolerance 内部调查显示,问题是由磨损的测试探针接触印刷电路板上的测试点造成的。我们更换了测试探针,现在电压已在允许范围内。
View full article
请求将已归档的 S32K3 FreeRTOS 2.0.0 和 TCP/IP 1.0.1 软件包添加到我的 NXP 帐户 您好,NXP支持团队, 我正在使用 S32 Design Studio 3.4 和 S32K3 RTD 2.0.0 开发一个 S32K344 项目。我有一个现有的以太网/lwIP项目,该项目最初是用以下软件版本创建的: S32 设计工作室:3.4 S32K3 RTD:2.0.0 FreeRTOS:10.4.6 UOS 2.0.0 S32K3 TCP/IP 协议栈:RTM 1.0.1 我现在需要在配置工具中修改项目,以添加 FlexCAN 配置。但是,我目前的 S32DS 安装中没有安装匹配的 FreeRTOS 和 TCP/IP 配置工具包。 因此,当我使用“更新代码”时,“配置工具”无法识别现有的 FreeRTOS/lwIP 组件,并建议删除诸如以下文件: FreeRTOSConfig.h lwipcfg.h lwipopts.h lwippools.h netifcfg.h netifcfg.c 我账户中可用的较新软件包与此项目不兼容。例如,FreeRTOS 2.0.1 和 TCP/IP 1.0.1 HF1 与 RTD 2.0.1 一致,而我的项目基于 RTD 2.0.0。 我知道配套的 FreeRTOS 2.0.0 软件包已被归档。请将以下已存档代码包/软件包的访问权限添加到我的 NXP 帐户中? SW32K3_FreeRTOS_10_4_6_UOS_2_0_0_DS_updatesite_D2204.zip 如果可能,还要提供匹配的 TCP/IP 数据包: S32K3_TCPIP_RTM_1_0_1_D2205_updatesite.zip 需要这些软件包,以便我可以使用最初开发该项目时使用的相同软件版本打开并重新生成现有项目,而无需将整个项目迁移到不同的 RTD 版本。 我的目标是:   MCU: S32K344 S32DS: 3.4 S32K3 RTD: 2.0.0 FreeRTOS: 10.4.6 UOS 2.0.0 TCP/IP Stack: RTM 1.0.1 请问能否为我的账户启用这些存档下载功能,或者提供获取它们的正确步骤? 谢谢! Re: Request to add archived S32K3 FreeRTOS 2.0.0 and TCP/IP 1.0.1 packages to my NXP account 你好@Aaditya773 , 我了解到您正在尝试访问旧版本。这些旧软件包已过时且不再维护,但是,如果该帐户之前申请过访问该软件包,您应该可以通过 Flexera 门户中的“以前”选项卡看到它: Julin_AragnM_0-1788887530794.pngJulin_AragnM_0-1788887530794.pngJulin_AragnM_0-1788887530794.png 如果该帐户没有访问权限,我想引导您走上一条更可持续的道路:将您的项目迁移到 RTD 6.0.0 或 RTD 7.0.0。较新的 RTD(以及 FreeRTOS 和 Stack 版本)提供了已记录的已知问题、错误修复、优化,以及对 K3 衍生品的更广泛支持。 社区中有很多利用新型RTD封装实现以太网功能的案例: 示例 S32K358 GMAC lwIP FreeRTOS RDBESS S32DS 3.6.1 RTD600 示例 S32K389 GMAC1 SABRE lwIP FreeRTOS S32DS 3.6.1 RTD600 示例 S32K344 EMAC lwIP FreeRTOS miniEVB S32DS 3.6.1 RTD 6.0.0 [RTD600 MCAL] 示例 FRDM-A-S32K358 EMAC lwIP FreeRTOS S32DS 3.6 RTD 6.0.0 对于 RTD 6.0.0,您可以安装以下兼容软件包: SW32K3_S32M27x_RTD_R21-11_6.0.0_D2506_DesignStudio_updatesite.zip SW32K3_FreeRTOS_11.1.0_6.0.0_CD1_D2506_DesignStudio_updatesite.zip SW32K3_TCPIP_STACK_3.0.0_D2507_DesignStudio_updatesite.zip 对于 RTD 7.0.1,您可以安装以下兼容的 代码包,软件包: SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip SW32K3_FreeRTOS_11.1.0_7.0.0_CD1_HF1_D2511_DesignStudio_updatesite.zip SW32K3_TCPIP_STACK_5.0.0_CD01_D2605_DesignStudio_updatesite.zip 如果您确定需要使用旧版软件包才能继续使用旧版软件进行开发,请联系您指定的代理商或 NXP 联系人,以帮助我解决问题。 此致, 朱利安 Re: Request to add archived S32K3 FreeRTOS 2.0.0 and TCP/IP 1.0.1 packages to my NXP account 你好,朱利安, 感谢您的回复,并分享了 RTD 6.0.0 的迁移路径。 我已经尝试设置新的环境,但不幸的是,旧的 S32K344-WB 项目在新软件栈下仍然无法正常工作。该项目最初是围绕较旧的 S32DS 3.4 / PlatformSDK 2.0.0 版本创建的,原始配置的几个部分无法顺利已翻译为较新的环境。 该项目具体依赖于: S32 设计工作室 3.4 S32K344 / S32K3 平台 SDK 2.0.0 ${PLATFORMSDK_S32K3_2022_03_S32K344_M7_2.0.0_PATH} SW32K3_RTD_4_4_2_0_0_D2203 SW32K3_FreeRTOS_10_4_6_UOS_2_0_0_DS_updatesite_D2204.zip S32K3_TCPIP_RTM_1_0_1_D2205_updatesite.zip 我已查看可用下载和先前下载记录,但我的帐户中找不到这些已存档的软件包。 目前看来,较新的软件包似乎无法替代这个特定的遗留项目,因此,如果 NXP 能将所需的已归档的 S32DS 3.4 兼容软件包提供给我的帐户,我将非常感激。 具体来说,能否请您添加或提供以下访问权限: S32K3 / S32K344 平台SDK 2.0.0 / RTD 2.0.0 SW32K3_FreeRTOS_10_4_6_UOS_2_0_0_DS_updatesite_D2204.zip S32K3_TCPIP_RTM_1_0_1_D2205_updatesite.zip S32DS 3.4 下 S32K344 所需的任何匹配的 S32 配置工具/设备支持包 如果能将这些存档软件包添加到我的可用下载列表中,我将非常感激,因为我一直找不到其他能与此项目正确配合使用的安装程序。 非常感谢您的帮助。 Re: Request to add archived S32K3 FreeRTOS 2.0.0 and TCP/IP 1.0.1 packages to my NXP account 你好@Aaditya773 , 由于“上一页”选项卡中没有该软件包,因此该帐户很可能一开始就没有访问过该软件包的权限。 如果您有指定的现场应用工程师 (FAE) 或销售代表,请联系他们,以便他们申请访问您的帐户。 另一方面,如果您想将 S32K344-WB 项目迁移到更新的 RTD,我可以协助您解决过程中遇到的任何问题。 此致, 朱利安
View full article
MCU SDKにI2Cドライバを追加 NXPチームの皆様、こんにちは。 MCU SDKに24cxxシリーズのeeprom i2cドライバを追加したいと考えています。どうやって追加できるのでしょうか? ありがとうございます。 Re: Add I2C driver to MCU SDK こんにちは、 @taw さん。 あなたが共有してくれた情報からすると、カスタムSDKを探しているのだと思います。 このプロセスは使っているIDEによって異なります。 MCUXpresso for VS Codeについては、以下のドキュメントを参照してください。 MCUXpresso SDK:カスタムマニフェストの作成 MCUXpresso IDEについては、以下のドキュメントを参照してください。 カスタム基板サポートパッケージの作成 |NXP半導体 もしこれがあなたの言及でなければ、申請の詳細を教えていただけますか? よろしくお願いします、 パブロ
View full article
Request to add archived S32K3 FreeRTOS 2.0.0 and TCP/IP 1.0.1 packages to my NXP account Hello NXP Support Team, I am working on an S32K344 project using S32 Design Studio 3.4 and S32K3 RTD 2.0.0. I have an existing working Ethernet/lwIP project that was originally created with the following software versions: S32 Design Studio: 3.4 S32K3 RTD: 2.0.0 FreeRTOS: 10.4.6 UOS 2.0.0 S32K3 TCP/IP Stack: RTM 1.0.1 I now need to modify the project in Configuration Tools to add a FlexCAN configuration. However, my current S32DS installation does not have the matching FreeRTOS and TCP/IP Configuration Tools packages installed. Because of this, when I use Update Code, Configuration Tools does not recognize the existing FreeRTOS/lwIP components and proposes deleting files such as: FreeRTOSConfig.h lwipcfg.h lwipopts.h lwippools.h netifcfg.h netifcfg.c The newer packages available in my account are not compatible with this project. For example, FreeRTOS 2.0.1 and TCP/IP 1.0.1 HF1 are aligned with RTD 2.0.1, while my project is based on RTD 2.0.0. I understand that the matching FreeRTOS 2.0.0 package has been archived. Could you please add access to the following archived packages to my NXP account? SW32K3_FreeRTOS_10_4_6_UOS_2_0_0_DS_updatesite_D2204.zip and, if possible, the matching TCP/IP package: S32K3_TCPIP_RTM_1_0_1_D2205_updatesite.zip These packages are required so I can open and regenerate the existing project using the same software versions it was originally developed with, without migrating the entire project to a different RTD release. My target is:   MCU: S32K344 S32DS: 3.4 S32K3 RTD: 2.0.0 FreeRTOS: 10.4.6 UOS 2.0.0 TCP/IP Stack: RTM 1.0.1 Could you please enable these archived downloads for my account, or provide the correct procedure for obtaining them? Thank you. Re: Request to add archived S32K3 FreeRTOS 2.0.0 and TCP/IP 1.0.1 packages to my NXP account Hello @Aaditya773, I understand you are trying to access the older releases. These older packages are outdated and no longer actively maintained, however, if the account had requested access to the package before, you should be able to see it through the 'Previous' tab inside the Flexera portal: Julin_AragnM_0-1788887530794.pngJulin_AragnM_0-1788887530794.pngJulin_AragnM_0-1788887530794.png If the account does not have access, I would like to guide you toward a more sustainable path: migrating your project to RTD 6.0.0 or RTD 7.0.0. Newer RTD (as well as FreeRTOS and Stack releases) provide documented known issues, bugfixes, optimizations, as well as a broader support for K3 derivatives. There are various community examples for Ethernet enablement with newer RTD packages:  Example S32K358 GMAC lwIP FreeRTOS RDBESS S32DS 3.6.1 RTD600 Example S32K389 GMAC1 SABRE lwIP FreeRTOS S32DS 3.6.1 RTD600 Example S32K344 EMAC lwIP FreeRTOS miniEVB S32DS 3.6.1 RTD 6.0.0 [RTD600 MCAL] Example FRDM-A-S32K358 EMAC lwIP FreeRTOS S32DS 3.6 RTD 6.0.0  For RTD 6.0.0, you can install the following compatible packages: SW32K3_S32M27x_RTD_R21-11_6.0.0_D2506_DesignStudio_updatesite.zip SW32K3_FreeRTOS_11.1.0_6.0.0_CD1_D2506_DesignStudio_updatesite.zip SW32K3_TCPIP_STACK_3.0.0_D2507_DesignStudio_updatesite.zip For RTD 7.0.1, you can install the following compatible packages: SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip SW32K3_FreeRTOS_11.1.0_7.0.0_CD1_HF1_D2511_DesignStudio_updatesite.zip SW32K3_TCPIP_STACK_5.0.0_CD01_D2605_DesignStudio_updatesite.zip In case you determine the older package is necessary to continue your development with the older SW version, please help me by contacting your assigned distributor or NXP contact. Best regards, Julián Re: Request to add archived S32K3 FreeRTOS 2.0.0 and TCP/IP 1.0.1 packages to my NXP account Hello Julián, Thank you for your response and for sharing the RTD 6.0.0 migration path. I have tried setting up the newer environment, but unfortunately the older S32K344-WB project still does not work correctly under the newer software stack. The project was originally created around the older S32DS 3.4 / PlatformSDK 2.0.0 generation, and several parts of the original configuration do not translate cleanly to the newer environment. The project specifically depends on: S32 Design Studio 3.4 S32K344 / S32K3 PlatformSDK 2.0.0 ${PLATFORMSDK_S32K3_2022_03_S32K344_M7_2.0.0_PATH} SW32K3_RTD_4_4_2_0_0_D2203 SW32K3_FreeRTOS_10_4_6_UOS_2_0_0_DS_updatesite_D2204.zip S32K3_TCPIP_RTM_1_0_1_D2205_updatesite.zip I have checked the available and Previous downloads, but I cannot find these archived packages for my account. At this point, the newer packages do not seem to be a workable replacement for this particular legacy project, so I would be very grateful if NXP could make the required archived S32DS 3.4-compatible packages available to my account. In particular, could you please add or provide access to: S32K3 / S32K344 PlatformSDK 2.0.0 / RTD 2.0.0 SW32K3_FreeRTOS_10_4_6_UOS_2_0_0_DS_updatesite_D2204.zip S32K3_TCPIP_RTM_1_0_1_D2205_updatesite.zip any matching S32 Configuration Tools / device-support package required for S32K344 under S32DS 3.4 I would really appreciate it if these archived packages could be added to my available downloads, since I have not been able to find another setup that works correctly with this project. Thank you very much for your help. Re: Request to add archived S32K3 FreeRTOS 2.0.0 and TCP/IP 1.0.1 packages to my NXP account Hello @Aaditya773, Since the SW package is not available through the 'Previous' tab, most likely the account never had access to the package in the first place. If you have an assigned FAE, or Sales representative, please help me by contacting them so they can request access for your account. On the other hand, if you would like to work on migrating the S32K344-WB projects to newer RTD, I can assist you with any issues during the process. Best regards, Julián
View full article
向MCU SDK添加I2C驱动程序 您好,NXP团队, 我们希望在MCU SDK中添加我们的24cxx系列eeprom i2c驱动程序。我们该如何添加它? 谢谢 & 此致敬礼, Re: Add I2C driver to MCU SDK 嗨@taw , 根据您提供的信息,我推测您正在寻找定制的 SDK。 具体过程取决于您使用的集成开发环境 (IDE)。 对于 VS Code 版 MCUXpresso,您可以参考以下文档: MCUXpresso SDK:创建自定义清单 对于 MCUXpresso IDE,您可以参考以下文档: 创建定制板支持包 | 恩智浦半导体 如果您指的不是这个,请您提供更多关于您的请求的详细信息好吗? 此致, 巴勃罗
View full article
Plumber Fairfield CA Fast & Reliable Local Plumbers Plumber Fairfield CA provides professional plumbing services for homeowners and businesses dealing with everyday plumbing needs and unexpected emergencies. From leaking faucets and clogged drains to water heater problems and damaged pipes, having access to a dependable local plumber can help prevent small plumbing issues from becoming more serious and costly. The main idea behind choosing a Plumber Fairfield CA is simple: get reliable local help when you need plumbing repairs, maintenance, or emergency assistance. Professional plumbers can diagnose plumbing problems, recommend the appropriate solution, and complete repairs using the right tools and techniques. Whether you are dealing with a slow drain, a hidden leak, low water pressure, sewer problems, or a water heater issue, a qualified plumber in Fairfield, CA can help keep your residential or commercial plumbing system working properly.
View full article
科罗拉多州洛夫兰市水管工常见管道问题及何时寻求帮助 最后更新日期:2026年9月9日(官方网站链接见评论框) Loveland Co 管道公司指的是科罗拉多州 Loveland 市提供的专业管道服务,旨在帮助房主和企业处理常见的管道需求。从水龙头漏水、排水管堵塞到热水器问题以及更复杂的管道维修,经验丰富的管道工可以提供切实可行的解决方案,使管道系统正常运转。这就是为什么在科罗拉多州洛夫兰市选择一位可靠的水管工,以便在需要及时可靠的服务时非常重要的原因之一。 Plumber Loveland Co 的主要理念很简单:为客户提供专业的管道服务,包括日常维修、维护、安装和突发的管道问题。合格的当地水管工可以帮助找出问题的原因,推荐合适的解决方案,并安全高效地完成必要的工作。无论您需要小修小补还是大型管道工程方面的帮助,拥有值得信赖的管道专业人员都能帮助保护您的财产,并保持您家中管道系统的顺畅运行。
View full article
安装 S32K312 的 RTD 我正在尝试在 S32 Design Studio v 3.6.6上为 S32K312 设置开发环境,具体步骤如下: 1. 下载了 SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip 2. 在 S32 Design Studio 3.6.6 中打开了“S32Extensions and Updates”。在 Windows 11 系统上运行,并已安装 S32K3 实时驱动程序,如下所示: durga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.pngdurga_choudhury_0-1788877584959.png 3. 按照提示重启了IDE(我也尝试过重启电脑)。 由此看来,我无法看到对 K3 系列的支持。“新建项目”对话框中没有显示此选项: durga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.pngdurga_choudhury_1-1788877756997.png 如果我尝试安装如下所示的“S32K3XX”驱动程序: durga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.pngdurga_choudhury_2-1788877862245.png 我收到如下所示的错误信息: durga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.pngdurga_choudhury_3-1788877910412.png 现在在 S32DS v 3.6.2 上重复整个过程略有改善:现在“新建项目”对话框中列出了 K312 选项,但没有列出其 SDK: durga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.pngdurga_choudhury_4-1788878190320.png 我做错了什么? Re: Installing RTD for S32K312 嗨@VaneB 很遗憾,我在S32DS 3.6.6上没有对应的版本。我已经尝试将 RTD 版本从 7.0.1 降级到 6.0.0。 是否有适用于 3.6.6 的特定版本? Re: Installing RTD for S32K312 你好@durga_choudhury 截图来自我的 S32DS 3.6.10 系统。安装过程;但是,您应该会在 IDE 中看到类似的设置。 VaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.pngVaneB_0-1788893776567.png 另外,根据你分享的截图,我可以看到你已经成功安装了 RTD 7.0.1。由于 RTD 7.0.1 依赖于 S32K3 开发包,因此该软件包很可能已经安装。 Re: Installing RTD for S32K312 嗨@VaneB 请详细说明一下您的评论。 我看到我安装了 S32K1xx 的“开发包”(这也是我使用的 MCU 系列): durga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.pngdurga_choudhury_0-1788891225434.png 但我发现K3并没有类似的功能。 那么我该如何安装呢?重申一下,我目前为止所做的工作是: 1. 下载了 SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip 2. 已将其添加为 S32 DS v 3.6.6的更新站点 3. 安装了以下软件: durga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.pngdurga_choudhury_1-1788891394005.png Re: Installing RTD for S32K312 你好@durga_choudhury 来自您的 S32DS 3.6.6安装过程中,似乎没有安装 S32K3 开发包。 关于 S32DS 3.6.2,请注意,RTD 7.0.1 是使用 S32DS 3.6.4 开发和验证的。因此,我们建议使用 S32DS 3.6.4 版本。或者使用更新的版本以确保兼容性并避免潜在问题。 此外,还需要验证工具链。创建项目时,请确保已安装 NXP GCC 10.2.0 并选择其作为项目工具链。 BR,VaneB Re: Installing RTD for S32K312 你好@durga_choudhury 我的配置是RTD 7.0.0。随 S32DS 3.6.6 一起安装。但是,如前所述,RTD 7.0.1 应该可以正常工作,因为这些版本的设置非常相似。 能否分享一下您的安装详情? Re: Installing RTD for S32K312 你好@durga_choudhury 请注意,提供的链接并非常规网址。它对应于 S32DS 使用的更新站点,用于访问可用的软件包和更新。 要查看完整的更新站点列表,请打开 S32DS 扩展和更新窗口,然后选择“管理站点”。您可以在这里找到 IDE 识别的所有更新站点。 Re: Installing RTD for S32K312 你好@durga_choudhury 请您尝试以下操作?在 S32DS 中,转到“帮助”→“安装新软件”……这将打开安装窗口。在“使用以下方式操作:”字段中,输入以下更新站点: https://www.nxp.com/lgfiles/updates/Eclipse/S32DS_3.6 应该会显示一个可用更新列表,类似于下面显示的内容。请检查列表中是否能找到 S32 Design Studio S32K3xx 开发包,并尝试安装。 VaneB_0-1789057150680.pngVaneB_0-1789057150680.pngVaneB_0-1789057150680.pngVaneB_0-1789057150680.pngVaneB_0-1789057150680.pngVaneB_0-1789057150680.png 如果代码包,软件包未出现或安装失败,我建议更新到最新的 S32DS 版本。当前安装可能缺少某些元器件,或者在安装/更新过程中某些文件损坏。 Re: Installing RTD for S32K312 嗨@VaneB 很遗憾,它对我不起作用: durga_choudhury_0-1789083559046.pngdurga_choudhury_0-1789083559046.pngdurga_choudhury_0-1789083559046.pngdurga_choudhury_0-1789083559046.pngdurga_choudhury_0-1789083559046.png Re: Installing RTD for S32K312 嗨@VaneB 以下是我尝试过的两个文件(都存在同样的问题): durga_choudhury_0-1789048352154.pngdurga_choudhury_0-1789048352154.pngdurga_choudhury_0-1789048352154.pngdurga_choudhury_0-1789048352154.png 以下是关于S32DS的信息: durga_choudhury_1-1789048467186.pngdurga_choudhury_1-1789048467186.pngdurga_choudhury_1-1789048467186.pngdurga_choudhury_1-1789048467186.png 以下是一些安装细节,尽可能全部显示在一张屏幕截图中。您还需要其他信息吗? durga_choudhury_2-1789048687291.pngdurga_choudhury_2-1789048687291.pngdurga_choudhury_2-1789048687291.pngdurga_choudhury_2-1789048687291.png Re: Installing RTD for S32K312 嗨@VaneB 感谢您的支持。请您再次确认一下网址好吗?如果我尝试从这里更新,S32 DS 会报错,如下所示: durga_choudhury_0-1789063889394.pngdurga_choudhury_0-1789063889394.pngdurga_choudhury_0-1789063889394.png 如果我尝试通过 REST 类型的应用程序访问它,例如:使用 wget 下载时,出现 HTTP 错误 404(未找到)。 会不会是恩智浦内部的问题(例如,(不在面向公众的服务器上)? Re: Installing RTD for S32K312 你好@durga_choudhury 请您在另一台机器上测试一下好吗? 此外,最好与您的 IT 团队确认是否存在防火墙、代理或网络安全策略阻止访问更新站点。 Re: Installing RTD for S32K312 这似乎确实是我们的代理服务器出了问题。它可以在公司网络之外的计算机上运行。 非常感谢您的支持。
View full article
POWER consumption at runtime on NXP i.MX93 & i.MX8MPLUS EVK I am using NXP i.MX93 & i.MX8MPLUS EVK and want to monitor the POWER consumption at runtime how can I get this data ? The agenda is to monitor the power during the inference of AI-models. How can I monitor the power metrics ?  How can I monitor power metrics using only software, without any external hardware? Re: POWER consumption at runtime on NXP i.MX93 & i.MX8MPLUS EVK Thank you for this detailed information and reference to ANI3054. This is very helpful. Does the i.MX93 EVK also have a similar power measurement setup , or is there a different approach recommended for i.MX93? Re: POWER consumption at runtime on NXP i.MX93 & i.MX8MPLUS EVK Please refer to the document AN13054 i.MX 8M Plus Power Consumption Measurement To measure the power consumption, the PWR CPU board is designed with current sense resistors of suitable value inserted between the PMIC and CPU for each key power rail. The power data is obtained by sampling the average voltage drop across the sense resistors using power monitor chip PAC1934. The voltage drop for each power supply is divided by its sense resistor value within the BCU PC software tool to calculate the current.
View full article
ハードウェアシミュレーションには、システムVerilogやVAMS、またはPCA9698DGG,512(GPIOエキスパンダー)のspiseモデルが必要です。 システム用Verilog、VAMS、またはIOエクスパンダーの部品番号のSPICEモデルが必要です - PCA9698DGG,512。重要な業務に必要なため、至急ご提供ください。 データシートリンク - PCA9698 40ビットFm+ I2Cバス:RESET、OE、INT対応の高度なI/Oポート
View full article
IMXRT1176 应用程序崩溃,之后 IMXRT 无法启动。 您好, 我正在使用 IMXRT1176 定制板,在应用程序和辅助引导加载程序开发过程中,我的应用程序崩溃了,之后我无法刷写我的应用程序。我尝试进入串口下载器模式,然后擦除FLEXSPI NOR Flash,即使这样它仍然显示: “Flash Driver V.2 启动失败 - rc Ef(55): 动态闪存驱动程序启动未能提供闪存参数。终止 (0x0, 0x0, 0x0) 状态 0x40 - 驱动程序报告初始化失败 - EXTSPIJ 驱动程序 rc 20107 (0x4E8B) 芯片初始化失败 - Ef(55): 动态闪存驱动程序启动无法提供闪存参数。初始化闪存驱动程序 MIMXRT1170_SFDP_QSPI.cfx##" 我尝试通过 USB 将 NXP 启动实用程序连接到 MCU,并看到了以下日志。 "--------MCU设备ROM信息-------- 唯一 ID[31:00] = 0x8295ad77 唯一 ID[63:32] = 0x242cc80e 当前版本 = K3.0.1 目标版本 = T3.0.0 生命周期状态 = HAB 开放 --------MCU Flashloader 信息------- 当前版本 = K2.8.0 目标版本 = T1.0.1 --------MCU 设备 eFusemap-------- (0x940) SYSBT_CFG0 = 0x0 (0x950) SYSBT_CFG1 = 0x0 (0x960) SYSBT_CFG2 = 0x8 BT_FUSE_SEL = 1'b0 当 BMOD[1:0] = 2'b00(从熔丝启动)且引导设备中没有应用程序时,MCU 直接进入串口下载器模式。 当 BMOD[1:0] = 2'b10(内部启动)时,MCU 将根据 BOOT_CFGx 引脚和熔丝 BOOT_CFGx 启动应用程序。 ----------FlexRAM 存储器----------- IOMUXC_GPR->GPR16 = -------- --------MCU设备ROM信息-------- 唯一 ID[31:00] = 0x8295ad77 唯一 ID[63:32] = 0x242cc80e 当前版本 = K3.0.1 目标版本 = T3.0.0 生命周期状态 = HAB 开放 --------MCU Flashloader 信息------- 当前版本 = K2.8.0 目标版本 = T1.0.1 --------MCU 设备 eFusemap-------- (0x940) SYSBT_CFG0 = 0x0 (0x950) SYSBT_CFG1 = 0x0 (0x960) SYSBT_CFG2 = 0x8 BT_FUSE_SEL = 1'b0 当 BMOD[1:0] = 2'b00(从熔丝启动)且引导设备中没有应用程序时,MCU 直接进入串口下载器模式。 当 BMOD[1:0] = 2'b10(内部启动)时,MCU 将根据 BOOT_CFGx 引脚和熔丝 BOOT_CFGx 启动应用程序。 ----------FlexRAM 存储器----------- IOMUXC_GPR->GPR16 = -------- --------MCU设备ROM信息-------- 唯一 ID[31:00] = 0x8295ad77 唯一 ID[63:32] = 0x242cc80e 当前版本 = K3.0.1 目标版本 = T3.0.0 生命周期状态 = HAB 开放 --------MCU Flashloader 信息------- 当前版本 = K2.8.0 目标版本 = T1.0.1 --------MCU 设备 eFusemap-------- (0x940) SYSBT_CFG0 = 0x0 (0x950) SYSBT_CFG1 = 0x0 (0x960) SYSBT_CFG2 = 0x8 BT_FUSE_SEL = 1'b0 当 BMOD[1:0] = 2'b00(从熔丝启动)且引导设备中没有应用程序时,MCU 直接进入串口下载器模式。 当 BMOD[1:0] = 2'b10(内部启动)时,MCU 将根据 BOOT_CFGx 引脚和熔丝 BOOT_CFGx 启动应用程序。 ----------FlexRAM 存储器----------- IOMUXC_GPR->GPR16 = -------- --------MCU设备ROM信息-------- 唯一 ID[31:00] = 0x8295ad77 唯一 ID[63:32] = 0x242cc80e 当前版本 = K3.0.1 目标版本 = T3.0.0 生命周期状态 = HAB 开放 --------MCU Flashloader 信息------- 当前版本 = K2.8.0 目标版本 = T1.0.1 --------MCU 设备 eFusemap-------- (0x940) SYSBT_CFG0 = 0x0 (0x950) SYSBT_CFG1 = 0x0 (0x960) SYSBT_CFG2 = 0x8 BT_FUSE_SEL = 1'b0 当 BMOD[1:0] = 2'b00(从熔丝启动)且引导设备中没有应用程序时,MCU 直接进入串口下载器模式。 当 BMOD[1:0] = 2'b10(内部启动)时,MCU 将根据 BOOT_CFGx 引脚和熔丝 BOOT_CFGx 启动应用程序。 ----------FlexRAM 存储器----------- IOMUXC_GPR->GPR16 = --------" 它显示“MCU 已进入 Flash 加载器,但配置外部存储器失败,请 RESET 板并设置正确的引导设备,然后重试”。 我的 或非 Flash 是 W25Q32JV 四通道SPI。 请您在这件事上帮帮我。 谢谢! 纳根德拉 Re: IMXRT1176 Application Crashed , Later IMXRT doesnot boot 嗨@Gavin_Jia , 感谢您的回复。 1.我从内存运行示例,得到的 ID 为 0。 2. Flash 连接到 FlexSPI A FlexSPI1 信号 RT1176 球/焊盘名称 FLEXSPI1_A_SCLK GPIO_SD_B2_07 FLEXSPI1_A_DATA0 GPIO_SD_B2_08 FLEXSPI1_A_DATA1 GPIO_SD_B2_09 FLEXSPI1_A_DATA2 GPIO_SD_B2_10 FLEXSPI1_A_DATA3 GPIO_SD_B2_11 FLEXSPI1_A_SS0_B GPIO_SD_B1_06 这块板之前可以正常用于我们的应用程序,我曾用它按照 FlexSPI 示例程序,通过擦除和重新编程闪存,为我们的应用程序实现辅助引导加载程序。但在此期间,应用程序卡住了,从那以后我就无法再刷写闪存了。 Re: IMXRT1176 Application Crashed , Later IMXRT doesnot boot 你好@Nagendra_Kumar , 日志显示 MCU、ROM 和 Flashloader 都正常(HAB 打开,串行下载器连接)。故障发生在 FlexSPI 到 W25Q32JV 的初始化过程中:工具甚至无法读取 SFDP 参数,因此这是板/配置问题,而不是烧录工具的问题。由于新刷机也失败了,请按以下顺序检查: 首先从内部 RAM 运行 flexspi_nor_polling_transfer_cm7 示例,并读取 W25Q32JV 的 JEDEC ID。如果无法读取 ID,则确认存在硬件/引脚问题——暂时不要关注刷机工具。 确认闪存位于哪个 FlexSPI 实例/引脚组上。默认的 .cfx 文件MCUBootUtility 假定 FlexSPI1 端口 A(EVK 接线)。如果您的 FlexSPI2 或 FlexSPI1 是辅助接口,请修改 option0 中的引脚组字段,并烧录 FLEXSPI_PIN_GROUP_SEL 熔丝(地址 0x9A0[10]);在 MCUBootUtility 中显式选择匹配的实例。 建议使用安全配置工具 (SPT) ,它内置了 W25Q 系列的 FCB 模板和启动内存配置功能,以便首先验证设置。 另外,请确认:这块板之前是否曾通过W25Q32JV成功编程和启动过? 此致, 加文 Re: IMXRT1176 Application Crashed , Later IMXRT doesnot boot 您好, 我忘了说,我还把 或非 闪存换成了新的。错误依然存在。 Re: IMXRT1176 Application Crashed , Later IMXRT doesnot boot 你好@Nagendra_Kumar , 谢谢你的更新! 我发现表格显示: FLEXSPI1_A_SS0_B GPIO_SD_B1_06 应该是 GPIO_SD_B2_06。这是笔误还是实际连接状态?RAM 代码返回的 JEDEC ID 为 0,表明闪存硬件完全没有响应。因此,如果您的连接正确,则应检查硬件连接和电源,并使用示波器检查波形。 此致, 加文 Re: IMXRT1176 Application Crashed , Later IMXRT doesnot boot 嗨@Gavin_Jia , FLEXSPI1_A_SS0_B GPIO_SD_B1_06 GPIO_SD_B1_06 是拼写错误。对此我深感抱歉。实际上它只连接到GPIO_SD_B2_06 。我用示波器检查了表格中的 FLEXSPI 引脚,发现这些引脚上没有任何活动。 此外,当我从 RAM 运行您提到的示例时,SS0_B 信号始终为低电平。我有多个相同类型的板,但在正常工作的板上,我得到的 ID 却是 0xEF。这个问题具体出现在我测试辅助引导加载程序实现的一块电路板上,当时电路板死机了。我不明白软件/应用程序崩溃怎么会导致这种行为,我也不知道是否应该用其他开发板来测试该软件。很遗憾,我无法提供我编写的代码。为了让您有个概念,我使用 SDK 中的 FreeRTOS 示例编写了我的应用程序,并构建了我的应用程序,然后使用 flexspi 轮询示例来实现辅助引导加载程序!我使用了 2 个 LPSPI(采用 DMA)、2 个 UART(采用 DMA)和 2 个 CAN。这是一个小型应用程序。我使用的是SDK版本2.8.1。 期待您的回复。 纳根德拉·库马尔。
View full article