2411826_ja-JP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2411826_ja-JP

2411826_ja-JP

FRDM-IMX95のサスペンド時の消費電力を可能な限り低く抑える

FRDM-IMX95ボードでサスペンドモード時の消費電力を可能な限り低く抑える方法についてのガイダンスをお探しですか?ベアメタルm7コードを使用し、a55sをオフにすることで、約2.2Wまで消費電力を下げることができました。これは、エキスパンダー/PHY/PD_NETC の電源を完全に切った後の状態です。FRDM-IMX95はどのくらい低く設定できるのでしょうか?

FRDMトレーニングRe: Lowest possible SUSPEND power consumption of FRDM-IMX95

最新の調査結果を自分の投稿に追記します…EXT_5V0とEXT_3V3_PWR_ENをオフにしてみましたが、それ以上の改善は見られませんでした。次にDDRセルフリフレッシュをテストしたところ、約193mA/1.1Wまで下げることができました。できればもっと値下げしたいのですが…。

Re: Lowest possible SUSPEND power consumption of FRDM-IMX95

当社の i.MX 95消費電力測定を参照し、参照できる低消費電力のユースケースが多数あります。

i.MX 95の消費電力測定

Re: Lowest possible SUSPEND power consumption of FRDM-IMX95

これ閉めていいよ。低電力モードをすべて確実にテストでき、必要な結果を得ることができました。

Tags (1)
No ratings
Version history
Last update:
4 weeks ago
Updated by: