Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
RT1051: ENET IEEE1588タイマークロックソース こんにちは、 RT1050 の リファレンス マニュアル には 以下の 情報 があります: mastupristi_0-1789736651417.png IEEE1588タイマーのクロックソースが何なのか知りたいです。例えば、AUDIO_PLLから派生したルートクロックを選べますか? IEEE1588タイマーのクロックソースを制御するレジスタはどれですか? よろしくお願いいたします 最大 i.MXRT 105x Re: RT1051: ENET IEEE1588 Timer Clock source 私の知る限り、このタイマーは「ENET_25M_REF_CLK」とラベル付けされたクロック(MCUXpressoの設定ツールより)でクロックされており、常に25MHzです。「ネットワーク速度に関係なく」というのは、イーサネットが10Mbpsで動作しているときに速度が遅くならないという意味だと思います。 追伸もし1588タイマーの比較・キャプチャ機能を使う予定なら、これはRT1050で正しく使うのが最も難しいペリフェラルの一つであり、注意すべき多くの落とし穴があることを覚えておいてください。例えば、イベントインnとイベントアウトのnピンを同時に使うことはできません(ここでnは0..3です)。例えば、Event Out 1とEvent In 1を同時に使うことはできませんが、Event In 1とEvent Out 0を同時に使うことは可能です。また、4チャネルのうちDMAサポートは2つだけです。
View full article
S32K314编程错误 您好 当我通过debug尝试往DFLASH中写数据时失败了 下面是我的代码大概流程 write 0xFFFFF800 to 0x40268350   wtire 0x10000000 to PFCPGM_PEARR_L register write 0xFFFFFFFF to Program DATA0 set MCR[ERS] to 1   MCR[ERS] choose sector set MCR[EHV] to 1 wait MCRS[DONE] be 1 check MCRS[PEG] set MCR[EHV] to 0  SETMCR[ERS]to 0 after erase 11 sectors wtire 0x10000000 to PFCPGM_PEARR_L register write 256 bit data to DATA0~DATA7 set MCR[PGM] to 1  set MCR[EHV] to 1 read MCRS register get 0x0000C100 但是当我第二次循环 wtire 0x10000000 to PFCPGM_PEARR_L register write 256 bit data to DATA0~DATA7 set MCR[PGM] to 1  set MCR[EHV] to 1 read MCRS register get 0x00008100 我想知道这种情况可能会是什么原因造成的 Lika 回复: S32K314编程错误 补充一下,在我确认擦除/编程完成后我采取了下面步骤 set 0 to MCR[EHV] set 0 to MCR[PGM/ERS]
View full article
RT1xxx ENET: Does Correction Counter reset when writing ATCOR to change the Wrap-Around value? Hi, I wonder if the Correction Counter (in the ENET peripheral) is reset upon a write of ATCOR. Or maybe it is reset only if the value in ATCOR is changed? best regards Max i.MXRT 102x i.MXRT 105x Re: RT1xxx ENET: Does Correction Counter reset when writing ATCOR to change the Wrap-Around value? Hello @mastupristi,  When the ATCOR value is updated, the new value does not take effect immediately, it still uses the old value for one correction period. The updated ATCOR value is applied only after the correction counter resets, and a new correction period begins. BR Habib
View full article
S32K314 programming error Hello When I tried to write data to the DFLASH using debug mode, it failed. Below is a rough outline of my code. write 0xFFFFF800 to 0x40268350 wtire 0x10000000 to PFCPGM_PEARR_L register write 0xFFFFFFFF to Program DATA0 set MCR[ERS] to 1 MCR[ERS] choose sector Set MCR[EHV] to 1 wait MCRS[DONE] be 1 check MCRS[PEG] set MCR[EHV] to 0 SETMCR[ERS]to 0 after erase 11 sectors wtire 0x10000000 to PFCPGM_PEARR_L register write 256 bit data to DATA0~DATA7 set MCR[PGM] to 1 set MCR[EHV] to 1 read MCRS register get 0x0000C100 But when I looped for the second time wtire 0x10000000 to PFCPGM_PEARR_L register write 256 bit data to DATA0~DATA7 set MCR[PGM] to 1 set MCR[EHV] to 1 read MCRS register get 0x00008100 I'd like to know what might be causing this situation. Lika 回复: S32K314编程错误 To add to that, after confirming that the erase/programming was complete, I took the following steps. set 0 to MCR[EHV] set 0 to MCR[PGM/ERS]
View full article
RT1051: ENET IEEE1588 Timer Clock source Hi, In the RT1050 reference manual, I find the following: mastupristi_0-1789736651417.png I would like to know what the clock sources for the IEEE1588 timer can be. For example, can I choose a root clock derived from AUDIO_PLL? Which registers control the clock source of the IEEE1588 timer? best regards Max i.MXRT 105x Re: RT1051: ENET IEEE1588 Timer Clock source As far as I am aware, this timer is clocked by the clock labeled "ENET_25M_REF_CLK" (from MCUXpresso Config Tools), and it is always 25MHz. I think that by "independently of network speed" they just mean that it doesn't get slower if Ethernet is running at 10Mbps. P.S. If you are planning on using the 1588 timer compare/capture feature, be aware that it is (IMO) one of the most difficult peripherals on RT1050 to use correctly and has a large amount of gotchas to watch out for. For instance, you cannot use the Event In n and Event Out n pins at the same time (where n is 0..3). For example, you cannot use Event Out 1 and Event In 1 at the same time, but you can use Event In 1 and Event Out 0 at the same time. Also, only two of the four channels have DMA support.
View full article
RT1xxx ENET:写入 ATCOR 以更改循环值时,校正计数器是否会重置? 您好, 我想知道在写入 ATCOR 时,校正计数器(在 ENET 外设中)是否会重置。 或者,也许只有当 ATCOR 中的值发生变化时才会重置? 顺祝商祺! 最大值 i.MX RT102x i.MX RT105x Re: RT1xxx ENET: Does Correction Counter reset when writing ATCOR to change the Wrap-Around value? 你好@mastupristi , 当 ATCOR 值更新时,新值不会立即生效,在一个校正周期内仍使用旧值。更新后的 ATCOR 值仅在校正计数器重置后,新的校正周期开始时才会应用。 BR 哈比卜
View full article
RT1051:ENET IEEE1588 定时器时钟源 您好, 在 RT1050 参考 手册 中 , 我 发现了 以下内容 : mastupristi_0-1789736651417.png 我想知道IEEE1588定时器的时钟源有哪些。例如,我可以选择从 AUDIO_PLL 派生的根时钟吗? 哪些寄存器控制 IEEE1588 定时器的时钟源? 顺祝商祺! 最大值 i.MX RT105x Re: RT1051: ENET IEEE1588 Timer Clock source 据我所知,这个定时器由标记为“ENET_25M_REF_CLK”(来自 MCUXpresso 配置工具)的时钟提供时钟信号,并且始终为 25MHz。我认为他们所说的“与网络速度无关”仅仅是指,如果以太网以 10Mbps 的速度运行,速度不会变慢。 附言如果您打算使用 1588 定时器比较/捕获功能,请注意,在我看来,它是 RT1050 上最难正确使用的外设之一,并且有很多陷阱需要注意。例如,你不能同时使用 Event In n 和 Event Out n 引脚(其中 n 为 0..3)。例如,你不能同时使用 Event Out 1 和 Event In 1,但你可以同时使用 Event In 1 和 Event Out 0。此外,四个通道中只有两个支持 DMA。
View full article
PN7160 NXP-NCI MCUxpresso for VS Code Example Project for MCXA156 Introduction This document provides a guide on how to integrate the FRDM-MCXA156 as a host for the PN7160 using the examples provided in the “PN7160 NXP-NCI MCUXpresso Example Project” package. The hardware required to follow this guide is: FRDM-MCXA156 development board as host MCU. OM27160A1/OM27160B1 (PN7160 EVK) as the NFC controller. MCUxpresso for VS code extension Software setup. PN7160 NXP-NCI MCUXpresso Example Project version: 1.2 MCXN947 SDK version: 26.06 PN7160 version: 12.50.11. Hardware connections. When using OM27160B1 (SPI Host Interface): The FRDM-MCXA156 schematic document is available on this page. In the case of SPI connections, to use PN7160 directly with the Arduino headers a rework is needed for the FRDM because SDO(MOSI) and SS (Chip select) are not connected as default (as shown in the next figure). You should move R59 and R60 from pad 2 to pad 3 to enable these connections. Habib_MS_0-1781809327131.png Note: You can connect the SPI pins available in Mikro bus header with jumpers, but in this example, the signals are routed through the pins enabled by the rework configuration. Once clarified this, these are the pins used in this example. Name PORT I2C0_SDA P0_16 I2C0_SCL P0_17 LPSPI1_SDI P2_16 LPSPI1_SDO P2_13 LPSPI1_SCK P2_12 LPSPI1_SS P2_6 IRQ P1_15 VEN P1_14 REQ P3_16   Software Changes This section describes the software changes required to run an “NXP-NCI2.0” example with the MCXA156, which consists in a detection loop that displays in a terminal information (like UID, SAK, and Product Type for MIFARE product-based cards) about any tag detected by the PN7160. To begin the integration, we first need to import a hello_world project from the FRDM-MCXA156 SDK (v26.06.00) into MCUXpresso IDE for VS Code. For this purpose, download and install the FRDM-MCXA156 repository (version 26.06) using the extension available in the Quickstart panel by selecting Import Repository. For more information about this process, you can consult the corresponding guide. Importing NCI2.0 examples Download the “PN7160 NXP-NCI MCUXpresso Example Project” zip from the product page and extract in a known folder. This will be useful for later use.  Importing base project 1. In the Quick Start panel click on “Import Example from Repository” in VS code. Habib_MS_1-1781809359168.png 2. Select “FRDM-MCXA156” in board setting.   Habib_MS_1-1785802139304.png 3. In the template will search for the “hello_world” example, select Freestanding Applications, chose the location and click on “import”. Habib_MS_0-1785802110562.png Importing SDK drivers Once the project is added to the workspace we will need to add the required drivers, which are the SPI driver in case the OM27160B1HN is being used, or the I2C driver if the OM27160A1HN is being used. For this we need to add the following code in the prj.cfg file. Habib_MS_0-1781809845396.png Spoiler (Highlight to read) CONFIG_MCUX_COMPONENT_driver.lpi2c=y CONFIG_MCUX_COMPONENT_driver.lpspi=y CONFIG_MCUX_COMPONENT_driver.lpi2c=y CONFIG_MCUX_COMPONENT_driver.lpspi=y Add the example source code to the newly created MCXA156 project Delete the hello_world.c of the project files folder of the MCXA156 project. From the “NXP-NCI2.0_iMXRT1170_examples” extracted just drag and drop in the project files folder the following files and folders. Habib_MS_0-1781809900813.png Habib_MS_1-1781809927413.png When you drag and drop a file into VS code a window will appear asking whether you want to link the file or copy it. Please select “Copy files.” Habib_MS_2-1781809983781.png The project folder should look like this: Habib_MS_3-1781810001861.png After dragging and dropping all the files, the CMakeLists.txt file is automatically updated to include all the copied .c files. An example of this is shown below: Habib_MS_4-1781810063910.png However, .h files are not automatically linked, so they must be added manually. Please copy and paste the following includes into the CMakeLists.txt file: Habib_MS_5-1781810096008.png Spoiler (Highlight to read) mcux_add_include( BASE_PATH ${CMAKE_CURRENT_LIST_DIR} INCLUDES tool TML NfcLibrary/inc NfcLibrary/NdefLibrary/inc INCLUDES NfcLibrary/NxpNci20/inc . ) mcux_add_include( BASE_PATH ${CMAKE_CURRENT_LIST_DIR} INCLUDES tool TML NfcLibrary/inc NfcLibrary/NdefLibrary/inc INCLUDES NfcLibrary/NxpNci20/inc . ) Preprocessor Interface macro Depending on the interface to be used to communicate with the PN7160, a preprocessor macro must be defined in the CMakelist.txt BOARD_NXPNCI_INTERFACE_SPI (For using SPI with OM27160B1) BOARD_NXPNCI_INTERFACE_I2C (For using I2C with OM27160A1) Additionally, it is necessary to add the macro called REMOVE_P2P_SUPPORT. Please make sure that this Macro is included. Spoiler (Highlight to read) mcux_add_macro( CC "BOARD_NXPNCI_INTERFACE_I2C=1\ REMOVE_P2P_SUPPORT=1") mcux_add_macro( CC "BOARD_NXPNCI_INTERFACE_I2C=1\ REMOVE_P2P_SUPPORT=1") Note: The following sections are exemplified using the SPI interface (BOARD_NXPNCI_INTERFACE_SPI macro). After making the modifications described below, the interface used by the example can be changed simply by setting the macro to BOARD_NXPNCI_INTERFACE_I2C. Board definitions In the board.h file we will add the following definitions in order to refer to the different peripherals and clocks to be used, you can find this file in the following path: {PrjRootDirPath}\ frdmmcxa156\frdmmcxa156\board.h Habib_MS_1-1781810404448.png Spoiler (Highlight to read) #ifdef BOARD_NXPNCI_INTERFACE_I2C #define BOARD_NXPNCI_I2C_CLOCK (CLOCK_GetLpi2cClkFreq(0U)) #define BOARD_NXPNCI_I2C_INSTANCE (LPI2C0) #define BOARD_NXPNCI_I2C_BAUDRATE (100000) #define BOARD_NXPNCI_I2C_ADDR (0x28) #endif #ifdef BOARD_NXPNCI_INTERFACE_SPI #define BOARD_NXPNCI_SPI_CLOCK (CLOCK_GetLpspiClkFreq(1U)) #define BOARD_NXPNCI_SPI_INSTANCE (LPSPI1) #define BOARD_NXPNCI_SPI_BAUDRATE (400000) #endif #define BOARD_NXPNCI_IRQ_PORT (GPIO1) #define BOARD_NXPNCI_VEN_PORT (GPIO1) #define BOARD_NXPNCI_DWL_PORT (GPIO3) #define BOARD_NXPNCI_IRQ_PIN (15U) #define BOARD_NXPNCI_VEN_PIN (14U) #define BOARD_NXPNCI_DWL_PIN (16U) #ifdef BOARD_NXPNCI_INTERFACE_I2C #define BOARD_NXPNCI_I2C_CLOCK (CLOCK_GetLpi2cClkFreq(0U)) #define BOARD_NXPNCI_I2C_INSTANCE (LPI2C0) #define BOARD_NXPNCI_I2C_BAUDRATE (100000) #define BOARD_NXPNCI_I2C_ADDR (0x28) #endif #ifdef BOARD_NXPNCI_INTERFACE_SPI #define BOARD_NXPNCI_SPI_CLOCK (CLOCK_GetLpspiClkFreq(1U)) #define BOARD_NXPNCI_SPI_INSTANCE (LPSPI1) #define BOARD_NXPNCI_SPI_BAUDRATE (400000) #endif #define BOARD_NXPNCI_IRQ_PORT (GPIO1) #define BOARD_NXPNCI_VEN_PORT (GPIO1) #define BOARD_NXPNCI_DWL_PORT (GPIO3) #define BOARD_NXPNCI_IRQ_PIN (15U) #define BOARD_NXPNCI_VEN_PIN (14U) #define BOARD_NXPNCI_DWL_PIN (16U) Code modifications to the TML component In the source tml.c source file the following modifications are made, you can find this file in the following path: {{PrjRootDirPath }>frdmmcxa156_hello_world\TML Habib_MS_2-1781810455046.png Spoiler (Highlight to read) static Status tml_Reset(void) { /* Set DWL_REQ low for NCI protocol */ GPIO_PortClear(BOARD_NXPNCI_DWL_PORT, 1U << BOARD_NXPNCI_DWL_PIN); GPIO_PortClear(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); Sleep(10); GPIO_PortSet(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); Sleep(10); return SUCCESS; } static Status tml_Reset(void) { /* Set DWL_REQ low for NCI protocol */ GPIO_PortClear(BOARD_NXPNCI_DWL_PORT, 1U << BOARD_NXPNCI_DWL_PIN); GPIO_PortClear(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); Sleep(10); GPIO_PortSet(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); Sleep(10); return SUCCESS; } Habib_MS_3-1781810501153.png Spoiler (Highlight to read) static void INTF_INIT(void) { lpspi_master_config_t masterConfig; LPSPI_MasterGetDefaultConfig(&masterConfig); masterConfig.baudRate = BOARD_NXPNCI_SPI_BAUDRATE; masterConfig.whichPcs = (lpspi_which_pcs_t) kLPSPI_Pcs1; masterXfer.configFlags = kLPSPI_MasterPcs1 | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap; LPSPI_MasterInit(BOARD_NXPNCI_SPI_INSTANCE, &masterConfig, BOARD_NXPNCI_SPI_CLOCK); } static void INTF_INIT(void) { lpspi_master_config_t masterConfig; LPSPI_MasterGetDefaultConfig(&masterConfig); masterConfig.baudRate = BOARD_NXPNCI_SPI_BAUDRATE; masterConfig.whichPcs = (lpspi_which_pcs_t) kLPSPI_Pcs1; masterXfer.configFlags = kLPSPI_MasterPcs1 | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap; LPSPI_MasterInit(BOARD_NXPNCI_SPI_INSTANCE, &masterConfig, BOARD_NXPNCI_SPI_CLOCK); } Habib_MS_4-1781810544149.png Spoiler (Highlight to read) static Status tml_Init(void) { gpio_pin_config_t in_config = {kGPIO_DigitalInput, 0}; gpio_pin_config_t out_config = {kGPIO_DigitalOutput, 0}; GPIO_PinInit(BOARD_NXPNCI_IRQ_PORT, BOARD_NXPNCI_IRQ_PIN, &in_config); GPIO_PinInit(BOARD_NXPNCI_VEN_PORT, BOARD_NXPNCI_VEN_PIN, &out_config); GPIO_PinInit(BOARD_NXPNCI_DWL_PORT, BOARD_NXPNCI_DWL_PIN, &out_config); INTF_INIT(); return SUCCESS; } static Status tml_DeInit(void) { GPIO_PortClear(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); return SUCCESS; } static Status tml_Init(void) { gpio_pin_config_t in_config = {kGPIO_DigitalInput, 0}; gpio_pin_config_t out_config = {kGPIO_DigitalOutput, 0}; GPIO_PinInit(BOARD_NXPNCI_IRQ_PORT, BOARD_NXPNCI_IRQ_PIN, &in_config); GPIO_PinInit(BOARD_NXPNCI_VEN_PORT, BOARD_NXPNCI_VEN_PIN, &out_config); GPIO_PinInit(BOARD_NXPNCI_DWL_PORT, BOARD_NXPNCI_DWL_PIN, &out_config); INTF_INIT(); return SUCCESS; } static Status tml_DeInit(void) { GPIO_PortClear(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); return SUCCESS; } Code modifications for ports, pins and clocks initialization In the file “hardware_init.c” in the board folder of the project, write the following function as shown, in order to add port and clock peripheral initializations. Habib_MS_5-1781810589344.png Spoiler (Highlight to read) /* * Copyright 2024 NXP * * SPDX-License-Identifier: BSD-3-Clause */ /*${header:start}*/ #include "pin_mux.h" #include "fsl_clock.h" #include "fsl_reset.h" #include "board.h" #include /*${header:end}*/ /*${function:start}*/ void BOARD_InitHardware(void) { CLOCK_SetClockDiv(kCLOCK_DivLPI2C0, 1u); CLOCK_AttachClk(kFRO12M_to_LPI2C0); CLOCK_SetClockDiv(kCLOCK_DivLPSPI1, 1u); CLOCK_AttachClk(kFRO12M_to_LPSPI1); BOARD_InitPins(); BOARD_InitBootClocks(); BOARD_InitDebugConsole(); } /*${function:end}*/ /* * Copyright 2024 NXP * * SPDX-License-Identifier: BSD-3-Clause */ /*${header:start}*/ #include "pin_mux.h" #include "fsl_clock.h" #include "fsl_reset.h" #include "board.h" #include /*${header:end}*/ /*${function:start}*/ void BOARD_InitHardware(void) { CLOCK_SetClockDiv(kCLOCK_DivLPI2C0, 1u); CLOCK_AttachClk(kFRO12M_to_LPI2C0); CLOCK_SetClockDiv(kCLOCK_DivLPSPI1, 1u); CLOCK_AttachClk(kFRO12M_to_LPSPI1); BOARD_InitPins(); BOARD_InitBootClocks(); BOARD_InitDebugConsole(); } /*${function:end}*/ In the pin_mux.c file modifies the function called BOARD_InitPins(); accordingly, this file can be seen in the following path: {PrjRootDirPath}\ frdmmcxa156\hello_world \pin_mux.c Spoiler (Highlight to read) void BOARD_InitPins(void) { CLOCK_EnableClock(kCLOCK_GateGPIO1); /* GPIO3: Peripheral clock is enabled */ CLOCK_EnableClock(kCLOCK_GateGPIO3); /* PORT0: Peripheral clock is enabled */ CLOCK_EnableClock(kCLOCK_GatePORT0); CLOCK_EnableClock(kCLOCK_GatePORT1); CLOCK_EnableClock(kCLOCK_GatePORT2); CLOCK_EnableClock(kCLOCK_GatePORT3); /* GPIO1 peripheral is released from reset */ RESET_ReleasePeripheralReset(kGPIO1_RST_SHIFT_RSTn); /* GPIO3 peripheral is released from reset */ RESET_ReleasePeripheralReset(kGPIO3_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kLPUART0_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT0_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kLPSPI0_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT1_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kLPSPI1_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT3_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT2_RST_SHIFT_RSTn); const port_pin_config_t port0_2_pin78_config = {/* Internal pull-up resistor is enabled */ kPORT_PullUp, /* Low internal pull resistor value is selected. */ kPORT_LowPullResistor, /* Fast slew rate is configured */ kPORT_FastSlewRate, /* Passive input filter is disabled */ kPORT_PassiveFilterDisable, /* Open drain output is disabled */ kPORT_OpenDrainDisable, /* Low drive strength is configured */ kPORT_LowDriveStrength, /* Normal drive strength is configured */ kPORT_NormalDriveStrength, /* Pin is configured as LPUART0_RXD */ kPORT_MuxAlt2, /* Digital input enabled */ kPORT_InputBufferEnable, /* Digital input is not inverted */ kPORT_InputNormal, /* Pin Control Register fields [15:0] are not locked */ kPORT_UnlockRegister}; /* PORT0_2 (pin 78) is configured as LPUART0_RXD */ PORT_SetPinConfig(PORT0, 2U, &port0_2_pin78_config); const port_pin_config_t port0_3_pin79_config = {/* Internal pull-up resistor is enabled */ kPORT_PullUp, /* Low internal pull resistor value is selected. */ kPORT_LowPullResistor, /* Fast slew rate is configured */ kPORT_FastSlewRate, /* Passive input filter is disabled */ kPORT_PassiveFilterDisable, /* Open drain output is disabled */ kPORT_OpenDrainDisable, /* Low drive strength is configured */ kPORT_LowDriveStrength, /* Normal drive strength is configured */ kPORT_NormalDriveStrength, /* Pin is configured as LPUART0_TXD */ kPORT_MuxAlt2, /* Digital input enabled */ kPORT_InputBufferEnable, /* Digital input is not inverted */ kPORT_InputNormal, /* Pin Control Register fields [15:0] are not locked */ kPORT_UnlockRegister}; /* PORT0_3 (pin 79) is configured as LPUART0_TXD */ PORT_SetPinConfig(PORT0, 3U, &port0_3_pin79_config); const port_pin_config_t port2_13_pin35_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as LPSPI1_SDO */ kPORT_MuxAlt2, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT2, 13U, &port2_13_pin35_config); const port_pin_config_t port2_12_pin34_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as LPSPI1_SCK */ kPORT_MuxAlt2, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT2, 12U, &port2_12_pin34_config); const port_pin_config_t port2_16_pin37_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as LPSPI1_SDI */ kPORT_MuxAlt2, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT2, 16U, &port2_16_pin37_config); const port_pin_config_t port2_6_pin28_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as LPSPI1_PCS0 */ kPORT_MuxAlt2, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT2, 6U, &port2_6_pin28_config); const port_pin_config_t port1_15_pin8_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as GPIO1 15 */ kPORT_MuxAlt0, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT1, 15U, &port1_15_pin8_config); const port_pin_config_t port1_14_pin7_config = { kPORT_PullUp, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as GPIO1 14 */ kPORT_MuxAlt0, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT1, 14U, &port1_14_pin7_config); const port_pin_config_t port3_16_pin59_config = { kPORT_PullUp, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as GPIO3 16 */ kPORT_MuxAlt0, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT3, 16U, &port3_16_pin59_config); const port_pin_config_t port0_16_pin83_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as LPI2C0 SDA */ kPORT_MuxAlt2, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT0, 16U, &port0_16_pin83_config); const port_pin_config_t port0_17_pin84_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as LPI2C0 SCL */ kPORT_MuxAlt2, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT0, 17U, &port0_17_pin84_config); } void BOARD_InitPins(void) { CLOCK_EnableClock(kCLOCK_GateGPIO1); /* GPIO3: Peripheral clock is enabled */ CLOCK_EnableClock(kCLOCK_GateGPIO3); /* PORT0: Peripheral clock is enabled */ CLOCK_EnableClock(kCLOCK_GatePORT0); CLOCK_EnableClock(kCLOCK_GatePORT1); CLOCK_EnableClock(kCLOCK_GatePORT2); CLOCK_EnableClock(kCLOCK_GatePORT3); /* GPIO1 peripheral is released from reset */ RESET_ReleasePeripheralReset(kGPIO1_RST_SHIFT_RSTn); /* GPIO3 peripheral is released from reset */ RESET_ReleasePeripheralReset(kGPIO3_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kLPUART0_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT0_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kLPSPI0_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT1_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kLPSPI1_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT3_RST_SHIFT_RSTn); RESET_ReleasePeripheralReset(kPORT2_RST_SHIFT_RSTn); const port_pin_config_t port0_2_pin78_config = {/* Internal pull-up resistor is enabled */ kPORT_PullUp, /* Low internal pull resistor value is selected. */ kPORT_LowPullResistor, /* Fast slew rate is configured */ kPORT_FastSlewRate, /* Passive input filter is disabled */ kPORT_PassiveFilterDisable, /* Open drain output is disabled */ kPORT_OpenDrainDisable, /* Low drive strength is configured */ kPORT_LowDriveStrength, /* Normal drive strength is configured */ kPORT_NormalDriveStrength, /* Pin is configured as LPUART0_RXD */ kPORT_MuxAlt2, /* Digital input enabled */ kPORT_InputBufferEnable, /* Digital input is not inverted */ kPORT_InputNormal, /* Pin Control Register fields [15:0] are not locked */ kPORT_UnlockRegister}; /* PORT0_2 (pin 78) is configured as LPUART0_RXD */ PORT_SetPinConfig(PORT0, 2U, &port0_2_pin78_config); const port_pin_config_t port0_3_pin79_config = {/* Internal pull-up resistor is enabled */ kPORT_PullUp, /* Low internal pull resistor value is selected. */ kPORT_LowPullResistor, /* Fast slew rate is configured */ kPORT_FastSlewRate, /* Passive input filter is disabled */ kPORT_PassiveFilterDisable, /* Open drain output is disabled */ kPORT_OpenDrainDisable, /* Low drive strength is configured */ kPORT_LowDriveStrength, /* Normal drive strength is configured */ kPORT_NormalDriveStrength, /* Pin is configured as LPUART0_TXD */ kPORT_MuxAlt2, /* Digital input enabled */ kPORT_InputBufferEnable, /* Digital input is not inverted */ kPORT_InputNormal, /* Pin Control Register fields [15:0] are not locked */ kPORT_UnlockRegister}; /* PORT0_3 (pin 79) is configured as LPUART0_TXD */ PORT_SetPinConfig(PORT0, 3U, &port0_3_pin79_config); const port_pin_config_t port2_13_pin35_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as LPSPI1_SDO */ kPORT_MuxAlt2, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT2, 13U, &port2_13_pin35_config); const port_pin_config_t port2_12_pin34_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as LPSPI1_SCK */ kPORT_MuxAlt2, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT2, 12U, &port2_12_pin34_config); const port_pin_config_t port2_16_pin37_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as LPSPI1_SDI */ kPORT_MuxAlt2, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT2, 16U, &port2_16_pin37_config); const port_pin_config_t port2_6_pin28_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as LPSPI1_PCS0 */ kPORT_MuxAlt2, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT2, 6U, &port2_6_pin28_config); const port_pin_config_t port1_15_pin8_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as GPIO1 15 */ kPORT_MuxAlt0, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT1, 15U, &port1_15_pin8_config); const port_pin_config_t port1_14_pin7_config = { kPORT_PullUp, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as GPIO1 14 */ kPORT_MuxAlt0, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT1, 14U, &port1_14_pin7_config); const port_pin_config_t port3_16_pin59_config = { kPORT_PullUp, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as GPIO3 16 */ kPORT_MuxAlt0, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT3, 16U, &port3_16_pin59_config); const port_pin_config_t port0_16_pin83_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as LPI2C0 SDA */ kPORT_MuxAlt2, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT0, 16U, &port0_16_pin83_config); const port_pin_config_t port0_17_pin84_config = { kPORT_PullDisable, kPORT_LowPullResistor, kPORT_FastSlewRate, kPORT_PassiveFilterDisable, kPORT_OpenDrainDisable, kPORT_LowDriveStrength, kPORT_NormalDriveStrength, /* Pin is configured as LPI2C0 SCL */ kPORT_MuxAlt2, kPORT_InputBufferEnable, kPORT_InputNormal, kPORT_UnlockRegister}; PORT_SetPinConfig(PORT0, 17U, &port0_17_pin84_config); } Configure the main.c as follows: Habib_MS_0-1781813861103.png Spoiler (Highlight to read) #include #include #include "board.h" #include "app.h" #include "pin_mux.h" #include "fsl_debug_console.h" extern void nfc_example (void); int main(void) { BOARD_InitHardware(); #ifdef BOARD_NXPNCI_INTERFACE_I2C PRINTF("\nRunning the NXP-NCI2.0 example (I2C interface)\n"); #else PRINTF("\nRunning the NXP-NCI2.0 example (SPI interface)\n"); #endif nfc_example(); } #include #include #include "board.h" #include "app.h" #include "pin_mux.h" #include "fsl_debug_console.h" extern void nfc_example (void); int main(void) { BOARD_InitHardware(); #ifdef BOARD_NXPNCI_INTERFACE_I2C PRINTF("\nRunning the NXP-NCI2.0 example (I2C interface)\n"); #else PRINTF("\nRunning the NXP-NCI2.0 example (SPI interface)\n"); #endif nfc_example(); } Building and Debugging the example For building the example, please click on this button and if you followed this guide accordingly the project should compile without errors: Habib_MS_1-1781813991676.png Habib_MS_2-1781813999778.png Open a serial terminal such as Teraterm with the following settings: Habib_MS_3-1781814017721.png  Start a debug session by clicking this button: Habib_MS_4-1781814064724.png Once running, the example should look as follows: Habib_MS_5-1781814084057.png  When tapping a card on the antenna, the card information will be shown: Habib_MS_6-1781814110924.png NFC Controller Solutions
View full article
2026年美国领先的白标SEO专家 将客户的 SEO 工作交给外部合作伙伴,只有当该合作伙伴确实具备相应的技术实力时,才能奏效。广告公司需要的不仅仅是供应商,而是了解抓取预算、结构化数据、内容策略,以及日益重要的如何针对人工智能驱动的搜索进行优化的白标 SEO 专家,而不仅仅是承诺排名却没有明确方法论的公司。 本指南着眼于 2026 年为美国机构提供服务的领先白标 SEO 专家,特别评估他们的技术和战略能力的深度,而不仅仅是他们网站上列出的服务范围。 2026 年领先的白标 SEO 专家 1. 阿拉伯搜索引擎优化 Arab SEO 团队在技术 SEO、本地 SEO、电子商务 SEO、国际 SEO、AI SEO 和生成式引擎优化 (GEO) 方面拥有专家级的深度。真正的专家与普通供应商的区别在于方法论——Arab SEO 的多语言和人工智能驱动搜索方法建立在结构化、可重复的流程之上,而不是一次性的策略,这对于一家代理机构同时信任拥有数十个不同客户账户的合作伙伴来说至关重要。 2. SEO 通告 SEO Circular 的专家们专注于企业级技术 SEO——这类大型的、拥有数千页的网站,一个被忽视的抓取问题就可能抑制整个域的排名。其团队在国际和多语言 SEO 方面的经验也使其成为与跨国经营的客户合作的代理机构的有力选择。 3. 三重思维 Triple Minds 的团队以代理服务为核心,这意味着其专家完全专注于执行质量,而不是销售或客户获取——这在交付一致性方面是一个结构性优势。 4. 半化 Semify 的专家拥有多年构建可定制本地 SEO 活动的经验,其流程专门围绕帮助小型机构逐步扩展其 SEO 服务而构建。 5. SEOReseller SEOReseller 团队专注于提供全方位管理的服务,处理完整的 SEO 流程——技术、内容和链接——日常执行中几乎不需要代理机构的参与。 6. DashClicks DashClicks 将其 SEO 专家与专为报告和客户管理而构建的软件平台相结合,使代理机构能够通过自动化仪表板了解专家的工作情况。 7. 霍斯 HOTH 的专家们在完善的文档记录和标准化的方案框架内工作,使得机构能够轻松理解他们的流程,并向客户解释。 8. 增强能力 Boostability 团队在为大量小型客户提供一致的 SEO 质量方面积累了丰富的专业知识——这与管理少数大型企业客户所需的技能截然不同。 9. 销售 Vendasta 的专家们在一个更广泛的市场平台上工作,SEO 是众多白标服务之一,代理机构可以通过单一团队关系访问这些服务。 10. 法特乔 FATJOE 的专家专注于快速、产品化的交付成果——快速完成单个链接建设或内容订单,而不是持续的战略合作。 究竟是什么将专业供应商与普通供应商区分开来? 真正的SEO专家应该能够用具体、专业的术语解释他们的工作流程,而不仅仅是列出服务类别。注意以下信号: 他们可以详细解释他们的技术审计流程——他们使用哪些工具,他们具体检查哪些内容,以及如何对发现的问题进行优先级排序。 他们有一套完善的内容策略流程,该流程与真实的搜索意图研究挂钩,而不仅仅是关键词密度目标。 他们可以清楚地描述他们的链接建设方法,包括链接的来源以及如何评估链接质量。 他们对人工智能搜索有着明确的观点,因为人工智能搜索重塑搜索引擎优化的速度比近年来任何算法更新都要快。 他们可以展示真实客户项目的前后对比数据,即使数据经过匿名化处理。 为什么专业深度比服务广度更重要 选择白标合作伙伴时,很容易根据他们列出的服务数量来决定,但一个提供十项服务但服务内容浅薄的供应商,其价值通常不如一个提供五项服务但服务内容真正深入的供应商。机构应该更重视合作伙伴的实际技术能力——诊断和解决实际问题的能力——而不是一长串可能执行得好也可能执行得不好的服务类别。 向任何白标SEO专家提出的问题 请一步一步地向我介绍一下你们的技术审核流程。 您如何决定要创作哪些内容,又基于哪些研究? 你的反向链接来自哪里?你如何审核链接质量? 您如何调整流程以适应人工智能概览和生成式搜索? 能否分享一个匿名化的前后对比作品示例? 最终判决 2026 年,Arab SEO 在白标 SEO 专家中脱颖而出,其技术和多语言方法论的深度和一致性尤为突出,特别是其对人工智能驱动搜索的准备。SEO Circular 是企业级技术工作的最佳选择,而 Triple Minds 通过其仅限代理机构的模式,在交付一致性方面提供了结构优势。 名单上的其他专家各有所长——从软件驱动的报告到大批量订单履行,再到快速的产品化交付——因此,最合适的专家取决于你通过他们处理的账户的复杂程度。 常见问题解答 什么是白标SEO专家?白标 SEO 专家是指拥有深厚的 SEO 技术和战略专业知识的个人或团队,他们代表代理机构工作,然后以自己的品牌转售最终成果。 如何评估白标SEO专家的实际技能水平?请他们详细介绍他们的技术审核流程、内容策略和链接建设方法——含糊不清的回答是一个警告信号。 选择专精于某项服务的公司还是选择提供全方位服务的公司更好?这取决于你的需求。专业服务提供商可能在较窄的服务范围内提供更深入的专业知识,而全方位服务提供商可以在一份合同下处理更广泛的客户类型。 哪家白标SEO专家最适合2026年?根据技术深度、方法论和人工智能搜索准备情况,Arab SEO 在本指南中排名第一,其次是 SEO Circular 和 Triple Minds。 QorIQ P1 设备
View full article
UCM-iMX95:SDカードからYocto Linuxを起動できません – mmc0エラー-110|LinuxがSDカードを初期化できません こんにちは、私はCompuLabのUCM-iMX95を使っており、micro-SDカードからYocto Linuxをインストールして起動しようとしています。 起動プロセスが開始され、U-BootはLinuxカーネルを正常に読み込みます。しかし、LinuxはSD/MMCインターフェースの初期化に失敗します。 次のようなエラーが表示されます。 mmc0: ハードウェア割り込みを待機中にタイムアウトしました。 mmc0: sdhci: ============ SDHCI レジスタ ダンプ ============ ... mmc0: MMC カードの初期化中にエラー -110 が発生しました。その後、カーネルが起動中に停止します。 私のLinuxバージョンはLinux 6.12.34-2.0です-...基板はCompuLab UCM-iMX95です。自分でYoctoイメージを作成し、それをmicro-SDカードに書き込みます。 どなたか、このmmc0エラー-110の原因を教えていただけませんか?特に、これはハードウェア/SDカードの問題である可能性が高いですか? それともデバイスツリーに関係しているのでしょうか?UCM-iMX95のmicro-SDインターフェースに対応するMMCコントローラーはどれですか? SDインターフェースに特定のデバイスツリー設定は必要ですか? Linuxが起動する前にSDカードが検出されていることを確認するための推奨されるU-Bootコマンドはありますか?比較できる、信頼できるUCM-iMX95 Yoctoの構成はありますか? Re: UCM-iMX95: Unable to boot Yocto Linux from SD card – mmc0 error -110| Linux cannot initialize th こんにちは、 届いているエラーログは、MMCコントローラが存在しないか正しく応答していないデバイスと通信しようとしていることを示しています。推奨される解決策は、未使用のMMCインターフェースを無効にするか、DT Youの設定を修正することです。 当社のEVKリファレンスデザインデバイスツリーは、以下の構成を使用しています。 mmc0 usdhc1 eMMC mmc1 usdhc2 SD card 当社のデバイスツリーを参考にしてください: https://github.com/nxp-imx/linux-imx/blob/lf-6.18.y/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts よろしくお願いいたします。
View full article
PIC CLB 上的 Eureka 某些 PIC MCU(例如 pic16f13145 系列)具有类似 FPGA 的可编程逻辑,称为可配置逻辑块。 我使用的 pic16f13115 有 32 个单元,每个单元都有一个 4 输入查找表和一个 D 触发器。 为了学习如何使用这些工具,今天我实现了对 6 个 LED 的 Charlieplexing 的 PWM 亮度控制支持,并进行了模拟。我使用 Verilog 来定义电路,而不是使用逻辑 CAD 画布。 我差不多有一半的时间都在用头撞墙。我慢慢地把 Verilog 代码写对了,让它能够综合(构建),然后让它能够仿真。 CLB 编程逻辑即使在 CPU 休眠状态下也能正常工作,这很棒。它非常适合功能安全至关重要的应用。例如,可用于实现复杂的触发信号逻辑。CLB 逻辑与外围输入输出的连接方式非常灵活。它比PIC单片机中一直使用的笨重的CLC可编程逻辑电路灵活得多。 概述 Re: Eureka on PIC CLB 这真是对 PIC16F13115 的 CLB 的一种非常有趣的用法!使用 Verilog 实现 6 个 LED 的 Charlieplexing 设置并配合 PWM,听起来像是学习工作流程的好方法,而且在 CPU 休眠时逻辑电路也能继续运行,这为低功耗和功能安全关键型设计开辟了一些令人印象深刻的可能性。 Re: Eureka on PIC CLB 你好, 看来该设备属于另一家制造商。 请问您能否协助我们联系贵公司制造商? 如果您有兴趣更换为带有可编程逻辑单元 (PLC) 的 NXP 设备,可以参考 LPC804。 LPC804 可编程逻辑单元 (PLU) 顺祝商祺!
View full article
i.MX8QXP – Prevent normal boot after interrupted USB flashing on Yocto Scarthgap with A/B partitions Hi NXP Team, The installed UUU executable reports: libuuu_1.5.21-0-g1f42172 We use: sudo uuu -b emmc_all ~/Downloads/flash.bin *.wic The built-in emmc_all script writes the complete .wic image using: FB: flash -raw2sparse all _image It then writes the bootloader, configures eMMC boot selection, and finishes with FB: done. The script contains no explicit persistent flash-in-progress completion metadata handling or readback hash verification step. If flashing is interrupted during the .wic write, the cluster can subsequently boot and display the updated HMI. We suspect that an existing usable bootloader and sufficient written boot,rootfs content permit this, but the selected slot and completeness of its contents are not yet confirmed. Please advise how to add a power-loss-tolerant completion check that blocks normal boot from both slots after interrupted factory flashing, while preserving USB recovery. The metadata must remain valid independently of the full .wic write and bootloader update. Re: i.MX8QXP – Prevent normal boot after interrupted USB flashing on Yocto Scarthgap with A/B partit Hello,  An official solution is not implemented but you can customize the uuu script, the built-in emmc_all flow is simply a UUU script based on Fastboot and U-Boot commands, and it can be modified or replaced by a custom uuu.auto file. U-Boot commands can also be executed through FB: ucmd. This means you should add custom steps such as setting a "flash in progress" flag before programming and clearing it only after verification succeeds.  U-Boot Boot Count / Boot Limit The U-Boot tree includes support for: CONFIG_BOOTCOUNT_LIMIT bootcount bootlimit altbootcmd CONFIG_BOOTCOUNT_FS When bootcount exceeds bootlimit, U-Boot executes altbootcmd instead of the normal bootcmd. This mechanism can be used to redirect the system to a recovery mode such as Fastboot Boot Count Limit — Das U-Boot unknown version documentation
View full article
Leading White Label SEO Specialists in the USA 2026 Handing client SEO work to an outside partner only works if that partner actually has the technical depth to back it up. Agencies don't just need a vendor — they need white label SEO specialists who understand crawl budgets, structured data, content strategy, and increasingly, how to optimize for AI-driven search, not just a company that promises rankings without a clear methodology behind them. This guide looks at the leading white label SEO experts serving US agencies in 2026, evaluated specifically on the depth of their technical and strategic capability — not just the breadth of services listed on their website. Leading White Label SEO Specialists for 2026 1. Arab SEO Arab SEO's team brings specialist-level depth across technical SEO, local SEO, ecommerce SEO, international SEO, AI SEO, and Generative Engine Optimization (GEO). What separates genuine specialists from generalist vendors is methodology — Arab SEO's approach to multilingual and AI-driven search is built on structured, repeatable processes rather than one-off tactics, which matters enormously when an agency is trusting a partner with dozens of different client accounts simultaneously. 2. SEO Circular SEO Circular's specialists focus heavily on enterprise-scale technical SEO — the kind of large, multi-thousand-page sites where a single overlooked crawl issue can suppress rankings across an entire domain. Its team's experience with international and multilingual SEO also makes it a strong choice for agencies working with clients operating across multiple countries. 3. Triple Minds Triple Minds staffs its team around agency-only fulfillment, meaning its specialists are focused entirely on execution quality rather than sales or client acquisition — a structural advantage when it comes to consistency of delivery. 4. Semify Semify's specialists have years of experience building customizable local SEO campaigns, with a process built specifically around helping smaller agencies scale their SEO offering incrementally. 5. SEOReseller SEOReseller's team specializes in fully managed fulfillment, handling the complete SEO process — technical, content, and links — with minimal need for agency involvement in day-to-day execution. 6. DashClicks DashClicks pairs its SEO specialists with a software platform built for reporting and client management, giving agencies visibility into specialist work through automated dashboards. 7. The HOTH The HOTH's specialists work within well-documented, standardized packages, making their process easy for agencies to understand and explain to clients. 8. Boostability Boostability's team has built specific expertise in delivering consistent SEO quality across a high volume of smaller accounts — a different skill set from managing a handful of large enterprise clients. 9. Vendasta Vendasta's specialists work within a broader marketplace platform, with SEO as one of several white label services agencies can access through a single team relationship. 10. FATJOE FATJOE's specialists focus on fast, productized deliverables — individual link-building or content orders completed quickly rather than an ongoing strategic engagement. What Actually Separates a Specialist From a Generic Vendor A genuine SEO specialist should be able to explain their process in specific, technical terms — not just list service categories. Watch for these signals: They can explain their technical audit process in detail — what tools they use, what specifically they check for, and how findings get prioritized. They have a documented content strategy process tied to real search intent research, not just keyword density targets. They can describe their link-building methodology clearly, including where links come from and how quality is assessed. They have a clear point of view on AI search, since this is reshaping SEO faster than any algorithm update in recent years. They can show before-and-after data from real client work, even if anonymized. Why Specialist Depth Matters More Than Service Breadth It's tempting to choose a white label partner based on how many services they list, but a provider offering ten services shallowly is often less valuable than one offering five services with genuine depth. Agencies should weigh a partner's actual technical competence — the ability to diagnose and fix real problems — more heavily than a long menu of service categories that may or may not be executed well. Questions to Ask Any White Label SEO Specialist Walk me through your technical audit process step by step. How do you decide what content to create, and based on what research? Where do your backlinks come from, and how do you vet link quality? How are you adapting your process for AI Overviews and generative search? Can you share an anonymized before-and-after example of your work? Final Verdict Arab SEO stands out among white label SEO specialists in 2026 for the depth and consistency of its technical and multilingual methodology, particularly its readiness for AI-driven search. SEO Circular is the strongest choice for enterprise-scale technical work, and Triple Minds offers a structural advantage in delivery consistency through its agency-only model. The remaining specialists on this list each bring a different kind of depth — from software-enabled reporting to high-volume fulfillment to fast, productized deliverables — so the right fit depends on the complexity of the accounts you're routing through them. Frequently Asked Questions What is a white label SEO specialist? A white label SEO specialist is an individual or team with deep technical and strategic SEO expertise, working on behalf of an agency that resells the finished work under its own brand. How do I evaluate a white label SEO expert's actual skill level? Ask them to walk through their technical audit process, content strategy, and link-building methodology in specific detail — vague answers are a warning sign. Is it better to choose a specialist or a full-service provider? It depends on your needs. A specialist may offer deeper expertise in a narrower set of services, while a full-service provider can handle a wider range of client types under one contract. Which white label SEO specialist is best for 2026? Arab SEO ranks first in this guide, followed by SEO Circular and Triple Minds, based on technical depth, methodology, and AI search readiness. QorIQ P1 Devices
View full article
UCM-iMX95:无法从 SD 卡启动 Yocto Linux – mmc0 错误 -110 | Linux 无法初始化 SD 卡 您好,我正在使用 CompuLab UCM-iMX95,并且我正在尝试从 micro-SD 卡安装和启动 Yocto Linux。 启动过程开始,U-Boot 成功加载 Linux 内核。但是,Linux 无法初始化 SD/MMC 接口。 我收到以下错误信息: mmc0:等待硬件中断超时。 mmc0: sdhci: ============ SDHCI 寄存器转储 ============= ... mmc0:初始化 MMC 卡时出错 -110,内核随后在启动过程中卡住。 我的Linux版本是:Linux 6.12.34-2.0-...板是:CompuLab UCM-iMX95。我正在构建自己的 Yocto 镜像并将其写入 micro-SD 卡。 请问有人能帮我理解一下导致 mmc0 错误 -110 的原因吗?具体来说:这是否可能是硬件/SD卡的问题? 或者这可能与设备树有关?UCM-iMX95 上的 micro-SD 接口对应哪个 MMC 控制器? SD接口是否需要特定的设备树设置? 是否有推荐的 U-Boot 命令可以在 Linux 启动前验证 SD 卡是否被检测到?是否有已知的、性能良好的 UCM-iMX95 Yocto 配置可供我参考,以便与我的配置进行比较? Re: UCM-iMX95: Unable to boot Yocto Linux from SD card – mmc0 error -110| Linux cannot initialize th 你好, 您收到的错误日志告诉我们,MMC 控制器正在尝试与一个不存在或未正常响应的设备进行通信。建议的解决方案是禁用未使用的 MMC 接口或修复 DT 配置。 我们的 EVK 参考设计设备树采用以下配置: mmc0 usdhc1 eMMC mmc1 usdhc2 SD card 您可以参考我们的设备树: https://github.com/nxp-imx/linux-imx/blob/lf-6.18.y/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts 顺祝商祺!
View full article
PIC CLBのユーレカ 特定のPIC MCU(例:pic16f13145ファミリ)には、Configurable Logic Blockと呼ばれるFPGA風のプログラム可能なロジックがあります。 私が使用しているpic16f13115は、それぞれ4入力ルックアップテーブルとDフリップフロップを備えた32個のセルで構成されています。 ツールの使い方を学ぶために、今日はPWM明るさ制御付き6つのLEDのチャーリープレックス対応を実装し、シミュレーションしました。ロジックCADキャンバスを使用する代わりに、Verilogを使用して回路を定義しました。 私は時間の半分くらいを壁に頭を打ち付けて過ごしていた。少しずつ、Verilogを正しく記述し、合成(ビルド)を行い、そしてシミュレーションを実行できるようにした。 CLBでプログラムされたロジックがCPUがスリープ状態でも動作するのは素晴らしい。セーフティに関わるアプリケーションに最適です。例えば、複雑な割り込みトリガーロジックの実装に利用できます。CLBロジックをペリフェラルに接続する際の柔軟性は非常に高いです。これは、PICの定番となっている、扱いにくいCLCプログラマブルロジックよりもはるかに柔軟性が高い。 全般 Re: Eureka on PIC CLB PIC16F13115のCLBの非常に興味深い使い方ですね!6LEDのチャーリープレックスセットアップにVerilogを使うのはPWMでワークフローを学ぶのに最適で、CPUがスリープ中でもロジックを動作させ続けることで、低消費電力でセーフティに関わるデザインに素晴らしい可能性が開けます。 Re: Eureka on PIC CLB こんにちは、 問題の機器は別のメーカーのものであるようだ。 メーカーへの連絡を手伝ってもらえますか? プログラマブルロジックユニット付きのNXPデバイスへの切り替えに興味がある場合は、LPC804に相談してください LPC804プログラマブルロジックユニット(PLU) よろしくお願いいたします。
View full article
アメリカのトップホワイトラベルSEOスペシャリスト 2026 クライアントのSEO業務を外部パートナーに委託する場合、そのパートナーが実際にそれを裏付けるだけの技術的な能力を備えている場合にのみ有効となる。エージェンシーには単なるベンダーだけでなく、クロール予算、構造化データ、コンテンツ戦略、そしてますますAI駆動型検索の最適化方法を理解しているホワイトラベルSEOスペシャリストが必要です。明確な方法論のないランキングを約束する企業ではなく。 このガイドでは、2026年に米国の代理店にサービスを提供する主要なホワイトラベルSEO専門家を、ウェブサイトに掲載されているサービスの幅だけでなく、技術的かつ戦略的な能力の深さに基づいて評価します。 2026年のホワイトラベルSEOスペシャリスト 1. アラブSEO Arab SEOのチームは、技術的SEO、ローカルSEO、eコマースSEO、国際SEO、AI SEO、生成エンジン最適化(GEO)にわたり専門的な深みを持っています。本物の専門家とジェネラリストベンダーを分けるのは方法論です。アラブSEOの多言語かつAI駆動の検索アプローチは、一度きりの手法ではなく構造的で繰り返し可能なプロセスに基づいており、代理店が同時に数十の異なるクライアントアカウントをパートナーに託す際には非常に重要です。 2. SEOサーキュラー SEOサーキュラーの専門家は、エンタープライズ規模の技術SEOに重点を置いています。これは、単一のクロール問題が見落とされがちな大規模な数千ページ規模のサイトで、ドメイン全体のランキングを抑制する可能性があることです。同社チームは国際的な多言語SEOに関する豊富な経験を有しているため、複数の国で事業を展開するクライアントを抱える代理店にとって有力な選択肢となる。 3. トリプル・マインド Triple Mindsは代理店限定のフルフィルメントを中心にチームを配置しており、スペシャリストは営業や顧客獲得ではなく、実行の品質に専念しています。これは一貫性のある提供において構造的な優位性です。 4. セミファイ Semifyの専門家は、カスタマイズ可能なローカルSEOキャンペーンの構築において長年の経験を持ち、特に小規模な代理店がSEOサービスを段階的に拡大できるよう支援することに特化したプロセスを構築しています。 5. SEOReseller SEOResellerのチームは、完全管理型のサービス提供を専門としており、テクニカルSEO、コンテンツSEO、リンクSEOといったSEOプロセス全体を、日々の運用における代理店の関与を最小限に抑えながら処理します。 6. ダッシュクリック DashClicksは、SEOスペシャリストとレポートおよびクライアント管理のためのソフトウェアプラットフォームを組み合わせ、自動化されたダッシュボードを通じて専門的な業務を企業に可視化します。 7. ホス HOTHの専門家は、よく文書化された標準化されたパッケージ内で業務を行い、代理店がクライアントに理解し説明しやすいプロセスとなっています。 8. ブースト性 Boostabilityのチームは、多数の小規模アカウントに対して一貫したSEO品質を提供する専門知識を築いており、これは少数の大企業クライアントを管理するスキルセットとは異なります。 9. ヴェンダスタ Vendastaの専門家は、より広範なマーケットプレイスプラットフォーム内で活動しており、SEOは、代理店が単一のチームとの関係を通じてアクセスできる複数のホワイトラベルサービスの1つです。 10. ファットジョー FATJOEの専門家は、継続的な戦略的エンゲージメントではなく、迅速かつ商品化された成果物、つまり個別のリンク構築やコンテンツ注文を迅速に完了させることに注力しています。 専門家と一般的なベンダーを実際に区別するものは何か 真のSEOスペシャリストであれば、単にサービスの種類を羅列するのではなく、具体的な技術用語を用いて自身のプロセスを説明できるはずだ。以下の兆候に注意してください。 彼らは技術監査のプロセスを詳細に説明できます。使用するツール、具体的にチェックする点、そして結果の優先順位付け方法などです。 彼らはキーワード密度の目標だけでなく、実際の検索意図調査に結びついた文書化されたコンテンツ戦略プロセスを持っています。 リンク構築の手法を明確に説明し、リンクの出所や品質の評価方法などを説明できます。 彼らはAI検索に対して明確な見解を持っており、近年のどのアルゴリズム更新よりも速くSEOを変革しています。 匿名化されていても、実際のクライアント作業のビフォーアフターデータを見せることができます。 なぜ専門職の深さがサービスの幅広さよりもマターなのか サービス数を挙げているだけでホワイトラベルパートナーを選ぶ誘惑はありますが、浅い10のサービスを提供するプロバイダは、5つの深みのあるサービスを提供するプロバイダよりも価値が低いことが多いです。各機関は、パートナーの実際の技術的能力、つまり実際の問題を診断し解決する能力を、実行が適切かどうかわからない多数のサービス項目よりも重視すべきである。 ホワイトラベルSEOスペシャリストに尋ねるべき質問 技術監査のプロセスをステップごとに説明してください。 どのようなコンテンツを作成するかは、どのように決定し、どのような調査に基づいて決定するのですか? バックリンクはどこから来て、リンクの品質はどのように審査していますか? AIオーバービューや生成検索のためにどのようにプロセスを適応させていますか? あなたの作品の匿名化ビフォーアフターの例を教えてもらえますか? 最終評決 アラブSEOは、2026年のホワイトラベルSEOスペシャリストの中で、技術的かつ多言語手法の深さと一貫性、特にAI駆動検索への対応力で際立っています。SEOサーキュラーは企業規模の技術業務に最適な選択肢であり、Triple Mindsは代理店限定モデルを通じて一貫性の構造的優位性を提供します。 このリストの残りの専門家は、それぞれソフトウェア対応の報告から大量のフルフィルメント、迅速な製品化された成果物まで、異なる深みを持っています。したがって、最適な適合は彼らを通じてルーティングするアカウントの複雑さによります。 よくある質問 ホワイトラベルSEOスペシャリストとは何でしょうか?ホワイトラベルSEOスペシャリストとは、深い技術的かつ戦略的なSEOの専門知識を持つ個人またはチームであり、完成品を自社ブランドで再販する代理店のために働くことです。 ホワイトラベルSEOの専門家の実際のスキルレベルをどう評価すればいいのでしょうか?技術監査プロセス、コンテンツ戦略、リンクビルディング手法を具体的に説明してもらいましょう。曖昧な回答は警告サインです。 専門医とフルサービスのどちらを選ぶべきでしょうか?それはあなたのニーズによります。スペシャリストはより狭いサービスの範囲でより深い専門知識を提供する一方で、フルサービスプロバイダーは1つの契約でより幅広い顧客タイプを扱うことができます。 2026年に最適なホワイトラベルSEOスペシャリストはどこですか?このガイドではアラブSEOが1位にランクされ、その後に技術的な深さ、手法論、AI検索準備度に基づくSEOサーキュラーとトリプルマインドが続きます。 QorIQ P1デバイス
View full article
UCM-iMX95: Unable to boot Yocto Linux from SD card – mmc0 error -110| Linux cannot initialize the SD Hi, I am using a CompuLab UCM-iMX95 and I am trying to install and boot Yocto Linux from a micro-SD card. The boot process starts, and U-Boot successfully loads the Linux kernel. However, Linux fails to initialize the SD/MMC interface. I get the following error: mmc0: Timeout waiting for hardware interrupt. mmc0: sdhci: ============ SDHCI REGISTER DUMP ============ ... mmc0: error -110 whilst initialising MMC card The kernel then gets stuck during boot. My Linux version is: Linux 6.12.34-2.0-... The board is: CompuLab UCM-iMX95 I am building my own Yocto image and writing it to a micro-SD card. Could someone please help me understand what could be causing this mmc0 error -110? In particular: Is this likely to be a hardware/SD-card issue, or could it be related to the device tree? Which MMC controller corresponds to the micro-SD interface on the UCM-iMX95? Are there any specific device-tree settings required for the SD interface? Is there a recommended U-Boot command to verify that the SD card is detected before Linux boots? Is there a known-good UCM-iMX95 Yocto configuration that I can compare my configuration against? Re: UCM-iMX95: Unable to boot Yocto Linux from SD card – mmc0 error -110| Linux cannot initialize th Hello, The error log you are getting tell us that the MMC controller is attempting to communicate with a device that either wasn't present or wasn't responding properly. The recommended solution is to disable the unused MMC interfaces or fix the DT you configuration. Our EVK reference design device tree uses the next configuration: mmc0 usdhc1 eMMC mmc1 usdhc2 SD card You can use our device tree as reference: https://github.com/nxp-imx/linux-imx/blob/lf-6.18.y/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts Best regards.
View full article
i.MX8QXP – 防止在 Yocto Scarthgap 系统上使用 A/B 分区时,USB 刷写中断后无法正常启动 您好,NXP团队: 已安装的 UUU 可执行文件报告: libuuu_1.5.21-0-g1f42172 我们使用: sudo uuu -b emmc_all ~/Downloads/flash.bin *.wic 内置的 emmc_all 脚本使用以下命令写入完整的 .wic 镜像: FB:flash -raw2sparse 所有_image 然后写入引导加载程序,配置 eMMC 引导选择,最后显示 FB: done。 该脚本不包含显式的持久性闪存进行中完成元数据处理或回读哈希验证步骤。 如果在 .wic 期间闪光灯闪烁中断写入后,集群即可启动并显示更新后的 HMI。我们怀疑现有的可用引导加载程序和足够的已写入启动、根文件系统内容允许这样做,但所选插槽及其内容的完整性尚未得到确认。 请问如何添加一个断电容错完成检查,在工厂刷机中断后阻止从两个插槽正常启动,同时保留 USB 恢复功能?元数据必须独立于完整的 .wic 文件保持有效。写入和引导加载程序更新。 Re: i.MX8QXP – Prevent normal boot after interrupted USB flashing on Yocto Scarthgap with A/B partit 你好, 虽然没有官方的解决方案,但您可以自定义 uuu 脚本,内置的 emmc_all 流程只是一个基于 Fastboot 和 U-Boot 命令的 UUU 脚本,它可以被修改或替换为自定义的 uuu.auto 文件。U-Boot 命令也可以通过 FB:ucmd 执行。这意味着您应该添加自定义步骤,例如在编程前设置“闪存正在进行中”标志,并在验证成功后才清除该标志。 U-Boot 启动次数/启动限制 U-Boot 库包含对以下功能的支持: 配置启动次数限制 启动计数 启动限制 altbootcmd 配置启动计数_FS 当启动次数超过启动限制时,U-Boot 会执行 altbootcmd 而不是正常的 bootcmd。此机制可用于将系统重定向到恢复模式,例如 Fastboot 模式。 启动次数限制 — Das U-Boot 未知版本文档
View full article
Eureka on PIC CLB Certain PIC MCUs (e.g., pic16f13145 family) have FPGA-like programmable logic called Configurable Logic Block. The pic16f13115 I'm using has 32 cells each with a 4-input lookup table and a D flip-flop. To learn to use the tools, today I implemented and simulated support for Charlieplexing of 6 LEDs with PWM brightness control. I used Verilog to define the circuit instead of using the logic CAD canvas. I was pounding my head on the wall for about half my time. Slowly, I got the Verilog right, got it to synthesize (build), then got it simulating. It is cool that the CLB programmed logic works even when the CPU is sleeping. It's perfect for safety-critical applications. Can be used, for example, to implement complex interrupt trigger logic. There is great flexibility in hooking up CLB logic to peripheral inputs and outputs. It's much more flexible than the clunkier CLC programmable logic that's been a fixture of PICs. General Re: Eureka on PIC CLB That’s a really interesting use of the PIC16F13115’s CLB! Using Verilog for a 6-LED Charlieplexing setup with PWM sounds like a great way to learn the workflow, and having the logic continue operating while the CPU sleeps opens up some impressive possibilities for low-power and safety-critical designs. Re: Eureka on PIC CLB Hello, It appears that the device in question belong to a different manufacturer. Could you help us contacting your manufacturer, please If you are interested in changing to an NXP device with a Programmable Logic Unit you can consult the LPC804 The LPC804 Programmable Logic Unit (PLU) Best Regards
View full article
i.MX8QXP – A/BパーティションでYocto ScarthgapのUSBフラッシュが中断された後の通常起動を防ぐ こんにちは、NXP チームの皆様、 インストールされたUUU実行ファイルは以下を報告します。 libuuu_1.5.21-0-g1f42172 私たちは以下を使用しています: sudo uuu -b emmc_all ~/Downloads/flash.bin *.wic 組み込みのemmc_allスクリプトは、以下の方法で完全な.wicイメージを書き込みます。 FB: flash -raw2sparse all _image その後、ブートローダーを書き込み、eMMCブート選択を設定し、FB: doneで終了します。 このスクリプトには、進行中のフラッシュ処理完了メタデータの明示的な処理や、読み戻しハッシュの検証手順は含まれていません。 .wic の実行中にフラッシュが中断された場合writeすると、クラスタはその後起動し、更新されたHMIを表示できます。既存の使用可能なブートローダーと、十分な量のboot、rootfsの内容が書き込まれていればこれが可能になると思われますが、選択されたスロットとその内容の完全性はまだ確認されていません。 工場出荷時フラッシュが中断された後、両方のスロットからの通常起動をブロックしつつ、USBリカバリ機能を維持するための、電源喪失耐性のある完了チェックを追加する方法について教えてください。メタデータは、完全な.wicファイルとは独立して有効でなければならない。書き込みとブートローダーのアップデート。 Re: i.MX8QXP – Prevent normal boot after interrupted USB flashing on Yocto Scarthgap with A/B partit こんにちは、 公式の解決策は実装されていませんが、uuuスクリプトをカスタマイズでき、組み込みのemmc_allフローはFastbootやU-Bootコマンドに基づくUUUスクリプトで、カスタムのuuu.autoファイルで修正または置き換えが可能です。U-BootコマンドはFB: ucmdを通じても実行可能です。つまり、プログラミング前に「フラッシュ処理中」フラグを設定し、検証が成功した後にのみそのフラグを解除するなど、カスタム手順を追加する必要があるということです。 U-Bootの起動回数/起動制限 U-Bootツリーには以下のサポートが含まれています: CONFIG_BOOTCOUNT_LIMIT ブートカウント ブート制限 altbootcmd CONFIG_BOOTCOUNT_FS ブート回数がブート制限を超えると、U-Bootは通常のbootcmdの代わりにaltbootcmdを実行します。この仕組みは、システムをFastbootのようなリリバリモードにリダイレクトするために使用できます ブートカウント制限 — Das U-Boot 不明バージョンドキュメント
View full article