2414316_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2414316_en-US

2414316_en-US

UCM-iMX95: Unable to boot Yocto Linux from SD card – mmc0 error -110| Linux cannot initialize the SD

Hi, I am using a CompuLab UCM-iMX95 and I am trying to install and boot Yocto Linux from a micro-SD card.

The boot process starts, and U-Boot successfully loads the Linux kernel. However, Linux fails to initialize the SD/MMC interface.

I get the following error:

mmc0: Timeout waiting for hardware interrupt.

mmc0: sdhci: ============ SDHCI REGISTER DUMP ============ ...

mmc0: error -110 whilst initialising MMC card The kernel then gets stuck during boot.

My Linux version is: Linux 6.12.34-2.0-... The board is: CompuLab UCM-iMX95 I am building my own Yocto image and writing it to a micro-SD card.

Could someone please help me understand what could be causing this mmc0 error -110? In particular: Is this likely to be a hardware/SD-card issue,

or could it be related to the device tree? Which MMC controller corresponds to the micro-SD interface on the UCM-iMX95?

Are there any specific device-tree settings required for the SD interface?

Is there a recommended U-Boot command to verify that the SD card is detected before Linux boots? Is there a known-good UCM-iMX95 Yocto configuration that I can compare my configuration against?

Re: UCM-iMX95: Unable to boot Yocto Linux from SD card – mmc0 error -110| Linux cannot initialize th

Hello,

The error log you are getting tell us that the MMC controller is attempting to communicate with a device that either wasn't present or wasn't responding properly. The recommended solution is to disable the unused MMC interfaces or fix the DT you configuration.

Our EVK reference design device tree uses the next configuration:

mmc0        usdhc1        eMMC
mmc1        usdhc2        SD card

You can use our device tree as reference:

https://github.com/nxp-imx/linux-imx/blob/lf-6.18.y/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dt...

Best regards.

Tags (1)
No ratings
Version history
Last update:
Friday
Updated by: