FLEXCAN EDMA - ACK errors while receiving a burst of CAN messages On i.MXRT1176 we are using FLEXCAN with EDMA. (SDK 26.03) We have a callback defined for DMA transfer complete. This is our flow: 1. Call `FLEXCAN_TransferReceiveFifoEDMA()` to start the transfer. 2. On DMA transfer completion, user-defined callback is called. 3. Data is copied from DMA buffers, and `FLEXCAN_TransferReceiveFifoEDMA()` is called to continue receiving messages. 4. Repeat Steps 2-4 We noticed that when we transmit messages from another node in a burst with just the bare minimum Inter-Frame Space, we see an increase in number of ACK errors - the iMX is unable to ACK the messages. Going through the flow, it appears that every time there is a DMA transfer complete callback, DMA is disabled on FLEXCAN. It is re-enabled again when `FLEXCAN_TransferReceiveFifoEDMA()` is called. This is done by calling `FLEXCAN_EnableRxFifoDMA()`. The enabling/disabling DMA updates the DMA bit in FLEXCAN's MCR register, and it can only be done in Freeze mode. As we are receiving messages in a burst, it is possible that a transmission is actively in progress when FLEXCAN is put it freeze mode. And it is unable to ACK the incoming message. We confirmed that removing that call to `FLEXCAN_EnableRxFifoDMA()` removes all ACK errors, though now we are dropping some messages. Also, we tried spacing out the messages, and that also got rid of the ACK errors. Can you please confirm if this is indeed an issue with the implementation, or if we should be rearchitecting it in a different way? Re: FLEXCAN EDMA - ACK errors while receiving a burst of CAN messages Hi @r-uv ,
Thank you for the detailed analysis. Your observation is consistent with the SDK implementation.
FLEXCAN_TransferReceiveFifoEDMA() is a finite-length transactional API. After each DMA completion, the driver disables the Rx FIFO DMA request, and the next call enables it again. Because changing MCR[DMA] requires Freeze mode, the next frame in minimum-IFS traffic may arrive before FlexCAN returns to Normal mode, resulting in a missed ACK.
This also explains why removing the repeated DMA enable/disable operation eliminates the ACK errors but still causes dropped frames: the Freeze-related ACK gap is removed, but the eDMA transfer is not continuously rearmed.
For continuous burst traffic, we recommend keeping the Rx FIFO DMA request enabled and using hardware-chained ping-pong/scatter-gather TCDs so that the next buffer is activated automatically. This requires a continuous DMA receive path rather than repeatedly restarting FLEXCAN_TransferReceiveFifoEDMA().
Best regards, Gavin Re: FLEXCAN EDMA - ACK errors while receiving a burst of CAN messages Thanks for the response. Are there any plans of adding this support in the SDK? A continuous DMA based implementation instead of just the current transactional API implementation?
View full article