2393584_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2393584_en-US

2393584_en-US

S32G399A serial boot IO confirm

Hi 

I am reading the S32G3 Reference Manual.

The Serial Boot section mentions that the CAN and UART interfaces use:

  • UART: RX = PAD[42], TX = PAD[41]
  • CAN: RX = PAD[43], TX = PAD[44]

However, I cannot find PAD[41], PAD[42], PAD[43], or PAD[44] in the SoC pad list or pin descriptions.

Could you please clarify which physical SoC pins or signals correspond to PAD[41], PAD[42], PAD[43], and PAD[44]?

Also, are these pads associated with a specific LINFlexD instance and FlexCAN instance used by the BootROM Serial Boot mode?

MichaelTao_0-1783673199172.pngMichaelTao_0-1783673199172.png

MichaelTao_1-1783673210769.pngMichaelTao_1-1783673210769.png


Re: S32G399A serial boot IO confirm

Hi,MichaelTao

Thank you for contacting us.

I have received your question and will help you to check it.

BR

Joey

Re: S32G399A serial boot IO confirm

Hi,MichaelTao

Please refer to the attachment S32G_IOMUX.xlsx in the S32G3 Reference Manual to obtain more information regarding the pin correspondence as you described.

Joey_z_0-1783907635236.pngJoey_z_0-1783907635236.pngJoey_z_1-1783907648304.pngJoey_z_1-1783907648304.png

Hope this information can help you.

BR

Joey

Tags (1)
No ratings
Version history
Last update:
‎07-14-2026 04:31 AM
Updated by: