imx93 cannot load elf in mcimx93evk_ethosu_apps (sdk2.14) I need try sdk2.14 demo: mcimx93evk_ethosu_apps after the elf is get .I load this elf to m33. it failed: remoteproc remoteproc0: Registered carveout doesn't fit da request [ 236.970879] rproc-virtio: probe of rproc-virtio.1.auto failed with error -12 [ 236.984471] remoteproc remoteproc0: Registered carveout doesn't fit da request [ 236.992036] rproc-virtio: probe of rproc-virtio.2.auto failed with error -12 I donnot know what happen. Re: imx93 cannot load elf in mcimx93evk_ethosu_apps (sdk2.14) Hi @bighero77,
Thank you for contacting NXP Support.
According to the README file, the application required for your use case is ethosu_apps_rpmsg, not ethosu_apps.
README extract:
4. Test process
---------------
4.1 Example ethosu_apps_rpmsg is built as .out or .elf and installed in rootfs. In Linux command line,
user can run the following command to do inference for the model.
#./inference_runner -d /dev/ethosu0 -n mobilenet_v1_1.0_224_pb_int8_vela.tflite -i stopwatch.bmp -l labels.txt -o output_data_detection -t 1080000000
When the examples runs, the log and inference result would be seen on the terminal as below.
Send Ping
Send version request
Send capabilities request
Capabilities:
version_status:1
version:{ major=0, minor=0, patch=0 }
product:{ major=6, minor=0, patch=0 }
architecture:{ major=1, minor=0, patch=6 }
driver:{ major=0, minor=16, patch=0 }
macs_per_cc:8
cmd_stream_version:0
custom_dma:false
Create network
Create inference
Wait for inferences
Inference status: success
Detected: jinrikisha, confidence:70
Detected: horse cart, confidence:70
Detected: academic gown, confidence:70
Detected: howler monkey, confidence:70
For other demos, such as face recognition, please refer to the user manual.
4.2 Example ethous_apps is built as .bin. In U-Boot prompt, user can run the following command to do
inference for the conv2d op model.
u-boot=> tftp 0x80000000 ethosu_apps.bin;cp.b 0x80000000 0x201e0000 0x20000;bootaux 0x201e0000 0
When the example runs, the log and inference result would be seen on the terminal as below.
Initialize Arm Ethos-U
Inference status: success
Based on the documentation, if your goal is to run inference from Linux using /dev/ethosu0, then ethosu_apps_rpmsg is the correct application to use.
Best regards, Alejandro Garcia
View full article