Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
外部ブート S32k S32k344デバイスは、最初に内部ROMから変更不可能な第1段階ブートローダーを実行しますか?もしそうなら、このROMブートローダーは外部フラッシュなどの外部ソースから二次ブートローダー(またはアプリケーションイメージ)をロードするように設定できますか? 外部ブートをサポートしている場合、初期ブートローダーがどこから引き出せばよいか、どのように設定すればよいのでしょうか? Re: External Boot S32k こんにちは、 @CTCoder1さん はい、S32K344にはリセット後に実行されるSBAFコードが含まれています。しかし、これは任意の外部メモリから直接アプリケーションをロードできる設定可能なブートローダーとは見なすべきではありません。外部ブートはサポートされていません。 通常のS32K3ブートフローでは、内部コードのフラッシュのみにブート情報やアプリケーションが反映されることを期待します。例えば、ユーザーのブートローダーを内部フラッシュの開始(IVTは0x00400000)に配置し、必要な更新/読み込みメカニズムを実行することができます。 したがって、アプリケーションを外部フラッシュに保存する意図がある場合、通常の解決策はユーザーブートローダーを内部フラッシュに設定することです。このブートローダーは必要なペリフェラル/外部メモリインターフェースを初期化し、外部デバイスからイメージを読み込み、それを内部フラッシュにプログラムするか、アプリケーションの要件に応じて処理します。 SBAF(あるいはBootROM)構成は存在しません。単に外部フラッシュアドレスやデバイスを指定して、S32K344 SBAFがそこからアプリケーションを直接起動させるようなものです。これは完全にソフトウェアで管理する必要があります。 よろしくお願いいたします。 ルーカス
記事全体を表示
E6500 / E5500割り込みパス、RFI対RFCIおよびその他のファミリ命令 こんにちは、 RFIやその他のファミリ命令は、さまざまな割り込みや例外からの返却に使用されます。 E5500およびE6500プロセッサで、SRR0とSRR1が正しい値に戻されている限り(CSRR0、CRSRR1、MCSRR0、MCSRR1などから最初に読み取れる可能性が高い)、それともプロセッサ内部の機構が壊れるのか知りたいです。 よろしくお願いいたします。 アレクシー・トーレス QorIQ T1 デバイス QorIQ T2デバイス Re: E6500 / E5500 Interrupt Path, RFI vs RFCI and other family instructions 迅速なご回答ありがとうございます。それは我々が考えていたことを裏付けるものだ。 Re: E6500 / E5500 Interrupt Path, RFI vs RFCI and other family instructions E5500およびE6500では、SRR0/SRR1レジスタにCSRR0/CSRR1またはMCSRR0/MCSRR1からコピーした値を手動でプリロードした場合でも、「RFI」を他の割り込み復帰命令(「RFCI」、「RFMCI」など)に普遍的に置き換えることは推奨されません。 各リターン命令は、特定の保存/復元レジスタペアからMSRを復元します。「RFI」を使うと必ずSRR1から復元されますが、回復されるMSRビット(マスクや強制されるもの)は命令によって異なる場合があります。レジスタ値だけでなく、ハードウェアレベルでは、`RFCI` または `RFMCI` によって一部のビットの処理方法が異なる場合があります。 「RFCI」と「RFMCI」は「CSSR」/「MCSR」の状態をクリアし、割り込みレベルの内部プロセッサトラッキングを更新します(例:MSRの「CE」/「ME」有効ビット)。手動でコピーした値を「RFI」だけ使用すると、クリティカル/マシンチェック割り込み状態が正しく再有効化またはクリアされず、プロセッサが内部的に不整合な状態に陥る可能性があります。 Power Architecture Embedded Environment(EREF)仕様では、各例外クラスから返すためにどの命令を使うべきかを明示的に定義しています。これから逸脱するとアーキテクチャ的に定義された挙動の範囲外であり、これらのコアに予測不可能な結果をもたらす可能性があります。 推奨される方法は、rfi は標準/非クリティカルな戻り値にのみ使用し、関連する割り込みクラスには rfci、rfdi、rfgi、または rfmci を使用することです。
記事全体を表示
RT685 DPD wake via PMIC_IRQ_N not working HW: RT685 + PCA9420, PMIC_IRQ_N connected to RT685 dedicated pin. Problem: POWER_EnterDeepPowerDown(exclude_from_pd={0,0,0,0}) → MCU loses power (VDDCORE off). Pull PMIC_IRQ_N low → no wake. Manually shorting PMIC_IRQ_N to GND for ~1s also does not wake.  Code before entry  :   BOARD_InitPmic(); BOARD_ConfigPMICModes(); BOARD_SetPmicVoltageBeforeDeepPowerDown(); POWER_EnableInterrupts(kPMC_INT_INTRPAD); EnableDeepSleepIRQ(PMC_PMIC_IRQn); BOARD_EnterDeepPowerDown(exclude_from_pd); ```   PMC->FLAGS after failed wake: 0x60170000, DEEPPDF (bit31) = 0. WAKE_UP_WITH_PMIC_IRQ_N = 1. Questions : Is additional RT685-side config needed to make PMIC_IRQ_N a valid DPD wake source? Does PCA9420 stop driving PMIC_IRQ_N when VDDCORE is cut via DPD Anyone successfully used PMIC_IRQ_N to wake RT685 from DPD? Working config?     i.MX-RT600  SERVER-POWER-CONTROL                       Power Re: RT685 DPD wake via PMIC_IRQ_N not working Hi @wx1 , Regarding PMC->FLAGS after failed wake: 0x60170000, DEEPPDF (bit31) = 0. WAKE_UP_WITH_PMIC_IRQ_N = 1.  The reason to have this result is due to that  DEEPPDF (bit 31 of PMC->FLAGS ) is only set when the MCU successfully completes a full DPD cycle and wakes from it. A value of 0 means the MCU never cleanly entered DPD. The co-existing WAKE_UP_WITH_PMIC_IRQ_N = 1 tells you that the PMC detected a low pulse on PMIC_IRQ_N, but the DPD state was never committed. This pattern almost always means PMIC_IRQ_N was already asserted (logic-low) at the moment DPD entry was attempted, causing an immediate phantom wake before DPD could latch. When PMIC_MODE[1:0] transitions to 0b10 (DPD mode, VDDCORE off), the PCA9420 internally detects that SW1_OUT is dropping. This can trigger a brief INTB pulse due to the PCA9420's voltage supervisor logic firing on the SW1 output. If that pulse reaches the PMC before DPD is fully committed, you get exactly what you are seeing. Is additional RT685-side config needed to make PMIC_IRQ_N a valid DPD wake source? Before arming DPD, drain any pending PCA9420 interrupts so that INTB is deasserted (high) when DPD latches. Does PCA9420 stop driving PMIC_IRQ_N when VDDCORE is cut via DPD PMIC_IRQ_N is on the VDD_AO1V8 always-on domain, which stays powered throughout DPD. The PCA9420 INTB output is open-drain and powered from VIN, so as long as VIN (your system supply) is present the PCA9420 can still drive INTB low.   Hope that makes sense,   Have a great day, Kan ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
記事全体を表示
S32K314 get stuck at 0x2040012C WFI during HSE recovery in AB swap Hello NXP Support Team, I am testing HSE recovery in AB swap as following steps. Firstly, I use lauterbach to execute HSE FW erase to erase HW, then test the recovery process. The CPU always stops at at 0x2040012C WFI instruction after step 9 issue a functional reset, I need to power off, then power on to get out of this.  Could you please give some tips on what's going wrong?  leo_cheng_0-1789995644535.png leo_cheng_1-1789995683683.png Re: S32K314 get stuck at 0x2040012C WFI during HSE recovery in AB swap Hi @leo_cheng  If it hangs at 0x2040012C after reset, it means that the device entered JTAG based recovery  mode. You can take a look at “2.6.1.3 Recovery Mode” section in the HSE-B Firmware reference manual. If you want to recover using Lauterbach debugger, I wrote attached script which follows section “3.3.1  MU Installation Steps by Host in AB_SWAP Configuration”. It works for installation of the firmware on brand new device and it works for recovery when the firmware is erased completely or when there’s backup image in passive partition. Regards, Lukas
記事全体を表示
S32K314 が AB スワップ中の HSE リカバリ中に 0x2040012C WFI で停止する こんにちは、NXPサポートチームの皆さん、 以下の手順で、ABスワップにおけるHSEリカバリのテストを行っています。まず、lauterbachを使用してHSE FW eraseを実行し、ハードウェアを消去してから、リカバリプロセスをテストします。ステップ9で機能リセットを発行した後、CPUは常に0x2040012CのWFI命令で停止します。この状態から抜け出すには、電源をオフにしてからオンにする必要があります。何がうまくいっていないのか、アドバイスをいただけますか? leo_cheng_0-1789995644535.png leo_cheng_1-1789995683683.png Re: S32K314 get stuck at 0x2040012C WFI during HSE recovery in AB swap こんにちは、 @leo_cheng さん。 リセット後に0x2040012Cでハングアップする場合、デバイスがJTAGベースのリカバリモードに入ったことを意味します。「2.6.1.3」をご覧ください。HSE-Bファームウェアリファレンスマニュアルの「リカバリーモード」セクションに記載されています。 Lauterbach デバッガーを使用して復旧したい場合は、セクション「3.3.1」に従って、添付のスクリプトを作成しました。「AB_SWAP構成におけるホストごとのMUインストール手順」これは、新品のデバイスへのファームウェアのインストールに有効であり、ファームウェアが完全に消去された場合や、パッシブパーティションにバックアップイメージが存在する場合の復旧にも有効です。 よろしくお願いいたします。 ルーカス
記事全体を表示
RT685 DPDのPMIC_IRQ_Nによるウェイクアップが機能しない HW:RT685 + PCA9420、PMIC_IRQ_N RT685専用ピンに接続されています。 問題: POWER_EnterDeepPowerDown(exclude_from_pd={0,0,0}) →MCUが電源を失います(VDDコアがオフ)。ウェイク→PMIC_IRQ_Nを下げてください。手動でGNDにショートPMIC_IRQ_Nさせて~1秒も起動しません。 入力前にコードを入力してください  :   BOARD_InitPmic(); BOARD_ConfigPMICModes(); BOARD_SetPmicVoltageBeforeDeepPowerDown(); POWER_EnableInterrupts(kPMC_INT_INTRPAD); EnableDeepSleepIRQ(PMC_PMIC_IRQn); BOARD_EnterDeepPowerDown(exclude_from_pd); 「`」   PMC->FLAGS ウェイク失敗後: 0x60170000、DEEPPDF (bit31) = 0。 PMIC_IRQ_Nで起動 = 1. 質問 : PMIC_IRQ_Nを有効なDPDウェイクソースにするには、RT685側で追加の設定が必要ですか? DPD を介して VDDCORE が切断された場合、PCA9420 は PMIC_IRQ_N の駆動を停止しますか? PMIC_IRQ_Nを使用してRT685をDPDからウェイクアップすることに成功した方はいますか?動作する設定はありますか?     i.MX-RT600サーバー電源制御                     パワー Re: RT685 DPD wake via PMIC_IRQ_N not working こんにちは、 @wx1 さん。 PMC->FLAGSについて:0x60170000、DEEPPDF(ビット31)= 0. WAKE_UP_WITH_PMIC_IRQ_N = 1。この結果が出る理由は 、 DEEPPDF ( PMC->FLAGS のビット31)がMCUが完全なDPDサイクルを完了し、そこからウェイクアップした場合にのみ設定されるためです。値が 0 の場合は、MCUがDPDにきれいに入っていなかったことを意味します。共存する WAKE_UP_WITH_PMIC_IRQ_N = 1 は、PMC が PMIC_IRQ_N で低パルスを検出したが、DPD 状態がコミットされなかったことを示しています。このパターンはほとんどの場合、 DPDの入力が試みられた時点ですでにPMIC_IRQ_Nが主張されていた(論理低値)であり、DPDがラッチする前に即座にファントムウェイクが発生しています。 PMIC_MODE[1:0] が 0b10 に遷移すると(DPDモード、VDDCOREオフ)、PCA9420は内部的にSW1_OUTが低下していることを検出します。これにより、PCA9420の電圧スーパーバイザロジックがSW1出力で発動するため、短いINTBパルスがトリガーされることがあります。そのパルスがDPDが完全に作動する前にPMCに到達すると、まさに今見ているような現象が起こります。 PMIC_IRQ_Nを有効なDPDウェイクソースにするには、RT685側で追加の設定が必要ですか? DPDを起動する前に、保留中のPCA9420中断中の割り込みを排水し、DPDがラッチしたときにINTBが解除される(高く)します。 DPD を介して VDDCORE が切断された場合、PCA9420 は PMIC_IRQ_N の駆動を停止しますか? PMIC_IRQ_Nは VDD_AO1V8 常時オンドメイン上にあり、DPD期間中ずっと電源が供給されています。PCA9420のINTB出力はオープンドレインでVINから電力が供給されているため、VINが存在している限りPCA9420はINTBの低電圧を駆動できます。   これで意味が通じるといいのですが。   すてきな一日を、 カン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「正解としてマーク」ボタンをクリックしてください。ありがとうございます! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 -------------------------------------------------------------------------------
記事全体を表示
i.MX95 19x19 EVK – M2-JODY-W6 Wi-Fi Card Availability and Camera Module Compatibility Hello NXP Team, We are working with the NXP i.MX95 19x19 EVK (IMX95LPD5EVK-19) for an Android Automotive OS project. We would like to get clarification on the following: 1. M2-JODY-W6 Wi-Fi Card The M2-JODY-W6 Wi-Fi card is not included in our i.MX95 EVK kit. Could you please provide information on: - Availability of the M2-JODY-W6 Wi-Fi card - How we can obtain/purchase the card - Whether NXP provides a sample or recommended ordering channel - Any required documentation or compatibility information for the i.MX95 19x19 EVK 2. Camera Module Compatibility We would also like information about a camera module officially supported/validated with the i.MX95 19x19 EVK. Could you please provide: - Recommended/validated camera module - Exact module/part number - Camera sensor used - Hardware connection/interface information - Relevant documentation - Linux/Android driver or software support information - Any available reference design or configuration information Board: NXP i.MX95 19x19 EVK Part Number: IMX95LPD5EVK-19 Software: Android Automotive OS 16 NXP BSP We would appreciate your guidance on the above questions. Thanks and Regards, Gnana Prasanna Gunakala Re: i.MX95 19x19 EVK – M2-JODY-W6 Wi-Fi Card Availability and Camera Module Compatibility Hello,  For your first question please open a technical case, for the second question please refer to the following AN: https://www.nxp.com/docs/en/application-note/AN14853.pdf  Regards.
記事全体を表示
S32K314 在 AB 交换期间的 HSE 恢复中卡在 0x2040012C WFI。 您好,NXP支持团队, 我正在按以下步骤测试 AB 互换中的 HSE 恢复情况。首先,我使用 lauterbach 执行 HSE FW erase 来擦除硬件,然后测试恢复过程。CPU 在步骤 9 发出功能性复位指令后,总是停留在 0x2040012C WFI 指令处,我需要断电重启才能解决这个问题。请问您能否就哪里出了问题提供一些建议? leo_cheng_0-1789995644535.png leo_cheng_1-1789995683683.png Re: S32K314 get stuck at 0x2040012C WFI during HSE recovery in AB swap 嗨@leo_cheng 如果 RESET 后卡在 0x2040012C,则表示设备已进入基于 JTAG 的恢复模式。您可以查看“2.6.1.3”。HSE-B 固件参考手册中的“恢复模式”部分。 如果您想使用 Lauterbach 调试器进行恢复,我编写了附件脚本,该脚本遵循“3.3.1”节。AB_SWAP 配置中主机 MU 安装步骤”。它适用于在新设备上安装固件,也适用于固件完全擦除或被动分区中有备份映像时的恢复。 此致, Lukas
記事全体を表示
RT685 DPD 通过 PMIC_IRQ_N 唤醒不起作用 硬件:RT685 + PCA9420,PMIC_IRQ_N 连接到 RT685 专用引脚。 问题: POWER_EnterDeepPowerDown(exclude_from_pd={0,0,0,0}) → MCU 断电(VDDCORE 关闭)。将 PMIC_IRQ_N 拉低 → 无法唤醒。手动将 PMIC_IRQ_N 短接到 GND 约 1 秒也无法唤醒。 入口前需输入代码  :   BOARD_InitPmic(); BOARD_ConfigPMICModes(); BOARD_SetPmicVoltageBeforeDeepPowerDown(); POWER_EnableInterrupts(kPMC_INT_INTRPAD); EnableDeepSleepIRQ(PMC_PMIC_IRQn); BOARD_EnterDeepPowerDown(exclude_from_pd); ```   PMC->FLAGS 唤醒失败后:0x60170000,DEEPPDF(位31)= 0。 WAKE_UP_WITH_PMIC_IRQ_N = 1. 问题 : 是否需要额外的 RT685 端配置才能使 PMIC_IRQ_N 成为有效的 DPD 唤醒源? 当通过 DPD 切断 VDDCORE 时,PCA9420 是否会停止驱动 PMIC_IRQ_N? 有人成功使用 PMIC_IRQ_N 从 DPD 唤醒 RT685 吗?配置可行吗?     i.MX-RT600服务器电源控制                     电源 Re: RT685 DPD wake via PMIC_IRQ_N not working 嗨@wx1 , 关于唤醒失败后的 PMC->FLAGS :0x60170000,DEEPPDF(位31)= 0。 WAKE_UP_WITH_PMIC_IRQ_N = 1. 出现此结果的原因是,只有当 MCU 成功完成一个完整的 DPD 周期并从中唤醒时, DEEPPDF ( PMC->FLAGS 的第 31 位)才会设置。值为 0 表示 MCU 从未干净地进入 DPD。共存的 WAKE_UP_WITH_PMIC_IRQ_N = 1 表示 PMC检测到 PMIC_IRQ_N 上的低脉冲,但 DPD 状态从未被提交。这种模式几乎总是意味着在尝试进入 DPD 时 PMIC_IRQ_N 已经钳位(逻辑低) ,导致在 DPD 锁存之前立即出现幻觉唤醒。 当 PMIC_MODE[1:0] 过渡到 0b10 (DPD 模式,VDDCORE 关闭)时,PCA9420 内部检测到 SW1_OUT 正在下降。由于 PCA9420 的电压监控逻辑在 SW1 输出端触发,这可能会触发短暂的 INTB 脉冲。如果该脉冲在 DPD 完全执行之前到达 PMC,就会出现你现在看到的情况。 是否需要额外的 RT685 端配置才能使 PMIC_IRQ_N 成为有效的 DPD 唤醒源? 在启用 DPD 之前,清除所有待处理的 PCA9420 中断,以便在 DPD 锁存时 INTB 被取消置位(高电平)。 当通过 DPD 切断 VDDCORE 时,PCA9420 是否会停止驱动 PMIC_IRQ_N? PMIC_IRQ_N 位于 VDD_AO1V8 始终开启功能域中,在整个 DPD 期间保持通电状态。PCA9420 INTB 输出为开漏输出,由 VIN 供电,因此只要 VIN(您的系统电源)存在,PCA9420 仍然可以将 INTB 拉低。   希望我解释清楚了。   祝你有美好的一天, 坎 ------------------------------------------------------------------------------- 笔记: - 如果此回复解答了您的问题,请点击“标记为正确答案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 -------------------------------------------------------------------------------
記事全体を表示
E6500 / E5500 Interrupt Path, RFI vs RFCI and other family instructions Hello, The RFI and other family instructions are used to return from different types of interrupts / exceptions.  I would like to know if it is possible on the E5500 and E6500 processor to always use RFI as long as the SRR0 and SRR1 are restored to the correct value (potentially initially read from CSRR0, CRSRR1 or MCSRR0, MCSRR1, etc.) or if it would break some internal mechanism of the processor. Best Regards, Alexy Torres QorIQ T1 Devices QorIQ T2 Devices Re: E6500 / E5500 Interrupt Path, RFI vs RFCI and other family instructions Thank you for the quick answer. That confirms what we have been thinking. Re: E6500 / E5500 Interrupt Path, RFI vs RFCI and other family instructions On the E5500 and E6500, it is not recommended to universally substitute  “RFI” for the other return-from-interrupt instructions (“RFCI”, “RFMCI”, etc.), even if the SRR0/SRR1 registers are manually pre-loaded with values copied from CSRR0/CSRR1 or MCSRR0/MCSRR1. Each return instruction restores the MSR from a specific save/restore register pair. Using `RFI` always restores from SRR1, but the MSR bits that are restored (and which are masked or forced) can differ depending on the instruction. Some bits may be handled differently by `RFCI` or `RFMCI` at the hardware level, beyond just the register values. `RFCI` and `RFMCI` also clear the `CSSR`/`MCSR` state and update internal processor tracking of the interrupt level (e.g., the `CE`/`ME` enable bits in MSR). Simply using `RFI` with manually copied values may not correctly re-enable or clear the critical/machine-check interrupt state, potentially leaving the processor in an inconsistent internal state. The Power Architecture Embedded Environment (EREF) specification explicitly defines which instruction must be used to return from each exception class. Deviating from this is outside the architecturally defined behavior and could produce unpredictable results on these cores. The recommended approach is to use rfi only for standard/noncritical returns, and use rfci , rfdi , rfgi , or rfmci for their associated interrupt classes.
記事全体を表示
E6500 / E5500 中断路径、RFI 与 RFCI 以及其他系列指令 你好, RFI 和其他系列指令用于从不同类型的中断/异常中返回。 我想知道,在 E5500 和 E6500 处理器上,只要 SRR0 和 SRR1 恢复到正确的值(可能最初是从 CSRR0、CRSRR1 或 MCSRR0、MCSRR1 等读取),是否可以始终使用 RFI,或者这样做是否会破坏处理器的某些内部机制。 顺祝商祺! 阿莱克西·托雷斯 QorIQ T1 设备 QorIQ T2 设备 Re: E6500 / E5500 Interrupt Path, RFI vs RFCI and other family instructions 感谢您的快速回复。这证实了我们一直以来的想法。 Re: E6500 / E5500 Interrupt Path, RFI vs RFCI and other family instructions 在 E5500 和 E6500 上,即使 SRR0/SRR1 寄存器已手动预加载了从 CSRR0/CSRR1 或 MCSRR0/MCSRR1 复制的值,也不建议普遍用“RFI”代替其他中断返回指令(“RFCI”、“RFMCI”等)。 每条返回指令都会从特定的保存/恢复寄存器对恢复 MSR。使用 `RFI` 总是从 SRR1 恢复,但恢复的 MSR 位(以及被屏蔽或强制的位)可能因指令而异。除了寄存器值之外,`RFCI` 或 `RFMCI` 在硬件层面上可能会以不同的方式处理某些位。 `RFCI` 和 `RFMCI` 还会清除 `CSSR`/`MCSR` 状态,并更新内部处理器对中断级别的跟踪(例如,MSR 中的 `CE`/`ME` 使能位)。简单地使用 `RFI` 并手动复制值可能无法正确地重新启用或清除关键/机器检查中断状态,从而可能导致处理器处于不一致的内部状态。 Power Architecture Embedded Environment (EREF) 规范明确定义了从每个异常类返回时必须使用哪个指令。偏离此行为超出了架构定义的行为范围,可能会在这些核心上产生不可预测的结果。 建议的做法是仅对标准/非关键返回使用 rfi,而对相关的中断类使用 rfci、rfdi、rfgi 或 rfmci。
記事全体を表示
IoT ToolboxアプリがKW45-EVK – NXP OTAPサンプル使用時にOTAPメニューでクラッシュする こんにちは、 現在、 NXP OTAPのサンプルプロジェクト を KW45-EVK ボード 上で 実行 し、 NXP IoT Toolbox モバイルアプリケーションをOTAPプロセスに 使 おうとしています。 しかし、 OTAPメニュー のIoT Toolboxアプリで問題が発生しています 。 問題 IoT ToolboxアプリでOTAPメニューを開いてスキャンを開始すると: スマホで 位置情報がオフの場合 、 スキャン ボタンを押すと 読み込み/スキャン表示が表示されますが、アプリはデバイスを見つけられません。 位置情報がオンの場合、 OTAPメニュー中にアプリケーションがクラッシュします。 複数のAndroid端末 で試 しました が、問題は変わりませんでした。 まれに、KW45-EVKデバイスがスキャン結果に一瞬だけ現れるのを一瞬だけ見かけることがあり、その後アプリケーションがクラッシュします。 私が試したこと 複数のスマートフォンでテスト済み。 位置情報サービスのオン/オフ両方でテストしました。 スキャンを複数回繰り返した。 KW45-EVKがNXP OTAPのサンプルプログラムを実行していることを確認しました。 私がテストしたすべてのスマートフォンで、この現象は再現可能です。 NXP IoT ToolboxのOTAPアプリケーションとKW45-EVK で同様の問題を経験した方はいらっし ゃいますか? これをさらにデバッグしたり、IoT Toolboxアプリを使ってOTAPをうまく実行する方法について、何かアドバイスがあれば教えてください。 よろしくお願いします! Re: IoT Toolbox app crashes in OTAP menu when using KW45-EVK – NXP OTAP example こんにちは、お元気でお過ごしでしょうか。 ご報告ありがとうございます。同様の問題を再現できたため、現在社内チームと調査を進めております。 その間に、以下の情報を教えていただけますか? どのモデルとAndroidバージョンのデバイスでテストしましたか?どのバージョンのIoT Toolboxでテストしましたか?Androidで「およその位置」と「正確な位置」を使う場合、挙動に違いを感じますか? 補足として、iPhoneデバイスでこの問題は発生しなかったため、これはAndroid特有の挙動であることが確認されました。 今のところ、可能であればiPhoneデバイスを使用するか、ボード間接続を利用することをお勧めします。詳しい情報が入り次第、すぐにお知らせします。 よろしくお願いします、 ソフィア。 Re: IoT Toolbox app crashes in OTAP menu when using KW45-EVK – NXP OTAP example Androidバージョン:13 IOT Toolboxの最新バージョン 「AndroidでApproximate LocationとPrecise Locationを使っている場合、挙動に違いを感じますか?」 検査はしていません。
記事全体を表示
i.MX95 19x19 EVK – M2-JODY-W6 Wi-Fi 卡的可用性和相机模块兼容性 您好,NXP团队, 我们正在与 NXP i.MX95 19x19 EVK (IMX95LPD5EVK-19) 合作开发 Android Automotive OS 项目。 我们想就以下问题获得澄清: 1. M2-JODY-W6 无线网卡 我们的 i.MX95 EVK 套件中不包含 M2-JODY-W6 Wi-Fi 卡。 请问您能否提供以下信息: - M2-JODY-W6 Wi-Fi 卡的供货情况 - 我们如何获得/购买这张卡 - NXP是否提供样品或推荐的订购渠道 - i.MX95 19x19 EVK 所需的任何文档或兼容性信息 2. 摄像头模块兼容性 我们还希望获得有关 i.MX95 19x19 EVK 官方支持/验证的相机模块的信息。 请问您能否提供以下信息: - 推荐/已验证的摄像头模块 - 确切的模块/零件编号 - 使用的相机传感器 - 硬件连接/接口信息 相关文件 - Linux/Android 驱动程序或软件支持信息 - 任何可用的参考设计或配置信息 板: NXP i.MX95 19x19 EVK 零件编号:IMX95LPD5EVK-19 软件: Android Automotive OS 16 NXP BSP 希望您能就以上问题提供指导。 谢谢,此致敬礼! 格纳纳·普拉桑纳·古纳卡拉 Re: i.MX95 19x19 EVK – M2-JODY-W6 Wi-Fi Card Availability and Camera Module Compatibility 你好, 第一个问题请提交技术案例,第二个问题请参考以下应用笔记: https://www.nxp.com/docs/en/application-note/AN14853.pdf 此致问候
記事全体を表示
i.MX95 19x19 EVK – M2-JODY-W6 Wi-Fiカードの入手可能性とカメラモジュールの互換性 NXPチームの皆様、こんにちは。 私たちはAndroid オートモーティブ OSプロジェクトのためにNXP i.MX95 19x19 EVK(IMX95LPD5EVK-19)を使用しています。 以下の点についてご説明をいただきたい。 1. M2-JODY-W6 Wi-Fiカード M2-JODY-W6 Wi-Fiカードは、当社のi.MX95 EVKキットには含まれていません。 以下の情報を教えていただけますか: - M2-JODY-W6 Wi-Fiカードの入手可能性 - カードの取得・購入方法 - NXPがサンプルまたは推奨ご注文チャネルを提供するかどうか - i.MX95 19x19 EVKに必要なドキュメントや互換性情報 2. カメラモジュールの互換性 i.MX95 19x19 EVKで公式にサポート/検証済みのカメラモジュールに関する情報も提供していただけると幸いです。 以下の情報を提供していただけますか: - 推奨/検証済みカメラモジュール - 正確なモジュール/部品番号 - 使用カメラセンサ - ハードウェア接続/インターフェース情報 - ドキュメント - Linux/Androidドライバまたはソフトウェアのサポート情報 - 利用可能なリファレンス・デザインや構成情報 ボード: NXP i.MX95 19x19 EVK 部品番号:IMX95LPD5EVK-19 ソフトウェア: Android オートモーティブ OS 16 NXP BSP 上記の質問について、ご助言いただければ幸いです。 よろしくお願いいたします。 グナナ・プラサンナ・グナカラ Re: i.MX95 19x19 EVK – M2-JODY-W6 Wi-Fi Card Availability and Camera Module Compatibility こんにちは、 最初の質問については技術的なケースを開いてください。2つ目の質問については以下のANを参照してください:https://www.nxp.com/docs/en/application-note/AN14853.pdf  よろしくお願いします。
記事全体を表示
使用 KW45-EVK 时,IoT Toolbox 应用在 OTAP 菜单中崩溃 – NXP OTAP 示例 您好, 我目前正在尝试 在 KW45-EVK 板上运行 NXP OTAP 示例项目 ,并使用 NXP IoT Toolbox 移动应用程序进行 OTAP 流程。 但是,我在 OTAP 菜单 中的 IoT Toolbox 应用遇到了问题 。 问题 当我在 IoT Toolbox 应用中打开 OTAP 菜单并开始扫描时: 如果 我的手机上的 位置服务已关闭 ,按下 扫描按钮 会显示正在加载/扫描的指示,但应用程序似乎找不到设备。 如果 位置信息已开启 , 则在 OTAP 菜单中 应用程序 会崩溃 。 我用 多部安卓手机 测试过 ,但问题依旧存在。 在极少数情况下,我可以在扫描结果中短暂地看到我的 KW45-EVK 设备出现不到一秒钟,之后应用程序就会崩溃。 我尝试过 已使用多部手机测试。 已在开启和关闭定位功能的情况下进行测试。 重复扫描多次。 已确认 KW45-EVK 正在运行 NXP OTAP 示例。 我在测试过的所有手机上都出现了这种现象。 有人在使用 NXP IoT Toolbox OTAP 应用程序和 KW45-EVK 时 遇到过类似的问题吗 ? 非常感谢您能提供任何关于如何进一步调试此问题或如何使用 IoT Toolbox 应用程序成功执行 OTAP 的建议。 谢谢您! Re: IoT Toolbox app crashes in OTAP menu when using KW45-EVK – NXP OTAP example 你好,希望你一切都好。 感谢您的报告,我已经重现了类似的问题,我们目前正在与内部团队一起调查此事。 与此同时,您能否提供以下信息? 你们测试时使用的是哪些型号和安卓版本的设备?您测试时使用的是哪个版本的物联网工具箱?在安卓系统上使用“大致位置”和“精确位置”时,您是否注意到行为上有任何区别? 另外,我在 iPhone 设备上测试过,没有出现这个问题,这证实了这是 Android 特有的行为。 目前,我建议尽可能使用 iPhone 设备或板对板连接方式。一旦有更多信息,我会立即通知您。 此致, 索菲亚。 Re: IoT Toolbox app crashes in OTAP menu when using KW45-EVK – NXP OTAP example Android 版本:13 最新版本的物联网工具箱 “您在使用安卓系统的大致位置和精确位置时,是否注意到行为上有任何区别?” 未进行测试。
記事全体を表示
IoT Toolbox app crashes in OTAP menu when using KW45-EVK – NXP OTAP example Hi, I am currently trying to run the NXP OTAP example project on a KW45-EVK board and use the NXP IoT Toolbox mobile application for the OTAP process. However, I am facing an issue with the IoT Toolbox app in the OTAP menu. Issue When I open the OTAP menu in the IoT Toolbox app and start scanning: If Location is OFF on my phone, pressing Scan shows the loading/scanning indication, but the application does not seem to find the device. If Location is ON, the application crashes while in the OTAP menu. I have tested this with multiple Android phones, but the issue remains the same. In rare cases, I can briefly see my KW45-EVK device appear in the scan results for a fraction of a second, after which the application crashes. What I have tried Tested with multiple phones. Tested with Location ON and OFF. Repeated the scan multiple times. Confirmed that the KW45-EVK is running the NXP OTAP example. The behavior is reproducible across the phones I have tested. Has anyone experienced a similar issue with the NXP IoT Toolbox OTAP application and KW45-EVK? Any suggestions on how I can debug this further or successfully perform OTAP using the IoT Toolbox app would be appreciated. Thanks! Re: IoT Toolbox app crashes in OTAP menu when using KW45-EVK – NXP OTAP example Hello, hope you are doing well. Thank you for your report, I have replicated a similar issue and we are currently investigating this with the internal team. In the meantime, could you help us with the following information? Which model and Android version devices did you test with? Which version of the IOT Toolbox did you test with? Do you notice any difference in behavior when using Approximate location vs Precise location on Android? As an additional note, I have tested this on an iPhone device and the issue does not occur, which confirms this is Android-specific behavior. For now, I would recommend if possible, to use an iPhone device or a board-to-board setup. I will let you know as soon as I have more infromation available. Best regards, Sofia. Re: IoT Toolbox app crashes in OTAP menu when using KW45-EVK – NXP OTAP example Android version: 13 Latest version of IOT Toolbox "Do you notice any difference in behavior when using Approximate location vs Precise location on Android?" Didn't test.
記事全体を表示
RT1064 オンラインアップグレードプラン 下記は、当製品のハードウェア拡張図です。 1. PCとメインボードはTCPで接続されています 2. メインボードは4つのサブボードに4つのSPIバスを介して接続されており、サブボードの機能は同じです 3. メインボードのUART4は、シリアルポートのスイッチを介して4つのサブボードのうちUART1に切り替えることができます foreverwlh2025_0-1789970732170.png プロジェクトの要件により、 PCは4つのサブボード(RT1064)からTCPまでのファームウェアプログラムをアップグレードする必要があります。ハードウェア拡張に基づいて、上位コンピュータ開発、メインボード開発、サブボード開発の作業負荷を考慮して、サブボードファームウェアのアップグレードに最も簡単な解決策を提供できますか? i.MXRT 106x Re: RT1064 Online Upgrade Plan @foreverwlh2025様、 ご質問ありがとうございます。 推奨されるアプローチ PCはTCPを介してマザーボードと通信します。マザーボードはTCPサーバーとして機能し、UART透過ブリッジを実装しています。メインボード上のUART4はシリアルスイッチチップを経由して選択したサブボードのUART1インターフェースにルーティングされます。サブボードはRT1064 ROMブートローダーを動作させるため、サブボード側で追加のブートローダーやファームウェア開発は不要です。 単一サブボードのアップグレード手順(ステップバイステップ): サブボードNでRESET信号をアサートし、BOOT_MODE[1:0]を01(シリアルダウンローダーモード)に設定する。 シリアルスイッチチップを切り替えてUART4をサブボードNのUART1に接続します リリースRESET — サブボードNがRT1064 ROMブートローダーに入り、UARTコマンドを待つ TCP↔UART4バイト転送を有効にする RESETを切り替えてBOOT_MODEを通常に戻すと、サブボードNが新しいファームウェアで起動します。 シリアルセレクタを次のサブボードに切り替えて繰り返します ハードウェアの前提条件 実装前に、以下のハードウェア条件が満たされていることをご確認ください。 メインボードは、各サブボードのBOOT_MODE[1:0]ピンを独立してGPIO制御できます。 メインボードは、各サブボードのRESETピンを個別にGPIO制御できます。 シリアルスイッチチップはメインボードのGPIOで制御可能で、4つのサブボードすべて間のスイッチングをサポートします ご質問や、導入の詳細についてさらに話し合いたい場合は、お気軽にご連絡ください。 Re: RT1064 Online Upgrade Plan @foreverwlh2025様、 ファームウェアのアップグレードに関するお客様のシナリオに対し、弊社が推奨するソリューションの概要を以下にご説明いたします。 1. PCツール PC側では blhost というオープンソースのコマンドラインクライアントを提供しており、NXPのMCUブートローダープライベートフレーミングプロトコル(BSD/MITライセンス)を実装しています。デバイス側プロトコルはMCUオンチップROMブートローダーによって実装されます。これら2つの機能により、ファームウェアのダウンロードとデバイスの設定が可能になります。 このツールはUSBとUART1に対応していますが、TCPには対応していません。 オープンソースリポジトリ: https://github.com/nxp-mcuxpresso/spsdk blhostとROMブートローダーは独自のフレーミングパケットプロトコルで通信します。ご参照ください: MCU Bootloader v2.5.0 リファレンス・マニュアル(MCUBOOTRM) ファームウェアイメージの生成およびパッケージングについては、NXPのSPSDK(Secure Provisioning SDK)に含まれるnxpimageツールをご利用ください。 2. 推奨ソリューション:マザーボード経由のTCP透過転送 あなたのシナリオ(PC→マザーボード→サブボード)の場合、最小限の手間で済む方法は、マザーボードを透過的なTCP-UARTブリッジとして機能させ、blhostを少し変更してシリアルデータをTCPでラップすることです。 建築: PC (modified blhost) ↓ TCP packet (include original UART byte stream) Main Board (TCP Server) ↓ Unpack and forward to sub-board via UART Sub-board (ROM Bootloader) 主な変更点: blhostトランスポート層の変更:blhostソースコードに新しいTCPトランスポートモジュールを追加します。既存のUARTバイトストリーム(フレーミングパケット)は、送信経路ではそのままTCPパケットにラップされ、受信経路ではアンラップされる。 メインボードはTCPサーバーを実装しています。PCからTCPデータを受信し、ペイロードをバイト単位でUART1経由でサブボードに転送します。サブボードからの応答は、同じ透過的な方法でTCP経由でPCに転送されます。 サブボードに変更は不要です。サブボードMCUは単にISPモードでROMブートローダーが動作し、標準UARTコマンドを待つだけで済みます。 Re: RT1064 Online Upgrade Plan 4. TCP↔UART4バイト転送を有効にする すみません、このデータ伝送のステップのために、追加の上位コンピュータを開発する必要があるのでしょうか?例えば、PCは画像データをどのような形式で送信すべきか、サブボードから返された応答データをどのように解析すべきか、そしてどのように相互作用すべきか、といった点です。 Re: RT1064 Online Upgrade Plan いくつか質問があります。 1. mcuXpressIDEから直接コンパイルしたbinのファームウェアは使えませんか?nxpimageを使わなければならないのですか? 2. サブボードのアップグレードを完了するには、MCUの起動モードを切り替え、自社の上位コンピュータソフトウェアでチャネルを切り替える必要があるようです。つまり、私たちは自分たちの上層コンピュータとblhostソフトウェアを同時に使わなければなりません。4つのサブ基板をアップグレードすると、頻繁に切り替えが少し面倒になることがあります 3. BLhostがサブボードと通信するには、まずマザーボードのTCPが透過モードに入る必要があります。操作が完了した後、マザーボードを透過モードからTCP受信モードに切り替え、サブボードが通常の起動モードに入るようにするにはどうすればよいのでしょうか 4. blhostのソースコードに新しいTCP送信モジュールを追加します - 例はありますか? 5. マザーボード上でシリアルポートの透過伝送を実現するための提案はありますか?例えば、DMAの使用や割り込みとブロッキングの実装など。
記事全体を表示
Inline ECC validation method Hello,  I am working on Inline ECC implementation for iMX8M Plus on external DDR memory. ECC appears to be working (U-Boot modifications done, EDAC driver showing up in Linux, /sys/devices/system/edac/mc/mc0/ virtual files are present). I'm looking for ways to test and validate the protection. My understanding is that error injection is not possible into the data itself, and that ECC parity bits must be corrupted instead. AN 13566 section 3.2.9 states : "Further information on this feature is available on request." How can I request this information ? Is there a specific NXP contact/channel for this ? Thank you in advance, Re: Inline ECC validation method Hello, I am implementing Inline ECC on an i.MX 8M Plus with external DDR. ECC appears to be working correctly: U-Boot has been configured, the Linux EDAC driver is active, and /sys/devices/system/edac/mc/mc0/ is present. I would now like to validate the ECC protection by deliberately generating correctable and uncorrectable errors. AN13566, section 3.2.9, states that Inline ECC errors can be injected by unlocking the ECC region using ECC_REGION_PARITY_LOCK and overriding the ECC parity bits. It also mentions that further information on this feature is available on request.  Re: Inline ECC validation method Hello, Sure we can provide it, but for this I would require you to create a support ticket https://support.nxp.com/s/?language=en_US You may mention me in the body of the request so I can track the ticket and provide the material. Best regards/Saludos, Aldo.
記事全体を表示
MIMXRT1176 ADP – SEGGER J-Link のデバッグの問題 こんにちは、皆さん 現在、 MIMXRT1176 / i.MX RT1170プラットフォーム を使っています 。最初 は MIMXRT1170-EVKB を使って 開発していましたが、現在 は 並列RGBパネルのインターフェース用 に MIMXRT1176-ADP に切り替えました。 ADPボード上でSEGGER J-Linkデバッグを 行う際に問題が発生しています 。 環境: ボード: MIMXRT1176-ADP ボード改訂: 700-51950 REV A1 回路図改訂版: SCH-51950 REV B1 MCUXpresso IDE: v25.6.136 MCUXpresso SDK: v25.09.00 SEGGER J-Link:最新バージョン EVKB では 、 J-LinkとLinkServerの両方が問題なく動作しました 。しかし、ADPでは次の問題が発生しました。 ファームウェアの書き込みに成功しました。 デバッガーはmain()の最初の行に到達しました。 私が 一度 ステップオーバーする と、次の場所で停止します。 デバッグ情報がない、またはプログラムコード外のアドレス「0xdeadbeee」でブレークします。 他の場所にあるブレークポイントは正常に機能し、正しくヒットします。 しかし、 ブレークポイントからの 再開/継続では、 再び 0xDEADBEEE が発生します 。 MIMXRT1176-ADPのMCUXpresso IDEでJ-Linkが完全にサポートされている か 、また特定の J-Linkスクリプト、リセット/デバッグ設定、またはADP固有の初期化 が必要かどうか 、誰か確認していただけます か? これは メモリ構成、外部フラッシュ/SDRAM、あるいは ADPの 起動コード に関連しているのでしょうか? ADP用のJ-Link設定に関するガイダンスや動作確認済みの設定情報があれば、大変ありがたいです。 よろしくお願いします! Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue こんにちは、 @HasanIqbalKhan さん。 ご質問ありがとうございます! 私の知る限り、MCUXpresso IDEでRT1170-ADPを使ってJLinkを使う場合、サポートされるのは「attach」のみで、直接デバッグはサポートされていません。これはおそらくJLinkフラッシュローダーのサポート問題でしょう。IARでは、この問題は解決済みです。ご迷惑をおかけして申し訳ございません。 よろしくお願いします、 ギャビン Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue USB(J33)経由でデバッグを行うことは可能ですか? Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue もう一つ試したのは、外部のMCU-Linkを接続し、MCUXpresso IDEのLinkServer経由でデバッグを試みたことです。 実行はmain関数に到達し、そこからステップ実行できますが、実行を再開しようとすると「アドレス「0x0」でブレークしました。デバッグ情報がありません。またはプログラムコード外です。」というエラーが表示され、また、実行を再開しようとすると「アドレス「0x2230c8」でブレークしました。デバッグ情報がありません。またはプログラムコード外です。」というエラーが表示される場合もあります。 参考までに、私は「MIMXRT1176_dashboard_bt_ble_multiprofile」プロジェクトを実行しようとしています。ボード上のSW1は01に設定され、ボード上のSW5は000000000000に設定されています。 EVKBボードも同じ動作なのでMCU-Linkでテストしてみました。 また、Jlinkは使えないと思います。彼らのウェブサイトにはADPボードが使っているオクタルフラッシュのサポートがないと明記されているからです。 ありがとう。 Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue こんにちは、 @HasanIqbalKhan さん。 1. J33はUSB-OTG1で、デバッグには使用できません。 2. JLinkがオクタルフラッシュをサポートしていないわけではありません。ただデフォルトではEVK/EVKBのフラッシュのみを認識しているだけです。IARに関しては、対応するダウンロードアルゴリズムが提供されているため、このような対応が可能となっています。このテーマに興味があれば、RT-UFLプロジェクトを参照してください。 3. 現在のデバッガ/IDEサポートに関する情報は、AN14387: を参照してください https://docs.nxp.com/bundle/AN14378/page/topics/download_images_to_ADP_board.html よろしくお願いします、 ギャビン
記事全体を表示
S32K3 浮点配置 各位团队成员,大家好! 在我的项目中,我尝试使用浮点数据进行算术运算,但计算结果并未按预期进行。 #define 宏 -31.374 当我尝试使用 UTILS PRINTF 函数在宏中打印值时,我得到的是 -32.374。类似地,其他值的值也递增 1。 正因如此,我的计算结果才没有按预期进行。 我需要为此修改什么配置文件吗? 我目前的目标设定 nirmal_masilamani_0-1790009448678.pngnirmal_masilamani_0-1790009448678.png Re: S32K3 Floating point cfg 你好@nirmal_masilamani 请问您能否解释一下“UTILS PRINTF”是什么意思? 你是如何进行计算的?结果是否存储在浮点变量中?如果是,那么在调试器中查看变量时,该变量是否已经包含错误的值,还是只有在打印该变量时才会出现问题? BR,VaneB Re: S32K3 Floating point cfg 你好@VaneB , 感谢您的支持,是的,问题出在 PRINTF 函数上,调试时我能够读取到正确的数据。
記事全体を表示