2414991_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2414991_en-US

2414991_en-US

i.MX95 19x19 EVK – M2-JODY-W6 Wi-Fi Card Availability and Camera Module Compatibility

Hello NXP Team,

We are working with the NXP i.MX95 19x19 EVK (IMX95LPD5EVK-19) for an Android Automotive OS project.

We would like to get clarification on the following:

1. M2-JODY-W6 Wi-Fi Card

The M2-JODY-W6 Wi-Fi card is not included in our i.MX95 EVK kit.

Could you please provide information on:
- Availability of the M2-JODY-W6 Wi-Fi card
- How we can obtain/purchase the card
- Whether NXP provides a sample or recommended ordering channel
- Any required documentation or compatibility information for the i.MX95 19x19 EVK

2. Camera Module Compatibility

We would also like information about a camera module officially supported/validated with the i.MX95 19x19 EVK.

Could you please provide:
- Recommended/validated camera module
- Exact module/part number
- Camera sensor used
- Hardware connection/interface information
- Relevant documentation
- Linux/Android driver or software support information
- Any available reference design or configuration information

Board:
NXP i.MX95 19x19 EVK
Part Number: IMX95LPD5EVK-19

Software:
Android Automotive OS 16
NXP BSP

We would appreciate your guidance on the above questions.

Thanks and Regards,
Gnana Prasanna Gunakala

Re: i.MX95 19x19 EVK – M2-JODY-W6 Wi-Fi Card Availability and Camera Module Compatibility

Hello, 

For your first question please open a technical case, for the second question please refer to the following AN: https://www.nxp.com/docs/en/application-note/AN14853.pdf 

Regards.

标记 (1)
无评分
版本历史
最后更新:
星期四
更新人: