2394645_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2394645_en-US

2394645_en-US

lowlight opensource ai-isp test on imx95

 

    There are many open-source low-light AI-ISP models. The table below is a comparison table provided by Copilot. 


Algorithm

GitHub

Type

i.MX95 NPU Suitability

FPGA Suitability

MSR (Retinex)

jsrsinchana/.../MSR-algorithm

Non-AI (ISP)

Medium

Very High

Zero-DCE++

arnabroy734/low_light_enhancement

Lightweight CNN + Curve

Very High

Very High

RetinexNet

weichen582/RetinexNet

CNN (Retinex)

Medium

High

EnlightenGAN

VITA-Group/EnlightenGAN

GAN (CNN)

Very High (lite)

Low

FLOL

cidautai/FLOL

Lightweight CNN

High

Low

SNR-aware

JIA-Lab-research/SNR-Aware

Transformer + CNN

Low

Low

KinD

zhangyhuaee/KinD

Retinex + CNN

Medium

Medium

RetinexNet-lite

Derived

Light CNN

Medium

High

EnlightenGAN-lite

Derived

Small CNN

Very High

Low

Fast LLIE CNN

Various

Small CNN

High

Medium



We selected some open-source models and used UVC to perform performance tests on the exip-os08a20 module with no HDR mode. We found that SCI(GitHub - vis-opt-group/SCI: [CVPR 2022] This is the official code for the paper "Toward Fast, Flexib...) computation is relatively small, low-light performance is good in subjective evaluations, and it can basically run on the IMX95. The testing method involves copying the tflite file and test script to the /root/ directory of the IMX95 and running the following command: `python3 test_sci_cvpr_illu_imx95_int8.py --model sci_tpami_illu_imx95_int8.tflite`. The comparison interface shown below is displayed.

Image (7).jfifImage (7).jfif





タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-13-2026 11:07 PM
更新者: