Hello NXP Team,
I am integrating a TensorFlow Lite Micro model into my MCUXpresso project for the MCXN947. My application is written in C, while the TensorFlow Lite Micro inference code and generated model are in C++.
I am encountering compilation and linking issues when combining the C and C++ source files. I have already tried using "extern C", but the issue remains.
Could you please advise on the following?
Is it recommended to mix C and C++ source files in an MCUXpresso project?
What is the recommended approach for integrating a C++ TensorFlow Lite Micro model into a C-based application?
Are there any required compiler/linker settings or reference examples for this integration?
Any guidance would be greatly appreciated. Thank you.
Hello @sivamankomb ,
Thanks for your post.
Of course you can mix C and C++ source files in an MCUXpresso project. In fact, this is also the approach used in our SDK demos. For reference, you can review several eIQ-related example projects included in the SDK. The SDK is available for download from Select Board | MCUXpresso SDK Builder.
Celeste_Liu_0-1784012914332.png
The key points are as follows:
- .c files are compiled as C code.
- .cpp files are compiled as C++ code.
- The final linking stage must use a toolchain that supports the C++ runtime and C++ symbol resolution.
- C code should only call functions exposed through extern "C" wrappers and should not directly include or use TFLM C++ classes, templates, or namespaces.
Therefore, the recommended approach is to encapsulate the TFLM inference implementation in a .cpp file and expose only a C ABI-compatible wrapper interface to the C application.
For example, in the SDK's tflm_label_image demo, the core TFLM inference logic is implemented in common/tflm/model.cpp. This file uses the TFLM C++ APIs, such as
#include "tensorflow/lite/micro/micro_interpreter.h"
#include "tensorflow/lite/micro/micro_op_resolver.h"
static const tflite::Model* s_model = nullptr;
static tflite::MicroInterpreter* s_interpreter = nullptr;
extern tflite::MicroOpResolver &MODEL_GetOpsResolver();
Then creating a tflite::MicroInterpreter instance and calling AllocateTensors() within MODEL_Init() to perform initialization.
The externally exposed model.h, provides a C-friendly interface.
#if defined(__cplusplus)
extern "C" {
#endif
status_t MODEL_Init(void);
uint8_t* MODEL_GetInputTensorData(tensor_dims_t* dims, tensor_type_t* type);
uint8_t* MODEL_GetOutputTensorData(tensor_dims_t* dims, tensor_type_t* type);
void MODEL_ConvertInput(uint8_t* data, tensor_dims_t* dims, tensor_type_t type);
status_t MODEL_RunInference(void);
const char* MODEL_GetModelName(void);
#if defined(__cplusplus)
}
#endif
The function declarations are exported through extern "C", allowing C source files to simply #include "model.h" and call functions such as MODEL_Init() and MODEL_RunInference() without needing any knowledge of C++ types like tflite::MicroInterpreter or MicroMutableOpResolver.
This architecture is also the approach adopted by our SDK examples and is generally recommended when integrating TFLM into a C-based application, as it cleanly isolates the C++ implementation details while preserving a pure C interface for the application layer.
If you want to integrate customer ML model to SDK demo, you can refer to AN14241 .
Hope it helps.
BR
Celeste