Query Regarding OTP Programming of FS2643D Blank OTP Variant Hi, I am planning to use the FS2643D variant, specifically the MFS2643HMDA0AD blank OTP variant, for my 24 V application. I understand that the KITFS26SKTEVM socket board can be used for OTP configuration and programming. However, using the socket board may complicate the workflow, as the IC needs to be placed in the socket for programming and then soldered onto the target PCB. Is there an alternative method to configure and program the OTP directly on the target PCB using an external programmer or target board, without requiring the KITFS26SKTEVM socket board? Could you please advise whether this approach is supported and recommend a suitable solution? https://www.nxp.com/part/MFS2643HMDA0AD Thanks. Re: Query Regarding OTP Programming of FS2643D Blank OTP Variant Hi Sakshi,
for prototyping, using the socket board, our other hardware and the NXP Ringo GUI is recommended for benchmarking. For designing your prototype board, please follow the FS26 datasheet and our other documents. Especially the AN12995.
To be able to download these confidential documents, you need to have a valid NDA with NXP. If you have not an NDA yet and you would like to sign one, please create a new ticket here and an NXP representative for NDA matters will help you with the process.
Without the FS26 datasheet and other confidential documents would not be possible to work with the FS26.
Once you will have your prototype schematic, we can check it for you. Please note, we do not check layouts. Alternatively you can contact our authorized distributors, they have engineers who can also check the schematic for you.
With Best Regards,
Jozef Re: Query Regarding OTP Programming of FS2643D Blank OTP Variant Hi Jozef, Thank you for the feedback. Since we are currently in the prototyping phase, our initial volume count is low, and we are focused strictly on bench evaluation and system validation. Given that this is a low-volume prototype phase, could you let us know how you recommend we proceed for our initial boards? Do you recommend we work with an authorized distributor (such as Arrow or Avnet) to get a small batch programmed, or is there an alternative path you suggest for early benchmarking? We want to ensure we align with NXP’s safety and validation guidelines while we bring up our custom target prototype. Best regards, Re: Query Regarding OTP Programming of FS2643D Blank OTP Variant Hi Sakshi,
please note, that our evaluation boards and socket boards are designed and recommended to be used for evaluation of our components only. OTP programming of our components are allowed only by NXP or by our authorized distributors. Depending on annual volume of the specific component. Please let me know your annual volume for your project using the FS2643D Blank OTP Variant.
We do not allow to program the OTP of our components by our customers. If customers will program themselves, then we do not guarantee safe and correct function of such components.
With Best Regards,
Jozef
View full article