2403844_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2403844_en-US

2403844_en-US

MPXM2053GS air leakage

We have assembled MPXM2053GS pressure sensors onto our PCB. During initial testing, a number of units were found to have an output voltage of 0V, which we guess is due to air leakage. After removing the defective devices from the board, we inspected the bottom vent holes and found that they differ visibly from those of the good units. Specifically, the interior of the vent holes on the failed parts appears to contain melted or heat-damaged material. What is the possible root cause of this defect?

Re: MPXM2053GS air leakage

Hi David,

The most effective prevention is to define a solder paste exclusion zone on your PCB stencil directly beneath the vent hole location. This ensures no paste is deposited in that area and cannot be drawn into the hole during reflow. Additionally, using a no-clean flux minimizes residue that could otherwise migrate into the opening.

For further support, I would recommend contacting STMicroelectronics directly, as they are the current owner of the MPXM2053 and are best positioned to provide support.

BRs, Tomas

Re: MPXM2053GS air leakageDo you have any suggestion how to prevent solder paste or flux intrusion from entering the bottom vent?Re: MPXM2053GS air leakage

Hi David,

The melted/heat-damaged material inside the vent holes is most likely caused by solder paste or flux intrusion during reflow soldering or by exceeding the maximum permitted peak package body temperature of 250°C (max. 30 seconds). Since the MPXM2053GS is a vented gauge sensor that uses the bottom vent as its atmospheric reference, any blockage of that hole will cause a loss of reference and result in 0V output.

One additional note for your awareness: as of February 2, 2026, NXP MEMS sensor products — including the MPXM2053 series — have been transitioned to STM. For formal failure analysis or ongoing product support, STM is the appropriate contact.

BRs, Tomas

Re: MPXM2053GS air leakage

Hi, 

We decapped a zero-output unit and found the die inside was cracked. Is this crack caused by a foreign object, or are there other contributing factors? We suspect the pick-up nozzle might be the culprit, since it directly contacts the inlet port; however, we're uncertain whether the nozzle pressure is high enough to fracture the die.

Tags (1)
No ratings
Version history
Last update:
‎08-20-2026 03:29 AM
Updated by: