Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board In MCXNx4x, SmartDMA can be used to implement the Camera interface. According to the MCXNx4x DataSheet, the Pinmux Assignments of Ethernet and SmartDMA conflict. For this reason, I thought that Ethernet and Camera could not be used at the same time. However, the FRDM-MCXN947 Board User Manual (UM12018) states the following: > If Ethernet functionality is still desired while using the camera, an alternative workaround is to move the SJ16 and SJ26 jumpers from their default position. Is there any way to use Ethernet and camera at the same time? Development Board MCXN Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board Hi @dubian1shu  I have rechecked the content of the document and confirmed that there is an issue with the description in the document. We will make timely changes to the document. SmartDMA (EZH_CAMERA) and Ethernet (ENET) can be used at the same time, but you need to find some pins that are not shared for the camera to use. You can refer to this article. MCX N947: Simultaneous Implementation of Ethernet and Camera Functions - NXP Community Hope this will help you. BR Hang Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board Thanks for checking and replying @Harry_Zhang  Since SmartDMA supports P1_X and P3_X, I understand that MCXNx4x can use SmartDMA and Ethernet functions at the same time. But can I use SmartDMA and Ethernet functions using FRDM-MCXN947? J9 (Camera Header) of FRDM-MCXN947 has seven pins that conflict with Ethernet pins. The solution for P1_4 described in the FRDM-MCXN947 board user manual (UM12018) only solves one of them, and does not mention the other six conflicts. For example, P1_5, P1_13, and P1_15 are in conflict between SmartDMA and Ethernet. As far as I can see from the schematic document (SCH-90818), there seems to be no solution to resolve this conflict. Is there a way to use SmartDMA (EZH_CAMERA) and Ethernet (ENET) at the same time on FRDM-MCXN947? Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board Hi @dubian1shu  I checked the MCXNx4x DataSheet, there are indeed some pins Ethernet and SmartDMA conflicting. But if you want to use the Ethernet and SmartDMA at the same time. you can choose some pins that do not conflict with Ethernet and SmartDMA. For example, you can choose the P3_X as the SmartDMA pin, and choose the P1_X as the Ethernet pin. And move the jumper referring to the FRDM-MCXN947 Board User Manual (UM12018). Hope this will help you. BR Hang
記事全体を表示
S32K312 PLL_LOL Problem Hi NXP,     We found S32K312 will reset while  doing (ESD)Air discharge ±15kV test. And we found reset reason is PLL_LOL. Then we use NXP S32K312EVB-Q172 to do the same test, it will reset too.    We try to change GM_SET register to improve crystal diver strength,but it has no improvement. And we try to set DCMRWP3[9] to 1, S32K will not reset when PLL_LOL,but mcu will stop, only reset can recover it.    We need S32K3 keep running while the ESD test. Can cpu clock switch to FIRC while PLL_LOL? Could you give me some suggestions,Thanks! Re: S32K312 PLL_LOL Problem Hi Daniel,     Thanks,disable automatic level controller can slove this problem. Re: S32K312 PLL_LOL Problem What do you mean by higher-power oscillator? Did you disable the automatic level controller (FXOSC_CTRL[ALC_D] = 1)? BR, Daniel Re: S32K312 PLL_LOL Problem Hi @danielmartynek ,   Thanks for your reply. CMU is disable and I am sure the reset reason is PLL Loss of Lock. When PLL LOL,MCU will reset. When set DCMRWP3[9] to 1, mcu will not reset while PLL LOL but mcu will stop running. Thus we cannot change the system clock back to FIRC when PLL LOL. We try to replace the Crystal Oscillator with a higher-power one, it seems better. Re: S32K312 PLL_LOL Problem Hi @zhengjianfei1, Are you sure the FXOSC is that cause of the PLL Loss of Lock? Do you have the FXOSC clock monitor enabled? It could be just the PLL. Is the lastmile regulator enabled? You could try to change the system clock back to FIRC within the interrupt. MUX_0_CSC[SAFE_SW] = 1 Regards, Daniel
記事全体を表示
i.MX95 上的 dm-eiq-genai-flow 演示器需要电路板支持包版本 嗨,团队、 我正在探索 i.MX95 平台上的 dm-eiq-genai-flow-demonstrator(GenAI Flow),它在 Yocto 环境中运行。请您澄清一下: 1.端到端运行演示版的最低要求是哪个电路板支持包(例如 L6.12.20_2.0.0)? 2.此电路板支持包是否包含支持 LLM 推理 (RAG) 的所有必要元素,例如更新的 Neutron 委托、TfLite 运行时和工具? 3.这个演示中还有其他推荐的 Yocto 元层或图像配方(例如 meta-eiq-genai)吗? 预先感谢您的真知灼见! 致以最崇高的敬意, Varshil Gandhi Re: BSP Version Required for dm-eiq-genai-flow-demonstrator on i.MX95 你好 Varshil, 谢谢你的提问。 让我试着回答他们: 1.该代码包最初是为第一季度的 电路板支持包。 L6.12.3-1.0.0 制作的,适用于 i.MX95 修订版 Ax。 2。本第一季度的 电路板支持包。 不直接包括在 LLM 推断中利用中子所必需的内容。这就是该代码包提供元层的原因。 3.这个 meta-eiq-genai-flow 元层提供了添加 Onnxruntime 中子执行提供程序的可能性,以加速 Neutron 上的 LLM 操作并释放一些 CPU 资源,以及内核和 Neutron Fw 的相关补丁/文件。请注意,我们在这个项目中使用的是 onnxruntime 而不是 TF 精简版。 话虽如此,第二季度电路板支持包。(例如L6.12.20_2. 0.0)将于今天发布。它支持 i.MX95 的 B0 版本,但没有 Neutron 上的 LLM 加速,只有 CPU 模式可以运行。 谢谢,并致以最崇高的敬意、 皮埃尔
記事全体を表示
S32K3xx SpiBaudrateConfigRef set Hi, Configuration Components for SDK Peripheral Drivers— LPSPI: 1. Lpspi → SpiExternalDevice → SpiUseBaudrateConfig → SpiBaudrateConfigRef? What is the purpose of this setting, and how do you configure it? 2. What is the difference between SpiUseBaudrateConfig and SpiCalculatedBaudRate for SPI baud rate selection? 3. I need a user-friendly way to configure the SPI baud rate. How can I do that? Regards, Karmegan C Re: S32K3xx SpiBaudrateConfigRef set Hi @daniel_ll, I've sent you a private message regarding this issue. Re: S32K3xx SpiBaudrateConfigRef set Hi Julián, Do you have a link to the Jira bug? And/or more info about in what RTD release this will be fixed? Facing the same issue with RTD 5.0.0 Re: S32K3xx SpiBaudrateConfigRef set Hi @karmegancjk I've confirmed with the internal team, and this is a bug. It is planned to be fixed in the next RTD release. Best regards, Julián Re: S32K3xx SpiBaudrateConfigRef set Hi @karmegancjk, Apparently, only the MCAL Spi component generates a valid SpiBaudRateConfigRef value. I did not notice this since I was basing the project in MCAL and not IP: I think this is not intended, so for now, either configure the SPI component without the "UseBaudrateConfig" parameter or with the MCAL component to generate the reference. I will ask internally to see if this is expected behavior. Best regards, Julián Re: S32K3xx SpiBaudrateConfigRef set Hi, I am not able to assign SpiBaudrateConfig_0 to SpiBaudrateConfigRef in Lpspi Driver. IDE : S32DS 3.5.13. RTD : R22_11 V4.0.0. How do I set the path of SpiBaudrateConfig_0 in SpiBaudrateConfigRef? Re: S32K3xx SpiBaudrateConfigRef set Hi @karmegancjk, All of the configuration parameters are described inside the respective driver user manual. Under "C:\NXP\S32DS.3.6.1\S32DS\software\PlatformSDK_S32K3\RTD\Spi_TS_T40D34M50I0R0\doc" you can find RTD_SPI_UM.pdf.  1. SpiBuadrateConfigRef is the reference node used in order to calculate the Spi baud rate. 2. SpiUseBaudrateConfig uses the reference node, SpiCalculatedBaudRate uses the following formula: SpiCalculatedBaudrate = Function clock / (SpiPrescalerValue * (SpiScaler + 2)) 3. You can use the existing example "Spi_Transfer_S32K344" to use as base. Also, chapter 3.6.13 of the previously mentioned file shows how to configure baud rate: Best regards, Julián
記事全体を表示
S32G-VNP-RDB32 (SJA1110) 交换机中的寄存器访问 你好, 我想把值写进寄存器你能不能给我一个完整的地址来 读写地址 名称访问RESET描述 8Ch DYN_BE_LKP_ ENTRY0 R/W 0h (ffffFFe h) 8ch 之前的基址是什么?比如它会有 0x3fc0008c 所以在这个动态入口表中我们会有完整的地址你能不能给我 8Ch DYN_BE_LKP_ ENTRY0 R/W 0h (fffffF eh) 90h DYN_BE_LKP_ ENTRY1 R/W 0h 94h DYN_BE_LKP_ ENTRY2 R/W 0h 98h DYN_BE_LKP_ R/W 0h 98h DYN_BE_LKP_ ENTRY3 R/W 0h 9Ch DYN_BE_LKP_ ENTRY4 R/W 0h a0h a0h DYN_BE_LKP_ ENTRY5 R/W 0h A4H DYN_BE_LKP _CTRL R/W 0h (ff800000H) 你能不能给我提供在寄存器中配置动态条目的完整地址? 以及需要在 SJA1110 Switch 中实现此功能的地方 Re: Register Access in S32G-VNP-RDB32 (SJA1110) Switch 你好@Atkinson、 我知道这乍看起来可能并不简单,但实际上这个概念非常简单。 最终的寄存器地址取决于访问方法--是通过 AHB 在内部访问 M7 内核,还是通过 SPI_AP 接口从外部访问。基本地址因接入点而异。 寄存器地址使用 UM11107 表 2 中提供的基地址计算。例如,对于交换机子系统,SPI_AP 访问的基地址为0x00000000 ,AHB 访问的基地址为0xFF000000 。 在这种情况下,通过 AHB 访问寄存器0x8C (DYN_BE_LKP_ENTRY0)时,寄存器会变成0xFF00008C 。 现在,可能会让人感到困惑的地方来了:SDK 驱动程序定义了以下内容: #define SJA1110_L2_ART_LE_ADDR(0x3fc00023) /**< l2ArtLockedEntry 寄存器的地址 *   SWITCH_DRV_Write 例程将地址左移 2 位 (<< 2),用于内部 (AHB) 访问。对于 SPI 传输(级联开关设置中使用),不应用移位。因此,0x3fc00023 << 2 的结果是0xFF00008C。   我希望通过上面的解释,现在有感知了。   顺祝商祺! 帕维尔
記事全体を表示
i.MX95 上の dm-eiq-genai-flow-demonstrator に必要な BSP バージョン こんにちは、チーム 私は、Yocto 環境内で動作する i.MX95 プラットフォーム上の dm-eiq-genai-flow-demonstrator (GenAI Flow) を調査しています。以下を明確にしていただけますか: 1.デモをエンドツーエンドで実行するために最低限必要な BSP バージョン (例: L6.12.20_2.0.0) は何ですか? 2.この BSP には、LLM 推論 (RAG) をサポートするために必要なすべての要素 (更新された Neutron デリゲート、TFLite ランタイム、ツールなど) が含まれていますか? 3.このデモに推奨される追加の Yocto メタレイヤーまたはイメージレシピ (たとえば、meta-eiq-genai) はありますか? ご意見をよろしくお願いします! よろしくお願いします、 ヴァルシル・ガンジー Re: BSP Version Required for dm-eiq-genai-flow-demonstrator on i.MX95 こんにちは、ヴァルシルさん。 ご質問ありがとうございます。 それらの質問に答えてみたいと思います。 1. このパッケージは当初、i.MX95 rev Ax の Q1 BSP L6.12.3-1.0.0 用に作成されました。 2. このQ1 BSPには、LLM推論でNeutronを活用するために必要な機能が直接含まれていません。そのため、このパッケージはメタレイヤーを提供しています。 3. この meta-eiq-genai-flow メタレイヤーは、Neutron 上の LLM 操作を高速化し、CPU リソースの一部を解放するための Onnxruntime Neutron 実行プロバイダーを追加する可能性を提供します。これにはカーネルと Neutron Fw 用の関連パッチ/ファイルが含まれます。なお、このプロジェクトでは TF Lite ではなく onnxruntime を使用しています。 とはいえ、 Q2 BSP (例:L6.12.20_2.0.0)が本日リリースされます。i.MX95のB0リビジョンをサポートしていますが、NeutronのLLMアクセラレーションが利用できないため、CPUモードのみで動作します。 ありがとう、そしてよろしく。 ピエール  
記事全体を表示
問い合わせ: S32N55 システム電源モード API こんにちは、チームの皆さん FSS は、システムの電源モードを設定するために使用できる 2 つの API をサポートしていることがわかりました。 A1、Scmi_SystemPowerRequestProtocolMessageAttributesSynch A2、Scmi_PowerRequestSystemModeSynch また、A1 はコホート モードと状態の設定にもCAN。ただし、コホート状態を設定するための専用のコホート API があります (例: Scmi_BtmWarmResetCohortSynch、Scmi_BtmSuspendCohortSynch)。 A1 API の機能は他の 2 種類の API と重複しているようです。 質問です。A1 APIは何に使われるのでしょうか? あるいは、どのようなシナリオで使われるのでしょうか? よろしくお願いいたします。 唐生。 FSS_FW 優先度: 中 Re: Inquiry: S32N55 system power mode APIs ありがとう、マリウス。混乱を非常にわかりやすく説明してくれました。 Re: Inquiry: S32N55 system power mode APIs こんにちは@Tangsheng_Zhouさん パワー ドメイン プロトコルとブート プロトコルは、Tunis に追加された元のプロトコルです。さまざまな理由から、これは Tunis の使用事例には適していましたが、SCMI 仕様とは完全には互換性がありませんでした。その結果、Luxor プラットフォームのサポートを追加するとともに、ARM SCMI 準拠のシステム パワー プロトコルも追加しました。そのため、重複が生じています。 実装と将来のサポートに関しては: - Scmi_SystemPowerStateSetSynch( ) などの API は、Btm_* API のラッパーとして実装されており、両方ともサポートされ、両方ともまったく同じことを行います。AUTOSAR/Tunis ユーザーは既存の Btm API を使用できますが、Linux では新しい SystemPower API を使用することが予想されます。 Scmi_PowerRequestSystemModeSynch などの PowerDomain プロトコルの API は廃止される予定であり、いずれにしても、SystemPower の新しい SCMI 互換 API を使用することをお勧めします。 社内には、ユーザーマニュアルの更新と説明を追跡するためのチケットがあります。FSF-29425 ありがとうございます マリウス
記事全体を表示
OTPミラーレジスタマップ 件名: PF5020 OTPミラーレジスタマップドキュメントのリクエスト こんにちは、 現在、PF5020 PMIC と NXP コントローラ間の通信に取り組んでいます。PF5020 データシートを確認したところ、OTP 構成に関連するレジスタ アドレスやピン レベルの説明など、OTP ミラー レジスタ マップに関する詳細情報は見つかりませんでした。 必要な出力電圧は1.1V、1.8Vです3.3V この情報は別の文書で入手できるかどうか教えていただけますか?これは、システム内の OTP 関連の設定を正しく解釈して構成するために不可欠です。 ご指導や、共有していただける関連ドキュメントがあれば、ぜひお知らせください。 お手数ですが、よろしくお願いいたします。 シヴァニ Re: OTP mirror register map こんにちは、 PF5020 データシートのセクション 16.1 には、次の内容を含む完全な OTP ミラー レジスタ マップが記載されています。 - アドレスを登録する - 次のような構成フィールド: 降圧出力電圧用のOTP_VSWx LDO出力電圧用のOTP_VLDOx 電源投入シーケンス用のOTP_SWx_SEQ パワーダウングループ化用のOTP_SWx_PDGRP 電流制限設定用のOTP_SWxILIM UV/OVしきい値用のOTP_SWxUV_THとOTP_SWxOV_TH VDDOTP ピンは、デバイスが次から構成をロードするかどうかを決定します。 - OTPヒューズ(VDDOTP = GNDの場合) - ハードワイヤードデフォルト(VDDOTP = V1P5Dの場合) TBBEN ピンは Try-Before-Buy (TBB) モードを有効にし、ヒューズ プログラミングをコミットする前に OTP 設定を一時的に構成およびテストできるようにします。 お客様による本番環境での OTP プログラミングは許可されていないことに注意してください。これを実行できるのは、NXP または認定パートナー (少量) のみです。開発中は、KITPF502xSKTEVM を CAN 使用できます。 PF5020 を 1.1V、1.8V、3.3V に設定するには、次のようにします。 - OTP_VSWxまたはOTP_VSWND1を1.1Vおよび1.8Vの適切な値に設定します - 電流要件に応じて、OTP_VLDO1 または OTP_VSWND1 を 3.3V に設定します。 これらの値は OTP ミラー レジスタでプログラム可能であり、コミITする前に TBB モードでテストできます。 BRs、トーマス
記事全体を表示
S32K3xx SpiBaudrateConfigRef 设置 您好, SDK 外设驱动程序的配置元器件— LPSPI: 1.Lpspi → SpiExternalDevice → SpiUseBaudrateConfig → SpiBaudrateConfigRef?此设置的目的是什么,如何配置? 2.在 SPI 波特率选择方面,SpiUseBaudrateConfig 和 SpiCalculatedBaudRate 有什么区别? 3.我需要一种方便用户的方法来配置 SPI 波特率。我该怎么做? 此致, 卡尔梅根 C Re: S32K3xx SpiBaudrateConfigRef set 你好,我是@daniel_ll、 关于这个问题,我已经给您发送了一条私人信息。 Re: S32K3xx SpiBaudrateConfigRef set 你好,胡利安、 你有 Jira 错误的链接吗?和/或有关将在哪个RTD版本中修复此问题的更多信息?使用 RTD 5.0.0 时遇到同样的问题 Re: S32K3xx SpiBaudrateConfigRef set 你好@karmegancjk 我已与内部团队确认,这是一个错误。计划在下一个RTD版本中对其进行修复。 致以最诚挚的问候, Julián Re: S32K3xx SpiBaudrateConfigRef set 嗨,@karmegancjk、 显然,只有 MCAL Spi 元器件会生成有效的 spibaudrateConfigref 值。我没有注意到这一点,因为我是以 MCAL 而不是 IP 作为项目基础的: 我认为这不是故意的,所以就目前而言,要么在没有 " useBaudrateConfig " 参数的情况下配置 SPI 元器件,要么使用 MCAL 元器件来生成参考。我会向内部询问这是否是预期行为。 致以最诚挚的问候, Julián Re: S32K3xx SpiBaudrateConfigRef set 您好, 我无法在 Lpspi 驱动程序中将 SpiBaudrateConfig_0 分配给 SpiBaudrateConfigRef。 ide : s32ds 3.5.13. rtd : r22_11 v4.0.0. 如何在 SpiBaudrateConfigRef 中设置 SpiBaudrateConfig_0 的路径? Re: S32K3xx SpiBaudrateConfigRef set 嗨,@karmegancjk、 所有配置参数都在相应的驱动程序用户手册中有所说明。Under"C:\NXP\S32DS.3.6.1\S32DS\software\PlatformSDK_S32K3\RTD\Spi_TS_T40D34M50I0R0\doc"您可以找到RTD_SPI_UM.pdf。 1。SpiBuadrateConfigRef 是用于计算 Spi 波特率的参考节点。 2。SpiUseBaudrateConfig 使用参考节点,SpiCalculatedBaudRate 使用以下公式: SpiCalculatedBaudrate = Function clock / (SpiPrescalerValue * (SpiScaler + 2)) 3.您可以使用现有示例"Spi_Transfer_S32K344" 作为基础。此外,前面提到的文件第 3.6.13 章介绍了如何配置波特率: 致以最诚挚的问候, Julián
記事全体を表示
BSP Version Required for dm-eiq-genai-flow-demonstrator on i.MX95 Hi Team, I’m exploring the dm-eiq-genai-flow-demonstrator (GenAI Flow) on the i.MX95 platform working within a Yocto environment. Could you please clarify:      1. Which BSP version (e.g., L6.12.20_2.0.0) is minimum required to run the demo end-to-end?     2. Does this BSP include all necessary elements—such as updated Neutron delegate, TFLite  runtime, and tooling—to support LLM inference (RAG)?     3. Are there any additional Yocto meta-layers or image recipes (for example meta-eiq-        genai) recommended for this demo? Thanks in advance for your insights! Best regards, Varshil Gandhi Re: BSP Version Required for dm-eiq-genai-flow-demonstrator on i.MX95 Hi Varshil, Thanks for your questions. Let me try to answer them: 1. The package was initially made for Q1 BSP L6.12.3-1.0.0 for i.MX95 rev Ax. 2. This Q1 BSP does not directly include what's necessary to leverage Neutron on LLM inferences. That's why the package provides a meta-layer. 3. This meta-eiq-genai-flow meta-layer provides the possibility to add a Onnxruntime Neutron Execution Provider to accelerate the LLM operations on Neutron and free up some CPU resources, with associated patches/files for Kernel and Neutron Fw. Please note that we are using onnxruntime and not TF lite for this project. That being said, Q2 BSP (e.g., L6.12.20_2.0.0) is being released this days. It supports the B0 revision of i.MX95 but without LLM acceleration on Neutron, only CPU mode is functional. Thanks and best regards, Pierre  
記事全体を表示
在 FRDM-MXCN947 板上同时使用以太网和摄像头 在 MCXNx4x 中,SmartDMA 可用于实现摄像头接口。 根据 MCXNx4x 数据表,以太网和 SmartDMA 的 Pinmux 分配有冲突。因此,我认为以太网和摄像头不能同时使用。 但是,FRDM-MCXN947 板用户手册 (UM12018) 规定了以下内容: > 如果在使用摄像机时仍然需要以太网功能, ,将 SJ16 和 SJ26 跳线从默认位置移开。 有没有办法同时使用以太网和摄像头? 开发板 MCX N Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board 你好@dubian1shu 我重新检查了文件内容,确认文件中的描述存在问题。 我们将及时修改文件。 可以同时使用SmartDMA (EZH_CAMERA) 和以太网 (ENET),但需要找到一些不共享的引脚供摄像头使用。 您可以参考这篇文章。 MCX N947:同时实现以太网和摄像头功能 - NXP 社区 希望能帮到你。 BR 挂 Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board 感谢@Harry_Zhang的检查和回复 由于 SmartDMA 支持 P1_X 和 P3_X,我认为 MCXNx4x 可以同时使用 SmartDMA 和以太网功能。 但使用 FRDM-MCXN947 能否使用 SmartDMA 和以太网功能? FRDM-MCXN947 的 J9(摄像头接头)有七个引脚与以太网引脚冲突。FRDM-MCXN947 主板用户手册 (UM12018) 中描述的 P1_4 的解决方案仅解决了其中一个问题,没有提及其他六个冲突。 例如,P1_5、P1_13 和 P1_15 在 SmartDMA 和以太网之间存在冲突。从原理图文件(SCH-90818)来看,似乎没有解决这一冲突的办法。 有办法在 FRDM-MCXN947 上同时使用 SmartDMA (EZH_CAMERA) 和以太网 (ENET) 吗? Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board 你好@dubian1shu 我查看了MCXNx4x 数据表,确实有一些引脚以太网与 SmartDMA 冲突。但如果你想同时使用以太网和 SmartDMA,可以选择一些以太网和 SmartDMA 不冲突的引脚。 例如,可以选择 P3_X 作为 SmartDMA 引脚,选择 P1_X 作为以太网引脚。 然后参照 FRDM-MCXN947 主板用户手册 (UM12018) 移动跳线。 希望能帮到你。 BR 挂
記事全体を表示
OTP mirror register map Subject: Request for PF5020 OTP Mirror Register Map Documentation Hi, We are currently working on communication between the PF5020 PMIC and an NXP controller. During our review of the PF5020 datasheet, we could not find detailed information regarding the OTP mirror register map, including register addresses and pin-level descriptions related to OTP configuration. The output voltages we need are 1.1v,1.8v and3.3v Could you please advise if this information is available in a separate document? This is essential for us to correctly interpret and configure the OTP-related settings in our system. We would appreciate your guidance or any relevant documentation you can share. Thank you in advance! Shivani  Re: OTP mirror register map Hi, Section 16.1 of the PF5020 datasheet provides a complete OTP mirror register map, including: - Register addresses  - Configuration fields such as:    OTP_VSWx for buck output voltages    OTP_VLDOx for LDO output voltages    OTP_SWx_SEQ for power-up sequencing    OTP_SWx_PDGRP for power-down grouping    OTP_SWxILIM for current limit settings    OTP_SWxUV_TH and OTP_SWxOV_TH for UV/OV thresholds The VDDOTP pin determines whether the device loads configuration from: - OTP fuses (when VDDOTP = GND) - Hardwired defaults (when VDDOTP = V1P5D) The TBBEN pin enables Try-Before-Buy (TBB) mode, allowing temporary configuration and testing of OTP settings before committing to fuse programming. Keep in mind that OTP programming is not allowed in production by the customer. Only NXP or authorized partners (lower volume) should perform this. During development you can use the KITPF502xSKTEVM. To configure the PF5020 for 1.1V, 1.8V and 3.3V, you would: - Set OTP_VSWx or OTP_VSWND1 to the appropriate values for 1.1V and 1.8V - Set OTP_VLDO1 or OTP_VSWND1 to 3.3V, depending on current requirements These values are programmable in the OTP mirror registers and can be tested in TBB mode before committing. BRs, Tomas
記事全体を表示
Register Access in S32G-VNP-RDB32 (SJA1110) Switch Hi, I am looking to write the values into the Register  can you give me the complete address for Reading and writing  Address Name Access Reset Description 8Ch DYN_BE_LKP_ ENTRY0 R/W 0h (FFFFFFFEh) before 8ch  what would be the base address? like for example it will have 0x3fc0008c so for this dynamic entry table we will have a complete address can you give me the complete address for  8Ch DYN_BE_LKP_ ENTRY0 R/W 0h (FFFFFFFEh) 90h DYN_BE_LKP_ ENTRY1 R/W 0h 94h DYN_BE_LKP_ ENTRY2 R/W 0h 98h DYN_BE_LKP_ ENTRY3 R/W 0h 9Ch DYN_BE_LKP_ ENTRY4 R/W 0h A0h DYN_BE_LKP_ ENTRY5 R/W 0h A4h DYN_BE_LKP_CTRL R/W 0h (FF800000h) can you Provide me the full address for configuring the Dynamic Entry in the register ? and where this implementation need to be take place in SJA1110 Switch  Re: Register Access in S32G-VNP-RDB32 (SJA1110) Switch Hello @Atkinson , I understand it might not seem straightforward at first, but the concept is actually quite simple. The final register address depends on the access method - whether you're accessing it internally via the M7 core over AHB, or externally via the SPI_AP interface. The base addresses differ depending on the access point. The register address is calculated using the base address provided in Table 2 of UM11107. For example, for the switch subsystem, the base address is 0x00000000 for SPI_AP access and 0xFF000000 for AHB access. In your case, the register 0x8C (DYN_BE_LKP_ENTRY0) becomes 0xFF00008C when accessed via AHB. Now, here’s where it might get confusing: the SDK driver defines the following: #define SJA1110_L2_ART_LE_ADDR (0x3fc00023) /**< Address of the l2ArtLockedEntry register *   The SWITCH_DRV_Write routine shifts the address left by 2 bits (<< 2) for internal (AHB) access. For SPI transfers (used in cascaded switch setups), no shift is applied. So, 0x3fc00023 << 2 results in 0xFF00008C.   I hope that with the explanation above, it makes sense now.   Best regards, Pavel
記事全体を表示
S32G-VNP-RDB32 (SJA1110) スイッチのレジスタアクセス こんにちは、 レジスタに値を書き込む方法を探しています 読み書きの完全な住所を教えていただけますか? 住所 名前 アクセス リセット 説明 8Ch DYN_BE_LKP_ エントリー0 読み取り/書き込み 0h (FFFFFFFEh) 8chより前のベースアドレスは何でしたか? 例えば0x3fc0008cになりますので、この動的エントリテーブルには完全なアドレスがあります。完全なアドレスを教えていただけますか? 8Ch DYN_BE_LKP_ エントリー0 読み取り/書き込み 0h (FFFFFFFEh) 90時間 DYN_BE_LKP_ エントリー1 読み取り/書き込み 0h 94時間 DYN_BE_LKP_ エントリー2 読み取り/書き込み 0h 98時間 DYN_BE_LKP_ エントリー3 読み取り/書き込み 0h 9Ch DYN_BE_LKP_ エントリー4 読み取り/書き込み 0h A0h DYN_BE_LKP_ エントリー5 読み取り/書き込み 0h A4h DYN_BE_LKP_CTRL 読み取り/書き込み 0h (FF800000h) レジスター内の動的エントリを構成するための完全なアドレスを教えていただけますか? この実装はSJA1110 スイッチで行う必要がある Re: Register Access in S32G-VNP-RDB32 (SJA1110) Switch こんにちは@Atkinson 、 最初は簡単ではないと思われるかもしれませんが、コンセプトは実際には非常にシンプルです。 最終的なレジスタ アドレスは、アクセス方法 (AHB 経由の M7 コア経由で内部的にアクセスしているか、SPI_AP インターフェース経由で外部的にアクセスしているか) によって異なります。ベース アドレスはアクセス ポイントによって異なります。 レジスタ アドレスは、UM11107 の表 2 に示されているベース アドレスを使用して計算されます。たとえば、スイッチ サブシステムの場合、ベース アドレスは SPI_AP アクセスの場合は0x00000000 、AHB アクセスの場合は0xFF000000です。 あなたのCASE、レジスタ0x8C (DYN_BE_LKP_ENTRY0) は、AHB 経由でアクセスすると0xFF00008Cになります。 ここで混乱が生じる可能性があります。SDK ドライバは次のように定義します。 #define SJA1110_L2_ART_LE_ADDR ( 0x3fc00023 ) /**< l2ArtLockedEntryレジスタのアドレス *   SWITCH_DRV_Write ルーチンは、内部 (AHB) アクセスのためにアドレスを 2 ビット (<< 2) 左にシフトします。SPI 転送 (カスケード スイッチ セットアップで使用される) の場合、シフトは適用されません。SO、 0x3fc00023 << 2 は0xFF00008Cになります。   上記の説明で理解が深まったかと思います。   よろしくお願いいたします。 パベル
記事全体を表示
Inquiry: S32N55 system power mode APIs Hello Team, I learned that the FSS supports 2 APIs which can be used to set the system power mode. A1, Scmi_SystemPowerRequestProtocolMessageAttributesSynch A2, Scmi_PowerRequestSystemModeSynch And A1 can be used to set the cohort mode and state as well. However, there are dedicated cohort APIs to set cohort state, for example:  Scmi_BtmWarmResetCohortSynch, Scmi_BtmSuspendCohortSynch. It seems that the functionality of A1 API overlaps with the other 2 types of APIs. My question is: What is the A1 API used for? Or what kind of scenario is the A1 API used under? Best regards, Tangsheng. FSS_FW Priority: MEDIUM Re: Inquiry: S32N55 system power mode APIs Thanks Marius,  explain the confusion very clearly. Re: Inquiry: S32N55 system power mode APIs Hi @Tangsheng_Zhou , The Power Domain protocol and the Boot protocol were the original protocols added for Tunis; for various reasons, this was well adapted to the Tunis usecases but not fully compatible with the SCMI spec; as a result, alongside adding support for Luxor platform we added also the System Power protocol, which is the ARM SCMI compliant one -> hence the overlap. In terms of implementation and future support: - APIs like Scmi_SystemPowerStateSetSynch( ) are implemented as wrappers over the Btm_* APIs, both are going to be supported and both are going to do the exact same thing; Autosar/Tunis users can use the existing Btm APIs, while Linux is expected to use the new SystemPower APIs. APIs from PowerDomain protocols like Scmi_PowerRequestSystemModeSynch are going to be deprecated and anyway everyone is recommended to use the new, SCMI compatible API of SystemPower. Internally we have ticket for tracking the UserManual updates and clarifications. FSF-29425 Thanks, Marius
記事全体を表示
S32K312 PLL_LOL 問題 こんにちは、NXPさん S32K312は、 ( ESD )空中放電±15kV試験中にリセットされることが分かりました。リセットの理由はPLL_LOLでした。そこで、NXP S32K312EVB-Q172を使用して同じテストを行ったところ、こちらもリセットされました。 クリスタルダイバーの強度を向上させるために GM_SET レジスタを変更しようとしましたが、改善は見られませんでした。そして、DCMRWP3[9]を1に設定しようとすると、PLL_LOL時にS32Kはリセットされませんが、MCUは停止し、リセットのみが回復できます。 ESD テスト中は S32K3 を実行し続ける必要があります。PLL_LOL のときに CPU クロックを FIRC に切り替えることはできますか?いくつか提案をいただけませんか。よろしくお願いします! Re: S32K312 PLL_LOL Problem こんにちは、ダニエル。 ありがとうございます。自動レベルコントローラを無効にすると、この問題を解決できます。 Re: S32K312 PLL_LOL Problem 高出力発振器とはどういう意味ですか? 自動レベルコントローラ(FXOSC_CTRL[ALC_D] = 1)を無効にしましたか? BR、ダニエル Re: S32K312 PLL_LOL Problem こんにちは@danielmartynek 、 ご返信ありがとうございます。CMUは無効になっており、リセットの理由はPLLロックアウト(LOL)であると確信しています。PLLがLOLになると、MCUはリセットされます。DCMRWP3[9]を1に設定すると、PLLがLOLの間はMCUはリセットされませんが、動作を停止します。そのため、PLLがLOLの間はシステムクロックをFIRCに戻すことができません。水晶発振器をより高出力のものに交換してみると良いでしょう。 Re: S32K312 PLL_LOL Problem こんにちは@zhengjianfei1さん FXOSC が PLL ロック喪失の原因であると確信していますか?FXOSC クロック モニターは有効になっていますか? それはPLLだけの問題かもしれません。ラストマイルレギュレータは有効になっていますか? 割り込み内でシステム クロックを FIRC に戻すこともできます。 MUX_0_CSC[SAFE_SW] = 1 よろしくお願いいたします。 ダニエル
記事全体を表示
FRDM-MXCN947ボードでイーサネットとカメラを同時に使用する MCXNx4x では、SmartDMA を使用してカメラ インターフェースを実装できます。 MCXNx4x データシートによると、イーサネット と SmartDMA の Pinmux 割り当てが競合します。このため、イーサネットとカメラを同時に使用することはできないと考えました。 ただし、FRDM-MCXN947 ボード ユーザー マニュアル (UM12018) には次のよう記載されています。 > カメラの使用中にイーサネット機能が必要な場合は、別の回避策があります SJ16 および SJ26 ジャンパーをデフォルトの位置から移動することです。 イーサネットとカメラを同時に使用する方法はありますか? 開発ボード MCX N Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board こんにちは@dubian1shu 書類の内容を再確認したところ、書類の記載内容に問題があることが確認できました。 文書には適時変更を加えます。 SmartDMA (EZH_CAMERA) と イーサネット (ENET)は同時に使用できますが、カメラが使用するには共有されていないピンを見つける必要があります。 こちらの記事を参考にCAN。 MCX N947:イーサネットとカメラ機能の同時実装 - NXPコミュニティ これがお役に立てれば幸いです。 BR 下がる Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board 確認して返信してくれてありがとう@Harry_Zhang SmartDMA は P1_X と P3_X をサポートしているので、MCXNx4x は SmartDMA と イーサネット 機能を同時に使用 CAN と理解しています。 しかし、FRDM-MCXN947 を使用して SmartDMA および イーサネット 機能を使用することはできますか? FRDM-MCXN947 の J9 (カメラ ヘッダー) には、イーサネット ピンと競合する 7 つのピンがあります。FRDM-MCXN947 ボードのユーザー マニュアル (UM12018) に記載されている P1_4 の解決策では、そのうちの 1 つだけが解決され、他の 6 つの競合については触れられていません。 たとえば、P1_5、P1_13、および P1_15 は SmartDMA と イーサネット 間で競合します。回路図ドキュメント (SCH-90818) から見る限り、この競合を解決する解決策はないようです。 FRDM-MCXN947でSmartDMA(EZH_CAMERA)とイーサネット(ENET)を同時に使用する方法はありますか? Re: Simultaneous use of Ethernet and camera on the FRDM-MXCN947 board こんにちは@dubian1shu MCXNx4xのデータシートを確認したところ、確かにイーサネットとSmartDMAが競合するピンがいくつかあります。ただし、イーサネットとSmartDMAを同時に使用したい場合は、イーサネットとSmartDMAが競合しないピンを選択できます。 たとえば、SmartDMA ピンとして P3_X を選択し、イーサネット ピンとして P1_X を選択できます。 FRDM-MCXN947 ボード ユーザー マニュアル (UM12018) を参照してジャンパーを移動します。 これがお役に立てれば幸いです。 BR 下がる
記事全体を表示
S32K312 PLL_LOL 问题 你好,恩智浦、 我们发现 S32K312 将在进行 (ESD) 空气放电 ±15kV 测试时 RESET。我们发现 RESET 的原因是 PLL_LOL。然后我们使用恩智浦 S32K312EVB-Q172 进行同样的测试,它也会 RESET。 我们尝试更改 GM_SET 寄存器以提高晶体分歧强度,但没有任何改善。而且我们尝试将 DCMRWP3 [9] 设置为 1,当 PLL_LOL 时 S32K 不会 RESET,但是 mcu 会停止,只有 RESET 才能恢复。 在进行 ESD 测试时,我们需要 S32K3 保持运行。CPU 时钟能否在 PLL_LOL 时切换到 FIRC?您能给我一些建议吗? Re: S32K312 PLL_LOL Problem 嗨,丹尼尔 谢谢,禁用自动液位控制器可以解决这个问题。 Re: S32K312 PLL_LOL Problem 更大功率振荡器是什么意思? 您是否禁用了自动电平控制器(FXOSC_CTRL[ALC_D] = 1)? BR,丹尼尔 Re: S32K312 PLL_LOL Problem 你好,我是@danielmartynek、 感谢您的答复。CMU 已禁用,我确信 RESET 原因是 PLL 失锁。当 PLL LOL 时,MCU 将 RESET。当将 DCMRWP3 [9] 设置为 1 时,mcu 不会 RESET,而 PLL 哈哈但是 mcu 会停止运行。因此,当 PLL 哈哈时,我们无法将系统时钟改回 FIRC。我们尝试用更高功率的晶振取代晶振,看起来更好。 Re: S32K312 PLL_LOL Problem 你好@郑建飞1、 您确定 FXOSC 是导致 PLL 失锁的原因吗?你启用了 FXOSC 时钟监测吗? 可能只是 PLL 的问题。最后一英里调节器是否启用? 您可以尝试在中断中将系统时钟改回 FIRC。 mux_0_csc[safe_sw] = 1 此致, 丹尼尔
記事全体を表示
查询:S32N55 系统电源模式 API 你好,团队、 我了解到 FSS 支持 2 个 API,可用于设置系统电源模式。 A1, Scmi_SystemPowerRequestProtocolMessageAttributesSynch A2, Scmi_PowerRequestSystemModeSynch A1 也可用于设置队列模式和状态。但是,有专用的群组 API 可以设置群组状态,例如:scmi_btmwarmResetCohortSynch、scmi_btmsuspendCohortSynch、scmi_btmsuspendCohortSynch。 A1 应用程序接口的功能似乎与其他两类应用程序接口重叠。 我的问题是:A1 API 的用途是什么?或者说,A1 应用程序接口是在什么样的情况下使用的? 顺祝商祺! 唐生。 FSS_FW 优先级:中等 Re: Inquiry: S32N55 system power mode APIs 谢谢你,马略。 Re: Inquiry: S32N55 system power mode APIs 你好@Tangsheng_Zhou、 功率域协议和启动协议是为突尼斯添加的原始协议;出于各种原因,它很好地适应了突尼斯的用例,但与SCMI规范不完全兼容;因此,除了增加对卢克索平台的支持外,我们还添加了系统电源协议,这是符合Arm SCMI的协议—— > 因此存在重叠之处。 在实施和未来支持方面: - Scmi_SystemPowerStateSetSynch( ) 等应用程序接口是作为 Btm_* 应用程序接口的包装器实现的,两者都将得到支持,而且两者将做完全相同的事情;Autosar/Tunis 用户可以使用现有的 Btm 应用程序接口,而 Linux 预计将使用新的 SystemPower 应用程序接口。 PowerDomain 协议的 API(如 Scmi_PowerRequestSystemModeSynch)将被淘汰,因此建议大家使用 SystemPower 的新 SCMI 兼容 API。 我们内部有用于跟踪《用户手册》更新和说明的票据。 FSF-29425 谢谢! Marius
記事全体を表示
S32K3xx SpiBaudrateConfigRef 設定 こんにちは、 SDKs ペリフェラル ドライバの構成コンポーネント - LPSPI: 1. Lpspi → SpiExternalDevice → SpiUseBaudrateConfig → SpiBaudrateConfigRef? この設定の目的は何ですか?また、どのように設定しますか? 2. SPI ボーレート選択における SpiUseBaudrateConfig と SpiCalculatedBaudRate の違いは何ですか? 3. SPI ボーレートを設定するためのユーザーフレンドリーな方法が必要です。どうすればそれがCANますか? よろしくお願いいたします。 カルメガン C Re: S32K3xx SpiBaudrateConfigRef set こんにちは@daniel_ll 、 この件に関してプライベートメッセージをお送りしました。 Re: S32K3xx SpiBaudrateConfigRef set こんにちは、ジュリアン Jira のバグへのリンクはありますか? また、どの RTD リリースでこのバグが修正されるのか、詳しい情報はありますか?RTD 5.0.0でも同じ問題に直面している Re: S32K3xx SpiBaudrateConfigRef set こんにちは@karmegancjk 社内チームに確認したところ、これはバグです。次の RTD リリースで修正される予定です。 よろしくお願いします、 ジュリアン Re: S32K3xx SpiBaudrateConfigRef set こんにちは@karmegancjkさん、 どうやら、MCAL Spi コンポーネントのみが有効な SpiBaudRateConfigRef 値を生成します。私はプロジェクトを IP ではなく MCAL に基づいていたため、これに気づきませんでした。 これは意図されたものではないと思うSO、現時点では、SPI コンポーネントを「UseBaudrateConfig」パラメータなしで構成するか、MCAL コンポーネントを使用して参照を生成する必要があります。これが想定された動作であるかどうかを社内で確認してみます。 よろしくお願いします、 ジュリアン Re: S32K3xx SpiBaudrateConfigRef set こんにちは、 Lpspi ドライバで SpiBaudrateConfig_0 を SpiBaudrateConfigRef に割り当てることができません。 IDEs: S32DS 3.5.13。 RTD: R22_11 V4.0.0。 SpiBaudrateConfigRef で SpiBaudrateConfig_0 のパスを設定するにはどうすればよいですか? Re: S32K3xx SpiBaudrateConfigRef set こんにちは@karmegancjkさん、 すべての構成パラメータについては、それぞれのドライバのユーザー マニュアルに記載されています。「C:\NXP\S32DS.3.6.1\S32DS\ソフトウェア\PlatformSDK_S32K3\RTD\Spi_TS_T40D34M50I0R0\doc」の下RTD_SPI_UM.pdfが見つかります。 1. SpiBuadrateConfigRef は、Spi ボー レートを計算するために使用される参照ノードです。 2. SpiUseBaudrateConfig は参照ノードを使用し、SpiCalculatedBaudRate は次の式を使用します。 SpiCalculatedBaudrate = 関数クロック / (SpiPrescalerValue * (SpiScaler + 2)) 3. 既存の例「Spi_Transfer_S32K344」をベースとしてCAN使用できます。また、前述のファイルの第 3.6.13 章では、ボー レートを設定する方法が示されています。 よろしくお願いします、 ジュリアン
記事全体を表示