Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Can I delete a key in the secure NV storage area of NCJ29D5 by Trace32? Hi All, I'm working with NCJ29D5 for UWB ranging. I succeed to store a key into NV area, but is there any way to erase it using the trace32? When I tried it with 'FLASH.ERASE' command, i failed. I think the memory area is secured area, but I want to know any method. Thanks. Re: Can I delete a key in the secure NV storage area of NCJ29D5 by Trace32? Hello, Hope you are doing well. Sorry for the inconvenience this might cause you but as the information of this product it's under NDA (Non-Disclosure Agreement) the information it's not public. For more information about the chip could you please contact one of our distributors available in the Distributor Network|NXP? Or if you have any direct contact who helped you getting this device, please contact them. Regards, Ricardo
View full article
S32G2 LLCE payload features Hello, i know that LLCE can filter specific CAN IDs which supports host offloading. i want to know if there is any ways we can filter certain payload in LLCE.    For example, drops the frame if ID = 0x20 and first byte of payload = 0x00 Re: S32G2 LLCE payload features hi,chansookang Thank you for contacting us. I know what you mean. I think you can operate the payload in software. LLCEAF cannot recognize the messages inside LLCE. If you want to do so, you can purchase FDK and modify the LLCE code. In addition, refer to the LLCE_firmware_user_guide, no payload manipulation is implemented (e.g. payload split). BR Joey
View full article
使用ldf文件配置s32k116 我有一个主节点,它可以发送 2 个帧 ID 为 0x30 的信号,并且想将 s32116 evb 配置为从属节点。 就我而言,当我发送帧 ID 为 0x30 的信号时,结果为 0x01 0xff 0xff 0xff。任何一个 gpio 引脚都应该为高电平(led 应该发光)或者当发送帧 ID 为 0x30 的信号(即 0x00 0xff 0xff 0xff)时,配置了 led 的相同 gpio 应该变为低电平。 非常感谢与此相关的任何建议或简单示例。 提前致谢! 谢谢与问候, 桑托什
View full article
MPXV2010GPを使用して回路カードにコンフォーマルコーティングを適用します MPXV2010GPを使用する回路カードの生産を開始しようとしています。部品の下部にある通気口について理解したところで、底部の通気口を削らずにカードにコンフォーマルコーティングを施すためのベストプラクティスやアドバイスはありますか?私が思いつく唯一の解決策は、その部分をマスキングして、コンフォーマルコーティングを施した後にのみ部品を取り付けることです。次に、部品のリードにブラシでコンフォーマルコーティングを施します。 よろしくお願い申し上げます。 圧力センサ Re: MPXV2010GPを使用して回路カードにコンフォーマルコーティングを適用します こんにちは、デイブベイツ47 残念ながら、特定の技術に関する文書はありません。通常、お客様がセンサーをどのように使用したいかによって異なります。時々、人々はセンサーの配置に関して非常に創造的です。 しかし、あなたのアイデアは良さそうです。それを補足する文書を2つだけお勧めします。 AN1646、内蔵圧力センサーのノイズに関する考慮事項 AN3150、圧力センサー装置のはんだ付けの推奨事項-アプリケーションノート これらのファイルにアクセスするにはアカウントが必要です この情報がお役に立てば幸いですので、他に何か助けが必要な場合はお知らせください。 素晴らしい一日を過ごし、幸運を祈ります。
View full article
Applying Conformal Coating to a circuit card using a MPXV2010GP We are about to start production of a circuit card which will use the MPXV2010GP. With the understanding of the vent on the bottom of the part, I am wondering if there are any best practices or advice available on applying conformal coating to the card without gumming up the vent on the bottom? The one solution I can come up with is masking off that area and only installing the part after conformal coating is applied. We would then apply conformal coating to the part's leads with a brush. Thank you Pressure Sensors Re: Applying Conformal Coating to a circuit card using a MPXV2010GP Hi davebates47 Unfortunately, we don't have a document with a specific technique; it generally depends on how the customer wants to use the sensor. Sometimes, people are very creative when it comes to sensor placement. But your idea sounds good, let me recommend just two documents to complement it. AN1646, Noise Considerations for Integrated Pressure Sensors AN3150, Soldering Recommendations for Pressure Sensor Devices - Application Notes You need an account to access to these files I hope this information has helped you, please let me know if you need help with anything else. Have a great day and best of luck.
View full article
使用 MPXV2010GP 将保形涂层应用于电路卡 我们即将开始生产使用 MPXV2010GP 的电路卡。通过了解零件底部的通风口,我想知道是否有任何最佳实践或建议可用于在卡片上施加保形涂层而不会堵塞底部的通风口?我能想到的一个解决方案是遮蔽该区域并仅在应用保形涂层后安装该部件。然后,我们会用刷子将保形涂层涂抹到零件的引线上。 谢谢 压力传感器 回复:使用 MPXV2010GP 将保形涂层应用于电路卡 你好,davebates47 不幸的是,我们没有包含特定技术的文件;这通常取决于客户想要如何使用传感器。有时,人们在传感器放置方面非常有创造力。 但你的想法听起来不错,让我推荐两份文件来补充它。 AN1646,集成压力传感器的噪声考虑因素 AN3150,压力传感器设备焊接建议 - 应用笔记 您需要一个帐户才能访问这些文件 我希望这些信息对您有所帮助,如果您需要任何其他帮助,请告诉我。 祝您度过愉快的一天并好运。
View full article
ldfファイルを使用したs32k116の設定 フレームID 0x30の2つの信号を送信できるマスターノードがあり、s32116 evbをスレーブノードとして設定したいと考えています。 私の場合、フレームIDが0x30の信号を0x01 0xff 0xff 0xffとして送信すると。GPIOピンのいずれかがHigh(LEDが光るはずです)か、フレームIDが0x30の0x00 0xff 0xff 0xffの信号が送信されると、LEDで構成された同じGPIOがローになるはずです。 これに関連する提案や簡単な例は大歓迎です。 前もって感謝します! ありがとう & よろしく、サントッシュ
View full article
rt1170 MIPI DSIはビデオモードを使用してDCSコマンドを送信します こんにちは、 私は現在、rt1170評価キットでST7703I TFTモバイルシングルチップドライバーに対応しようとしています。ST7703Iはビデオモードのみをサポートしており、DCSコマンドはビデオモードを使用して送信する必要があります。 MIPI DSIドライバー ( https://mcuxpresso.nxp.com/api_doc/dev/2207/a00014.html) には、" dsi_SetdpiConfigでビデオモードを開始できると書かれています。 "DSI_SetDpiConfig () を呼び出した後、" dsi_TransferBlocking () " という関数が付いたDSCコマンドは、ビデオモードで転送されますか?
View full article
rt1170 MIPI DSI 使用视频模式发送 dcs 命令 你好, 我目前正在尝试使用 rt1170 评估套件来解决 ST7703I TFT 移动单芯片驱动器。ST7703I 仅支持视频模式,并且必须使用视频模式传输 dcs 命令。 在 MIPI DSI 驱动程序( https://mcuxpresso.nxp.com/api_doc/dev/2207/a00014.html )中,描述了可以使用“ DSI_SetDpiConfig ”启动视频模式。调用DSI_SetDpiConfig()后,是否使用函数“ DSI_TransferBlocking() ”通过视频模式传输 DSC 命令?
View full article
Configuration for s32k116 with ldf file I have master node which can send 2 signals with frame id 0x30 and would like to configure s32116 evb as slave node.  In my case, when I send a signal with frame id 0x30 as 0x01 0xff 0xff 0xff. any one of the gpio pin should be High(led should glow) or when the signal wih frame id 0x30 as 0x00 0xff 0xff 0xff is sent, the same gpio configured with led should go low.  Any suggestions or simple examples related to this are highly appreciated. Thanks in advance! Thanks & regards, Santhosh Re: Configuration for s32k116 with ldf file Hi @santhosh23, Could you try searching for the LIN package with "Product Search" as "SW32K1 SW32M24X LIN Stack version 1.0.2"? Also, keep in mind that this package is only compatible with S32 Design Studio v3.5. I'm not sure since the software is relatively old, please look at the community post: Example S32K_printf_implementation - S32DS_1.0 - NXP Community. It uses the ewl library instead of newlib. Best regards, Julián Re: Configuration for s32k116 with ldf file Thank you @Julián_AragónM for your quick response! I tried to access the Flexera portal, but couldn't succeed. It is showing that I've already requested evaluation version for this product. As per my knowledge, I did not requested this product before.  And regarding printf, I can't see newlib Semihosting option on my screen.  For your kind information i am using S32DS_ARM_v2018.R1 software version.  Do you think this is because of software version or is there anything else i am missing out? Best regards, santhosh Re: Configuration for s32k116 with ldf file Hi @santhosh23, Please access the Flexera portal and go into "Automotive SW - S32K1 Reference Software > Automotive SW - S32K1_S32M24X - LIN Stacks" and select the updatesite.zip LIN Stack for S32K1. Keep in mind you also need the RTD package for S32K1, see Getting Started with the Real-Time Drivers (RTD). As for the printf functionallity, you will need to select "newlib Semihosting" and enable semihosting in the debugger configuration: After this, you should be able to see the message printed in the P&E Semihosting Console: You can also take a look into this LPUART implementation from community: Example S32K_printf_implementation - S32DS_1.0 - NXP Community How to use printf() to print string to Console and UART in S32 Design Studio for S32 Platform - NXP Community Best regards, Julián Re: Configuration for s32k116 with ldf file I am not able to see that example solution in my window. Could you please tell me how to include that example in my folder?  Also, Could you please let me know how to use printf in s32 Design studio for ARM? Where can I see the output printed ? I will be looking forward for your response. Best regards, santhosh Re: Configuration for s32k116 with ldf file Hi @santhosh23, You can refer to the S32K1xx LIN STACK 1.0.2 Example Projects. There are no S32K116 examples readily available, but you can just copy over the configuration. The example describes LIN communication between S32K1XX Slave and other board Master using unconditional frames. You can look at the "description.txt" for more information. These examples include an LDF file in the "src" folder as the one I've attached. Best regards, Julián
View full article
LPC802 SPI 调整 LPC802 SPI 外设的 TXDAT 和 RXDAT 寄存器中的数据有何意义?输出首先选择 LSB 还是 MSB 有关系吗? 用户手册中没有提到这个主题。 回复:LPC802 SPI 理由 谢谢! 回复:LPC802 SPI 理由 谢谢,但这没有回答我的问题。 让我举个例子。假设您已将传输配置为 12 位长度,并且您接收数据,假设全部为 1。 数据寄存器是 0xFFF0(左对齐)还是 0x0FFF(右对齐)?
View full article
PT200xHM測定機能、電圧なし OA機能では、電圧設定のための設定は出来ません。 私は次のように書いています。 1AAh=426日 b6=oa1_g1 b5-3= oa_sel1 b2-1=oa1_gain b0=oa1_en 0000 000 0001 0001 0x0011 '000':電流測定ブロック1からの出力 '001':電流測定ブロック3からの出力 '010':OA_Meas1:測定機能からの出力、未処理の信号 '011':OA_Meas2:測定機能からの出力、ローパス+ハイパスフィルタリング 「100」:OA_Meas3:測定機能からの出力、LP+HPフィルタリングの2倍 「101」:2.5ボルト '110':OA_Meas4:測定機能からの出力、ローパスフィルタリング meas_func1レジスタ(1ACh) 予約済み B12-9= dac_fb_sel B8=cur_volt0, B7-5 =d_ls_sel B4-2=s_hs_sel B1-0 oa_cur 000 0000 0 001/.0100.01 00 = 0044h HS2 - LS1 meas_func2レジスタ(1ADh) b15=offset_hp2_sel、b14=offset_hp1_sel、b13-10=fc_hp2_sel、b9-7=gain_hp1_sel b6-3=fcut_hp1_sel b2-1=volt_att xxxx xxxx xxxx x000=0 フィルタされていない div by 30 スコープは0Vでフラットラインを示します はい、パーツ名にMが入っています。 何を見逃したのか? ソレノイドコントローラー Re:PT200xHM測定機能、電圧なし はい、動作します。週末はいい休みを。
View full article
PT200xHM测量功能,无电压 使用 OA 功能,我无法设置电压设置。 我写信给: 1AAh = 426d b6=oa1_g1 b5-3= oa_sel1 b2-1=oa1_gain b0=oa1_en 0000 000 0001 0001 0x0011 ‘000’:电流测量块 1 的输出 '001':电流测量块 3 的输出 ‘010’:OA_Meas1:测量功能的输出,未处理的信号 '011': OA_Meas2:测量函数输出,低通+高通滤波 '100': OA_Meas3: 测量函数输出,LP + 两次 HP 滤波 '101':2.5伏 ‘110’: OA_Meas4: 测量功能输出,低通滤波 meas_func1寄存器(1ACh) 保留 b12-9= dac_fb_sel b8=cur_volt0, b7-5 =d_ls_sel b4-2=s_hs_sel b1-0 oa_cur 000 0000 0 001/.0100.01 00 = 0044h HS2 - LS1 meas_func2寄存器(1ADh) b15=offset_hp2_sel、b14=offset_hp1_sel、b13-10=fc_hp2_sel、b9-7=gain_hp1_sel b6-3=fcut_hp1_sel b2-1=volt_att xxxx xxxx xxxx x000=0 未过滤除以 30 示波器显示 0V 处为平线 是的,它的部分名称中包含 M。 我错过了什么? 电磁阀控制器 回复:PT200xHM 测量功能,无电压 是的,它确实有效。周末休息得很好。
View full article
dsp56805 flash.cfg Help me please i need the dsp56805 flash.cfg for program DSP56F805 with Codewarrior USB TAP. Re: dsp56805 flash.cfg Thank you. Re: dsp56805 flash.cfg Hi, If you have source code and project, you can use CodeWarrior for DSP56800E ver8.3 tools and generate the file and download via usbtap device. If you just have S-Record file, you have to use FlashOverJtag.exe tools and Wiggler with PC with 25 pin printer port. Hope it can help you BR XiangJun Rong Re: dsp56805 flash.cfg How can i download CodeWarrior 8.2.3 ? Re: dsp56805 flash.cfg Could you explain how can i flash the  .s file into dsp56f805 via usb tap on code warrior 8.3 please. Re: dsp56805 flash.cfg Hi, As you know that the DSP56F805 was launched in Motorola in 2000 year, it uses DSP56800 core instead of DSP56800E core, so the 56800E Flash Programmer does not support DSP56F805. You have to use flashoverjtag.exe tools to download code via JTAG with Wiggler(parallel command converter) and PC with 25 pin printer port. If you use USBTAP device, you have to use CodeWarrior for DSP56800E ver8.3 tools, but the CodeWarrior for DSP56800E ver8.3 tools can work on Win XP, it has issue to run on Win 10 OS. Hope it can help you BR XiangJun Rong Re: dsp56805 flash.cfg Hi. I tried but this file doesn't work on 56800E Flash Programmer on CodeWarrior 8.3. I have .s file and can't programming it to dsp56805 MCU. Re: dsp56805 flash.cfg Hi, Pls try to use the file I attached. Pls try to change the extension name from txt to cfg, because I can not attach the file with cfg as extension name. Hope it can help you BR XiangJun Rong
View full article
LPC802 SPI Justification What is the justification for data in the TXDAT and RXDAT registers for the SPI peripheral for the LPC802?  Does it matter if the output is selected as LSB or MSB first? The User's Manual is silent on the subject. Re: LPC802 SPI Justification Thanks! Re: LPC802 SPI Justification Hi Q:Let me give an example. Say you have the transfer configured for 12-bit length, and you receive data, say all ones. Would the data register be 0xFFF0 (left justification) or 0x0FFF (right justification)? >>>>>The LPC802 SPI always use right justification, for example, if you want to receive 12 bits data with all bits 1, you will receive  0x0FFF in the receiver reg. Hope it can help you BR XiangJun Rong Re: LPC802 SPI Justification Thank you, but that doesn't answer my question. Let me give an example.  Say you have the transfer configured for 12-bit length, and you receive data, say all ones. Would the data register be 0xFFF0 (left justification) or 0x0FFF (right justification)? Re: LPC802 SPI Justification Hi, You can select the MSB first or LSB first, but the master spi and slave spi devices must match. Pls refer to section 14.6.1 SPI Configuration register in the UM11045.pdf The LSBF bit in the CFG reg defines the MSB/LSB first. Hope it can help you BR XiangJun Rong
View full article
PT200xHM measurement function, no voltage With OA feature, I can not setup for voltage setting. I write to: 1AAh = 426d b6=oa1_g1 b5-3= oa_sel1 b2-1=oa1_gain b0=oa1_en 0000 000 0001 0001 0x0011 '000': output from current measurement block 1 '001': output from current measurement block 3 '010': OA_Meas1: output from measurement function, unprocessed signal '011': OA_Meas2: output from measurement function, low-pass + high-pass filtering '100': OA_Meas3: output from measurement function, LP + two times HP filtering '101': 2.5 Volt '110': OA_Meas4: output from measurement function, low-pass filtering meas_func1 register (1ACh) reserved b12-9= dac_fb_sel b8=cur_volt0, b7-5 =d_ls_sel b4-2=s_hs_sel b1-0 oa_cur 000 0000 0 001/.010 0.01 00 = 0044h HS2 - LS1 meas_func2 register (1ADh) b15=offset_hp2_sel, b14=offset_hp1_sel, b13-10=fc_hp2_sel, b9-7=gain_hp1_sel b6-3=fcut_hp1_sel b2-1=volt_att xxxx xxxx xxxx x000=0 Unfiltered div by 30 Scope shows flat line at 0V Yes it has M in part name. What have I missed? Solenoid Controller Re: PT200xHM measurement function, no voltage Yes it does work. Nice rest over weekend. 
View full article
i.MX8MP maximum memory density Hi NXP team, What is the maximum supported LPDDR4 memory density of i.MX8MP? Thanks Re: i.MX8MP maximum memory density Hi Daniel, This info is very useful. Regards, Simon Re: i.MX8MP maximum memory density Hi @simonng  Please refer to below link for i.MX 8M Quad/8M Mini/ 8M Nano/ 8M plus -LPDDR4 memory compatibility guide,   you can get the density info. i.MX 8M Quad/8M Mini/8M Nano/8M Plus - LPDDR4, DDR4 and DDR3L memory compatibility guide - NXP Community Regards Daniel Re: i.MX8MP maximum memory density The memory density of i.MX8MP  is 32 Gb (gigabits) per die, which translates to 4 GB (gigabytes) per die. Hope you got your answer.
View full article
LPC802 SPIの正当化 LPC802のSPIペリフェラルのTXDATレジスタとRXDATレジスタのデータにはどのような理由がありますか?最初に出力をLSBとMSBのどちらに選択してもいいですか? ユーザーズマニュアルは、この件については沈黙しています。 日時:LPC802 SPIの正当化 ありがとうございます! 日時:LPC802 SPIの正当化 ありがとう、しかしそれは私の質問に答えていません。 例を挙げましょう。転送が 12 ビット長に設定されていて、データを受信するとします。たとえば、すべてのビット長です。 データレジスタは0xFFF0(左揃え)ですか、それとも0x0FFF(右揃え)ですか?
View full article
NXP S32K324-Internal Temperature Reading Issues with ADC0 Channel 49 Dear NXP Support Team, I am encountering issues while attempting to read the internal temperature sensor on the S32K324 microcontroller using ADC hardware instance 0, channel 49. My VREF voltage is configured to 3.3V (0x35), but the temperature readings I am obtaining do not match my expected values.     Could you please provide any guidance or reference materials to help me resolve this issue and achieve accurate temperature readings?   Regards, Ranjith kumar Re: NXP S32K324-Internal Temperature Reading Issues with ADC0 Channel 49 Hi@Ranjith_kumar I don't quite understand what your new question is? In my previous reply, I have provided you with a test demo, and I haven't seen any of your projects. Re: NXP S32K324-Internal Temperature Reading Issues with ADC0 Channel 49 Dear Senlent, I followed the steps you mentioned in the shared video to read the internal temperature sensor on the S32K324 controller. However, I am not obtaining stable or expected temperature values. As I mentioned in my previous post, I am reading the raw ADC values from the internal temperature sensor, but the temperature readings show sudden spikes and are not constant. For reference, I am also using an external temperature sensor near the controller, which shows a stable temperature range of 32 to 35°C. In contrast, the internal temperature sensor readings are showing negative and fluctuating values. I have attached a video demonstrating the issue and the software I developed for this purpose. Could you please help me verify whether the values I am getting are correct or if there might be an issue with my approach? Any guidance or example code to correctly read and interpret the internal temperature sensor data would be greatly appreciated. Thank you for your support. Regards, Ranjith kumar Re: NXP S32K324-Internal Temperature Reading Issues with ADC0 Channel 49 Hi@Ranjith_kumar From your video, it seems that you didn't even read the raw value of the internal temperature sensor. I made a very basic example for your reference, the hardware is S32K344, the RTD is 3.0.0+P07. Re: NXP S32K324-Internal Temperature Reading Issues with ADC0 Channel 49 Dear Senlent, As per your suggestion and referring to the provided link, I have attempted to read the internal temperature sensor on the NXP S32K324 controller using RTD 3.0.0. However, the values I am obtaining do not match our expected results. Could you please share any example code or reference implementation that demonstrates the correct procedure for reading and converting the internal temperature sensor data? Additionally, I would appreciate your guidance on how to determine appropriate threshold temperature values for our application. I have attached the relevant document for your reference. Kindly assist me in resolving this issue. Thank you for your support. Best regards, Ranjith kumar Re: NXP S32K324-Internal Temperature Reading Issues with ADC0 Channel 49 Hi@Ranjith_kumar There is a similar demo in this link for your reference https://community.nxp.com/t5/S32K/S32K344-Temperature-Sensor/m-p/1876707#M35929 If you still have questions, please provide me with a basic project and I will help you check it
View full article
RAM KEY loading with Crypto_43_HSE RTD v5.0.0 Hello, I am using Crypto_43_HSE RTD v5.0.0. I want to load a new RAM_KEY in the HSE. I configured the RAM Key in the following way: CryptoKeyType is formed by: CipherProof, KeyMaterial, MacProof. RAM KEY Key Material is configured as: (no HseKeyFlags are configured) with the related ram key catalog: accessible by both MU instances 0 and 1. I am trying to import the RAM Key as an encrypted key, thus by using calculation of M1M2M3. I am able to calculate M1, M2 and M3 correctly (I already checked the correctness by trying to import the NvM catalog keys and the import was successful). The M1M2M3 values I have are configured according to the following parameters: new_key=b'\xAB\xAB\xAB\xAB\xAB\xAB\xAB\xAB\xAB\xAB\xAB\xAB\xAB\xAB\xAB\xAB' #key I want to import auth_key=b'\x00\x01\x02\x03\x04\x05\x06\x07\x08\x09\x0A\x0B\x0C\x0D\x0E\x0F' #my master key uid="000000000000000000000000000000" new_key_id=AutosarKeySlots.RAM_KEY (0x0E) auth_key_id=AutosarKeySlots.MASTER_ECU_KEY (0x01) counter=1 flags.fid = 0 # all flags set to zero the calculated M1M2M3 values are: static uint8 sKeyUpdateM1M2M3[64u] __attribute__((aligned)) = { /* M1 */ 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0xe1, /* M2 */ 0x2b, 0x11, 0x1e, 0x2d, 0x93, 0xf4, 0x86, 0x56, 0x6b, 0xcb, 0xba, 0x1d, 0x7f, 0x7a, 0x97, 0x97, 0x29, 0x8d, 0x4e, 0xa0, 0x6, 0xa2, 0x80, 0xc1, 0x5d, 0xd2, 0xa3, 0xe5, 0x6f, 0x4f, 0x5b, 0x6, /* M3 */ 0x4c, 0x1b, 0xcb, 0x77, 0x87, 0xb3, 0x9, 0x19, 0xfb, 0x6e, 0x73, 0x9c, 0xa6, 0xab, 0x48, 0xf4, }; When I try to call the Crypto_43_HSE_KeyElementSet with the cryptoKeyId=CryptoConf_CryptoKey_CryptoKey_SHE_RAM_KEY and by using the M1M2M3 values that I provided above, I get the result code =0x09 that should mean CRYPTO_E_KEY_NOT_VALID, returned upon HSE responding with status code HSE_SRV_RSP_KEY_INVALID. What could be the cause of this issue? Is there any configuration step that I have missed? Kind regards Re: RAM KEY loading with Crypto_43_HSE RTD v5.0.0 I solved the problem by changing the parameters used to calculate M1M2M3. According to AUTOSAR standard, the RAM Key must have flags and counter set to zero, and it can be updated only by using one of the other KEY_n (KEY1...KEY10) as authentication keys. By doing so, I was able to load the RAM Key correctly. Re: RAM KEY loading with Crypto_43_HSE RTD v5.0.0 Also, I just wanted to add that I performed the HSE KeyCatalog formatting just one time at the HSE installation. At startup I only perform the Crypto_43_HSE_Init.
View full article