1910030_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1910030_en-US

1910030_en-US

dsp56805 flash.cfg

Help me please i need the dsp56805 flash.cfg for program DSP56F805 with Codewarrior USB TAP.


Re: dsp56805 flash.cfg

Thank you.

Re: dsp56805 flash.cfg

Hi,

If you have source code and project, you can use CodeWarrior for DSP56800E ver8.3 tools and generate the file and download via usbtap device.

If you just have S-Record file, you have to use FlashOverJtag.exe tools and Wiggler with PC with 25 pin printer port.

Hope it can help you

BR

XiangJun Rong


Re: dsp56805 flash.cfg

How can i download CodeWarrior 8.2.3 ?

Re: dsp56805 flash.cfg

Could you explain how can i flash the  .s file into dsp56f805 via usb tap on code warrior 8.3 please.

Re: dsp56805 flash.cfg

Hi,

As you know that the DSP56F805 was launched in Motorola in 2000 year, it uses DSP56800 core instead of DSP56800E core, so the 56800E Flash Programmer does not support DSP56F805.

You have to use flashoverjtag.exe tools to download code via JTAG with Wiggler(parallel command converter) and PC with 25 pin printer port.

If you use USBTAP device, you have to use CodeWarrior for DSP56800E ver8.3 tools, but the CodeWarrior for DSP56800E ver8.3 tools can work on Win XP, it has issue to run on Win 10 OS.

Hope it can help you

BR

XiangJun Rong


Re: dsp56805 flash.cfgHi. I tried but this file doesn't work on 56800E Flash Programmer on CodeWarrior 8.3.
I have .s file and can't programming it to dsp56805 MCU.
Re: dsp56805 flash.cfg

Hi,

Pls try to use the file I attached.

Pls try to change the extension name from txt to cfg, because I can not attach the file with cfg as extension name.

Hope it can help you

BR

XiangJun Rong

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 09:28 PM
更新者: