Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
長距離HiTagの展開条件は何ですか? 長期的な解決策を実現する方法を教えていただけますか?リーダー側に要件や特別なデザインはありますか?例えば、電力やアンテナのサイズ/直径などでしょうか? 私の会社は家畜マネジメントの解決策を探しており、そのデメンドには以下が含まれます:1. 長距離:埋め込みタグとリーダーの距離が35cmを超えています。2. リーダーのサイズ(直径約5cm)と重量は小さく軽量です。 オンライン認証 Re: what are the deployment conditions of long range HiTag? こんにちは、@kevin9611さん コンパクトリーダー(~直径5cm)の場合、読書距離>35cm)のご要望について: 低周波(LF、125/134 kHz、例:HITAG / ISO11784/11785)技術は誘導結合に基づいています。根本的な物理的制約のため、特にアンテナサイズが小さい場合、そのような長距離の読み取りを実現することは一般的に不可能である。 実際には、LF埋め込み型タグは通常、短距離(大型アンテナを使用した最適化された条件下では数センチメートルから約20~30センチメートル)で動作します。したがって、あなたの要件(>35cm、5cmのリーダー)はLFテクノロジでは満たせません。 より長い読書距離を実現するためには、UHF RFID(860–960 MHz)を検討しており、コンパクトなリーダーアンテナでも数メートルの読み取り距離を容易にサポートできます。 ただし、以下の点に留意することが重要です。 UHF RFIDは、動物組織内で強い信号減衰のため、埋め込み型アプリケーションには適していません。 UHFソリューションは、埋め込み型トランスポンダーではなく、耳標や首輪と組み合わせて使用されるのが一般的です。 結論: 埋め込み型タグが必須→ならLFテクノロジ(HITAG / ISO11784/85)が必要ですが、リーダーデザインはコンパクトではなく大型(例:スティックリーダーやゲートアンテナ)である必要があります。 長距離読み取りと小型リーダーが必須条件である場合、UHFイヤータグベースのソリューションのみが実現可能です。
記事全体を表示
Type 2 Tag Emulation with PN5190 We have a custom Linux platform where we have successfully made the PN5190 to work as a card reader. Now we want to try out to make it work as a Type 2 tag, just to send a URL (as fast as possible) to any smartphone tapped on it. Is there an example that I can use in the NFCReaderLibrary to achieve this? If not, can you please guide me on how to achieve this ? Re: Type 2 Tag Emulation with PN5190 Hello sir, Thank you so much for your interest in our products. Unfortunately, our NFC Reader Library only has a Host Card Emulation example of a Type 4 Tag. Is the Example 8_HCE_T4T.   Fabian_R_1-1782166840649.png I hope this information may be helpful.
記事全体を表示
EB official demo compilation The EB project was compiled according to the following steps: (1)Modify the project_parameters.mk file NXP2_2-1782092925146.png NXP2_3-1782092953674.png NXP2_4-1782092967359.png (2)Since S32DS was used, the content related to T32 was annotated in the check_build_params.mk file. NXP2_5-1782093055565.png (3)"Make generate" is acceptable. NXP2_6-1782093128512.png (4)"make build" is incorrect. NXP2_7-1782093250946.png Could you please tell me what caused this? Is it necessary to modify the makefile? Re: EB official demo compilation Hi@NXP2 The version of GCC you selected is incorrect. Senlent_0-1782107597492.png Re: EB official demo compilation Thank you!
記事全体を表示
DTM configuration for KW36 Hi estephania_martinez‌, I configured KW36 DTM as mentioned in the below link (Through a 2-wire UART interface) Direct Test Mode (DTM) Configurations for the KW family  But to verify the DTM behavior I tested using the below commands 1. LE Reset      (a)  0x0000     (b)  0x0204     (c)  0x0300 2. LE Transmitter Test       0x8000 3. LE Receiver Test       0x4000 4. LE Test End       0xC000 In the above-mentioned commands, LE Reset is not getting passed with all the 3 commands and LE Test End command is also failed. Can you please check this issue? Hardware used: USB to TTL converter (3.3v logic level) Thanks! Regards, Naven Suresh Re: DTM configuration for KW36 which firmware did you used? Re: DTM configuration for KW36 Did you tried it over development board or your own application? Re: DTM configuration for KW36 Hi, Thanks for the response. It is not the test tool. It is a third-party tool and now it is working fine the issue was in address configuration. Thanks! Regards, Naven Suresh Re: DTM configuration for KW36 Hello, Are you using test tool? Could you please share with me the complete command you sent and the response ? Regards, Estephania
記事全体を表示
KW36 的 DTM 配置 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好estephania_martinez ‌, 我按照以下链接中的说明配置了KW36 DTM(通过2线UART接口)。 KW系列直接测试模式(DTM)配置 为了验证 DTM 的行为,我使用以下命令进行了测试。 1. LE RESET (a)0x0000 (b)0x0204 (c)0x0300 2. 低功耗发射器测试 0x8000 3. LE接收机测试 0x4000 4. LE 测试结束 0xC000 在上述命令中,LE Reset 命令在所有 3 个命令中均未通过,LE Test End 命令也失败了。 请您帮忙查看一下这个问题? 使用的硬件: USB 转 TTL 变流器(3.3V 逻辑电平) 谢谢您! 此致, 纳文·苏雷什 Re: DTM configuration for KW36 你使用的是哪个固件版本? Re: DTM configuration for KW36 您是在开发板上还是在您自己的应用程序中尝试过的? Re: DTM configuration for KW36 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您好, 谢谢你的回复。 它不是测试工具。这是一个第三方工具,现在运行正常,问题出在地址配置上。 谢谢您! 此致, 纳文·苏雷什 Re: DTM configuration for KW36 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好, 你使用的是测试工具吗?请问您能否将您发送的完整命令和响应分享给我? 此致, 埃斯特法尼亚
記事全体を表示
EB官方演示合辑 EB项目是按照以下步骤编制的: (1)修改 project_parameters.mk 文件 NXP2_2-1782092925146.png NXP2_3-1782092953674.png NXP2_4-1782092967359.png (2)由于使用了 S32DS,因此在 check_build_params.mk 文件中对与 T32 相关的内容进行了注释。 NXP2_5-1782093055565.png (3)“生成”是可以接受的。 NXP2_6-1782093128512.png (4)“make 版本”不正确。 NXP2_7-1782093250946.png 请问这是什么原因造成的?是否需要修改Makefile文件? Re: EB official demo compilation 您好@ NXP2 您选择的GCC版本不正确。 Senlent_0-1782107597492.png Re: EB official demo compilation 谢谢!
記事全体を表示
EB公式デモ集 EBプロジェクトは以下の手順に従ってコンパイルされました。 (1)project_parameters.mk ファイルを修正する NXP2_2-1782092925146.png NXP2_3-1782092953674.png NXP2_4-1782092967359.png (2)S32DSが使用されたため、T32に関連する内容がcheck_build_params.mkファイルに注釈付けされました。 NXP2_5-1782093055565.png (3)「生成する」は許容されます。 NXP2_6-1782093128512.png (4)「make build」は誤りです。 NXP2_7-1782093250946.png これが何が原因だったのか教えていただけますか?メイクファイルを変更する必要はありますか? Re: EB official demo compilation こんにちは@ NXP2 選択したGCCのバージョンが間違っています。 Senlent_0-1782107597492.png Re: EB official demo compilation ご回答をお待ちしています。
記事全体を表示
KW36のDTM構成 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、 estephania_martinez さん、 以下のリンクに記載されているようにKW36 DTMを設定しました(2線式UARTインターフェースを介して) KWファミリ向けの直接テストモード(DTM)構成  しかし、DTMの動作を確認するために、以下のコマンドを使用してテストしました。 1. LEリセット (a) 0x0000 (b) 0x0204 (c) 0x0300 2. LEトランスミッタ試験 0x8000 3. LEレシーバーテスト 0x4000 4. LEテスト終了 0xC000 上記のコマンドでは、LE Reset が 3 つのコマンドすべてで合格せず、LE Test End コマンドも失敗しています。 この問題を確認してもらえますか? 使用ハードウェア: USBからTTLへのコンバータ(3.3Vロジックレベル) よろしくお願いします! よろしくお願いいたします。 ナヴェン・スレシュ Re: DTM configuration for KW36 どのファームウェアを使用しましたか? Re: DTM configuration for KW36 開発ボードで試しましたか、それとも自分のアプリケーションで試しましたか? Re: DTM configuration for KW36 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、 ご回答ありがとうございます。 これはテストツールではありません。これはサードパーティ製のツールで、現在は正常に動作しています。問題はアドレス設定にありました。 よろしくお願いします! よろしくお願いいたします。 ナヴェン・スレシュ Re: DTM configuration for KW36 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、 テストツールを使用していますか?送ったコマンドの全文と返信内容を教えていただけますか? よろしくお願いいたします。 エステファニア
記事全体を表示
Ara-240 - NVM Memory Compatibility Guide The purpose of this document is to provide extended guidance for selection of compatible Non-Volatile Memory (NVM) devices that are supported by the Ara240 (aka Ara-2) processors. In all cases, it is strongly recommended to follow the memory layout guidelines outlined in the specific SoC requirement documents. Manufacturer Memory Part Number Capacity Renesas NOR SPI FLASH AT25SL321-UUE-T 32Mbit (4MB) ISSI NOR SPI FLASH IS25WJ032F-JTLE-TR 32Mbit (4MB) ISSI NOR SPI FLASH IS25WP032D-JBLE 32Mbit (4MB) Winbond NOR SPI FLASH W25Q16JVSNIQ 16Mbit (2MB) Winbond NOR SPI FLASH W25Q32JWUUIQ 32Mbit (4MB) Winbond NOR SPI FLASH W25Q64JWSSIQ 64Mbit (8MB) XMC NOR SPI FLASH XM25LU64CVIQT 64Mbit (8MB) Note 1: All memory parts are in production unless stated otherwise. Checked June 2026 Re: Ara-240 - NVM Memory Compatibility Guide Cross reference: Ara240 - LPDDR4 Memory Compatibility Guide
記事全体を表示
SJA1110 Rev. D ではホストへのトラップが機能しません SJA1110-EVMボードの開発に取り組んでおり、ホストプロセッサ(Cortex-M7)で特定のフレームを読み取るソフトウェアを作成しました。そのため、ボードに付属している「hello world」の例を使い、そこからアプリケーションを構築しました。 私はAutosar-RTDでS32DSを使っていました。 今はスイッチを使って別のボードに切り替えました。しかし、そのスイッチの異なるバージョンを使っています(Rev.D)設定をきちんと調整しました。 しかし、ホストプロセッサにトラップされるべきフレームを受信できません。トラップフラグを設定したL2エントリを使用してフレームをトラップしています。L2エントリが、私が捕捉しようとしているフレームで実際に使用されていることを確認しました。さらに、私は「乱交」が有効になっていることを確認しました。ホスト側からフレームを送信することも可能です。統計登録によると、受信されるはずのフレームはドロップされず、スイッチに入った後も消えてしまう(つまりL2ルールは有効ですが、ホストポートには届かない??)。 問題をさらに絞り込む方法や、ハードウェアの問題を確認または除外する方法がわかりません。 Re: Trap to host not working on SJA1110 Rev. D こんにちは、 @flxwly さん。 SJA1110-MGS-EVMでSJA1110Dを使っているのか、それともご自身のカスタムボードで使っているのか、教えていただけますか? オリジナルのSJA1110-EVMはSJA1110Aをベースとしていましたが、新しいSJA1110-MGS-EVMはSJA1110Dを使用しています。同時に、SJA1110ファミリはピン互換かつソフトウェア互換と説明されているため、トラップ・トゥ・ホストの概念自体が改訂ごとに異なるとは思えません。これは、一般的なRev.Dの制限というよりも、基板固有の構成の不一致である可能性が高いことを示しています。 EthTrcv_43_PHYの設定が適切に変更されていること、およびPHYインスタンスがEthSwt_43_SJA11XXに正しくマッピングされていることを確認してください。EthSwt_43_SJA11XX の MACConfigurationTable が、実際のボードのトポロジーに合わせて更新されていることを確認してください。使用されていないポートは無効にすべきです。 可能であれば、.mex ファイルも共有してください。設定を確認するためにファイルしてください。 よろしくお願いいたします。 パベル Re: Trap to host not working on SJA1110 Rev. D こんにちは、 @PavelL さん。 迅速なご対応ありがとうございます。直ったようです。どうやらデフォルトのVLAN 0を正しく設定し忘れていたようです。しかし、なぜL2エントリでフレームを他のポートにルーティングできるのにホストには行けないのか、やはり気になります。 私が自作した基板にはSJA1110Dが使用されています。.mexファイルを添付しました。私はS32SDK_SJA1110_RTM_1.0.0を使用しています。 よろしくお願いします、 ネポムク Re: Trap to host not working on SJA1110 Rev. D こんにちは、 @flxwly さん。 はい、この動作はVLANメンバーシップフィルタリングと一致しています。 L2エントリは一致して転送先を選択する可能性はありますが、フレームは対応するVLANに属するポートにのみ配信されます。デフォルトのVLAN 0が正しく設定されていなかった場合、他のポートへの転送は機能していた一方で、ホストポートはVMEMB_PORTに含まれていないためにフレームを受信できなかった可能性があります。 あなたの.mexファイルを確認しました。ファイルに加え、VLAN 0の修正に加えて、MACConfigurationTableやL2フォワーディングテーブルの未使用ポートをすべて無効にすることも検討し、実際のボードトポロジーにできるだけ近い構成に仕上げることを検討してください。 よろしくお願いいたします。 パベル Re: Trap to host not working on SJA1110 Rev. D こんにちは、 @flxwly さん。 ご注意ください:回答が解決済みとしてマークされると、元の質問はシステム上で追跡されなくなります。私は更新情報の購読メールしか受け取らず、それも時々見逃されることがあります。 さらにサポートが必要な場合は、新しいクエリを作成するのが最善の方法です。 よろしくお願いいたします。 パベル Re: Trap to host not working on SJA1110 Rev. D こんにちは、 @PavelL さん。 どうもありがとうございます。現在は意図したとおりに動作しています。しかし、インバンド制御拡張機能に関して、もう一つ質問があります。ホストからスイッチへのトレーラーフレームのトレーラーにはホストポート(0)が含まれていますか?UM11107の5.8.2.1のドキュメントには、ポートの設定方法について正確に記載されていません。ポートごとに1ビットだと想定していました。また、予告編の情報が完全に削除されていないようです。 よろしくお願いいたします。 ネポムク
記事全体を表示
NXP、链接器脚本和适用于 VS Code 的 MCUxpresso 扩展 编辑:目前我正在手动编辑链接器脚本,虽然可以正常工作,但我想知道是否有“更好”的方法。 我尝试使用 256KB 的辅助 SRAM 区域(链接器脚本中的 m_data2)作为我的 .bss 文件。部分 通常情况下,我只需要编辑项目的链接器脚本,然后从那里开始。这就是我在STM32环境下所做的。 但在我着手处理项目文件之前,先来看看 ./armgcc 的内容。项目下的文件夹是否已重新生成?(我对此表示怀疑,我只是想验证一下我的假设。) 另外,如果它们被重新生成,或者以其他方式,是否有更好的方法来使用我芯片上的辅助 256KB 同步动态随机存取存储器(SDRAM) 区域?默认情况下,它似乎没有映射到我的代码中的任何区域。 Re: NXP, Linker scripts, and MCUxpresso extension for VS Code 嗨@litch 你使用的是哪款芯片? BR 哈里
記事全体を表示
NXP, Linker scripts, and MCUxpresso extension for VS Code Edit: Currently hand editing the linker scripts and it works, but wondering if there isn't something "better" i should be doing. I am trying to use the 256KB secondary SRAM region (m_data2 in the linker scripts) as my .bss segment Normally, I'd just edit the linker scripts for my projects and go from there. That's what I do on my STM32 environments. But before I go and start ripping up project files, are the contents of the ./armgcc folder under the project regenerated ever? (I doubt it, I just want to check my assumptions) And also, if they are regenerated, or otherwise, is there a better way to use the secondary 256KB SDRAM region on my chip? By default it seems it's not mapped to any region in my code. Re: NXP, Linker scripts, and MCUxpresso extension for VS Code Hi @litch  Which chip you are using? BR Harry
記事全体を表示
The created control displays incorrectly after being aligned to the center. The simulated position also appears incorrect. Below the screen, I created a TabView. Tab1 contains a chart. Currently, if I manually align it, the simulated screen appears to be off-center to the right. However, if I use the program's center and bottom alignment options, it results in an image upload error. All of these are incorrect. 回复: 创建的控件位置在对齐局中后,出现显示不正常。模拟出来的位置也不正常的情况 Hi @qujun I tested it on my end.  Harry_Zhang_0-1782188126176.png I did not reproduce the issue you mentioned. Which version are you using? How to reproduce this problem? BR Harry
記事全体を表示
VS Code 用の NXP、リンカー スクリプト、および MCUxpresso 拡張機能 追記:現在はリンカースクリプトを手動で編集して動作させていますが、もっと「良い」方法があるのではないかと考えています。 256KBのセカンダリSRAM領域(リンカスクリプトのm_data2)を.bssとして使用しようとしていますセグメント 通常であれば、プロジェクトのリンカースクリプトを編集して、そこから作業を進めます。それが私がSTM32環境で行っていることです。 しかし、プロジェクトファイルを破壊し始める前に、./armgcc の内容はプロジェクト内のフォルダは再生成されたことがありますか?(そうは思わないけど、自分の推測が正しいか確認したいだけ) また、それらが再生される場合、あるいはそうでない場合、チップ上の256KBのセカンダリSDRAM領域をより有効に活用する方法はありますか?デフォルトでは、私のコードではどの領域にもマッピングされていないようです。 Re: NXP, Linker scripts, and MCUxpresso extension for VS Code こんにちは、 @litchさん どのチップを使用していますか? BR ハリー
記事全体を表示
S32K5 こんにちは。プロジェクト用にS32K5のデータシートの安全なアクセスを2日前からリクエストしていますが、返答がなく、どなたか助けていただけませんか? Re: S32K5 ハイ NXPと秘密保持契約(NDA)に署名したかどうか確認いただけますか? もしなければ、 https://www.nxp.com.cn/docs/en/user-guide/nxp-secure-access-rights-registration.pdf を参照してください。 既に有効なNDAをお持ちの場合は、PDFファイルを[email protected]までお送りください。   よろしくお願いします、 ロビン ------------------------------------------------------------------------------- 注記: この投稿があなたの質問への回答になっている場合は、「解決策として承認」ボタンをクリックしてください。ありがとう! - 前回の投稿から7週間Threadをフォローしており、その後の返信は無視しています もし後で関連する質問があれば、新しいThreadを開き、閉じたThreadを参照してください。 -------------------------------------------------------------------------------
記事全体を表示
作成したコントロールを中央に揃えると、表示が正しくありません。シミュレーションされた位置も正しくないようです。 画面の下にTabViewを作成しました。Tab1にはグラフが含まれています。現在、手動で位置を調整すると、シミュレーション画面が右にずれて表示されます。しかし、プログラムの中央揃えと下揃えのオプションを使用すると、画像アップロードエラーが発生します。これらはすべて正しくありません。 回复: 创建的控件位置在对齐局中后,出现显示不正常。模拟出来的位置也不正常的情况 こんにちは@qujun 私自身もテストしてみました。 Harry_Zhang_0-1782188126176.png ご指摘の症状は再現できませんでした。どのバージョンをお使いですか?この問題を再現するにはどうすればよいですか? BR ハリー
記事全体を表示
S32K5 您好,我两天前申请获取S32K5数据手册的安全访问权限,用于一个项目,但一直没有收到回复,请问有人可以帮帮我吗? Re: S32K5 HI 请问您是否已与恩智浦半导体签署保密协议(NDA)? 如果还没有,请参阅https://www.nxp.com.cn/docs/en/user-guide/nxp-secure-access-rights-registration.pdf 。 如果您已经签署了有效的保密协议,请将 pdf 文件发送至[email protected] 。   此致, 罗宾 ------------------------------------------------------------------------------- 笔记: - 如果此帖解答了您的问题,请点击“接受为解决方案”按钮。谢谢你! - 我们会持续关注帖子,从最后一条回复发出后持续7周,之后的回复将被忽略。 如果您之后有相关问题,请另开新帖并引用已关闭的帖子。 -------------------------------------------------------------------------------
記事全体を表示
Trap to host not working on SJA1110 Rev. D I've been working on the SJA1110-EVM board and created software to read certain frames on the host processor (Cortex-M7). For that I used the "hello world" example provided with the board and build the application from there.  I was using S32DS with Autosar-RTD. Now I switched to another board also using the SJA1110. However it is using a different revision of said switch (Rev. D). I made sure to adapt the configuration. However I can't receive any frames that should be trapped to host on the host processor there. I am trapping the frames via L2 entry with trap flag set. I made sure the L2 entry is actually used for the frames I am trying to trap. In addition I made sure that promiscuous is activated. I am also able to send frames from the host. According to the stat registers the frames, that should be received, are not dropped but still vanish after entering the switch (so the L2 rule works but they never reach the host port??). I am unsure how to narrow down the problem further and how to confirm or rule out any hardware problems. Re: Trap to host not working on SJA1110 Rev. D Hello @flxwly , Could you please clarify whether you are using SJA1110D on the SJA1110-MGS-EVM or on your own custom board? The original SJA1110-EVM was based on SJA1110A, while the newer SJA1110-MGS-EVM uses SJA1110D. At the same time, the SJA1110 family is described as pin-compatible and software-compatible, so I would not expect the trap-to-host concept itself to differ between revisions. This makes a board-specific configuration mismatch more likely than a generic Rev. D limitation. Please ensure that the EthTrcv_43_PHY configuration has been adapted accordingly and that the PHY instances are mapped correctly in EthSwt_43_SJA11XX. Please also verify that the MACConfigurationTable in EthSwt_43_SJA11XX has been updated to match your actual board topology. Unused ports should be disabled. If possible, please also share your .mex file so we can review the configuration. Best regards, Pavel Re: Trap to host not working on SJA1110 Rev. D Hello @PavelL , thank you for your quick response. I've seem to fixed it. It appears I missed to correctly configure the default VLAN 0. However I am still curious to why I could use the L2 entry to route my frames to other ports but not the host. My own custom board is using the SJA1110D.  I've attached the .mex. I am using S32SDK_SJA1110_RTM_1.0.0. Best regards, Nepomuk Re: Trap to host not working on SJA1110 Rev. D Hello @flxwly , Yes, this behavior is consistent with VLAN membership filtering. The L2 entry may still match and select the forwarding destination, but the frame will only be delivered to ports that are members of the corresponding VLAN. If default VLAN 0 was not configured correctly, it is possible that forwarding to other ports still worked while the host port could not receive the frame because it was not included in VMEMB_PORT. I have reviewed your .mex file and in addition to the VLAN 0 correction, you may also consider disabling all unused ports in the MACConfigurationTable as well as in the L2 Forwarding Table, so that the configuration matches your actual board topology as closely as possible. Best regards, Pavel Re: Trap to host not working on SJA1110 Rev. D Hello @PavelL, thank you very much. It is working as intended now. Still I have one more question regarding the in-band control extensions. Is the host port (0) included in the trailer for host-to-switch frames with trailer? The documentation in UM11107 under 5.8.2.1 does not state how exactly the ports should be set. I assumed its one bit per port. Also it seems the trailer information is not stripped completly. Best regards, Nepomuk Re: Trap to host not working on SJA1110 Rev. D Hello @flxwly , Please note: Once an answer is marked as a solution, the original query is no longer actively tracked in our system. I only receive subscription emails for updates and those can occasionally be missed. If you need further assistance, the best approach is to create a new query. Best regards, Pavel
記事全体を表示
创建的控件位置在对齐局中后,出现显示不正常。模拟出来的位置也不正常的情况 Screen下面做了一个tabview tab1里面放了一个chart现在是我如果手动对齐的话模拟出来画面偏右。如果用程序里面的局中对齐和下对齐就出现上传图片那样。全部是错误的。 回复: 创建的控件位置在对齐局中后,出现显示不正常。模拟出来的位置也不正常的情况 嗨@qujun 我这边测试过了。 Harry_Zhang_0-1782188126176.png 我没有重现您提到的问题。你使用的是哪个版本?如何重现此问题? BR 哈里
記事全体を表示
S32K5 Hi there i have requested a secure access for the S32K5 datasheet for a project since two days now but i have no response can anyone help me? Re: S32K5 Hi Could you please confirm whether you have signed a Non-Disclosure Agreement (NDA) with NXP? If not, please refer to https://www.nxp.com.cn/docs/en/user-guide/nxp-secure-access-rights-registration.pdf. If you already have a valid NDA in place, please send the pdf file to [email protected].   Best Regards, Robin ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
記事全体を表示