993145_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

993145_en-US

993145_en-US

DTM configuration for KW36

Hi estephania_martinez‌,

I configured KW36 DTM as mentioned in the below link (Through a 2-wire UART interface)

Direct Test Mode (DTM) Configurations for the KW family 

But to verify the DTM behavior I tested using the below commands

1. LE Reset 

    (a)  0x0000

    (b)  0x0204

    (c)  0x0300

2. LE Transmitter Test

      0x8000

3. LE Receiver Test

      0x4000

4. LE Test End

      0xC000

In the above-mentioned commands, LE Reset is not getting passed with all the 3 commands and LE Test End command is also failed.

Can you please check this issue?

Hardware used: USB to TTL converter (3.3v logic level)

Thanks!

Regards,

Naven Suresh

Re: DTM configuration for KW36

which firmware did you used?


Re: DTM configuration for KW36

Did you tried it over development board or your own application?


Re: DTM configuration for KW36

Hi,

Thanks for the response.

It is not the test tool. It is a third-party tool and now it is working fine the issue was in address configuration.

Thanks!

Regards,

Naven Suresh

Re: DTM configuration for KW36

Hello,

Are you using test tool? Could you please share with me the complete command you sent and the response ?

Regards,

Estephania

Tags (1)
No ratings
Version history
Last update:
‎06-23-2026 02:31 AM
Updated by: