Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
i.MX8ULP LPADC compare function Hello, I'm trying to use the i.MX8ULP ADC in comparator mode from the M33 core, specifically, setup the ADC such that if the conversion value falls below a threshold I get an interrupt to process the event. My understanding from the reference manual is that this should be possible: - setup the ADC with a fifo watermark of 1, so any data triggers the interrupt (this part works, in the example below I removed the interrupt code to make the code simpler) - setup the compare function with "Repeat compare until true", CVH/CVL appropriately and trigger will then sample the ADC continuously and raise the data once it is appropriate Unfortunately I've not been able to make the compare values work at all, the manual states that various operations are possible depending on CVL/CVH but none of them seemed to work for me using ADC1 / command 1 / trigger 1: Experimentally, I've seen: - CVL < CVH (manual says true if outside range e.g. val < CVL || val > CVH): value always returned (even if it falls within range) - CVH max, CVL set (should be less than CVL): maximum value is not specified so I wasn't sure, setting CVH to 0xfff or 0x1000 the value is always returned regardless of CVL, setting CVH to 0xffff the value is never returned - CVL min, CVH set (should be greater than CVH): value is always returned - CVL > CVH (should be inside range e.g. CVH < val < CVL): value is never returned Here's the code I used: lpadc_config_t adcConfig; LPADC_GetDefaultConfig(&adcConfig); adcConfig.FIFOWatermark = 0; adcConfig.enableAnalogPreliminary = true; LPADC_Init(ADC1, &adcConfig); lpadc_conv_trigger_config_t triggerConfig; LPADC_GetDefaultConvTriggerConfig(&triggerConfig); triggerConfig.targetCommandId = 1; triggerConfig.enableHardwareTrigger = true; LPADC_SetConvTriggerConfig(ADC1, 0, &triggerConfig); lpadc_conv_command_config_t commandConfig; LPADC_GetDefaultConvCommandConfig(&commandConfig); commandConfig.channelNumber = 5; commandConfig.sampleChannelMode = kLPADC_SampleChannelSingleEndSideB; commandConfig.sampleScaleMode = kLPADC_SampleFullScale; commandConfig.hardwareAverageMode = kLPADC_HardwareAverageCount2; commandConfig.hardwareCompareMode = kLPADC_HardwareCompareRepeatUntilTrue; commandConfig.hardwareCompareValueHigh = v_high; commandConfig.hardwareCompareValueLow = v_low; LPADC_SetConvCommandConfig(ADC1, 1, &commandConfig); SDK_DelayAtLeastUs(1000, SDK_DEVICE_MAXIMUM_CPU_CLOCK_FREQUENCY); LPADC_DoSoftwareTrigger(ADC1, 1 << 0); // this is LPADC_GetConvResultBlocking() with a timeout uint32_t tmp, cnt = 0; tmp = ((ADC_Type *)ADC1)->RESFIFO; while (ADC_RESFIFO_VALID_MASK != (tmp & ADC_RESFIFO_VALID_MASK) && cnt < 100000) { tmp = ((ADC_Type *)ADC1)->RESFIFO; cnt++; } if (ADC_RESFIFO_VALID_MASK != (tmp & ADC_RESFIFO_VALID_MASK)) { PRINTF("ADC timeout\r\n"); } else { tmp &= ADC_RESFIFO_D_MASK; tmp >>= 3; PRINTF("got %d (%#x) in %d\r\n", tmp, tmp, cnt); } I've also dumped registers, I'm confident the "compare repeat until true" part works because the STAT register considers the trigger/command to still be running, and I got identical results with "Store on true" setting (And fiddling with CV (compare value) while the command is running gets weird results, but properly returns the triggers that were waiting for condition to be true - I'm sure we're not supposed to change CV while running so let's ignore this bit) Here's registers while waiting for conversion, with CVL = 0xffe and CVH = 0x1 (so should return any value between the two): ADC1 0x280a2000 VERID: 0x200101a PARAM: 0xf041004 CTRL: 0x1 ^ ADCEN STAT: 0x1000800 ^ CMDACT 1, ADC_ACTIVE IE: 0 DE: 0 CFG: 0x10800000 ^ PWREN, PUDLY = 0x80 PAUSE: 0 TSTAT: 0 TCTRL[0]: 0x1000001 ^ TCMD = CMD1, HTEN (no difference when disabled) FCTRL: 0 CMD[0].CMDL: 0x2025 ^ CSCALE full-scale, ABSEL = B, CH5 CMD[0].CMDH: 0x1003 ^ AVGS = 2 conversions, CMPEN = repeat until true CV[0]: 0x10ffe ^ compare value, CVH=1 and CVL=0xffe Am I holding this wrong? Thanks, Dominique Re: i.MX8ULP LPADC compare function Thank you @joanxie  I can confirm shifting the compare value appear to work! (I need to slow down the adc clock because the ADC is sampling too fast, even with convPauseDelay = 1023, but that is something I can probably figure out) Is the shift something one is supposed to be aware of, or will the ADC_CV_CVL_SHIFT / ADC_CV_CVH_SHIFT macros in e.g. MIMX8UD5_cm33.h be updated so setting hardwareCompareValueHigh/Low just works? There's no example available at all in https://github.com/nxp-mcuxpresso/mcuxsdk-examples so I'd like to confirm what (if anything) will be updated to clarify this in the future (either the comment in fsl_lpadc.h describing hardwareCompareValueHigh or the device macro to make it work) -- if the macro is updated I'll need to be careful when updating the SDK, so it'd be great to know ahead of time to plan for it Thank you Re: i.MX8ULP LPADC compare function hardwardCompareValueHigh/Low stores the raw CV register values, you need to align them to the RESFIFO D-field format themselves, I checked internal data base, I didn't find  a confirmed SDK roadmap item indicating that the existing field-shift macros will be changed or that the driver will automatically apply this conversion. Re: i.MX8ULP LPADC compare function refer to the Table 725. Data result register format description of reference manual,  the data is D[14:3], for the compare value, I think you should 3bits shift , like commandConfig.hardwareCompareValueHigh = v_high << 3; //CVH=0x8 commandConfig.hardwareCompareValueLow = v_low << 3;//CVL=0x7ff0 Re: i.MX8ULP LPADC compare function Okay, I'll handle it in our code, thank you for confirming.
View full article
i.MX95 support for UYVY422 format Can i.MX95 support for UYVY422 format because in datasheet YUV422 is mentioned.  Serializer outputs UYVY422 format. I need to process this using i.MX95 ISI. Can this be possible.  I know that UYVY and YUV byte order is different. Is hardware byte swapping is supported before the data enters the ISI? Re: i.MX95 support for UYVY422 format Hi @Gobi  i.MX95 supports the UYVY422 format, which is the native default format for the CSI Pixel Formatter. And, The outputs UYVY422, which can be directly processed by the ISI without requiring hardware byte swapping. B.R
View full article
i.MX95 UYVY422フォーマットのサポート i.MX95はUYVY422フォーマットをサポートしていますか?データシートにYUV422が記載されています。 シリアライザはUYVY422形式で出力します。これをi.MX95 ISIを使用して処理する必要があります。これは可能なのでしょうか。 UYVYとYUVのバイト順序が異なることは承知しています。データがISIに入る前に、ハードウェアによるバイトスワッピングはサポートされていますか? Re: i.MX95 support for UYVY422 format こんにちは@ゴビ i.MX95はCSIピクセルフォーマターのネイティブデフォルトフォーマットであるUYVY422フォーマットをサポートしています。 また、出力はハードウェアのバイトスワッピングを必要とせず、ISIが直接処理できるUYVY422です。 B.R
View full article
i.MX95 支持 UYVY422 格式 i.MX95是否支持UYVY422格式?因为数据手册中提到了YUV422。 序列化器输出 UYVY422 格式。我需要使用 i.MX95 ISI 处理此问题。这有可能吗? 我知道 UYVY 和 YUV 的字节顺序不同。在数据进入ISI之前是否支持硬件字节交换? Re: i.MX95 support for UYVY422 format 嗨@戈壁 i.MX95 支持 UYVY422 格式,这是 CSI 像素格式化器的原生默认格式。 而且,输出 UYVY422 可以直接由 ISI 处理,无需硬件字节交换。 B.R
View full article
特定のフィットイメージにcsfヘッダーファイルが関連付けられていることを確認します。 セキュアブートは正常に動作しており、esbc_validateを使用してU-Bootが何をしているのかおおよそ理解しています。しかし、私は、cst 2.x で生成された特定のヘッダーファイルが、特定のフィット (カーネル、dtbs、ルートファイルシステム) イメージに関連付けられていることを検証するアップグレードユーティリティを作成しようとしています。 CSFセキュリティヘッダーを正しいオフセットに配置し、フィットイメージをオフセットに配置すれば、起動時には問題なく動作します。しかし、それらをそれぞれの場所に配置する前に、確認しておきたいのです。 公開鍵はCSFに埋め込まれているので、それを抽出しなければならないと理解しています。その後、少し混乱しています。RSA署名を抽出して、抽出した公開鍵を使ってハッシュを取得する必要があると思うのですが、そのハッシュは何らかの形でフィットイメージに関連付けられているものの、単にフィットイメージのハッシュではないのでしょうか? すでにSRKHを切れたヒューズから引き抜くことができたので比較できます。 今のところ、Google/Geminiはあまり役に立っていません。 ヒントをいただけますか? QorIQ LS1デバイス Re: Verify a csf header file is associated with a specific fit image. 署名は単にFITのハッシュではありません。このセキュアブートフローでは、CSFヘッダーのSHA-256ダイジェスト、そのヘッダーで指定されたイメージバイト、公開鍵マテリアル、および使用されている場合はSGテーブルを認証します。検証では、鍵と融合されたSRKHとの照合も行われます。 SO、どちらのファイルをインストールする前に、ユーティリティは候補ヘッダーを解析し、そのサイズとオフセットフィールドを使って候補FITから正しいバイトを選択し、署名済みデータのダイジェストを計算し、抽出したRSA署名を検証済み公開鍵で検証しなければなりません。検証が成功すると、そのヘッダーは認証済みのFITバイトに関連付けられます。FITのみのSHA-256比較では機能しません。
View full article
URLとバックリンクのための最高のインスタントインデックスツール、インスタントインデクサー2026 https://www.indexingurl.comを試してみてください あるいはお問い合わせ T g srma25 Whats app +8801602923484         評価ボード
View full article
Looking for FS5600 FRDM-K82F firmware I am restoring aFRDM-K82F that has been used with the KITFS5600FRDMEVM. It was set up some years ago and the files and knowledge for that have been difficult to find. I followed the firmware recovery procedure in UM11526. The OpenSDA firmware has been successfully restored and the board now enumerates as FRDM-K82FD. The next step in UM11526 requires the following firmware: nxp-gui-fw-frdmk82f-usb_hid-fs5600_xxx.bin The manual states that this file is located in the MCU folder of the NXP GUI package. However, the current NXPGUI_PR_11.1.0 package no longer contains the K82F firmware; its MCU directory only contains KL25Z and S32K144 firmware. Does anyone know where to find this frimware or an older NXPGUI package containing it? I only need the FS5600 application firmware at this point. The K20/OpenSDA bootloader and FRDM-K82F interface firmware are already working. Thanks in advance. PMIC for i.MX Re: Looking for FS5600 FRDM-K82F firmware Thank you guoweisun. It worked great and I will try to remember to use the support ticket when appropriate. Thank you! Re: Looking for FS5600 FRDM-K82F firmware Hi jbarns Please try to download from attached. By the way for DFAE please prioritize asking questions on salesforce submit ticket instead of in community.
View full article
LPC4088 U盘支持 你好。我正在 LPC4088 上实现 USB Host 功能,以支持 U 盘。该代码在 LPC QuickStart 板上运行正常,但无法枚举我们定制硬件上的设备。 具体来说,在枚举过程中,`USB_Host_SendControlRequest()` 返回 `HOST_SENDCONTROL_PipeError` 而不是 `HOST_SENDCONTROL_Successful`。我怀疑问题出在 `HcdControlTransfer()` 函数中,可能与管道配置有关,但我一直无法确定根本原因。 任何见解都将不胜感激。 LPC40xx Re: LPC4088 pendrive support 嗨@Nipperkin 由于相同的固件在 LPC4088 QuickStart 板上可以正常工作,因此问题很可能是硬件相关的,而不是 HcdControlTransfer() 本身的问题。我建议您查看: USB VBUS 5V 电源和电源开关控制 D+/D− 布线和引脚配置 USB 48 MHz 时钟配置 USB主机DMA结构(HCCA/ED/TD)在USB可访问RAM中的放置/对齐 BR 哈里
View full article
DDRCLK frequency of P1020 and P2020 Hello  I have a question about DDRCLK frequency of P1020 and P2020. The data sheets say that minimum DDRCLK frequency of P1020 is 66.66MHz and P2020 is 66.7MHz. Is this small gap from spec difference/change or is this just a result of rounding off to one decimal place? Best regards  Re: DDRCLK frequency of P1020 and P2020 This is a rounding difference only. Both devices specify a maximum DDRCLK period of 15 ns (≈66.67 MHz). P2020 rounds it to 66.7 MHz, while P1020 lists 66.66 MHz. Thanks Re: DDRCLK frequency of P1020 and P2020 Thank you June_Lu for your help. BR,
View full article
最佳URL和反向链接即时索引工具2026 试试https://www.indexingurl.com 或联系 T g srma25 WhatsApp +8801602923484         评估板
View full article
正在寻找 FS5600 FRDM-K82F 固件 我正在修复一台与 KITFS5600FRDMEVM 一起使用的 FRDM-K82F。它是几年前建立的,相关的文件和知识很难找到。 我按照UM11526中的固件恢复步骤进行了操作。OpenSDA 固件已成功恢复,现在板的型号为FRDM-K82FD。 UM11526 的下一步需要以下固件: nxp-gui-fw-frdmk82f-usb_hid-fs5600_xxx.bin 手册中指出,该文件位于NXP GUI软件包的MCU文件夹中。然而,当前的NXPGUI_PR_11.1.0软件包已不再包含K82F固件;其MCU目录仅包含KL25Z和S32K144固件。 请问有人知道哪里可以找到这个固件,或者包含它的旧版 NXPGUI 软件包吗? 目前我只需要FS5600应用固件。K20/OpenSDA引导加载程序和FRDM-K82F接口固件已经可以正常工作。 先行致谢。 i.MX 的 PMIC Re: Looking for FS5600 FRDM-K82F firmware 谢谢郭伟孙。效果很好,我会尽量记住在适当的时候使用支持工单。 谢谢! Re: Looking for FS5600 FRDM-K82F firmware 嗨 jbarns 请尝试从附件下载。 顺便提一下,DFAE 的各位,请优先在 Salesforce 提交工单中提问,而不是在社区中提问。
View full article
FS5600 FRDM-K82Fのファームウェアを探しています KITFS5600FRDMEVMで使用されていたFRDM-K82Fを修復しています。それは数年前に設置されたもので、それに関するファイルや知識を見つけるのは困難だった。 UM11526 に記載されているファームウェア復旧手順に従いました 。OpenSDAファームウェアは正常に復元され、ボードは FRDM-K82FD として認識されるようになりました 。 UM11526の次のステップでは、以下のファームウェアが必要です。 nxp-gui-fw-frdmk82f-usb_hid-fs5600_xxx.bin マニュアルには、このファイルはNXP GUIパッケージのMCUフォルダ内にあると記載されています。しかし、現在の NXPGUI_PR_11.1.0 パッケージにはもはやK82Fファームウェアは含まれていません。そのMCUディレクトリにはKL25ZとS32K144ファームウェアのみが入っています。 このフリムウェアや、古いNXPGUIパッケージが入っている場所をご存知の方はいませんか? 今はFS5600アプリケーションのファームウェアだけが必要です。K20/OpenSDAのブートローダーとFRDM-K82Fインターフェースのファームウェアはすでに動作しています。 よろしくお願いいたします。 i.MX用PMIC Re: Looking for FS5600 FRDM-K82F firmware ありがとうグオウェイサン。うまくいきましたし、適切なタイミングでサポートチケットを使うように心がけます。 ご回答をお待ちしています。 Re: Looking for FS5600 FRDM-K82F firmware こんにちは、jbarnsさん 添付ファイルからダウンロードしてみてください。 ちなみに、DFAEに関するご質問は、コミュニティではなくSalesforceのチケット送信フォームからお寄せいただくことを優先してください。
View full article
Best Instant Indexing Tool for URLs and Backlinks instant indexer 2026 try https://www.indexingurl.com   or contact T g  srma25 Whats app +8801602923484         Evaluation Board
View full article
FRDM-MCXN947のI3CインターフェースをI2C通信に使用した場合、Clkの伸縮機能は機能しませんでした こんにちは、現在問題に直面しています。FRDM-MCXN947のI3Cインターフェースを使ってI2C通信をしたいのですが、接続しているスレーブデバイスがデータ準備中にクロックストレッチが発生するため、データ転送が開始される前にスレーブデバイスがSCL信号を放出するのを待たなければなりません。 MCXNP184M150F70RM リファレンスファイルにある設定可能なレジスタ (MCONFIG[SKEW] = 0、MCONFIG[HKEEP] = 0b11、MCONFIG[MSTENA] = 0b11 など) を使ってみましたが、うまく動作しないようです。どうすれば解決できるでしょうか? #FRDM-MCXN947 #I3C 通信・制御(I3C |I2C |SPI |FlexCAN |イーサネット |FlexIO) MCX N Re: When using the FRDM-MCXN947's I3C interface for I2C communication, the Clk stretching capability こんにちは、 @kevin_Jhuang レジスタ設定は現在、I3C_MasterInit()より前に適用されているため、SDKの初期化によって上書きされることがあります。 有効にしてください: masterConfig->disableTimeout = true; 次に、I3C_MasterInit() の後に、MSTENA = 3、HKEEP = 3、SKEW = 0 を設定します。|= を使用する代わりに、対応するレジスタフィールドを書き込む前にクリアしてください。 初期化後、MCONFIGを読み込んで設定が有効になっていることを確認してください。クロックストレッチングの失敗直後に取得したMSTATUS値とMERRWARN値も提供してください。 SCLとSDAがオープンドレイン動作に設定されていること、および外部プルアップ抵抗が取り付けられていることも確認してください。 BR ハリー Re: When using the FRDM-MCXN947's I3C interface for I2C communication, the Clk stretching capability こんにちは、ハリーさん。 ご返信いただき、誠にありがとうございます。テストのために、MCONFIGを再度設定してみました。 1.テストでは、disableTimeoutをtrueに設定しました。 2. 画像は現在のレジスタ設定を示しており、MCONFIG、MSTATUS、MERRWARNの値やI2Cバス信号も含まれます。(構成Aと構成Bの違いはMSTENAの設定です。構成A:MCONFIG[MSTENA] = 3、構成B:MCONFIG[MSTENA] = 1)。 3. 例に従って、SDA/SCL IO ピンを openDrainEnable = kPORT_OpenDrainDisable に設定し、プルアップ抵抗 (4.7K) を接続する必要があります。存在する必要がある。 現時点では、I2Cバスの伸縮機能の実装が難しいようです。 Re: When using the FRDM-MCXN947's I3C interface for I2C communication, the Clk stretching capability 上記の回答に続いて、Bの画像を設定します。 ありがとう Re: When using the FRDM-MCXN947's I3C interface for I2C communication, the Clk stretching capability こんにちは、 @kevin_Jhuang 問題を再現でき、引き続き調査します。何か分かったことがあれば、またご連絡します。 BR ハリー Re: When using the FRDM-MCXN947's I3C interface for I2C communication, the Clk stretching capability こんにちは、 @kevin_Jhuang この件については社内チームに確認しました。彼らのテストに基づき、MSTENA = 11b(I2Cコントローラモード)を使用する場合、以下の条件も満たされるべきです。 PPBAUD = 0 I2CBAUD < 15 BR ハリー
View full article
MCXN947VKLT 包装规格 我在恩智浦的网站上找不到MCXN947VKLT的封装规格。 我可以在哪里找到这份文件? 谢谢! MCX N Re: MCXN947VKLT packing spec MCXN947VKLT的包装详情如下: 包装类型:托盘 托盘类型:可烘烤型,干包装多件装 最小包装数量:90 件 最低订购量:450件 封装:HLQFP100,100个引脚,引脚间距0.5 mm,封装尺寸14 × 14 × 1.5 mm 如果您正在寻找托盘图纸/规格及尺寸信息,请注意,此信息不公开,需要通过提交支持工单进行申请: https://support.nxp.com/s/? language=en_US 谢谢。 Re: MCXN947VKLT packing spec 感谢您的回复。我会通过工单跟进。
View full article
P1020 和 P2020 的 DDRCLK 频率 你好 我有一个关于P1020和P2020的DDRCLK频率的问题。 数据手册显示,P1020 的最低 DDRCLK 频率为 66.66MHz,P2020 的最低 DDRCLK 频率为 66.7MHz。 这个微小的差距是由于规格差异/变化造成的,还是仅仅因为四舍五入到小数点后一位造成的? 此致 Re: DDRCLK frequency of P1020 and P2020 这只是四舍五入造成的误差。 这两个设备的最大 DDRCLK 周期均为 15 ns(≈66.67 MHz)。P2020 将其四舍五入为 66.7 MHz,而 P1020 列出的是 66.66 MHz。 谢谢! Re: DDRCLK frequency of P1020 and P2020 感谢 June_Lu 的帮助。 BR,
View full article
LPC4088 ペンドライブのサポート こんにちは。ペンドライブ対応のためにLPC4088にUSB Host機能を実装しています。このコードはLPC QuickStartボード上では正しく動作しますが、当社独自のハードウェア上ではデバイスの列挙に失敗します。 具体的には、列挙時に `USB_Host_SendControlRequest()` が `HOST_SENDCONTROL_Successful` ではなく `HOST_SENDCONTROL_PipeError` を返します。問題は`HcdControlTransfer()`関数内にあると推測しており、おそらくパイプの設定に関連していると思われますが、根本原因を特定できていません。 何かご意見があれば大変ありがたいです。 LPC40xx Re: LPC4088 pendrive support こんにちは、 @Nipperkin さん。 同じファームウェアがLPC4088 QuickStartボードで正常に動作することから、問題はHcdControlTransfer()自体ではなく、ハードウェアに関連している可能性が高い。確認することをお勧めします: USB VBUS 5V 電源および電源スイッチ制御 D+/D− ルーティングおよびピン構成 USB 48 MHz クロック構成 USBアクセス可能なRAMにおけるUSBホストDMA構造(HCCA/ED/TD)の配置/アラインメント BR ハリー
View full article
P1020およびP2020のDDRCLK周波数 こんにちは P1020とP2020のDDRCLK周波数について質問があります。 データシートによると、P1020のDDRCLK最低周波数は66.66MHz、P2020は66.7MHzとされています。 このわずかな差は、仕様の違いや変更によるものですか、それとも単に小数点以下第1位への四捨五入の結果ですか? よろしくお願いします Re: DDRCLK frequency of P1020 and P2020 これは端数処理による差にすぎません。 両デバイスとも、最大DDRCLK周期は15ナノ秒(約66.67MHz)と規定している。P2020では66.7MHzと丸められているのに対し、P1020では66.66MHzと記載されている。 よろしくお願いします。 Re: DDRCLK frequency of P1020 and P2020 June_Luさん、ご協力ありがとうございました。 BR、
View full article
MCXN947VKLT 梱包仕様 NXPのウェブサイトでMCXN947VKLTの梱包仕様書を見つけることができませんでした。 この書類はどこで見つけられますか? よろしくお願いします。 MCX N Re: MCXN947VKLT packing spec MCXN947VKLTの梱包詳細は以下のとおりです。 梱包形態:トレイ トレイの種類:オーブン対応、ドライパック入り複数個 最低パッケージ数:90個 最小注文数量:450個 パッケージ:HLQFP100、端子100個、ピッチ0.5mm、ボディ14 × 14 × 1.5 mm ボディ 特にトレイの図面や寸法付きの仕様をお探しの場合は、この情報は公開されておらず、サポートチケットを通じてリクエストする必要があります。https://support.nxp.com/s/?language=en_US ありがとう。 Re: MCXN947VKLT packing spec ご回答ありがとうございます。チケットを通してフォローアップいたします。
View full article
LPC4088 pendrive support Hello. I am implementing USB Host functionality on the LPC4088 for pendrive support. The code works correctly on the LPC QuickStart board, but fails to enumerate devices on our custom hardware. Specifically, `USB_Host_SendControlRequest()` returns `HOST_SENDCONTROL_PipeError` instead of `HOST_SENDCONTROL_Successful` during enumeration. I suspect the issue lies within `HcdControlTransfer()`, possibly related to pipe configuration, but I have been unable to identify the root cause. Any insights would be greatly appreciated. LPC40xx Re: LPC4088 pendrive support Hi @Nipperkin  Since the same firmware works on the LPC4088 QuickStart board, the issue is likely hardware-related rather than in HcdControlTransfer() itself. I would recommend checking: USB VBUS 5V power and power-switch control D+/D− routing and pin configuration USB 48 MHz clock configuration Placement/alignment of USB Host DMA structures (HCCA/ED/TD) in USB-accessible RAM BR Harry
View full article