Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Logging ASM330LHH IMU Data to W25Q64JV External Flash Using S32K344 HI team I am working on an implementation where the ASM330LHH IMU sensor is interfaced with the S32K344 MCU, and the acquired sensor data (for example, accelerometer and gyroscope measurements) must be stored in a W25Q64JVSSIQ external QSPI Flash memory using S32 Design Studio (S32DS) 3.6.8. Currently, I am facing challenges in integrating the IMU data acquisition with the external Flash storage mechanism. I would appreciate guidance on the following topics: 1. External Flash (W25Q64JV) Enablement Through QSPI What are the recommended steps to configure the QuadSPI (QSPI) peripheral in S32K344 for interfacing with the W25Q64JV external Flash? I have already QSPI RTD drivers and configuration modules should be used in S32DS 3.6.8 How can the QSPI communication be validated after initialization? What is the recommended procedure to read the JEDEC ID and verify that the external Flash is detected correctly? 2. Integration of ASM330LHH Sensor Data with External Flash Storage What is the recommended software architecture for integrating the ASM330LHH sensor driver with the W25Q64JV Flash driver? What sequence should be followed to: Initialize the IMU sensor. Acquire accelerometer/gyroscope data. Buffer the sensor samples in RAM. Program the buffered data into external Flash memory. Are there any best practices for implementing page-aligned Flash writes, sector erase management, and circular logging mechanisms? How should timestamps and sensor records be organized to support efficient data retrieval? 3. Verification and Validation of Stored Data What is the recommended approach to verify that the IMU data stored in external Flash matches the originally acquired sensor data? Should read-back verification be performed after every page program operation? What validation methods are commonly used to ensure data integrity, such as: Flash read/write verification Checksum or CRC validation Memory dump analysis UART/CAN diagnostic logging How can the stored accelerometer and gyroscope data be compared against real-time sensor readings to confirm correctness?   Re: Logging ASM330LHH IMU Data to W25Q64JV External Flash Using S32K344 Hello @sharathkumar2026, 1. There is an already existing example for communicating with the on-board W25Q64 Winbond memory for the FRDM-A-S32K344 board in our Application Code Hub: QSPI Flash Memory Read/Write demo for FRDM-A-S32K344.  The example performs a device identification via JEDEC ID and status register readout, a continuous sector erase, page write, read-back, and data integrity verification, with RGB LED feedback via GPIO to indicate operation progress and pass/fail status. You can import it directly through S32DS:  2. The ASM330LHH is a third-party device, so you must look for its datasheet, or user manual in order to know which commands to send and how to read the data. I can recommend going over the Motion Sensing using FreeMASTER example. It reads 3-axis acceleration data from an FXLS8964AF accelerometer over LPI2C: It is based on S32K312, and uses FreeMASTER, however, it may prove useful to use it as reference. 3. This depends on the level of robustness your application needs. Read-back verification is usually not needed, simply check returned status after every operation and validate each record with CRC. Best regards, Julián
View full article
FRDM i.MX 95におけるDDR構成とテスト こんにちは、NXPコミュニティの皆さん、 私はUbuntu上でFRDM i.MX 95ボードを使用してi.MX 26.09用Config Toolsを使い始めたばかりの初心者です。 LPDDR4Xの設定方法、適切なDDRプリセットの選択方法、およびDDRテストの実行方法について指導が必要です。 DDRテストウィンドウでは、テストが「キューイング中」の状態のままになっており、シリアル接続またはUSB HIDオプションの設定方法がわかりません。 前提条件、DDRテストの実施、生成された設定をブートファームウェアに統合する手順など、正しいステップバイステップの手順を誰か説明してもらえますか? 参考のためにスクリーンショットを添付しました。公式のドキュメントや初心者向けのチュートリアルがあれば教えてください。 ご回答をお待ちしています。 Re: DDR Configuration and Testing on FRDM i.MX 95 ERR051301: DDRC:メモリコントローラのパフォーマンス低下 書き込みトラフィック記述中に特定の書き込みトランザクションのプロセッシング中に書き込み性能が低下します。回避策:書き込みパフォーマンスの低下を防ぐには、ビット7(値0x80)をDDRCレジスタ空間内のレジスタオフセット0xf04に設定します。注: 「*_timing.c」DDRツールによって生成されたファイルは回避策を実装しています AN15053 i.Mx9 での DDR クイックブートと AN14606 i.mx DDR ツール用設定ツールを使用したマルチボード設定の実行に関する参考情報 顧客ボードや公式評価キットを使っていますか?このエラーは低クロック周波数でも起こり得ますか? Re: DDR Configuration and Testing on FRDM i.MX 95 こんにちは、 @deepak_k さん。 現在、DDR設定ツールはUbuntu環境ではサポートされていません。そのため、設定ツールはWindows OS上で実行してください。 詳細な使用方法については、添付ファイル内の設定ツールのユーザーガイドをご参照ください。 B.R
View full article
FRDM i.MX 95 上的 DDR 配置和测试 NXP社区的各位朋友,大家好! 我是一名新手,正在使用 Ubuntu 系统上的 i.MX 26.09 版本配置工具,搭配 FRDM i.MX 95 板。 我需要有关如何配置 LPDDR4X、选择正确的 DDR 预设以及运行 DDR 测试的指导。 在 DDR 测试窗口中,测试一直处于“已排队”状态,我不确定如何配置串行连接或 USB HID 选项。 能否请哪位解释一下正确的步骤,包括前提条件、运行 DDR 测试以及将生成的配置集成到启动固件中? 我附上了截图供您参考。任何官方文档或适合初学者的教程都将不胜感激。 谢谢! Re: DDR Configuration and Testing on FRDM i.MX 95 ERR051301: DDRC: 内存控制器性能在写入流量期间下降 描述 在处理某些写入事务期间,写入性能下降。解决方法:为防止写入性能下降,将 DDRC 寄存器空间内寄存器偏移量 0xf04 的位 7(值为 0x80)设置为 0x80。注意:"*_timing.c"DDR 工具生成的文件实现了该变通方案。 供参考:AN15053 DDR 快速启动(适用于 i.MX9 和 AN14606),以及使用 i.MX DDR 配置工具运行多板设置 你们使用的是客户提供的评测板还是官方评测工具包?这种错误会在低时钟频率下发生吗? Re: DDR Configuration and Testing on FRDM i.MX 95 嗨@deepak_k 目前,DDR 配置工具在 Ubuntu 环境下不受支持;因此,请确保在 Windows 操作系统上运行配置工具。 有关详细使用说明,请参阅附件中的配置工具用户指南。 B.R
View full article
使用 S32K344 将 ASM330LHH IMU 数据记录到 W25Q64JV 外部闪存 大家好 我正在开发一个实现方案,其中ASM330LHH IMU 传感器与S32K344 MCU连接,并且必须使用S32 Design Studio (S32DS) 3.6.8将采集到的传感器数据(例如,加速度计和陀螺仪测量值)存储在W25Q64JVSSIQ 外部 QSPI Flash 存储器中。 目前,我在将IMU数据采集与外部闪存存储机制集成方面面临挑战。 我希望就以下几个方面获得指导: 1. 通过 QSPI 启用外部闪存 (W25Q64JV) 在 S32K344 中配置QuadSPI (QSPI) 外设以与 W25Q64JV 外部 Flash 连接时,推荐的步骤是什么? 我已经有了QSPI RTD驱动程序,并且需要在S32DS 3.6.8中使用配置模块。 初始化后如何验证QSPI通信? 读取 JEDEC ID 并验证外部闪存是否被正确检测到的推荐步骤是什么? 2. 将 ASM330LHH 传感器数据与外部闪存存储集成 将ASM330LHH 传感器驱动程序与W25Q64JV Flash 驱动程序集成,推荐的软件架构是什么? 应该按照什么顺序进行: 初始化IMU传感器。 获取加速度计/陀螺仪数据。 将传感器样本缓存到内存中。 将缓存的数据编程到外部闪存中。 对于实现页对齐闪存写入、扇区擦除管理和循环日志记录机制,有哪些最佳实践? 应如何组织时间戳和传感器记录以支持高效的数据检索? 3. 存储数据的验证和确认 验证存储在外部闪存中的 IMU 数据与原始采集的传感器数据是否匹配的推荐方法是什么? 每次页面程序操作后是否都应该执行回读验证? 常用的数据完整性验证方法有哪些?例如: 闪存读写验证 校验和或 CRC 验证 内存转储分析 UART/CAN诊断日志记录 如何将存储的加速度计和陀螺仪数据与实时传感器读数进行比较,以确认其正确性?   Re: Logging ASM330LHH IMU Data to W25Q64JV External Flash Using S32K344 你好@sharathkumar2026 , 1.在我们的应用程序代码中心,已经有一个与 FRDM-A-S32K344 板载 W25Q64 Winbond 存储器通信的示例: FRDM-A-S32K344 的 QSPI Flash Memory Read/Write demo 。 该示例通过 JEDEC ID 和状态寄存器读取执行设备识别、连续扇区擦除、页面写入、读取和数据完整性验证,并通过 GPIO 使用 RGB LED 反馈来指示操作进度和通过/失败状态。 您可以通过S32DS直接导入: 2. ASM330LHH 是第三方设备,因此您必须查找其数据手册或用户手册,才能知道要发送哪些命令以及如何读取数据。 我建议您参考一下使用 FreeMASTER 进行运动传感的示例。它通过 LPI2C 协议读取FXLS8964AF加速度计的三轴加速度数据:该示例基于 S32K312 协议,并使用了 FreeMASTER 库,但您可以将其作为参考。 3. 这取决于您的应用程序所需的健壮性级别。通常不需要回读验证,只需在每次操作后检查返回状态并使用 CRC 验证每个记录即可。 此致, 朱利安
View full article
s32k396 Basic Secure Boot qeustion 32K396 上使用 HSE FW 0.2.50.0 FULL_MEM,当前生命周期为 CUST_DEL。 测试过程:原始运行正常,现在修改认证范围内的地址 0x00453FF0 从 0xFF 修改为 0xFE,保持 AppBL Header、认证标签和 IVT 不变,IVT bootCfgWord 为 0x00000009。板卡断电重新上电后,使用 J-Link Attach 连接,不下载镜像,并通过空 SetupTarget 禁用了连接时的 RAM/ECC 初始化。此时 PC 停在 0x2040012E,0x2040012C~0x2040012E 的指令为 WFI 和跳回 WFI 的分支,符合 JTAG Recovery 等待循环,目前未配置用户 Secure Recovery 应用。 问题:请确认该版本在 BSB 认证失败后的完整处理流程及可靠判据:为什么已经进入 JTAG Recovery 等待循环,GPR3 bit5 仍为 0,是否与该位仅表示“SBAF 引导应用核进入 Recovery”、而本次恢复路径由 HSE FW 触发有关,以及应该通过哪个状态位或错误信息明确确认失败原因是 AppBL 认证不通过? Re: s32k396 Basic Secure Boot qeustion 感谢您提供的详细测试说明。这里需要指出的是,没有配置任何用户安全恢复应用程序。 请问您能否详细说明一下在您的配置中,恢复流程是如何工作的?尤其: 如果未配置安全恢复应用程序,AppBL 身份验证失败后预期会采取什么恢复措施? 是否已明确配置并启用 JTAG 恢复功能? 观察到的 WFI 回路本身是否被认为是意外的,还是仅仅担心 GPR3[5] 仍然被清除? 请提供与 J-Link 连接后立即读取的相关恢复配置和 HSE/SBAF 状态信息。 如果没有配置用户安全恢复应用程序,则可能会出现 WFI 循环。因此,请先明确AppBL认证失败后的预期恢复流程和设备预期行为。 Re: s32k396 Basic Secure Boot qeustion 观察到这个gpr3的bit5没有置位,这是个标志位,手册里面写的恢复模式会置1,为啥没回复?具体测试为附件
View full article
AMMCLIB 1.1.44を提供してください。S32DSプラグインはRTD 7.0.0と互換性があります。 こんにちは、S32 Design StudioにAMMCLIBプラグインをインストールした際にバージョン依存の問題に直面しました。 私は同僚と同じプロジェクトに取り組んでおり、両者ともRTDバージョン7.0.0とS32DSバージョン3.6以上を使用しています。私の同僚がAMMCLIB 1.1.44をインストールしました。正常に動作しています。しかし、S32DSの拡張機能とアップデートではAMMCLIB 1.1.46しか見つかりません。 バージョン1.1.46をインストールする際、プロンプトには、以下の依存関係が不足していることを示しています。 必要な依存関係が見落とされていること: com.nxp.RTD.S32K3_S32M27X 7.0.1は見つかりませんでした。 欠けている要件: com.nxp.AMMCLIB.S32K3xx.root.feature.feature.group 1.1.46.202609081018 は必要です com.nxp.RTD.S32K3_S32M27X.feature.feature.group [7.0.1,99.99.99) チームの開発環境の一貫性を維持するため、RTD 7.0.0 を引き続き使用したいと考えています。+ AMMCLIB 1.1.44、RTDプラグイン方法を通じてそれらを統合します。 以下の点を確認するのをご協力ください: 1. AMMCLIB 1.1.44用のS32DSプラグインのダウンロードリンク、過去の更新サイト、またはオフラインインストールパッケージを提供していただけますか?S32K3xx用ですか? 2. このプラグインは、具体的にどのS32DSバージョンとアップデートをサポートしていますか?RTD 7.0.0と互換性がありますか? 3.もし旧バージョンの公式ダウンロードがもう入手できない場合、同僚のすでにインストールされている1.1.44からプラグインを入手・インストールするサポート方法はありますか?環境? 必要なのはS32DSプラグイン/更新サイトインストールパッケージで、S32設定ツールを使ってAMMCLIBコンポーネントを追加しコードを生成することです。 添付ファイルは、インストール失敗を示すエラーメッセージのスクリーンショットです。ありがとう! Re: Please provide the AMMCLIB 1.1.44 S32DS plugin compatible with RTD 7.0.0 こんにちは、 @feixingren1さん S32DS拡張およびアップデートを通じて利用可能なAMMCLibパッケージは、パッケージ名からも示すようにRTDに依存しています。つまり、特定のRTDバージョンに対応して設計されており、ソフトウェア依存関係もインストールする必要があります。あなたの場合、エラーメッセージはパッケージにRTD 7.0.1が必要であることを示しています。したがって、必要なRTDバージョンとその依存関係がS32DSのインストールに存在しない限り、インストールは完了できません。 あなたが特にAMMCLib v1.1.44に興味を持っているため、S32DS Extensions and Updates を通じて入手できるバージョンをインストールする必要はありません。代わりに、 オートモーティブ Math and モータ制御 Library Set for S32K3から、希望のバージョンのスタンドアロンパッケージを直接ダウンロードできます。 統合に関しては、NXP S32K3xx、MWCT2DxxS、MWCT20xxS Devices向けオートモーティブ数学・モータ制御ライブラリセットユーザーマニュアルには、ライブラリをS32 Design Studio for S32 Platformに単独で統合する方法を説明した専用セクションがあります。 BR、VaneB
View full article
KEILとLID2634の互換性 コミュニティの皆さん、こんにちは。 LID2634ボードの購入手続きを進めております。 しかし、NXPファームウェアを書き込むには、KEIL MDK 5.36のライセンスが必要です。(私はこの分野は初心者です。) 問い合わせたところ、KEILは現在バージョン6を提供しているとのことでしたが、それ以前のバージョンで作業するには、KEILからプロフェッショナルライセンスを購入する必要があるとのことでした。 私の質問は以下の通りです。 1.KEILのプロフェッショナルライセンスは必須ですか、それともKEIL 5.36が必須ですか?そうでなければ、Essential/Communityライセンスで進めるべきでしょうか? 2. 文書にはKEIL 5.36バージョンしか記載されていなかった。購入前に、コンパイラやデバッガのオプションなど、互換性に関する他の事項も確認しておくべきでしょうか? 3. CASのサンプルコードのほとんどがPythonで書かれているようですが、これはKEILはファームウェアの書き込みにのみ使用し、残りのPythonベースのロジックはオンボードコンピュータに組み込むという意味でしょうか?NXPのMACレイヤー上で作業する予定がある場合。 4. また、ボードの設定、マルチタグやマルチアンカーの設定など、すぐに始められる設定例やgitリポジトリがあれば教えていただきたいです。 ありがとう Re: KEIL compatibility with LID2634 こんにちは、 あなたの調子が良いといいのですが。ご不便をおかけして申し訳ありませんが、この製品の情報はNDA(秘密保持契約)に基づいており、公開されていません。この情報を共有する安全なチャネルではなく、同じ理由で私もデータを持っていません。 このため、代理店ネットワークに掲載されている当社の代理店のいずれかにご連絡いただくことをお勧めします。NXP。また、この製品やIC取得の際に直接のお問い合わせがいれば、直接連絡を取ってください。 ご迷惑をおかけして申し訳ございません。 よろしくお願いいたします。 リカルド
View full article
Can_43_LLCE 1.0.9 (S32G): ビルド後のロード可能な構成はサポートされていますか、または予定されていますか? こんにちは、 「CAN_LLCEと LLCE_Af Postbuild Loadable をサポートしているのか?」についてフォローアップしています(2025年4月)NXPのサポートはCan_43_LLCEの「ポストビルドモデル」と答えました。ロード可能な問題が未解決のまま残された。CAN_LLCEとLLCE_AfはPostbuild Loadableをサポートしていますか?- NXPコミュニティ セットアップ: S32G274A、S32G_LLCE_1_0_9 (Can_43_LLCE 1.0.9、RTD AUTOSAR 4.4)。 目標:CANの設定をビルド後読み込み可能に更新し、アプリケーションイメージ全体を再フラッシュせずに実現すること。 1.0.9パッケージでは、以下の通りです: ポストビルドテーブルは絶対ポインタを持つコンスタント構造体で、アプリケーションイメージにコンパイルされます。 ビルド後のデータ用のロード可能または再配置可能なフォーマット、Sレコード出力、またはローダーは見つかりませんでした。 質問: Can_43_LLCEでは、ビルド後のロード可能な設定がサポートされていますか、または予定されていますか?はいの場合、どのバージョンで、いつからですか? もしそうでなければ、完全な再フラッシュなしでCANフィルターを更新するサポート方法は何ですか? Can_43_LLCEやLlce_Afでのポストビルドに関するアプリケーションノートはありますか? 前もって感謝します、 アイマン Re: Can_43_LLCE 1.0.9 (S32G): is post-build loadable configuration supported or planned? こんにちは、アイマンユニスさん お問い合わせいただき、また情報をお寄せいただきありがとうございます。 ご質問を拝受いたしました。確認させていただきます。 BR ジョーイ Re: Can_43_LLCE 1.0.9 (S32G): is post-build loadable configuration supported or planned? こんにちは、アイマンユニスさん お問い合わせいただきありがとうございます。 最新のLLCEマニュアルによると、現在、CAN_LLCEとLLCE_AfはPostbuild Loadableをサポートしていません。この機能を追加する具体的な計画はありません。 社内からの提案によると、お客様が新しい変更リクエストを提案したい場合、マーケティング部門に相談する必要があります。より詳細な企業情報を提供する必要があります。 現在、参考となる関連資料はございません。ご迷惑をおかけして申し訳ございません。 BR ジョーイ
View full article
KW47: Is it necessary to wait for gAdvertisingStateChanged_c before calling Gap_StartAdvertising? Hello, I am implementing advertising control on the KW47. To stop advertising, I use Gap_StopAdvertising(). However, there are cases where I would like to start advertising again before receiving the gAdvertisingStateChanged_c event after issuing the stop request. In this situation, is it safe to call Gap_StartAdvertising() while the Gap_StopAdvertising() operation is still in progress? Specifically, which of the following sequences is recommended? --- Gap_StopAdvertising() ↓ Wait for gAdvertisingStateChanged_c ↓ Gap_StartAdvertising() ---- or --- Gap_StopAdvertising() ↓ Gap_StartAdvertising() --- Does the SDK handle the state transition internally, or is it necessary to wait for the gAdvertisingStateChanged_c event that indicates advertising has stopped before calling Gap_StartAdvertising()? Thank you for your support. Best regards. Protocol: Bluetooth Re: KW47: Is it necessary to wait for gAdvertisingStateChanged_c before calling Gap_StartAdvertising Hello @hyama, Could you provide a more context on the scenario where you would like to restart advertising before receiving the gAdvertisingStateChanged_c event? The recommended approach is to wait for the gAdvertisingStateChanged_c event to verify that the advertising state transition has completed successfully. While Gap_StopAdvertising() initiates the procedure, the callback confirms the result of the operation. For example, instead of receiving a gAdvertisingStateChanged_c event, the application may receive a gAdvertisingCommandFailed_c event indicating that the requested operation could not be completed. BR Habib Re: KW47: Is it necessary to wait for gAdvertisingStateChanged_c before calling Gap_StartAdvertising Thank you for the clarification. We asked this question because we expected the SDK might internally handle the stop and start requests in sequence, even if Gap_StartAdvertising() was called before receiving the gAdvertisingStateChanged_c event. Since waiting for the gAdvertisingStateChanged_c event is the recommended approach, we will modify our implementation accordingly. Thank you for your support.
View full article
S32R41:Cortex-M7ロックステップ機能の有効化と検証方法 NXPチームの皆様、こんにちは。 NXP S32R41の自動車用レーダーSoCを扱い、デバッグにはLauterbach TRACE32を使っています。 S32R41のCortex-M7コアのハードウェアロックステップ機能を有効にして検証する方法を理解したいです。 以下の質問について、教えていただけますか? ロックステップを有効にする方法: S32R41ではCortex-M7のロックステップモードはデフォルトで有効ですか?それとも設定が必要ですか?設定が必要な場合、具体的な手順は何でしょうか?ハードウェア設定、DCFレコード、起動ソフトウェア、または特定のレジスタで制御されますか? 構成レジスタ: S32R41固有のレジスタやビットフィールドは、ロックステップが有効かどうかを示しますか?レジスタ名、アドレス、ビット位置、期待値をご提供ください。 ロックステップの検証方法: Cortex-M7コアが独立モードではなく、実際にハードウェアのロックステップモードで動作していることを確認するにはどうすればよいですか?設定レジスタの確認だけで十分ですか、それとも追加のステータスレジスタが必要ですか? ロックステップエラー検出: どのレジスタがロックステップコンパレータの状態を示しますか?コンパレータが正しく動作しているか、またロックステップの不一致が検出されていないかをどうやって判断すればよいですか? TRACE32デバッグ:ロックステップ構成とステータスを検査するための推奨されるTRACE32コマンドシーケンスまたはデバッグ手順はありますか? ドキュメント: S32R41リファレンスマニュアル、セーフティマニュアル、またはロックステップの設定および検証手順を説明した他の公式文書の関連セクションを教えていただけますか? ロックステップ機能が正しく有効化されていること、そしてその動作がS32R41専用のドキュメント化された方法で検証できることを確認したいのです。 なお、私はS32R41について質問しており、S32K3ファミリについてはお願いしているので、S32R41に適用されるレジスタの定義や手順を教えていただけると助かります。 再開まで今しばらくお待ちください。 よろしくお願いいたします。 Re: S32R41: How to Enable and Verify Cortex-M7 Lockstep Functionality こんにちは、 S32R41では、Cortex-M7プロセッサがハードウェアのロックステップコアペアとして実装されています。ロックステップ操作はS32R41のハードウェア構成の一部であり、アプリケーションソフトウェア、スタートアップコード、またはS32K3スタイルのUTEST_MISC[LOCKSTEP_EN] DCFレコードによって有効化されるわけではありません。NXP S32R41の製品情報には、Cortex-M7の実装がロックステップコア構成であると明示的に記述されています。 1.ソフトウェアの有効化シーケンスは必要ありません 2. 設定はS32K3レジスタを使用して検証してはならない。 3. デバッガーの可視性は実用的なアーキテクチャ上の指標を提供する TRACE32論理的なCortex-M7プロセッサに接続されます。冗長なチェッカーコアを、独立してデバッグ可能な追加のCortex-M7として提示するわけではありません。したがって、各ロックステップペアの機能的なメンバーのみがデバッグ対象として表示されることが想定されます。 4. 同期不一致の報告 Cortex-M7のロックステップ比較ロジックで検出された不一致は、S32R41のセーフティ故障管理経路を通じて報告されます。アプリケーションは対応するFCCU故障およびその必要な反応をS32R41セーフティマニュアルに従って設定しなければなりません。 5. ロックステップを有効にするために特別なTRACE32コマンドは必要ありません。 6. 以下のS32R41関連文書を参照してください。 S32R41リファレンスマニュアル、特にCortex-M7、FCCUおよびリセット/故障管理の章; S32R41セーフティマニュアル、特にCortex-M7のロックステップ実行、ロックステップ比較、FCCU故障処理に関する安全機構; 該当するS32R41改訂版に関連するデバイス固有のFCCU故障マッピング、 サポートされたS32R41ソフトウェア/デバッグパッケージに付属していたTRACE32 S32R41の起動スクリプト。 よろしくお願いいたします。 ピーター
View full article
[S32K3] about LVD Interrupt Hello, I am trying to use the LVD interrupt feature on the S32K3 MCU. I set LVDIEEnable = true in the MCU configuration. Although 5V is currently supplied to the MCU, Power_Ip_PMC_VoltageErrorIsr() keeps being triggered continuously. I would like to ask if this is normal behavior, or if I have misconfigured something. Re: [S32K3] about LVD Interrupt Hello, @danielmartynek  A voltage of 5V is being applied to the following pins: Using a 100-pin MCU (FS32K312NHT0VPAST) VREFH: PIN 8 VDD_HV_A: PIN 10 VDD_HV_A-2: PIN 37 VDD_HV_A-3: PIN 62 VDD_HV_A-4: PIN 87 Although 5V is supplied, the LVD5AF flag register keeps being set. Are there any additional points or registers I should check? BRs, Sean Re: [S32K3] about LVD Interrupt Hi @ssean, If LVD5AF stays set after you clear it. The voltage must be lower than the specified threshold: Can you measure the voltage? Thanks, Daniel Re: [S32K3] about LVD Interrupt Can you please specif the part number? Which RTD revision do you use? Thank you, Daniel Re: [S32K3] about LVD Interrupt Hello @danielmartynek  I am currently using RTD 4.0.0 HF04. I identified a few errors in the RTD code as well as an issue in my configuration. After making the necessary adjustments, I confirmed that the interrupt is triggered properly at the LVD voltage level. Thank you for your support. BRs, Sean Sung
View full article
[S32K3] 关于 低压检测 中断 你好, 我正在尝试在 S32K3 MCU 上使用 低压检测 中断功能。 我在MCU配置中设置了LVDIEEnable = true。 虽然目前已向 MCU 提供 5V 电压,但 Power_Ip_PMC_VoltageErrorIsr() 仍然持续触发信号。 我想请问这是正常现象吗?还是我的配置出了问题? Re: [S32K3] about LVD Interrupt 你好, @danielmartynek 在以下引脚上施加 5V 电压: 使用100引脚MCU(FS32K312NHT0VPAST) VREFH:引脚 8 VDD_HV_A:引脚 10 VDD_HV_A-2:引脚 37 VDD_HV_A-3:引脚 62 VDD_HV_A-4:引脚 87 虽然提供了 5V 电压,但 LVD5AF 标志寄存器仍然被置位。 还有其他需要检查的地方或登记簿吗? BRs, 肖恩 Re: [S32K3] about LVD Interrupt 嗨@ssean , 如果清除 LVD5AF 后它仍然保持设置状态。 电压必须低于规定的阈值: 你能测量一下电压吗? 谢谢! 丹尼尔 Re: [S32K3] about LVD Interrupt 请问可以提供零件编号吗? 你使用的是哪个版本的RTD? 谢谢! 丹尼尔 Re: [S32K3] about LVD Interrupt 你好@danielmartynek 我目前使用的是 RTD 4.0.0 版本。HF04。 我发现 RTD 代码中存在一些错误,我的配置中也存在一个问题。 经过必要的调整后,我确认在低压检测电压等级下可以正确触发中断。 感谢您的支持。 BRs, 宋
View full article
KEIL compatibility with LID2634 Hello community, We are in progress of purchasing LID2634 board. But to flash the NXP firmware there is a need of KEIL MDK 5.36 license. (Am new to this). When enquired KEIL has version of 6 right now - but if I wish to work on backward versions I must buy Professional License from them. My questions are : 1. Is Professional License of KEIL is must, or KEIL 5.36 is must? Else should I go ahead with Essential/Community license? 2. Documents had mentioned only KEIL 5.36 version. Should I also ensure other things like compiler, debugger options for compatibility before purchase. 3. I see most of the CAS example samples are in python - Does that mean I will use KEIL only for flashing firmware and rest of the python based logics go inside onboard computer? If I'm planning to work on top of NXPs MAC layer. 4. I also wish to know any examples or git repo available on setting up the board, Multi Tag and Multi Anchor configured setups etc to quickly start with. Thanks Re: KEIL compatibility with LID2634 Hello, Hope you are doing well. Sorry for the inconvenience this might cause you but as the information of this product it's under NDA (Non-Disclosure Agreement) the information it's not public, this is not a secure channel to share any information of this device, and I do not have the data as well for the same reason. For this reason, I recommend you contacting one of our distributors available in the Distributor Network|NXP. Or if you have a direct contact who helped you with information about this product or getting the IC in a first place, please communicate directly with him/her. I apologize for the inconveniences this might cause you. Best Regards, Ricardo
View full article
Please provide the AMMCLIB 1.1.44 S32DS plugin compatible with RTD 7.0.0 Hello, I encountered a version dependency issue when installing the AMMCLIB plugin in S32 Design Studio. I am collaborating with a colleague on the same project, and we are both using RTD version 7.0.0 and S32DS versions above 3.6. My colleague has installed AMMCLIB 1.1.44 and it is functioning normally; however, in my S32DS Extensions and Updates, I can only find AMMCLIB 1.1.46. When installing version 1.1.46, a prompt indicates that the following dependencies are missing: Missing required dependency: com.nxp.RTD.S32K3_S32M27X 7.0.1 could not be found. Missing requirement: com.nxp.AMMCLIB.S32K3xx.root.feature.feature.group 1.1.46.202609081018 requires com.nxp.RTD.S32K3_S32M27X.feature.feature.group [7.0.1,99.99.99) To maintain consistency in our team's development environment, we hope to continue using RTD 7.0.0 + AMMCLIB 1.1.44, integrating them through the RTD plugin method. Please assist in confirming: 1. Can you provide the download link, historical update site, or offline installation package for the S32DS plugin for AMMCLIB 1.1.44 for S32K3xx? 2. Which specific S32DS versions and updates are supported by this plugin? Is it compatible with RTD 7.0.0? 3. If the official download for the old version is no longer available, is there a supported method to obtain and install the plugin from a colleague's already installed 1.1.44 environment? What we need is the S32DS plugin/update site installation package, so as to use the S32 Configuration Tools to add the AMMCLIB component and generate code. The attachment is a screenshot of the error message indicating the installation failure. Thank you! Re: Please provide the AMMCLIB 1.1.44 S32DS plugin compatible with RTD 7.0.0 Hi @feixingren1  The AMMCLib package available through S32DS Extensions and Updates is RTD-dependent, as indicated by the package name. This means that it is designed to work with specific RTD versions and has software dependencies that must also be installed. In your case, the error message indicates that the package requires RTD 7.0.1, so the installation cannot be completed unless the required RTD version and its associated dependencies are present in your S32DS installation. Since you are specifically interested in AMMCLib v1.1.44, there is no need to install the version available through S32DS Extensions and Updates. Instead, you can download the standalone package for the desired version directly from Automotive Math and Motor Control Library Set for S32K3. Regarding integration, the User Manual for Automotive Math and Motor Control Library Set for NXP S32K3xx, MWCT2DxxS, and MWCT20xxS Devices includes a dedicated section that explains how to integrate the library into S32 Design Studio for S32 Platform as a standalone package. BR, VaneB
View full article
请提供 AMMCLIB 1.1.44S32DS插件与RTD 7.0.0兼容 您好,我在 S32 Design Studio 中安装 AMMCLIB 插件时遇到了版本依赖问题。 我正在与一位同事合作进行同一个项目,我们都在使用 RTD 版本 7.0.0 和 S32DS 版本 3.6 以上。我的同事安装了 AMMCLIB 1.1.44它运行正常;但是,在我的 S32DS 扩展和更新中,我只能找到 AMMCLIB 1.1.46。 安装 1.1.46 版本时,提示信息表明缺少以下依赖项: 缺少必需的依赖项: 找不到 com.nxp.RTD.S32K3_S32M27X 7.0.1。 缺少要求: com.nxp.AMMCLIB.S32K3xx.root.feature.feature.group 1.1.46.202609081018 需要 com.nxp.RTD.S32K3_S32M27X.feature.feature.group [7.0.1,99.99.99) 为了保持团队开发环境的一致性,我们希望继续使用 RTD 7.0.0 版本。+ AMMCLIB 1.1.44,通过RTD插件方法集成它们。 请协助确认: 1. 能否提供适用于 AMMCLIB 1.1.44 的 S32DS 插件的下载链接、历史更新站点或离线安装包?适用于 S32K3xx? 2. 此插件支持哪些具体的 S32DS 版本和更新?它与RTD 7.0.0兼容吗? 3.如果旧版本的官方下载已不再可用,是否有受支持的方法可以从同事已安装的 1.1.44 版本中获取并安装该插件?环境? 我们需要的是 S32DS 插件/更新站点软件包,以便使用 S32 配置工具添加 AMMCLIB 元器件并生成代码。 附件是显示安装失败的错误信息的屏幕截图。谢谢你! Re: Please provide the AMMCLIB 1.1.44 S32DS plugin compatible with RTD 7.0.0 你好@feixingren1 通过 S32DS 扩展和更新提供的 AMMCLib 软件包是 RTD 相关的,正如软件包名称所示。这意味着它设计用于特定的 RTD 版本,并且具有必须安装的软件依赖项。就您的情况而言,错误信息表明该软件包需要 RTD 7.0.1 版本。因此,除非您的 S32DS 安装中存在所需的 RTD 版本及其相关依赖项,否则无法完成安装。 既然您对 AMMCLib v1.1.44 特别感兴趣,无需安装通过 S32DS 扩展和更新提供的版本。或者,您可以直接从S32K3 汽车数学和电机控制库集下载所需版本的独立组网 (SA)软件包。 关于集成,NXP S32K3xx、MWCT2DxxS 和 MWCT20xxS 器件的汽车数学和电机控制库集用户手册包含一个专用的章节,解释了如何将该库作为独立软件包内置到 S32 平台的 S32 设计工作室中。 BR,VaneB
View full article
s32k396 基本セキュアブートに関する質問 32K396では、HSE FW 0.2.50.0 FULL_MEMが使用され、現在の有効期間はCUST_DELです。 テストプロセス:最初は、システムは正常に動作しました。次に、認証範囲内のアドレス 0x00453FF0 を 0xFF から 0xFE に変更し、AppBL ヘッダー、認証タグ、および IVT は変更しませんでした。IVT bootCfgWord を 0x00000009 に設定しました。電源をオフにしてから再度オンにした後、イメージをダウンロードせずに J-Link Attach 接続を使用し、空の SetupTarget を使用して接続中の RAM/ECC 初期化を無効にしました。この時点で、PC は 0x2040012E で停止しました。0x2040012C から 0x2040012E までの命令は WFI および WFI に戻る分岐であり、JTAG リカバリ待機ループと一致しています。現在、ユーザーのセキュアリカバリアプリケーションは構成されていません。 質問: BSB認証失敗後のこのバージョンの完全な処理プロセスと信頼できる基準を確認してください。JTAGリカバリ待機ループに入った後もGPR3ビット5が0のままなのはなぜですか?このビットは「SBAFブートアプリケーションカーネルがリカバリに入った」ことのみを示し、リカバリパスはHSE FWによってトリガーされることに関係していますか?また、どのステータスビットまたはエラーメッセージを使用して、失敗の原因がAppBL認証失敗であることを明確に確認する必要がありますか? Re: s32k396 Basic Secure Boot qeustion 詳細なテスト説明をありがとうございました。ここで重要なのは、ユーザーのSecure Recoveryアプリケーションが設定されていないということです。 あなたの設定でリカバリーフローがどのように機能するのか、詳しく教えていただけますか?特に: Secure Recoveryアプリケーションが設定されていない場合、AppBL認証失敗後にどのような復旧アクションが期待されますか? JTAGリカバリは明示的に設定され、有効化されていましたか? 観測されたWFIループ自体は予期せぬものとみなされるのか、それともGPR3[5]がクリアされたままであることだけが懸念事項なのか? J-Linkとの接続直後に読み取った、関連する復旧構成情報とHSE/SBAFステータス情報を提供してください。 ユーザーのSecure Recoveryアプリケーションが設定されていなければ、観察されるWFIループは予想されます。したがって、まずはAppBL認証失敗後の想定される回復フローとデバイスの動作を明確にしてください。 Re: s32k396 Basic Secure Boot qeustion gpr3のビット5が設定されていないことを確認しました。これはフラグビットであり、マニュアルにはリカバリモードでは1に設定されるべきと記載されています。なぜリカバリされなかったのでしょうか?詳細なテスト結果を添付します。
View full article
[S32K3] LVD割り込みについて こんにちは、 S32K3 MCUのLVD割り込み機能を使おうとしています。 MCUの設定でLVDIEEnable = trueに設定しています。 現在MCUには5Vが供給されていますが、Power_Ip_PMC_VoltageErrorIsr()は継続的にトリガーされています。 これは正常な動作なのか、それとも私が何か設定を間違えたのか教えていただきたいです。 Re: [S32K3] about LVD Interrupt こんにちは、 @danielmartynek 以下のピンに5Vの電圧が印加されています。 100ピンMCUの使用(FS32K312NHT0VPAST) VREFH: PIN 8 VDD_HV_A: ピン10 VDD_HV_A-2: ピン37 VDD_HV_A-3: ピン62 VDD_HV_A-4: ピン87 5Vが供給されているにもかかわらず、LVD5AFフラグレジスタが常にセットされたままになっている。 他に確認すべき箇所や記録簿はありますか? よろしくお願いいたします。 ショーン Re: [S32K3] about LVD Interrupt こんにちは、 @ssean さん。 LVD5AFをクリアした後も設定が維持される場合。 電圧は規定のしきい値よりも低くなければならない。 電圧を測定できますか? ありがとうございます ダニエル Re: [S32K3] about LVD Interrupt 部品番号を教えてもらえますか? あなたはどのRTD改訂版を使用していますか? ありがとうございました。 ダニエル Re: [S32K3] about LVD Interrupt こんにちは、 @danielmartynek さん。 現在、RTD 4.0.0を使用しています。HF04。 RTDコードにいくつかエラーがあることと、私の設定に問題があることを特定しました。 必要な調整を行った後、LVD電圧レベルで割り込みが正しくトリガーされることを確認しました。 再開まで今しばらくお待ちください。 よろしくお願いいたします。 ショーン・ソン
View full article
KEIL 与 LID2634 的兼容性 大家好, 我们正在采购LID2634板。 但是要刷写 NXP 固件,需要 KEIL MDK 5.36 许可证。(我是新手)。 经询问,KEIL 目前有 6 版本——但如果我想使用旧版本,我必须从他们那里购买专业许可证。 我的问题是: 1.是必须持有 KEIL 专业执照,还是必须持有 KEIL 5.36 证书?否则我应该选择基础版/社区版许可证吗? 2. 文件只提到了 KEIL 5.36 版本。购买前是否也应该确认一下编译器、调试器选项等兼容性问题? 3. 我看到大多数 CAS 示例都是用 Python 编写的——这是否意味着我只需要使用 KEIL 来烧录固件,而其余基于 Python 的逻辑都放在板载计算机中?如果我计划在NXP的MAC层之上进行开发。 4. 我还想知道是否有关于设置板、多标签和多锚点配置设置等的示例或 git 仓库可供参考,以便快速入门。 谢谢 Re: KEIL compatibility with LID2634 你好, 希望你一切都好。很抱歉给您带来不便,但由于该产品的信息受保密协议(NDA)约束,因此不对外公开。这不是分享该设备任何信息的安全渠道,出于同样的原因,我也没有相关数据。 因此,我建议您联系我们代理商网络|NXP中的一家代理商。或者,如果您有直接联系人曾帮助您了解该产品的信息或最初帮助您获得集成电路,请直接与他/她联系。 由此给您带来的不便,我深表歉意。 顺祝商祺! 里卡多
View full article
KW47:在调用 Gap_StartAdvertising 之前,是否必须等待 gAdvertisingStateChanged_c? 你好, 我正在 KW47 上实现广告控制。 要停止广告,我使用 Gap_StopAdvertising()。但是,有些情况下,在发出停止请求后,我希望在收到 gAdvertisingStateChanged_c 事件之前重新开始投放广告。 在这种情况下,当 Gap_StopAdvertising() 操作仍在进行时,调用 Gap_StartAdvertising() 是否安全? 具体来说,推荐使用以下哪种顺序? --- Gap_停止广告() ↓ 等待 gAdvertisingStateChanged_c ↓ Gap_StartAdvertising() ---- 或 --- Gap_停止广告() ↓ Gap_StartAdvertising() --- SDK 是否在内部处理状态转换,还是必须等待指示广告已停止的 gAdvertisingStateChanged_c 事件,然后才能调用 Gap_StartAdvertising()? 感谢您的支持。 顺祝商祺! 协议:蓝牙 Re: KW47: Is it necessary to wait for gAdvertisingStateChanged_c before calling Gap_StartAdvertising 你好@hyama , 能否提供更多关于您希望在收到 gAdvertisingStateChanged_c 事件之前重新启动广告的场景的背景信息? 建议的做法是等待 gAdvertisingStateChanged_c 事件,以验证广告状态转换是否已成功完成。Gap_StopAdvertising() 启动该过程,回调函数确认操作结果。例如,应用程序可能不会收到 gAdvertisingStateChanged_c 事件,而是收到 gAdvertisingCommandFailed_c 事件,这表明请求的操作无法完成。 BR 哈比卜 Re: KW47: Is it necessary to wait for gAdvertisingStateChanged_c before calling Gap_StartAdvertising 谢谢你的解释。 我们提出这个问题是因为我们预期 SDK 可能会在内部按顺序处理停止和启动请求,即使在收到 gAdvertisingStateChanged_c 事件之前调用了 Gap_StartAdvertising()。 由于等待 gAdvertisingStateChanged_c 事件是推荐的做法,我们将相应地修改我们的实现。 感谢您的支持。
View full article
s32k396 Basic Secure Boot qeustion On a 32K396, HSE FW 0.2.50.0 FULL_MEM is used, and the current lifetime is CUST_DEL. Testing Process: Initially, the system ran normally. Then, the address 0x00453FF0 within the authentication range was changed from 0xFF to 0xFE, while keeping the AppBL Header, authentication tag, and IVT unchanged. The IVT bootCfgWord was set to 0x00000009. After powering off and on again, a J-Link Attach connection was used, without downloading the image, and RAM/ECC initialization during connection was disabled using an empty SetupTarget. At this point, the PC stopped at 0x2040012E. The instructions from 0x2040012C to 0x2040012E are WFI and branches that jump back to WFI, consistent with the JTAG Recovery wait loop. Currently, no user Secure Recovery application is configured. Question: Please confirm the complete handling process and reliable criteria for this version after BSB authentication failure: Why is GPR3 bit5 still 0 even after entering the JTAG Recovery waiting loop? Is it related to the fact that this bit only indicates "SBAF boot application kernel into Recovery" and the current recovery path is triggered by HSE FW? And which status bit or error message should be used to clearly confirm that the failure is due to AppBL authentication failure? Re: s32k396 Basic Secure Boot qeustion Thank you for the detailed test description. The statement that no user Secure Recovery application is configured may be important here. Could you please clarify how the recovery flow is intended to work in your configuration? In particular: What recovery action is expected after the AppBL authentication failure if no Secure Recovery application is configured? Was JTAG Recovery explicitly configured and enabled? Is the observed WFI loop itself considered unexpected, or is the concern only that GPR3[5] remains cleared? Please provide the relevant recovery configuration and the HSE/SBAF status information read immediately after connecting with J-Link. The observed WFI loop may be expected if no user Secure Recovery application is configured. Therefore, please first clarify the intended recovery flow and the expected device behavior after the AppBL authentication failure. Re: s32k396 Basic Secure Boot qeustion We observed that bit 5 of gpr3 was not set. This is a flag bit, and the manual states that it should be set to 1 in recovery mode. Why didn't it recover? Detailed tests are attached.
View full article