On a 32K396, HSE FW 0.2.50.0 FULL_MEM is used, and the current lifetime is CUST_DEL.
Testing Process: Initially, the system ran normally. Then, the address 0x00453FF0 within the authentication range was changed from 0xFF to 0xFE, while keeping the AppBL Header, authentication tag, and IVT unchanged. The IVT bootCfgWord was set to 0x00000009. After powering off and on again, a J-Link Attach connection was used, without downloading the image, and RAM/ECC initialization during connection was disabled using an empty SetupTarget. At this point, the PC stopped at 0x2040012E. The instructions from 0x2040012C to 0x2040012E are WFI and branches that jump back to WFI, consistent with the JTAG Recovery wait loop. Currently, no user Secure Recovery application is configured.
Question: Please confirm the complete handling process and reliable criteria for this version after BSB authentication failure: Why is GPR3 bit5 still 0 even after entering the JTAG Recovery waiting loop? Is it related to the fact that this bit only indicates "SBAF boot application kernel into Recovery" and the current recovery path is triggered by HSE FW? And which status bit or error message should be used to clearly confirm that the failure is due to AppBL authentication failure?