Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
S32R41: How to Enable and Verify Cortex-M7 Lockstep Functionality Hello NXP Team, I am working with the NXP S32R41 automotive radar SoC and using Lauterbach TRACE32 for debugging. I would like to understand how to enable and verify the hardware lockstep functionality of the Cortex-M7 cores on the S32R41. Could you please help clarify the following questions? How to enable Lockstep: Is the Cortex-M7 lockstep mode enabled by default on the S32R41, or does it need to be configured? If configuration is required, what are the exact steps to enable it? Is it controlled by hardware configuration, DCF records, startup software, or specific registers? Configuration registers: Which S32R41-specific registers and bit fields indicate whether Lockstep is enabled? Please provide the register names, addresses, bit positions, and expected values. How to verify Lockstep: How can I confirm that the Cortex-M7 cores are actually operating in hardware lockstep mode rather than independent mode? Is checking the configuration register sufficient, or are additional status registers required? Lockstep error detection: Which registers indicate the status of the lockstep comparator? How can I determine whether the comparator is functioning correctly and whether any lockstep mismatch has been detected? TRACE32 debugging: Is there a recommended TRACE32 command sequence or debugging procedure to inspect the lockstep configuration and status? Documentation: Could you point me to the relevant sections of the S32R41 Reference Manual, Safety Manual, or other official documentation describing the lockstep configuration and verification procedure? I want to ensure that the lockstep functionality is correctly enabled and that its operation can be verified using documented, S32R41-specific methods. Please note that I am specifically asking about the S32R41, not the S32K3 family, so I would appreciate register definitions and procedures applicable to the S32R41. Thank you for your support. Best regards Re: S32R41: How to Enable and Verify Cortex-M7 Lockstep Functionality Hello, On the S32R41, the Cortex‑M7 processors are implemented as hardware lockstep core pairs. Lockstep operation is part of the S32R41 hardware configuration and is not enabled by application software, startup code, or an S32K3-style UTEST_MISC[LOCKSTEP_EN] DCF record. The NXP S32R41 product information explicitly describes the Cortex‑M7 implementation as having a lockstep core configuration. 1. No software enable sequence is required 2. The configuration should not be verified using S32K3 registers 3. Debugger visibility provides a practical architectural indication TRACE32 connects to the logical Cortex‑M7 processor. It does not present the redundant checker core as an additional independently debuggable Cortex‑M7. Therefore, only the functional member of each lockstep pair is expected to appear as a debug target. 4. Lockstep mismatch reporting A mismatch detected by the Cortex‑M7 lockstep comparison logic is reported through the S32R41 safety fault-management path. The application must configure the corresponding FCCU fault and its required reaction in accordance with the S32R41 Safety Manual. 5. No special TRACE32 command is required to enable lockstep. 6. Please refer to the following S32R41-specific documents: S32R41 Reference Manual, particularly the Cortex‑M7, FCCU and reset/fault-management chapters; S32R41 Safety Manual, particularly the safety mechanisms covering Cortex‑M7 lockstep execution, lockstep comparison and FCCU fault handling; the device-specific FCCU fault mapping associated with the applicable S32R41 revision; the TRACE32 S32R41 startup scripts supplied with the supported S32R41 software/debug package. Best regards, Peter
View full article
Can_43_LLCE 1.0.9 (S32G):是否支持或计划支持构建后可加载配置? 你好, 我们正在跟进“CAN_LLCE 和 LLCE_Af 是否支持 Postbuild Loadable?”这个问题。(2025年4月)NXP 支持人员回答了 Can_43_LLCE 的“Postbuild 模型”。可加载的问题仍未解决。CAN_LLCE 和 LLCE_Af 是否支持 Postbuild Loadable? - NXP 社区 设置:S32G274A,S32G_LLCE_1_0_9(Can_43_LLCE 1.0.9,RTD AUTOSAR 4.4)。 目标:更新 CAN 配置,使其可在版本后加载,而无需重新刷写整个应用程序映像。 在 1.0.9 版本软件包中,我们看到: 构建后表是带有绝对指针的常量结构,会被编译到应用程序映像中。 我们没有找到任何可加载或可重定位的格式、S 记录输出或构建后数据的加载器。 问题: Can_43_LLCE 是否支持/计划支持版本后可加载配置?如果是,是哪个版本?何时发布的? 如果不行,那么在不完全重新刷写固件的情况下,更新 CAN 滤波器的官方方法是什么? 是否有关于使用 Can_43_LLCE 和 Llce_Af 进行构建后处理的应用笔记? 提前致谢, 艾曼 Re: Can_43_LLCE 1.0.9 (S32G): is post-build loadable configuration supported or planned? 你好, AymanYounis 感谢您与我们联系并提供信息。 我已经收到您的问题,我会帮您核实。 BR 乔伊 Re: Can_43_LLCE 1.0.9 (S32G): is post-build loadable configuration supported or planned? 你好, AymanYounis 感谢您与我们联系。 根据最新的 LLCE 手册,目前 CAN_LLCE 和 LLCE_Af 不支持 Postbuild Loadable。目前还没有添加此功能的明确计划。 根据内部建议,如果客户想要提出新的变更请求,则需要咨询市场部。需要提供更多业务信息。 我们目前没有相关文件可供参考,引用。给您带来的不便,敬请谅解。 BR 乔伊
View full article
S32R41:如何启用和验证 Cortex-M7 锁步功能 您好,NXP团队, 我正在使用 NXP S32R41 汽车雷达 SoC,并使用 Lauterbach TRACE32 进行调试。 我想了解如何在 S32R41 上启用和验证 Cortex-M7 内核的硬件锁步功能。 请问您能否帮忙解答以下问题? 如何启用锁步模式: S32R41 是否默认启用 Cortex-M7 锁步模式,还是需要手动配置?如果需要配置,具体步骤是什么?它是通过硬件配置、DCF 记录、启动软件还是特定寄存器来控制的? 配置寄存器:哪些S32R41特有的寄存器和位域指示是否启用了锁步功能?请提供寄存器名称、地址、位位置和预期值。 如何验证硬件锁步模式:如何确认 Cortex-M7 内核确实运行在硬件锁步模式而不是独立模式下?检查配置寄存器是否足够,还是需要额外的状态寄存器? 锁步错误检测:哪些寄存器指示锁步比较器的状态?如何确定比较器是否正常工作以及是否检测到任何锁步不匹配? TRACE32 调试:是否有推荐的 TRACE32 命令序列或调试程序来检查锁步配置和状态? 文档:能否指出 S32R41 参考手册、功能安全手册或其他官方文档中描述锁定步骤配置和验证程序的相关章节? 我希望确保锁定步进功能已正确启用,并且可以使用已记录的、S32R41 特定方法验证其运行情况。 请注意,我特指S32R41 ,而不是 S32K3 系列,因此我希望得到适用于 S32R41 的寄存器定义和程序。 感谢您的支持。 顺祝商祺! Re: S32R41: How to Enable and Verify Cortex-M7 Lockstep Functionality 你好, 在 S32R41 上,Cortex-M7 处理器以硬件锁步内核对的形式实现。锁步操作是 S32R41 硬件配置的一部分,并非通过应用程序软件、启动代码或 S32K3 风格的 UTEST_MISC[LOCKSTEP_EN] DCF 记录启用。NXP S32R41 产品信息明确描述了 Cortex-M7 实现采用锁步内核配置。 1.无需软件启用序列 2. 不应使用 S32K3 寄存器验证配置。 3. 调试器可见性提供了实际的架构指示 TRACE32 连接到逻辑 Cortex-M7 处理器。它没有将冗余的检查器核心作为额外的、可独立调试的 Cortex-M7 呈现出来。因此,只有每个锁步对的功能成员才会作为调试目标出现。 4. 锁步不匹配报告 Cortex-M7 锁步比较逻辑检测到的不匹配将通过 S32R41 功能安全故障管理路径报告。应用程序必须按照 S32R41 功能安全手册配置相应的 FCCU 故障及其所需的响应。 5. 无需特殊的 TRACE32 命令即可启用锁步。 6. 请参阅以下与 S32R41 相关的文档: S32R41 参考手册,特别是 Cortex-M7、FCCU 和复位/故障管理章节; S32R41 功能安全手册,特别是涵盖 Cortex-M7 锁步执行、锁步比较和 FCCU 故障处理的安全机制; 与适用的 S32R41 版本相关的设备特定 FCCU 故障映射; TRACE32 S32R41 启动脚本随受支持的 S32R41 软件/调试软件包一起提供。 顺祝商祺! Peter
View full article
Can_43_LLCE 1.0.9 (S32G): is post-build loadable configuration supported or planned? Hello, We are following up on "Do CAN_LLCE and LLCE_Af support Postbuild Loadable?" (April 2025). NXP support answered "Postbuild model" for Can_43_LLCE. The loadable question was left open. Do CAN_LLCE and LLCE_Af support Postbuild Loadable? - NXP Community Setup: S32G274A, S32G_LLCE_1_0_9 (Can_43_LLCE 1.0.9, RTD AUTOSAR 4.4). Goal: update CAN config as post-build loadable without reflashing the full application image. In the 1.0.9 package, we see: Post-build tables are const structures with absolute pointers, compiled into the application image. We found no loadable or relocatable format, S-record output, or loader for post-build data. Questions: Is post-build loadable configuration supported/planned for Can_43_LLCE? If yes, which version and when? If not, what is the supported way to update CAN filters without a full reflash? Is there an application note for post-build with Can_43_LLCE and Llce_Af? Thanks in advance, Ayman Re: Can_43_LLCE 1.0.9 (S32G): is post-build loadable configuration supported or planned? Hi,AymanYounis Thank you for contacting us and your information. I have received your question and will help you to check it. BR Joey Re: Can_43_LLCE 1.0.9 (S32G): is post-build loadable configuration supported or planned? Hi,AymanYounis Thank you for contacting us. According to the latest LLCE manual, currently CAN_LLCE and LLCE_Af do not support Postbuild Loadable. There are no definite plans to add this feature. According to internal suggestions, if a customer wants to propose a new change request, this requires consulting the marketing. More business information needs to be provided. We currently do not have relevant documents for reference. Apologize for the inconvenience caused. BR Joey
View full article
KW47: Gap_StartAdvertisingを呼び出す前に、gAdvertisingStateChanged_cを待つ必要がありますか? こんにちは、 KW47に広告制御機能を実装しています。 広告表示を停止するには、Gap_StopAdvertising() を使用します。しかし、停止リクエストを出した後にgAdvertisingStateChanged_cイベントを受け取る前に再び広告を始めたい場合もあります。 この状況において、Gap_StopAdvertising() 操作がまだ進行中である間に Gap_StartAdvertising() を呼び出すのは安全でしょうか? 具体的に、以下のどの手順が推奨されますか? --- Gap_StopAdvertising() ↓ gAdvertisingStateChanged_c を待機します ↓ Gap_StartAdvertising() ---- または --- Gap_StopAdvertising() ↓ Gap_StartAdvertising() --- SDKsは内部で状態遷移を処理しているのか、それとも広告が停止したことを示すgAdvertisingStateChanged_cイベント情報を待ってからGap_StartAdvertising()を呼び出す必要があるのか? 再開まで今しばらくお待ちください。 よろしくお願いいたします。 プロトコル:Bluetooth Re: KW47: Is it necessary to wait for gAdvertisingStateChanged_c before calling Gap_StartAdvertising こんにちは、 @hyama さん。 gAdvertisingStateChanged_cイベントを受け取る前に広告を再開したい場合の状況について、もう少し詳しく教えていただけますか? 推奨される方法は、広告状態の移行が成功裏に完了したことを確認するためにgAdvertisingStateChanged_cイベントを待つことです。Gap_StopAdvertising() は処理を開始し、コールバックは処理結果を確認します。例えば、gAdvertisingStateChanged_cイベントを受け取る代わりに、アプリケーションはリクエストされた操作が完了できないことを示すgAdvertisingCommandFailed_cイベントを受け取ることがあります。 BR ハビブ Re: KW47: Is it necessary to wait for gAdvertisingStateChanged_c before calling Gap_StartAdvertising ご説明いただきありがとうございます。 この質問をしたのは、たとえGap_StartAdvertising()がgAdvertisingStateChanged_cイベント情報を受け取る前に呼び出されていても、SDKsが内部で停止・開始リクエストを順番に処理する可能性があると予想していたからです。 gAdvertisingStateChanged_cイベントを待つことが推奨されているため、それに応じて実装を修正します。 再開まで今しばらくお待ちください。
View full article
Recommended BSP / Neutron SDK versioning strategy Hello, We are developing a PoC for an automotive application using the i.MX95 as our platform and would like to clarify the recommended Neutron SDK versioning strategy. We have read the "Neutron SDK Version Compatibility with Yocto BSP" table in NeutronSDKUserGuide.md and understand that the compiler and runtime must come from the same SDK. However, the guide does not say which version is recommended. Should we always use the latest Neutron SDK version (with the runtime upgraded) on our current BSP, or should we use the SDK version that is Default for that BSP? Environment - Board: IMX95LPD5EVK-19 - BSP: LF_6.18.20_2.0.0 - Neutron SDK: eiq-neutron-sdk-linux-3.2.3 - NeutronFirmware.elf, libNeutronDriver.so, and libneutron_delegate.so have been updated to the versions from Neutron SDK 3.2.3. Thank you! Re: Recommended BSP / Neutron SDK versioning strategy Hi, Thank you for your interest in NXP Semiconductor products, You can find what Neutron SDK version is included with every BSP at the end of Machine Learning User's Guide, e.g. Neutron SDK v3.2.1 is included in LF6.18.37_2.1.0 However, for development, customers are encouraged to use latest SDK revision, and documentation advises copying the binaries (used for conversion) to target: - Updating the Neutron Runtime - To update the neutron runtime on a target device, upload the files to the ir designated directories, as follows: | File | Target Directory | |------|------------------| | `NeutronFirmware.elf` | `/lib/firmware/` | | `libNeutronDriver.so` | `/lib/` | | `libneutron_delegate.so` | `/lib/` | Regards Re: Recommended BSP / Neutron SDK versioning strategy Hi Joseph, Thank you for your reply. We will use the latest SDK revision as recommended. Regards
View full article
Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project Hi Team, We are using S32 Design Studio 3.6.10 for the development of a Non-AUTOSAR application on the NXP S32K312 Mini Board. The project is currently based on FreeRTOS, using SW32K3_FreeRTOS_11.1.0_0.8.0_CD1_D2603_DesignStudio_updatesite.zip, which in turn uses SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip as the RTD version. We have successfully implemented the following UDS services: Service 0x10 – Diagnostic Session Control Service 0x22 – Read Data By Identifier Service 0x27 – Security Access Service 0x3E – Tester Present As part of the next development phase, we plan to implement UDS Service 0x29 (Authentication) and would like to leverage HSE/Crypto support for the implementation. To enable this, we installed: SW32K3_RTD_R23-11_7.0.1_P02_D2603_DesignStudio_updatesite.zip The installation completed successfully, and we can see Crypto-related folders (e.g., Crypto_43_HSE, CryIf, Csm, etc.) under the RTD installation directory. However, we are unable to find any HSE/Crypto components in: S32 Configuration Tools (.mex) Peripherals/Drivers view Sample Applications/Examples To verify the setup, we also created a new S32K312 sample project. However, the HSE/Crypto components are still not available for selection. Could you please help clarify the following: How can HSE/Crypto support be enabled for an S32K312 project in S32 Design Studio? Are any additional packages, plugins, SDKs, or HSE firmware required? Is there a specific RTD version or project configuration recommended for using HSE/Crypto together with FreeRTOS on the S32K312? Are the Crypto_43_HSE modules provided by the package intended only for AUTOSAR/EB Tresos-based projects, or can they also be used in Non-AUTOSAR S32 Design Studio projects? Are there any example projects or reference documents available for integrating HSE/Crypto in a Non-AUTOSAR S32K312 application? Any guidance or reference documentation related to HSE/Crypto integration would be greatly appreciated. Thanks & Regards, Pramod Jadhav Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project Hi @pramodj2  In the thread S32DS 3.6.7 RTD 7.0.1 P02 HSE code generation error, I shared a step-by-step guide describing how I installed S32K3 Real-Time Drivers ASR R23-11 Version 7.0.1 P02. You may find it helpful to compare those steps with your current installation process. Also, when working with HSE, it is necessary to include the HSE Interface files in your project. These files can be obtained from the HSE Firmware package, specifically from the interface folder (C:\NXP\HSE_FW_S32K344_0_2_55_0\hse_full_mem\interface). Finally, although there are no RTD examples specifically developed for the S32K312, the examples available for other S32K3 devices can be used as a good reference, as the implementation is very similar across the family. You may also find the examples included in the HSE Demo App and the S32K3 MCUs for General Purpose HSE Demo Examples helpful. While these examples do not directly use the Crypto/Hse_Ip drivers, they demonstrate how to work with HSE services. BR, VaneB Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project Hi @pramodj2  The HSE-B Reference Manual, training presentations, and application notes are under NDA and are therefore not publicly available. Access to these materials is provided only through Secure Files. If you do not currently have access to Secure Files, you can request it by following the procedure described in the NXP Secure Access Rights First-Time User Registration Guide. Additionally, the HSE Service API Reference Manual, which contains detailed information on how to install, configure, and use HSE, is included in the SE Interface files. It can be found, for example, at the following location: C:\NXP\HSE_FW_S32K344_0_2_55_0\docs If you plan to use the Hse_Ip/Crypto drivers, we also recommend referring to the Driver User Manual and Integration Manual. These documents provide detailed information about hardware and software requirements, supported configurations, usage guidelines, integration steps, and known limitations. These documents can be found, for example, at: C:\NXP\S32DS.3.6.5\S32DS\software\PlatformSDK_S32K3\RTD_CRYPTO\Crypto_43_HSE_TS_T40D34M70I1R0\doc Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project Thank you for the quick support. I was able to successfully add the HSE driver by following the steps provided in the shared link. Could you please share any reference user manuals, application notes, or documentation that we can use to configure the HSE in the application and validate its functionality on the target board? Thank you for your assistance.
View full article
为在 S32K312 非 AUTOSAR 项目中启用 HSE/加密支持所需指南 大家好, 我们使用的是S32 设计工作室 3.6.10 版本。用于在NXP S32K312 Mini 板上开发非 AUTOSAR 应用程序。该项目目前基于FreeRTOS ,使用SW32K3_FreeRTOS_11.1.0_0.8.0_CD1_D2603_DesignStudio_updatesite.zip ,而SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zip作为 RTD 版本。 我们已成功实施以下UDS服务: 服务 0x10 – 诊断会话控制 服务 0x22 – 通过标识符读取数据 服务 0x27 – 网络安全访问 服务 0x3E – 测试人员已就绪 作为下一开发阶段的一部分,我们计划实现UDS 服务 0x29(身份验证) ,并希望利用HSE/Crypto支持来实现该服务。 为了实现这一点,我们安装了: SW32K3_RTD_R23-11_7.0.1_P02_D2603_DesignStudio_updatesite.zip 安装已成功完成,我们可以在 RTD 安装目录下看到与加密相关的文件夹(例如Crypto_43_HSE 、 CryIf 、 Csm等)。但是,我们无法在以下位置找到任何HSE/Crypto 元器件: S32 配置工具(.mex) 外设/驱动程序视图 应用示例/范例 为了验证设置,我们还创建了一个新的 S32K312 示例项目。然而,HSE/Crypto 元器件目前仍无法选择。 请问您能否帮忙澄清以下问题: 如何在 S32 Design Studio 中为 S32K312 项目启用 HSE/加密支持? 是否需要其他软件包、插件、SDK 或 HSE 固件? 在 S32K312 上使用 HSE/Crypto 和 FreeRTOS 时,是否有推荐的特定 RTD 版本或项目配置? 该软件包提供的Crypto_43_HSE模块是否仅用于基于 AUTOSAR/EB Tresos 的项目,还是也可以用于非 AUTOSAR S32 Design Studio 项目? 是否有任何示例项目或参考文档可用于将 HSE/Crypto 集成到非 AUTOSAR S32K312 应用程序中? 任何与 HSE/Crypto 集成相关的指导或参考资料都将不胜感激。 谢谢,此致敬礼! 普拉莫德·贾达夫 Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project 嗨@pramodj2 在S32DS 3.6.7 RTD 7.0.1 P02 HSE 代码生成错误主题中,我分享了一个分步指南,描述了我是如何安装 S32K3 实时驱动程序 ASR R23-11 版本 7.0.1 P02 的。您可以将这些步骤与您当前的安装过程进行比较,这可能会对您有所帮助。 另外,在使用 HSE 时,必须将 HSE 接口文件包含在您的项目中。这些文件可以从 HSE 固件代码包,软件包中获取,具体来说,可以从接口文件夹(C:\NXP\HSE_FW_S32K344_0_2_55_0\hse_full_mem\interface)中获取。 最后,虽然没有专门为 S32K312 开发的 RTD 示例,但其他 S32K3 设备的示例可以作为很好的参考,引用,因为该系列器件的实现方式非常相似。 您可能还会发现 HSE Demo App 中包含的示例和S32K3 MCU 通用 HSE Demo 示例很有帮助。虽然这些示例没有直接使用 Crypto/Hse_Ip 驱动程序,但它们演示了如何使用 HSE 服务。 BR,VaneB Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project 嗨@pramodj2 HSE-B 参考手册、培训演示文稿和应用笔记均受保密协议约束,因此不对外公开。只有通过安全文件才能访问这些资料。 如果您目前没有访问安全文件的权限,您可以按照NXP 安全访问权限首次用户注册指南中描述的步骤提出申请。 此外,SE 接口文件中还包含 HSE 服务 API 参考手册,其中包含有关如何安装、配置和使用 HSE 的详细信息。例如,可以在以下地点找到它: C:\NXP\HSE_FW_S32K344_0_2_55_0\docs 如果您计划使用 Hse_Ip/Crypto 驱动程序,我们也建议您参考驱动程序用户手册和集成手册。这些文档提供了有关硬件和软件要求、支持的配置、使用指南、集成步骤和已知限制的详细信息。例如,您可以在以下位置找到这些文件: C:\NXP\S32DS.3.6.5\S32DS\software\PlatformSDK_S32K3\RTD_CRYPTO\Crypto_43_HSE_TS_T40D34M70I1R0\doc Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project 感谢您的快速支持。我按照分享链接中提供的步骤,成功添加了 HSE 驱动程序。 能否提供一些参考用户手册、应用笔记或文档,以便我们在应用程序中配置 HSE 并验证其在目标板上的功能? 谢谢你的帮助。
View full article
PF09 文档 我正在寻找演示板 KITPF09FRDMEVB 的电路原理图。 我下载了 KITPF09FRDMEVB-DESIGN-FILES,但是 .DSN 文件已损坏。 请问您能否告诉我哪里可以找到电路图文件(PDF格式也行)? 先行致谢。 Re: PF09 documentation 谢谢! Re: PF09 documentation 你好, 请尝试使用 Allegro Capture CIS 打开 DSN 文件。我打开它没有任何问题。 如果您无法使用 捕获 CIS,请提交支持工单以获取进一步帮助。很遗憾,我无法通过这个渠道分享设计文件。 同时,请查阅附件中的PDF文件。
View full article
PF09 documentation Im looking for the electric schematics of the demo board KITPF09FRDMEVB. I downloaded KITPF09FRDMEVB-DESIGN-FILES but the .DSN file is corrupted. Please could tou tell me where can i find the electric schmatics files (also in PDF) Thanks in advance. Re: PF09 documentation THank you. Re: PF09 documentation Hello, Please try opening the DSN file using Allegro Capture CIS. I was able to open it without any issues. If you are unable to use Capture CIS, please open a support ticket for further assistance. Unfortunately, I cannot share the design files through this channel. In the meantime, please find the PDF file attached for your reference.
View full article
PF09のドキュメント デモボードKITPF09FRDMEVBの電気回路図を探しています。 KITPF09FRDMEVB-DESIGN-FILESをダウンロードしましたが、DSNファイルが破損しています。 エレクトリック・シュマティクスのファイル(PDFも含む)がどこで見つかるか教えていただけませんか? よろしくお願いいたします。 Re: PF09 documentation よろしくお願いします。 Re: PF09 documentation こんにちは、 Allegro Capture CISを使用してDSNファイルを開いてみてください。問題なく開けることができました。 Capture CISをご利用できない場合は、 サポートチケット を開設してさらなるサポートを依頼してください。残念ながら、このチャネルを通じてデザインファイルを共有することはできません。 参考資料として、添付のPDFファイルをご確認ください。
View full article
CLRD730と701の互換性 こんにちは、 私たちのお客様には多くのCLRD 701が導入されています。彼らはもっと買いたいと思っている。コードを変更せずに730でアプリケーションを動かす可能性はどんなものでしょうか? どうもありがとうございました。よろしくお願いいたします。 Re: CLRD730 compatibility with 701 こんにちは、@fox13 さん。 お元気でお過ごしでしょうか。 NXP製品を引き続きご利用いただきありがとうございます。 ご質問についてですが、CLRD730をアプリケーションに組み合わせることは可能なはずです。 Pegoda CLRD730デスクトップリーダーは、デフォルトのWindows CCIDドライバーで動作するよう設計されていることをご考慮ください。また 、 CLRD730データシート のセクション6.8「 PC/SCモード」 のご確認もお勧めします 統合に関する関連情報をカバーしています。 敬具 ジェイミー。
View full article
非AUTOSARプロジェクトでHSE/暗号資産サポートを有効にするためのガイダンスS32K312必要 チームの皆さん、こんにちは。 私たちはS32 Design Studio 3.6.10を使っていますNXP S32K312 Mini Board上で非AUTOSARアプリケーションの開発のために。このプロジェクトは現在、 FreeRTOSをベースとしており、 SW32K3_FreeRTOS_11.1.0_0.8.0_CD1_D2603_DesignStudio_updatesite.zipを使用しています。この FreeRTOS は、RTD バージョンとしてSW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite.zipを使用しています。 以下のUDSサービスを正常に実装しました。 サービス0x10 – 診断セッション制御 サービス0x22 – 識別子によるデータ読み取り サービス0x27 – セキュリティアクセス サービス0x3E – テスター存在 次の開発段階では、 UDSサービス0x29(認証) を実装する予定で、 HSE/暗号 サポートを活用して実装したいと考えています。 これを実現するために、以下をインストールしました。 SW32K3_RTD_R23-11_7.0.1_P02_D2603_DesignStudio_updatesite.zip インストールは無事完了し、RTDのインストールディレクトリの下にはCrypto関連のフォルダ(例: Crypto_43_HSE、 CryIf、 CSMなど)が確認できます。しかし、以下の場所にはHSE/Cryptoコンポーネントが見つかりません。 S32設定ツール(.mexファイル) ペリフェラル/ドライバビュー アプリケーション・例 設定を確認するため、S32K312用の新しいサンプルプロジェクトも作成しました。しかし、HSE/Cryptoコンポーネントはまだ選択できません。 以下の点を教えていただけますか? S32 Design StudioでS32K312プロジェクトに対してHSE/Cryptoのサポートを有効にするにはどうすればよいですか? 追加のパッケージ、プラグイン、SDKs、HSEファームウェアは必要ですか? S32K312上でFreeRTOSとHSE/Cryptoを併用する場合、推奨される特定のRTDバージョンやプロジェクト構成はありますか? パッケージに含まれる Crypto_43_HSE モジュールはAUTOSAR/EB Tresosベースのプロジェクト専用ですか?それともAUTOSAR以外のS32 Design Studioプロジェクトでも使用可能ですか? 非AUTOSAR S32K312アプリケーションでHSE/暗号資産を統合するための例となるプロジェクトや参考文献はありますか? HSE/暗号資産統合に関する指針や参考ドキュメントがあれば、ぜひ教えていただけると助かります。 よろしくお願いいたします。 プラモド・ジャダブ Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project こんにちは、@pramodj2さん In the ThreadS32DS 3.6.7 RTD 7.0.1 P02 HSEコード生成エラー」では、S32K3 リアルタイム・ドライバ ASR R23-11 バージョン7.0.1 P02のインストール方法を説明するステップバイステップガイドを共有しました。これらの手順を現在のインストール手順と比較してみると、参考になるかもしれません。 また、HSEを扱う際には、プロジェクトにHSEインターフェースファイルを含める必要があります。これらのファイルはHSEファームウェアパッケージから入手可能で、特にインターフェースフォルダ(C:\NXP\HSE_FW_S32K344_0_2_55_0\hse_full_mem\interface)から入手可能です。 最後に、S32K312向けに特別に開発されたRTDの例はありませんが、他のS32K3デバイスの例はファミリ全体で非常に似た実装であるため、良い参考資料として利用できます。 HSEデモアプリに含まれているサンプルや、汎用HSEデモサンプル用のS32K3 MCUのサンプルも参考になるかもしれません。これらの例はCrypto/Hse_Ipドライバを直接使用していませんが、HSEサービスの扱い方を示しています。 BR、VaneB Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project こんにちは、@pramodj2さん HSE-Bリファレンス・マニュアル、トレーニング発表、アプリケーションノートはNDAに属するため、公開されていません。これらの資料へのアクセスはSecure Filesを通じてのみ提供されます。 現在Secure Filesにアクセスできない場合は、 NXPのSecure アクセス Rights First Time ユーザー Registration Guideに記載された手順に従って申請できます。 さらに、HSEサービスのAPIリファレンス・マニュアルには、HSEのインストール、設定、使用方法に関する詳細な情報がSEインターフェースファイルに含まれています。例えば、以下の場所で見つけることができます。 C:\NXP\HSE_FW_S32K344_0_2_55_0\docs Hse_Ip/Cryptoドライバーを使用する予定がある場合は、ドライバーユーザーマニュアルおよび統合マニュアルも参照することをお勧めします。これらの文書は、ハードウェアおよびソフトウェアの要件、対応構成、使用ガイドライン、統合ステップ、既知の制限事項に関する詳細な情報を提供します。これらの文書は、例えば以下で見つけることができます: C:\NXP\S32DS.3.6.5\S32DS\software\PlatformSDK_S32K3\RTD_CRYPTO\Crypto_43_HSE_TS_T40D34M70I1R0\doc Re: Guidance Required for Enabling HSE/Crypto Support on S32K312 Non-AUTOSAR Project 迅速なサポートありがとうございます。共有リンクの手順に従ってHSEドライバを無事に追加できました。 HSEをアプリケーション内で設定し、ターゲットボード上でその機能を検証するための参考ユーザーマニュアル、アプリケーションノート、ドキュメントなどを教えていただけますか? ご協力ありがとうございました。
View full article
Title: RW612 Flash Programming Verification Failed at 0x08400000 on Murata Type 2FR EVK Hello NXP Community, I am using the Murata Type 2FR (LBES0ZZ2FR-EVK) based on the NXP RW612 MCU and need help resolving a flash programming issue. Initially, I followed the Murata Type 2FR Wi-Fi CLI project and its documentation. I successfully built and flashed the Wi-Fi CLI application and connected the device to a Wi-Fi network. After that, I tried the Wi-Fi MQTT example, which also worked successfully on the same board. However, after some time, I suddenly became unable to program new firmware into the device. Problem description I have tried flashing different firmware binaries at their respective addresses: Application firmware: 0x08000000 Wi-Fi firmware: 0x08400000 Bluetooth firmware: 0x08540000 I also tried reflashing the previously working Wi-Fi CLI and Wi-Fi MQTT projects, but the problem persists. I can connect to the RW612 using SEGGER J-Link over SWD, and I can read the existing flash contents. However, programming fails during flash verification. The issue occurs with different firmware images and is not limited to one project or address. I came across the NXP Community article titled “How to solve flashing problems in FRDM-RW612 (flash lock)” and tried to follow the suggested recovery approach using MCUXpresso Secure Provisioning Tool. However, I have not been able to resolve the problem. I also tried the ROM ISP recovery approach using USB and UART, but neither method worked successfully. When using the USB approach, blhost -- list-memory reports: Specified USB HID device not found: 0x1FC9, 0x0020 The device is visible in Windows Device Manager as a USB serial port (COM16), but the provisioning tool does not detect the expected USB HID device. Current J-Link error I am using J-Link Commander V8.44 with the RW612 target selected. The debugger successfully connects to the Cortex-M33 over SWD, and the target voltage is approximately 3.3 V. When programming the Wi-Fi firmware binary rw61x_sb_wifi_a2.bin at 0x08400000, I receive the following error: J-Link>loadfile "...\\rw61x_sb_wifi_a2.bin" 0x8400000 Downloading file [...] J-Link: Flash download: Bank 0 @ 0x08000000: 1 range affected (589824 bytes) J-Link: Flash download: Total: 4.538s J-Link: Flash download: Program speed: 249 KB/s ****** Error: Verification failed @ address 0x08400000 Error while programming flash: Verify failed. Unable to perform operation! Command failed with exit code 1 The same general problem occurs when I try programming the application firmware and other previously working binaries. What I need help with Could this be caused by a flash write lock, security configuration, flash protection, or an incorrect flash programming algorithm? Is there a reliable procedure to recover or unlock the RW612 flash on the Murata Type 2FR EVK using MCUXpresso Secure Provisioning Tool? Can the FRDM-RW612 flash recovery procedure be safely applied to the Murata Type 2FR EVK? Are there any board-specific differences in entering ROM ISP mode? Since the debugger can connect and read flash contents, but programming fails verification, what should I check next? Is there a way to restore flash programming access without damaging the existing board configuration or permanently disabling debug access? I would appreciate a step-by-step recovery procedure, particularly for the MCUXpresso Secure Provisioning Tool and ROM ISP method. The board was previously working correctly with both the Wi-Fi CLI and Wi-Fi MQTT examples. The problem appeared later, without any intentional change to the hardware. Thank you for your help. Re: Title: RW612 Flash Programming Verification Failed at 0x08400000 on Murata Type 2FR EVK Hello @sakshee, hope you are doing well. I will address your questions below: > Could this be caused by a flash write lock, security configuration, flash protection, or an incorrect flash programming algorithm? The flash locking occurs when an application is written to the flash with an invalid flash configuration block (FCB), for example, when the application was built considering a different external flash device. In the case of the Murata Type 2FR it contains a different flash from the FRDM-RW612, hence, a different FCB is required for each board. Could you please confirm if an application build for the FRDM-RW612 was built and flashed to the 2FR EVK? > Is there a reliable procedure to recover or unlock the RW612 flash on the Murata Type 2FR EVK using MCUXpresso Secure Provisioning Tool? If the previous case happened and the flash was locked, the reliable way to unlock it is as stated in the mentioned post: How to solve flashing problems in FRDM-RW612 (flash lock), however, this guide focuses on unlocking the FRDM-RW612. In order to apply this guide to the Murata's flash, I'd recommend following the general steps below (referencing both the Secure Provisioning Tool and the post itself): Set the board to ISP mode. Open the workspace, and select the RD-RW612-BGA option, as well as the "rdrw612bga_gpio_led_output_extfls.s19" source executable image. Configure the UART interface. Once in the main workspace menu, make sure the flash configurations match with the EVK's flash configurations in the Boot Memory Configuration window (please see the image below) Follow the rest of the guide as-is. > Can the FRDM-RW612 flash recovery procedure be safely applied to the Murata Type 2FR EVK? Are there any board-specific differences in entering ROM ISP mode? No, both boards have different flash memories each, therefore you must consider the steps shared in the previous answer. Also, I'd recommend checking the migration guide for RW612 development boards as it provides specific considerations regarding this same topic and application customization. > Since the debugger can connect and read flash contents, but programming fails verification, what should I check next? Please first check the mentioned procedure and information and let me know your findings. > Is there a way to restore flash programming access without damaging the existing board configuration or permanently disabling debug access? The shared procedure should not generate any damage to your board configuration, nor the debug access ports. Please let me know if this helps.
View full article
推荐的 电路板支持包。/Neutron SDK 版本控制策略 你好, 我们正在使用 i.MX95 作为平台开发汽车应用的 PoC,并希望澄清推荐的 Neutron SDK 版本策略。 我们已经阅读了 NeutronSDKUserGuide.md 中的“Neutron SDK 版本与 Yocto 电路板支持包的兼容性”表格,并了解到编译器和运行时必须来自同一个 SDK。但是,该指南并未说明推荐哪个版本。 我们应该始终在当前的 电路板支持包。 上使用最新的 Neutron SDK 版本(运行时已升级),还是应该使用该 电路板支持包。 的默认 SDK 版本? 环境 - 板:IMX95LPD5EVK-19 - 电路板支持包:LF_6.18.20_2.0.0 - Neutron SDK:eiq-neutron-sdk-linux-3.2.3 - NeutronFirmware.elf、libNeutronDriver.so 和 libneutron_delegate.so 已更新至 Neutron SDK 3.2.3 的版本。 谢谢! Re: Recommended BSP / Neutron SDK versioning strategy 您好, 感谢您对恩智浦半导体产品的关注, 您可以在《机器学习用户指南》的末尾找到每个电路板支持包所包含的 Neutron SDK 版本,例如:Neutron SDK v3.2.1 包含在 LF6.18.37_2.1.0 中。 但是,对于开发工作,我们鼓励客户使用最新的 SDK 版本,并且文档建议将二进制文件(用于转换)复制到目标位置: - 更新 Neutron 运行时 - 要更新目标设备上的中子运行时间,请将文件上传到 其指定目录如下: 文件 | 目标目录 | |------|------------------| | `NeutronFirmware.elf`| `/lib/firmware/` | | `libNeutronDriver.so`| `/lib/` | | `libneutron_delegate.so` | `/lib/` | 此致 Re: Recommended BSP / Neutron SDK versioning strategy 嗨,约瑟夫, 感谢你的回复。我们将按照建议使用最新的SDK版本。 问候
View full article
标题:Murata Type 2FR EVK 上的 RW612 闪存编程验证失败,错误地址为 0x08400000 NXP社区的各位朋友,大家好! 我正在使用基于 NXP RW612 MCU 的 Murata Type 2FR (LBES0ZZ2FR-EVK) ,需要帮助解决闪存编程问题。 最初,我参考了 Murata Type 2FR Wi-Fi CLI 项目及其文档。我已成功构建并刷写了 Wi-Fi CLI 应用程序,并将设备连接到了 Wi-Fi 网络。之后,我尝试了 Wi-Fi MQTT 示例,该示例在同一块板上也成功运行。 然而,过了一段时间后,我突然无法将新的固件编程到设备中。 问题描述 我已尝试将不同的固件二进制文件刷入到各自的地址: 应用程序固件: 0x08000000 Wi-Fi固件版本: 0x08400000 蓝牙固件版本: 0x08540000 我还尝试重新刷写之前运行正常的 Wi-Fi CLI 和 Wi-Fi MQTT 项目,但问题仍然存在。 我可以通过 SEGGER J-Link 经由 SWD 连接到 RW612,并且可以读取现有的闪存内容。然而,在闪存验证过程中编程失败。该问题在不同的固件镜像中都会出现,并且不局限于某个项目或地址。 我偶然看到NXP社区一篇题为“如何解决FRDM-RW612的烧录问题(闪存锁定)”的文章,并尝试使用MCUXpresso安全配置工具按照建议的方法进行恢复。然而,我仍然无法解决问题。 我还尝试了使用 USB 和 UART 进行 ROM ISP 恢复的方法,但两种方法都失败了。使用 USB 方法时, blhost -- list-memory命令报告: 未找到指定的 USB HID 设备:0x1FC9、0x0020 该设备在 Windows 设备管理器中显示为 USB 串行端口 (COM16),但配置工具无法检测到预期的 USB HID 设备。 当前 J-Link 错误 我正在使用 J-Link Commander V8.44,并选择了 RW612 目标。调试器通过 SWD 成功连接到 Cortex-M33,目标电压约为 3.3 V。 当对地址为0x08400000 的Wi-Fi 固件二进制文件rw61x_sb_wifi_a2.bin进行编程时,出现以下错误: J-Link>loadfile "...\\rw61x_sb_wifi_a2.bin" 0x8400000 Downloading file [...] J-Link: Flash download: Bank 0 @ 0x08000000: 1 range affected (589824 bytes) J-Link: Flash download: Total: 4.538s J-Link: Flash download: Program speed: 249 KB/s ****** Error: Verification failed @ address 0x08400000 Error while programming flash: Verify failed. Unable to perform operation! Command failed with exit code 1 当我尝试对应用程序固件和其他以前可以正常运行的二进制文件进行编程时,都会出现同样的问题。 我需要哪些方面的帮助? 这可能是由于闪存写入锁定、网络安全配置、闪存保护或错误的闪存编程算法造成的吗? 使用 MCUXpresso Secure Provisioning Tool 是否有可靠的方法来恢复或解锁 Murata Type 2FR EVK 上的 RW612 闪存? FRDM-RW612 的闪存恢复程序可以安全地应用于 Murata Type 2FR EVK 吗?进入 ROM ISP 模式时,不同板之间是否存在板级差异? 既然调试器可以连接并读取闪存内容,但编程验证失败,接下来我应该检查什么? 有没有办法在不损坏现有板配置或永久禁用调试访问的情况下恢复闪存编程访问权限? 我希望能够获得详细的恢复步骤说明,特别是针对 MCUXpresso 安全配置工具和 ROM ISP 方法的说明。 该板之前使用 Wi-Fi CLI 和 Wi-Fi MQTT 示例都能正常工作。问题出现于之后,并非人为对硬件进行任何改动。 感谢您的帮助。 Re: Title: RW612 Flash Programming Verification Failed at 0x08400000 on Murata Type 2FR EVK 你好@sakshee ,希望你一切都好。 下面我将回答您的问题: 这可能是由于闪存写入锁定、网络安全配置、闪存保护或错误的闪存编程算法引起的吗? 当应用程序使用无效的闪存配置块 (FCB) 写入闪存时,就会发生闪存锁定,例如,当应用程序在构建时考虑了不同的外部闪存设备。以 Murata Type 2FR 为例,它包含与 FRDM-RW612 不同的闪存,因此每块板都需要不同的 FCB。请问是否已构建 FRDM-RW612 的应用程序版本并将其刷写到 2FR EVK 中? > 是否有可靠的方法可以使用 MCUXpresso Secure Provisioning Tool 恢复或解锁 Murata Type 2FR EVK 上的 RW612 闪存? 如果发生了上述情况并且闪存被锁定,则可靠的解锁方法如上述帖子中所述:如何解决 FRDM-RW612 的刷机问题(闪存锁定) ,但是,本指南重点介绍如何解锁 FRDM-RW612。为了将本指南应用于 Murata 的闪存,我建议按照以下一般步骤操作(参考安全配置工具和本文本身): 将板设置为ISP模式。 打开工作区,选择 RD-RW612-BGA 选项,以及“rdrw612bga_gpio_led_output_extfls.s19”;源可执行映像。 配置UART接口。 进入主工作区菜单后,请确保闪存配置与 EVK 的启动内存配置窗口中的闪存配置相匹配(请参见下图)。 请按指南其余部分的步骤操作。 > FRDM-RW612 的闪存恢复程序可以安全地应用于 Murata Type 2FR EVK 吗?进入 ROM ISP 模式时,不同板之间是否存在差异? 不,两块板的闪存各不相同,因此您必须考虑上一个答案中提到的步骤。另外,我建议您查看RW612 开发板的迁移指南,因为它提供了有关此主题和应用程序定制的具体注意事项。 既然调试器可以连接并读取闪存内容,但编程验证失败,接下来我应该检查什么? 请先核对上述步骤和信息,并将您的核对结果告知我。 > 是否有办法在不损坏现有板配置或永久禁用调试访问的情况下恢复闪存编程访问权限? 共享程序不应对您的电路板配置或调试访问端口造成任何损坏。 请告诉我这是否有帮助。
View full article
タイトル: RW612 フラッシュプログラミング検証が、Murata Type 2FR EVK の 0x08400000 で失敗しました こんにちは、NXPコミュニティの皆さん、 私はNXP RW612 MCUをベースにしたMurata Type 2FR(LBES0ZZ2FR-EVK)を使っており、フラッシュプログラミングの問題を解決する助けが必要です。 最初は村田Type 2FR Wi-Fi CLIプロジェクトとそのドキュメントをフォローしていました。Wi-Fi CLIアプリケーションを無事に構築・フラッシュし、デバイスをWi-Fiネットワークに接続しました。その後、Wi-Fi MQTTのサンプルを試してみたところ、同じボード上で正常に動作しました。 しかし、しばらくすると、突然、デバイスに新しいファームウェアを書き込むことができなくなってしまった。 問題の説明 それぞれのファームウェアバイナリを、対応するアドレスに書き込んでみました。 アプリケーションファームウェア:0x08000000 Wi-Fiファームウェア: 0x08400000 Bluetoothファームウェア: 0x08540000 以前正常に動作していたWi-Fi CLIとWi-Fi MQTTプロジェクトを再フラッシュしてみましたが、問題は解決しませんでした。 SEGGER J-Linkを使ってSWD経由でRW612に接続でき、既存のフラッシュの内容も読み取れます。しかし、フラッシュ検証中にプログラミングが失敗する。この問題は様々なファームウェアイメージで発生し、特定のプロジェクトやアドレスに限定されるものではありません。 NXPコミュニティの「FRDM-RW612(フラッシュロック)のフラッシュ問題の解決方法」という記事を見つけ、MCUXpresso Secure Provisioning Toolを使って提案された回復方法を試しました。しかし、問題を解決できていません。 USBとUARTを使ったROM ISP復旧方法も試しましたが、どちらもうまくいきませんでした。USB方法を使うと、 blhost -- list-memory の報告: 指定されたUSB HIDデバイスが見つかりません: 0x1FC9、0x0020 デバイスはWindowsデバイスマネージャーでUSBシリアルポート(COM16)として表示されますが、プロビジョニングツールは期待されるUSB HIDデバイスを検出しません。 現在のJ-Linkエラー 私はRW612ターゲットを選択したJ-Link Commander V8.44を使用しています。デバッガはSWD経由でCortex-M33に接続し、目標電圧は約3.3Vです。 Wi-Fiファームウェアバイナリrw61x_sb_wifi_a2.binをアドレス0x08400000に書き込む際に、以下のエラーが発生します。 J-Link>loadfile "...\\rw61x_sb_wifi_a2.bin" 0x8400000 Downloading file [...] J-Link: Flash download: Bank 0 @ 0x08000000: 1 range affected (589824 bytes) J-Link: Flash download: Total: 4.538s J-Link: Flash download: Program speed: 249 KB/s ****** Error: Verification failed @ address 0x08400000 Error while programming flash: Verify failed. Unable to perform operation! Command failed with exit code 1 同じような一般的な問題は、アプリケーションのファームウェアや以前は動作していたバイナリをプログラムしようとすると発生します。 私が助けを必要としているのは これはフラッシュ書き込みロック、セキュリティ設定、フラッシュ保護、あるいは誤ったフラッシュプログラミングアルゴリズムが原因かもしれません。 MCUXpresso Secure Provisioning Toolを使用して、Murata Type 2FR EVKのRW612フラッシュを復元またはロック解除するための信頼できる手順はありますか? FRDM-RW612フラッシュリカバリー手順は村田タイプ2FR EVKに安全に適用できますか?ROM ISPモードに入る際、基板固有の違いはありますか? デバッガは接続してフラッシュの内容を読み取れるのに、プログラムが検証に失敗するので、次に何を確認すればいいのでしょうか? 既存のボード構成を壊さず、デバッグアクセスを永久に無効化せずにフラッシュプログラミングアクセスを復元する方法はありますか? 特にMCUXpressoセキュアプロビジョニングツールとROM ISP方法について、段階的な復旧手順を教えていただけるとありがたいです。 以前は、このボードはWi-Fi CLIとWi-Fi MQTTの両方のサンプルで正常に動作していました。問題は後になって発生したが、ハードウェアに意図的な変更は一切加えていない。 ご協力ありがとうございます。 Re: Title: RW612 Flash Programming Verification Failed at 0x08400000 on Murata Type 2FR EVK こんにちは、 @sakshee さん。お元気でお過ごしでしょうか。 ご質問にお答えします。 > これはフラッシュ書き込みロック、セキュリティ設定、フラッシュ保護、または誤ったフラッシュプログラミングアルゴリズムによって引き起こされる可能性はありますか? フラッシュロックは、アプリケーションが無効なフラッシュ構成ブロック(FCB)でフラッシュに書き込みられた場合、例えば異なる外部フラッシュデバイスを想定してアプリケーションが構築された場合に発生します。村田タイプ2FRの場合はFRDM-RW612とは異なるフラッシュを搭載しているため、各基板ごとに異なるFCBが必要です。FRDM-RW612のアプリケーションビルドが2FR EVKにビルドされ、フラッシュされたかどうか確認していただけますか? MCUXpresso Secure Provisioning Toolを使用して、Murata Type 2FR EVKのRW612フラッシュを復元またはロック解除するための信頼できる手順はありますか? 前述のケースでフラッシュがロックされている場合、信頼できる解除方法は前述の投稿「 FRDM-RW612(フラッシュロック)でのフラッシュ問題の解決方法」ですが、このガイドではFRDM-RW612の解除に焦点を当てています。このガイドを村田製作所製フラッシュメモリに適用するには、以下の一般的な手順に従うことをお勧めします(セキュアプロビジョニングツールとこの記事の両方を参照してください)。 ボードをISPモードに設定してください。 ワークスペースを開き、RD-RW612-BGAオプションと「rdrw612bga_gpio_led_output_extfls.s19」を選択します。ソース実行可能イメージ。 UARTインターフェースの設定をしてください。 メインワークスペースメニューに入ったら、ブートメモリ構成ウィンドウで、フラッシュ構成がEVKのフラッシュ構成と一致していることを確認してください(下の画像を参照)。 残りの手順はガイドの指示通りに行ってください。 >FRDM-RW612フラッシュリカバリー手順は村田タイプ2FR EVKに安全に適用できますか?ROM ISPモードに入る際に基板固有の違いはありますか? いいえ、両方のボードはそれぞれ異なるフラッシュメモリーを持っているので、前の回答で説明した手順を考慮する必要があります。また、 RW612開発ボードの移行ガイド も確認することをお勧めします。同じトピックやアプリケーションのカスタマイズに関する具体的な注意点が記載されています。 > デバッガは接続してフラッシュの内容を読み取れるのに、プログラミングが検証に失敗するので、次に何を確認すればいいでしょうか? まず、記載されている手順と情報をご確認いただき、その結果をお知らせください。 > 既存の基板構成を損傷したり、デバッグアクセスを永久に無効にしたりせずに、フラッシュプログラミングへのアクセスを復元する方法はありますか? 共有手順はボード構成やデバッグアクセスポートにダメージを与えることはありません。 これが役に立つかどうか教えてください。
View full article
CLRD730 compatibility with 701 Hello, We have a customer with many CLRD 701 deployed. They would like to buy more. What is the chance to have their application working with the 730 without modifying the code ?  Thanks a lot and best regards. Re: CLRD730 compatibility with 701 Hello @fox13 , Hope you are doing great. Thank you for continuing to choose NXP products. Regarding your question, it should be possible to use the CLRD730 with your application. Please consider that the Pegoda CLRD730 desktop reader is designed to work with the default Windows CCID driver.  We also encourage you to review Section 6.8 "PC/SC mode" of the CLRD730 datasheet, which covers relevant information for your integration. Best Regards, Jaime.
View full article
推奨されるBSP / Neutron SDKのバージョン管理戦略 こんにちは、 私たちはi.MX95をプラットフォームとして用いる自動車アプリケーション向けのPoCを開発しており、推奨されるNeutron SDKのバージョン管理戦略について明確にしたいと思います。 NeutronSDKUserGuide.md 年の「Neutron SDK Version Compatibility with Yocto BSP」の表を読み、コンパイラとランタイムは同じSDKから来なければならないと理解しています。しかし、ガイドにはどのバージョンが推奨されているかは明記されていない。 現在のBSPでは常に最新のNeutron SDKバージョン(ランタイムがアップグレードされたもの)を使うべきでしょうか、それともそのBSPのデフォルトバージョンを使うべきでしょうか? 環境 - ボード:IMX95LPD5EVK-19 - BSP:LF_6.18.20_2.0.0 - Neutron SDK: eiq-neutron-sdk-linux-3.2.3 - NeutronFirmware.elf、libNeutronDriver.so、libneutron_delegate.soはNeutron SDK 3.2.3のバージョンに更新されています。 ご回答をお待ちしています。 Re: Recommended BSP / Neutron SDK versioning strategy こんにちは、 NXP Semiconductors製品にご関心いただきありがとうございます。 機械 学習ユーザーガイドの最後に、すべてのBSPに含まれるNeutron SDKバージョンを確認できます。Neutron SDK v3.2.1はLF6.18.37_2.1.0に含まれています。 しかし、開発に関しては、お客様に最新のSDKリビジョンを使用することが推奨されており、ドキュメントには変換に使われるバイナリをコピーして以下を対象にすることが推奨されています: - Neutron ランタイムの更新 - ターゲットデバイスでNeutronランタイムを更新するには、ファイルを IRは以下の通りにディレクトリを指定しています: | ファイル | 対象ディレクトリ | |------|------------------| | `NeutronFirmware.elf`|'/lib/firmware/' | |「libNeutronDriver.so」|'/lib/' | |『libneutron_delegate.so』 |『/lib/』 | よろしくお願いします。 Re: Recommended BSP / Neutron SDK versioning strategy こんにちは、ジョセフさん。 お返事ありがとうございます。推奨される最新のSDKリビジョンを使用します。 よろしくお願いいたします
View full article
CLRD730 与 701 的兼容性 你好, 我们有一位客户部署了许多 CLRD 701。他们还想买更多。不修改代码,他们的应用程序与730兼容的可能性有多大? 非常感谢,并致以最诚挚的问候。 Re: CLRD730 compatibility with 701 你好@fox13 , 希望你一切都好。 感谢您一直以来选择恩智浦产品。 关于您的问题,CLRD730 应该可以与您的应用程序一起使用。 请注意,Pegoda CLRD730 桌面读卡器设计用于默认的 Windows CCID 驱动程序。我们还建议您查阅 CLRD730 数据手册 的 6.8 节“ PC/SC 模式” ,其中包含与您的集成相关的必要信息。 此致, 杰米。
View full article