Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
NXP MCUXpresso 入门指南 嘿,各位!我是一名软件工程师。我想用我的 K66F 评估板来亲自动手试试——这比他们的旗舰产品 K64F 要好一些。我一直想从头开始真正了解嵌入式系统——所以我买了一个 P&E Microlink 探针,然后就开始了。我成功地让一个 SDK 示例连接到了我本科电子工程专业时留下的 SPI TFT 模块。它有一个电阻式触摸屏——虽然示例中使用的是相邻的 SPI 电容式触摸传感器,但我认为几个板载 ADC 和一个简单的分压电路应该就能完成这项工作。只需要将读取电容设备 x 和 y 读数的回调函数替换为与 adc 类似的回调函数即可。可惜的是,这些示例似乎并不是为了扩展而设计的。添加其他元器件导致了一些新生成的包含错误,我已解决这些错误,但由于某种原因,最终还是出现了内存分配问题。虽然我取得了一些进展,但我认为现在可能是四处询问资源的好时机https://100001.onl/ 。 Re: Getting started with NXP's MCUXpresso 你好@louis22 , 感谢您的详细描述。听起来您在 FRDM-K66F 和 SPI TFT 显示屏方面已经取得了不错的进展。 你利用ADC通道读取电阻式触摸屏的方法很有道理。SDK 示例还可以用作起点,并可通过添加其他驱动程序和应用程序代码进行扩展。SDK 可在此处找到:选择开发板 | MCUXpresso SDK 构建器。 关于内存分配问题,我首先想了解具体的错误信息,然后再断定它是由 SDK 示例引起的。FRDM-K66F 上的 MK66FN2M0 设备具有 2 MB Flash 和 256 KB SRAM,因此通常只需添加 ADC 驱动程序就不会占用大量内存。 请问您能否提供以下信息? 你最初是从哪个 SDK 示例开始的? 您使用的是哪个版本的MCUXpresso IDE和SDK? 添加 ADC 功能后,具体的版本/链接器错误是什么? 如果可能,请提供失败版本的内存使用信息或链接器映射文件。 这将有助于我们确定问题是与 Flash/RAM 使用情况、堆或栈分配、链接器配置还是添加的元器件有关。 为了学习外设,我还建议查看 MCUXpresso SDK 中包含的驱动程序示例。就你的情况而言,ADC 示例是独立初始化和读取 K66 ADC 的良好参考。然后,您只需将所需的 ADC 初始化和读取功能集成到 TFT 应用程序中即可。 期待你的答复。 BR 塞莱斯特
View full article
build SE-PLUG-TRUST-MW-ADDON-TPM SE05x on IMX8MQEVK Hi everyone, I need to use the "Create Primary Key with TPM2 Create Primary" feature. I have tested it with the TPM on my PC using the following command: tpm2_createprimary -C o -G rsa -c primary.ctx The result returned as expected: name-alg: value: sha256 raw: 0xb attributes: value: fixedtpm|fixedparent|sensitivedataorigin|userwithauth|restricted|decrypt raw: 0x30072 type: value: ecc raw: 0x23 curve-id: value: NIST p256 raw: 0x3 kdfa-alg: value: null raw: 0x10 kdfa-halg: value: (null) raw: 0x0 scheme: value: null raw: 0x10 scheme-halg: value: (null) raw: 0x0 sym-alg: value: aes raw: 0x6 sym-mode: value: cfb raw: 0x43 sym-keybits: 128 x: 502d66098d74aa06ebf10736a6f2b2db435dcaa0a7afc6a1b43302d6e7f25cc5 y: e07d40eb7bd7a454f9b0aff1643c120c5396e230a0396e9e60a42872f96e48cc When I tried this feature on the I.MX8 Kit connected to the SE050 Kit, using the following command: ./tpm2_tool_createprimary -C o -G rsa -c primary.ctx /dev/i2c-1:0x48 I received the following message: root@imx8mqevk:~/customer/tpm2/bin/imx# ./tpm2_tool_createprimary -C o -G rsa -c primary.ctx /dev/i2c-1:0x48 App :INFO :Running ./tpm2_tool_createprimary App :INFO :Using PortName='/dev/i2c-1:0x48' (CLI) App :INFO :PlugAndTrust_v04.07.00_20250210 sss :INFO :atr (Len=35) 01 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 00 01 00 00 00 00 64 13 88 0A 00 65 53 45 30 35 31 00 00 00 sss :WARN :Communication channel is Plain. sss :WARN :!!!Not recommended for production use.!!! ERROR: Esys_CreatePrimary(0x70002) - (null) ERROR: Unable to run ./tpm2_tool_createprimary App :INFO :ex_sss Finished Additionally, I noticed that in the tpm2-tools.cmake file of the SE-PLUG-TRUST-MW-ADDON-TPM, some tools were commented out: # TPM2TOOL(create) # TPM2TOOL(createprimary) TPM2TOOL(encryptdecrypt) TPM2TOOL(getcap) TPM2TOOL(getrandom) TPM2TOOL(hash) TPM2TOOL(hmac) # TPM2TOOL(load) TPM2TOOL(pcrallocate) TPM2TOOL(pcrevent) TPM2TOOL(pcrextend) TPM2TOOL(pcrread) TPM2TOOL(pcrreset) TPM2TOOL(rsadecrypt) TPM2TOOL(rsaencrypt) TPM2TOOL(sign) TPM2TOOL(stirrandom) TPM2TOOL(verifysignature) I have uncommented them, rebuilt the project, and got the results as described above. I am not sure whether the SE050 supports the "Create Primary Key with TPM2 Create Primary" feature, or if it does, what is the correct way to perform this operation? Please support me. Thank you!   i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlus Linux Security Re: build SE-PLUG-TRUST-MW-ADDON-TPM SE05x on IMX8MQEVK Hi, What I mean is that I connected the SE05x and the i.MX8 as shown in the figure below, and I am trying to implement the TPM feature supported by the SE05x. Please guide me if anyone has previously worked on the TPM functionality with the SE05x.   Re: build SE-PLUG-TRUST-MW-ADDON-TPM SE05x on IMX8MQEVK Hello, We don;t have any S05 connected to MX8M but your problem look more like i2C, however please check the S05 documentation page: https://www-nxp-com.translate.goog/products/SE050?_x_tr_sl=en&_x_tr_tl=es&_x_tr_hl=es&_x_tr_pto=tc#documentation Regards Re: build SE-PLUG-TRUST-MW-ADDON-TPM SE05x on IMX8MQEVK Hello, Have you managed to solve the issue?  For now I`m evaluating some TPM platforms. What is the download link for the TPM add on : Plug&Trust_TPM_addon_20200903.zip The one referenced in https://www.nxp.com/docs/en/application-note/AN12663.pdf. Can you share the link or the add-on archive. Thanks
View full article
PN5190 NFC读取器库 v07.13.00:如果命令没有收到中断请求 (IRQ),则发现循环将无限期挂起。 软件包: NXP NFC读取器库 v07.13.00 (NfcrdlibEx1_DiscoveryLoop, PN5190, Linux OSAL)。版本说明 RN00009。 运行发现循环示例时,phacDiscLoop_Run(POLL) 有时永远不会返回。该进程持续运行。这种情况会在没有刷卡的情况下发生,而且没有固定的周期。 phhalHw_Pn5190_WaitIrq() 会等待除 EXCHANGE_RF_DATA 之外的每条指令,并等待 PHOSAL_MAX_DELAY。在这种情况下,命令是 READ_REGISTER (0x04),并且 IRQ 引脚从未变为高电平,因此 phOsal_EventPend() 不会返回。中止路径 phhalHw_Pn5190_Wait_IrqAbortHandling() 的等待方式相同。 这种无限等待是故意的吗?应用程序应该如何在不重启电源的情况下恢复 PN5190? 我添加了许多来自演示示例的日志,并将 WaitIrq 的超时时间从无限缩短到 10 秒。 关于如何处理这件事,大家有什么建议吗? 附件是示例程序的日志。 Re: PN5190 NFC Reader Library v07.13.00: discovery loop hangs forever if a command gets no IRQ 补充信息:PN5190 版本 信息:芯片 ID:0x00,硬件:v83,ROM:v3,固件:v770 Re: PN5190 NFC Reader Library v07.13.00: discovery loop hangs forever if a command gets no IRQ 您能否尝试一下最新版本的NFC读取器库? NFC读取器库 | 恩智浦半导体 Re: PN5190 NFC Reader Library v07.13.00: discovery loop hangs forever if a command gets no IRQ 嗨,吉米, 我们将使用最新的 NFC读取器库 (07.18.00) 进行重新测试,并报告是否可以重现同样的故障。 我们还发现了主机端的问题。在 i.MX93 上,PN5190 位于 LPSPI5 上。当 SPI 输出焊盘处于快速转换速率和驱动强度 X6 (0x3fe) 时,发现循环轮询失败。phacDiscLoop_Run 返回 PHAC_DISCLOOP_FAILURE (0x0080),我们将其记录为“轮询模式失败”。 降低 i.MX93 输出边沿的速度可以消除这种故障。目前稳定的鼠标垫设置如下: LPSPI5_SCK:0x02(慢速转换,驱动 X1) LPSPI5_SOUT:0x02(慢速转换,驱动 X1) SPI 片选:0x02(慢速转换,驱动 X1) LPSPI5_SIN:保留在 0x3fe,因为此引脚为输入引脚 PN5190 IRQ GPIO:未更改 由于 SCK、SOUT 和芯片选择边沿速度较慢,轮询得以继续,我们不再看到“轮询模式故障”。快速边沿敲击到 PN5190 时钟引脚。我们将于 07.18.00 再次确认此事。 如果((DiscLoopStatus & PH_ERR_MASK) == PHAC_DISCLOOP_FAILURE)
View full article
Getting started with NXP's MCUXpresso Hey folks! Software engineer here. I thought I'd get my hands dirty using my K66F evaluation board - which is a bit of an upgrade from their flagship K64F. I've wanted to really understand embedded systems from the ground up for some time - so I picked up a P&E Microlink probe and got started. I've managed to get an SDK example to connect to a SPI TFT module I have leftover from my EE undergrad days. It has a resistive touchscreen - and while the example was set up for an adjacent SPI capacitive touch sensor, I thought a couple of onboard ADCs and a humble voltage division circuit should get the job done. Just needed to replace the callbacks which read in the cap device's x and y readings with similar callbacks to the adc's Unfortunately, it seems the examples were not really made to be expanded. Adding additional components caused some newly generated include errors which I resolved, but for some reason still wound up with memory allocation issues. So while I've made some progress, I thought it might be a good time to ask around for resources https://100001.onl/ . Re: Getting started with NXP's MCUXpresso Hello @louis22 , Thanks for the detailed description. It sounds like you have already made good progress with the FRDM-K66F and the SPI TFT display. Your approach of using the ADC channels to read a resistive touchscreen makes sense. The SDK examples can also be used as a starting point and extended with additional drivers and application code. SDK can be found here: Select Board | MCUXpresso SDK Builder. For the memory allocation issue, I would first like to understand the exact error before concluding that it is caused by the SDK example. The MK66FN2M0 device on the FRDM-K66F has 2 MB Flash and 256 KB SRAM, so simply adding the ADC driver should not normally consume a large amount of memory. Could you please share the following information? Which SDK example did you start from? Which MCUXpresso IDE and SDK versions are you using? The exact build/linker error after adding the ADC functionality. If possible, the memory usage information or linker map file from the failed build. This will help us determine whether the problem is related to Flash/RAM usage, heap or stack allocation, the linker configuration, or an added software component. For learning the peripherals, I also recommend looking at the driver examples included with the MCUXpresso SDK. In your case, the ADC examples are a good reference for initializing and reading the K66 ADC independently. You can then integrate only the required ADC initialization and read functions into your TFT application. Looking forward to your reply. BR Celeste
View full article
IMX8MQEVK で SE-PLUG-TRUST-MW-ADDON-TPM SE05x をビルドする こんにちは、皆さん 「TPM2 Create Primary でプライマリキーを作成する」機能を使用する必要があります。次のコマンドを使用して、PC 上の TPM でテストしました。 tpm2_createprimary -C o -G rsa -c primary.ctx 予想通りの結果が返されました: 名前代名詞: 値: sha256 生: 0xb 属性: 値: fixedtpm|fixedparent|sensitivedataorigin|userwithauth|restricted|decrypt 生データ: 0x30072 タイプ: 値: ecc 生データ: 0x23 曲線ID: 値: NIST p256 生データ: 0x3 kdfa-alg: 値: null 生データ: 0x10 kdfa-halg: 値: (null) 生データ: 0x0 スキーム: 値: null 生データ: 0x10 スキームhalg: 値: (null) 生データ: 0x0 対称代数: 値: aes 生データ: 0x6 sym-mode: 値: cfb 生データ: 0x43 sym-keybits: 128 ×: 502d66098d74aa06ebf10736a6f2b2db435dcaa0a7afc6a1b43302d6e7f25cc5 y: e07d40eb7bd7a454f9b0aff1643c120c5396e230a0396e9e60a42872f96e48cc 次のコマンドを使用して、SE050 キットにコネクテッドされた I.MX8 キットでこの機能を試してみました。 ./tpm2_tool_createprimary -C o -G rsa -c primary.ctx /dev/i2c-1:0x48 次のメッセージを受け取りました: root@imx8mqevk:~/customer/tpm2/bin/imx# ./tpm2_tool_createprimary -C o -G rsa -c primary.ctx /dev/i2c-1:0x48 アプリ:INFO:./tpm2_tool_createprimaryを実行中 アプリ:INFO:PortName='/dev/i2c-1:0x48' を使用 (CLI) アプリ:情報:PlugAndTrust_v04.07.00_20250210 sss :INFO :atr (長さ=35) 01 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 00 01 00 00 00 00 64 13 88 0A 00 65 53 45 30 35 31 00 00 00 sss :警告:通信チャネルはプレーンです。 sss :警告:!!!本番環境での使用は推奨されません。!!! エラー: Esys_CreatePrimary(0x70002) - (null) エラー: ./tpm2_tool_createprimary を実行できません アプリ:INFO:ex_sss 終了 さらに、SE-PLUG-TRUST-MW-ADDON-TPM の tpm2-tools.cmake ファイルで、いくつかのツールがコメント アウトされていることに気付きました。 # TPM2TOOL(作成) # TPM2TOOL(プライマリを作成) TPM2TOOL(暗号化/復号化) TPM2TOOL(取得キャップ) TPM2TOOL(ランダム値を取得) TPM2TOOL(ハッシュ) TPM2TOOL(hmac) # TPM2TOOL(ロード) TPM2TOOL(pcrallocate) TPM2TOOL(pcrevent) TPM2TOOL(pcrextend) TPM2TOOL(pcrread) TPM2TOOL(pcrリセット) TPM2TOOL(rsadecrypt) TPM2TOOL(rsaencrypt) TPM2TOOL(サイン) TPM2TOOL(ランダム攪拌) TPM2TOOL(署名検証) コメントを解除し、プロジェクトを再構築して、上記のような結果が得られました。 SE050 が「TPM2 Create Primary によるプライマリキーの作成」機能をサポートしているかどうかわかりません。また、サポートしている場合は、この操作を実行する正しい方法は何ですか? 応援して下さい。ありがとう!   i.MX 8ファミリ | i.MX 8QuadMax (8QM) | 8QuadPlus Linux Security Re: build SE-PLUG-TRUST-MW-ADDON-TPM SE05x on IMX8MQEVK こんにちは、 つまり、下の図のように SE05x と i.MX8 をコネクテッドし、SE05x でサポートされている TPM 機能を実装しようとしているのです。以前に SE05x で TPM 機能に取り組んだことがある方がいらっしゃいましたら、ご指導ください。   Re: build SE-PLUG-TRUST-MW-ADDON-TPM SE05x on IMX8MQEVK こんにちは、 MX8M に S05 はコネクテッドされていませんが、問題は i2C のように見えます。ただし、S05 のドキュメント ページを確認してください。 https://www-nxp-com.translate.goog/products/SE050?_x_tr_sl=en&_x_tr_tl=es&_x_tr_hl=es&_x_tr_pto=tc#ドキュメント よろしくお願いします。 Re: build SE-PLUG-TRUST-MW-ADDON-TPM SE05x on IMX8MQEVK こんにちは、 問題は解決しましたか?今はTPMプラットフォームをいくつか評価しています。 TPMアドオンのダウンロードリンクは何ですか?:Plug&Trust_TPM_addon_20200903.zip https://www.nxp.com/docs/en/application-note/AN12663.pdfで参照されているものです。 リンクやアドオンアーカイブを共有できますか? よろしくお願いします。
View full article
imx7ulp A7はIOMUXC0(LPUART0~3およびI2C)上のパッドを設定します。 こんにちは、 私たちはカスタムのimx7ulp(MCIMX7U3)ボードで作業している学生です。Linux(A7)で8台すべてのLPUARTと一部のI2C回線を制御したいと考えています。 LPUART4~7はIOMUXC1(A7ドメイン)を使用しており、当社のDTSでは正常に動作しています。しかし、LPUART0~3と当社のI2CラインはIOMUXC0 (M4ドメイン)のパッドを使用しています。 LinuxのpinctrlドライバとU-Bootのソースを見ると、IOMUXC1がA7のデフォルトで、U-Bootは特定の IOMUX_CONFIG_MPORTSフラグを使ってIOMUXC0に触れているようです。リファレンス・マニュアルにはIOMUXCが「所有権ゲート」と書かれています。 IOMUXC0のピン設定手順で詰まっています。 私たちの質問: A7がLinuxから直接IOMUXC0パッドを設定できるサポート方法(DTSノードまたはドライバーフラグを通じて)はありますか? もしそうでなければ、M4ファームウェアの標準的なフローは起動時にこれらのピンを多番に処理し、その後A7がUART/I2Cコントローラを引き継ぐ形になっているのでしょうか? 障害は周辺プロトコルではなくパッドコントローラーなので、I2C回線もUARTsと同じ制限を受けていると考えてよいでしょうか? この件に関する標準的なアプローチについてご教示いただければ大変ありがたいです。 追加情報:私たちはWrynrose Yoctoリリースを基にNXP BSPを使ってLinuxをビルディングしています
View full article
imx7ulp A7 configure pads on IOMUXC0 (LPUART0–3 and I2C) Hello, We are students working on a custom imx7ulp (MCIMX7U3) board. We want Linux (A7) to control all 8 LPUARTs, plus some I2C lines. LPUART4–7 use IOMUXC1 (A7 domain) and are working fine in our DTS. However, LPUART0–3 and our I2C lines use pads in IOMUXC0 (M4 domain). Looking at the Linux pinctrl driver and U-Boot source, it seems IOMUXC1 is the default for A7, and U-Boot uses a specific IOMUX_CONFIG_MPORTS flag to touch IOMUXC0. The reference manual also mentions IOMUXC is "ownership-gated." We are stuck on the pin configuration step for IOMUXC0. Our questions: Is there a supported way (via DTS node or driver flag) for the A7 to configure IOMUXC0 pads directly from Linux? If not, is the standard intended flow for the M4 firmware to mux these pins during boot, and then the A7 just takes over the UART/I2C controllers? Since the obstacle is the pad controller (not the peripheral protocol), can we assume the I2C lines face the exact same restriction as the UARTs? Any guidance on the standard approach for this would be greatly appreciated. Extra info: We're building our linux on the Wrynrose Yocto release using the NXP BSP 
View full article
MCAL 需要源代码以进行代码生成。 您好,NXP技术支持, MCAL 版本:SW32K3_S32M27x_RTD_4.4_4.0.0_P24 当我重命名以下 .h 文件时如果文件格式为 .hh,ADC 生成将会失败。 为什么在代码生成过程中需要生成的源代码? 我问这个问题是因为我的工作场所没有本地源代码策略,我只能在本地电脑上安装 ARXML 等非源代码配置。 BR/熊本熊 Re: MCAL expects source code for code generation 嗨@kumamon 配置生成不一定仅基于 ARXML。在生成过程中,MCAL 配置工具还需要作为已安装的 RTD/MCAL 软件包的一部分提供的文件,包括包含生成器所需的定义或信息的头文件。 因此,如果其中一个预期的 .h 文件存在,则如果文件重命名为 .hh,生成器可能无法再找到或处理该依赖项,这可能会导致代码生成失败。 BR,VaneB Re: MCAL expects source code for code generation 你好@VaneB , 谢谢你的回答。 现在很清楚了。 BR/熊本熊
View full article
MCAL expects source code for code generation Hello NXP Support, MCAL Version: SW32K3_S32M27x_RTD_4.4_4.0.0_P24 When I rename the following .h file to .hh, the ADC generation will fail. Why is generated source code needed during code generation? I asked because there is no local source policy in my working place, I can only put non-source code configuration like ARXML in local PC. BR/Kumamon Re: MCAL expects source code for code generation Hi @kumamon  The configuration generation is not necessarily based only on the ARXML. During the generation process, the MCAL configuration tool also require files provided as part of the installed RTD/MCAL package, including header files containing definitions or information required by the generator. Therefore, if one of the expected .h files is renamed to .hh, the generator may no longer be able to locate or process that dependency, which can cause the code generation to fail. BR, VaneB Re: MCAL expects source code for code generation Hello @VaneB , Thanks for your answer. It is clear now. BR/Kumamon
View full article
MCALはコード生成のためにソースコードを必要とします。 こんにちは、NXPサポートの皆さん、 MCALバージョン: SW32K3_S32M27x_RTD_4.4_4.0.0_P24 以下の.hファイルの名前を変更するとファイルを.hhに変換すると、ADC生成が失敗します。 コード生成時に生成されたソースコードが必要なのはなぜですか? 私の職場にはローカルソースポリシーがなく、ARXMLのような非ソースコードの設定しかローカルPCに入れられないので質問しました。 BR/くまモン Re: MCAL expects source code for code generation こんにちは、 @kumamon さん。 構成生成は必ずしもARXMLのみに基づいて行われるわけではない。生成プロセス中、MCAL設定ツールはインストールされたRTD/MCALパッケージの一部として、定義やジェネレーターに必要な情報を含むヘッダーファイルも提供する必要があります。 したがって、期待される .h のいずれかがファイル名が.hhに変更されると、ジェネレーターがその依存関係を特定・処理できなくなる可能性があり、コード生成が失敗することがあります。 BR、VaneB Re: MCAL expects source code for code generation こんにちは、 @VaneB さん。 ご回答ありがとうございます。 今や明らかになった。 BR/くまモン
View full article
NXPのセキュリティ ~まとめページ~ (日本語ブログ) NXPのセキュリティ概要 と 本ページの目的   近年、IoTデバイスやエッジ機器の普及に伴い、セキュリティ要件はますます高度かつ複雑になっています。NXPでは、プロセッサ、セキュアエレメント、ソフトウェア/ツール、関連ドキュメントを含む総合的なセキュリティ・ソリューションを提供しており、開発者が設計段階からセキュアなシステムを構築できる環境を整えています。 本まとめページでは、NXPのセキュリティ関連情報を一つに集約し、必要な情報に素早くアクセスできるように整理しています。記事は、NXPデバイスの基礎知識から実装ハンズオンまで幅広くカバーしており、これからNXP製品を用いてセキュア設計を進める方に最適な構成となっています。 Tech Blog記事一覧(リンクと概要) ◆入門・導入事例◆ ポイント 記事 概要 JC-STAR概説とNXPの製品 日本におけるセキュリティ要件適合評価及びラベリング制度(JC-STAR)の開始と、セキュリティ機能を支えるNXP製品 (日本語ブログ) JC-STARで議論されているセキュリティ要件の概要を紹介。NXP製品がどのように要件に対応しているかを体系的に解説。セキュリティ設計の全体像を理解するための入門記事。 ユースケース例 製品・企業価値の向上にもつながる組み込み製品におけるセキュリティのユースケース例 (日本語ブログ) 組み込み製品におけるセキュリティの重要性を、ユースケースを例に脅威・インパクト、対策の観点からわかりやすく、簡潔に解説。 ハードウェア・セキュリティのメリット セキュリティ対応の容易化・工数削減に貢献するNXPのハードウェア・セキュリティ・ソリューション (日本語ブログ) NXPのハードウェア・セキュリティ(暗号アクセラレータ内蔵MCU/MPU、EdgeLock®セキュア・エンクレーブ内蔵MCU/MPU、セキュア・エレメント/オーセンティケータ、EdgeLock 2GO:セキュア・プロビジョニング・サービス)を活用すると何が良いのか?またそれぞれの特徴を解説。 NXP製セキュリティ機能搭載製品を選択するメリット (日本語ブログ) PQC(耐量子暗号)対応 PQC対応は出荷後では遅い!セキュアブートとファームウェア・アップデートから考える耐量子対策 (日本語ブログ) 現時点、量子コンピューターは発展途上ですが、産業機器のような長期利用が想定される機器においては早めの対応必須です。後から対応しようでは手遅れになる可能性も。 製造から廃棄まで、製品ライフサイクルをセキュアに支えるNFCタグIC 製造から廃棄まで、1チップで製品ライフサイクルをセキュアに支えるNFCタグIC「NTAG X DNA」の紹介 (日本語ブログ) 一台の産業機器が製造され、設置・運用・メンテナンスを経て廃棄されるまでの流れに沿って、各フェーズでNFCタグIC(NTAG X DNA)がどう役立つかを紹介します。 ◆テーマ別・実践コーナー◆ 「重要なセキュリティ技術の実装」 セキュア・ブート & アップデート テーマ 分類 記事 セキュア・ブート セキュア・アップデート 基礎 MCUにおけるセキュアブート、セキュア(OTA)アップデートの基本 (日本語ブログ) セキュリティ対応において重要な「セキュアブート」「セキュア/OTAアップデート」の概要について解説します。MPUにおいても基本的な考え方は同様です。 セキュア・ブート (i.MX) 解説 i.MX 93プロセッサ: セキュアブートの署名と認証の仕組みを解説 (日本語ブログ) i.MX 93 のセキュアブート構造を詳細解説。署名・検証の流れを図解ベースで理解できる内容。 実践 i.MX 93プロセッサ: セキュアブートの実装方法 - 実践編 (日本語ブログ) 上記「i.MX93の署名と認証の仕組み」を踏まえて、実際のハンズオン手順を解説。開発者が実際に動かしながら理解できる実践的な内容。 解説 実践 i.MX 95 SPSDK によるセキュアブート (日本語ブログ) i.MX 95を用いたセキュアブートの解説と実装方法をハンズオン形式で解説。開発者が実際に動かしながら理解できる実践的な内容。 セキュア・ブート (i.MX RT) 解説 実践 NXP® MIMXRT1060-EVKCで始めるZephyr®と MCUbootによるセキュアブート (アイティアクセス株式会社) NXPの高性能マイコン評価ボード「MIMXRT1060-EVKC」を例に、Zephyrとセキュアブートローダ「MCUboot」を組み合わせた実践的な開発手順を紹介しています。実機を用いたビルドから書き込み、ファームウェア更新までの流れを通じて、Zephyrを用いたセキュアな組込みシステム開発の具体像を理解できます。 セキュア・エレメント テーマ 分類 記事 セキュア・エレメントを使うための準備 解説 & 実践 セキュアエレメントSE05xの使用方法 : Raspberry PiでのPlug and Trust Middlewareのセットアップ(日本語ブログ) セキュアエレメントSE05xの使用方法 : FRDM-IMX93開発ボード上でのPlug and Trust Middlewareのセットアップ(日本語ブログ) NXPのセキュア・エレメントSE05xには、Plug and Trust Middlewareというミドルウェアが提供されています。SE05xを使用するための専用APIに加えて、OpenSSLやmbed-TLSといった広く使用されているライブラリに対するプラグインも含まれています。Plug and Trust Middlewareのセットアップを、Raspberry PiとFRDM-IMX93(i.MX 93向け開発ボード) 向けに行う手順を紹介。 OpenSSL 実践 セキュアエレメントSE05xの使用方法 : OpenSSL経由でのSE050の使用(日本語ブログ) セキュア・エレメント(SE05x) と OpenSSL を連携させた実践的な使い方を解説 Azure IoT Hubへの接続 実践 セキュアエレメントSE05xの使用方法 : Eclipse Mosquitto clientを使用したAzure IoT Hubへの接続(日本語ブログ) Eclipse Mosquitto clientを使用したAzure IoT Hubへの接続方法を紹介します。   鍵管理 テーマ 分類 記事 SoC内のセキュリティエンジンを用いた鍵管理 解説 & 実践 i.MX 93のEdgeLock® Secure Enclave(ELE)の使用方法 : PKCS#11経由での暗号鍵の保存と使用 (日本語ブログ) i.MX 93内蔵のEdgeLock® Secure Enclave(ELE)の暗号アクセラレータおよび鍵管理の機能をPKCS#11経由で使用する方法について解説します。 Secure Provisioning Tool  ~ NXP MCU向け セキュリティ機能を使用するためのツール ~  Secure Provisioning Tool は、MCUXpresso for VSCや、MCUXpresso IDE にて開発評価済みのアプリケーションに対して、製品リリースに向けたイメージのセキュリティー対応や書き込みなどの作業を行うためのMCU向けツールです。セキュア・ブート、セキュア・アップデート、デバッグ認証、デバイス認識などを行えます。 テーマ 分類 記事 Secure Provisioning Tool 解説 実践 Secure Provisioning Tool のインストール方法、使い方 (株式会社マクニカ) Secure Provisioning Tool の便利機能紹介 (株式会社マクニカ) Secure Provisioning Tool(以降、SPT と略します)と呼ばれるツールの使い方を分かりやすく紹介しています。 ◆基礎技術・学習コーナー◆  カテゴリ 記事 概要 用語解説 半導体ハードウェア・セキュリティでよく耳にする機能について解説 (セキュアエレメント、セキュアエンクレーブ、TPM、HSM、TEE、TrustZoneなど) (日本語ブログ) セキュアエレメント、セキュアエンクレーブ、TPM、HSM、TEE、TrustZoneなどについて、機能の役割、分類、それと概要を紹介します。 さいごに NXPのセキュリティ対応製品は、多様なユースケースの要件に対応できる柔軟性と拡張性を備えています。本まとめページを活用することで、必要な情報に素早くアクセスし、製品選定から実装までスムーズに進めることを期待します。新しい記事も随時追加予定ですので、最新情報をチェックいただければ幸いです。 セキュリティに関連するコンテンツの要望や改善点などございましたら、以下よりお気軽にお問い合わせください。 NXPジャパン 技術ブログ(日本語) コンテンツ要望・改善アンケート – フォーム​に記入する =========================​​ お問い合わせの際には「NXPへの技術質問 - 問い合わせ方法 (日本語ブログ)」もご活用ください。​ (既に弊社NXP代理店、もしくはNXPとお付き合いのある方は、直接担当者へご質問いただいてもかまいません。) 近年、IoTデバイスやエッジ機器の普及に伴い、セキュリティ要件はますます高度かつ複雑になっています。NXPでは、プロセッサ、セキュアエレメント、ソフトウェア/ツール、関連ドキュメントを含む総合的なセキュリティ・ソリューションを提供しており、開発者が設計段階からセキュアなシステムを構築できる環境を整えています。 本まとめページでは、NXPのセキュリティ関連情報を一つに集約し、必要な情報に素早くアクセスできるように整理しています。記事は、NXPデバイスの基礎知識から実装ハンズオンまで幅広くカバーしており、これからNXP製品を用いてセキュア設計を進める方に最適な構成となっています。 Security Technology Focus 日本語ブログ
View full article
NXP Security - Summary Page (Japanese blog) NXP Security Overview and the Purpose of This Page   In recent years, with the spread of IoT devices and edge equipment, security requirements have become increasingly sophisticated and complex. NXP provides comprehensive security solutions including processors, secure elements, software/tools, and related documentation, creating an environment in which developers can build secure systems from the design stage . This summary page brings together all of NXP's security-related information in one place , organized for quick access to the information you need. The articles cover a wide range of topics, from basic knowledge of NXP devices to hands-on implementation exercises, making it ideal for anyone planning to use NXP products to design secure systems. Tech Blog Article List (Links and Summary) ◆Introduction and Case Studies◆ point article overview JC-STAR Overview and NXP Products The launch of the Japan Security Requirements Conformity Assessment and Labeling System (JC-STAR) in Japan and NXP products that support security functions (Japanese blog) This article provides an overview of the security requirements discussed in JC-STAR. It systematically explains how NXP products meet the requirements. It is an introductory article to help you understand the overall picture of security design. Use Case Example Security use cases for embedded products that can improve product and corporate value (Japanese blog) The importance of security in embedded products is explained in an easy-to-understand and concise manner from the perspectives of threats, impacts, and countermeasures, using use cases as examples. The Benefits of Hardware Security NXP's hardware security solutions simplify security implementation and reduce man-hours (Japanese blog) What are the benefits of using NXP's hardware security (MCU/MPU with built-in cryptographic accelerator, MCU/MPU with built-in EdgeLock ® Secure Enclave, Secure Element/Authenticator, EdgeLock 2GO: Secure Provisioning Service)? We also explain the features of each. The benefits of choosing products with NXP security features (Japanese blog) PQC (Post-Quantum Cryptography) compatible PQC compliance is too late after shipment! Quantum-proofing measures considered from the perspective of secure boot and firmware updates (Japanese blog) While quantum computers are still under development, early action is essential for equipment intended for long-term use, such as industrial machinery. Delaying action could mean it's too late. NFC tag IC securely supports the entire product lifecycle, from manufacturing to disposal. Introducing "NTAG X DNA," an NFC tag IC that securely supports the entire product lifecycle from manufacturing to disposal with a single chip (Japanese blog) This presentation will illustrate how NFC tag ICs ( NTAG X DNA ) are useful at each phase of the process, from the manufacturing of an industrial piece of equipment to its installation, operation, maintenance, and eventual disposal. ◆Theme-specific/Practical Corner◆ "Implementation of Important Security Technologies" Secure Boot & Updates theme classification article Secure Boot, Secure Update basics The basics of secure boot and secure (OTA) updates in MCUs (Japanese blog) This document explains the basics of "Secure Boot" and "Secure/OTA Updates," which are crucial for security. The same fundamental concepts apply to MPUs as well. Secure Boot (i.MX) Commentary i.MX 93 Processor: Explaining Secure Boot Signing and Authentication A detailed explanation of the i.MX 93 secure boot structure. The signing and verification process is explained with diagrams. Practice i.MX 93 Processor: How to Implement Secure Boot - Practical Guide (Japanese blog) Based on the above explanation of "i.MX93 signing and authentication mechanisms," this section explains the actual hands-on procedure. It's practical content that developers can understand by actually running the code. Explanation and Practice Secure Boot with i.MX 95 SPSDK (Japanese Blog) This guide provides a hands-on explanation of secure boot using i.MX 95 and how to implement it. It's practical and allows developers to understand the concepts by actually running the code. Secure Boot (i.MX RT) Explanation and Practice Getting Started with Zephyr ® and Secure Boot using MCUboot on NXP ® MIMXRT1060-EVKC (IT Access Co., Ltd.) This guide uses NXP's high-performance microcontroller evaluation board "MIMXRT1060-EVKC" as an example to demonstrate practical development procedures combining Zephyr and the secure bootloader "MCUboot." Through the entire process, from building and programming to firmware updates using actual hardware, you can gain a concrete understanding of secure embedded system development using Zephyr. Secure element theme classification article Preparing to use the secure element Explanation & Practice How to use Secure Element SE05x: Setting up Plug and Trust Middleware on Raspberry Pi (Japanese blog) How to use Secure Element SE05x: Setting up Plug and Trust Middleware on the FRDM-IMX93 development board (Japanese blog) NXP's Secure Element SE05x comes with middleware called Plug and Trust Middleware. In addition to a dedicated API for using the SE05x, it also includes plugins for widely used libraries such as OpenSSL and mbed-TLS. This document describes the procedure for setting up Plug and Trust Middleware for Raspberry Pi and FRDM-IMX93 (a development board for i.MX 93). OpenSSL Practice How to use SecureElement SE05x: Using SE050 via OpenSSL (Japanese blog) This article explains practical ways to use Secure Element (SE05x) in conjunction with OpenSSL. Connecting to Azure IoT Hub Practice How to use Secure Element SE05x: Connecting to Azure IoT Hub using Eclipse Mosquitto client (Japanese blog) This guide explains how to connect to Azure IoT Hub using the Eclipse Mosquitto client.   key management theme classification article Key management using the security engine within the SoC Explanation & Practice How to use the EdgeLock® Secure Enclave (ELE) on i.MX 93: Storing and using encryption keys via PKCS#11 (Japanese blog) This document explains how to use the cryptographic accelerator and key management functions of the i.MX 93's built-in EdgeLock® Secure Enclave (ELE) via PKCS#11. Secure Provisioning Tool ~ A tool for using security features for NXP MCUs ~ The Secure Provisioning Tool is an MCU-specific tool for performing tasks such as securing and writing images for product releases of applications developed and evaluated using MCUXpresso for VSC or MCUXpresso IDE. It enables secure boot, secure updates, debug authentication, device recognition, and more. theme classification article Secure Provisioning Tool Explanation Practice How to install and use the Secure Provisioning Tool (Macnica, Inc.) Introduction to the useful features of the Secure Provisioning Tool (Macnica, Inc.) This guide provides a clear explanation of how to use a tool called the Secure Provisioning Tool (hereinafter abbreviated as SPT). ◆Basic skills and learning corner◆ category article overview Glossary Explaining Common Semiconductor Hardware Security Features (Secure Element, Secure Enclave, TPM, HSM, TEE, TrustZone, etc.) (Japanese blog) This article introduces the functional roles, classifications, and overviews of secure elements, secure enclaves, TPMs, HSMs, TEEs, TrustZones, etc. Finally NXP's security-enabled products are flexible and scalable to meet the requirements of a wide variety of use cases. We hope that by using this summary page, you will be able to quickly access the information you need and smoothly proceed from product selection to implementation. New articles will be added from time to time, so please check back for the latest information. If you have any requests or suggestions for improvements regarding security-related content, please feel free to contact us using the information below. NXP Japan Technical Blog (Japanese) Content Request/Improvement Survey – Fill out the form ============================ When making inquiries, please also use the " Technical Questions to NXP - How to Contact Us( Japanese Blog) "(If you are already an NXP distributor or have a relationship with NXP, you may ask the person in charge directly.) In recent years, with the spread of IoT devices and edge equipment, security requirements have become increasingly sophisticated and complex. NXP provides comprehensive security solutions including processors, secure elements, software/tools, and related documentation, creating an environment in which developers can build secure systems from the design stage . This summary page brings together all of NXP's security-related information in one place , organized for quick access to the information you need. The articles cover a wide range of topics, from basic knowledge of NXP devices to hands-on implementation exercises, making it ideal for anyone planning to use NXP products to design secure systems. Security Technology Focus Japanese Blog
View full article
NXP Security - 摘要页面(日语博客) NXP 安全概述及本页目的   近年来,随着物联网设备和边缘设备的普及,安全需求变得日益复杂。恩智浦提供全面的安全解决方案,包括处理器、安全元件、软件/工具及相关文档,为开发人员从设计阶段构建安全系统创造了有利环境。 本汇总页面将恩智浦所有安全相关信息集中于一处,方便您快速查找所需信息。文章涵盖广泛的主题,从恩智浦器件的基础知识到实践操作练习,是计划使用恩智浦产品设计安全系统的人员的理想之选。 技术博客文章列表(链接和摘要) ◆引言和案例研究◆ 要点 文章 概述 JC-STAR 概述和 NXP 产品 日本安全要求合格评定和标签系统(JC-STAR)在日本的推出以及恩智浦支持安全功能的产品(日本博客) 本文概述了JC-STAR中讨论的安全要求,并系统地阐述了恩智浦产品如何满足这些要求。这是一篇入门文章,旨在帮助您了解安全设计的整体框架。 用例示例 嵌入式产品的安全应用案例,可提升产品和企业价值(日文博客) 本文从威胁、影响和应对措施的角度,以通俗易懂的方式,通过用例举例说明了嵌入式产品安全性的重要性。 硬件安全的优势 恩智浦的硬件安全解决方案简化了安全实施,并减少了人工工时(日本博客) 使用恩智浦半导体的硬件安全解决方案(内置加密加速器的MCU/MPU、内置EdgeLock ®安全隔离区的MCU/MPU、安全元件/认证器、EdgeLock 2GO:安全配置服务)有哪些优势?我们还将解释每项解决方案的特性。 选择具有恩智浦安全功能的产品的好处(日文博客) 兼容后量子密码学(PQC)。 PQC合规性在发货后才发现为时已晚!从安全启动和固件更新的角度考虑量子攻击防护措施(日文博客) 虽然量子计算机仍在研发中,但对于工业机械等长期使用的设备而言,尽早采取行动至关重要。拖延行动可能意味着为时已晚。 NFC标签IC可安全地支持产品的整个生命周期,从制造到报废。 推出“NTAG X DNA”,这是一款NFC标签IC,仅需一枚芯片即可安全支持从制造到报废的整个产品生命周期(日本博客)。 本次演示将阐述 NFC 标签 IC( NTAG X DNA )在工业设备制造、安装、操作、维护和最终处置的各个阶段的用途。 ◆专题/实用专栏◆ “重要安全技术的实施” 安全启动和更新 主题 分类 文章 安全启动,安全更新 基础知识 MCU 中的安全启动和安全(OTA)更新基础知识(日文博客) 本文档解释了“安全启动”和“安全/OTA更新”的基本原理,这两项技术对安全性至关重要。这些基本概念同样适用于MPU(微型处理器)。 安全启动 (i.MX) 评论 i.MX 93 处理器:安全启动签名和身份验证详解 本文详细解释了 i.MX 93 安全启动结构,并用图表说明了签名和验证过程。 实践 i.MX 93 处理器:如何实现安全启动 - 实用指南(日语博客) 基于以上对“i.MX93签名和认证机制”的解释,本节将介绍实际操作步骤。这些实用内容可以通过实际运行代码来理解。 讲解与练习 使用 i.MX 95 SPSDK 实现安全启动(日本博客) 本指南通过实际操作讲解了如何使用 i.MX 95 实现安全启动。它注重实践,使开发人员能够通过实际运行代码来理解相关概念。 安全启动 (i.MX RT) 讲解与练习 在 NXP ® MIMXRT1060-EVKC (IT Access Co., Ltd.) 上使用 MCUboot 实现 Zephyr ®和安全启动入门 本指南以恩智浦半导体的高性能微控制器评估板“MIMXRT1060-EVKC”为例,演示结合Zephyr和安全引导加载程序“MCUboot”的实际开发流程。通过从构建、编程到使用实际硬件进行固件更新的整个过程,您可以深入了解如何使用Zephyr进行安全嵌入式系统开发。 安全元件 主题 分类 文章 准备使用安全元件 解释 & 实践 如何使用安全元件 SE05x:在树莓派上设置即插即用中间件(日文博客) 如何使用安全元件 SE05x:在 FRDM-IMX93 开发板上设置即插即用中间件(日文博客) NXP 的安全元件 SE05x 附带名为 Plug and Trust Middleware 的中间件。除了用于 SE05x 的专用 API 外,它还包含 OpenSSL 和 mbed-TLS 等常用库的插件。本文档介绍了在 Raspberry Pi 和 FRDM-IMX93(i.MX 93 的开发板)上设置 Plug and Trust Middleware 的步骤。 OpenSSL 实践 如何使用 SecureElement SE05x:通过 OpenSSL 使用 SE050(日语博客) 本文介绍了将安全元件 (SE05x) 与 OpenSSL 结合使用的实用方法。 连接到 Azure IoT 中心 实践 如何使用安全元件 SE05x:使用 Eclipse Mosquitto 客户端连接到 Azure IoT 中心(日语博客) 本指南说明如何使用 Eclipse Mosquitto 客户端连接到 Azure IoT 中心。   关键管理 主题 分类 文章 利用SoC内部的安全引擎进行密钥管理。 解释 & 实践 如何在 i.MX 93 上使用 EdgeLock® 安全隔离区 (ELE):通过 PKCS#11 存储和使用加密密钥(日语博客) 本文档解释了如何通过 PKCS#11 使用 i.MX 93 内置 EdgeLock® 安全隔离区 (ELE) 的加密加速器和密钥管理功能。 安全配置工具 ~用于启用NXP MCU安全功能的工具~ 安全配置工具是一款专为 MCU 设计的工具,用于执行诸如保护和写入使用 MCUXpresso for VSC 或 MCUXpresso IDE 开发和评估的应用程序的产品版本镜像等任务。它支持安全启动、安全更新、调试身份验证、设备识别等功能。 主题 分类 文章 安全配置工具 解释 实践 如何安装和使用安全配置工具(Macnica公司) 安全配置工具(Macnica公司)实用功能简介 本指南清晰地解释了如何使用名为安全配置工具(以下简称 SPT)的工具。 ◆基本技能和学习角◆ 类别 文章 概述 词汇表 解释常见的半导体硬件安全特性(安全元件、安全隔离区、TPM、HSM、TEE、TrustZone 等)(日语博客) 本文介绍了安全元件、安全飞地、TPM、HSM、TEE、TrustZones 等的功能角色、分类和概述。 最后 恩智浦的安全产品灵活且可扩展,能够满足各种应用场景的需求。我们希望通过本概要页面,您能够快速获取所需信息,并顺利完成从产品选型到实施的整个流程。我们将不定期更新文章,敬请关注最新资讯。 如果您对安全相关内容有任何改进要求或建议,请随时使用以下信息与我们联系。 NXP日本技术博客(日语)内容请求/改进调查——请填写表格 ============================ 如有疑问,请同时参考“ NXP 技术 问题 咨询 - 如何 联系我们 ( 日语博客 ) ”。 (如果您已经是 恩智浦的 分销商或 与 恩智浦 有业务往来 ,您可以直接咨询负责人。) 近年来,随着物联网设备和边缘设备的普及,安全需求变得日益复杂。恩智浦提供全面的安全解决方案,包括处理器、安全元件、软件/工具及相关文档,为开发人员从设计阶段构建安全系统创造了有利环境。 本汇总页面将恩智浦所有安全相关信息集中于一处,方便您快速查找所需信息。文章涵盖广泛的主题,从恩智浦器件的基础知识到实践操作练习,是计划使用恩智浦产品设计安全系统的人员的理想之选。 安全 技术聚焦 日本博客
View full article
MCP Server is unavailable I'm trying to import NXP's MCP service into VS Code by referring to the Agentic AI Development - NXP Community documentation, but it's not working after importing. The logs show "Discovered 0 tools." Is this the reason it's not working? If so, what are some solutions?
View full article
2026年版 ベストデータ削除サービス:90日間テスト&専門家分析(2026年11月) おすすめ商品: 私たちは実際のユーザーが行うようにテストを行いました。有料サブスクリプション、シードされたアイデンティティ、そして同じブローカーパネルに対して30日/60日/90日ごとの再確認です。その結果、マーケットのトップをめぐる二頭の争いが繰り広げられ、個人データが再表示された後も再提出し続けてこそ、データ削除サービスが機能するという明確な警告となります。 Incogniは、完全自動化された削除機能で第1位を獲得し、プレミアムプランでは最も高いコストパフォーマンスを実現しています。年間プランの場合、月額約6.49ドル(年間一括請求で約77.88ドル)です。自動再提出サイクルとデロイトによる監査済みのレポート機能により、継続的な労力をかけずに問題を解決したい人にとって、このソリューションは最適な選択肢となる。 INCOGNIから始めましょう DeleteMeは、人間主導のコンシェルジュモデルと、私たちが測定した最も広いブローカーのフットプリントである750+のアクティブマネジメントブローカーを基に#2を獲得。複雑な案件、係争案件、あるいは繰り返し再掲載される案件においては、人的要素こそが「要請された」案件と「削除された」案件を分ける決定的な要素となる。 DeleteMe を試してください → 両者に共通する点、そして2026年の最終候補リストに必ず求められる点は、継続的な再監視です。つまり、ブローカーがデータを再掲載するたびに、自動的に再チェックと再提出が行われるということです。それがなければ、削除は一時的なリストからの削除に過ぎず、あなたのデジタル上の足跡は静かに再構築されてしまう。 クイック比較表:2026年版おすすめデータ削除サービス インコグニー:オートメーションと価値 ·~月額6.49ドル(年間77.88ドル)·完全オートメーション ·420+ ブローカー(Unlimitedで3,000+)·★★★★★ 5.0 DeleteMe :人間による削除サービス · 月額約10.75ドル(年間129ドル)·ハイブリッド ·400+車載/560+カスタム ·★★★★★ 4.8 オプトリー:削除の証明が確認済み・~月額3.25ドル(年間39ドルから)・完全オートメーション ·365〜635のブローカー(階層依存)·★★★★1/2 4.5 プライバシービー:最大ブローカーカバレッジ ·~月額8.00ドル(年間96ドルから)·フルオートメーション ·1,128+ ブローカー ·★★★★ 4.0 オーラ:オールインワンセキュリティバンドル ·~月$12.00(年間144ドル)·完全オートメーション ·~140人のブローカー ·★★★★ 4.0 EasyOptOuts :予算設定後はお任せ · 月額約1.67ドル(年間19.99ドル)·完全オートメーション ·200+の高負荷サイト ·★★★★ 4.0 最高のデータ削除サービスをテストし、ランキング付けした方法 私たちは、一貫した名前、生年月日、過去の住所2件、電話番号1件、メールアドレス1件を含む、管理されたテスト用IDを1つ作成し、Whitepages、Spokeo、BeenVerified、Intelius、MyLifeなどのトラフィック量の多い人物検索サイトやデータブローカーサイトの固定パネル全体にそれを散布しました。私たちは各サービスに自費で加入した後、同一の基準となるブローカーを3つのチェックポイントで再確認しました。 30日目:早期除去の兆候。重要な理由:速いサービスは実際の削除を表示し、遅いサービスは「進行中」と表示します。 60日目:安定した確認済み除去率。重要な理由:ほとんどの正当なオプトアウトは4〜6週間以内にクリアされます 90日目:耐久性と再出現。なぜマターなのか:データブローカーはリストを再掲載するため、残ったものを数えています 私たちは、実際に結果に影響を与える4つの変数に重み付けを行いました。 除去の持続性 ― 30日目だけでなく、90日目にどれだけ残っていたか。 カスタム削除能力 — 人間が頑固または争いのあるブローカーをエスカレーションできるかどうか レポートの透明性 — スクリーンショット、アクティビティログ、監査済み請求 一人当たりの年間費用 ― 年間請求額と世帯割引後の実質価格 2024年のコンシューマー・レポートの実地調査は、依然として外部ベンチマークとなっている。有料サービス全体で、平均して4ヶ月以内に削除された掲載情報はわずか約35%だった。その数字は、それ以下の順位の企業が生き残るために乗り越えなければならない現実を突きつけるものだ。 ブローカーが実際に収集するデータとは、なぜ重要なのか データブローカーは、整然とした単一のレコードを販売するわけではない。彼らは公的記録、ロイヤルティプログラム、アプリの権限、スクレイピングしたウェブページなどから複合的な個人情報を作成し、それをマーケティング会社、身元調査サービス、そして悪用されれば犯罪者に転売する。ほとんどの データブローカー は人検索、マーケティングセグメンテーション、リスクスコアリング、本人確認を専門としていますが、結果は同じです。つまり、あなたが同意していない永続的なプロフィールです。 一般的な個人情報パッケージには、ホーム住所、メールアドレス、電話番号、生年月日、親族、不動産記録、そしてソーシャルプロフィールから取得した写真や動画が含まれます。推定される健康関心、財務シグナル、位置履歴などの機密データを加えることで、プライバシー専門家が「個人識別情報(Personally Identifiable Information)」と呼ぶ最も商業的に有用な形が完成します。 だからこそ、単一の検索エンジン検索で、あなたが作成していない個人プロフィールが現れることがあるのです。Google検索結果やその他の検索エンジンは、データブローカーサイト、ブローカーサイト、ピープルファインダーサイトのページをインデックス化しており、メインストリームの検索結果には決して現れない影のサイトも含まれます。個人プロフィールが多ければ多いほど、それらを完全な個人データドシエにクロス・リファレンスしやすくなります。 私たちのテスト用IDは、データ投入から2週間以内に40以上のデータブローカーサイトに表示された。中には明らかに人探しのページもあれば、検索結果の3ページも埋もれたデータブローカーサイトもありました。目に見える暴露と目に見えない暴露の間のギャップこそが、暴露報告書と継続的なモニタリングなしにDIYによる清掃が失敗する理由なのです。 1. Incogni — オートメーション削除と価値において総合的に最適 最適な用途: 幅広いブローカーリーチと定期的なオートメーションを最低プレミアム価格で望む手を離すユーザー。 Incogniはオートメーションを第一にするリーダーであり、プレミアムティアで最も価値の高い存在です。スタンダード年間プランの料金は年間約77.88ドル(月額約6.49ドル)で、420社以上のデータブローカーに対応し、削除リクエストも完全に自動化されています。無制限プラン(年間179.88ドル)無制限のカスタム削除リクエストを追加し、対象範囲を3,000以上のソースに拡大します。 Incogniの特徴は、透明度レイヤーにある。ダッシュボードにはブローカーごとの解決時間や活動履歴が表示され、同社の主張はデロイトの保証レポートによって裏付けられています。これは多くの競合他社がいまだに追及できない第三者によるチェックです。自動再提出は60日から90日のサイクルで実行され、一度限りの削除を無意味にする再露出のライフサイクルに直接対抗します。繰り返し戻ってくる個人データの場合、そのサイクルが製品です。 長所: 最上位の自動化サービスの中で最も低価格(年間約77.88ドル) 420以上の自動化ブローカー、無制限の3,000以上の情報源 デロイト監査済みの撤去請求 継続的な再スキャンと自動再送信 無制限プランでは、カスタム削除リクエストを無制限にご利用いただけます。 短所: 標準プランでは、プロファイルごとに名前を1つしか指定できません。 複雑なエスカレーションに対応する人間のコンシェルジュ層はありません 個々の削除に関するスクリーンショットレベルの証拠はありません 結論: 設定して忘れて最低のプレミアム価格で除去したい大多数のユーザーにとって、Incogniは価値とオートメーションの深さの面で合理的な#1です。 2. DeleteMe — 最高級のデータ削除サービス(人間による対応) 最適なケース:複雑な露出、複数の住所、そして人間による確認済みの削除を希望するすべての人。 DeleteMeは、エリート向けのコンシェルジュ級のオプションであり、自動オプトアウトが滞った場合に人間のケースワーカーが介入するという理由から、第2位にランクインしました。スタンダードプランは1人用129ドル(月10.75ドル)から始まり、ファミリプランは2人用(年間229ドル)と4人用(329ドル/年)のティアがあります。自動削除は400以上のソースを対象とし、カスタム削除は560以上のソースを対象とします。これには、テンプレート削除要求を日常的に無視する頑固なデータブローカーも含まれます。 DeleteMeはさらに、追加料金なしで積極的なプライバシーツールキットをバンドルしています。メールマスキング、電話番号マスキング、クレジットカードマスク機能など、私たちがテストした他のサービスには基本プランには含まれていない機能です。ダッシュボードには、レビューされた情報源の数と、削除に成功した件数が表示されます。過去の住所や旧姓に分散している個人データの場合、人的要素がリクエストと結果の差を生む。 長所: 頑固または複雑なブローカーCASEに対する人間主導のエスカレーション 400以上の自動削除ソース / 560以上のカスタム削除ソース メール、電話、クレジットカード情報のマスキング機能が含まれています ファミリプランは1人あたりのコストを削減します 迅速なカスタマーサポートと活発なユーザーコミュニティ 短所: プレミアム価格:1人あたり年間129ドル ダッシュボードにはスクリーンショットレベルのビフォーアフター証明はありません 標準プランでは、カスタム撤去は年間40回までに制限されます。 結論:あなたの個人情報が複雑な場合(よくある名前、引っ越しの履歴、あるいはあまり知られていない地域ディレクトリのデータなど)、DeleteMeの人的介入が「削除依頼」と「削除済み」の分かれ目となる。 3~10。その他の主要データ削除サービスとの比較 3. Optery — 削除証明の確認に最適 Opteryは検証可能性において第3位にランクインした。そのダッシュボードは、削除の証拠としてスクリーンショットを表示する機能を備えており、競合他社のほとんどが未だに提供していない、削除前後の証拠を提示する。コアプランの料金は年間39ドルからで、最大40社のブローカーへのエクスポージャーを対象とした無料のセルフサービススキャンが付属します。すべてのアカウントには、削除開始前に発見されたプロファイルを正確に一覧表示する暴露レポートが含まれています。独立したテストにおいて、Opteryは約68%の除去率を達成し、管理されたベンチマークの中で最高のスコアを記録した。そのトレードオフとしては、コンシェルジュの深さがDeleteMeにまだ及びず、ニッチな地域ブローカーの個人データの処理に時間がかかることもあります。 4. プライバシービー — 最大限のブローカーカバレッジに最適なサービス プライバシー BeeはPCMagで初めてデータ削除カテゴリーで満点の5つ星評価を獲得し、1,128のデータブローカーをカバーし、185,000以上のカスタムサイトからの削除をサポートしています。料金は年間約96ドルからで、より詳細な監視機能が必要な場合は上位プランも用意されています。これは、最も幅広い公開されたブローカーリストと、削除カテゴリーの細かい管理を求めるユーザーに最適な選択肢です。独立機関による検査では、その除菌率は約45%と評価されている。これは立派な数字だが、目に見える効果という点ではトップ企業に劣る。あまり知られていないブローカーサイト上の個人データに関しては、その網羅性は非常に役立つ。 5. オーラ — ベストオールインワンセキュリティバンドル Auraはデータ削除とウイルス対策、VPN、個人情報盗難保険を一つのサブスクリプションにまとめており、年間約144ドル(月約12ドル)から始まります。自動削除は約140のブローカーをカバーしており、専門業者よりも狭い範囲ですが、3つの別々のサブスクリプションよりも単一のセキュリティスタックを望むファミリにはこのバンドルが理にかなっています。家族全員に一つのセキュリティソリューションを求めるなら、Auraのファミリープランが最大の魅力です。削除エンジンは一般的な個人データ漏洩には適切に対応しますが、専門のブローカー兼削除スペシャリストの代わりになるものではありません。 6. EasyOptOuts — 最も予算に優しい選択肢 EasyOptOutsは年間19.99ドルで、今回テストしたサービスの中で最も低価格です。管理されたベンチマークテストでは約65%の除去率を達成し、Opteryに次ぐ2位、いくつかのプレミアムツールを上回る結果となった。設計上、設定して忘れるタイプで、カスタム削除がなく、ダッシュボードも最小限に抑えられ、セキュリティレポートも少ないです。予算が限られている低リスクユーザーにとっては、個人データのクリーンアップの合理的な入り口となります。 7. Onerep — 最高の無駄な単独除去 Onerepは複数のバンドル製品の除去エンジンであり、年間90ドルから99.96ドル(月7.49ドルから8.33ドル)で直接販売されています。一般的な検索サイトを確実にクリアし、設置も迅速です。カバー範囲は中間的ですが、最上位サービスの追加機能を必要としないユーザーにとって、単体でスキャナー兼リムーバーとして機能します。 8. Kanary — 個人情報暴露とソーシャルメディア露出に最適な場所 Kanaryはニッチなサービスで、ソーシャルメディアの個人情報の監視や、場合によってはドキシングの対策を支援できます。これは多くの競合他社が持っていない機能です。料金は月額9.99ドルから50ドルで、無料プランも用意されています。トレードオフとしては、最も高価な階層のみが完全自動化され、無料版はモバイル専用です。 9. IDX Complete — ベスト・フル・アイデンティティ・トミート・スイート IDX Completeは、データ削除と個人情報盗難監視、3つの信用情報機関にわたる信用監視、パスワードマネージャー、VPN、ダークウェブ監視を統合した完全なセキュリティおよびプライバシースイートです。年間355.32ドル(月額約29.61ドル)年間請求の場合)、このリストの中で最も高額なオプションですが、複数の個別のサブスクリプションを置き換えることができます。データ削除サービスは100社以上のブローカーを対象としており、専門業者に比べると対象範囲は狭いものの、その周辺環境の保護は比類のないものです。 10. ノートン社のReputationDefender ― 著名人に最適 ReputationDefenderは、継続的なデータ漏洩監視と評判保護を必要とする専門家や著名人向けに開発されています。料金は見積もり制で公表されておらず、第三者機関による見積もりでは、基本的なブローカー削除サービスで年間約99ドルから、最高レベルの評判管理サービスで年間25,000ドルまで幅があります。これは低価格帯の選択肢ではないが、経営幹部や著名人にとって、評判管理サービスは差別化要因となる。 データブローカー削除サービスの料金:実際に支払う金額は? 以下の表は、年間料金、自動化されたブローカーによる補償、および人的エスカレーション層という、実際に結果に影響を与える3つの変数を比較したものです。カスタム削除とカスタム削除依頼は同じものではないことに注意してください。前者は通常、手動でのエスカレーションを意味し、後者は標準の自動リスト以外で、お客様に代わって送信される依頼を意味します。 インコグニ:約77.88ドル/年·自動ブローカー:420+(Unlimitedで3,000+)·カスタム削除:Unlimitedでの無制限カスタム削除リクエスト ·人間のエスカレーション:なし DeleteMe:年間129ドル・自動ブローカー:400+ ·カスタム引越し:560+ ソース;標準版で年間40件のカスタム削除 ·人間のエスカレーション:はい(コンシェルジュ) Optery:$39(コア)/ $249(Ultimate)/年 ·自動ブローカー:365–635(ティア依存)·カスタム削除:最大1,345サイト(Ultimate)·人間のエスカレーション:いいえ プライバシービー:年間~$96から・自動ブローカー:1,128+ ·カスタム削除:185,000+サイト ·人間のエスカレーション:部分的 オーラ:~年間$144 ·自動ブローカー:~140 ·カスタム削除:限定的・人為的エスカレーション:なし EasyOptOuts:年間$19.99 ·自動ブローカー:200+ ハイインパクト ·カスタム削除:なし ·人間のエスカレーション:なし Onerep: ~$90–$99.96/年金·自動ブローカー:300+ People-検索 ·カスタム削除:なし ·人間のエスカレーション:なし カナリー:年間約120ドルから・自動ブローカー:下位ティアでは手動・カスタム削除:なし ·人為的エスカレーション:なし IDX完了:年間$355.32・自動化されたブローカー:100以上 ・カスタム削除:なし ・人的エスカレーション:部分的 ReputationDefender:見積もりベース · 自動ブローカー:100以上のソース · カスタム削除:管理対象 · 人間によるエスカレーション:あり(管理対象) 価格が買うもの: Incogniの低いエントリー価格は純粋なオートメーションとデロイト監査による効率性を反映しています。DeleteMeのプレミアム料金は、人件費を反映したものです。Opteryの透明性は、その中間に位置する。EasyOptOutsは削除ループ以外のすべてを削除しますが、それでも削除率の面ではいくつかの有料ツールを上回ります。データブローカーがプロフィールを再掲載する場合、安価なサービスでは多くの場合、ユーザーがそれに気づいて手動で再提出する必要がありますが、プレミアムサービスではそのプロセスが自動化されています。それが、ダッシュボードに表示される削除リクエストの背後にある本当の違いです。 データ削除を超えて:個人情報保護の必須事項 ブローカーのデータベースから個人データを削除することで、情報漏洩のリスクを一つ減らすことはできますが、なりすまし、フィッシング、アカウント乗っ取りを防ぐことはできません。包括的な多層防御アプローチは、駆除と以下の対策を組み合わせたものです。 個人情報盗難防止機能 ― 新規口座開設を監視し、不審な活動を検知すると警告を発します。アラートだけでなく、復旧サポートを含む個人情報盗難防止サービスを探しましょう。 個人情報保護 ― 合成IDやクレジットカードヘッダーの不正使用に対する個人情報保護を含む、より広範なカテゴリー。 信用情報モニタリング ― 主要3つの信用情報機関における変更を追跡します。クレジットモニタリングとクレジットレポーティングレビューを組み合わせて、許可していない照会を見つけることができます。 パスワードマネージャー — 専用のパスワードマネージャーは、オンライン攻撃の最も一般的な侵入口である再利用認証情報を排除します。 ウイルス対策ソフト — 最新のウイルス対策ソフトは、認証情報やセッションクッキーを収集するインフォスティーラーをブロックします。 ダークウェブスキャン ― ダークウェブスキャンは、データ漏洩後に認証情報や個人情報が流出した場合に警告を発します。国立公共データの漏洩は、漏洩後の監視がいかに重要かを示す最も明確な最近の例です。 個人情報盗難保険 ― 個人情報盗難保険は復旧費用を補償しますが、盗難そのものを防ぐものではありません。 デジタルセキュリティ — 多層的なデジタルセキュリティ構成には、MFA、デバイスアップデート、信頼できるセキュリティサービスが含まれます。あなたのオンラインプライバシーはこれらすべてが連携して働くことに依存しています。 単一のセキュリティソリューションがすべてをカバーするものはありません。最も強力なスタックは、削除サービスとパスワードマネージャー、ウイルス対策ソフト、個人情報盗難防止を組み合わせており、個人データを一度のクリーンアップではなく継続的に監視すべきものとして扱います。2回目のデータ漏洩は、数か月にわたるクリーンアップを一つの通知で元に戻すこともあります。 DIY方式:オプトアウト申請、ガイド、およびその限界 手作業による除去は予算ゼロでも可能ですが、規律が求められます。ほとんどのデータブローカーはオプトアウトページを提供しており、多くは具体的な手順を説明するオプトアウトガイドを公開している。問題は規模です。データブローカーサイトが公開記録を再収集するため、数十件のオプトアウト要求を提出し、確認を追跡し、数か月ごとにこのプロセスを繰り返す必要があります。 自分の露出度を見つけましょう。主要な人物検索サイトやデータブローカーサイトで、名前、都市、旧住所を検索してください。URLを保存しておいてください。後で必要になります。 オプトアウトのリクエストは1件ずつ提出してください。各サイトオーナーによってワークフローは異なり、メールアドレスの認証が必要な場合もあれば、身分証明書のアップロードが必要な場合もある。 確認メールには一時的なメールアドレスを使用してください。これにより、削除依頼の処理中に、メインの受信トレイがブローカーのマーケティングリストから除外されます。 すべてを記録しておきましょう。確認メールやスクリーンショットは保存してください;それらがなければ、削除申請が提出されたことを証明できません。 四半期ごとに繰り返す。同じデータブローカーサイトや検索結果を再確認してください。新しいブローカーサイトが絶えず出現し、古いサイトも再掲載される。 大手証券会社には優れた無料のオプトアウトガイドが用意されており、まずはそれらを参考にすると良いでしょう。しかし、DIYは数百のデータブローカーサイトにスケールできず、時間経過で追跡できる曝露レポートも生成しません。ほとんどの人にとって、有料サービスを利用する方が、カスタム削除やカスタム削除依頼を手動で管理するのに必要な時間よりも安価です。ご自身で設定される場合は、弊社のオプトアウトガイドをチェックリストとして活用し、繰り返しの実施予定をカレンダーに記録してください。 データ削除サービスは本当に効果があるのか? はい、ただし、そのサービスに定期的な再除去が含まれている場合、そして、一度限りの除去率ではなく、耐久性に基づいて評価する場合に限ります。独立したテストでは、サービスによって方法論やブローカーパネルが異なるものの、削除される物件の割合は概ね27%から70%と、大きなばらつきがあることが一貫して示されている。OpteryとEasyOptOutsは、それぞれ約68%と65%で、比較対象ベンチマークをリードしました。一方、DeleteMeは、同じ2024年のコンシューマー・レポートの調査で約27%と中位に位置しました。 より重要な数字は、90日後に除去された状態が維持されているかどうかである。データブローカーは、45日から90日の周期で公開記録を再収集し、プロフィールを再掲載する。初月に68%を削除したものの、再掲載後に再提出を怠るサービスは、50%を削除し、それを継続的に抑制するサービスよりも、実質的な保護効果は低い。そのため、当社のランキングでは、90日目の持続性を60日目の除去率と同等に重視しており、Incogniの自動化された60~90日ごとの再提出サイクルは、マーケティング上の付加情報ではなく、真の運用上の利点となっています。同じ論理はあらゆる個人データのクリーンアップにも当てはまります。一度限りの削除は有効な戦略ではありません。 データ削除サービスの費用はいくらですか?+ 最終評決 今回ランキング対象としたサービスの年間料金は、個人向けプランの場合、年間19.99ドルから355.32ドルまで幅があります。プレミアムサービスの年間料金の中央値は96ドルから144ドル程度です。月額料金は、ほぼ例外なく年間実質料金の約2倍になります。例えば、Incogniのスタンダードプランは、月額約15.98ドルであるのに対し、年間プランでは月額6.49ドルです。ファミリプランは特にDeleteMeやAuraを使えば、1人あたりのコストを大幅に削減でき、ほとんどのプロバイダは4〜5人の大人をカバーするファミリプランを提供しています。削除に数週間かかり、再掲載が継続的に行われるカテゴリーでは、1か月のサービスはほとんど意味がなく、ファミリプランは通常、世帯を守る最も安価な方法です。 最終順位: Incogni ― 完全自動化された削除サービス、デロイト監査による透明性、そして最低価格のプレミアムプランでナンバーワン。手を離してデジタルフットプリントのクリーンアップを求めるほとんどのユーザーに最適です。 DeleteMe — プレミアム/エリート向けランキング第2位。人間による検証済みの除去、複雑な露出処理、カスタム除去、および付属のマスキングツールキットが必要な場合は、こちらを選択してください。 Optery ― 削除証明と予算レベルが最も明確に検証されており、明確な露出レポートも提供されます。 プライバシー Bee — マイナーサイトにおける個人データに関する最も広範な公開されたブローカー報道。 Aura — 特にファミリープラン向けのオールインワンセキュリティバンドルでおすすめです。 EasyOptOuts ― 最も低コストで、設定後は放置できるオプションです。 Onerep ― 最もシンプルで使いやすいスタンドアロン型削除エンジン。 Kanary — 個人情報暴露やソーシャルメディア露出に最適です。 IDX Complete — クレジットモニタリングとパスワードマネージャーを備えた最高の完全な身分盗難対策スイート。 ReputationDefender ― 著名人や評判管理に最適なツール。 結論として、あなたのデータ痕跡を100%削除できるサービスはありません。もしそうでないと謳うランキングがあれば、それはテストではなく販売戦略です。上位3人を分けるのはランディングページのブローカー数ではなく、データブローカーが再リストした際にサービスが再提出するかどうか、そしてオートメーションが失敗した際に人間が介入できるかどうかです。Incogniは、1ドルあたりの自動化された耐久性において優位に立っている。DeleteMeは人間的な側面で勝っている。リスクの複雑さに合わせてサービスを選択し、一度限りの復旧ではなく、継続的な保護のための予算を確保しましょう。最高のデータ削除サービスとは、最初の暴露レポート後も継続的に機能するサービスです。なぜなら、あなたのデジタルフットプリント、個人データ、そしてそれらをホストするデータブローカーサイトは常に変化し続けるからです。削除を身元保護、パスワードマネージャー、クレジット監視と組み合わせ、データ削除機能を一時的な解決策ではなく、より広範なデジタルセキュリティ戦略の一層として扱うべきです。
View full article
Best Data Removal Services 2026: 90-Day Test & Expert Analysis (November 2026) Our Top Picks: We ran the test the way a real user would: paid subscriptions, seeded identities, and 30/60/90-day re-checks against the same broker panel. The outcome is a two-horse race at the top of the market — and a clear reminder that data removal services only work when they keep re-submitting after your personal data reappears. Incogni takes #1 for fully automated removals and the strongest value in the premium tier — roughly $6.49 per month on an annual plan (~$77.88 billed once a year). Its automated re-submission cycle and Deloitte-audited reporting make it the default pick for anyone who wants the problem handled without ongoing effort. Start with INCOGNI DeleteMe takes #2 on the strength of its human-led concierge model and the widest broker footprint we measured — 750+ brokers under active management. For complex, contested, or repeatedly re-listed exposure, that human layer is what separates “requested” from “removed.” Try DeleteMe → What both share — and what any 2026 shortlist must demand — is continuous re-monitoring: automated re-checks and re-submissions every time a broker re-lists your data. Without it, a removal is only a temporary delisting, and your digital footprint quietly rebuilds itself. Quick Comparison Table: Best Data Removal Services 2026 Incogni: automation & value · ~$6.49/month ($77.88/yr) · full automation · 420+ brokers (3,000+ on Unlimited) · ★★★★★ 5.0 DeleteMe: human-led removal · ~$10.75/month ($129/yr) · hybrid · 400+ auto / 560+ custom · ★★★★★ 4.8 Optery: verified proof of removal · ~$3.25/month (from $39/yr) · full automation · 365–635 brokers (tier-dependent) · ★★★★½ 4.5 Privacy Bee: maximum broker coverage · ~$8.00/month (from $96/yr) · full automation · 1,128+ brokers · ★★★★ 4.0 Aura: all-in-one security bundle · ~$12.00/month ($144/yr) · full automation · ~140 brokers · ★★★★ 4.0 EasyOptOuts: budget set-and-forget · ~$1.67/month ($19.99/yr) · full automation · 200+ high-impact sites · ★★★★ 4.0 How We Tested and Ranked the Best Data Removal Services We built one controlled test identity — a consistent name, date of birth, two prior addresses, one phone number, and one email — and seeded it across a fixed panel of high-traffic people-finder sites and data broker sites including Whitepages, Spokeo, BeenVerified, Intelius, and MyLife. After subscribing to each service with our own money, we re-checked the identical baseline brokers at three checkpoints. Day 30: early removal signal. Why it matters: fast services show real removals, slow ones show “in progress” Day 60: stabilized verified removal rate. Why it matters: most legitimate opt-outs clear within 4–6 weeks Day 90: durability and reappearance. Why it matters: data brokers re-list, so we count what stayed gone We weighted four variables that actually change outcomes: Removal durability — how much stayed gone at Day 90, not just Day 30 Custom-removal capacity — whether a human can escalate stubborn or contested brokers Report transparency — screenshots, activity logs, and audited claims Cost per person per year — the real price after annual billing and household discounts The 2024 Consumer Reports field test remains the external benchmark: across paid services, only about 35% of listings were removed within four months on average. That number is the reality check every ranking below has to survive. What Data Brokers Actually Collect — and Why It Matters Data brokers do not sell one tidy record. They assemble a composite identity from public records, loyalty programs, app permissions, and scraped web pages, then resell it to marketers, background-check services, and — in the wrong hands — criminals. Most data brokers specialize in people-search, marketing segmentation, risk scoring, or identity verification, but the output is the same: a persistent profile you never consented to. A typical Personal Information package includes Home addresses, Email addresses, phone numbers, birthdates, relatives, property records, and Photos and videos pulled from social profiles. Add Sensitive data such as inferred health interests, financial signals, and location history, and you have what privacy professionals call Personally Identifiable Information in its most commercially useful form. This is why a single search engine query can surface a personal profile that you never created. Google Search Results and other Search Engines index pages from data broker websites, broker sites, and people-finder sites — including shadowy and unseen sites that never appear in mainstream search results. The more personal profiles exist, the easier it is to cross-reference them into a full personal data dossier. Our test identity appeared on more than 40 data broker sites within two weeks of seeding. Some were obvious people-search pages; others were data broker websites buried three pages deep in search results. That gap between visible and invisible exposure is exactly why DIY cleanup fails without an Exposure Report and ongoing monitoring. 1. Incogni — Best Overall for Automated Removal & Value Best for: Hands-off users who want wide broker reach and recurring automation at the lowest premium price. Incogni is the automation-first leader and the strongest value in the premium tier. The Standard annual plan costs ~$77.88 per year (about $6.49/month), covering 420+ data brokers with fully automated removal requests. The Unlimited plan ($179.88/year) adds unlimited custom removal requests and expands coverage to over 3,000 sources. What sets Incogni apart is the transparency layer. Its dashboard shows per-broker resolution times and activity history, and the company’s claims are backed by a Deloitte assurance report — a third-party check that most competitors still cannot match. Automated re-submission runs on a 60-to-90-day cycle, directly countering the re-exposure lifecycle that makes one-time removals obsolete. For personal data that keeps coming back, that cycle is the product. Pros: Lowest entry price among top-tier automated services (~$77.88/year) 420+ automated brokers; 3,000+ sources on Unlimited Deloitte-audited removal claims Continuous re-scanning and automatic re-submission Unlimited custom removal requests on the Unlimited plan Cons: Standard plan allows only one name per profile No human concierge tier for complex escalations No screenshot-level proof of each individual removal Verdict: For the majority of users who want set-and-forget removal at the lowest premium price, Incogni is the rational #1 on value and automation depth. 2. DeleteMe — Best Premium Data Removal Service (Human-Led) Best for: Complex exposure, multiple addresses, and anyone who wants human-verified removals. DeleteMe is the elite, concierge-grade option and earns the #2 slot for one reason: when automated opt-outs stall, a human caseworker steps in. The Standard plan starts at $129 per year for one person ($10.75/month), with family plans at two-person ($229/year) and four-person ($329/year) tiers. Automated removals cover over 400 sources, while custom removals reach over 560 sources — including stubborn data brokers that routinely ignore template removal requests. DeleteMe also bundles a proactive privacy toolkit at no extra charge: email masking, phone-number masking, and credit-card masking — features no other service we tested includes in the base plan. The dashboard shows how many sources were reviewed and how many removals succeeded. For personal data spread across old addresses and maiden names, the human layer is the difference between a request and a result. Pros: Human-led escalation for stubborn or complex broker cases 400+ automated sources / 560+ custom-removal sources Email, phone, and credit-card masking included Family plans reduce per-person cost Fast customer support and an active user community Cons: Premium price: $129/year for one person No screenshot-level before/after proof in the dashboard Standard plan limits custom removals to 40 per year Verdict: If your exposure is messy — a common name, a history of moves, or data on obscure regional directories — DeleteMe’s human layer is the difference between “requested” and “removed.” 3–10. Other Top Data Removal Services Compared 3. Optery — Best for Verified Proof of Removal Optery ranks #3 for verifiability. Its dashboard provides screenshot-based proof of removals — before-and-after evidence that most competitors still do not offer. Pricing starts at $39 per year for the Core tier, with a free self-service scan covering up to 40 broker exposures. Every account includes an Exposure Report that lists exactly which profiles were found before removal begins. In independent testing, Optery reached approximately 68% removal — the highest score in controlled benchmarks. The trade-off: its concierge depth does not yet match DeleteMe, and personal data on niche regional brokers can take longer to clear. 4. Privacy Bee — Best for Maximum Broker Coverage Privacy Bee holds PCMag’s first perfect 5-star rating in the data removal category and covers 1,128 data brokers, with support for removals from over 185,000 custom sites. Pricing starts around $96 per year, with higher tiers for deeper monitoring. This is the pick for users who want the broadest published broker list and granular control over removal categories. Independent testing places its removal rate around 45% — respectable, but trailing the leaders on visible results. For personal data on obscure broker sites, the breadth is genuinely useful. 5. Aura — Best All-in-One Security Bundle Aura bundles data removal with antivirus, VPN, and identity-theft insurance into one subscription, starting around $144 per year (~$12/month). Automated removal covers roughly 140 brokers — narrower than the specialists — but the bundle makes sense for families that want a single security stack rather than three separate subscriptions. If you want one security solution for the whole household, Aura’s family plans are the main draw. The removal engine handles common personal data exposures well, but it is not a substitute for a dedicated broker-removal specialist. 6. EasyOptOuts — Best Budget Option At $19.99 per year, EasyOptOuts is the lowest-priced service we tested. It reached approximately 65% removal in controlled benchmarks, second only to Optery and ahead of several premium tools. It is set-and-forget by design: no custom removals, a minimal dashboard, and fewer security reports. For low-risk users on a tight budget, it is the rational entry point for personal data cleanup. 7. Onerep — Best No-Frills Standalone Removal Onerep is the removal engine behind several bundled products, sold direct at $90–$99.96 per year ($7.49–$8.33/month). It clears the common people-search sites reliably and is fast to set up. Coverage is middle of the pack, but it works well as a standalone scanner-plus-remover for users who do not need the extra features of the top-tier services. 8. Kanary — Best for Doxxing and Social Media Exposure Kanary is a niche service that can help monitor social media for private information and tackle doxxing in some instances — a capability most competitors lack. Pricing runs $9.99–$50 per month, with a free plan available. The trade-off: only the most expensive tier is fully automated, and the free version is mobile-only. 9. IDX Complete — Best Full Identity-Theft Suite IDX Complete is a full security and privacy suite that bundles data removal with identity-theft monitoring, credit monitoring across three bureaus, a password manager, a VPN, and dark web monitoring. At $355.32 per year (~$29.61/month on annual billing), it is the most expensive option on this list, but it replaces several separate subscriptions. Data removal covers 100+ brokers — narrower than the specialists, but the surrounding protection is unmatched. 10. ReputationDefender by Norton — Best for High-Profile Individuals ReputationDefender is built for professionals and high-profile individuals who need constant data-leak monitoring and reputation protection. Pricing is quote-based and not publicly published, with third-party estimates ranging from ~$99/year for basic broker removal to $25,000/year for top managed reputation tiers. It is not a budget option, but for executives and public figures, the managed reputation layer is the differentiator. Data Broker Removal Service Pricing: What You Actually Pay For The table below compares annual pricing, automated broker coverage, and the human-escalation layer — the three variables that actually change outcomes. Note that custom removals and custom removal requests are not the same thing: the former usually means manual escalation, the latter means a request submitted on your behalf outside the standard automated list. Incogni: ~$77.88/yr · automated brokers: 420+ (3,000+ on Unlimited) · custom removals: unlimited custom removal requests on Unlimited · human escalation: No DeleteMe: $129/yr · automated brokers: 400+ · custom removals: 560+ sources; 40 custom removals/year on Standard · human escalation: Yes (Concierge) Optery: $39 (Core) / $249 (Ultimate)/yr · automated brokers: 365–635 (tier-dependent) · custom removals: up to 1,345 sites (Ultimate) · human escalation: No Privacy Bee: from ~$96/yr · automated brokers: 1,128+ · custom removals: 185,000+ sites · human escalation: Partial Aura: ~$144/yr · automated brokers: ~140 · custom removals: limited · human escalation: No EasyOptOuts: $19.99/yr · automated brokers: 200+ high-impact · custom removals: No · human escalation: No Onerep: ~$90–$99.96/yr · automated brokers: 300+ people-search · custom removals: No · human escalation: No Kanary: from ~$120/yr · automated brokers: manual on lower tiers · custom removals: No · human escalation: No IDX Complete: $355.32/yr · automated brokers: 100+ · custom removals: No · human escalation: Partial ReputationDefender: quote-based · automated brokers: 100+ sources · custom removals: managed · human escalation: Yes (managed) What the price buys: Incogni’s lower entry price reflects pure automation and Deloitte-audited efficiency. DeleteMe’s premium reflects human labor. Optery’s transparency sits in the middle. EasyOptOuts strips everything except the removal loop — and still outperforms several premium tools on raw removal percentage. When data brokers re-list profiles, the cheaper services often require you to notice and re-submit manually; the premium services automate that loop. That is the real difference behind the removal requests you see in a dashboard. Beyond Data Removal: Identity Protection Essentials Removing personal data from broker databases closes one exposure vector, but it does not prevent identity theft, phishing, or account takeover. A complete defense-in-depth approach combines removal with the following controls: Identity theft protection — monitors new account openings and alerts you to suspicious activity. Look for identity theft protection that includes restoration support, not just alerts. Identity protection — a broader category that includes identity protection against synthetic identities and credit header misuse. Credit monitoring — tracks changes across the three major bureaus. Pair credit monitoring with Credit reporting reviews so you can spot inquiries you did not authorize. Password manager — a dedicated password manager eliminates reused credentials, which remain the most common entry point for online attacks. Antivirus software — modern antivirus software blocks infostealers that harvest credentials and session cookies. Dark web scanning — dark web scanning alerts you when credentials or Personal Information surface after a data breach. The National Public Data breach is the clearest recent example of why post-breach monitoring matters. Identity theft insurance — identity theft insurance covers recovery costs, but it does not prevent the theft itself. Digital security — a layered digital security setup includes MFA, device updates, and a reputable security service for monitoring. Your online privacy depends on all of these working together. No single security solution covers everything. The strongest stacks combine a removal service with a password manager, antivirus software, and identity theft protection — and they treat personal data as something that must be continuously monitored, not cleaned once. A second data breach can undo months of cleanup in a single notification. The DIY Route: Opt-Out Requests, Guides, and Their Limits Manual removal is possible on a zero budget, but it demands discipline. Most data brokers provide an opt-out page, and many publish opt-out guides that explain the exact steps. The problem is scale: you will file dozens of opt-out requests, track confirmations, and repeat the process every few months because data broker sites re-scrape public records. Find your exposure. Search your name, city, and old addresses on major people-finder sites and data broker sites. Save the URLs — you will need them again. File opt-out requests one by one. Each site owner has a different workflow; some require email verification, others require ID upload. Use a temporary email address for confirmations. This keeps your primary inbox out of broker marketing lists while you work through removal requests. Document everything. Save confirmation emails and screenshots; without them, you cannot prove a removal request was submitted. Repeat quarterly. Re-check the same data broker sites and search results. New broker sites appear constantly, and old ones re-list. There are excellent free opt-out guides for the largest brokers, and they are worth using as a starting point. But DIY does not scale to hundreds of data broker websites, and it does not generate an Exposure Report you can track over time. For most people, a paid service is cheaper than the hours required to maintain custom removals and custom removal requests manually. If you do go DIY, use our opt-out guides as a checklist and calendar the repeats. Do Data Removal Services Actually Work? Yes — but only if the service includes recurring re-removal, and only if you judge it on durability, not one-time percentage. Independent testing consistently shows a wide range: roughly 27% to 70% of listings removed across services, depending on methodology and broker panel. Optery and EasyOptOuts led controlled benchmarks at approximately 68% and 65% respectively; DeleteMe landed mid-pack in the same 2024 Consumer Reports study at around 27%. The more important number is what stays removed at 90 days. Data brokers re-scrape public records and re-list profiles on a 45-to-90-day cycle. A service that removes 68% in month one but fails to re-submit after re-listing delivers less real protection than a service that removes 50% and suppresses it continuously. That is why our ranking weights Day 90 durability as heavily as Day 60 removal rate — and why Incogni’s automated 60-to-90-day re-submission cycle is a genuine operational advantage, not a marketing footnote. The same logic applies to any personal data cleanup: one-time deletion is not a strategy. How Much Do Data Removal Services Cost? + Final Verdict Annual pricing across the services we ranked spans $19.99 to $355.32 per year for individual coverage. The median premium service sits near $96–$144 per year. Monthly billing is almost always roughly double the annual effective rate — Incogni’s Standard plan, for example, is roughly $15.98 month-to-month versus $6.49/month on the annual plan. Family plans can cut the per-person cost significantly, especially with DeleteMe and Aura, and most providers offer family plans that cover four to five adults. For a category where removal takes weeks and re-listing is continuous, a single month of service rarely makes sense — and family plans are usually the cheapest way to protect a household. Final ranking: Incogni — #1 for fully automated removal, Deloitte-audited transparency, and the lowest premium entry price. Best for most users who want a hands-off digital footprint cleanup. DeleteMe — #2 premium/elite pick. Choose it for human-verified removals, complex exposure, custom removals, and the bundled masking toolkit. Optery — best verified proof of removal and budget tiers, with a clear Exposure Report. Privacy Bee — broadest published broker coverage for personal data on obscure sites. Aura — best all-in-one security bundle, especially for family plans. EasyOptOuts — best low-cost, set-and-forget option. Onerep — best no-frills standalone removal engine. Kanary — best for doxxing and social media exposure. IDX Complete — best full identity-theft suite with credit monitoring and a password manager. ReputationDefender — best for high-profile individuals and managed reputation. The bottom line: no service deletes 100% of your footprint, and any ranking that promises otherwise is selling, not testing. What separates the top three is not the broker count on the landing page — it is whether the service re-submits when data brokers re-list, and whether a human can intervene when automation fails. Incogni wins on automated durability per dollar. DeleteMe wins on the human layer. Match the service to the complexity of your exposure, and budget for ongoing protection, not a one-time cleanup. The best data removal services are the ones that keep working after the first Exposure Report — because your digital footprint, your personal data, and the data broker sites that host them will keep changing. Pair removal with identity protection, a password manager, and credit monitoring, and treat data removal capabilities as one layer of a broader digital security strategy rather than a one-time fix.
View full article
SC16IS752 Demo Board (OM6273) reference schematic design Hi NXP support team, May I have the SC16IS752 Demo Board (OM6273) reference schematic design? Br, Jimmy Hung
View full article
SC16IS752 デモボード(OM6273)参照回路図デザイン こんにちは、NXPサポートチームの皆さん、 SC16IS752デモボード(OM6273)の参考回路図デザインをいただけますか? Br、 ジミー・ハン
View full article
Wordle vs Scrabble:哪款文字游戏更适合脑力训练? Wordle 和 Scrabble 是世界上最受欢迎的两款文字游戏。根据你想训练的技能以及你能投入多少时间玩游戏,Wordle 和 Scrabble 都可以用来训练你的大脑。 游戏玩法 Wordle每天都会让你猜一个5个字母的单词。你有 6 次机会猜出 Wordle 中的单词是什么。如果字母正确,则将其涂成绿色;如果字母在 Wordle 单词中但位置不正确,则将其涂成黄色;如果字母不正确,则将其涂成灰色。每个拼图只需要大约 2-5 分钟。 拼字游戏需要你将字母方块放置在板上,组成相互连接的单词。该游戏可供 2-4 名玩家进行。每个字母都值一定的分数,但也有奖励方格可以增加你的分数。一局普通游戏可能需要 45 分钟到 1 小时以上,并且需要掌握短词、计分和板块管理方面的知识。 使用的认知技能 工作记忆 这两款游戏都需要操作记忆力才能玩。Wordle 需要运用工作记忆,因为你需要记住哪些字母已被排除,哪些字母在正确的位置,以及单词可能的形状是什么。而拼字游戏则要求你记住你的字母牌、仍然可用的高级方格、对手的字母牌倾向以及你自己的 7 个字母牌架。因此,拼字游戏需要更多的工作记忆。 演绎推理 Wordle 需要你运用演绎推理。你的每一个猜测都是一个假设,而彩色的回复就是你的数据。然后,你用排除法来找出答案。这与科学方法非常相似。而拼字游戏则不需要太多的演绎推理,因为你需要知道一些生僻的单词才能获胜。 词汇 在竞技拼字游戏中,玩家会学到成千上万个生僻词。他们不需要知道这些词的意思,只需要知道这些词是可以用来得分的有效词语即可。而 Wordle 使用的是常用词汇,因此您可以熟悉高频词汇。如果你想提高词汇量,Wordle 会更实用。如果你想提高词汇量,拼字游戏能提供更广泛的词汇选择。 战略思维 玩拼字游戏需要你提前思考。优秀的玩家可能会使用低分单词来阻止对手获得三倍单词方格。或者为下一轮设置一个高分词。战略思维是一种高层次的认知技能。Wordle 不需要策略性思考,因为所有事情都在 6 次猜测之内发生。 时间 Wordle 是一款每日游戏,每次游戏时间不到 5 分钟。而拼字游戏则需要更多的时间,还需要有人愿意和你对战。如果你很忙,Wordle 更容易融入你的日常生活中。而如果你想要一款更深入的游戏,拼字游戏(Scrabble)会提供更多参与感。 社会 Wordle 利用表情符号网格创造了一种全球性的日常习惯。数以百万计的人以同样的方式发布他们的结果,却不透露答案。而拼字游戏则更具竞争性,需要与他人一起玩。 哪种方法最适合训练大脑? 两款游戏客观上没有孰优孰劣之分。wordleunlimited.dev可以帮助您进行演绎推理、约束满足和工作记忆。而玩拼字游戏则有助于提高词汇量、策略思维和注意力。大多数人会发现同时玩这两款游戏更有益。每天玩 Wordle,每周玩一次 Scrabble。
View full article
2026 年最佳数据清除服务:90 天测试及专家分析(2026 年 11 月) 我们的精选推荐: 我们以真实用户的方式进行了测试:付费订阅、种子身份,以及针对同一经纪商面板进行 30/60/90 天的复查。最终结果是市场顶端出现两强争霸的局面——这也清楚地提醒我们,数据删除服务只有在你的个人数据再次出现后不断重新提交才能真正有效。 Incogni 在全自动删除方面排名第一,并且在高级套餐中性价比最高——年付计划每月约 6.49 美元(每年一次计费约 77.88 美元)。其自动重新提交流程和德勤审计的报告使其成为任何希望无需持续努力即可解决问题的人的首选。 从 INCOGNI 开始 DeleteMe凭借其以人为本的礼宾服务模式和我们衡量过的最广泛的经纪人覆盖范围(750多名经纪人处于积极管理之下)位列第二。对于复杂、有争议或反复重新列出的曝光,正是人为层将“请求”与“移除”区分开来。 试试删除我 → 两者的共同点——也是任何 2026 年入围名单都必须要求的——是持续的重新监控:每次经纪商重新列出您的数据时,都要进行自动重新检查和重新提交。如果没有它,删除只是暂时的除名,你的数字足迹会悄悄地重建。 快速对比表:2026 年最佳数据清除服务 Incogni :自动化与价值 · 约 6.49 美元/月(77.88 美元/年)· 全自动 · 420+ 家经纪商(无限版超过 3000 家) · ★★★★★ 5.0 DeleteMe :人工删除 · 约 10.75 美元/月(每年 129 美元)· 混合动力 · 400 多款自动挡车型 / 560 多款定制车型 · ★★★★★ 4.8 Optery :已验证的移除证明 · 约 3.25 美元/月(39 美元/年起) · 完全自动化 · 365-635 位经纪人(取决于级别) · ★★★★½ 4.5 Privacy Bee :覆盖范围最广,经纪人覆盖率最高 · 每月约 8 美元(原价每年 96 美元) · 完全自动化 · 覆盖 1128+ 家经纪人 · ★★★★ 4.0 Aura :一体化网络安全套装 · 约 12 美元/月(每年 144 美元)· 全自动化 · 约 140 位经纪人 · ★★★★ 4.0 EasyOptOuts :预算设置后即可轻松管理 · 每月约 1.67 美元(每年 19.99 美元)· 全自动化 · 200 多个高影响力网站 · ★★★★ 4.0 我们如何测试并排名最佳数据删除服务 我们创建了一个受控测试身份——一个一致的姓名、出生日期、两个以前的地址、一个电话号码和一个电子邮件——并将其部署到一组固定的高流量人员查找网站和数据经纪网站,包括 Whitepages、Spokeo、BeenVerified、Intelius 和 MyLife。我们用自己的钱订阅了每项服务后,在三个检查点对相同的基准经纪商进行了重新检查。 第 30 天:提前移除信号。重要性:快速的服务显示实际删除操作,慢速的服务显示“正在进行中”。 第 60 天:清除率稳定且已验证。重要性:大多数合法的退出选项会在 4-6 周内生效 第 90 天:耐久性和再外观。重要性:数据经纪商会重新上架数据,所以我们需要统计哪些数据已经消失。 我们对四个实际影响结果的变量进行了加权: 清除持久性——第 90 天(而不仅仅是第 30 天)还有多少清除剂残留 海关移除能力——人能否应对顽固或有争议的中间商 报告透明度——屏幕截图、活动日志和经审计的索赔 每人每年的费用——扣除年度账单和家庭折扣后的实际价格 2024 年《消费者报告》实地测试仍然是外部基准:在付费服务中,平均只有约 35% 的列表在四个月内被删除。这个数字是所有排名低于它的排名都必须面对的现实检验。 数据经纪商实际收集哪些数据——以及为什么这很重要 数据经纪人出售的并非一份完整的记录。他们利用公共记录、会员计划、应用程序权限和抓取的网页信息拼凑出一个综合身份,然后将其转售给营销人员、背景调查服务机构,以及——如果落入不法分子手中——犯罪分子。大多数数据经纪商专注于人员搜索、市场细分、风险评分或身份验证,但最终结果都是一样的:一个你从未同意过的永久我的。 典型的个人信息软件包包括家庭住址、电子邮件地址、电话号码、出生日期、亲属信息、房产记录以及从我的社交媒体中提取的照片和视频。再加上推断的健康兴趣、财务信号和位置历史记录等敏感数据,你就得到了隐私专家所说的最具商业价值的个人身份信息。 这就是为什么一次搜索引擎查询就可能找到你从未创建过的我的。Google 搜索结果和其他搜索引擎会索引来自数据经纪网站、经纪网站和人员查找网站的页面——包括那些永远不会出现在主流搜索结果中的隐秘网站。个人资料越多,就越容易将它们交叉引用到完整的个人数据档案中。 我们的测试身份在投放种子数据后的两周内就出现在了 40 多个数据经纪网站上。有些是显而易见的人员搜索页面;另一些是数据经纪网站,隐藏在搜索结果的三页之后。可见暴露和不可见暴露之间的差距正是为什么如果没有暴露报告和持续监测,DIY 清理工作会失败的原因。 1. Incogni — 自动化删除功能最佳,性价比最高 最适合:希望以最低溢价获得广泛经纪商覆盖范围和定期自动化服务的无需人工干预的用户。 Incogni 是自动化优先领域的领导者,也是高级版产品中最具价值的产品。标准年度计划每年费用约为 77.88 美元(约 6.49 美元/月),涵盖 420 多个数据经纪商,并提供全自动删除请求。无限流量套餐(179.88美元/年)增加了无限量的自定义删除请求,并将覆盖范围扩大到 3000 多个来源。 Incogni 的独特之处在于其透明层。其仪表盘显示每个经纪人的解决时间和活动历史记录,并且该公司的说法得到了德勤鉴证报告的支持——这是大多数竞争对手仍然无法匹敌的第三方检查。自动重新提交以 60 至 90 天为周期运行,直接抵消了重新曝光的生命周期,使得一次性删除变得过时。对于不断返回的个人数据而言,这种循环就是最终产品。 优点: 顶级自动化服务中最低的入门价格(约 77.88 美元/年) 420+ 个自动化经纪商;3000+ 个无限量数据源 德勤审计的移除索赔 持续重新扫描和自动重新提交 无限套餐包含无限次自定义移除请求 缺点: 标准套餐每个个人资料仅允许一个姓名。 没有针对复杂升级问题的人工客服层级 没有截图级别的证据证明每次删除操作。 结论:对于大多数希望以最低溢价实现一劳永逸的删除功能的用户而言,Incogni 在价值和自动化深度方面是合理的首选。 2. DeleteMe — 最佳高级数据删除服务(人工服务) 最适合:涉及复杂情况、多个地址,以及任何希望进行人工验证移除的人员。 DeleteMe 是精英级、管家式的服务,位列第二,原因只有一个:当自动退出程序停滞不前时,会有人工客服介入。标准套餐起价为单人每年 129 美元(每月 10.75 美元),家庭套餐分为双人套餐(每年 229 美元)和四人套餐(每年 329 美元)。自动删除功能覆盖 400 多个来源,而自定义删除功能覆盖 560 多个来源——包括那些经常忽略模板删除请求的顽固数据经纪商。 DeleteMe 还捆绑了一套主动隐私工具包,无需额外付费:电子邮件掩码、电话号码掩码和信用卡掩码——我们测试过的其他服务在基本计划中都没有包含这些功能。仪表盘显示了审查了多少个来源以及成功删除了多少个来源。对于散落在旧地址和婚前姓名中的个人数据而言,人工层决定了请求与结果之间的区别。 优点: 针对棘手或复杂的经纪人案件,由人工主导的升级处理程序。 400 多个自动化来源 / 560 多个自定义删除来源 包含电子邮件、电话和信用卡信息掩码 家庭计划可降低人均费用 快速的客户支持和活跃的用户社区 缺点: 高级价格:每人每年 129 美元 控制面板中没有截图级别的修改前后对比证据。 标准套餐将定制搬家服务限制为每年 40 次。 结论:如果你的信息很混乱——例如常用名、搬家记录或不知名地区目录中的数据——DeleteMe 的人工审核层决定了你的信息是“已请求删除”还是“已删除”。 3–10。与其他顶级数据清除服务对比 3. Optery — 最适合提供已移除证明的验证服务 Optery在可验证性方面排名第3 。其控制面板提供基于屏幕截图的移除证明——移除前后对比证据,而大多数竞争对手仍然没有提供。核心套餐的定价从每年 39 美元起,包含一次免费的自助扫描,最多可扫描 40 个经纪商的风险敞口。每个账户都包含一份曝光报告,其中列出了在开始删除之前发现的所有我的。在独立测试中,Optery 的去除率达到了约 68%——这是受控基准测试中的最高分。权衡之下:其礼宾服务的深度还不及 DeleteMe,而且清除特定区域经纪商的个人数据可能需要更长时间。 4. Privacy Bee — 最大限度覆盖经纪人的最佳选择 Privacy Bee 在 PCMag 的数据删除类别中获得了第一个完美的 5 星评级,涵盖 1,128 个数据经纪商,支持从超过 185,000 个自定义网站删除数据。定价从每年 96 美元起,更高级别的套餐可提供更深入的监控。这是为那些想要最广泛的已发布经纪商列表和对移除类别进行精细控制的用户而选择的产品。独立测试显示其清除率约为 45%——虽然可观,但在可见效果方面落后于领先者。对于不知名经纪网站上的个人数据而言,其覆盖范围确实非常有用。 5. Aura——最佳一体化网络安全套装 Aura 将数据清除、防病毒、VPN 和身份盗窃保险捆绑到一个订阅中,起价约为每年 144 美元(约 12 美元/月)。自动移除服务涵盖大约 140 家经纪商——比专家的范围要窄——但对于想要单一网络安全方案而不是三个单独订阅的系列来说,这种捆绑方案是有意义的。如果您想要一套适用于全家的网络安全解决方案,Aura 的家庭套餐是主要吸引力。删除引擎可以很好地处理常见的个人数据泄露,但它不能替代专用的经纪人删除专家。 6. EasyOptOuts — 最佳预算选择 EasyOptOuts 的年费为 19.99 美元,是我们测试过的价格最低的服务。在受控基准测试中,其去除率达到了约 65%,仅次于 Optery,领先于几款高级工具。它的设计理念是“设置后即可忘记”:无需自定义删除,仪表板极简,网络安全报告也较少。对于预算紧张的低风险用户来说,这是个人数据清理的合理切入点。 7. Onerep — 最佳简易独立组网 (SA)移除工具 Onerep 是多个捆绑产品背后的删除引擎,这些产品直接销售,每年售价为 90 至 99.96 美元(每月 7.49 至 8.33 美元)。它能可靠地清除常用的人员搜索网站,而且设置速度很快。覆盖范围属于中等水平,但对于不需要顶级服务额外功能的用户来说,它作为一款独立组网 \(SA\)扫描器兼移除器来说效果很好。 8. Kanary——最适合人肉搜索和社交媒体曝光 Kanary 是一项小众服务,可以帮助监测社交媒体上的私人信息,并在某些情况下应对人肉搜索——这是大多数竞争对手所不具备的能力。定价为每月 9.99 美元至 50 美元,并提供免费套餐。权衡之下:只有最贵的版本是全自动的,而免费版本仅限移动设备使用。 9. IDX Complete — 最佳全功能身份盗窃防护套件 IDX Complete 是一款完整的网络安全和隐私套件,它将数据删除与身份盗窃监控、跨三个信用机构的信用监控、密码管理器、VPN 和暗网监控捆绑在一起。每年 355.32 美元(约合每月 29.61 美元)按年计费),它是列表中最贵的选项,但它可以取代几个单独的订阅。数据删除服务涵盖 100 多家经纪商——虽然比专业经纪商的范围要窄,但其提供的全方位保护是无与伦比的。 10. Norton 的 ReputationDefender — 最适合高知名度人士 ReputationDefender 专为需要持续监控数据泄露和保护声誉的专业人士和知名人士而设计。定价基于报价,不公开,第三方估价从基本经纪人移除服务的每年约 99 美元到顶级声誉管理服务的每年 25,000 美元不等。虽然这不是一个经济实惠的选择,但对于高管和公众人物来说,声誉管理层才是真正的差异化优势。 数据经纪商移除服务定价:您实际需要支付的费用 下表比较了年度定价、自动经纪人覆盖范围和人工升级层——这三个变量实际上会改变结果。请注意,自定义移除和自定义移除请求并不相同:前者通常意味着手动升级,后者意味着在标准自动列表之外代表您提交的请求。 Incogni:约 77.88 美元/年· 自动代理:420+(无限版超过 3000 个)· 自定义移除:无限版可提交无限次自定义移除请求· 人工升级:否 DeleteMe:129 美元/年 · 自动经纪人:400 多个 · 自定义删除:560 多个来源;标准版每年 40 次自定义删除 · 人工升级:有(礼宾服务) Optery:39 美元(核心版)/ 249 美元(旗舰版)/ 年 · 自动代理:365-635 个(取决于套餐) · 自定义移除:最多 1,345 个站点(旗舰版) · 人工升级:无 Privacy Bee:每年约 96 美元起 · 自动代理:1128 个以上 · 自定义删除:超过 185000 个网站 · 人工升级:部分 Aura:约 144 美元/年 · 自动经纪人:约 140 个 · 自定义移除:有限 · 人工升级:否 轻松选择退出:19.99 美元/年 · 自动代理:200 多个高效代理 · 自定义移除:否 · 人工升级:否 单次执行:约 90-99.96 美元/年· 自动化经纪人:搜索超过 300 人 · 自定义移除:否 · 人工升级:否 Kanary:约 120 美元/年起 · 自动经纪人:低级别需人工操作 · 自定义移除:否 · 人工升级:否 IDX Complete:每年 355.32 美元· 自动代理:100+ · 自定义移除:否 · 人工升级:部分 声誉卫士:基于报价 · 自动化代理:100 多个来源 · 自定义移除:已管理 · 人工升级:是(已管理) 价格体现了什么: Incogni 较低的入门价格反映了其完全自动化和经德勤审计的效率。DeleteMe 的高级收费体现了人工成本。Optery的透明度处于中间位置。EasyOptOuts 会移除除移除循环之外的所有内容,并且在原始移除率方面仍然优于几个高级工具。当数据经纪商重新发布个人资料时,价格较低的服务通常需要您手动注意到并重新提交;而高级服务则会自动执行此循环。这就是你在控制面板中看到的移除请求背后的真正区别。 超越数据删除:身份保护要点 从经纪商数据库中删除个人数据可以消除一个风险渠道,但并不能阻止身份盗窃、网络钓鱼或账户盗用。完整的纵深防御策略将清除行动与以下控制措施相结合: 身份盗窃保护——监测新账户的开立情况,并在发现可疑活动时发出警报。寻找包含恢复支持而不仅仅是警报的身份盗窃保护措施。 身份保护——一个更广泛的类别,包括防止合成身份和信用卡抬头滥用的身份保护。 信用监控——跟踪三大信用机构的信用变化。将信用监控与信用报告审查结合起来,这样您就可以发现未经您授权的查询。 密码管理器——专用的密码管理器可以消除重复使用的凭据,而重复使用的凭据仍然是网络攻击最常见的入口点。 现代防病毒软件可以阻止窃取凭据和会话 cookie 的信息窃取程序。 暗网扫描——暗网扫描会在数据泄露后,当凭证或个人信息出现时发出警报。国家公共数据泄露事件是近期最清楚地说明泄露后监测为何至关重要的例子。 身份盗窃保险——身份盗窃保险涵盖追回费用,但并不能阻止盗窃本身。 数字网络安全——多层数字网络安全设置包括多因素身份验证 (MFA)、设备更新和信誉良好的网络安全服务进行监控。您的在线隐私取决于所有这些因素的协同作用。 没有哪一种网络安全解决方案能够涵盖所有情况。最强大的安全解决方案将删除服务与密码管理器、防病毒软件和身份盗窃保护相结合——并且他们将个人数据视为必须持续监测的内容,而不是一次性清理的内容。第二次数据泄露事件可能只需一次通知就使数月的清理工作付诸东流。 DIY途径:退出请求、指南及其局限性 即使预算为零,也可以手动清除,但这需要极大的自律性。大多数数据经纪商都提供退出页面,许多公司还发布退出指南,解释具体的退出步骤。问题在于规模:您需要提交数十份退出请求,跟踪确认情况,并且每隔几个月就要重复此过程,因为数据经纪网站会重新抓取公共记录。 找到你的曝光机会。在主要寻人网站和数据经纪网站上搜索您的姓名、城市和旧地址。保存这些网址——你以后还会用到它们。 逐个提交退出请求。每个网站所有者的工作流程都不同;有些需要电子邮件验证,有些需要上传身份证件。 使用临时邮箱地址进行确认。这样可以防止您的主收件箱被经纪人营销名单收录,同时您可以处理移除请求。 把所有事情都记录下来。请保存确认邮件和屏幕截图;否则,您将无法证明已提交删除请求。 每季度重复一次。再次查看相同的数据经纪网站和搜索结果。新的经纪商网站层出不穷,旧的经纪商网站也会重新上线。 针对大型经纪商,有一些非常优秀的免费退出指南,值得作为入门参考。但是 DIY 无法扩展到数百个数据经纪网站,也无法生成您可以随时间跟踪的风险敞口报告。对于大多数人来说,付费服务比手动维护自定义删除和自定义删除请求所需的时间更便宜。如果你选择自行操作,请使用我们的退出指南作为清单,并将重复事项安排在日历上。 数据删除服务真的有效吗? 是的——但前提是该服务包含定期重新清除,并且你评判的标准是耐用性,而不是一次性百分比。独立测试始终显示范围很广:根据方法和经纪人小组的不同,各个服务中大约有 27% 到 70% 的房源被删除。Optery 和 EasyOptOuts 在受控基准测试中分别以约 68% 和 65% 的成绩领先;DeleteMe 在同一项 2024 年消费者报告研究中排名中游,成绩约为 27%。 更重要的数字是90天后哪些物质仍然被清除。数据经纪商每隔 45 到 90 天重新抓取公共记录并重新发布我的。一项服务如果在第一个月内移除 68% 的垃圾邮件,但在重新上架后未能重新提交,那么它提供的实际保护不如一项移除 50% 的垃圾邮件并持续抑制其传播的服务。这就是为什么我们的排名将第 90 天的持久性与第 60 天的移除率同等重视——以及为什么 Incogni 的 60 至 90 天自动重新提交周期是一个真正的运营优势,而不是一个营销脚注。同样的道理也适用于任何个人数据清理:一次性删除并非长久之计。 数据删除服务费用是多少?+ 最终判决 我们排名的各项服务的年度定价范围为每年 19.99 美元至 355.32 美元(个人保险)。高级服务的年均价格约为 96 至 144 美元。每月账单金额几乎总是年度实际费率的两倍左右——例如,Incogni 的标准计划每月大约 15.98 美元,而年度计划每月 6.49 美元。家庭套餐可以大幅降低人均费用,尤其是 DeleteMe 和 Aura 的套餐,而且大多数供应商提供的家庭套餐可覆盖四到五名成年人。对于移除需要数周时间且重新上架需要持续进行的类别来说,一个月的服务通常并不划算——而且家庭计划通常是保护家庭最便宜的方式。 最终排名: Incogni — 全自动删除排名第一,经德勤审计,透明度高,且高级会员入门价格最低。最适合大多数希望无需人工干预即可清理数字足迹的用户。 DeleteMe — 高级/精英之选第 2 名。选择它可进行人工验证移除、复杂曝光、自定义移除以及使用捆绑的遮罩工具包。 Optery——最佳的移除证明和预算等级,并提供清晰的暴露报告。 Privacy Bee——目前已发布的针对隐秘网站上个人数据的最广泛的经纪商覆盖范围。 Aura——最佳一体化网络安全套餐,尤其适合系列计划。 EasyOptOuts——最佳低成本、一劳永逸的选择。 Onerep——最佳的简洁独立组网 (SA)删除引擎。 Kanary——最适合人肉搜索和社交媒体曝光。 IDX Complete — 最佳全功能身份盗窃防护套件,具备信用监控和密码管理功能。 ReputationDefender——最适合高知名度人士和需要管理声誉的人士。 结论是:没有任何服务可以 100% 删除你的痕迹,任何承诺可以做到这一点的排名都是在推销,而不是在测试。前三名之间的区别不在于登录页面上的经纪人数量,而在于当数据经纪人重新发布信息时,服务是否会重新提交,以及当自动化失败时是否有人可以介入。Incogni凭借每美元的自动化耐用性胜出。DeleteMe 在人性层面胜出。根据您面临的风险复杂程度选择合适的服务,并为持续保护而非一次性清理做好预算。最好的数据清除服务是在首次曝光报告之后仍然有效——因为你的数字足迹、你的个人数据以及托管这些数据的数据经纪网站都会不断变化。将数据删除功能与身份保护、密码管理器和信用监控相结合,并将数据删除功能视为更广泛的数字网络安全策略中的一层,而不是一次性解决方案。
View full article