2313620_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2313620_en-US

2313620_en-US

NXP Security - Summary Page (Japanese blog)

NXP Security Overview and the Purpose of This Page

 
In recent years, with the spread of IoT devices and edge equipment, security requirements have become increasingly sophisticated and complex. NXP provides comprehensive security solutions including processors, secure elements, software/tools, and related documentation, creating an environment in which developers can build secure systems from the design stage .
This summary page brings together all of NXP's security-related information in one place , organized for quick access to the information you need. The articles cover a wide range of topics, from basic knowledge of NXP devices to hands-on implementation exercises, making it ideal for anyone planning to use NXP products to design secure systems.


Tech Blog Article List (Links and Summary)


◆Introduction and Case Studies◆


point article overview
JC-STAR Overview and NXP Products

The launch of the Japan Security Requirements Conformity Assessment and Labeling System (JC-STAR) in... and NXP products that support security functions (Japanese blog)

This article provides an overview of the security requirements discussed in JC-STAR. It systematically explains how NXP products meet the requirements. It is an introductory article to help you understand the overall picture of security design.
Use Case Example

Security use cases for embedded products that can improve product and corporate value (Japanese blog...

The importance of security in embedded products is explained in an easy-to-understand and concise manner from the perspectives of threats, impacts, and countermeasures, using use cases as examples.
The Benefits of Hardware Security

NXP's hardware security solutions simplify security implementation and reduce man-hours (Japanese bl...

What are the benefits of using NXP's hardware security (MCU/MPU with built-in cryptographic accelerator, MCU/MPU with built-in EdgeLock ® Secure Enclave, Secure Element/Authenticator, EdgeLock 2GO: Secure Provisioning Service)? We also explain the features of each.

The benefits of choosing products with NXP security features (Japanese blog)



◆Theme-specific/Practical Corner◆ "Implementation of Important Security Technologies"


Secure Boot


theme classification article
Secure Boot
(i.MX)


Commentary

i.MX 93 Processor: Explaining Secure Boot Signing and Authentication

A detailed explanation of the i.MX 93 secure boot structure. The signing and verification process is explained with diagrams.

Practice

i.MX 93 Processor: How to Implement Secure Boot - Practical Guide (Japanese blog)

Based on the above explanation of "i.MX93 signing and authentication mechanisms," this section explains the actual hands-on procedure. It's practical content that developers can understand by actually running the code.


Explanation and Practice

Secure Boot with i.MX 95 SPSDK (Japanese Blog)

This guide provides a hands-on explanation of secure boot using i.MX 95 and how to implement it. It's practical and allows developers to understand the concepts by actually running the code.

Secure Boot
(i.MX RT)

Explanation and Practice

Getting Started with Zephyr ® and Secure Boot using MCUboot on NXP ® MIMXRT1060-EVKC (IT Access Co., Ltd.)

This guide uses NXP's high-performance microcontroller evaluation board "MIMXRT1060-EVKC" as an example to demonstrate practical development procedures combining Zephyr and the secure bootloader "MCUboot." Through the entire process, from building and programming to firmware updates using actual hardware, you can gain a concrete understanding of secure embedded system development using Zephyr.



Secure element


theme classification article
Preparing to use the secure element

Explanation
&
Practice

How to use Secure Element SE05x: Setting up Plug and Trust Middleware on Raspberry Pi (Japanese blog...

How to use Secure Element SE05x: Setting up Plug and Trust Middleware on the FRDM-IMX93 development ...

NXP's Secure Element SE05x comes with middleware called Plug and Trust Middleware. In addition to a dedicated API for using the SE05x, it also includes plugins for widely used libraries such as OpenSSL and mbed-TLS. This document describes the procedure for setting up Plug and Trust Middleware for Raspberry Pi and FRDM-IMX93 (a development board for i.MX 93).

OpenSSL Practice

How to use SecureElement SE05x: Using SE050 via OpenSSL (Japanese blog)

This article explains practical ways to use Secure Element (SE05x) in conjunction with OpenSSL.

Connecting to Azure IoT Hub Practice

How to use Secure Element SE05x: Connecting to Azure IoT Hub using Eclipse Mosquitto client (Japanes...

This guide explains how to connect to Azure IoT Hub using the Eclipse Mosquitto client.


 

key management


theme classification article
Key management using the security engine within the SoC

Explanation
&
Practice

How to use the EdgeLock® Secure Enclave (ELE) on i.MX 93: Storing and using encryption keys via PKCS...

This document explains how to use the cryptographic accelerator and key management functions of the i.MX 93's built-in EdgeLock® Secure Enclave (ELE) via PKCS#11.



Secure Provisioning Tool ~ A tool for using security features for NXP MCUs ~


Keita_Nagashima_0-1782703328411.pngKeita_Nagashima_0-1782703328411.png

The Secure Provisioning Tool is an MCU-specific tool for performing tasks such as securing and writing images for product releases of applications developed and evaluated using MCUXpresso for VSC or MCUXpresso IDE. It enables secure boot, secure updates, debug authentication, device recognition, and more.


theme classification article
Secure Provisioning Tool

Explanation
Practice

How to install and use the Secure Provisioning Tool (Macnica, Inc.)

Introduction to the useful features of the Secure Provisioning Tool (Macnica, Inc.)

This guide provides a clear explanation of how to use a tool called the Secure Provisioning Tool (hereinafter abbreviated as SPT).



◆Basic skills and learning corner◆


category article overview
Glossary

Explaining Common Semiconductor Hardware Security Features (Secure Element, Secure Enclave, TPM, HSM...

This article introduces the functional roles, classifications, and overviews of secure elements, secure enclaves, TPMs, HSMs, TEEs, TrustZones, etc.


Finally


NXP's security-enabled products are flexible and scalable to meet the requirements of a wide variety of use cases. We hope that by using this summary page, you will be able to quickly access the information you need and smoothly proceed from product selection to implementation. New articles will be added from time to time, so please check back for the latest information.



If you have any requests or suggestions for improvements regarding security-related content, please feel free to contact us using the information below.

NXP Japan Technical Blog (Japanese) Content Request/Improvement Survey – Fill out the form

============================

When making inquiries, please also use the " Technical Questions to NXP -
How to Contact Us( Japanese Blog) "(If you are already an NXP distributor or have a relationship with NXP, you may ask the person in charge directly.)

In recent years, with the spread of IoT devices and edge equipment, security requirements have become increasingly sophisticated and complex. NXP provides comprehensive security solutions including processors, secure elements, software/tools, and related documentation, creating an environment in which developers can build secure systems from the design stage .
This summary page brings together all of NXP's security-related information in one place , organized for quick access to the information you need. The articles cover a wide range of topics, from basic knowledge of NXP devices to hands-on implementation exercises, making it ideal for anyone planning to use NXP products to design secure systems.
SecurityTechnology FocusJapanese Blog
タグ(1)
評価なし
バージョン履歴
最終更新日:
2 週間前
更新者: