# README This is a mcan sdk demo on MPC5777C. Transmit data in turn and received data. CANFD is not used and extended id is used. Both Tx and Rx use interrupt. All documents are in [mpc5777c_test_mcan/mpc5777c_test_mcan_Z7_0/Documentation] folder. ## Board MPC5777C-416DS + MPC57xx MOTHERBOARD (SCH-27237 REV C) ## CAN PC Client PCAN-View ## Compiler powerpc-eabivle-gcc with S32 Design Studio for Power Architecture IDE ## MCAN MCAN0 ## Pin PC[19] - MCAN0 Tx PC[20] - MCAN0 Rx ## SDK S32_SDK_S32PA_EAR_1.8.0 ## Caution 1. Error to send data bytes which are not multiple times of 4 with MCAN_StartSendData() in mcan_driver.c. So MCAN_StartSendData() must be modified. Modified position is 606 to 607 lines in mcan_driver.c. 2. MCAN_DRV_InstallEventCallback() hasn't been implemented yet, must be added. ## Revision History Release 1.0.0 - 2018/12/19 - Jacob Peng -
[email protected] * Mod: MCAN_StartSendData() in mcan_driver.c * Add: MCAN_DRV_InstallEventCallback() in mcan_driver.c * Add: Demo application