MPC5xxx知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5xxx Knowledge Base

标签

讨论

排序依据:
******************************************************************************** * Detailed Description: * Purpose of the example is to show how to generate Multi-bit or Single-bit * ECC error in internal FLASH (user must choose it in the option at the end of * main function). * Flash over-programming is used to generate a non-correctable (or single-bit) * ECC error in FLASH. The bad data is accessed then, so the IVOR1 exception (or * ERM combined interrupt service routine) is generated and handled. * Example also offers useful macros for EIM and ERM modules. * The example displays notices in the terminal window (USBtoUART bridge J21) * (19200-8-no parity-1 stop bit-no flow control on eSCI_A). * No other external connection is required. * * ------------------------------------------------------------------------------ * Test HW:         MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C * MCU:             PPC5777CMM03 2N45H CTZZS1521A * Fsys:            PLL1 = core_clk = 264MHz, PLL0 = 192MHz * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection:  eSCI_A is USBtoUART bridge (connector J21) * ********************************************************************************
查看全文
Detailed Description:                      This config tool simplifies DCF records calculation for MPC5744P device.                 Look at HowToUse sheet for simple guideline, then work with DCF sheet                 Notes: - Macros have to be enabled!         BR, Petr
查看全文
******************************************************************************** * Detailed Description: * Purpose of the example is to show how to simulate Multi-bit or Single-bit ECC * error in internal DMA TCD RAM (user must choose it in the option at the end of * main function). * EIM (Error Injection Module) is used to simulate a multi-bit or single-bit * ECC error in DMA TCD RAM (Peripheral RAM). * When corrupted data is accessed the IVOR1 exception handler is called in case * of multi-bit ECC error (IVOR1 exception occurs) and FCCU_Alarm_Interrupt * handler is called in case of single-bit ECC error (FCCU interrupt occurs). * Both function calls MEMU handler. * The example displays notices in the terminal window (connector J19 on * MPC57xx_Motherboard)(19200-8-no parity-1 stop bit-no flow control on eSCI_A). * No other external connection is required. * ------------------------------------------------------------------------------ * Test HW:         MPC57xx_Motherboard + MPC5744P-144DC * MCU:             PPC5744PFMLQ8,0N15P,QQAA1515N, Rev2.1B * Fsys:            200 MHz PLL with 40 MHz crystal reference * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH, RAM * Terminal:        19200-8-no parity-1 stop bit-no flow control * EVB connection:  default ********************************************************************************
查看全文
******************************************************************************** * Detailed Description: * This example shows, how to use interrupt hardware vector mode. In the example * PIT0 interrupt and external interrupt source 1 are implemented. PIT interrupt * toggle LED every second, external interrupt causes IVOR1 exception. * * This example also shows, how to use exceptions, while HW vector mode is used. * After SW1 button is pressed, uninitialized RAM is read and IVOR1 exception is * reached. In IVOR1, only endless loop is implemented and micro has to be reset * externally if you want to get out from this loop. * * * For correct HW vector mode setup, following files was added to the project: * *  - exceptions.s *  - handlers_vle.s *  - HW_vector.c * * * Following files was modified (all changes are marked by comment): * *  - mem.ld *  - sections.ld *  - Vector.c *  - MPC57xx__Interrupt_Init.c * * *  Following files was removed from project (files are still place in project, but *  not compiled and linked) * *  - intc_sw_handlers.S *  - intc_SW_mode_isr_vectors_MPC5744P.c * * * * Test HW:         X-MPC5744P-144DC, MPC57xx motherboard * MCU:             PPC5744PFMLQ8 0N15P * Fsys:            200 MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          internal_FLASH (debug mode, release mode) * EVB connection:  User LED 1 connected to A0 (P8.0), *                    User switch SW1 connected to A1 (P8.1) * * * ------------------------------------------------------------------------------ * ********************************************************************************
查看全文
******************************************************************************** * Detailed Description: * Application performs basic initialization then it initializes EBI for external * SRAM connected to MPC5777C-516DS and test it by write and read of block of * data. * * ------------------------------------------------------------------------------ * Test HW:         MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C * MCU:             PPC5777CMM03 3N45H * Fsys:            PLL1 = core_clk = 264MHz, PLL0 = 192MHz * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection:  jumper J4 on position 1-2 (choosing CS0) * ********************************************************************************
查看全文
******************************************************************************** * Detailed Description: * Enable external interrupt on pin PA[3]. * If falling edge is detected, interrupt is triggered and LED1 on PE[4] is * toggled. * * Connect external signal to PA[3] or connect push button by wire. * * ------------------------------------------------------------------------------ * Test HW:  TRK-MPC5606B, SPC5606B 0N32E * Target :  internal_FLASH, RAM * Fsys:     64 MHz PLL with 8 MHz crystal reference * ********************************************************************************
查看全文
This config tool simplifies PLL setting calculation and clock configuration for MPC5777C device. Version 1.3 added option to select between 264/300 MHz MCU versions.                 Follow these steps                 Note: Macros have to be enabled!                 1. Enter frequency of used XOSC and desired PLL0 and PLL1 output.      - put values into cells B14, Q13 and Q20 of the "Clocks" sheet      - check if it is Valid or Invalid      - "PLLconfig" sheet shows possible PLLs configurations                   2. Configure System and AUX clock selectors and its Dividers      - check calculated frequency of System/Peripheral clocks      - if Invalid change source clock and Divider value to keep Max freq                 3. Copy generated code by pressing "Copy Code" button
查看全文
******************************************************************************** * Detailed Description: * * Purpose of the example is to show how to intentionally generate FCCU fault * causing reset either directly or by FOSU (simulating by non-handled FCCU * fault). Example configures FCCU, then an error is injected with using of * Noncritical Fault Fake register and after re-booting reset cause is evaluated. * The example displays notices in the terminal window (connector J19 on * MPC57xx_Motherboard)(19200-8-no parity-1 stop bit-no flow control on eSCI_A). * No other external connection is required. * * ------------------------------------------------------------------------------ * Test HW:         MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C * MCU:             PPC5777CMM03 2N45H CTZZS1521A * Fsys:            PLL1 = core_clk = 264MHz, PLL0 = 192MHz * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection:  eSCI_A is USBtoUART bridge (connector J21) * ********************************************************************************
查看全文
******************************************************************************** * Detailed Description: * This example demonstrates frequency modulation at 20kHz with 250 steps. * System frequency which is modulated is 40MHz. * ------------------------------------------------------------------------------ * Test HW:   MPC57xx EVB + MPC5748G minimodule * Maskset:   1N81M * Target :     SRAM * Fsys:        40 MHz PLL * ******************************************************************************** Revision History: 1.0     Oct-29-2014     b21190(Vlna Peter)  Initial Version 1.1    Nov-20-2014    b21190(Vlna Peter)  Modified for Cut2.0 1.2    Nov-20-2014    b21190(Vlna Peter)  Added SWT_0 dissabling in startup 1.3    Mar-10-2016    b21190(Vlna Peter)  Fixed clock configuraion for PLL 1.4    Jun-30-2017    b21190(Vlna Peter)  Added 20kHz frequency modulation *******************************************************************************/ Measure modulated system Frequency at PG[7] - SYSCLK0 pin.
查看全文
******************************************************************************** * Detailed Description: * Example of core watchdog implementation on Cobra 55. It executes on core 0 * All the functions are in the file "watchdog.c" *WatchDogCreate(delay, FirstTimeout, SecondTimeout) -> create/configure the wathdog timer *WatchDogStart() -> start the watchdog timer *WatchDogService() -> acknowledge the watchdog timer * ------------------------------------------------------------------------------ * Test HW:         MPC5777C-416DS Rev.A + MPC57xx MOTHER BOARD Rev.C * MCU:             PPC5777CMM03 2N45H CTZZS1521A * Fsys:            PLL1 = core_clk = 264MHz, PLL0 = 192MHz * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * ********************************************************************************
查看全文
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * initializes interrupts, blinking one LED by interrupt, second LED by software * loop (by second core), initializes and display notice via UART terminal and * then terminal ECHO. * The example configures the device for maximum performance (OPTIMIZATIONS_ON). * For XPC567XKIT516 it initializes EBI for mounted external SRAM device. * * ------------------------------------------------------------------------------ * Test HW:         XPC567XKIT516 - MPC567xADAT516 Rev.D, MPC567XEVBFXMB Rev.C * MCU:             PPC5676RDMVY1 3N23A * Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A * Fsys:            180MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          RAM, internal_FLASH * EVB connection:  ETPUC0(J24-0) -> USER_LED_8 (J5-8) *                  ETPUC1(J24-1) -> USER_LED_7 (J5-7)(to see blinking LEDs) * ********************************************************************************
查看全文
******************************************************************************** * Detailed Description: * Purpose of the example is to show how to generate Multi bit ECC error in * internal SRAM or FLASH (user can choose it in the option at the end of main * function) and how to handle this error with respect to constraints given by * MPC5675K architecture (ECSM/RGM/FCCU relation and ECC error handling through * reset). The example is only possible to run in internal_FLASH target. Power- * -on-reset is required after downloading the code into MCU's flash. The example * displays notices in the terminal window (setting specified below). No other * external connection is required. * Example also shows impact of enabled cache (macro OPTIMIZATIONS_ON). * * ------------------------------------------------------------------------------ * Test HW:        MPC5675KEVB * MCU:            PPC5675KFMMSJ in Lock-Step mode * Fsys:           180/150 MHz CORE_CLK * Debugger:       Lauterbach Trace32 *                 PeMicro USB-ML-PPCNEXUS * Target:         RAM, internal_FLASH * Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection: default * ********************************************************************************
查看全文
This excel tool helps to configure MMU on e200z cores. It generates asm code and also command for Lauterbach debugger for selected configuration of TLB entry.
查看全文
******************************************************************************** * Detailed Description: * * * This example demonstrate functionality of XBIC_1 error injection *  capability. The fault is generated on DMA transfer to SRAM. *  After fault generation it is propagated to FCCU unit as NCF[59]. * * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N65H * Target :  internal_FLASH * Fsys:     200 MHz PLL with 40 MHz crystal reference * ********************************************************************************
查看全文
******************************************************************************** * Detailed Description: * * This example shows possible implementation of frequency and duty cycle * measurement with the help of eMIOS module. * Two eMIOS channels are used and set to IPWM and IPM modes. The first channel * measures the positive pulse width and the second channel measures the period. * * EVB connection: * PJ7.5 to PJ7.6 ... connect external pulse signal to this * * See result on PC terminal (9600, 8N1) * ------------------------------------------------------------------------------ * Test HW:  XPC56xxMB2 + XPC564xB/C, SPC5646C 0N32E silicon * Target :  internal_FLASH, RAM * Fsys:     120 MHz PLL0 * Debugger: Lauterbach Trace32. script for internal_FALSH run_from_flash.cmm *                               script for RAM: run_from_ram_vle.cmm * ********************************************************************************     BR, Petr
查看全文
******************************************************************************** * Detailed Description: * A simple example configures eTPU engine B channels 0/1 for GPO/GPI. It is * needed to connect these pins by wire. Output wave is generated by eTPU GPIO * output function and inputs are read by fs_etpu_gpio_input_immed function * latching just current pin state. Pin history is displayed in ISR. * * Note: It is needed to configure IGF module, otherwise inputs does not pass * to eTPU module. * * ------------------------------------------------------------------------------ * Test HW:         MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C * MCU:             PPC5777CMM03 2N45H CTZZS1521A * Fsys:            PLL1 = core_clk = 264MHz, PLL0 = 192MHz * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection:  ETPUB0 (PortR P25-1) --> ETPUB1 (PortR P25-0) by wire * ********************************************************************************
查看全文
******************************************************************************** * Detailed Description: * * Application performs basic initialization, setup PLLs. * DSPI_A is configured as master using DMA to send/receive 8 words. * * Two DMA descriptors are initialized: * - TCD[32] master transmit * - TCD[33] master receive * * * EVB connection: * * Do external loopback to connect SOUT to SIN * * PM6 ... SCKA * PM7 ... SINA * PM8 ... SOUTA * PM13... PCSA0 ** * ------------------------------------------------------------------------------ * Test HW: MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C * MCU: PPC5777CMM03 3N45H * Fsys: PLL1 = core_clk = 260MHz, PLL0 = 200MHz * Debugger: Lauterbach Trace32 * Target: internal_FLASH * *********************************************************************************
查看全文
******************************************************************************** * Detailed Description: * This SW provides the example of clearing of FCCU faults. * * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N65H * Target :  internal_FLASH * Fsys:     200 MHz PLL with 40 MHz crystal reference + FCCU fault clearing example code. * ******************************************************************************** Revision History: 1.0     Jan-05-2016     nxa13250(Vlna Peter)  Initial Version *******************************************************************************/
查看全文
******************************************************************************** * Detailed Description:   * Example shows MCU's temperature measurement with the help of TSENS. * Calibration constants for TSENS are read from TSENS registers and * eQADC is set to measure Vbg and TSENS outputs. eQADC calibration is also done. * Calculated internal temperature can be displayed on the Terminal. * * See results on PC terminal (19200, 8N1, None). You should see following text * (with different values for sure) * *    fsys = 150MHz * *    TSENS temperature calculation * *    Calibration constants read from TSENS registers * *    T_LOW = 25 *    T_HIGH = 145 *    TSENS_CODE_T_LOW = 5441 *    TSENS_CODE_T_HIGH = 7305 *    VBG_CODE_T_LOW = 4010 * * *                 (TSENS_CODE_T*beta - TSENS_CODE_T_LOW)*(T_HIGH - T_LOW) *    T = T_LOW - --------------------------------------------------------- [degC] *                       (TSENS_CODE_T_HIGH - TSENS_CODE_T_LOW) * * *    VBG_CODE_T (ch45)  = 3959 => beta = 1.01288 *    TSENS_CODE_T (ch128) = 5608 * *    Temp = 31.80 degC *    * ------------------------------------------------------------------------------ * Test HW:        XPC564AKIT208S and XPC564AKIT324S * MCU:            SPC5644AMMG1,0M14X and SPC5644AMVZ1,0M14X * Fsys:           150/132/120/12 MHz * Debugger:       Lauterbach Trace32 *                 PeMicro USB-ML-PPCNEXUS * Target:         RAM, internal_FLASH * Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection: default * ********************************************************************************
查看全文
******************************************************************************** * Detailed Description: * DRUN with PLL 160MHz active. * Example of INTC configuration. PIT timer is triggering an * interrupt which is served in PIT ISR. * * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N06M * Target :  Internal Flash * Fsys:     160 MHz PLL * ******************************************************************************** Revision History: 1.0     Oct-29-2014     b21190(Vlna Peter)  Initial Version 1.1    Nov-20-2014    b21190(Vlna Peter)  Modified for Cut2.0 1.2    Apr-23-2015    b21190(Vlna Peter)  Added INTC driver and PIT ISR 1.3    May-14-2015    b21190(Vlna Peter)  Dissabling SWT in Startup code 1.4     Jun-06-2017    b21190(Vlna Peter)  ported for MPC5746C *******************************************************************************/
查看全文